//===-- StatepointDefaultGC.cpp - The default statepoint GC strategy ------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file contains a GCStrategy which serves as an example for the usage // of a statepoint based lowering strategy. This GCStrategy is intended to // suitable as a default implementation usable with any collector which can // consume the standard stackmap format generated by statepoints, uses the // default addrespace to distinguish between gc managed and non-gc managed // pointers, and has reasonable relocation semantics. // //===----------------------------------------------------------------------===// #include "llvm/CodeGen/GCStrategy.h" #include "llvm/IR/Value.h" #include "llvm/IR/DerivedTypes.h" using namespace llvm; namespace { class StatepointGC : public GCStrategy { public: StatepointGC() { UseStatepoints = true; // These options are all gc.root specific, we specify them so that the // gc.root lowering code doesn't run. InitRoots = false; NeededSafePoints = 0; UsesMetadata = false; CustomRoots = false; CustomSafePoints = false; } Optional isGCManagedPointer(const Value *V) const override { // Method is only valid on pointer typed values. PointerType *PT = cast(V->getType()); // For the sake of this example GC, we arbitrarily pick addrspace(1) as our // GC managed heap. We know that a pointer into this heap needs to be // updated and that no other pointer does. return (1 == PT->getAddressSpace()); } }; } static GCRegistry::Add X("statepoint-example", "an example strategy for statepoint"); namespace llvm { void linkStatepointExampleGC() {} }