//===-- AutoUpgrade.cpp - Implement auto-upgrade helper functions ---------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the auto-upgrade helper functions // //===----------------------------------------------------------------------===// #include "llvm/AutoUpgrade.h" #include "llvm/DebugInfo.h" #include "llvm/IR/Constants.h" #include "llvm/IR/Function.h" #include "llvm/IR/IRBuilder.h" #include "llvm/IR/Instruction.h" #include "llvm/IR/IntrinsicInst.h" #include "llvm/IR/LLVMContext.h" #include "llvm/IR/Module.h" #include "llvm/Support/CFG.h" #include "llvm/Support/CallSite.h" #include "llvm/Support/ErrorHandling.h" #include using namespace llvm; // Upgrade the declarations of the SSE4.1 functions whose arguments have // changed their type from v4f32 to v2i64. static bool UpgradeSSE41Function(Function* F, Intrinsic::ID IID, Function *&NewFn) { // Check whether this is an old version of the function, which received // v4f32 arguments. Type *Arg0Type = F->getFunctionType()->getParamType(0); if (Arg0Type != VectorType::get(Type::getFloatTy(F->getContext()), 4)) return false; // Yes, it's old, replace it with new version. F->setName(F->getName() + ".old"); NewFn = Intrinsic::getDeclaration(F->getParent(), IID); return true; } static bool UpgradeIntrinsicFunction1(Function *F, Function *&NewFn) { assert(F && "Illegal to upgrade a non-existent Function."); // Quickly eliminate it, if it's not a candidate. StringRef Name = F->getName(); if (Name.size() <= 8 || !Name.startswith("llvm.")) return false; Name = Name.substr(5); // Strip off "llvm." switch (Name[0]) { default: break; case 'a': { if (Name.startswith("arm.neon.vclz")) { Type* args[2] = { F->arg_begin()->getType(), Type::getInt1Ty(F->getContext()) }; // Can't use Intrinsic::getDeclaration here as it adds a ".i1" to // the end of the name. Change name from llvm.arm.neon.vclz.* to // llvm.ctlz.* FunctionType* fType = FunctionType::get(F->getReturnType(), args, false); NewFn = Function::Create(fType, F->getLinkage(), "llvm.ctlz." + Name.substr(14), F->getParent()); return true; } if (Name.startswith("arm.neon.vcnt")) { NewFn = Intrinsic::getDeclaration(F->getParent(), Intrinsic::ctpop, F->arg_begin()->getType()); return true; } break; } case 'c': { if (Name.startswith("ctlz.") && F->arg_size() == 1) { F->setName(Name + ".old"); NewFn = Intrinsic::getDeclaration(F->getParent(), Intrinsic::ctlz, F->arg_begin()->getType()); return true; } if (Name.startswith("cttz.") && F->arg_size() == 1) { F->setName(Name + ".old"); NewFn = Intrinsic::getDeclaration(F->getParent(), Intrinsic::cttz, F->arg_begin()->getType()); return true; } break; } case 'o': // We only need to change the name to match the mangling including the // address space. if (F->arg_size() == 2 && Name.startswith("objectsize.")) { Type *Tys[2] = { F->getReturnType(), F->arg_begin()->getType() }; if (F->getName() != Intrinsic::getName(Intrinsic::objectsize, Tys)) { F->setName(Name + ".old"); NewFn = Intrinsic::getDeclaration(F->getParent(), Intrinsic::objectsize, Tys); return true; } } break; case 'x': { if (Name.startswith("x86.sse2.pcmpeq.") || Name.startswith("x86.sse2.pcmpgt.") || Name.startswith("x86.avx2.pcmpeq.") || Name.startswith("x86.avx2.pcmpgt.") || Name.startswith("x86.avx.vpermil.") || Name == "x86.avx.movnt.dq.256" || Name == "x86.avx.movnt.pd.256" || Name == "x86.avx.movnt.ps.256" || Name == "x86.sse42.crc32.64.8" || (Name.startswith("x86.xop.vpcom") && F->arg_size() == 2)) { NewFn = 0; return true; } // SSE4.1 ptest functions may have an old signature. if (Name.startswith("x86.sse41.ptest")) { if (Name == "x86.sse41.ptestc") return UpgradeSSE41Function(F, Intrinsic::x86_sse41_ptestc, NewFn); if (Name == "x86.sse41.ptestz") return UpgradeSSE41Function(F, Intrinsic::x86_sse41_ptestz, NewFn); if (Name == "x86.sse41.ptestnzc") return UpgradeSSE41Function(F, Intrinsic::x86_sse41_ptestnzc, NewFn); } // frcz.ss/sd may need to have an argument dropped if (Name.startswith("x86.xop.vfrcz.ss") && F->arg_size() == 2) { F->setName(Name + ".old"); NewFn = Intrinsic::getDeclaration(F->getParent(), Intrinsic::x86_xop_vfrcz_ss); return true; } if (Name.startswith("x86.xop.vfrcz.sd") && F->arg_size() == 2) { F->setName(Name + ".old"); NewFn = Intrinsic::getDeclaration(F->getParent(), Intrinsic::x86_xop_vfrcz_sd); return true; } // Fix the FMA4 intrinsics to remove the 4 if (Name.startswith("x86.fma4.")) { F->setName("llvm.x86.fma" + Name.substr(8)); NewFn = F; return true; } break; } } // This may not belong here. This function is effectively being overloaded // to both detect an intrinsic which needs upgrading, and to provide the // upgraded form of the intrinsic. We should perhaps have two separate // functions for this. return false; } bool llvm::UpgradeIntrinsicFunction(Function *F, Function *&NewFn) { NewFn = 0; bool Upgraded = UpgradeIntrinsicFunction1(F, NewFn); // Upgrade intrinsic attributes. This does not change the function. if (NewFn) F = NewFn; if (unsigned id = F->getIntrinsicID()) F->setAttributes(Intrinsic::getAttributes(F->getContext(), (Intrinsic::ID)id)); return Upgraded; } bool llvm::UpgradeGlobalVariable(GlobalVariable *GV) { // Nothing to do yet. return false; } // UpgradeIntrinsicCall - Upgrade a call to an old intrinsic to be a call the // upgraded intrinsic. All argument and return casting must be provided in // order to seamlessly integrate with existing context. void llvm::UpgradeIntrinsicCall(CallInst *CI, Function *NewFn) { Function *F = CI->getCalledFunction(); LLVMContext &C = CI->getContext(); IRBuilder<> Builder(C); Builder.SetInsertPoint(CI->getParent(), CI); assert(F && "Intrinsic call is not direct?"); if (!NewFn) { // Get the Function's name. StringRef Name = F->getName(); Value *Rep; // Upgrade packed integer vector compares intrinsics to compare instructions if (Name.startswith("llvm.x86.sse2.pcmpeq.") || Name.startswith("llvm.x86.avx2.pcmpeq.")) { Rep = Builder.CreateICmpEQ(CI->getArgOperand(0), CI->getArgOperand(1), "pcmpeq"); // need to sign extend since icmp returns vector of i1 Rep = Builder.CreateSExt(Rep, CI->getType(), ""); } else if (Name.startswith("llvm.x86.sse2.pcmpgt.") || Name.startswith("llvm.x86.avx2.pcmpgt.")) { Rep = Builder.CreateICmpSGT(CI->getArgOperand(0), CI->getArgOperand(1), "pcmpgt"); // need to sign extend since icmp returns vector of i1 Rep = Builder.CreateSExt(Rep, CI->getType(), ""); } else if (Name == "llvm.x86.avx.movnt.dq.256" || Name == "llvm.x86.avx.movnt.ps.256" || Name == "llvm.x86.avx.movnt.pd.256") { IRBuilder<> Builder(C); Builder.SetInsertPoint(CI->getParent(), CI); Module *M = F->getParent(); SmallVector Elts; Elts.push_back(ConstantInt::get(Type::getInt32Ty(C), 1)); MDNode *Node = MDNode::get(C, Elts); Value *Arg0 = CI->getArgOperand(0); Value *Arg1 = CI->getArgOperand(1); // Convert the type of the pointer to a pointer to the stored type. Value *BC = Builder.CreateBitCast(Arg0, PointerType::getUnqual(Arg1->getType()), "cast"); StoreInst *SI = Builder.CreateStore(Arg1, BC); SI->setMetadata(M->getMDKindID("nontemporal"), Node); SI->setAlignment(16); // Remove intrinsic. CI->eraseFromParent(); return; } else if (Name.startswith("llvm.x86.xop.vpcom")) { Intrinsic::ID intID; if (Name.endswith("ub")) intID = Intrinsic::x86_xop_vpcomub; else if (Name.endswith("uw")) intID = Intrinsic::x86_xop_vpcomuw; else if (Name.endswith("ud")) intID = Intrinsic::x86_xop_vpcomud; else if (Name.endswith("uq")) intID = Intrinsic::x86_xop_vpcomuq; else if (Name.endswith("b")) intID = Intrinsic::x86_xop_vpcomb; else if (Name.endswith("w")) intID = Intrinsic::x86_xop_vpcomw; else if (Name.endswith("d")) intID = Intrinsic::x86_xop_vpcomd; else if (Name.endswith("q")) intID = Intrinsic::x86_xop_vpcomq; else llvm_unreachable("Unknown suffix"); Name = Name.substr(18); // strip off "llvm.x86.xop.vpcom" unsigned Imm; if (Name.startswith("lt")) Imm = 0; else if (Name.startswith("le")) Imm = 1; else if (Name.startswith("gt")) Imm = 2; else if (Name.startswith("ge")) Imm = 3; else if (Name.startswith("eq")) Imm = 4; else if (Name.startswith("ne")) Imm = 5; else if (Name.startswith("true")) Imm = 6; else if (Name.startswith("false")) Imm = 7; else llvm_unreachable("Unknown condition"); Function *VPCOM = Intrinsic::getDeclaration(F->getParent(), intID); Rep = Builder.CreateCall3(VPCOM, CI->getArgOperand(0), CI->getArgOperand(1), Builder.getInt8(Imm)); } else if (Name == "llvm.x86.sse42.crc32.64.8") { Function *CRC32 = Intrinsic::getDeclaration(F->getParent(), Intrinsic::x86_sse42_crc32_32_8); Value *Trunc0 = Builder.CreateTrunc(CI->getArgOperand(0), Type::getInt32Ty(C)); Rep = Builder.CreateCall2(CRC32, Trunc0, CI->getArgOperand(1)); Rep = Builder.CreateZExt(Rep, CI->getType(), ""); } else { bool PD128 = false, PD256 = false, PS128 = false, PS256 = false; if (Name == "llvm.x86.avx.vpermil.pd.256") PD256 = true; else if (Name == "llvm.x86.avx.vpermil.pd") PD128 = true; else if (Name == "llvm.x86.avx.vpermil.ps.256") PS256 = true; else if (Name == "llvm.x86.avx.vpermil.ps") PS128 = true; if (PD256 || PD128 || PS256 || PS128) { Value *Op0 = CI->getArgOperand(0); unsigned Imm = cast(CI->getArgOperand(1))->getZExtValue(); SmallVector Idxs; if (PD128) for (unsigned i = 0; i != 2; ++i) Idxs.push_back(Builder.getInt32((Imm >> i) & 0x1)); else if (PD256) for (unsigned l = 0; l != 4; l+=2) for (unsigned i = 0; i != 2; ++i) Idxs.push_back(Builder.getInt32(((Imm >> (l+i)) & 0x1) + l)); else if (PS128) for (unsigned i = 0; i != 4; ++i) Idxs.push_back(Builder.getInt32((Imm >> (2 * i)) & 0x3)); else if (PS256) for (unsigned l = 0; l != 8; l+=4) for (unsigned i = 0; i != 4; ++i) Idxs.push_back(Builder.getInt32(((Imm >> (2 * i)) & 0x3) + l)); else llvm_unreachable("Unexpected function"); Rep = Builder.CreateShuffleVector(Op0, Op0, ConstantVector::get(Idxs)); } else { llvm_unreachable("Unknown function for CallInst upgrade."); } } CI->replaceAllUsesWith(Rep); CI->eraseFromParent(); return; } std::string Name = CI->getName().str(); CI->setName(Name + ".old"); switch (NewFn->getIntrinsicID()) { default: llvm_unreachable("Unknown function for CallInst upgrade."); case Intrinsic::ctlz: case Intrinsic::cttz: assert(CI->getNumArgOperands() == 1 && "Mismatch between function args and call args"); CI->replaceAllUsesWith(Builder.CreateCall2(NewFn, CI->getArgOperand(0), Builder.getFalse(), Name)); CI->eraseFromParent(); return; case Intrinsic::objectsize: CI->replaceAllUsesWith(Builder.CreateCall2(NewFn, CI->getArgOperand(0), CI->getArgOperand(1), Name)); CI->eraseFromParent(); return; case Intrinsic::arm_neon_vclz: { // Change name from llvm.arm.neon.vclz.* to llvm.ctlz.* CI->replaceAllUsesWith(Builder.CreateCall2(NewFn, CI->getArgOperand(0), Builder.getFalse(), "llvm.ctlz." + Name.substr(14))); CI->eraseFromParent(); return; } case Intrinsic::ctpop: { CI->replaceAllUsesWith(Builder.CreateCall(NewFn, CI->getArgOperand(0))); CI->eraseFromParent(); return; } case Intrinsic::x86_xop_vfrcz_ss: case Intrinsic::x86_xop_vfrcz_sd: CI->replaceAllUsesWith(Builder.CreateCall(NewFn, CI->getArgOperand(1), Name)); CI->eraseFromParent(); return; case Intrinsic::x86_sse41_ptestc: case Intrinsic::x86_sse41_ptestz: case Intrinsic::x86_sse41_ptestnzc: { // The arguments for these intrinsics used to be v4f32, and changed // to v2i64. This is purely a nop, since those are bitwise intrinsics. // So, the only thing required is a bitcast for both arguments. // First, check the arguments have the old type. Value *Arg0 = CI->getArgOperand(0); if (Arg0->getType() != VectorType::get(Type::getFloatTy(C), 4)) return; // Old intrinsic, add bitcasts Value *Arg1 = CI->getArgOperand(1); Value *BC0 = Builder.CreateBitCast(Arg0, VectorType::get(Type::getInt64Ty(C), 2), "cast"); Value *BC1 = Builder.CreateBitCast(Arg1, VectorType::get(Type::getInt64Ty(C), 2), "cast"); CallInst* NewCall = Builder.CreateCall2(NewFn, BC0, BC1, Name); CI->replaceAllUsesWith(NewCall); CI->eraseFromParent(); return; } } } // This tests each Function to determine if it needs upgrading. When we find // one we are interested in, we then upgrade all calls to reflect the new // function. void llvm::UpgradeCallsToIntrinsic(Function* F) { assert(F && "Illegal attempt to upgrade a non-existent intrinsic."); // Upgrade the function and check if it is a totaly new function. Function *NewFn; if (UpgradeIntrinsicFunction(F, NewFn)) { if (NewFn != F) { // Replace all uses to the old function with the new one if necessary. for (Value::use_iterator UI = F->use_begin(), UE = F->use_end(); UI != UE; ) { if (CallInst *CI = dyn_cast(*UI++)) UpgradeIntrinsicCall(CI, NewFn); } // Remove old function, no longer used, from the module. F->eraseFromParent(); } } } void llvm::UpgradeInstWithTBAATag(Instruction *I) { MDNode *MD = I->getMetadata(LLVMContext::MD_tbaa); assert(MD && "UpgradeInstWithTBAATag should have a TBAA tag"); // Check if the tag uses struct-path aware TBAA format. if (isa(MD->getOperand(0)) && MD->getNumOperands() >= 3) return; if (MD->getNumOperands() == 3) { Value *Elts[] = { MD->getOperand(0), MD->getOperand(1) }; MDNode *ScalarType = MDNode::get(I->getContext(), Elts); // Create a MDNode Value *Elts2[] = { ScalarType, ScalarType, Constant::getNullValue(Type::getInt64Ty(I->getContext())), MD->getOperand(2) }; I->setMetadata(LLVMContext::MD_tbaa, MDNode::get(I->getContext(), Elts2)); } else { // Create a MDNode Value *Elts[] = {MD, MD, Constant::getNullValue(Type::getInt64Ty(I->getContext()))}; I->setMetadata(LLVMContext::MD_tbaa, MDNode::get(I->getContext(), Elts)); } } Instruction *llvm::UpgradeBitCastInst(unsigned Opc, Value *V, Type *DestTy, Instruction *&Temp) { if (Opc != Instruction::BitCast) return 0; Temp = 0; Type *SrcTy = V->getType(); if (SrcTy->isPtrOrPtrVectorTy() && DestTy->isPtrOrPtrVectorTy() && SrcTy->getPointerAddressSpace() != DestTy->getPointerAddressSpace()) { LLVMContext &Context = V->getContext(); // We have no information about target data layout, so we assume that // the maximum pointer size is 64bit. Type *MidTy = Type::getInt64Ty(Context); Temp = CastInst::Create(Instruction::PtrToInt, V, MidTy); return CastInst::Create(Instruction::IntToPtr, Temp, DestTy); } return 0; } Value *llvm::UpgradeBitCastExpr(unsigned Opc, Constant *C, Type *DestTy) { if (Opc != Instruction::BitCast) return 0; Type *SrcTy = C->getType(); if (SrcTy->isPtrOrPtrVectorTy() && DestTy->isPtrOrPtrVectorTy() && SrcTy->getPointerAddressSpace() != DestTy->getPointerAddressSpace()) { LLVMContext &Context = C->getContext(); // We have no information about target data layout, so we assume that // the maximum pointer size is 64bit. Type *MidTy = Type::getInt64Ty(Context); return ConstantExpr::getIntToPtr(ConstantExpr::getPtrToInt(C, MidTy), DestTy); } return 0; } /// Check the debug info version number, if it is out-dated, drop the debug /// info. Return true if module is modified. bool llvm::UpgradeDebugInfo(Module &M) { if (getDebugMetadataVersionFromModule(M) == DEBUG_METADATA_VERSION) return false; return StripDebugInfo(M); }