//===- lib/Linker/LinkModules.cpp - Module Linker Implementation ----------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the LLVM module linker. // //===----------------------------------------------------------------------===// #include "llvm/Linker.h" #include "llvm-c/Linker.h" #include "llvm/ADT/Optional.h" #include "llvm/ADT/SetVector.h" #include "llvm/ADT/SmallString.h" #include "llvm/IR/Constants.h" #include "llvm/IR/Module.h" #include "llvm/IR/TypeFinder.h" #include "llvm/Support/Debug.h" #include "llvm/Support/raw_ostream.h" #include "llvm/Transforms/Utils/Cloning.h" using namespace llvm; //===----------------------------------------------------------------------===// // TypeMap implementation. //===----------------------------------------------------------------------===// namespace { typedef SmallPtrSet TypeSet; class TypeMapTy : public ValueMapTypeRemapper { /// MappedTypes - This is a mapping from a source type to a destination type /// to use. DenseMap MappedTypes; /// SpeculativeTypes - When checking to see if two subgraphs are isomorphic, /// we speculatively add types to MappedTypes, but keep track of them here in /// case we need to roll back. SmallVector SpeculativeTypes; /// SrcDefinitionsToResolve - This is a list of non-opaque structs in the /// source module that are mapped to an opaque struct in the destination /// module. SmallVector SrcDefinitionsToResolve; /// DstResolvedOpaqueTypes - This is the set of opaque types in the /// destination modules who are getting a body from the source module. SmallPtrSet DstResolvedOpaqueTypes; public: TypeMapTy(TypeSet &Set) : DstStructTypesSet(Set) {} TypeSet &DstStructTypesSet; /// addTypeMapping - Indicate that the specified type in the destination /// module is conceptually equivalent to the specified type in the source /// module. void addTypeMapping(Type *DstTy, Type *SrcTy); /// linkDefinedTypeBodies - Produce a body for an opaque type in the dest /// module from a type definition in the source module. void linkDefinedTypeBodies(); /// get - Return the mapped type to use for the specified input type from the /// source module. Type *get(Type *SrcTy); FunctionType *get(FunctionType *T) {return cast(get((Type*)T));} /// dump - Dump out the type map for debugging purposes. void dump() const { for (DenseMap::const_iterator I = MappedTypes.begin(), E = MappedTypes.end(); I != E; ++I) { dbgs() << "TypeMap: "; I->first->dump(); dbgs() << " => "; I->second->dump(); dbgs() << '\n'; } } private: Type *getImpl(Type *T); /// remapType - Implement the ValueMapTypeRemapper interface. Type *remapType(Type *SrcTy) { return get(SrcTy); } bool areTypesIsomorphic(Type *DstTy, Type *SrcTy); }; } void TypeMapTy::addTypeMapping(Type *DstTy, Type *SrcTy) { Type *&Entry = MappedTypes[SrcTy]; if (Entry) return; if (DstTy == SrcTy) { Entry = DstTy; return; } // Check to see if these types are recursively isomorphic and establish a // mapping between them if so. if (!areTypesIsomorphic(DstTy, SrcTy)) { // Oops, they aren't isomorphic. Just discard this request by rolling out // any speculative mappings we've established. for (unsigned i = 0, e = SpeculativeTypes.size(); i != e; ++i) MappedTypes.erase(SpeculativeTypes[i]); } SpeculativeTypes.clear(); } /// areTypesIsomorphic - Recursively walk this pair of types, returning true /// if they are isomorphic, false if they are not. bool TypeMapTy::areTypesIsomorphic(Type *DstTy, Type *SrcTy) { // Two types with differing kinds are clearly not isomorphic. if (DstTy->getTypeID() != SrcTy->getTypeID()) return false; // If we have an entry in the MappedTypes table, then we have our answer. Type *&Entry = MappedTypes[SrcTy]; if (Entry) return Entry == DstTy; // Two identical types are clearly isomorphic. Remember this // non-speculatively. if (DstTy == SrcTy) { Entry = DstTy; return true; } // Okay, we have two types with identical kinds that we haven't seen before. // If this is an opaque struct type, special case it. if (StructType *SSTy = dyn_cast(SrcTy)) { // Mapping an opaque type to any struct, just keep the dest struct. if (SSTy->isOpaque()) { Entry = DstTy; SpeculativeTypes.push_back(SrcTy); return true; } // Mapping a non-opaque source type to an opaque dest. If this is the first // type that we're mapping onto this destination type then we succeed. Keep // the dest, but fill it in later. This doesn't need to be speculative. If // this is the second (different) type that we're trying to map onto the // same opaque type then we fail. if (cast(DstTy)->isOpaque()) { // We can only map one source type onto the opaque destination type. if (!DstResolvedOpaqueTypes.insert(cast(DstTy))) return false; SrcDefinitionsToResolve.push_back(SSTy); Entry = DstTy; return true; } } // If the number of subtypes disagree between the two types, then we fail. if (SrcTy->getNumContainedTypes() != DstTy->getNumContainedTypes()) return false; // Fail if any of the extra properties (e.g. array size) of the type disagree. if (isa(DstTy)) return false; // bitwidth disagrees. if (PointerType *PT = dyn_cast(DstTy)) { if (PT->getAddressSpace() != cast(SrcTy)->getAddressSpace()) return false; } else if (FunctionType *FT = dyn_cast(DstTy)) { if (FT->isVarArg() != cast(SrcTy)->isVarArg()) return false; } else if (StructType *DSTy = dyn_cast(DstTy)) { StructType *SSTy = cast(SrcTy); if (DSTy->isLiteral() != SSTy->isLiteral() || DSTy->isPacked() != SSTy->isPacked()) return false; } else if (ArrayType *DATy = dyn_cast(DstTy)) { if (DATy->getNumElements() != cast(SrcTy)->getNumElements()) return false; } else if (VectorType *DVTy = dyn_cast(DstTy)) { if (DVTy->getNumElements() != cast(SrcTy)->getNumElements()) return false; } // Otherwise, we speculate that these two types will line up and recursively // check the subelements. Entry = DstTy; SpeculativeTypes.push_back(SrcTy); for (unsigned i = 0, e = SrcTy->getNumContainedTypes(); i != e; ++i) if (!areTypesIsomorphic(DstTy->getContainedType(i), SrcTy->getContainedType(i))) return false; // If everything seems to have lined up, then everything is great. return true; } /// linkDefinedTypeBodies - Produce a body for an opaque type in the dest /// module from a type definition in the source module. void TypeMapTy::linkDefinedTypeBodies() { SmallVector Elements; SmallString<16> TmpName; // Note that processing entries in this loop (calling 'get') can add new // entries to the SrcDefinitionsToResolve vector. while (!SrcDefinitionsToResolve.empty()) { StructType *SrcSTy = SrcDefinitionsToResolve.pop_back_val(); StructType *DstSTy = cast(MappedTypes[SrcSTy]); // TypeMap is a many-to-one mapping, if there were multiple types that // provide a body for DstSTy then previous iterations of this loop may have // already handled it. Just ignore this case. if (!DstSTy->isOpaque()) continue; assert(!SrcSTy->isOpaque() && "Not resolving a definition?"); // Map the body of the source type over to a new body for the dest type. Elements.resize(SrcSTy->getNumElements()); for (unsigned i = 0, e = Elements.size(); i != e; ++i) Elements[i] = getImpl(SrcSTy->getElementType(i)); DstSTy->setBody(Elements, SrcSTy->isPacked()); // If DstSTy has no name or has a longer name than STy, then viciously steal // STy's name. if (!SrcSTy->hasName()) continue; StringRef SrcName = SrcSTy->getName(); if (!DstSTy->hasName() || DstSTy->getName().size() > SrcName.size()) { TmpName.insert(TmpName.end(), SrcName.begin(), SrcName.end()); SrcSTy->setName(""); DstSTy->setName(TmpName.str()); TmpName.clear(); } } DstResolvedOpaqueTypes.clear(); } /// get - Return the mapped type to use for the specified input type from the /// source module. Type *TypeMapTy::get(Type *Ty) { Type *Result = getImpl(Ty); // If this caused a reference to any struct type, resolve it before returning. if (!SrcDefinitionsToResolve.empty()) linkDefinedTypeBodies(); return Result; } /// getImpl - This is the recursive version of get(). Type *TypeMapTy::getImpl(Type *Ty) { // If we already have an entry for this type, return it. Type **Entry = &MappedTypes[Ty]; if (*Entry) return *Entry; // If this is not a named struct type, then just map all of the elements and // then rebuild the type from inside out. if (!isa(Ty) || cast(Ty)->isLiteral()) { // If there are no element types to map, then the type is itself. This is // true for the anonymous {} struct, things like 'float', integers, etc. if (Ty->getNumContainedTypes() == 0) return *Entry = Ty; // Remap all of the elements, keeping track of whether any of them change. bool AnyChange = false; SmallVector ElementTypes; ElementTypes.resize(Ty->getNumContainedTypes()); for (unsigned i = 0, e = Ty->getNumContainedTypes(); i != e; ++i) { ElementTypes[i] = getImpl(Ty->getContainedType(i)); AnyChange |= ElementTypes[i] != Ty->getContainedType(i); } // If we found our type while recursively processing stuff, just use it. Entry = &MappedTypes[Ty]; if (*Entry) return *Entry; // If all of the element types mapped directly over, then the type is usable // as-is. if (!AnyChange) return *Entry = Ty; // Otherwise, rebuild a modified type. switch (Ty->getTypeID()) { default: llvm_unreachable("unknown derived type to remap"); case Type::ArrayTyID: return *Entry = ArrayType::get(ElementTypes[0], cast(Ty)->getNumElements()); case Type::VectorTyID: return *Entry = VectorType::get(ElementTypes[0], cast(Ty)->getNumElements()); case Type::PointerTyID: return *Entry = PointerType::get(ElementTypes[0], cast(Ty)->getAddressSpace()); case Type::FunctionTyID: return *Entry = FunctionType::get(ElementTypes[0], makeArrayRef(ElementTypes).slice(1), cast(Ty)->isVarArg()); case Type::StructTyID: // Note that this is only reached for anonymous structs. return *Entry = StructType::get(Ty->getContext(), ElementTypes, cast(Ty)->isPacked()); } } // Otherwise, this is an unmapped named struct. If the struct can be directly // mapped over, just use it as-is. This happens in a case when the linked-in // module has something like: // %T = type {%T*, i32} // @GV = global %T* null // where T does not exist at all in the destination module. // // The other case we watch for is when the type is not in the destination // module, but that it has to be rebuilt because it refers to something that // is already mapped. For example, if the destination module has: // %A = type { i32 } // and the source module has something like // %A' = type { i32 } // %B = type { %A'* } // @GV = global %B* null // then we want to create a new type: "%B = type { %A*}" and have it take the // pristine "%B" name from the source module. // // To determine which case this is, we have to recursively walk the type graph // speculating that we'll be able to reuse it unmodified. Only if this is // safe would we map the entire thing over. Because this is an optimization, // and is not required for the prettiness of the linked module, we just skip // it and always rebuild a type here. StructType *STy = cast(Ty); // If the type is opaque, we can just use it directly. if (STy->isOpaque()) { // A named structure type from src module is used. Add it to the Set of // identified structs in the destination module. DstStructTypesSet.insert(STy); return *Entry = STy; } // Otherwise we create a new type and resolve its body later. This will be // resolved by the top level of get(). SrcDefinitionsToResolve.push_back(STy); StructType *DTy = StructType::create(STy->getContext()); // A new identified structure type was created. Add it to the set of // identified structs in the destination module. DstStructTypesSet.insert(DTy); DstResolvedOpaqueTypes.insert(DTy); return *Entry = DTy; } //===----------------------------------------------------------------------===// // ModuleLinker implementation. //===----------------------------------------------------------------------===// namespace { class ModuleLinker; /// ValueMaterializerTy - Creates prototypes for functions that are lazily /// linked on the fly. This speeds up linking for modules with many /// lazily linked functions of which few get used. class ValueMaterializerTy : public ValueMaterializer { TypeMapTy &TypeMap; Module *DstM; std::vector &LazilyLinkFunctions; public: ValueMaterializerTy(TypeMapTy &TypeMap, Module *DstM, std::vector &LazilyLinkFunctions) : ValueMaterializer(), TypeMap(TypeMap), DstM(DstM), LazilyLinkFunctions(LazilyLinkFunctions) { } virtual Value *materializeValueFor(Value *V); }; /// ModuleLinker - This is an implementation class for the LinkModules /// function, which is the entrypoint for this file. class ModuleLinker { Module *DstM, *SrcM; TypeMapTy TypeMap; ValueMaterializerTy ValMaterializer; /// ValueMap - Mapping of values from what they used to be in Src, to what /// they are now in DstM. ValueToValueMapTy is a ValueMap, which involves /// some overhead due to the use of Value handles which the Linker doesn't /// actually need, but this allows us to reuse the ValueMapper code. ValueToValueMapTy ValueMap; struct AppendingVarInfo { GlobalVariable *NewGV; // New aggregate global in dest module. Constant *DstInit; // Old initializer from dest module. Constant *SrcInit; // Old initializer from src module. }; std::vector AppendingVars; unsigned Mode; // Mode to treat source module. // Set of items not to link in from source. SmallPtrSet DoNotLinkFromSource; // Vector of functions to lazily link in. std::vector LazilyLinkFunctions; public: std::string ErrorMsg; ModuleLinker(Module *dstM, TypeSet &Set, Module *srcM, unsigned mode) : DstM(dstM), SrcM(srcM), TypeMap(Set), ValMaterializer(TypeMap, DstM, LazilyLinkFunctions), Mode(mode) { } bool run(); private: /// emitError - Helper method for setting a message and returning an error /// code. bool emitError(const Twine &Message) { ErrorMsg = Message.str(); return true; } /// getLinkageResult - This analyzes the two global values and determines /// what the result will look like in the destination module. bool getLinkageResult(GlobalValue *Dest, const GlobalValue *Src, GlobalValue::LinkageTypes <, GlobalValue::VisibilityTypes &Vis, bool &LinkFromSrc); /// getLinkedToGlobal - Given a global in the source module, return the /// global in the destination module that is being linked to, if any. GlobalValue *getLinkedToGlobal(GlobalValue *SrcGV) { // If the source has no name it can't link. If it has local linkage, // there is no name match-up going on. if (!SrcGV->hasName() || SrcGV->hasLocalLinkage()) return 0; // Otherwise see if we have a match in the destination module's symtab. GlobalValue *DGV = DstM->getNamedValue(SrcGV->getName()); if (DGV == 0) return 0; // If we found a global with the same name in the dest module, but it has // internal linkage, we are really not doing any linkage here. if (DGV->hasLocalLinkage()) return 0; // Otherwise, we do in fact link to the destination global. return DGV; } void computeTypeMapping(); bool linkAppendingVarProto(GlobalVariable *DstGV, GlobalVariable *SrcGV); bool linkGlobalProto(GlobalVariable *SrcGV); bool linkFunctionProto(Function *SrcF); bool linkAliasProto(GlobalAlias *SrcA); bool linkModuleFlagsMetadata(); void linkAppendingVarInit(const AppendingVarInfo &AVI); void linkGlobalInits(); void linkFunctionBody(Function *Dst, Function *Src); void linkAliasBodies(); void linkNamedMDNodes(); }; } /// forceRenaming - The LLVM SymbolTable class autorenames globals that conflict /// in the symbol table. This is good for all clients except for us. Go /// through the trouble to force this back. static void forceRenaming(GlobalValue *GV, StringRef Name) { // If the global doesn't force its name or if it already has the right name, // there is nothing for us to do. if (GV->hasLocalLinkage() || GV->getName() == Name) return; Module *M = GV->getParent(); // If there is a conflict, rename the conflict. if (GlobalValue *ConflictGV = M->getNamedValue(Name)) { GV->takeName(ConflictGV); ConflictGV->setName(Name); // This will cause ConflictGV to get renamed assert(ConflictGV->getName() != Name && "forceRenaming didn't work"); } else { GV->setName(Name); // Force the name back } } /// copyGVAttributes - copy additional attributes (those not needed to construct /// a GlobalValue) from the SrcGV to the DestGV. static void copyGVAttributes(GlobalValue *DestGV, const GlobalValue *SrcGV) { // Use the maximum alignment, rather than just copying the alignment of SrcGV. unsigned Alignment = std::max(DestGV->getAlignment(), SrcGV->getAlignment()); DestGV->copyAttributesFrom(SrcGV); DestGV->setAlignment(Alignment); forceRenaming(DestGV, SrcGV->getName()); } static bool isLessConstraining(GlobalValue::VisibilityTypes a, GlobalValue::VisibilityTypes b) { if (a == GlobalValue::HiddenVisibility) return false; if (b == GlobalValue::HiddenVisibility) return true; if (a == GlobalValue::ProtectedVisibility) return false; if (b == GlobalValue::ProtectedVisibility) return true; return false; } Value *ValueMaterializerTy::materializeValueFor(Value *V) { Function *SF = dyn_cast(V); if (!SF) return NULL; Function *DF = Function::Create(TypeMap.get(SF->getFunctionType()), SF->getLinkage(), SF->getName(), DstM); copyGVAttributes(DF, SF); LazilyLinkFunctions.push_back(SF); return DF; } /// getLinkageResult - This analyzes the two global values and determines what /// the result will look like in the destination module. In particular, it /// computes the resultant linkage type and visibility, computes whether the /// global in the source should be copied over to the destination (replacing /// the existing one), and computes whether this linkage is an error or not. bool ModuleLinker::getLinkageResult(GlobalValue *Dest, const GlobalValue *Src, GlobalValue::LinkageTypes <, GlobalValue::VisibilityTypes &Vis, bool &LinkFromSrc) { assert(Dest && "Must have two globals being queried"); assert(!Src->hasLocalLinkage() && "If Src has internal linkage, Dest shouldn't be set!"); bool SrcIsDeclaration = Src->isDeclaration() && !Src->isMaterializable(); bool DestIsDeclaration = Dest->isDeclaration(); if (SrcIsDeclaration) { // If Src is external or if both Src & Dest are external.. Just link the // external globals, we aren't adding anything. if (Src->hasDLLImportLinkage()) { // If one of GVs has DLLImport linkage, result should be dllimport'ed. if (DestIsDeclaration) { LinkFromSrc = true; LT = Src->getLinkage(); } } else if (Dest->hasExternalWeakLinkage()) { // If the Dest is weak, use the source linkage. LinkFromSrc = true; LT = Src->getLinkage(); } else { LinkFromSrc = false; LT = Dest->getLinkage(); } } else if (DestIsDeclaration && !Dest->hasDLLImportLinkage()) { // If Dest is external but Src is not: LinkFromSrc = true; LT = Src->getLinkage(); } else if (Src->isWeakForLinker()) { // At this point we know that Dest has LinkOnce, External*, Weak, Common, // or DLL* linkage. if (Dest->hasExternalWeakLinkage() || Dest->hasAvailableExternallyLinkage() || (Dest->hasLinkOnceLinkage() && (Src->hasWeakLinkage() || Src->hasCommonLinkage()))) { LinkFromSrc = true; LT = Src->getLinkage(); } else { LinkFromSrc = false; LT = Dest->getLinkage(); } } else if (Dest->isWeakForLinker()) { // At this point we know that Src has External* or DLL* linkage. if (Src->hasExternalWeakLinkage()) { LinkFromSrc = false; LT = Dest->getLinkage(); } else { LinkFromSrc = true; LT = GlobalValue::ExternalLinkage; } } else { assert((Dest->hasExternalLinkage() || Dest->hasDLLImportLinkage() || Dest->hasDLLExportLinkage() || Dest->hasExternalWeakLinkage()) && (Src->hasExternalLinkage() || Src->hasDLLImportLinkage() || Src->hasDLLExportLinkage() || Src->hasExternalWeakLinkage()) && "Unexpected linkage type!"); return emitError("Linking globals named '" + Src->getName() + "': symbol multiply defined!"); } // Compute the visibility. We follow the rules in the System V Application // Binary Interface. Vis = isLessConstraining(Src->getVisibility(), Dest->getVisibility()) ? Dest->getVisibility() : Src->getVisibility(); return false; } /// computeTypeMapping - Loop over all of the linked values to compute type /// mappings. For example, if we link "extern Foo *x" and "Foo *x = NULL", then /// we have two struct types 'Foo' but one got renamed when the module was /// loaded into the same LLVMContext. void ModuleLinker::computeTypeMapping() { // Incorporate globals. for (Module::global_iterator I = SrcM->global_begin(), E = SrcM->global_end(); I != E; ++I) { GlobalValue *DGV = getLinkedToGlobal(I); if (DGV == 0) continue; if (!DGV->hasAppendingLinkage() || !I->hasAppendingLinkage()) { TypeMap.addTypeMapping(DGV->getType(), I->getType()); continue; } // Unify the element type of appending arrays. ArrayType *DAT = cast(DGV->getType()->getElementType()); ArrayType *SAT = cast(I->getType()->getElementType()); TypeMap.addTypeMapping(DAT->getElementType(), SAT->getElementType()); } // Incorporate functions. for (Module::iterator I = SrcM->begin(), E = SrcM->end(); I != E; ++I) { if (GlobalValue *DGV = getLinkedToGlobal(I)) TypeMap.addTypeMapping(DGV->getType(), I->getType()); } // Incorporate types by name, scanning all the types in the source module. // At this point, the destination module may have a type "%foo = { i32 }" for // example. When the source module got loaded into the same LLVMContext, if // it had the same type, it would have been renamed to "%foo.42 = { i32 }". TypeFinder SrcStructTypes; SrcStructTypes.run(*SrcM, true); SmallPtrSet SrcStructTypesSet(SrcStructTypes.begin(), SrcStructTypes.end()); for (unsigned i = 0, e = SrcStructTypes.size(); i != e; ++i) { StructType *ST = SrcStructTypes[i]; if (!ST->hasName()) continue; // Check to see if there is a dot in the name followed by a digit. size_t DotPos = ST->getName().rfind('.'); if (DotPos == 0 || DotPos == StringRef::npos || ST->getName().back() == '.' || !isdigit(static_cast(ST->getName()[DotPos+1]))) continue; // Check to see if the destination module has a struct with the prefix name. if (StructType *DST = DstM->getTypeByName(ST->getName().substr(0, DotPos))) // Don't use it if this actually came from the source module. They're in // the same LLVMContext after all. Also don't use it unless the type is // actually used in the destination module. This can happen in situations // like this: // // Module A Module B // -------- -------- // %Z = type { %A } %B = type { %C.1 } // %A = type { %B.1, [7 x i8] } %C.1 = type { i8* } // %B.1 = type { %C } %A.2 = type { %B.3, [5 x i8] } // %C = type { i8* } %B.3 = type { %C.1 } // // When we link Module B with Module A, the '%B' in Module B is // used. However, that would then use '%C.1'. But when we process '%C.1', // we prefer to take the '%C' version. So we are then left with both // '%C.1' and '%C' being used for the same types. This leads to some // variables using one type and some using the other. if (!SrcStructTypesSet.count(DST) && TypeMap.DstStructTypesSet.count(DST)) TypeMap.addTypeMapping(DST, ST); } // Don't bother incorporating aliases, they aren't generally typed well. // Now that we have discovered all of the type equivalences, get a body for // any 'opaque' types in the dest module that are now resolved. TypeMap.linkDefinedTypeBodies(); } /// linkAppendingVarProto - If there were any appending global variables, link /// them together now. Return true on error. bool ModuleLinker::linkAppendingVarProto(GlobalVariable *DstGV, GlobalVariable *SrcGV) { if (!SrcGV->hasAppendingLinkage() || !DstGV->hasAppendingLinkage()) return emitError("Linking globals named '" + SrcGV->getName() + "': can only link appending global with another appending global!"); ArrayType *DstTy = cast(DstGV->getType()->getElementType()); ArrayType *SrcTy = cast(TypeMap.get(SrcGV->getType()->getElementType())); Type *EltTy = DstTy->getElementType(); // Check to see that they two arrays agree on type. if (EltTy != SrcTy->getElementType()) return emitError("Appending variables with different element types!"); if (DstGV->isConstant() != SrcGV->isConstant()) return emitError("Appending variables linked with different const'ness!"); if (DstGV->getAlignment() != SrcGV->getAlignment()) return emitError( "Appending variables with different alignment need to be linked!"); if (DstGV->getVisibility() != SrcGV->getVisibility()) return emitError( "Appending variables with different visibility need to be linked!"); if (DstGV->getSection() != SrcGV->getSection()) return emitError( "Appending variables with different section name need to be linked!"); uint64_t NewSize = DstTy->getNumElements() + SrcTy->getNumElements(); ArrayType *NewType = ArrayType::get(EltTy, NewSize); // Create the new global variable. GlobalVariable *NG = new GlobalVariable(*DstGV->getParent(), NewType, SrcGV->isConstant(), DstGV->getLinkage(), /*init*/0, /*name*/"", DstGV, DstGV->getThreadLocalMode(), DstGV->getType()->getAddressSpace()); // Propagate alignment, visibility and section info. copyGVAttributes(NG, DstGV); AppendingVarInfo AVI; AVI.NewGV = NG; AVI.DstInit = DstGV->getInitializer(); AVI.SrcInit = SrcGV->getInitializer(); AppendingVars.push_back(AVI); // Replace any uses of the two global variables with uses of the new // global. ValueMap[SrcGV] = ConstantExpr::getBitCast(NG, TypeMap.get(SrcGV->getType())); DstGV->replaceAllUsesWith(ConstantExpr::getBitCast(NG, DstGV->getType())); DstGV->eraseFromParent(); // Track the source variable so we don't try to link it. DoNotLinkFromSource.insert(SrcGV); return false; } /// linkGlobalProto - Loop through the global variables in the src module and /// merge them into the dest module. bool ModuleLinker::linkGlobalProto(GlobalVariable *SGV) { GlobalValue *DGV = getLinkedToGlobal(SGV); llvm::Optional NewVisibility; if (DGV) { // Concatenation of appending linkage variables is magic and handled later. if (DGV->hasAppendingLinkage() || SGV->hasAppendingLinkage()) return linkAppendingVarProto(cast(DGV), SGV); // Determine whether linkage of these two globals follows the source // module's definition or the destination module's definition. GlobalValue::LinkageTypes NewLinkage = GlobalValue::InternalLinkage; GlobalValue::VisibilityTypes NV; bool LinkFromSrc = false; if (getLinkageResult(DGV, SGV, NewLinkage, NV, LinkFromSrc)) return true; NewVisibility = NV; // If we're not linking from the source, then keep the definition that we // have. if (!LinkFromSrc) { // Special case for const propagation. if (GlobalVariable *DGVar = dyn_cast(DGV)) if (DGVar->isDeclaration() && SGV->isConstant() && !DGVar->isConstant()) DGVar->setConstant(true); // Set calculated linkage and visibility. DGV->setLinkage(NewLinkage); DGV->setVisibility(*NewVisibility); // Make sure to remember this mapping. ValueMap[SGV] = ConstantExpr::getBitCast(DGV,TypeMap.get(SGV->getType())); // Track the source global so that we don't attempt to copy it over when // processing global initializers. DoNotLinkFromSource.insert(SGV); return false; } } // No linking to be performed or linking from the source: simply create an // identical version of the symbol over in the dest module... the // initializer will be filled in later by LinkGlobalInits. GlobalVariable *NewDGV = new GlobalVariable(*DstM, TypeMap.get(SGV->getType()->getElementType()), SGV->isConstant(), SGV->getLinkage(), /*init*/0, SGV->getName(), /*insertbefore*/0, SGV->getThreadLocalMode(), SGV->getType()->getAddressSpace()); // Propagate alignment, visibility and section info. copyGVAttributes(NewDGV, SGV); if (NewVisibility) NewDGV->setVisibility(*NewVisibility); if (DGV) { DGV->replaceAllUsesWith(ConstantExpr::getBitCast(NewDGV, DGV->getType())); DGV->eraseFromParent(); } // Make sure to remember this mapping. ValueMap[SGV] = NewDGV; return false; } /// linkFunctionProto - Link the function in the source module into the /// destination module if needed, setting up mapping information. bool ModuleLinker::linkFunctionProto(Function *SF) { GlobalValue *DGV = getLinkedToGlobal(SF); llvm::Optional NewVisibility; if (DGV) { GlobalValue::LinkageTypes NewLinkage = GlobalValue::InternalLinkage; bool LinkFromSrc = false; GlobalValue::VisibilityTypes NV; if (getLinkageResult(DGV, SF, NewLinkage, NV, LinkFromSrc)) return true; NewVisibility = NV; if (!LinkFromSrc) { // Set calculated linkage DGV->setLinkage(NewLinkage); DGV->setVisibility(*NewVisibility); // Make sure to remember this mapping. ValueMap[SF] = ConstantExpr::getBitCast(DGV, TypeMap.get(SF->getType())); // Track the function from the source module so we don't attempt to remap // it. DoNotLinkFromSource.insert(SF); return false; } } // If the function is to be lazily linked, don't create it just yet. // The ValueMaterializerTy will deal with creating it if it's used. if (!DGV && (SF->hasLocalLinkage() || SF->hasLinkOnceLinkage() || SF->hasAvailableExternallyLinkage())) { DoNotLinkFromSource.insert(SF); return false; } // If there is no linkage to be performed or we are linking from the source, // bring SF over. Function *NewDF = Function::Create(TypeMap.get(SF->getFunctionType()), SF->getLinkage(), SF->getName(), DstM); copyGVAttributes(NewDF, SF); if (NewVisibility) NewDF->setVisibility(*NewVisibility); if (DGV) { // Any uses of DF need to change to NewDF, with cast. DGV->replaceAllUsesWith(ConstantExpr::getBitCast(NewDF, DGV->getType())); DGV->eraseFromParent(); } ValueMap[SF] = NewDF; return false; } /// LinkAliasProto - Set up prototypes for any aliases that come over from the /// source module. bool ModuleLinker::linkAliasProto(GlobalAlias *SGA) { GlobalValue *DGV = getLinkedToGlobal(SGA); llvm::Optional NewVisibility; if (DGV) { GlobalValue::LinkageTypes NewLinkage = GlobalValue::InternalLinkage; GlobalValue::VisibilityTypes NV; bool LinkFromSrc = false; if (getLinkageResult(DGV, SGA, NewLinkage, NV, LinkFromSrc)) return true; NewVisibility = NV; if (!LinkFromSrc) { // Set calculated linkage. DGV->setLinkage(NewLinkage); DGV->setVisibility(*NewVisibility); // Make sure to remember this mapping. ValueMap[SGA] = ConstantExpr::getBitCast(DGV,TypeMap.get(SGA->getType())); // Track the alias from the source module so we don't attempt to remap it. DoNotLinkFromSource.insert(SGA); return false; } } // If there is no linkage to be performed or we're linking from the source, // bring over SGA. GlobalAlias *NewDA = new GlobalAlias(TypeMap.get(SGA->getType()), SGA->getLinkage(), SGA->getName(), /*aliasee*/0, DstM); copyGVAttributes(NewDA, SGA); if (NewVisibility) NewDA->setVisibility(*NewVisibility); if (DGV) { // Any uses of DGV need to change to NewDA, with cast. DGV->replaceAllUsesWith(ConstantExpr::getBitCast(NewDA, DGV->getType())); DGV->eraseFromParent(); } ValueMap[SGA] = NewDA; return false; } static void getArrayElements(Constant *C, SmallVectorImpl &Dest) { unsigned NumElements = cast(C->getType())->getNumElements(); for (unsigned i = 0; i != NumElements; ++i) Dest.push_back(C->getAggregateElement(i)); } void ModuleLinker::linkAppendingVarInit(const AppendingVarInfo &AVI) { // Merge the initializer. SmallVector Elements; getArrayElements(AVI.DstInit, Elements); Constant *SrcInit = MapValue(AVI.SrcInit, ValueMap, RF_None, &TypeMap, &ValMaterializer); getArrayElements(SrcInit, Elements); ArrayType *NewType = cast(AVI.NewGV->getType()->getElementType()); AVI.NewGV->setInitializer(ConstantArray::get(NewType, Elements)); } /// linkGlobalInits - Update the initializers in the Dest module now that all /// globals that may be referenced are in Dest. void ModuleLinker::linkGlobalInits() { // Loop over all of the globals in the src module, mapping them over as we go for (Module::const_global_iterator I = SrcM->global_begin(), E = SrcM->global_end(); I != E; ++I) { // Only process initialized GV's or ones not already in dest. if (!I->hasInitializer() || DoNotLinkFromSource.count(I)) continue; // Grab destination global variable. GlobalVariable *DGV = cast(ValueMap[I]); // Figure out what the initializer looks like in the dest module. DGV->setInitializer(MapValue(I->getInitializer(), ValueMap, RF_None, &TypeMap, &ValMaterializer)); } } /// linkFunctionBody - Copy the source function over into the dest function and /// fix up references to values. At this point we know that Dest is an external /// function, and that Src is not. void ModuleLinker::linkFunctionBody(Function *Dst, Function *Src) { assert(Src && Dst && Dst->isDeclaration() && !Src->isDeclaration()); // Go through and convert function arguments over, remembering the mapping. Function::arg_iterator DI = Dst->arg_begin(); for (Function::arg_iterator I = Src->arg_begin(), E = Src->arg_end(); I != E; ++I, ++DI) { DI->setName(I->getName()); // Copy the name over. // Add a mapping to our mapping. ValueMap[I] = DI; } if (Mode == Linker::DestroySource) { // Splice the body of the source function into the dest function. Dst->getBasicBlockList().splice(Dst->end(), Src->getBasicBlockList()); // At this point, all of the instructions and values of the function are now // copied over. The only problem is that they are still referencing values in // the Source function as operands. Loop through all of the operands of the // functions and patch them up to point to the local versions. for (Function::iterator BB = Dst->begin(), BE = Dst->end(); BB != BE; ++BB) for (BasicBlock::iterator I = BB->begin(), E = BB->end(); I != E; ++I) RemapInstruction(I, ValueMap, RF_IgnoreMissingEntries, &TypeMap, &ValMaterializer); } else { // Clone the body of the function into the dest function. SmallVector Returns; // Ignore returns. CloneFunctionInto(Dst, Src, ValueMap, false, Returns, "", NULL, &TypeMap, &ValMaterializer); } // There is no need to map the arguments anymore. for (Function::arg_iterator I = Src->arg_begin(), E = Src->arg_end(); I != E; ++I) ValueMap.erase(I); } /// linkAliasBodies - Insert all of the aliases in Src into the Dest module. void ModuleLinker::linkAliasBodies() { for (Module::alias_iterator I = SrcM->alias_begin(), E = SrcM->alias_end(); I != E; ++I) { if (DoNotLinkFromSource.count(I)) continue; if (Constant *Aliasee = I->getAliasee()) { GlobalAlias *DA = cast(ValueMap[I]); DA->setAliasee(MapValue(Aliasee, ValueMap, RF_None, &TypeMap, &ValMaterializer)); } } } /// linkNamedMDNodes - Insert all of the named MDNodes in Src into the Dest /// module. void ModuleLinker::linkNamedMDNodes() { const NamedMDNode *SrcModFlags = SrcM->getModuleFlagsMetadata(); for (Module::const_named_metadata_iterator I = SrcM->named_metadata_begin(), E = SrcM->named_metadata_end(); I != E; ++I) { // Don't link module flags here. Do them separately. if (&*I == SrcModFlags) continue; NamedMDNode *DestNMD = DstM->getOrInsertNamedMetadata(I->getName()); // Add Src elements into Dest node. for (unsigned i = 0, e = I->getNumOperands(); i != e; ++i) DestNMD->addOperand(MapValue(I->getOperand(i), ValueMap, RF_None, &TypeMap, &ValMaterializer)); } } /// linkModuleFlagsMetadata - Merge the linker flags in Src into the Dest /// module. bool ModuleLinker::linkModuleFlagsMetadata() { // If the source module has no module flags, we are done. const NamedMDNode *SrcModFlags = SrcM->getModuleFlagsMetadata(); if (!SrcModFlags) return false; // If the destination module doesn't have module flags yet, then just copy // over the source module's flags. NamedMDNode *DstModFlags = DstM->getOrInsertModuleFlagsMetadata(); if (DstModFlags->getNumOperands() == 0) { for (unsigned I = 0, E = SrcModFlags->getNumOperands(); I != E; ++I) DstModFlags->addOperand(SrcModFlags->getOperand(I)); return false; } // First build a map of the existing module flags and requirements. DenseMap Flags; SmallSetVector Requirements; for (unsigned I = 0, E = DstModFlags->getNumOperands(); I != E; ++I) { MDNode *Op = DstModFlags->getOperand(I); ConstantInt *Behavior = cast(Op->getOperand(0)); MDString *ID = cast(Op->getOperand(1)); if (Behavior->getZExtValue() == Module::Require) { Requirements.insert(cast(Op->getOperand(2))); } else { Flags[ID] = Op; } } // Merge in the flags from the source module, and also collect its set of // requirements. bool HasErr = false; for (unsigned I = 0, E = SrcModFlags->getNumOperands(); I != E; ++I) { MDNode *SrcOp = SrcModFlags->getOperand(I); ConstantInt *SrcBehavior = cast(SrcOp->getOperand(0)); MDString *ID = cast(SrcOp->getOperand(1)); MDNode *DstOp = Flags.lookup(ID); unsigned SrcBehaviorValue = SrcBehavior->getZExtValue(); // If this is a requirement, add it and continue. if (SrcBehaviorValue == Module::Require) { // If the destination module does not already have this requirement, add // it. if (Requirements.insert(cast(SrcOp->getOperand(2)))) { DstModFlags->addOperand(SrcOp); } continue; } // If there is no existing flag with this ID, just add it. if (!DstOp) { Flags[ID] = SrcOp; DstModFlags->addOperand(SrcOp); continue; } // Otherwise, perform a merge. ConstantInt *DstBehavior = cast(DstOp->getOperand(0)); unsigned DstBehaviorValue = DstBehavior->getZExtValue(); // If either flag has override behavior, handle it first. if (DstBehaviorValue == Module::Override) { // Diagnose inconsistent flags which both have override behavior. if (SrcBehaviorValue == Module::Override && SrcOp->getOperand(2) != DstOp->getOperand(2)) { HasErr |= emitError("linking module flags '" + ID->getString() + "': IDs have conflicting override values"); } continue; } else if (SrcBehaviorValue == Module::Override) { // Update the destination flag to that of the source. DstOp->replaceOperandWith(0, SrcBehavior); DstOp->replaceOperandWith(2, SrcOp->getOperand(2)); continue; } // Diagnose inconsistent merge behavior types. if (SrcBehaviorValue != DstBehaviorValue) { HasErr |= emitError("linking module flags '" + ID->getString() + "': IDs have conflicting behaviors"); continue; } // Perform the merge for standard behavior types. switch (SrcBehaviorValue) { case Module::Require: case Module::Override: assert(0 && "not possible"); break; case Module::Error: { // Emit an error if the values differ. if (SrcOp->getOperand(2) != DstOp->getOperand(2)) { HasErr |= emitError("linking module flags '" + ID->getString() + "': IDs have conflicting values"); } continue; } case Module::Warning: { // Emit a warning if the values differ. if (SrcOp->getOperand(2) != DstOp->getOperand(2)) { errs() << "WARNING: linking module flags '" << ID->getString() << "': IDs have conflicting values"; } continue; } case Module::Append: { MDNode *DstValue = cast(DstOp->getOperand(2)); MDNode *SrcValue = cast(SrcOp->getOperand(2)); unsigned NumOps = DstValue->getNumOperands() + SrcValue->getNumOperands(); Value **VP, **Values = VP = new Value*[NumOps]; for (unsigned i = 0, e = DstValue->getNumOperands(); i != e; ++i, ++VP) *VP = DstValue->getOperand(i); for (unsigned i = 0, e = SrcValue->getNumOperands(); i != e; ++i, ++VP) *VP = SrcValue->getOperand(i); DstOp->replaceOperandWith(2, MDNode::get(DstM->getContext(), ArrayRef(Values, NumOps))); delete[] Values; break; } case Module::AppendUnique: { SmallSetVector Elts; MDNode *DstValue = cast(DstOp->getOperand(2)); MDNode *SrcValue = cast(SrcOp->getOperand(2)); for (unsigned i = 0, e = DstValue->getNumOperands(); i != e; ++i) Elts.insert(DstValue->getOperand(i)); for (unsigned i = 0, e = SrcValue->getNumOperands(); i != e; ++i) Elts.insert(SrcValue->getOperand(i)); DstOp->replaceOperandWith(2, MDNode::get(DstM->getContext(), ArrayRef(Elts.begin(), Elts.end()))); break; } } } // Check all of the requirements. for (unsigned I = 0, E = Requirements.size(); I != E; ++I) { MDNode *Requirement = Requirements[I]; MDString *Flag = cast(Requirement->getOperand(0)); Value *ReqValue = Requirement->getOperand(1); MDNode *Op = Flags[Flag]; if (!Op || Op->getOperand(2) != ReqValue) { HasErr |= emitError("linking module flags '" + Flag->getString() + "': does not have the required value"); continue; } } return HasErr; } bool ModuleLinker::run() { assert(DstM && "Null destination module"); assert(SrcM && "Null source module"); // Inherit the target data from the source module if the destination module // doesn't have one already. if (DstM->getDataLayout().empty() && !SrcM->getDataLayout().empty()) DstM->setDataLayout(SrcM->getDataLayout()); // Copy the target triple from the source to dest if the dest's is empty. if (DstM->getTargetTriple().empty() && !SrcM->getTargetTriple().empty()) DstM->setTargetTriple(SrcM->getTargetTriple()); if (!SrcM->getDataLayout().empty() && !DstM->getDataLayout().empty() && SrcM->getDataLayout() != DstM->getDataLayout()) errs() << "WARNING: Linking two modules of different data layouts!\n"; if (!SrcM->getTargetTriple().empty() && DstM->getTargetTriple() != SrcM->getTargetTriple()) { errs() << "WARNING: Linking two modules of different target triples: "; if (!SrcM->getModuleIdentifier().empty()) errs() << SrcM->getModuleIdentifier() << ": "; errs() << "'" << SrcM->getTargetTriple() << "' and '" << DstM->getTargetTriple() << "'\n"; } // Append the module inline asm string. if (!SrcM->getModuleInlineAsm().empty()) { if (DstM->getModuleInlineAsm().empty()) DstM->setModuleInlineAsm(SrcM->getModuleInlineAsm()); else DstM->setModuleInlineAsm(DstM->getModuleInlineAsm()+"\n"+ SrcM->getModuleInlineAsm()); } // Loop over all of the linked values to compute type mappings. computeTypeMapping(); // Insert all of the globals in src into the DstM module... without linking // initializers (which could refer to functions not yet mapped over). for (Module::global_iterator I = SrcM->global_begin(), E = SrcM->global_end(); I != E; ++I) if (linkGlobalProto(I)) return true; // Link the functions together between the two modules, without doing function // bodies... this just adds external function prototypes to the DstM // function... We do this so that when we begin processing function bodies, // all of the global values that may be referenced are available in our // ValueMap. for (Module::iterator I = SrcM->begin(), E = SrcM->end(); I != E; ++I) if (linkFunctionProto(I)) return true; // If there were any aliases, link them now. for (Module::alias_iterator I = SrcM->alias_begin(), E = SrcM->alias_end(); I != E; ++I) if (linkAliasProto(I)) return true; for (unsigned i = 0, e = AppendingVars.size(); i != e; ++i) linkAppendingVarInit(AppendingVars[i]); // Update the initializers in the DstM module now that all globals that may // be referenced are in DstM. linkGlobalInits(); // Link in the function bodies that are defined in the source module into // DstM. for (Module::iterator SF = SrcM->begin(), E = SrcM->end(); SF != E; ++SF) { // Skip if not linking from source. if (DoNotLinkFromSource.count(SF)) continue; // Skip if no body (function is external) or materialize. if (SF->isDeclaration()) { if (!SF->isMaterializable()) continue; if (SF->Materialize(&ErrorMsg)) return true; } linkFunctionBody(cast(ValueMap[SF]), SF); SF->Dematerialize(); } // Resolve all uses of aliases with aliasees. linkAliasBodies(); // Remap all of the named MDNodes in Src into the DstM module. We do this // after linking GlobalValues so that MDNodes that reference GlobalValues // are properly remapped. linkNamedMDNodes(); // Merge the module flags into the DstM module. if (linkModuleFlagsMetadata()) return true; // Process vector of lazily linked in functions. bool LinkedInAnyFunctions; do { LinkedInAnyFunctions = false; for(std::vector::iterator I = LazilyLinkFunctions.begin(), E = LazilyLinkFunctions.end(); I != E; ++I) { Function *SF = *I; if (!SF) continue; Function *DF = cast(ValueMap[SF]); // Materialize if necessary. if (SF->isDeclaration()) { if (!SF->isMaterializable()) continue; if (SF->Materialize(&ErrorMsg)) return true; } // Erase from vector *before* the function body is linked - linkFunctionBody could // invalidate I. LazilyLinkFunctions.erase(I); // Link in function body. linkFunctionBody(DF, SF); SF->Dematerialize(); // Set flag to indicate we may have more functions to lazily link in // since we linked in a function. LinkedInAnyFunctions = true; break; } } while (LinkedInAnyFunctions); // Now that all of the types from the source are used, resolve any structs // copied over to the dest that didn't exist there. TypeMap.linkDefinedTypeBodies(); return false; } Linker::Linker(Module *M) : Composite(M) { TypeFinder StructTypes; StructTypes.run(*M, true); IdentifiedStructTypes.insert(StructTypes.begin(), StructTypes.end()); } Linker::~Linker() { } bool Linker::linkInModule(Module *Src, unsigned Mode, std::string *ErrorMsg) { ModuleLinker TheLinker(Composite, IdentifiedStructTypes, Src, Mode); if (TheLinker.run()) { if (ErrorMsg) *ErrorMsg = TheLinker.ErrorMsg; return true; } return false; } //===----------------------------------------------------------------------===// // LinkModules entrypoint. //===----------------------------------------------------------------------===// /// LinkModules - This function links two modules together, with the resulting /// Dest module modified to be the composite of the two input modules. If an /// error occurs, true is returned and ErrorMsg (if not null) is set to indicate /// the problem. Upon failure, the Dest module could be in a modified state, /// and shouldn't be relied on to be consistent. bool Linker::LinkModules(Module *Dest, Module *Src, unsigned Mode, std::string *ErrorMsg) { Linker L(Dest); return L.linkInModule(Src, Mode, ErrorMsg); } //===----------------------------------------------------------------------===// // C API. //===----------------------------------------------------------------------===// LLVMBool LLVMLinkModules(LLVMModuleRef Dest, LLVMModuleRef Src, LLVMLinkerMode Mode, char **OutMessages) { std::string Messages; LLVMBool Result = Linker::LinkModules(unwrap(Dest), unwrap(Src), Mode, OutMessages? &Messages : 0); if (OutMessages) *OutMessages = strdup(Messages.c_str()); return Result; }