//===-- ARMAsmPrinter.h - Print machine code to an ARM .s file --*- C++ -*-===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // ARM Assembly printer class. // //===----------------------------------------------------------------------===// #ifndef ARMASMPRINTER_H #define ARMASMPRINTER_H #include "ARM.h" #include "ARMTargetMachine.h" #include "llvm/CodeGen/AsmPrinter.h" #include "llvm/Support/Compiler.h" namespace llvm { class MCOperand; namespace ARM { enum DW_ISA { DW_ISA_ARM_thumb = 1, DW_ISA_ARM_arm = 2 }; } class LLVM_LIBRARY_VISIBILITY ARMAsmPrinter : public AsmPrinter { /// Subtarget - Keep a pointer to the ARMSubtarget around so that we can /// make the right decision when printing asm code for different targets. const ARMSubtarget *Subtarget; /// AFI - Keep a pointer to ARMFunctionInfo for the current /// MachineFunction. ARMFunctionInfo *AFI; /// MCP - Keep a pointer to constantpool entries of the current /// MachineFunction. const MachineConstantPool *MCP; /// InConstantPool - Maintain state when emitting a sequence of constant /// pool entries so we can properly mark them as data regions. bool InConstantPool; public: explicit ARMAsmPrinter(TargetMachine &TM, MCStreamer &Streamer) : AsmPrinter(TM, Streamer), AFI(NULL), MCP(NULL), InConstantPool(false) { Subtarget = &TM.getSubtarget(); } virtual const char *getPassName() const { return "ARM Assembly Printer"; } void printOperand(const MachineInstr *MI, int OpNum, raw_ostream &O, const char *Modifier = 0); virtual bool PrintAsmOperand(const MachineInstr *MI, unsigned OpNum, unsigned AsmVariant, const char *ExtraCode, raw_ostream &O); virtual bool PrintAsmMemoryOperand(const MachineInstr *MI, unsigned OpNum, unsigned AsmVariant, const char *ExtraCode, raw_ostream &O); void EmitJumpTable(const MachineInstr *MI); void EmitJump2Table(const MachineInstr *MI); virtual void EmitInstruction(const MachineInstr *MI); bool runOnMachineFunction(MachineFunction &F); virtual void EmitConstantPool() {} // we emit constant pools customly! virtual void EmitFunctionBodyEnd(); virtual void EmitFunctionEntryLabel(); void EmitStartOfAsmFile(Module &M); void EmitEndOfAsmFile(Module &M); void EmitXXStructor(const Constant *CV); // lowerOperand - Convert a MachineOperand into the equivalent MCOperand. bool lowerOperand(const MachineOperand &MO, MCOperand &MCOp); private: // Helpers for EmitStartOfAsmFile() and EmitEndOfAsmFile() void emitAttributes(); // Helper for ELF .o only void emitARMAttributeSection(); // Generic helper used to emit e.g. ARMv5 mul pseudos void EmitPatchedInstruction(const MachineInstr *MI, unsigned TargetOpc); void EmitUnwindingInstruction(const MachineInstr *MI); // emitPseudoExpansionLowering - tblgen'erated. bool emitPseudoExpansionLowering(MCStreamer &OutStreamer, const MachineInstr *MI); public: void PrintDebugValueComment(const MachineInstr *MI, raw_ostream &OS); MachineLocation getDebugValueLocation(const MachineInstr *MI) const; /// EmitDwarfRegOp - Emit dwarf register operation. virtual void EmitDwarfRegOp(const MachineLocation &MLoc) const; virtual unsigned getISAEncoding() { // ARM/Darwin adds ISA to the DWARF info for each function. if (!Subtarget->isTargetDarwin()) return 0; return Subtarget->isThumb() ? ARM::DW_ISA_ARM_thumb : ARM::DW_ISA_ARM_arm; } MCOperand GetSymbolRef(const MachineOperand &MO, const MCSymbol *Symbol); MCSymbol *GetARMSetPICJumpTableLabel2(unsigned uid, unsigned uid2, const MachineBasicBlock *MBB) const; MCSymbol *GetARMJTIPICJumpTableLabel2(unsigned uid, unsigned uid2) const; MCSymbol *GetARMSJLJEHLabel(void) const; MCSymbol *GetARMGVSymbol(const GlobalValue *GV); /// EmitMachineConstantPoolValue - Print a machine constantpool value to /// the .s file. virtual void EmitMachineConstantPoolValue(MachineConstantPoolValue *MCPV); }; } // end namespace llvm #endif