//===- ConstantMerge.cpp - Merge duplicate global constants ---------------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file defines the interface to a pass that merges duplicate global // constants together into a single constant that is shared. This is useful // because some passes (ie TraceValues) insert a lot of string constants into // the program, regardless of whether or not an existing string is available. // // Algorithm: ConstantMerge is designed to build up a map of available constants // and eliminate duplicates when it is initialized. // //===----------------------------------------------------------------------===// #include "llvm/Transforms/IPO.h" #include "llvm/ADT/DenseMap.h" #include "llvm/ADT/PointerIntPair.h" #include "llvm/ADT/SmallPtrSet.h" #include "llvm/ADT/Statistic.h" #include "llvm/IR/Constants.h" #include "llvm/IR/DataLayout.h" #include "llvm/IR/DerivedTypes.h" #include "llvm/IR/Module.h" #include "llvm/IR/Operator.h" #include "llvm/Pass.h" using namespace llvm; #define DEBUG_TYPE "constmerge" STATISTIC(NumMerged, "Number of global constants merged"); namespace { struct ConstantMerge : public ModulePass { static char ID; // Pass identification, replacement for typeid ConstantMerge() : ModulePass(ID) { initializeConstantMergePass(*PassRegistry::getPassRegistry()); } // For this pass, process all of the globals in the module, eliminating // duplicate constants. bool runOnModule(Module &M) override; // Return true iff we can determine the alignment of this global variable. bool hasKnownAlignment(GlobalVariable *GV) const; // Return the alignment of the global, including converting the default // alignment to a concrete value. unsigned getAlignment(GlobalVariable *GV) const; const DataLayout *DL; }; } char ConstantMerge::ID = 0; INITIALIZE_PASS(ConstantMerge, "constmerge", "Merge Duplicate Global Constants", false, false) ModulePass *llvm::createConstantMergePass() { return new ConstantMerge(); } /// Find values that are marked as llvm.used. static void FindUsedValues(GlobalVariable *LLVMUsed, SmallPtrSet &UsedValues) { if (!LLVMUsed) return; ConstantArray *Inits = cast(LLVMUsed->getInitializer()); for (unsigned i = 0, e = Inits->getNumOperands(); i != e; ++i) { Value *Operand = Inits->getOperand(i)->stripPointerCastsNoFollowAliases(); GlobalValue *GV = cast(Operand); UsedValues.insert(GV); } } // True if A is better than B. static bool IsBetterCanonical(const GlobalVariable &A, const GlobalVariable &B) { if (!A.hasLocalLinkage() && B.hasLocalLinkage()) return true; if (A.hasLocalLinkage() && !B.hasLocalLinkage()) return false; return A.hasUnnamedAddr(); } bool ConstantMerge::hasKnownAlignment(GlobalVariable *GV) const { return DL || GV->getAlignment() != 0; } unsigned ConstantMerge::getAlignment(GlobalVariable *GV) const { unsigned Align = GV->getAlignment(); if (Align) return Align; if (DL) return DL->getPreferredAlignment(GV); return 0; } bool ConstantMerge::runOnModule(Module &M) { DataLayoutPass *DLP = getAnalysisIfAvailable(); DL = DLP ? &DLP->getDataLayout() : nullptr; // Find all the globals that are marked "used". These cannot be merged. SmallPtrSet UsedGlobals; FindUsedValues(M.getGlobalVariable("llvm.used"), UsedGlobals); FindUsedValues(M.getGlobalVariable("llvm.compiler.used"), UsedGlobals); // Map unique pairs to globals. We don't // want to merge globals of unknown alignment with those of explicit // alignment. If we have DataLayout, we always know the alignment. DenseMap, GlobalVariable*> CMap; // Replacements - This vector contains a list of replacements to perform. SmallVector, 32> Replacements; bool MadeChange = false; // Iterate constant merging while we are still making progress. Merging two // constants together may allow us to merge other constants together if the // second level constants have initializers which point to the globals that // were just merged. while (1) { // First: Find the canonical constants others will be merged with. for (Module::global_iterator GVI = M.global_begin(), E = M.global_end(); GVI != E; ) { GlobalVariable *GV = GVI++; // If this GV is dead, remove it. GV->removeDeadConstantUsers(); if (GV->use_empty() && GV->hasLocalLinkage()) { GV->eraseFromParent(); continue; } // Only process constants with initializers in the default address space. if (!GV->isConstant() || !GV->hasDefinitiveInitializer() || GV->getType()->getAddressSpace() != 0 || GV->hasSection() || // Don't touch values marked with attribute(used). UsedGlobals.count(GV)) continue; // This transformation is legal for weak ODR globals in the sense it // doesn't change semantics, but we really don't want to perform it // anyway; it's likely to pessimize code generation, and some tools // (like the Darwin linker in cases involving CFString) don't expect it. if (GV->isWeakForLinker()) continue; Constant *Init = GV->getInitializer(); // Check to see if the initializer is already known. PointerIntPair Pair(Init, hasKnownAlignment(GV)); GlobalVariable *&Slot = CMap[Pair]; // If this is the first constant we find or if the old one is local, // replace with the current one. If the current is externally visible // it cannot be replace, but can be the canonical constant we merge with. if (!Slot || IsBetterCanonical(*GV, *Slot)) Slot = GV; } // Second: identify all globals that can be merged together, filling in // the Replacements vector. We cannot do the replacement in this pass // because doing so may cause initializers of other globals to be rewritten, // invalidating the Constant* pointers in CMap. for (Module::global_iterator GVI = M.global_begin(), E = M.global_end(); GVI != E; ) { GlobalVariable *GV = GVI++; // Only process constants with initializers in the default address space. if (!GV->isConstant() || !GV->hasDefinitiveInitializer() || GV->getType()->getAddressSpace() != 0 || GV->hasSection() || // Don't touch values marked with attribute(used). UsedGlobals.count(GV)) continue; // We can only replace constant with local linkage. if (!GV->hasLocalLinkage()) continue; Constant *Init = GV->getInitializer(); // Check to see if the initializer is already known. PointerIntPair Pair(Init, hasKnownAlignment(GV)); GlobalVariable *Slot = CMap[Pair]; if (!Slot || Slot == GV) continue; if (!Slot->hasUnnamedAddr() && !GV->hasUnnamedAddr()) continue; if (!GV->hasUnnamedAddr()) Slot->setUnnamedAddr(false); // Make all uses of the duplicate constant use the canonical version. Replacements.push_back(std::make_pair(GV, Slot)); } if (Replacements.empty()) return MadeChange; CMap.clear(); // Now that we have figured out which replacements must be made, do them all // now. This avoid invalidating the pointers in CMap, which are unneeded // now. for (unsigned i = 0, e = Replacements.size(); i != e; ++i) { // Bump the alignment if necessary. if (Replacements[i].first->getAlignment() || Replacements[i].second->getAlignment()) { Replacements[i].second->setAlignment( std::max(getAlignment(Replacements[i].first), getAlignment(Replacements[i].second))); } // Eliminate any uses of the dead global. Replacements[i].first->replaceAllUsesWith(Replacements[i].second); // Delete the global value from the module. assert(Replacements[i].first->hasLocalLinkage() && "Refusing to delete an externally visible global variable."); Replacements[i].first->eraseFromParent(); } NumMerged += Replacements.size(); Replacements.clear(); } }