; RUN: llc < %s -mtriple=x86_64-apple-macosx | FileCheck %s ; This is supposed to be testing BranchFolding's common ; code hoisting logic, but has been erroneously passing due ; to there being a redundant xorl in the entry block ; and no common code to hoist. ; However, now that MachineSink sinks the redundant xor ; hoist-common looks at it and rejects it for hoisting, ; which causes this test to fail. ; Since it seems this test is broken, marking XFAIL for now ; until someone decides to remove it or fix what it tests. ; XFAIL: * ; Common "xorb al, al" instruction in the two successor blocks should be ; moved to the entry block above the test + je. ; rdar://9145558 define zeroext i1 @t(i32 %c) nounwind ssp { entry: ; CHECK-LABEL: t: ; CHECK: xorl %eax, %eax ; CHECK: test ; CHECK: je %tobool = icmp eq i32 %c, 0 br i1 %tobool, label %return, label %if.then if.then: ; CHECK: callq %call = tail call zeroext i1 (...)* @foo() nounwind br label %return return: ; CHECK: ret %retval.0 = phi i1 [ %call, %if.then ], [ false, %entry ] ret i1 %retval.0 } declare zeroext i1 @foo(...)