//===-- COFFDump.cpp - COFF-specific dumper ---------------------*- C++ -*-===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// /// /// \file /// \brief This file implements the COFF-specific dumper for llvm-objdump. /// It outputs the Win64 EH data structures as plain text. /// The encoding of the unwind codes is described in MSDN: /// http://msdn.microsoft.com/en-us/library/ck9asaa9.aspx /// //===----------------------------------------------------------------------===// #include "llvm-objdump.h" #include "llvm/Object/COFF.h" #include "llvm/Object/ObjectFile.h" #include "llvm/Support/Format.h" #include "llvm/Support/SourceMgr.h" #include "llvm/Support/Win64EH.h" #include "llvm/Support/raw_ostream.h" #include "llvm/Support/system_error.h" #include #include using namespace llvm; using namespace object; using namespace llvm::Win64EH; // Returns the name of the unwind code. static StringRef getUnwindCodeTypeName(uint8_t Code) { switch(Code) { default: llvm_unreachable("Invalid unwind code"); case UOP_PushNonVol: return "UOP_PushNonVol"; case UOP_AllocLarge: return "UOP_AllocLarge"; case UOP_AllocSmall: return "UOP_AllocSmall"; case UOP_SetFPReg: return "UOP_SetFPReg"; case UOP_SaveNonVol: return "UOP_SaveNonVol"; case UOP_SaveNonVolBig: return "UOP_SaveNonVolBig"; case UOP_SaveXMM128: return "UOP_SaveXMM128"; case UOP_SaveXMM128Big: return "UOP_SaveXMM128Big"; case UOP_PushMachFrame: return "UOP_PushMachFrame"; } } // Returns the name of a referenced register. static StringRef getUnwindRegisterName(uint8_t Reg) { switch(Reg) { default: llvm_unreachable("Invalid register"); case 0: return "RAX"; case 1: return "RCX"; case 2: return "RDX"; case 3: return "RBX"; case 4: return "RSP"; case 5: return "RBP"; case 6: return "RSI"; case 7: return "RDI"; case 8: return "R8"; case 9: return "R9"; case 10: return "R10"; case 11: return "R11"; case 12: return "R12"; case 13: return "R13"; case 14: return "R14"; case 15: return "R15"; } } // Calculates the number of array slots required for the unwind code. static unsigned getNumUsedSlots(const UnwindCode &UnwindCode) { switch (UnwindCode.getUnwindOp()) { default: llvm_unreachable("Invalid unwind code"); case UOP_PushNonVol: case UOP_AllocSmall: case UOP_SetFPReg: case UOP_PushMachFrame: return 1; case UOP_SaveNonVol: case UOP_SaveXMM128: return 2; case UOP_SaveNonVolBig: case UOP_SaveXMM128Big: return 3; case UOP_AllocLarge: return (UnwindCode.getOpInfo() == 0) ? 2 : 3; } } // Prints one unwind code. Because an unwind code can occupy up to 3 slots in // the unwind codes array, this function requires that the correct number of // slots is provided. static void printUnwindCode(ArrayRef UCs) { assert(UCs.size() >= getNumUsedSlots(UCs[0])); outs() << format(" 0x%02x: ", unsigned(UCs[0].u.CodeOffset)) << getUnwindCodeTypeName(UCs[0].getUnwindOp()); switch (UCs[0].getUnwindOp()) { case UOP_PushNonVol: outs() << " " << getUnwindRegisterName(UCs[0].getOpInfo()); break; case UOP_AllocLarge: if (UCs[0].getOpInfo() == 0) { outs() << " " << UCs[1].FrameOffset; } else { outs() << " " << UCs[1].FrameOffset + (static_cast(UCs[2].FrameOffset) << 16); } break; case UOP_AllocSmall: outs() << " " << ((UCs[0].getOpInfo() + 1) * 8); break; case UOP_SetFPReg: outs() << " "; break; case UOP_SaveNonVol: outs() << " " << getUnwindRegisterName(UCs[0].getOpInfo()) << format(" [0x%04x]", 8 * UCs[1].FrameOffset); break; case UOP_SaveNonVolBig: outs() << " " << getUnwindRegisterName(UCs[0].getOpInfo()) << format(" [0x%08x]", UCs[1].FrameOffset + (static_cast(UCs[2].FrameOffset) << 16)); break; case UOP_SaveXMM128: outs() << " XMM" << static_cast(UCs[0].getOpInfo()) << format(" [0x%04x]", 16 * UCs[1].FrameOffset); break; case UOP_SaveXMM128Big: outs() << " XMM" << UCs[0].getOpInfo() << format(" [0x%08x]", UCs[1].FrameOffset + (static_cast(UCs[2].FrameOffset) << 16)); break; case UOP_PushMachFrame: outs() << " " << (UCs[0].getOpInfo() ? "w/o" : "w") << " error code"; break; } outs() << "\n"; } static void printAllUnwindCodes(ArrayRef UCs) { for (const UnwindCode *I = UCs.begin(), *E = UCs.end(); I < E; ) { unsigned UsedSlots = getNumUsedSlots(*I); if (UsedSlots > UCs.size()) { outs() << "Unwind data corrupted: Encountered unwind op " << getUnwindCodeTypeName((*I).getUnwindOp()) << " which requires " << UsedSlots << " slots, but only " << UCs.size() << " remaining in buffer"; return ; } printUnwindCode(ArrayRef(I, E)); I += UsedSlots; } } // Given a symbol sym this functions returns the address and section of it. static error_code resolveSectionAndAddress(const COFFObjectFile *Obj, const SymbolRef &Sym, const coff_section *&ResolvedSection, uint64_t &ResolvedAddr) { if (error_code EC = Sym.getAddress(ResolvedAddr)) return EC; section_iterator iter(Obj->section_begin()); if (error_code EC = Sym.getSection(iter)) return EC; ResolvedSection = Obj->getCOFFSection(iter); return object_error::success; } // Given a vector of relocations for a section and an offset into this section // the function returns the symbol used for the relocation at the offset. static error_code resolveSymbol(const std::vector &Rels, uint64_t Offset, SymbolRef &Sym) { for (std::vector::const_iterator I = Rels.begin(), E = Rels.end(); I != E; ++I) { uint64_t Ofs; if (error_code EC = I->getOffset(Ofs)) return EC; if (Ofs == Offset) { Sym = *I->getSymbol(); break; } } return object_error::success; } // Given a vector of relocations for a section and an offset into this section // the function resolves the symbol used for the relocation at the offset and // returns the section content and the address inside the content pointed to // by the symbol. static error_code getSectionContents(const COFFObjectFile *Obj, const std::vector &Rels, uint64_t Offset, ArrayRef &Contents, uint64_t &Addr) { SymbolRef Sym; if (error_code ec = resolveSymbol(Rels, Offset, Sym)) return ec; const coff_section *Section; if (error_code EC = resolveSectionAndAddress(Obj, Sym, Section, Addr)) return EC; if (error_code EC = Obj->getSectionContents(Section, Contents)) return EC; return object_error::success; } // Given a vector of relocations for a section and an offset into this section // the function returns the name of the symbol used for the relocation at the // offset. static error_code resolveSymbolName(const std::vector &Rels, uint64_t Offset, StringRef &Name) { SymbolRef Sym; if (error_code EC = resolveSymbol(Rels, Offset, Sym)) return EC; if (error_code EC = Sym.getName(Name)) return EC; return object_error::success; } static void printCOFFSymbolAddress(llvm::raw_ostream &Out, const std::vector &Rels, uint64_t Offset, uint32_t Disp) { StringRef Sym; if (error_code EC = resolveSymbolName(Rels, Offset, Sym)) { error(EC); return ; } Out << Sym; if (Disp > 0) Out << format(" + 0x%04x", Disp); } static void printSEHTable(const COFFObjectFile *Obj, uint32_t TableVA, int Count) { if (Count == 0) return; const pe32_header *PE32Header; if (error(Obj->getPE32Header(PE32Header))) return; uint32_t ImageBase = PE32Header->ImageBase; uintptr_t IntPtr = 0; if (error(Obj->getVaPtr(TableVA, IntPtr))) return; const support::ulittle32_t *P = (const support::ulittle32_t *)IntPtr; outs() << "SEH Table:"; for (int I = 0; I < Count; ++I) outs() << format(" 0x%x", P[I] + ImageBase); outs() << "\n\n"; } static void printLoadConfiguration(const COFFObjectFile *Obj) { const coff_file_header *Header; if (error(Obj->getCOFFHeader(Header))) return; // Currently only x86 is supported if (Header->Machine != COFF::IMAGE_FILE_MACHINE_I386) return; const data_directory *DataDir; if (error(Obj->getDataDirectory(COFF::LOAD_CONFIG_TABLE, DataDir))) return; uintptr_t IntPtr = 0; if (DataDir->RelativeVirtualAddress == 0) return; if (error(Obj->getRvaPtr(DataDir->RelativeVirtualAddress, IntPtr))) return; const coff_load_configuration32 *LoadConf = reinterpret_cast(IntPtr); outs() << "Load configuration:" << "\n Timestamp: " << LoadConf->TimeDateStamp << "\n Major Version: " << LoadConf->MajorVersion << "\n Minor Version: " << LoadConf->MinorVersion << "\n GlobalFlags Clear: " << LoadConf->GlobalFlagsClear << "\n GlobalFlags Set: " << LoadConf->GlobalFlagsSet << "\n Critical Section Default Timeout: " << LoadConf->CriticalSectionDefaultTimeout << "\n Decommit Free Block Threshold: " << LoadConf->DeCommitFreeBlockThreshold << "\n Decommit Total Free Threshold: " << LoadConf->DeCommitTotalFreeThreshold << "\n Lock Prefix Table: " << LoadConf->LockPrefixTable << "\n Maximum Allocation Size: " << LoadConf->MaximumAllocationSize << "\n Virtual Memory Threshold: " << LoadConf->VirtualMemoryThreshold << "\n Process Affinity Mask: " << LoadConf->ProcessAffinityMask << "\n Process Heap Flags: " << LoadConf->ProcessHeapFlags << "\n CSD Version: " << LoadConf->CSDVersion << "\n Security Cookie: " << LoadConf->SecurityCookie << "\n SEH Table: " << LoadConf->SEHandlerTable << "\n SEH Count: " << LoadConf->SEHandlerCount << "\n\n"; printSEHTable(Obj, LoadConf->SEHandlerTable, LoadConf->SEHandlerCount); outs() << "\n"; } // Prints import tables. The import table is a table containing the list of // DLL name and symbol names which will be linked by the loader. static void printImportTables(const COFFObjectFile *Obj) { import_directory_iterator I = Obj->import_directory_begin(); import_directory_iterator E = Obj->import_directory_end(); if (I == E) return; outs() << "The Import Tables:\n"; for (; I != E; I = ++I) { const import_directory_table_entry *Dir; StringRef Name; if (I->getImportTableEntry(Dir)) return; if (I->getName(Name)) return; outs() << format(" lookup %08x time %08x fwd %08x name %08x addr %08x\n\n", static_cast(Dir->ImportLookupTableRVA), static_cast(Dir->TimeDateStamp), static_cast(Dir->ForwarderChain), static_cast(Dir->NameRVA), static_cast(Dir->ImportAddressTableRVA)); outs() << " DLL Name: " << Name << "\n"; outs() << " Hint/Ord Name\n"; const import_lookup_table_entry32 *entry; if (I->getImportLookupEntry(entry)) return; for (; entry->data; ++entry) { if (entry->isOrdinal()) { outs() << format(" % 6d\n", entry->getOrdinal()); continue; } uint16_t Hint; StringRef Name; if (Obj->getHintName(entry->getHintNameRVA(), Hint, Name)) return; outs() << format(" % 6d ", Hint) << Name << "\n"; } outs() << "\n"; } } // Prints export tables. The export table is a table containing the list of // exported symbol from the DLL. static void printExportTable(const COFFObjectFile *Obj) { outs() << "Export Table:\n"; export_directory_iterator I = Obj->export_directory_begin(); export_directory_iterator E = Obj->export_directory_end(); if (I == E) return; StringRef DllName; uint32_t OrdinalBase; if (I->getDllName(DllName)) return; if (I->getOrdinalBase(OrdinalBase)) return; outs() << " DLL name: " << DllName << "\n"; outs() << " Ordinal base: " << OrdinalBase << "\n"; outs() << " Ordinal RVA Name\n"; for (; I != E; I = ++I) { uint32_t Ordinal; if (I->getOrdinal(Ordinal)) return; uint32_t RVA; if (I->getExportRVA(RVA)) return; outs() << format(" % 4d %# 8x", Ordinal, RVA); StringRef Name; if (I->getSymbolName(Name)) continue; if (!Name.empty()) outs() << " " << Name; outs() << "\n"; } } void llvm::printCOFFUnwindInfo(const COFFObjectFile *Obj) { const coff_file_header *Header; if (error(Obj->getCOFFHeader(Header))) return; if (Header->Machine != COFF::IMAGE_FILE_MACHINE_AMD64) { errs() << "Unsupported image machine type " "(currently only AMD64 is supported).\n"; return; } const coff_section *Pdata = 0; for (section_iterator SI = Obj->section_begin(), SE = Obj->section_end(); SI != SE; ++SI) { StringRef Name; if (error(SI->getName(Name))) continue; if (Name != ".pdata") continue; Pdata = Obj->getCOFFSection(SI); std::vector Rels; for (relocation_iterator RI = SI->relocation_begin(), RE = SI->relocation_end(); RI != RE; ++RI) Rels.push_back(*RI); // Sort relocations by address. std::sort(Rels.begin(), Rels.end(), RelocAddressLess); ArrayRef Contents; if (error(Obj->getSectionContents(Pdata, Contents))) continue; if (Contents.empty()) continue; ArrayRef RFs( reinterpret_cast(Contents.data()), Contents.size() / sizeof(RuntimeFunction)); for (const RuntimeFunction *I = RFs.begin(), *E = RFs.end(); I < E; ++I) { const uint64_t SectionOffset = std::distance(RFs.begin(), I) * sizeof(RuntimeFunction); outs() << "Function Table:\n"; outs() << " Start Address: "; printCOFFSymbolAddress(outs(), Rels, SectionOffset + /*offsetof(RuntimeFunction, StartAddress)*/ 0, I->StartAddress); outs() << "\n"; outs() << " End Address: "; printCOFFSymbolAddress(outs(), Rels, SectionOffset + /*offsetof(RuntimeFunction, EndAddress)*/ 4, I->EndAddress); outs() << "\n"; outs() << " Unwind Info Address: "; printCOFFSymbolAddress(outs(), Rels, SectionOffset + /*offsetof(RuntimeFunction, UnwindInfoOffset)*/ 8, I->UnwindInfoOffset); outs() << "\n"; ArrayRef XContents; uint64_t UnwindInfoOffset = 0; if (error(getSectionContents(Obj, Rels, SectionOffset + /*offsetof(RuntimeFunction, UnwindInfoOffset)*/ 8, XContents, UnwindInfoOffset))) continue; if (XContents.empty()) continue; UnwindInfoOffset += I->UnwindInfoOffset; if (UnwindInfoOffset > XContents.size()) continue; const Win64EH::UnwindInfo *UI = reinterpret_cast (XContents.data() + UnwindInfoOffset); // The casts to int are required in order to output the value as number. // Without the casts the value would be interpreted as char data (which // results in garbage output). outs() << " Version: " << static_cast(UI->getVersion()) << "\n"; outs() << " Flags: " << static_cast(UI->getFlags()); if (UI->getFlags()) { if (UI->getFlags() & UNW_ExceptionHandler) outs() << " UNW_ExceptionHandler"; if (UI->getFlags() & UNW_TerminateHandler) outs() << " UNW_TerminateHandler"; if (UI->getFlags() & UNW_ChainInfo) outs() << " UNW_ChainInfo"; } outs() << "\n"; outs() << " Size of prolog: " << static_cast(UI->PrologSize) << "\n"; outs() << " Number of Codes: " << static_cast(UI->NumCodes) << "\n"; // Maybe this should move to output of UOP_SetFPReg? if (UI->getFrameRegister()) { outs() << " Frame register: " << getUnwindRegisterName(UI->getFrameRegister()) << "\n"; outs() << " Frame offset: " << 16 * UI->getFrameOffset() << "\n"; } else { outs() << " No frame pointer used\n"; } if (UI->getFlags() & (UNW_ExceptionHandler | UNW_TerminateHandler)) { // FIXME: Output exception handler data } else if (UI->getFlags() & UNW_ChainInfo) { // FIXME: Output chained unwind info } if (UI->NumCodes) outs() << " Unwind Codes:\n"; printAllUnwindCodes(ArrayRef(&UI->UnwindCodes[0], UI->NumCodes)); outs() << "\n\n"; outs().flush(); } } } void llvm::printCOFFFileHeader(const object::ObjectFile *Obj) { const COFFObjectFile *file = dyn_cast(Obj); printLoadConfiguration(file); printImportTables(file); printExportTable(file); }