//===- FileCheck.cpp - Check that File's Contents match what is expected --===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // FileCheck does a line-by line check of a file that validates whether it // contains the expected content. This is useful for regression tests etc. // // This program exits with an error status of 2 on error, exit status of 0 if // the file matched the expected contents, and exit status of 1 if it did not // contain the expected contents. // //===----------------------------------------------------------------------===// #include "llvm/Support/CommandLine.h" #include "llvm/Support/MemoryBuffer.h" #include "llvm/Support/PrettyStackTrace.h" #include "llvm/Support/Regex.h" #include "llvm/Support/SourceMgr.h" #include "llvm/Support/raw_ostream.h" #include "llvm/System/Signals.h" using namespace llvm; static cl::opt CheckFilename(cl::Positional, cl::desc(""), cl::Required); static cl::opt InputFilename("input-file", cl::desc("File to check (defaults to stdin)"), cl::init("-"), cl::value_desc("filename")); static cl::opt CheckPrefix("check-prefix", cl::init("CHECK"), cl::desc("Prefix to use from check file (defaults to 'CHECK')")); static cl::opt NoCanonicalizeWhiteSpace("strict-whitespace", cl::desc("Do not treat all horizontal whitespace as equivalent")); //===----------------------------------------------------------------------===// // Pattern Handling Code. //===----------------------------------------------------------------------===// class Pattern { /// FixedStr - If non-empty, this pattern is a fixed string match with the /// specified fixed string. StringRef FixedStr; /// RegEx - If non-empty, this is a regex pattern. std::string RegExStr; public: Pattern() { } bool ParsePattern(StringRef PatternStr, SourceMgr &SM); /// Match - Match the pattern string against the input buffer Buffer. This /// returns the position that is matched or npos if there is no match. If /// there is a match, the size of the matched string is returned in MatchLen. size_t Match(StringRef Buffer, size_t &MatchLen) const; private: void AddFixedStringToRegEx(StringRef FixedStr); }; bool Pattern::ParsePattern(StringRef PatternStr, SourceMgr &SM) { // Ignore trailing whitespace. while (!PatternStr.empty() && (PatternStr.back() == ' ' || PatternStr.back() == '\t')) PatternStr = PatternStr.substr(0, PatternStr.size()-1); // Check that there is something on the line. if (PatternStr.empty()) { SM.PrintMessage(SMLoc::getFromPointer(PatternStr.data()), "found empty check string with prefix '"+CheckPrefix+":'", "error"); return true; } // Check to see if this is a fixed string, or if it has regex pieces. if (PatternStr.size() < 2 || PatternStr.find("{{") == StringRef::npos) { FixedStr = PatternStr; return false; } // Otherwise, there is at least one regex piece. Build up the regex pattern // by escaping scary characters in fixed strings, building up one big regex. while (!PatternStr.empty()) { // Handle fixed string matches. if (PatternStr.size() < 2 || PatternStr[0] != '{' || PatternStr[1] != '{') { // Find the end, which is the start of the next regex. size_t FixedMatchEnd = PatternStr.find("{{"); AddFixedStringToRegEx(PatternStr.substr(0, FixedMatchEnd)); PatternStr = PatternStr.substr(FixedMatchEnd); continue; } // Otherwise, this is the start of a regex match. Scan for the }}. size_t End = PatternStr.find("}}"); if (End == StringRef::npos) { SM.PrintMessage(SMLoc::getFromPointer(PatternStr.data()), "found start of regex string with no end '}}'", "error"); return true; } StringRef RegexStr = PatternStr.substr(2, End-2); Regex R(RegexStr); std::string Error; if (!R.isValid(Error)) { SM.PrintMessage(SMLoc::getFromPointer(PatternStr.data()+2), "invalid regex: " + Error, "error"); return true; } RegExStr += RegexStr.str(); PatternStr = PatternStr.substr(End+2); } return false; } void Pattern::AddFixedStringToRegEx(StringRef FixedStr) { // Add the characters from FixedStr to the regex, escaping as needed. This // avoids "leaning toothpicks" in common patterns. for (unsigned i = 0, e = FixedStr.size(); i != e; ++i) { switch (FixedStr[i]) { // These are the special characters matched in "p_ere_exp". case '(': case ')': case '^': case '$': case '|': case '*': case '+': case '?': case '.': case '[': case '\\': case '{': RegExStr += '\\'; // FALL THROUGH. default: RegExStr += FixedStr[i]; break; } } } /// Match - Match the pattern string against the input buffer Buffer. This /// returns the position that is matched or npos if there is no match. If /// there is a match, the size of the matched string is returned in MatchLen. size_t Pattern::Match(StringRef Buffer, size_t &MatchLen) const { // If this is a fixed string pattern, just match it now. if (!FixedStr.empty()) { MatchLen = FixedStr.size(); return Buffer.find(FixedStr); } // Regex match. SmallVector MatchInfo; if (!Regex(RegExStr, Regex::Sub|Regex::Newline).match(Buffer, &MatchInfo)) return StringRef::npos; // Successful regex match. assert(!MatchInfo.empty() && "Didn't get any match"); StringRef FullMatch = MatchInfo[0]; MatchLen = FullMatch.size(); return FullMatch.data()-Buffer.data(); } //===----------------------------------------------------------------------===// // Check Strings. //===----------------------------------------------------------------------===// /// CheckString - This is a check that we found in the input file. struct CheckString { /// Pat - The pattern to match. Pattern Pat; /// Loc - The location in the match file that the check string was specified. SMLoc Loc; /// IsCheckNext - This is true if this is a CHECK-NEXT: directive (as opposed /// to a CHECK: directive. bool IsCheckNext; /// NotStrings - These are all of the strings that are disallowed from /// occurring between this match string and the previous one (or start of /// file). std::vector > NotStrings; CheckString(const Pattern &P, SMLoc L, bool isCheckNext) : Pat(P), Loc(L), IsCheckNext(isCheckNext) {} }; /// CanonicalizeInputFile - Remove duplicate horizontal space from the specified /// memory buffer, free it, and return a new one. static MemoryBuffer *CanonicalizeInputFile(MemoryBuffer *MB) { SmallVector NewFile; NewFile.reserve(MB->getBufferSize()); for (const char *Ptr = MB->getBufferStart(), *End = MB->getBufferEnd(); Ptr != End; ++Ptr) { // If C is not a horizontal whitespace, skip it. if (*Ptr != ' ' && *Ptr != '\t') { NewFile.push_back(*Ptr); continue; } // Otherwise, add one space and advance over neighboring space. NewFile.push_back(' '); while (Ptr+1 != End && (Ptr[1] == ' ' || Ptr[1] == '\t')) ++Ptr; } // Free the old buffer and return a new one. MemoryBuffer *MB2 = MemoryBuffer::getMemBufferCopy(NewFile.data(), NewFile.data() + NewFile.size(), MB->getBufferIdentifier()); delete MB; return MB2; } /// ReadCheckFile - Read the check file, which specifies the sequence of /// expected strings. The strings are added to the CheckStrings vector. static bool ReadCheckFile(SourceMgr &SM, std::vector &CheckStrings) { // Open the check file, and tell SourceMgr about it. std::string ErrorStr; MemoryBuffer *F = MemoryBuffer::getFileOrSTDIN(CheckFilename.c_str(), &ErrorStr); if (F == 0) { errs() << "Could not open check file '" << CheckFilename << "': " << ErrorStr << '\n'; return true; } // If we want to canonicalize whitespace, strip excess whitespace from the // buffer containing the CHECK lines. if (!NoCanonicalizeWhiteSpace) F = CanonicalizeInputFile(F); SM.AddNewSourceBuffer(F, SMLoc()); // Find all instances of CheckPrefix followed by : in the file. StringRef Buffer = F->getBuffer(); std::vector > NotMatches; while (1) { // See if Prefix occurs in the memory buffer. Buffer = Buffer.substr(Buffer.find(CheckPrefix)); // If we didn't find a match, we're done. if (Buffer.empty()) break; const char *CheckPrefixStart = Buffer.data(); // When we find a check prefix, keep track of whether we find CHECK: or // CHECK-NEXT: bool IsCheckNext = false, IsCheckNot = false; // Verify that the : is present after the prefix. if (Buffer[CheckPrefix.size()] == ':') { Buffer = Buffer.substr(CheckPrefix.size()+1); } else if (Buffer.size() > CheckPrefix.size()+6 && memcmp(Buffer.data()+CheckPrefix.size(), "-NEXT:", 6) == 0) { Buffer = Buffer.substr(CheckPrefix.size()+7); IsCheckNext = true; } else if (Buffer.size() > CheckPrefix.size()+5 && memcmp(Buffer.data()+CheckPrefix.size(), "-NOT:", 5) == 0) { Buffer = Buffer.substr(CheckPrefix.size()+6); IsCheckNot = true; } else { Buffer = Buffer.substr(1); continue; } // Okay, we found the prefix, yay. Remember the rest of the line, but // ignore leading and trailing whitespace. Buffer = Buffer.substr(Buffer.find_first_not_of(" \t")); // Scan ahead to the end of line. size_t EOL = Buffer.find_first_of("\n\r"); // Parse the pattern. Pattern P; if (P.ParsePattern(Buffer.substr(0, EOL), SM)) return true; Buffer = Buffer.substr(EOL); // Verify that CHECK-NEXT lines have at least one CHECK line before them. if (IsCheckNext && CheckStrings.empty()) { SM.PrintMessage(SMLoc::getFromPointer(CheckPrefixStart), "found '"+CheckPrefix+"-NEXT:' without previous '"+ CheckPrefix+ ": line", "error"); return true; } // Handle CHECK-NOT. if (IsCheckNot) { NotMatches.push_back(std::make_pair(SMLoc::getFromPointer(Buffer.data()), P)); continue; } // Okay, add the string we captured to the output vector and move on. CheckStrings.push_back(CheckString(P, SMLoc::getFromPointer(Buffer.data()), IsCheckNext)); std::swap(NotMatches, CheckStrings.back().NotStrings); } if (CheckStrings.empty()) { errs() << "error: no check strings found with prefix '" << CheckPrefix << ":'\n"; return true; } if (!NotMatches.empty()) { errs() << "error: '" << CheckPrefix << "-NOT:' not supported after last check line.\n"; return true; } return false; } static void PrintCheckFailed(const SourceMgr &SM, const CheckString &CheckStr, StringRef Buffer) { // Otherwise, we have an error, emit an error message. SM.PrintMessage(CheckStr.Loc, "expected string not found in input", "error"); // Print the "scanning from here" line. If the current position is at the // end of a line, advance to the start of the next line. Buffer = Buffer.substr(Buffer.find_first_not_of(" \t\n\r")); SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), "scanning from here", "note"); } /// CountNumNewlinesBetween - Count the number of newlines in the specified /// range. static unsigned CountNumNewlinesBetween(StringRef Range) { unsigned NumNewLines = 0; while (1) { // Scan for newline. Range = Range.substr(Range.find_first_of("\n\r")); if (Range.empty()) return NumNewLines; ++NumNewLines; // Handle \n\r and \r\n as a single newline. if (Range.size() > 1 && (Range[1] == '\n' || Range[1] == '\r') && (Range[0] != Range[1])) Range = Range.substr(1); Range = Range.substr(1); } } int main(int argc, char **argv) { sys::PrintStackTraceOnErrorSignal(); PrettyStackTraceProgram X(argc, argv); cl::ParseCommandLineOptions(argc, argv); SourceMgr SM; // Read the expected strings from the check file. std::vector CheckStrings; if (ReadCheckFile(SM, CheckStrings)) return 2; // Open the file to check and add it to SourceMgr. std::string ErrorStr; MemoryBuffer *F = MemoryBuffer::getFileOrSTDIN(InputFilename.c_str(), &ErrorStr); if (F == 0) { errs() << "Could not open input file '" << InputFilename << "': " << ErrorStr << '\n'; return true; } // Remove duplicate spaces in the input file if requested. if (!NoCanonicalizeWhiteSpace) F = CanonicalizeInputFile(F); SM.AddNewSourceBuffer(F, SMLoc()); // Check that we have all of the expected strings, in order, in the input // file. StringRef Buffer = F->getBuffer(); const char *LastMatch = Buffer.data(); for (unsigned StrNo = 0, e = CheckStrings.size(); StrNo != e; ++StrNo) { const CheckString &CheckStr = CheckStrings[StrNo]; StringRef SearchFrom = Buffer; // Find StrNo in the file. size_t MatchLen = 0; Buffer = Buffer.substr(CheckStr.Pat.Match(Buffer, MatchLen)); // If we didn't find a match, reject the input. if (Buffer.empty()) { PrintCheckFailed(SM, CheckStr, SearchFrom); return 1; } StringRef SkippedRegion(LastMatch, Buffer.data()-LastMatch); // If this check is a "CHECK-NEXT", verify that the previous match was on // the previous line (i.e. that there is one newline between them). if (CheckStr.IsCheckNext) { // Count the number of newlines between the previous match and this one. assert(LastMatch != F->getBufferStart() && "CHECK-NEXT can't be the first check in a file"); unsigned NumNewLines = CountNumNewlinesBetween(SkippedRegion); if (NumNewLines == 0) { SM.PrintMessage(CheckStr.Loc, CheckPrefix+"-NEXT: is on the same line as previous match", "error"); SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), "'next' match was here", "note"); SM.PrintMessage(SMLoc::getFromPointer(LastMatch), "previous match was here", "note"); return 1; } if (NumNewLines != 1) { SM.PrintMessage(CheckStr.Loc, CheckPrefix+ "-NEXT: is not on the line after the previous match", "error"); SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), "'next' match was here", "note"); SM.PrintMessage(SMLoc::getFromPointer(LastMatch), "previous match was here", "note"); return 1; } } // If this match had "not strings", verify that they don't exist in the // skipped region. for (unsigned ChunkNo = 0, e = CheckStr.NotStrings.size(); ChunkNo != e; ++ChunkNo) { size_t MatchLen = 0; size_t Pos = CheckStr.NotStrings[ChunkNo].second.Match(SkippedRegion, MatchLen); if (Pos == StringRef::npos) continue; SM.PrintMessage(SMLoc::getFromPointer(LastMatch+Pos), CheckPrefix+"-NOT: string occurred!", "error"); SM.PrintMessage(CheckStr.NotStrings[ChunkNo].first, CheckPrefix+"-NOT: pattern specified here", "note"); return 1; } // Otherwise, everything is good. Step over the matched text and remember // the position after the match as the end of the last match. Buffer = Buffer.substr(MatchLen); LastMatch = Buffer.data(); } return 0; }