diff --git a/CMakeLists.txt b/CMakeLists.txt
index 13e358a4619905cae95b45cc6e520173f6c9747a..27010d2c5321c4261423ba9e39642e89f5710f8c 100644 (file)
--- a/CMakeLists.txt
+++ b/CMakeLists.txt
"${CMAKE_CURRENT_SOURCE_DIR}/cmake/modules"
)
-set(PACKAGE_VERSION "3.1svn")
+set(LLVM_VERSION_MAJOR 3)
+set(LLVM_VERSION_MINOR 4)
-set_property(GLOBAL PROPERTY USE_FOLDERS ON)
+set(PACKAGE_VERSION "${LLVM_VERSION_MAJOR}.${LLVM_VERSION_MINOR}svn")
+
+option(LLVM_USE_FOLDERS "Enable solution folders in Visual Studio. Disable for Express versions." ON)
+if ( LLVM_USE_FOLDERS )
+ set_property(GLOBAL PROPERTY USE_FOLDERS ON)
+endif()
include(VersionFromVCS)
set(LLVM_LIBDIR_SUFFIX "" CACHE STRING "Define suffix of library directory name (32/64)" )
set(LLVM_ALL_TARGETS
+ AArch64
ARM
- CBackend
- CellSPU
CppBackend
Hexagon
Mips
- MBlaze
MSP430
+ NVPTX
PowerPC
- PTX
+ R600
Sparc
+ SystemZ
X86
XCore
)
# List of targets with JIT support:
-set(LLVM_TARGETS_WITH_JIT X86 PowerPC ARM Mips)
+set(LLVM_TARGETS_WITH_JIT X86 PowerPC AArch64 ARM Mips SystemZ)
-if( MSVC )
- set(LLVM_TARGETS_TO_BUILD X86
+set(LLVM_TARGETS_TO_BUILD "all"
CACHE STRING "Semicolon-separated list of targets to build, or \"all\".")
-else( MSVC )
- set(LLVM_TARGETS_TO_BUILD "all"
- CACHE STRING "Semicolon-separated list of targets to build, or \"all\".")
-endif( MSVC )
+
+set(LLVM_EXPERIMENTAL_TARGETS_TO_BUILD ""
+ CACHE STRING "Semicolon-separated list of experimental targets to build.")
+
+option(BUILD_SHARED_LIBS
+ "Build all libraries as shared libraries instead of static" OFF)
option(LLVM_ENABLE_CBE_PRINTF_A "Set to ON if CBE is enabled for printf %a output" ON)
if(LLVM_ENABLE_CBE_PRINTF_A)
set(ENABLE_TIMESTAMPS 1)
endif()
+option(LLVM_ENABLE_BACKTRACES "Enable embedding backtraces on crash." ON)
+if(LLVM_ENABLE_BACKTRACES)
+ set(ENABLE_BACKTRACES 1)
+endif()
+
option(LLVM_ENABLE_FFI "Use libffi to call external functions from the interpreter" OFF)
set(FFI_LIBRARY_DIR "" CACHE PATH "Additional directory, where CMake should search for libffi.so")
set(FFI_INCLUDE_DIR "" CACHE PATH "Additional directory, where CMake should search for ffi.h or ffi/ffi.h")
@@ -111,22 +123,20 @@ set(FFI_INCLUDE_DIR "" CACHE PATH "Additional directory, where CMake should sear
set(LLVM_TARGET_ARCH "host"
CACHE STRING "Set target to use for LLVM JIT or use \"host\" for automatic detection.")
+option(LLVM_ENABLE_TERMINFO "Use terminfo database if available." ON)
+
option(LLVM_ENABLE_THREADS "Use threads if available." ON)
+option(LLVM_ENABLE_ZLIB "Use zlib for compression/decompression if available." ON)
+
if( LLVM_TARGETS_TO_BUILD STREQUAL "all" )
set( LLVM_TARGETS_TO_BUILD ${LLVM_ALL_TARGETS} )
endif()
-set(LLVM_ENUM_TARGETS "")
-foreach(c ${LLVM_TARGETS_TO_BUILD})
- list(FIND LLVM_ALL_TARGETS ${c} idx)
- if( idx LESS 0 )
- message(FATAL_ERROR "The target `${c}' does not exist.
- It should be one of\n${LLVM_ALL_TARGETS}")
- else()
- set(LLVM_ENUM_TARGETS "${LLVM_ENUM_TARGETS}LLVM_TARGET(${c})\n")
- endif()
-endforeach(c)
+set(LLVM_TARGETS_TO_BUILD
+ ${LLVM_TARGETS_TO_BUILD}
+ ${LLVM_EXPERIMENTAL_TARGETS_TO_BUILD})
+list(REMOVE_DUPLICATES LLVM_TARGETS_TO_BUILD)
set(llvm_builded_incs_dir ${LLVM_BINARY_DIR}/include/llvm)
option(LLVM_ENABLE_PEDANTIC "Compile with pedantic enabled." ON)
option(LLVM_ENABLE_WERROR "Fail and stop if a warning is triggered." OFF)
-if( uppercase_CMAKE_BUILD_TYPE STREQUAL "RELEASE" )
+if( NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "DEBUG" )
option(LLVM_ENABLE_ASSERTIONS "Enable assertions" OFF)
else()
option(LLVM_ENABLE_ASSERTIONS "Enable assertions" ON)
endif()
+option(LLVM_USE_INTEL_JITEVENTS
+ "Use Intel JIT API to inform Intel(R) VTune(TM) Amplifier XE 2011 about JIT code"
+ OFF)
+
+if( LLVM_USE_INTEL_JITEVENTS )
+ # Verify we are on a supported platform
+ if( NOT CMAKE_SYSTEM_NAME MATCHES "Windows" AND NOT CMAKE_SYSTEM_NAME MATCHES "Linux" )
+ message(FATAL_ERROR
+ "Intel JIT API support is available on Linux and Windows only.")
+ endif()
+endif( LLVM_USE_INTEL_JITEVENTS )
+
+option(LLVM_USE_OPROFILE
+ "Use opagent JIT interface to inform OProfile about JIT code" OFF)
+
+# If enabled, verify we are on a platform that supports oprofile.
+if( LLVM_USE_OPROFILE )
+ if( NOT CMAKE_SYSTEM_NAME MATCHES "Linux" )
+ message(FATAL_ERROR "OProfile support is available on Linux only.")
+ endif( NOT CMAKE_SYSTEM_NAME MATCHES "Linux" )
+endif( LLVM_USE_OPROFILE )
+
+set(LLVM_USE_SANITIZER "" CACHE STRING
+ "Define the sanitizer used to build binaries and tests.")
+
+option(LLVM_USE_SPLIT_DWARF
+ "Use -gsplit-dwarf when compiling llvm." OFF)
+
# Define an option controlling whether we should build for 32-bit on 64-bit
# platforms, where supported.
if( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 )
set(LLVM_LIT_TOOLS_DIR "" CACHE PATH "Path to GnuWin32 tools")
endif()
-# On Win32 using MS tools, provide an option to set the number of parallel jobs
-# to use.
-if( MSVC_IDE AND ( MSVC90 OR MSVC10 ) )
- # Only Visual Studio 2008 and 2010 officially supports /MP. Visual Studio
- # 2005 supports it but it is experimental.
- set(LLVM_COMPILER_JOBS "0" CACHE STRING
- "Number of parallel compiler jobs. 0 means use all processors. Default is 0.")
-endif()
-
# Define options to control the inclusion and default build behavior for
# components which may not strictly be necessary (tools, runtime, examples, and
# tests).
@@ -204,9 +233,17 @@ option(LLVM_INCLUDE_TESTS "Generate build targets for the LLVM unit tests." ON)
# BEFORE this include, otherwise options will not be correctly set on
# first cmake run
include(config-ix)
+
+# By default, we target the host, but this can be overridden at CMake
+# invocation time.
+set(LLVM_DEFAULT_TARGET_TRIPLE "${LLVM_HOST_TRIPLE}" CACHE STRING
+ "Default target for which LLVM will generate code." )
+set(TARGET_TRIPLE "${LLVM_DEFAULT_TARGET_TRIPLE}")
+
include(HandleLLVMOptions)
-# Verify that we can find a Python interpreter,
+# Verify that we can find a Python 2 interpreter. Python 3 is unsupported.
+set(Python_ADDITIONAL_VERSIONS 2.7 2.6 2.5 2.4)
include(FindPythonInterp)
if( NOT PYTHONINTERP_FOUND )
message(FATAL_ERROR
"${LLVM_BINARY_DIR}/tools/llvm-config/LibraryDependencies.inc")
set(LLVMBUILDCMAKEFRAG
"${LLVM_BINARY_DIR}/LLVMBuild.cmake")
+
+# Create the list of optional components that are enabled
+if (LLVM_USE_INTEL_JITEVENTS)
+ set(LLVMOPTIONALCOMPONENTS IntelJITEvents)
+endif (LLVM_USE_INTEL_JITEVENTS)
+if (LLVM_USE_OPROFILE)
+ set(LLVMOPTIONALCOMPONENTS ${LLVMOPTIONALCOMPONENTS} OProfileJIT)
+endif (LLVM_USE_OPROFILE)
+
message(STATUS "Constructing LLVMBuild project information")
execute_process(
COMMAND ${PYTHON_EXECUTABLE} ${LLVMBUILDTOOL}
--native-target "${LLVM_NATIVE_ARCH}"
--enable-targets "${LLVM_TARGETS_TO_BUILD}"
+ --enable-optional-components "${LLVMOPTIONALCOMPONENTS}"
--write-library-table ${LLVMCONFIGLIBRARYDEPENDENCIESINC}
--write-cmake-fragment ${LLVMBUILDCMAKEFRAG}
- ERROR_VARIABLE LLVMBUILDOUTPUT
+ OUTPUT_VARIABLE LLVMBUILDOUTPUT
ERROR_VARIABLE LLVMBUILDERRORS
OUTPUT_STRIP_TRAILING_WHITESPACE
ERROR_STRIP_TRAILING_WHITESPACE
# Configure all of the various header file fragments LLVM uses which depend on
# configuration variables.
+set(LLVM_ENUM_TARGETS "")
set(LLVM_ENUM_ASM_PRINTERS "")
set(LLVM_ENUM_ASM_PARSERS "")
set(LLVM_ENUM_DISASSEMBLERS "")
foreach(t ${LLVM_TARGETS_TO_BUILD})
set( td ${LLVM_MAIN_SRC_DIR}/lib/Target/${t} )
+
+ list(FIND LLVM_ALL_TARGETS ${t} idx)
+ list(FIND LLVM_EXPERIMENTAL_TARGETS_TO_BUILD ${t} idy)
+ if( idx LESS 0 AND idy LESS 0 )
+ message(FATAL_ERROR "The target `${t}' does not exist.
+ It should be one of\n${LLVM_ALL_TARGETS}")
+ else()
+ set(LLVM_ENUM_TARGETS "${LLVM_ENUM_TARGETS}LLVM_TARGET(${t})\n")
+ endif()
+
file(GLOB asmp_file "${td}/*AsmPrinter.cpp")
if( asmp_file )
set(LLVM_ENUM_ASM_PRINTERS
include_directories( ${LLVM_BINARY_DIR}/include ${LLVM_MAIN_INCLUDE_DIR})
+if( ${CMAKE_SYSTEM_NAME} MATCHES FreeBSD )
+ # On FreeBSD, /usr/local/* is not used by default. In order to build LLVM
+ # with libxml2, iconv.h, etc., we must add /usr/local paths.
+ include_directories("/usr/local/include")
+ link_directories("/usr/local/lib")
+endif( ${CMAKE_SYSTEM_NAME} MATCHES FreeBSD )
+
if( ${CMAKE_SYSTEM_NAME} MATCHES SunOS )
SET(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -include llvm/Support/Solaris.h")
endif( ${CMAKE_SYSTEM_NAME} MATCHES SunOS )
+# Make sure we don't get -rdynamic in every binary. For those that need it,
+# use set_target_properties(target PROPERTIES ENABLE_EXPORTS 1)
+set(CMAKE_SHARED_LIBRARY_LINK_CXX_FLAGS "")
+
include(AddLLVM)
include(TableGen)
add_subdirectory(utils/count)
add_subdirectory(utils/not)
add_subdirectory(utils/llvm-lit)
-add_subdirectory(utils/json-bench)
+add_subdirectory(utils/yaml-bench)
add_subdirectory(projects)
add_subdirectory(utils/unittest)
add_subdirectory(unittests)
if (MSVC)
- # This utility is used to prevent chrashing tests from calling Dr. Watson on
+ # This utility is used to prevent crashing tests from calling Dr. Watson on
# Windows.
add_subdirectory(utils/KillTheDoctor)
endif()
+
+ # Add a global check rule now that all subdirectories have been traversed
+ # and we know the total set of lit testsuites.
+ get_property(LLVM_LIT_TESTSUITES GLOBAL PROPERTY LLVM_LIT_TESTSUITES)
+ get_property(LLVM_LIT_PARAMS GLOBAL PROPERTY LLVM_LIT_PARAMS)
+ get_property(LLVM_LIT_DEPENDS GLOBAL PROPERTY LLVM_LIT_DEPENDS)
+ get_property(LLVM_LIT_EXTRA_ARGS GLOBAL PROPERTY LLVM_LIT_EXTRA_ARGS)
+ add_lit_target(check-all
+ "Running all regression tests"
+ ${LLVM_LIT_TESTSUITES}
+ PARAMS ${LLVM_LIT_PARAMS}
+ DEPENDS ${LLVM_LIT_DEPENDS}
+ ARGS ${LLVM_LIT_EXTRA_ARGS}
+ )
endif()
add_subdirectory(cmake/modules)
# TODO: make and install documentation.
set(CPACK_PACKAGE_VENDOR "LLVM")
-set(CPACK_PACKAGE_VERSION_MAJOR 2)
-set(CPACK_PACKAGE_VERSION_MINOR 9)
-add_version_info_from_vcs(CPACK_PACKAGE_VERSION_PATCH)
+set(CPACK_PACKAGE_VERSION_MAJOR ${LLVM_VERSION_MAJOR})
+set(CPACK_PACKAGE_VERSION_MINOR ${LLVM_VERSION_MINOR})
+if( LLVM_APPEND_VC_REV )
+ add_version_info_from_vcs(CPACK_PACKAGE_VERSION_PATCH)
+else()
+ set(CPACK_PACKAGE_VERSION_PATCH "svn")
+endif()
+set(CPACK_RESOURCE_FILE_LICENSE "${LLVM_MAIN_SRC_DIR}/LICENSE.TXT")
+if(WIN32 AND NOT UNIX)
+ set(CPACK_PACKAGE_ICON "${LLVM_MAIN_SRC_DIR}\\\\cmake\\\\nsis_logo.bmp")
+ set(CPACK_NSIS_MODIFY_PATH "ON")
+endif()
include(CPack)
# Workaround for MSVS10 to avoid the Dialog Hell