diff --git a/CMakeLists.txt b/CMakeLists.txt
index 9878c7991d517878082f4fa3eb29bcc54cb5df50..27010d2c5321c4261423ba9e39642e89f5710f8c 100644 (file)
--- a/CMakeLists.txt
+++ b/CMakeLists.txt
"${CMAKE_CURRENT_SOURCE_DIR}/cmake/modules"
)
-set(PACKAGE_VERSION "2.9")
+set(LLVM_VERSION_MAJOR 3)
+set(LLVM_VERSION_MINOR 4)
+
+set(PACKAGE_VERSION "${LLVM_VERSION_MAJOR}.${LLVM_VERSION_MINOR}svn")
+
+option(LLVM_USE_FOLDERS "Enable solution folders in Visual Studio. Disable for Express versions." ON)
+if ( LLVM_USE_FOLDERS )
+ set_property(GLOBAL PROPERTY USE_FOLDERS ON)
+endif()
include(VersionFromVCS)
add_version_info_from_vcs(PACKAGE_VERSION)
endif()
-set(PACKAGE_NAME llvm)
+set(PACKAGE_NAME LLVM)
set(PACKAGE_STRING "${PACKAGE_NAME} ${PACKAGE_VERSION}")
-set(PACKAGE_BUGREPORT "llvmbugs@cs.uiuc.edu")
+set(PACKAGE_BUGREPORT "http://llvm.org/bugs/")
+# Sanity check our source directory to make sure that we are not trying to
+# generate an in-tree build (unless on MSVC_IDE, where it is ok), and to make
+# sure that we don't have any stray generated files lying around in the tree
+# (which would end up getting picked up by header search, instead of the correct
+# versions).
if( CMAKE_SOURCE_DIR STREQUAL CMAKE_BINARY_DIR AND NOT MSVC_IDE )
message(FATAL_ERROR "In-source builds are not allowed.
CMake would overwrite the makefiles distributed with LLVM.
This process created the file `CMakeCache.txt' and the directory `CMakeFiles'.
Please delete them.")
endif()
-
-# Run-time build mode; It is used for unittests.
-if(MSVC_IDE)
- # Expect "$(Configuration)", "$(OutDir)", etc.
- # It is expanded by msbuild or similar.
- set(RUNTIME_BUILD_MODE "${CMAKE_CFG_INTDIR}")
-elseif(NOT CMAKE_BUILD_TYPE STREQUAL "")
- # Expect "Release" "Debug", etc.
- # Or unittests could not run.
- set(RUNTIME_BUILD_MODE ${CMAKE_BUILD_TYPE})
-else()
- # It might be "."
- set(RUNTIME_BUILD_MODE "${CMAKE_CFG_INTDIR}")
-endif()
-
-string(TOUPPER "${CMAKE_BUILD_TYPE}" uppercase_CMAKE_BUILD_TYPE)
-
-set(LLVM_MAIN_SRC_DIR ${CMAKE_CURRENT_SOURCE_DIR})
-set(LLVM_MAIN_INCLUDE_DIR ${LLVM_MAIN_SRC_DIR}/include)
-set(LLVM_BINARY_DIR ${CMAKE_CURRENT_BINARY_DIR})
-set(LLVM_TOOLS_BINARY_DIR ${LLVM_BINARY_DIR}/bin)
-set(LLVM_EXAMPLES_BINARY_DIR ${LLVM_BINARY_DIR}/examples)
-set(LLVM_LIBDIR_SUFFIX "" CACHE STRING "Define suffix of library directory name (32/64)" )
-
if( NOT CMAKE_SOURCE_DIR STREQUAL CMAKE_BINARY_DIR )
file(GLOB_RECURSE
tablegenned_files_on_include_dir
- "${LLVM_MAIN_SRC_DIR}/include/llvm/*.gen")
+ "${CMAKE_CURRENT_SOURCE_DIR}/include/llvm/*.gen")
file(GLOB_RECURSE
tablegenned_files_on_lib_dir
- "${LLVM_MAIN_SRC_DIR}/lib/Target/*.inc")
+ "${CMAKE_CURRENT_SOURCE_DIR}/lib/Target/*.inc")
if( tablegenned_files_on_include_dir OR tablegenned_files_on_lib_dir)
message(FATAL_ERROR "Apparently there is a previous in-source build,
probably as the result of running `configure' and `make' on
-${LLVM_MAIN_SRC_DIR}.
+${CMAKE_CURRENT_SOURCE_DIR}.
This may cause problems. The suspicious files are:
${tablegenned_files_on_lib_dir}
${tablegenned_files_on_include_dir}
endif()
endif()
+string(TOUPPER "${CMAKE_BUILD_TYPE}" uppercase_CMAKE_BUILD_TYPE)
+
+set(LLVM_MAIN_SRC_DIR ${CMAKE_CURRENT_SOURCE_DIR})
+set(LLVM_MAIN_INCLUDE_DIR ${LLVM_MAIN_SRC_DIR}/include)
+set(LLVM_BINARY_DIR ${CMAKE_CURRENT_BINARY_DIR})
+set(LLVM_TOOLS_BINARY_DIR ${LLVM_BINARY_DIR}/bin)
+set(LLVM_EXAMPLES_BINARY_DIR ${LLVM_BINARY_DIR}/examples)
+set(LLVM_LIBDIR_SUFFIX "" CACHE STRING "Define suffix of library directory name (32/64)" )
+
set(LLVM_ALL_TARGETS
- Alpha
+ AArch64
ARM
- Blackfin
- CBackend
- CellSPU
CppBackend
+ Hexagon
Mips
- MBlaze
MSP430
+ NVPTX
PowerPC
- PTX
+ R600
Sparc
SystemZ
X86
XCore
)
-if( MSVC )
- set(LLVM_TARGETS_TO_BUILD X86
- CACHE STRING "Semicolon-separated list of targets to build, or \"all\".")
-else( MSVC )
- set(LLVM_TARGETS_TO_BUILD ${LLVM_ALL_TARGETS}
+# List of targets with JIT support:
+set(LLVM_TARGETS_WITH_JIT X86 PowerPC AArch64 ARM Mips SystemZ)
+
+set(LLVM_TARGETS_TO_BUILD "all"
CACHE STRING "Semicolon-separated list of targets to build, or \"all\".")
-endif( MSVC )
-set(CLANG_RESOURCE_DIR "" CACHE STRING
- "Relative directory from the Clang binary to its resource files.")
+set(LLVM_EXPERIMENTAL_TARGETS_TO_BUILD ""
+ CACHE STRING "Semicolon-separated list of experimental targets to build.")
+
+option(BUILD_SHARED_LIBS
+ "Build all libraries as shared libraries instead of static" OFF)
option(LLVM_ENABLE_CBE_PRINTF_A "Set to ON if CBE is enabled for printf %a output" ON)
if(LLVM_ENABLE_CBE_PRINTF_A)
set(ENABLE_TIMESTAMPS 1)
endif()
+option(LLVM_ENABLE_BACKTRACES "Enable embedding backtraces on crash." ON)
+if(LLVM_ENABLE_BACKTRACES)
+ set(ENABLE_BACKTRACES 1)
+endif()
+
option(LLVM_ENABLE_FFI "Use libffi to call external functions from the interpreter" OFF)
set(FFI_LIBRARY_DIR "" CACHE PATH "Additional directory, where CMake should search for libffi.so")
set(FFI_INCLUDE_DIR "" CACHE PATH "Additional directory, where CMake should search for ffi.h or ffi/ffi.h")
-set(C_INCLUDE_DIRS "" CACHE STRING
- "Colon separated list of directories clang will search for headers.")
-
set(LLVM_TARGET_ARCH "host"
CACHE STRING "Set target to use for LLVM JIT or use \"host\" for automatic detection.")
-set(LIT_ARGS_DEFAULT "-sv")
-if (MSVC OR XCODE)
- set(LIT_ARGS_DEFAULT "${LIT_ARGS_DEFAULT} --no-progress-bar")
-endif()
-set(LLVM_LIT_ARGS "${LIT_ARGS_DEFAULT}"
- CACHE STRING "Default options for lit")
+option(LLVM_ENABLE_TERMINFO "Use terminfo database if available." ON)
option(LLVM_ENABLE_THREADS "Use threads if available." ON)
-if( uppercase_CMAKE_BUILD_TYPE STREQUAL "RELEASE" )
- option(LLVM_ENABLE_ASSERTIONS "Enable assertions" OFF)
-else()
- option(LLVM_ENABLE_ASSERTIONS "Enable assertions" ON)
-endif()
-
-if( LLVM_ENABLE_ASSERTIONS )
- # MSVC doesn't like _DEBUG on release builds. See PR 4379.
- if( NOT MSVC )
- add_definitions( -D_DEBUG )
- endif()
- # On Release builds cmake automatically defines NDEBUG, so we
- # explicitly undefine it:
- if( uppercase_CMAKE_BUILD_TYPE STREQUAL "RELEASE" )
- add_definitions( -UNDEBUG )
- endif()
-else()
- if( NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "RELEASE" )
- add_definitions( -DNDEBUG )
- endif()
-endif()
+option(LLVM_ENABLE_ZLIB "Use zlib for compression/decompression if available." ON)
if( LLVM_TARGETS_TO_BUILD STREQUAL "all" )
set( LLVM_TARGETS_TO_BUILD ${LLVM_ALL_TARGETS} )
endif()
-set(LLVM_ENUM_TARGETS "")
-foreach(c ${LLVM_TARGETS_TO_BUILD})
- list(FIND LLVM_ALL_TARGETS ${c} idx)
- if( idx LESS 0 )
- message(FATAL_ERROR "The target `${c}' does not exist.
- It should be one of\n${LLVM_ALL_TARGETS}")
- else()
- set(LLVM_ENUM_TARGETS "${LLVM_ENUM_TARGETS}LLVM_TARGET(${c})\n")
- endif()
-endforeach(c)
-
-# Produce llvm/Config/Targets.def
-configure_file(
- ${LLVM_MAIN_INCLUDE_DIR}/llvm/Config/Targets.def.in
- ${LLVM_BINARY_DIR}/include/llvm/Config/Targets.def
- )
+set(LLVM_TARGETS_TO_BUILD
+ ${LLVM_TARGETS_TO_BUILD}
+ ${LLVM_EXPERIMENTAL_TARGETS_TO_BUILD})
+list(REMOVE_DUPLICATES LLVM_TARGETS_TO_BUILD)
set(llvm_builded_incs_dir ${LLVM_BINARY_DIR}/include/llvm)
include(AddLLVMDefinitions)
-if(WIN32)
- if(CYGWIN)
- set(LLVM_ON_WIN32 0)
- set(LLVM_ON_UNIX 1)
- else(CYGWIN)
- set(LLVM_ON_WIN32 1)
- set(LLVM_ON_UNIX 0)
- endif(CYGWIN)
- set(LTDL_SHLIB_EXT ".dll")
- set(EXEEXT ".exe")
- # Maximum path length is 160 for non-unicode paths
- set(MAXPATHLEN 160)
-else(WIN32)
- if(UNIX)
- set(LLVM_ON_WIN32 0)
- set(LLVM_ON_UNIX 1)
- if(APPLE)
- set(LTDL_SHLIB_EXT ".dylib")
- else(APPLE)
- set(LTDL_SHLIB_EXT ".so")
- endif(APPLE)
- set(EXEEXT "")
- # FIXME: Maximum path length is currently set to 'safe' fixed value
- set(MAXPATHLEN 2024)
- else(UNIX)
- MESSAGE(SEND_ERROR "Unable to determine platform")
- endif(UNIX)
-endif(WIN32)
-
option(LLVM_ENABLE_PIC "Build Position-Independent Code" ON)
-if( LLVM_ENABLE_PIC )
- if( XCODE )
- # Xcode has -mdynamic-no-pic on by default, which overrides -fPIC. I don't
- # know how to disable this, so just force ENABLE_PIC off for now.
- message(WARNING "-fPIC not supported with Xcode.")
- elseif( WIN32 )
- # On Windows all code is PIC. MinGW warns if -fPIC is used.
- else()
- include(CheckCXXCompilerFlag)
- check_cxx_compiler_flag("-fPIC" SUPPORTS_FPIC_FLAG)
- if( SUPPORTS_FPIC_FLAG )
- message(STATUS "Building with -fPIC")
- set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -fPIC")
- set(CMAKE_C_FLAGS "${CMAKE_CXX_FLAGS} -fPIC")
- else( SUPPORTS_FPIC_FLAG )
- message(WARNING "-fPIC not supported.")
- endif()
- endif()
-endif()
-
-include(config-ix)
-
-set( CMAKE_RUNTIME_OUTPUT_DIRECTORY ${LLVM_TOOLS_BINARY_DIR} )
-set( CMAKE_LIBRARY_OUTPUT_DIRECTORY ${LLVM_BINARY_DIR}/lib )
-set( CMAKE_ARCHIVE_OUTPUT_DIRECTORY ${LLVM_BINARY_DIR}/lib )
-
-# set(CMAKE_VERBOSE_MAKEFILE true)
-
-add_llvm_definitions( -D__STDC_LIMIT_MACROS )
-add_llvm_definitions( -D__STDC_CONSTANT_MACROS )
-
# MSVC has a gazillion warnings with this.
if( MSVC )
option(LLVM_ENABLE_WARNINGS "Enable compiler warnings." OFF)
option(LLVM_ENABLE_PEDANTIC "Compile with pedantic enabled." ON)
option(LLVM_ENABLE_WERROR "Fail and stop if a warning is triggered." OFF)
-if( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 )
- # TODO: support other platforms and toolchains.
- option(LLVM_BUILD_32_BITS "Build 32 bits executables and libraries." OFF)
- if( LLVM_BUILD_32_BITS )
- message(STATUS "Building 32 bits executables and libraries.")
- add_llvm_definitions( -m32 )
- list(APPEND CMAKE_EXE_LINKER_FLAGS -m32)
- list(APPEND CMAKE_SHARED_LINKER_FLAGS -m32)
- endif( LLVM_BUILD_32_BITS )
-endif( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 )
+if( NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "DEBUG" )
+ option(LLVM_ENABLE_ASSERTIONS "Enable assertions" OFF)
+else()
+ option(LLVM_ENABLE_ASSERTIONS "Enable assertions" ON)
+endif()
-if( MSVC )
- include(ChooseMSVCCRT)
-
- # Add definitions that make MSVC much less annoying.
- add_llvm_definitions(
- # For some reason MS wants to deprecate a bunch of standard functions...
- -D_CRT_SECURE_NO_DEPRECATE
- -D_CRT_SECURE_NO_WARNINGS
- -D_CRT_NONSTDC_NO_DEPRECATE
- -D_CRT_NONSTDC_NO_WARNINGS
- -D_SCL_SECURE_NO_DEPRECATE
- -D_SCL_SECURE_NO_WARNINGS
-
- -wd4146 # Suppress 'unary minus operator applied to unsigned type, result still unsigned'
- -wd4180 # Suppress 'qualifier applied to function type has no meaning; ignored'
- -wd4224 # Suppress 'nonstandard extension used : formal parameter 'identifier' was previously defined as a type'
- -wd4244 # Suppress ''argument' : conversion from 'type1' to 'type2', possible loss of data'
- -wd4267 # Suppress ''var' : conversion from 'size_t' to 'type', possible loss of data'
- -wd4275 # Suppress 'An exported class was derived from a class that was not exported.'
- -wd4291 # Suppress ''declaration' : no matching operator delete found; memory will not be freed if initialization throws an exception'
- -wd4345 # Suppress 'behavior change: an object of POD type constructed with an initializer of the form () will be default-initialized'
- -wd4351 # Suppress 'new behavior: elements of array 'array' will be default initialized'
- -wd4355 # Suppress ''this' : used in base member initializer list'
- -wd4503 # Suppress ''identifier' : decorated name length exceeded, name was truncated'
- -wd4624 # Suppress ''derived class' : destructor could not be generated because a base class destructor is inaccessible'
- -wd4715 # Suppress ''function' : not all control paths return a value'
- -wd4800 # Suppress ''type' : forcing value to bool 'true' or 'false' (performance warning)'
- -wd4065 # Suppress 'switch statement contains 'default' but no 'case' labels'
-
- -w14062 # Promote "enumerator in switch of enum is not handled" to level 1 warning.
- )
+option(LLVM_USE_INTEL_JITEVENTS
+ "Use Intel JIT API to inform Intel(R) VTune(TM) Amplifier XE 2011 about JIT code"
+ OFF)
- # Enable warnings
- if (LLVM_ENABLE_WARNINGS)
- add_llvm_definitions( /W4 /Wall )
- if (LLVM_ENABLE_PEDANTIC)
- # No MSVC equivalent available
- endif (LLVM_ENABLE_PEDANTIC)
- endif (LLVM_ENABLE_WARNINGS)
- if (LLVM_ENABLE_WERROR)
- add_llvm_definitions( /WX )
- endif (LLVM_ENABLE_WERROR)
-elseif( CMAKE_COMPILER_IS_GNUCXX )
- if (LLVM_ENABLE_WARNINGS)
- add_llvm_definitions( -Wall -W -Wno-unused-parameter -Wwrite-strings )
- if (LLVM_ENABLE_PEDANTIC)
- add_llvm_definitions( -pedantic -Wno-long-long )
- endif (LLVM_ENABLE_PEDANTIC)
- endif (LLVM_ENABLE_WARNINGS)
- if (LLVM_ENABLE_WERROR)
- add_llvm_definitions( -Werror )
- endif (LLVM_ENABLE_WERROR)
-endif( MSVC )
+if( LLVM_USE_INTEL_JITEVENTS )
+ # Verify we are on a supported platform
+ if( NOT CMAKE_SYSTEM_NAME MATCHES "Windows" AND NOT CMAKE_SYSTEM_NAME MATCHES "Linux" )
+ message(FATAL_ERROR
+ "Intel JIT API support is available on Linux and Windows only.")
+ endif()
+endif( LLVM_USE_INTEL_JITEVENTS )
-include_directories( ${LLVM_BINARY_DIR}/include ${LLVM_MAIN_INCLUDE_DIR})
+option(LLVM_USE_OPROFILE
+ "Use opagent JIT interface to inform OProfile about JIT code" OFF)
-if( ${CMAKE_SYSTEM_NAME} MATCHES SunOS )
- SET(CMAKE_CXX_FLAGS ${CMAKE_CXX_FLAGS} "-include llvm/Support/Solaris.h")
-endif( ${CMAKE_SYSTEM_NAME} MATCHES SunOS )
+# If enabled, verify we are on a platform that supports oprofile.
+if( LLVM_USE_OPROFILE )
+ if( NOT CMAKE_SYSTEM_NAME MATCHES "Linux" )
+ message(FATAL_ERROR "OProfile support is available on Linux only.")
+ endif( NOT CMAKE_SYSTEM_NAME MATCHES "Linux" )
+endif( LLVM_USE_OPROFILE )
-include(AddLLVM)
-include(TableGen)
+set(LLVM_USE_SANITIZER "" CACHE STRING
+ "Define the sanitizer used to build binaries and tests.")
-if( MINGW )
- get_system_libs(LLVM_SYSTEM_LIBS_LIST)
- foreach(l ${LLVM_SYSTEM_LIBS_LIST})
- set(LLVM_SYSTEM_LIBS "${LLVM_SYSTEM_LIBS} -l${l}")
- endforeach()
- set(CMAKE_CXX_STANDARD_LIBRARIES "${CMAKE_CXX_STANDARD_LIBRARIES}${LLVM_SYSTEM_LIBS}")
- set(CMAKE_C_STANDARD_LIBRARIES "${CMAKE_C_STANDARD_LIBRARIES}${LLVM_SYSTEM_LIBS}")
+option(LLVM_USE_SPLIT_DWARF
+ "Use -gsplit-dwarf when compiling llvm." OFF)
+
+# Define an option controlling whether we should build for 32-bit on 64-bit
+# platforms, where supported.
+if( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 )
+ # TODO: support other platforms and toolchains.
+ option(LLVM_BUILD_32_BITS "Build 32 bits executables and libraries." OFF)
endif()
-if( MINGW )
- # People report that -O3 is unreliable on MinGW. The traditional
- # build also uses -O2 for that reason:
- llvm_replace_compiler_option(CMAKE_CXX_FLAGS_RELEASE "-O3" "-O2")
+# Define the default arguments to use with 'lit', and an option for the user to
+# override.
+set(LIT_ARGS_DEFAULT "-sv")
+if (MSVC OR XCODE)
+ set(LIT_ARGS_DEFAULT "${LIT_ARGS_DEFAULT} --no-progress-bar")
endif()
+set(LLVM_LIT_ARGS "${LIT_ARGS_DEFAULT}" CACHE STRING "Default options for lit")
-add_subdirectory(lib/Support)
+# On Win32 hosts, provide an option to specify the path to the GnuWin32 tools.
+if( WIN32 AND NOT CYGWIN )
+ set(LLVM_LIT_TOOLS_DIR "" CACHE PATH "Path to GnuWin32 tools")
+endif()
+
+# Define options to control the inclusion and default build behavior for
+# components which may not strictly be necessary (tools, runtime, examples, and
+# tests).
+#
+# This is primarily to support building smaller or faster project files.
+option(LLVM_INCLUDE_TOOLS "Generate build targets for the LLVM tools." ON)
+option(LLVM_BUILD_TOOLS
+ "Build the LLVM tools. If OFF, just generate build targets." ON)
-# Everything else depends on Support:
-set(LLVM_COMMON_DEPENDS ${LLVM_COMMON_DEPENDS} ${LLVM_LIBS} )
+option(LLVM_INCLUDE_RUNTIME "Generate build targets for the LLVM runtimes" ON)
+option(LLVM_BUILD_RUNTIME
+ "Build the LLVM runtime libraries. If OFF, just generate build targets." ON)
-set(LLVM_TABLEGEN "tblgen" CACHE
- STRING "Native TableGen executable. Saves building one when cross-compiling.")
-# Effective tblgen executable to be used:
-set(LLVM_TABLEGEN_EXE ${LLVM_TABLEGEN})
+option(LLVM_BUILD_EXAMPLES
+ "Build the LLVM example programs. If OFF, just generate build targets." OFF)
+option(LLVM_INCLUDE_EXAMPLES "Generate build targets for the LLVM examples" ON)
-add_subdirectory(utils/TableGen)
+option(LLVM_BUILD_TESTS
+ "Build LLVM unit tests. If OFF, just generate build targets." OFF)
+option(LLVM_INCLUDE_TESTS "Generate build targets for the LLVM unit tests." ON)
-if( CMAKE_CROSSCOMPILING )
- # This adds a dependency on target `tblgen', so must go after utils/TableGen
- include( CrossCompileLLVM )
-endif( CMAKE_CROSSCOMPILING )
+# All options referred to from HandleLLVMOptions have to be specified
+# BEFORE this include, otherwise options will not be correctly set on
+# first cmake run
+include(config-ix)
-add_subdirectory(include/llvm)
+# By default, we target the host, but this can be overridden at CMake
+# invocation time.
+set(LLVM_DEFAULT_TARGET_TRIPLE "${LLVM_HOST_TRIPLE}" CACHE STRING
+ "Default target for which LLVM will generate code." )
+set(TARGET_TRIPLE "${LLVM_DEFAULT_TARGET_TRIPLE}")
-add_subdirectory(lib/VMCore)
-add_subdirectory(lib/CodeGen)
-add_subdirectory(lib/CodeGen/SelectionDAG)
-add_subdirectory(lib/CodeGen/AsmPrinter)
-add_subdirectory(lib/Bitcode/Reader)
-add_subdirectory(lib/Bitcode/Writer)
-add_subdirectory(lib/Transforms/Utils)
-add_subdirectory(lib/Transforms/Instrumentation)
-add_subdirectory(lib/Transforms/InstCombine)
-add_subdirectory(lib/Transforms/Scalar)
-add_subdirectory(lib/Transforms/IPO)
-add_subdirectory(lib/Transforms/Hello)
-add_subdirectory(lib/Linker)
-add_subdirectory(lib/Analysis)
-add_subdirectory(lib/Analysis/IPA)
-add_subdirectory(lib/MC)
-add_subdirectory(lib/MC/MCParser)
-add_subdirectory(lib/MC/MCDisassembler)
-add_subdirectory(lib/Object)
+include(HandleLLVMOptions)
-add_subdirectory(utils/FileCheck)
-add_subdirectory(utils/FileUpdate)
-add_subdirectory(utils/count)
-add_subdirectory(utils/not)
-add_subdirectory(utils/llvm-lit)
+# Verify that we can find a Python 2 interpreter. Python 3 is unsupported.
+set(Python_ADDITIONAL_VERSIONS 2.7 2.6 2.5 2.4)
+include(FindPythonInterp)
+if( NOT PYTHONINTERP_FOUND )
+ message(FATAL_ERROR
+"Unable to find Python interpreter, required for builds and testing.
+Please install Python or specify the PYTHON_EXECUTABLE CMake variable.")
+endif()
+
+######
+# LLVMBuild Integration
+#
+# We use llvm-build to generate all the data required by the CMake based
+# build system in one swoop:
+#
+# - We generate a file (a CMake fragment) in the object root which contains
+# all the definitions that are required by CMake.
+#
+# - We generate the library table used by llvm-config.
+#
+# - We generate the dependencies for the CMake fragment, so that we will
+# automatically reconfigure outselves.
+
+set(LLVMBUILDTOOL "${LLVM_MAIN_SRC_DIR}/utils/llvm-build/llvm-build")
+set(LLVMCONFIGLIBRARYDEPENDENCIESINC
+ "${LLVM_BINARY_DIR}/tools/llvm-config/LibraryDependencies.inc")
+set(LLVMBUILDCMAKEFRAG
+ "${LLVM_BINARY_DIR}/LLVMBuild.cmake")
+
+# Create the list of optional components that are enabled
+if (LLVM_USE_INTEL_JITEVENTS)
+ set(LLVMOPTIONALCOMPONENTS IntelJITEvents)
+endif (LLVM_USE_INTEL_JITEVENTS)
+if (LLVM_USE_OPROFILE)
+ set(LLVMOPTIONALCOMPONENTS ${LLVMOPTIONALCOMPONENTS} OProfileJIT)
+endif (LLVM_USE_OPROFILE)
+
+message(STATUS "Constructing LLVMBuild project information")
+execute_process(
+ COMMAND ${PYTHON_EXECUTABLE} ${LLVMBUILDTOOL}
+ --native-target "${LLVM_NATIVE_ARCH}"
+ --enable-targets "${LLVM_TARGETS_TO_BUILD}"
+ --enable-optional-components "${LLVMOPTIONALCOMPONENTS}"
+ --write-library-table ${LLVMCONFIGLIBRARYDEPENDENCIESINC}
+ --write-cmake-fragment ${LLVMBUILDCMAKEFRAG}
+ OUTPUT_VARIABLE LLVMBUILDOUTPUT
+ ERROR_VARIABLE LLVMBUILDERRORS
+ OUTPUT_STRIP_TRAILING_WHITESPACE
+ ERROR_STRIP_TRAILING_WHITESPACE
+ RESULT_VARIABLE LLVMBUILDRESULT)
+
+# On Win32, CMake doesn't properly handle piping the default output/error
+# streams into the GUI console. So, we explicitly catch and report them.
+if( NOT "${LLVMBUILDOUTPUT}" STREQUAL "")
+ message(STATUS "llvm-build output: ${LLVMBUILDOUTPUT}")
+endif()
+if( NOT "${LLVMBUILDRESULT}" STREQUAL "0" )
+ message(FATAL_ERROR
+ "Unexpected failure executing llvm-build: ${LLVMBUILDERRORS}")
+endif()
+
+# Include the generated CMake fragment. This will define properties from the
+# LLVMBuild files in a format which is easy to consume from CMake, and will add
+# the dependencies so that CMake will reconfigure properly when the LLVMBuild
+# files change.
+include(${LLVMBUILDCMAKEFRAG})
+
+######
+
+# Configure all of the various header file fragments LLVM uses which depend on
+# configuration variables.
+set(LLVM_ENUM_TARGETS "")
set(LLVM_ENUM_ASM_PRINTERS "")
set(LLVM_ENUM_ASM_PARSERS "")
set(LLVM_ENUM_DISASSEMBLERS "")
foreach(t ${LLVM_TARGETS_TO_BUILD})
- message(STATUS "Targeting ${t}")
- add_subdirectory(lib/Target/${t})
- add_subdirectory(lib/Target/${t}/TargetInfo)
set( td ${LLVM_MAIN_SRC_DIR}/lib/Target/${t} )
+
+ list(FIND LLVM_ALL_TARGETS ${t} idx)
+ list(FIND LLVM_EXPERIMENTAL_TARGETS_TO_BUILD ${t} idy)
+ if( idx LESS 0 AND idy LESS 0 )
+ message(FATAL_ERROR "The target `${t}' does not exist.
+ It should be one of\n${LLVM_ALL_TARGETS}")
+ else()
+ set(LLVM_ENUM_TARGETS "${LLVM_ENUM_TARGETS}LLVM_TARGET(${t})\n")
+ endif()
+
file(GLOB asmp_file "${td}/*AsmPrinter.cpp")
if( asmp_file )
set(LLVM_ENUM_ASM_PRINTERS
"${LLVM_ENUM_ASM_PRINTERS}LLVM_ASM_PRINTER(${t})\n")
endif()
- if( EXISTS ${td}/InstPrinter/CMakeLists.txt )
- add_subdirectory(lib/Target/${t}/InstPrinter)
- endif()
if( EXISTS ${td}/AsmParser/CMakeLists.txt )
- add_subdirectory(lib/Target/${t}/AsmParser)
set(LLVM_ENUM_ASM_PARSERS
"${LLVM_ENUM_ASM_PARSERS}LLVM_ASM_PARSER(${t})\n")
endif()
if( EXISTS ${td}/Disassembler/CMakeLists.txt )
- add_subdirectory(lib/Target/${t}/Disassembler)
set(LLVM_ENUM_DISASSEMBLERS
"${LLVM_ENUM_DISASSEMBLERS}LLVM_DISASSEMBLER(${t})\n")
endif()
- set(CURRENT_LLVM_TARGET)
endforeach(t)
-# Produce llvm/Config/AsmPrinters.def
+# Produce the target definition files, which provide a way for clients to easily
+# include various classes of targets.
configure_file(
${LLVM_MAIN_INCLUDE_DIR}/llvm/Config/AsmPrinters.def.in
${LLVM_BINARY_DIR}/include/llvm/Config/AsmPrinters.def
)
-
-# Produce llvm/Config/AsmParsers.def
configure_file(
${LLVM_MAIN_INCLUDE_DIR}/llvm/Config/AsmParsers.def.in
${LLVM_BINARY_DIR}/include/llvm/Config/AsmParsers.def
)
-
-# Produce llvm/Config/Disassemblers.def
configure_file(
${LLVM_MAIN_INCLUDE_DIR}/llvm/Config/Disassemblers.def.in
${LLVM_BINARY_DIR}/include/llvm/Config/Disassemblers.def
)
+configure_file(
+ ${LLVM_MAIN_INCLUDE_DIR}/llvm/Config/Targets.def.in
+ ${LLVM_BINARY_DIR}/include/llvm/Config/Targets.def
+ )
+
+# Configure the three LLVM configuration header files.
+configure_file(
+ ${LLVM_MAIN_INCLUDE_DIR}/llvm/Config/config.h.cmake
+ ${LLVM_BINARY_DIR}/include/llvm/Config/config.h)
+configure_file(
+ ${LLVM_MAIN_INCLUDE_DIR}/llvm/Config/llvm-config.h.cmake
+ ${LLVM_BINARY_DIR}/include/llvm/Config/llvm-config.h)
+configure_file(
+ ${LLVM_MAIN_INCLUDE_DIR}/llvm/Support/DataTypes.h.cmake
+ ${LLVM_BINARY_DIR}/include/llvm/Support/DataTypes.h)
+
+set( CMAKE_RUNTIME_OUTPUT_DIRECTORY ${LLVM_TOOLS_BINARY_DIR} )
+set( CMAKE_LIBRARY_OUTPUT_DIRECTORY ${LLVM_BINARY_DIR}/lib )
+set( CMAKE_ARCHIVE_OUTPUT_DIRECTORY ${LLVM_BINARY_DIR}/lib )
+
+set(CMAKE_INCLUDE_CURRENT_DIR ON)
+
+include_directories( ${LLVM_BINARY_DIR}/include ${LLVM_MAIN_INCLUDE_DIR})
+
+if( ${CMAKE_SYSTEM_NAME} MATCHES FreeBSD )
+ # On FreeBSD, /usr/local/* is not used by default. In order to build LLVM
+ # with libxml2, iconv.h, etc., we must add /usr/local paths.
+ include_directories("/usr/local/include")
+ link_directories("/usr/local/lib")
+endif( ${CMAKE_SYSTEM_NAME} MATCHES FreeBSD )
+
+if( ${CMAKE_SYSTEM_NAME} MATCHES SunOS )
+ SET(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -include llvm/Support/Solaris.h")
+endif( ${CMAKE_SYSTEM_NAME} MATCHES SunOS )
+
+# Make sure we don't get -rdynamic in every binary. For those that need it,
+# use set_target_properties(target PROPERTIES ENABLE_EXPORTS 1)
+set(CMAKE_SHARED_LIBRARY_LINK_CXX_FLAGS "")
+
+include(AddLLVM)
+include(TableGen)
+
+if( MINGW )
+ # People report that -O3 is unreliable on MinGW. The traditional
+ # build also uses -O2 for that reason:
+ llvm_replace_compiler_option(CMAKE_CXX_FLAGS_RELEASE "-O3" "-O2")
+endif()
+
+# Put this before tblgen. Else we have a circular dependence.
+add_subdirectory(lib/Support)
+add_subdirectory(lib/TableGen)
-add_subdirectory(lib/ExecutionEngine)
-add_subdirectory(lib/ExecutionEngine/Interpreter)
-add_subdirectory(lib/ExecutionEngine/JIT)
-add_subdirectory(lib/ExecutionEngine/MCJIT)
-add_subdirectory(lib/Target)
-add_subdirectory(lib/AsmParser)
-add_subdirectory(lib/Archive)
+add_subdirectory(utils/TableGen)
+
+add_subdirectory(include/llvm)
+
+add_subdirectory(lib)
+
+add_subdirectory(utils/FileCheck)
+add_subdirectory(utils/FileUpdate)
+add_subdirectory(utils/count)
+add_subdirectory(utils/not)
+add_subdirectory(utils/llvm-lit)
+add_subdirectory(utils/yaml-bench)
add_subdirectory(projects)
-option(LLVM_BUILD_TOOLS
- "Build the LLVM tools. If OFF, just generate build targets." ON)
-option(LLVM_INCLUDE_TOOLS "Generate build targets for the LLVM tools." ON)
if( LLVM_INCLUDE_TOOLS )
add_subdirectory(tools)
endif()
-option(LLVM_BUILD_EXAMPLES
- "Build the LLVM example programs. If OFF, just generate build targets." OFF)
-option(LLVM_INCLUDE_EXAMPLES "Generate build targets for the LLVM examples" ON)
+if( LLVM_INCLUDE_RUNTIME )
+ add_subdirectory(runtime)
+endif()
+
if( LLVM_INCLUDE_EXAMPLES )
add_subdirectory(examples)
endif()
-option(LLVM_BUILD_TESTS
- "Build LLVM unit tests. If OFF, just generate build targes." OFF)
-option(LLVM_INCLUDE_TESTS "Generate build targets for the LLVM unit tests." ON)
if( LLVM_INCLUDE_TESTS )
add_subdirectory(test)
add_subdirectory(utils/unittest)
add_subdirectory(unittests)
if (MSVC)
- # This utility is used to prevent chrashing tests from calling Dr. Watson on
+ # This utility is used to prevent crashing tests from calling Dr. Watson on
# Windows.
add_subdirectory(utils/KillTheDoctor)
endif()
+
+ # Add a global check rule now that all subdirectories have been traversed
+ # and we know the total set of lit testsuites.
+ get_property(LLVM_LIT_TESTSUITES GLOBAL PROPERTY LLVM_LIT_TESTSUITES)
+ get_property(LLVM_LIT_PARAMS GLOBAL PROPERTY LLVM_LIT_PARAMS)
+ get_property(LLVM_LIT_DEPENDS GLOBAL PROPERTY LLVM_LIT_DEPENDS)
+ get_property(LLVM_LIT_EXTRA_ARGS GLOBAL PROPERTY LLVM_LIT_EXTRA_ARGS)
+ add_lit_target(check-all
+ "Running all regression tests"
+ ${LLVM_LIT_TESTSUITES}
+ PARAMS ${LLVM_LIT_PARAMS}
+ DEPENDS ${LLVM_LIT_DEPENDS}
+ ARGS ${LLVM_LIT_EXTRA_ARGS}
+ )
endif()
add_subdirectory(cmake/modules)
PATTERN "*.h"
PATTERN "*.td"
PATTERN "*.inc"
+ PATTERN "LICENSE.TXT"
PATTERN ".svn" EXCLUDE
)
# TODO: make and install documentation.
set(CPACK_PACKAGE_VENDOR "LLVM")
-set(CPACK_PACKAGE_VERSION_MAJOR 2)
-set(CPACK_PACKAGE_VERSION_MINOR 9)
-add_version_info_from_vcs(CPACK_PACKAGE_VERSION_PATCH)
+set(CPACK_PACKAGE_VERSION_MAJOR ${LLVM_VERSION_MAJOR})
+set(CPACK_PACKAGE_VERSION_MINOR ${LLVM_VERSION_MINOR})
+if( LLVM_APPEND_VC_REV )
+ add_version_info_from_vcs(CPACK_PACKAGE_VERSION_PATCH)
+else()
+ set(CPACK_PACKAGE_VERSION_PATCH "svn")
+endif()
+set(CPACK_RESOURCE_FILE_LICENSE "${LLVM_MAIN_SRC_DIR}/LICENSE.TXT")
+if(WIN32 AND NOT UNIX)
+ set(CPACK_PACKAGE_ICON "${LLVM_MAIN_SRC_DIR}\\\\cmake\\\\nsis_logo.bmp")
+ set(CPACK_NSIS_MODIFY_PATH "ON")
+endif()
include(CPack)
# Workaround for MSVS10 to avoid the Dialog Hell