diff --git a/CMakeLists.txt b/CMakeLists.txt
index e3ddb267966352299bcb78a73ed604d0c3181199..f68cd4f1226b51b5c05c4452c34fcfa032e29f5d 100644 (file)
--- a/CMakeLists.txt
+++ b/CMakeLists.txt
project(LLVM)
+# The following only works with the Ninja generator in CMake >= 3.0.
+set(LLVM_PARALLEL_COMPILE_JOBS "" CACHE STRING
+ "Define the maximum number of concurrent compilation jobs.")
+if(LLVM_PARALLEL_COMPILE_JOBS)
+ set_property(GLOBAL APPEND PROPERTY JOB_POOLS compile_job_pool=${LLVM_PARALLEL_COMPILE_JOBS})
+ set(CMAKE_JOB_POOL_COMPILE compile_job_pool)
+endif()
+
+set(LLVM_PARALLEL_LINK_JOBS "" CACHE STRING
+ "Define the maximum number of concurrent link jobs.")
+if(LLVM_PARALLEL_LINK_JOBS)
+ set_property(GLOBAL APPEND PROPERTY JOB_POOLS link_job_pool=${LLVM_PARALLEL_LINK_JOBS})
+ set(CMAKE_JOB_POOL_LINK link_job_pool)
+endif()
+
# Add path for custom modules
set(CMAKE_MODULE_PATH
${CMAKE_MODULE_PATH}
)
set(LLVM_VERSION_MAJOR 3)
-set(LLVM_VERSION_MINOR 6)
+set(LLVM_VERSION_MINOR 7)
set(LLVM_VERSION_PATCH 0)
if (NOT PACKAGE_VERSION)
string(TOUPPER "${CMAKE_BUILD_TYPE}" uppercase_CMAKE_BUILD_TYPE)
+set(LLVM_LIBDIR_SUFFIX "" CACHE STRING "Define suffix of library directory name (32/64)" )
+
# They are used as destination of target generators.
set(LLVM_RUNTIME_OUTPUT_INTDIR ${CMAKE_CURRENT_BINARY_DIR}/${CMAKE_CFG_INTDIR}/bin)
-set(LLVM_LIBRARY_OUTPUT_INTDIR ${CMAKE_CURRENT_BINARY_DIR}/${CMAKE_CFG_INTDIR}/lib)
+set(LLVM_LIBRARY_OUTPUT_INTDIR ${CMAKE_CURRENT_BINARY_DIR}/${CMAKE_CFG_INTDIR}/lib${LLVM_LIBDIR_SUFFIX})
if(WIN32 OR CYGWIN)
# DLL platform -- put DLLs into bin.
set(LLVM_SHLIB_OUTPUT_INTDIR ${LLVM_RUNTIME_OUTPUT_INTDIR})
set(LLVM_EXAMPLES_BINARY_DIR ${LLVM_BINARY_DIR}/examples)
set(LLVM_INCLUDE_DIR ${CMAKE_CURRENT_BINARY_DIR}/include)
-set(LLVM_LIBDIR_SUFFIX "" CACHE STRING "Define suffix of library directory name (32/64)" )
set(LLVM_ALL_TARGETS
AArch64
Hexagon
Mips
MSP430
+ C6000
NVPTX
PowerPC
R600
"Build compiler-rt as an external project." OFF)
option(LLVM_BUILD_LLVM_DYLIB "Build libllvm dynamic library" OFF)
+option(LLVM_DISABLE_LLVM_DYLIB_ATEXIT "Disable llvm-shlib's atexit destructors." ON)
+if(LLVM_DISABLE_LLVM_DYLIB_ATEXIT)
+ set(DISABLE_LLVM_DYLIB_ATEXIT 1)
+endif()
# All options referred to from HandleLLVMOptions have to be specified
# BEFORE this include, otherwise options will not be correctly set on
include(HandleLLVMOptions)
# Verify that we can find a Python 2 interpreter. Python 3 is unsupported.
-set(Python_ADDITIONAL_VERSIONS 2.7 2.6 2.5)
+# FIXME: We should support systems with only Python 3, but that requires work
+# on LLDB.
+set(Python_ADDITIONAL_VERSIONS 2.7)
include(FindPythonInterp)
if( NOT PYTHONINTERP_FOUND )
message(FATAL_ERROR
Please install Python or specify the PYTHON_EXECUTABLE CMake variable.")
endif()
+if( ${PYTHON_VERSION_STRING} VERSION_LESS 2.7 )
+ message(FATAL_ERROR "Python 2.7 or newer is required")
+endif()
+
######
# LLVMBuild Integration
#
# They are not referenced. See set_output_directory().
set( CMAKE_RUNTIME_OUTPUT_DIRECTORY ${LLVM_BINARY_DIR}/bin )
-set( CMAKE_LIBRARY_OUTPUT_DIRECTORY ${LLVM_BINARY_DIR}/lib )
-set( CMAKE_ARCHIVE_OUTPUT_DIRECTORY ${LLVM_BINARY_DIR}/lib )
+set( CMAKE_LIBRARY_OUTPUT_DIRECTORY ${LLVM_BINARY_DIR}/lib${LLVM_LIBDIR_SUFFIX} )
+set( CMAKE_ARCHIVE_OUTPUT_DIRECTORY ${LLVM_BINARY_DIR}/lib${LLVM_LIBDIR_SUFFIX} )
set(CMAKE_BUILD_WITH_INSTALL_RPATH ON)
if (APPLE)
set(CMAKE_INSTALL_RPATH "@executable_path/../lib")
else(UNIX)
if(NOT DEFINED CMAKE_INSTALL_RPATH)
- set(CMAKE_INSTALL_RPATH "\$ORIGIN/../lib")
+ set(CMAKE_INSTALL_RPATH "\$ORIGIN/../lib${LLVM_LIBDIR_SUFFIX}")
if (${CMAKE_SYSTEM_NAME} MATCHES FreeBSD)
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -Wl,-z,origin")
set(CMAKE_SHARED_LINKER_FLAGS "${CMAKE_SHARED_LINKER_FLAGS} -Wl,-z,origin")
add_subdirectory(utils/unittest)
endif()
+foreach( binding ${LLVM_BINDINGS_LIST} )
+ if( EXISTS "${LLVM_MAIN_SRC_DIR}/bindings/${binding}/CMakeLists.txt" )
+ add_subdirectory(bindings/${binding})
+ endif()
+endforeach()
+
add_subdirectory(projects)
if(WITH_POLLY)