diff --git a/Makefile.common b/Makefile.common
index 18a4ace19fd00ef3cd0752ba9404db256868ad81..a157abaef274178cbfb12efda11b5230a73b9a5e 100644 (file)
--- a/Makefile.common
+++ b/Makefile.common
#===-- Makefile.common - Common make rules for LLVM --------*- Makefile -*--===#
-#
+#
# The LLVM Compiler Infrastructure
#
# This file is distributed under the University of Illinois Open Source
# License. See LICENSE.TXT for details.
-#
+#
#===------------------------------------------------------------------------===#
#
# This file is included by all of the LLVM makefiles. This file defines common
# The following functionality can be set by setting incoming variables.
# The variable $(LEVEL) *must* be set:
#
-# 1. LEVEL - The level of the current subdirectory from the top of the
-# source directory. This level should be expressed as a path, for
+# 1. LEVEL - The level of the current subdirectory from the top of the
+# source directory. This level should be expressed as a path, for
# example, ../.. for two levels deep.
#
# 2. DIRS - A list of subdirectories to be built. Fake targets are set up
# built in any order. All DIRS are built in order before PARALLEL_DIRS are
# built, which are then built in any order.
#
-# 4. Source - If specified, this sets the source code filenames. If this
-# is not set, it defaults to be all of the .cpp, .c, .y, and .l files
-# in the current directory. Also, if you want to build files in addition
-# to the local files, you can use the ExtraSource variable
+# 4. SOURCES - If specified, this sets the source code filenames. If this
+# is not set, it defaults to be all of the .cpp, .c, .y, and .l files
+# in the current directory.
#
# 5. SourceDir - If specified, this specifies a directory that the source files
# are in, if they are not in the current directory. This should include a
#
# Configuration file to set paths specific to local installation of LLVM
-#
+#
ifndef LLVM_OBJ_ROOT
include $(LEVEL)/Makefile.config
else