diff --git a/Makefile.common b/Makefile.common
index 2b0a6968d06b5b1ad67b5c887fb7012c860dde15..a157abaef274178cbfb12efda11b5230a73b9a5e 100644 (file)
--- a/Makefile.common
+++ b/Makefile.common
#===-- Makefile.common - Common make rules for LLVM --------*- Makefile -*--===#
-#
+#
# The LLVM Compiler Infrastructure
#
-# This file was developed by the LLVM research group and is distributed under
-# the University of Illinois Open Source License. See LICENSE.TXT for details.
-#
+# This file is distributed under the University of Illinois Open Source
+# License. See LICENSE.TXT for details.
+#
#===------------------------------------------------------------------------===#
#
# This file is included by all of the LLVM makefiles. This file defines common
# The following functionality can be set by setting incoming variables.
# The variable $(LEVEL) *must* be set:
#
-# 1. LEVEL - The level of the current subdirectory from the top of the
-# source directory. This level should be expressed as a path, for
+# 1. LEVEL - The level of the current subdirectory from the top of the
+# source directory. This level should be expressed as a path, for
# example, ../.. for two levels deep.
#
# 2. DIRS - A list of subdirectories to be built. Fake targets are set up
# built in any order. All DIRS are built in order before PARALLEL_DIRS are
# built, which are then built in any order.
#
-# 4. Source - If specified, this sets the source code filenames. If this
-# is not set, it defaults to be all of the .cpp, .c, .y, and .l files
-# in the current directory. Also, if you want to build files in addition
-# to the local files, you can use the ExtraSource variable
+# 4. SOURCES - If specified, this sets the source code filenames. If this
+# is not set, it defaults to be all of the .cpp, .c, .y, and .l files
+# in the current directory.
#
# 5. SourceDir - If specified, this specifies a directory that the source files
# are in, if they are not in the current directory. This should include a
#
# 6. LLVM_SRC_ROOT - If specified, points to the top of the LLVM source tree.
#
-# 8. BUILD_SRC_DIR - The directory which contains the current set of Makefiles
+# 8. PROJ_SRC_DIR - The directory which contains the current set of Makefiles
# and usually the source code too (unless SourceDir is set).
#
-# 9. BUILD_SRC_ROOT - The root directory of the source code being compiled.
+# 9. PROJ_SRC_ROOT - The root directory of the source code being compiled.
#
-# 10. BUILD_OBJ_DIR - The directory where object code should be placed.
+# 10. PROJ_OBJ_DIR - The directory where object code should be placed.
#
-# 11. BUILD_OBJ_ROOT - The root directory for where object code should be
+# 11. PROJ_OBJ_ROOT - The root directory for where object code should be
# placed.
#
# For building,
-# LLVM, LLVM_SRC_ROOT = BUILD_SRC_ROOT
+# LLVM, LLVM_SRC_ROOT = PROJ_SRC_ROOT
#
#===-----------------------------------------------------------------------====
#
# Configuration file to set paths specific to local installation of LLVM
-#
+#
+ifndef LLVM_OBJ_ROOT
include $(LEVEL)/Makefile.config
+else
+include $(LLVM_OBJ_ROOT)/Makefile.config
+endif
#
# Include all of the build rules used for making LLVM