diff --git a/Makefile.common b/Makefile.common
index 55e2b63434c8f70d621417581a2effa19b3dce63..a157abaef274178cbfb12efda11b5230a73b9a5e 100644 (file)
--- a/Makefile.common
+++ b/Makefile.common
# built in any order. All DIRS are built in order before PARALLEL_DIRS are
# built, which are then built in any order.
#
-# 4. Source - If specified, this sets the source code filenames. If this
+# 4. SOURCES - If specified, this sets the source code filenames. If this
# is not set, it defaults to be all of the .cpp, .c, .y, and .l files
# in the current directory.
#