diff --git a/Makefile.common b/Makefile.common
index 88cdd97c00ad647ff2ab321d11251ad382590497..a157abaef274178cbfb12efda11b5230a73b9a5e 100644 (file)
--- a/Makefile.common
+++ b/Makefile.common
-#===-- Makefile.common - Common make rules for LLVM -------*- makefile -*--====
+#===-- Makefile.common - Common make rules for LLVM --------*- Makefile -*--===#
+#
+# The LLVM Compiler Infrastructure
+#
+# This file is distributed under the University of Illinois Open Source
+# License. See LICENSE.TXT for details.
+#
+#===------------------------------------------------------------------------===#
#
# This file is included by all of the LLVM makefiles. This file defines common
-# rules to do things like compile a .cpp file or generate dependancy info.
-# These are platform dependant, so this is the file used to specify these
-# system dependant operations.
+# rules to do things like compile a .cpp file or generate dependency info.
+# These are platform dependent, so this is the file used to specify these
+# system dependent operations.
#
# The following functionality can be set by setting incoming variables.
# The variable $(LEVEL) *must* be set:
#
-# 1. LEVEL - The level of the current subdirectory from the top of the
-# MagicStats view. This level should be expressed as a path, for
+# 1. LEVEL - The level of the current subdirectory from the top of the
+# source directory. This level should be expressed as a path, for
# example, ../.. for two levels deep.
#
# 2. DIRS - A list of subdirectories to be built. Fake targets are set up
# built in any order. All DIRS are built in order before PARALLEL_DIRS are
# built, which are then built in any order.
#
-# 4. Source - If specified, this sets the source code filenames. If this
-# is not set, it defaults to be all of the .cpp, .c, .y, and .l files
-# in the current directory. Also, if you want to build files in addition
-# to the local files, you can use the ExtraSource variable
+# 4. SOURCES - If specified, this sets the source code filenames. If this
+# is not set, it defaults to be all of the .cpp, .c, .y, and .l files
+# in the current directory.
#
# 5. SourceDir - If specified, this specifies a directory that the source files
# are in, if they are not in the current directory. This should include a
# trailing / character.
#
-# 6. PROJ_COMPILE - If set to 1, then this makefile can also be used to
-# compile other projects using llvm. Note if this option is set then the
-# following *must* hold
-# PROJLEVEL should be set to the top of the source directory for the
-# project files
-# LEVEL should be set to the top of LLVM source tree
-# LLVM_LIB_DIR should be set to the top of the LLVM build tree
-#
-#===-----------------------------------------------------------------------====
-
-#
-# Configuration file to set paths specific to local installation of LLVM
-#
-include $(LEVEL)/Makefile.config
-
-###########################################################################
-# Directory Configuration
-# This section of the Makefile determines what is where. To be
-# specific, there are several locations that need to be defined:
-#
-# o LLVM_SRC_ROOT : The root directory of the LLVM source code.
-# o LLVM_OBJ_ROOT : The root directory containing the built LLVM code.
+# 6. LLVM_SRC_ROOT - If specified, points to the top of the LLVM source tree.
#
-# o BUILD_SRC_DIR : The directory containing the code to build.
-# o BUILD_SRC_ROOT : The root directory of the code to build.
+# 8. PROJ_SRC_DIR - The directory which contains the current set of Makefiles
+# and usually the source code too (unless SourceDir is set).
#
-# o BUILD_OBJ_DIR : The directory in which compiled code will be placed.
-# o BUILD_OBJ_ROOT : The root directory in which compiled code is placed.
+# 9. PROJ_SRC_ROOT - The root directory of the source code being compiled.
#
-###########################################################################
-
-#
-# Set the source build directory. That is almost always the current directory.
+# 10. PROJ_OBJ_DIR - The directory where object code should be placed.
#
-ifndef BUILD_SRC_DIR
-BUILD_SRC_DIR = $(shell pwd)
-endif
-
+# 11. PROJ_OBJ_ROOT - The root directory for where object code should be
+# placed.
#
-# Set the source root directory.
+# For building,
+# LLVM, LLVM_SRC_ROOT = PROJ_SRC_ROOT
#
-ifndef BUILD_SRC_ROOT
-BUILD_SRC_ROOT = $(shell cd $(BUILD_SRC_DIR)/$(LEVEL); pwd)
-endif
-
-#
-# Set the object build directory. Its location depends upon the source path
-# and where object files should go.
-#
-ifndef BUILD_OBJ_DIR
-ifeq ($(OBJ_ROOT),.)
-BUILD_OBJ_DIR = $(shell pwd)
-else
-BUILD_OBJ_DIR := $(OBJ_ROOT)$(patsubst $(shell dirname $(BUILD_SRC_ROOT))%,%,$(shell cd $(BUILD_SRC_DIR); pwd))
-endif
-endif
-
-#
-# Set the root of the object directory.
-#
-ifndef BUILD_OBJ_ROOT
-ifeq ($(OBJ_ROOT),.)
-BUILD_OBJ_ROOT = $(shell cd $(LEVEL); pwd)
-else
-BUILD_OBJ_ROOT := $(OBJ_ROOT)$(patsubst $(shell dirname $(BUILD_SRC_ROOT))%,%,$(shell cd $(BUILD_SRC_ROOT); pwd))
-endif
-endif
-
-#
-# Set the LLVM source directory.
-# It is typically the root directory of what we're compiling now.
-#
-ifndef LLVM_SRC_ROOT
-LLVM_SRC_ROOT = $(BUILD_SRC_ROOT)
-endif
+#===-----------------------------------------------------------------------====
#
-# Set the LLVM object directory.
+# Configuration file to set paths specific to local installation of LLVM
#
ifndef LLVM_OBJ_ROOT
-LLVM_OBJ_ROOT = $(BUILD_OBJ_ROOT)
-endif
-
-# Figure out how to do platform specific stuff on this platform. This is really
-# gross and should be autoconfiscated (automake actually), but should hopefully
-# work on Linux and solaris (SunOS).
-#
-UNAME := $(shell uname)
-include $(LLVM_SRC_ROOT)/Makefile.$(UNAME)
-
-ifdef SHARED_LIBRARY
-# if SHARED_LIBRARY is specified, the default is to build the dynamic lib
-dynamic ::
-endif
-
-# Default Rule: Make sure it's also a :: rule
-all ::
-
-# Default for install is to at least build everything...
-install ::
-
-# Default rule for test. It ensures everything has a test rule
-test::
-
-#--------------------------------------------------------------------
-# Variables derived from configuration options...
-#--------------------------------------------------------------------
-
-#BinInstDir=/usr/local/bin
-#LibInstDir=/usr/local/lib/xxx
-#DocInstDir=/usr/doc/xxx
-
-BURG_OPTS = -I
-
-PURIFY := $(PURIFY) -cache-dir="$(BUILD_OBJ_ROOT)/../purifycache" -chain-length="30" -messages=all
-
-ifdef ENABLE_PROFILING
- ENABLE_OPTIMIZED = 1
- CONFIGURATION := Profile
-else
- ifdef ENABLE_OPTIMIZED
- CONFIGURATION := Release
- else
- CONFIGURATION := Debug
- endif
-endif
-
-###########################################################################
-# Library Locations
-# These variables describe various library locations:
-#
-# DEST* = Location of where libraries that are built will be placed.
-# LLVM* = Location of LLVM libraries used for linking.
-# PROJ* = Location of previously built libraries used for linking.
-###########################################################################
-
-# Libraries that are being built
-DESTLIBDEBUG := $(BUILD_OBJ_ROOT)/lib/Debug
-DESTLIBRELEASE := $(BUILD_OBJ_ROOT)/lib/Release
-DESTLIBPROFILE := $(BUILD_OBJ_ROOT)/lib/Profile
-DESTLIBCURRENT := $(BUILD_OBJ_ROOT)/lib/$(CONFIGURATION)
-
-# LLVM libraries used for linking
-LLVMLIBDEBUGSOURCE := $(LLVM_OBJ_ROOT)/lib/Debug
-LLVMLIBRELEASESOURCE := $(LLVM_OBJ_ROOT)/lib/Release
-LLVMLIBPROFILESOURCE := $(LLVM_OBJ_ROOT)/lib/Profile
-LLVMLIBCURRENTSOURCE := $(LLVM_OBJ_ROOT)/lib/$(CONFIGURATION)
-
-# Libraries that were built that will now be used for linking
-PROJLIBDEBUGSOURCE := $(BUILD_OBJ_ROOT)/lib/Debug
-PROJLIBRELEASESOURCE := $(BUILD_OBJ_ROOT)/lib/Release
-PROJLIBPROFILESOURCE := $(BUILD_OBJ_ROOT)/lib/Profile
-PROJLIBCURRENTSOURCE := $(BUILD_OBJ_ROOT)/lib/$(CONFIGURATION)
-
-###########################################################################
-# Tool Locations
-# These variables describe various tool locations:
-#
-# DEST* = Location of where tools that are built will be placed.
-# LLVM* = Location of LLVM tools used for building.
-# PROJ* = Location of previously built tools used for linking.
-###########################################################################
-
-DESTTOOLDEBUG := $(BUILD_OBJ_ROOT)/tools/Debug
-DESTTOOLRELEASE := $(BUILD_OBJ_ROOT)/tools/Release
-DESTTOOLPROFILE := $(BUILD_OBJ_ROOT)/tools/Profile
-DESTTOOLCURRENT := $(BUILD_OBJ_ROOT)/tools/$(CONFIGURATION)
-
-LLVMTOOLDEBUG := $(LLVM_OBJ_ROOT)/tools/Debug
-LLVMTOOLRELEASE := $(LLVM_OBJ_ROOT)/tools/Release
-LLVMTOOLPROFILE := $(LLVM_OBJ_ROOT)/tools/Profile
-LLVMTOOLCURRENT := $(LLVM_OBJ_ROOT)/tools/$(CONFIGURATION)
-
-PROJTOOLDEBUG := $(BUILD_OBJ_ROOT)/tools/Debug
-PROJTOOLRELEASE := $(BUILD_OBJ_ROOT)/tools/Release
-PROJTOOLPROFILE := $(BUILD_OBJ_ROOT)/tools/Profile
-PROJTOOLCURRENT := $(BUILD_OBJ_ROOT)/tools/$(CONFIGURATION)
-
-# Verbosity levels
-ifndef VERBOSE
-VERB := @
-endif
-
-#---------------------------------------------------------
-# Compilation options...
-#---------------------------------------------------------
-
-###########################################################################
-# Special tools used while building the LLVM tree. Burg is built as part of the
-# utils directory.
-###########################################################################
-BURG := $(LLVMTOOLCURRENT)/burg
-RunBurg := $(BURG) $(BURG_OPTS)
-
-TBLGEN := $(LLVMTOOLCURRENT)/tblgen
-
-# Enable this for profiling support with 'gprof'
-# This automatically enables optimized builds.
-ifdef ENABLE_PROFILING
- PROFILE = -pg
-endif
-
-###########################################################################
-# Compile Time Flags
-###########################################################################
-
-#
-# Include both the project headers and the LLVM headers for compilation
-#
-CPPFLAGS += -I$(BUILD_SRC_ROOT)/include -I$(LLVM_SRC_ROOT)/include
-
-# By default, strip symbol information from executable
-ifndef KEEP_SYMBOLS
-STRIP = $(PLATFORMSTRIPOPTS)
-STRIP_WARN_MSG = "(without symbols) "
-endif
-
-# Allow gnu extensions...
-CPPFLAGS += -D_GNU_SOURCE
-
-# -Wno-unused-parameter
-CompileCommonOpts := -Wall -W -Wwrite-strings -Wno-unused -I$(LEVEL)/include
-CompileOptimizeOpts := -O3 -DNDEBUG -finline-functions -fshort-enums
-
-# Compile a cpp file, don't link...
-Compile := $(CXX) -c $(CPPFLAGS) $(CXXFLAGS) $(CompileCommonOpts)
-CompileG := $(Compile) -g -D_DEBUG
-CompileO := $(Compile) $(CompileOptimizeOpts) -felide-constructors -fomit-frame-pointer
-CompileP := $(Compile) $(CompileOptimizeOpts) -felide-constructors $(PROFILE)
-
-# Compile a c file, don't link...
-CompileC := $(CC) -c $(CPPFLAGS) $(CCFLAGS) $(CompileCommonOpts)
-CompileCG := $(CompileC) -g -D_DEBUG
-CompileCO := $(CompileC) $(CompileOptimizeOpts) -fomit-frame-pointer
-CompileCP := $(CompileC) $(CompileOptimizeOpts) $(PROFILE)
-
-
-# Link final executable
-
-ifdef ENABLE_PURIFY # To enable purify, build with 'gmake ENABLE_PURIFY=1'
-Link := $(PURIFY) $(CXX) -static
-else
-Link := $(CXX)
-endif
-
-ifdef PROJ_COMPILE
-# include both projlib source and llvmlib source
-LinkG := $(Link) -g -L$(PROJLIBDEBUGSOURCE) -L$(LLVMLIBDEBUGSOURCE) $(STRIP)
-LinkO := $(Link) -O3 -L$(PROJLIBRELEASESOURCE) -L$(LLVMLIBRELEASESOURCE)
-LinkP := $(Link) -O3 -L$(PROJLIBPROFILESOURCE) -L$(LLVMLIBPROFILESOURCE) $(PROFILE)
+include $(LEVEL)/Makefile.config
else
-LinkG := $(Link) -g -L$(LLVMLIBDEBUGSOURCE) $(STRIP)
-LinkO := $(Link) -O3 -L$(LLVMLIBRELEASESOURCE)
-LinkP := $(Link) -O3 -L$(LLVMLIBPROFILESOURCE) $(PROFILE)
-endif
-
-
-
-# Create one .o file from a bunch of .o files...
-Relink = ${LD} -r
-
-# MakeSO - Create a .so file from a .o files...
-MakeSO := $(CXX) $(MakeSharedObjectOption)
-MakeSOO := $(MakeSO) -O3
-MakeSOP := $(MakeSOO) $(PROFILE)
-
-# Create dependancy file from CPP file, send to stdout.
-Depend := $(CXX) -MM -I$(LEVEL)/include $(CPPFLAGS)
-DependC := $(CC) -MM -I$(LEVEL)/include $(CPPFLAGS)
-
-# Archive a bunch of .o files into a .a file...
-AR = ${AR_PATH} cq
-
-#----------------------------------------------------------
-
-# Source includes all of the cpp files, and objects are derived from the
-# source files...
-# The local Makefile can list other Source files via ExtraSource = ...
-#
-ifndef Source
-Source := $(ExtraSource) $(wildcard *.cpp *.c *.y *.l)
-endif
-
-Objs := $(sort $(patsubst Debug/%.o, %.o, $(addsuffix .o,$(notdir $(basename $(Source))))))
-ObjectsO := $(addprefix $(BUILD_OBJ_DIR)/Release/,$(Objs))
-ObjectsP := $(addprefix $(BUILD_OBJ_DIR)/Profile/,$(Objs))
-ObjectsG := $(addprefix $(BUILD_OBJ_DIR)/Debug/,$(Objs))
-
-
-#---------------------------------------------------------
-# Handle the DIRS and PARALLEL_DIRS options
-#---------------------------------------------------------
-
-ifdef DIRS
-all install clean test ::
- $(VERB) for dir in ${DIRS}; do \
- (cd $$dir; $(MAKE) $@) || exit 1; \
- done
-endif
-
-# Handle PARALLEL_DIRS
-ifdef PARALLEL_DIRS
-all :: $(addsuffix /.makeall , $(PARALLEL_DIRS))
-install :: $(addsuffix /.makeinstall, $(PARALLEL_DIRS))
-clean :: $(addsuffix /.makeclean , $(PARALLEL_DIRS))
-test :: $(addsuffix /.maketest , $(PARALLEL_DIRS))
-
-%/.makeall %/.makeinstall %/.makeclean %/.maketest:
- $(VERB) cd $(@D); $(MAKE) $(subst $(@D)/.make,,$@)
-endif
-
-ifdef OPTIONAL_DIRS
-all install clean test ::
- $(VERB) for dir in ${OPTIONAL_DIRS}; do \
- if [ -d $$dir ]; \
- then\
- (cd $$dir; $(MAKE) $@) || exit 1; \
- fi \
- done
+include $(LLVM_OBJ_ROOT)/Makefile.config
endif
-#---------------------------------------------------------
-# Handle the LIBRARYNAME option - used when building libs...
-#---------------------------------------------------------
#
-# When libraries are built, they are allowed to optionally define the
-# DONT_BUILD_RELINKED make variable, which, when defined, prevents a .o file
-# from being built for the library. This .o files may then be linked to by a
-# tool if the tool does not need (or want) the semantics a .a file provides
-# (linking in only object files that are "needed"). If a library is never to
-# be used in this way, it is better to define DONT_BUILD_RELINKED, and define
-# BUILD_ARCHIVE instead.
+# Include all of the build rules used for making LLVM
#
-# Some libraries must be built as .a files (libscalar for example) because if
-# it's built as a .o file, then all of the constituent .o files in it will be
-# linked into tools (for example gccas) even if they only use one of the parts
-# of it. For this reason, sometimes it's useful to use libraries as .a files.
-
-ifdef LIBRARYNAME
-
-# Make sure there isn't any extranous whitespace on the LIBRARYNAME option
-LIBRARYNAME := $(strip $(LIBRARYNAME))
-
-LIBNAME_O := $(DESTLIBRELEASE)/lib$(LIBRARYNAME).so
-LIBNAME_P := $(DESTLIBPROFILE)/lib$(LIBRARYNAME).so
-LIBNAME_G := $(DESTLIBDEBUG)/lib$(LIBRARYNAME).so
-LIBNAME_AO := $(DESTLIBRELEASE)/lib$(LIBRARYNAME).a
-LIBNAME_AP := $(DESTLIBPROFILE)/lib$(LIBRARYNAME).a
-LIBNAME_AG := $(DESTLIBDEBUG)/lib$(LIBRARYNAME).a
-LIBNAME_OBJO := $(DESTLIBRELEASE)/$(LIBRARYNAME).o
-LIBNAME_OBJP := $(DESTLIBPROFILE)/$(LIBRARYNAME).o
-LIBNAME_OBJG := $(DESTLIBDEBUG)/$(LIBRARYNAME).o
-
-# dynamic target builds a shared object version of the library...
-dynamic:: $(DESTLIBCURRENT)/lib$(LIBRARYNAME).so
-
-# Does the library want a .o version built?
-ifndef DONT_BUILD_RELINKED
-all:: $(DESTLIBCURRENT)/$(LIBRARYNAME).o
-endif
-
-# Does the library want an archive version built?
-ifdef BUILD_ARCHIVE
-all:: $(DESTLIBCURRENT)/lib$(LIBRARYNAME).a
-endif
-
-$(LIBNAME_O): $(ObjectsO) $(LibSubDirs) $(DESTLIBRELEASE)/.dir
- @echo ======= Linking $(LIBRARYNAME) release library =======
- $(VERB) $(MakeSOO) -o $@ $(ObjectsO) $(LibSubDirs) $(LibLinkOpts)
-
-$(LIBNAME_P): $(ObjectsP) $(LibSubDirs) $(DESTLIBPROFILE)/.dir
- @echo ======= Linking $(LIBRARYNAME) profile library =======
- $(VERB) $(MakeSOP) -o $@ $(ObjectsP) $(LibSubDirs) $(LibLinkOpts)
-
-$(LIBNAME_G): $(ObjectsG) $(LibSubDirs) $(DESTLIBDEBUG)/.dir
- @echo ======= Linking $(LIBRARYNAME) debug library =======
- $(VERB) $(MakeSO) -g -o $@ $(ObjectsG) $(LibSubDirs) $(LibLinkOpts)
-
-$(LIBNAME_AO): $(ObjectsO) $(LibSubDirs) $(DESTLIBRELEASE)/.dir
- @echo ======= Linking $(LIBRARYNAME) release library =======
- @rm -f $@
- $(VERB) $(AR) $@ $(ObjectsO) $(LibSubDirs)
-
-$(LIBNAME_AP): $(ObjectsP) $(LibSubDirs) $(DESTLIBPROFILE)/.dir
- @echo ======= Linking $(LIBRARYNAME) profile library =======
- @rm -f $@
- $(VERB) $(AR) $@ $(ObjectsP) $(LibSubDirs)
-
-$(LIBNAME_AG): $(ObjectsG) $(LibSubDirs) $(DESTLIBDEBUG)/.dir
- @echo ======= Linking $(LIBRARYNAME) debug library =======
- @rm -f $@
- $(VERB) $(AR) $@ $(ObjectsG) $(LibSubDirs)
-
-$(LIBNAME_OBJO): $(ObjectsO) $(LibSubDirs) $(DESTLIBRELEASE)/.dir
- @echo "Linking $@"
- $(VERB) $(Relink) -o $@ $(ObjectsO) $(LibSubDirs)
-
-$(LIBNAME_OBJP): $(ObjectsP) $(LibSubDirs) $(DESTLIBPROFILE)/.dir
- @echo "Linking $@"
- $(VERB) $(Relink) -o $@ $(ObjectsP) $(LibSubDirs)
-
-$(LIBNAME_OBJG): $(ObjectsG) $(LibSubDirs) $(DESTLIBDEBUG)/.dir
- @echo "Linking $@"
- $(VERB) $(Relink) -o $@ $(ObjectsG) $(LibSubDirs)
-
-endif
-
-#------------------------------------------------------------------------
-# Create a TAGS database for emacs
-#------------------------------------------------------------------------
-
-ifeq ($(LEVEL), .)
-tags:
- etags -l c++ `find include lib tools -name '*.cpp' -o -name '*.h'`
-all:: tags
-endif
-
-#------------------------------------------------------------------------
-# Handle the TOOLNAME option - used when building tool executables...
-#------------------------------------------------------------------------
-#
-# The TOOLNAME option should be used with a USEDLIBS variable that tells the
-# libraries (and the order of the libs) that should be linked to the
-# tool. USEDLIBS should contain a list of library names (some with .a extension)
-# that are automatically linked in as .o files unless the .a suffix is added.
-#
-ifdef TOOLNAME
-
-# TOOLEXENAME* - These compute the output filenames to generate...
-TOOLEXENAME_G := $(DESTTOOLDEBUG)/$(TOOLNAME)
-TOOLEXENAME_O := $(DESTTOOLRELEASE)/$(TOOLNAME)
-TOOLEXENAME_P := $(DESTTOOLPROFILE)/$(TOOLNAME)
-TOOLEXENAMES := $(DESTTOOLCURRENT)/$(TOOLNAME)
+include $(LLVM_SRC_ROOT)/Makefile.rules
-# USED_LIBS_OPTIONS - Compute the options line that add -llib1 -llib2, etc.
-PROJ_LIBS_OPTIONS := $(patsubst %.a.o, -l%, $(addsuffix .o, $(USEDLIBS)))
-PROJ_LIBS_OPTIONS_G := $(patsubst %.o, $(PROJLIBDEBUGSOURCE)/%.o, $(PROJ_LIBS_OPTIONS))
-PROJ_LIBS_OPTIONS_O := $(patsubst %.o, $(PROJLIBRELEASESOURCE)/%.o,$(PROJ_LIBS_OPTIONS))
-PROJ_LIBS_OPTIONS_P := $(patsubst %.o, $(PROJLIBPROFILESOURCE)/%.o,$(PROJ_LIBS_OPTIONS))
-
-LLVM_LIBS_OPTIONS := $(patsubst %.a.o, -l%, $(addsuffix .o, $(LLVMLIBS)))
-LLVM_LIBS_OPTIONS_G := $(patsubst %.o, $(LLVMLIBDEBUGSOURCE)/%.o, $(LLVM_LIBS_OPTIONS))
-LLVM_LIBS_OPTIONS_O := $(patsubst %.o, $(LLVMLIBRELEASESOURCE)/%.o,$(LLVM_LIBS_OPTIONS))
-LLVM_LIBS_OPTIONS_P := $(patsubst %.o, $(LLVMLIBPROFILESOURCE)/%.o,$(LLVM_LIBS_OPTIONS))
-
-LIB_OPTS_G := $(LLVM_LIBS_OPTIONS_G) $(PROJ_LIBS_OPTIONS_G)
-LIB_OPTS_O := $(LLVM_LIBS_OPTIONS_O) $(PROJ_LIBS_OPTIONS_O)
-LIB_OPTS_P := $(LLVM_LIBS_OPTIONS_P) $(PROJ_LIBS_OPTIONS_P)
-
-# USED_LIB_PATHS - Compute the path of the libraries used so that tools are
-# rebuilt if libraries change. This has to make sure to handle .a/.so and .o
-# files seperately.
-#
-STATICUSEDLIBS := $(patsubst %.a.o, lib%.a, $(addsuffix .o, $(USEDLIBS)))
-USED_LIB_PATHS_G := $(addprefix $(DESTLIBDEBUG)/, $(STATICUSEDLIBS))
-USED_LIB_PATHS_O := $(addprefix $(DESTLIBRELEASE)/, $(STATICUSEDLIBS))
-USED_LIB_PATHS_P := $(addprefix $(DESTLIBPROFILE)/, $(STATICUSEDLIBS))
-LINK_OPTS := $(TOOLLINKOPTS) $(PLATFORMLINKOPTS)
-
-
-
-
-
-
-# Tell make that we need to rebuild subdirectories before we can link the tool.
-# This affects things like LLI which has library subdirectories.
-$(USED_LIB_PATHS_G) $(USED_LIB_PATHS_O) $(USED_LIB_PATHS_P): \
- $(addsuffix /.makeall, $(PARALLEL_DIRS))
-
-all:: $(TOOLEXENAMES)
-
-clean::
- $(VERB) rm -f $(TOOLEXENAMES)
-
-$(TOOLEXENAME_G): $(ObjectsG) $(USED_LIB_PATHS_G) $(DESTTOOLDEBUG)/.dir
- @echo ======= Linking $(TOOLNAME) debug executable $(STRIP_WARN_MSG)=======
- $(VERB) $(LinkG) -o $@ $(ObjectsG) $(LIB_OPTS_G) $(LINK_OPTS)
-
-$(TOOLEXENAME_O): $(ObjectsO) $(USED_LIB_PATHS_O) $(DESTTOOLRELEASE)/.dir
- @echo ======= Linking $(TOOLNAME) release executable =======
- $(VERB) $(LinkO) -o $@ $(ObjectsO) $(LIB_OPTS_O) $(LINK_OPTS)
-
-$(TOOLEXENAME_P): $(ObjectsP) $(USED_LIB_PATHS_P) $(DESTTOOLPROFILE)/.dir
- @echo ======= Linking $(TOOLNAME) profile executable =======
- $(VERB) $(LinkP) -o $@ $(ObjectsP) $(LIB_OPTS_P) $(LINK_OPTS)
-
-endif
-
-
-
-#---------------------------------------------------------
-.PRECIOUS: $(BUILD_OBJ_DIR)/Depend/.dir
-.PRECIOUS: $(BUILD_OBJ_DIR)/Debug/.dir $(BUILD_OBJ_DIR)/Release/.dir
-
-# Create .o files in the ObjectFiles directory from the .cpp and .c files...
-$(BUILD_OBJ_DIR)/Release/%.o: $(SourceDir)%.cpp $(BUILD_OBJ_DIR)/Release/.dir
- @echo "Compiling $<"
- $(VERB) $(CompileO) $< -o $@
-
-$(BUILD_OBJ_DIR)/Release/%.o: $(SourceDir)%.c $(BUILD_OBJ_DIR)/Release/.dir
- $(VERB) $(CompileCO) $< -o $@
-
-$(BUILD_OBJ_DIR)/Profile/%.o: $(SourceDir)%.cpp $(BUILD_OBJ_DIR)/Profile/.dir
- @echo "Compiling $<"
- $(VERB) $(CompileP) $< -o $@
-
-$(BUILD_OBJ_DIR)/Profile/%.o: $(SourceDir)%.c $(BUILD_OBJ_DIR)/Profile/.dir
- @echo "Compiling $<"
- $(VERB) $(CompileCP) $< -o $@
-
-$(BUILD_OBJ_DIR)/Debug/%.o: $(SourceDir)%.cpp $(BUILD_OBJ_DIR)/Debug/.dir
- @echo "Compiling $<"
- $(VERB) $(CompileG) $< -o $@
-
-$(BUILD_OBJ_DIR)/Debug/%.o: $(SourceDir)%.c $(BUILD_OBJ_DIR)/Debug/.dir
- $(VERB) $(CompileCG) $< -o $@
-
-#
-# Rules for building lex/yacc files
-#
-LEX_FILES = $(filter %.l, $(Source))
-LEX_OUTPUT = $(LEX_FILES:%.l=%.cpp)
-YACC_FILES = $(filter %.y, $(Source))
-YACC_OUTPUT = $(addprefix $(YACC_FILES:%.y=%), .h .cpp .output)
-.PRECIOUS: $(LEX_OUTPUT) $(YACC_OUTPUT)
-
-# Create a .cpp source file from a flex input file... this uses sed to cut down
-# on the warnings emited by GCC...
-#
-# The last line is a gross hack to work around flex aparently not being able to
-# resize the buffer on a large token input. Currently, for uninitialized string
-# buffers in LLVM we can generate very long tokens, so this is a hack around it.
-# FIXME. (f.e. char Buffer[10000]; )
-#
-%.cpp: %.l
- $(FLEX) -t $< | sed '/^find_rule/d' | \
- sed 's/void yyunput/inline void yyunput/' | \
- sed 's/void \*yy_flex_realloc/inline void *yy_flex_realloc/' | \
- sed 's/#define YY_BUF_SIZE 16384/#define YY_BUF_SIZE (16384*64)/' > $@
-
-# Rule for building the bison parsers...
-%.c: %.y # Cancel built-in rules for yacc
-%.h: %.y # Cancel built-in rules for yacc
-%.cpp %.h : %.y
- @echo Bison\'ing $<...
- $(VERB) $(BISON) -v -d -p $(<:%Parser.y=%) $*.y
- $(VERB) mv -f $*.tab.c $*.cpp
- $(VERB) mv -f $*.tab.h $*.h
-
-# To create the directories...
-%/.dir:
- $(VERB) mkdir -p $*
- @date > $@
-
-# To create postscript files from dot files...
-%.ps: %.dot
- dot -Tps < $< > $@
-
-# 'make clean' nukes the tree
-clean::
- $(VERB) rm -rf $(BUILD_OBJ_DIR)/Debug $(BUILD_OBJ_DIR)/Release $(BUILD_OBJ_DIR)/Profile $(BUILD_OBJ_DIR)/Depend
- $(VERB) rm -f core core.[0-9][0-9]* *.o *.d *.so *~ *.flc
- $(VERB) rm -f $(LEX_OUTPUT) $(YACC_OUTPUT)
-
-# If dependencies were generated for the file that included this file,
-# include the dependancies now...
-#
-SourceBaseNames := $(basename $(notdir $(filter-out Debug/%, $(Source))))
-SourceDepend := $(SourceBaseNames:%=$(BUILD_OBJ_DIR)/Depend/%.d)
-
-# Create dependencies for the *.cpp files...
-#$(SourceDepend): \x
-$(BUILD_OBJ_DIR)/Depend/%.d: $(SourceDir)%.cpp $(BUILD_OBJ_DIR)/Depend/.dir
- $(VERB) $(Depend) $< | sed 's|$*\.o *|$(BUILD_OBJ_DIR)/Release/& $(BUILD_OBJ_DIR)/Profile/& $(BUILD_OBJ_DIR)/Debug/& $(BUILD_OBJ_DIR)/Depend/$(@F)|g' > $@
-
-# Create dependencies for the *.c files...
-#$(SourceDepend): \x
-$(BUILD_OBJ_DIR)/Depend/%.d: $(SourceDir)%.c $(BUILD_OBJ_DIR)/Depend/.dir
- $(VERB) $(DependC) $< | sed 's|$*\.o *|Release/& Profile/& Debug/& Depend/$(@F)|g' > $@
-
-ifneq ($(SourceDepend),)
--include $(SourceDepend)
-endif