diff --git a/Makefile.common b/Makefile.common
index e8cc9bad5dcd708554d06740de2246758ea49cfd..a157abaef274178cbfb12efda11b5230a73b9a5e 100644 (file)
--- a/Makefile.common
+++ b/Makefile.common
-#===-- Makefile.common - Common make rules for LLVM -------*- makefile -*--====
+#===-- Makefile.common - Common make rules for LLVM --------*- Makefile -*--===#
+#
+# The LLVM Compiler Infrastructure
+#
+# This file is distributed under the University of Illinois Open Source
+# License. See LICENSE.TXT for details.
+#
+#===------------------------------------------------------------------------===#
#
# This file is included by all of the LLVM makefiles. This file defines common
-# rules to do things like compile a .cpp file or generate dependancy info.
-# These are platform dependant, so this is the file used to specify these
-# system dependant operations.
+# rules to do things like compile a .cpp file or generate dependency info.
+# These are platform dependent, so this is the file used to specify these
+# system dependent operations.
#
# The following functionality can be set by setting incoming variables.
# The variable $(LEVEL) *must* be set:
#
-# 1. LEVEL - The level of the current subdirectory from the top of the
-# MagicStats view. This level should be expressed as a path, for
+# 1. LEVEL - The level of the current subdirectory from the top of the
+# source directory. This level should be expressed as a path, for
# example, ../.. for two levels deep.
#
# 2. DIRS - A list of subdirectories to be built. Fake targets are set up
# built in any order. All DIRS are built in order before PARALLEL_DIRS are
# built, which are then built in any order.
#
-# 4. Source - If specified, this sets the source code filenames. If this
-# is not set, it defaults to be all of the .cpp, .c, .y, and .l files
-# in the current directory. Also, if you want to build files in addition
-# to the local files, you can use the ExtraSource variable
+# 4. SOURCES - If specified, this sets the source code filenames. If this
+# is not set, it defaults to be all of the .cpp, .c, .y, and .l files
+# in the current directory.
#
-#===-----------------------------------------------------------------------====
-
-# Configuration file to set paths specific to local installation of LLVM
-#
-include $(LEVEL)/Makefile.config
-
-# These are options that can either be enabled here, or can be enabled on the
-# make command line (ie, make ENABLE_PROFILING=1)
+# 5. SourceDir - If specified, this specifies a directory that the source files
+# are in, if they are not in the current directory. This should include a
+# trailing / character.
#
-
-# When ENABLE_PROFILING is enabled, the llvm source base is built with profile
-# information to allow gprof to be used to get execution frequencies.
+# 6. LLVM_SRC_ROOT - If specified, points to the top of the LLVM source tree.
#
-#ENABLE_PROFILING = 1
-
-# When ENABLE_PURIFY is enabled, the LLVM tools are linked with purify (which
-# must be locally installed) to allow for some automated memory error debugging.
+# 8. PROJ_SRC_DIR - The directory which contains the current set of Makefiles
+# and usually the source code too (unless SourceDir is set).
#
-#ENABLE_PURIFY = 1
-
-# When ENABLE_OPTIMIZED is enabled, Release builds of all of the LLVM code are
-# turned on, and Debug builds are turned off.
+# 9. PROJ_SRC_ROOT - The root directory of the source code being compiled.
#
-#ENABLE_OPTIMIZED = 1
-
-
-# Figure out how to do platform specific stuff on this platform. This is really
-# gross and should be autoconfiscated (automake actually), but should hopefully
-# work on Linux and solaris (SunOS).
+# 10. PROJ_OBJ_DIR - The directory where object code should be placed.
#
-UNAME := $(shell uname)
-include $(LEVEL)/Makefile.$(UNAME)
-
-ifdef SHARED_LIBRARY
-# if SHARED_LIBRARY is specified, the default is to build the dynamic lib
-dynamic ::
-endif
-
-# Default Rule: Make sure it's also a :: rule
-all ::
-
-# Default for install is to at least build everything...
-install ::
-
-
-# Figure out which directory to build stuff into. We want to build into the
-# /shared directory by default because it is guaranteed to be local to the
-# current machine.
+# 11. PROJ_OBJ_ROOT - The root directory for where object code should be
+# placed.
#
-ifeq ($(LLVM_OBJ_DIR),.)
-BUILD_ROOT = $(LLVM_OBJ_DIR)
-BUILD_ROOT_TOP = $(LEVEL)
-else
-
-BUILD_ROOT := $(LLVM_OBJ_DIR)$(patsubst $(HOME)%,%,$(shell pwd))
-
-# Calculate the BUILD_ROOT_TOP variable, which is the top of the llvm/ tree.
-# Note that although this is just equal to $(BUILD_ROOT)/$(LEVEL), we cannot use
-# this expression because some of the directories on the source tree may not
-# exist in the build tree (for example the test/ heirarchy). Thus we evaluate
-# the directory to eliminate the ../'s
+# For building,
+# LLVM, LLVM_SRC_ROOT = PROJ_SRC_ROOT
#
-TOP_DIRECTORY := $(shell cd $(LEVEL); pwd)
-BUILD_ROOT_TOP := $(LLVM_OBJ_DIR)$(patsubst $(HOME)%,%,$(TOP_DIRECTORY))
-endif
-
-#--------------------------------------------------------------------
-# Variables derived from configuration options...
-#--------------------------------------------------------------------
-
-#BinInstDir=/usr/local/bin
-#LibInstDir=/usrl/local/lib/xxx
-#DocInstDir=/usr/doc/xxx
-
-BURG_OPTS = -I
-
-PURIFY := $(PURIFY) -cache-dir="$(BUILD_ROOT_TOP)/../purifycache" -chain-length="30" -messages=all
-
-# Shorthand for commonly accessed directories
-LIBDEBUG := $(BUILD_ROOT_TOP)/lib/Debug
-LIBRELEASE := $(BUILD_ROOT_TOP)/lib/Release
-LIBPROFILE := $(BUILD_ROOT_TOP)/lib/Profile
-TOOLDEBUG := $(BUILD_ROOT_TOP)/tools/Debug
-TOOLRELEASE := $(BUILD_ROOT_TOP)/tools/Release
-TOOLPROFILE := $(BUILD_ROOT_TOP)/tools/Profile
-
-# Verbosity levels
-ifdef VERBOSE
-VERB :=
-else
-VERB := @
-endif
-
-#---------------------------------------------------------
-# Compilation options...
-#---------------------------------------------------------
-
-# Special tools used while building the LLVM tree. Burg is built as part of the
-# utils directory.
-#
-BURG := $(TOOLDEBUG)/burg
-RunBurg := $(BURG) $(BURG_OPTS)
-
-
-# Enable this for profiling support with 'gprof'
-# This automatically enables optimized builds.
-ifdef ENABLE_PROFILING
- PROFILE = -pg
- ENABLE_OPTIMIZED = 1
-else
- PROFILE =
-endif
-
-# By default, strip symbol information from executable
-ifdef KEEP_SYMBOLS
-STRIP =
-else
-STRIP = -s
-endif
-
-# Allow gnu extensions...
-CPPFLAGS += -D_GNU_SOURCE
-
-# -Wno-unused-parameter
-CompileCommonOpts := -Wall -W -Wwrite-strings -Wno-unused -I$(LEVEL)/include
-
-# Compile a cpp file, don't link...
-Compile := $(CXX) -c $(CPPFLAGS) $(CXXFLAGS) $(CompileCommonOpts)
-CompileG := $(Compile) -g -D_DEBUG
-CompileO := $(Compile) -O3 -DNDEBUG -finline-functions -felide-constructors -fshort-enums ## DISABLE -freg-struct-return because of gcc3.2 bug
-CompileP := $(CompileO) $(PROFILE)
-
-# Compile a c file, don't link...
-CompileC := $(CC) -c $(CPPFLAGS) $(CCFLAGS) $(CompileCommonOpts)
-CompileCG := $(CompileC) -g -D_DEBUG
-CompileCO := $(CompileC) -O3 -DNDEBUG -finline-functions -felide-constructors -fshort-enums ## DISABLE -freg-struct-return because of gcc3.2 bug
-CompileCP := $(CompileCO) $(PROFILE)
-
-
-# Link final executable
-
-ifdef ENABLE_PURIFY # To enable purify, build with 'gmake ENABLE_PURIFY=1'
-Link := $(PURIFY) $(CXX) -static
-else
-Link := $(CXX)
-endif
-LinkG := $(Link) -g -L $(LIBDEBUG) $(STRIP)
-LinkO := $(Link) -O3 -L $(LIBRELEASE)
-LinkP := $(Link) -O3 -L $(LIBPROFILE) $(PROFILE)
-
-# Create one .o file from a bunch of .o files...
-Relink = ld -r
-
-# MakeSO - Create a .so file from a .o files...
-MakeSO := $(CXX) $(MakeSharedObjectOption)
-MakeSOO := $(MakeSO) -O3
-MakeSOP := $(MakeSOO) $(PROFILE)
-
-# Create dependancy file from CPP file, send to stdout.
-Depend := $(CXX) -MM -I$(LEVEL)/include $(CPPFLAGS)
-DependC := $(CC) -MM -I$(LEVEL)/include $(CPPFLAGS)
-
-# Archive a bunch of .o files into a .a file...
-AR = ar cq
-BISON = bison
-
-#----------------------------------------------------------
-
-# Source includes all of the cpp files, and objects are derived from the
-# source files...
-# The local Makefile can list other Source files via ExtraSource = ...
-#
-Source := $(ExtraSource) $(wildcard *.cpp *.c *.y *.l)
-
-Objs := $(sort $(patsubst Debug/%.o, %.o, $(addsuffix .o,$(basename $(Source)))))
-ObjectsO := $(addprefix $(BUILD_ROOT)/Release/,$(Objs))
-ObjectsP := $(addprefix $(BUILD_ROOT)/Profile/,$(Objs))
-ObjectsG := $(addprefix $(BUILD_ROOT)/Debug/,$(Objs))
-
-
-#---------------------------------------------------------
-# Handle the DIRS and PARALLEL_DIRS options
-#---------------------------------------------------------
-
-ifdef DIRS
-all install clean ::
- $(VERB) for dir in ${DIRS}; do \
- (cd $$dir; $(MAKE) $@) || exit 1; \
- done
-endif
-
-# Handle PARALLEL_DIRS
-ifdef PARALLEL_DIRS
-all :: $(addsuffix /.makeall , $(PARALLEL_DIRS))
-install :: $(addsuffix /.makeinstall, $(PARALLEL_DIRS))
-clean :: $(addsuffix /.makeclean , $(PARALLEL_DIRS))
-
-%/.makeall %/.makeinstall %/.makeclean:
- $(VERB) cd $(@D); $(MAKE) $(subst $(@D)/.make,,$@)
-
-endif
-
-#---------------------------------------------------------
-# Handle the LIBRARYNAME option - used when building libs...
-#---------------------------------------------------------
-#
-# When libraries are built, they are allowed to optionally define the
-# DONT_BUILD_RELINKED make variable, which, when defined, prevents a .o file
-# from being built for the library. This .o files may then be linked to by a
-# tool if the tool does not need (or want) the semantics a .a file provides
-# (linking in only object files that are "needed"). If a library is never to
-# be used in this way, it is better to define DONT_BUILD_RELINKED, and define
-# BUILD_ARCHIVE instead.
-#
-# Some libraries must be built as .a files (libscalar for example) because if
-# it's built as a .o file, then all of the constituent .o files in it will be
-# linked into tools (for example gccas) even if they only use one of the parts
-# of it. For this reason, sometimes it's useful to use libraries as .a files.
-
-ifdef LIBRARYNAME
-
-# Make sure there isn't any extranous whitespace on the LIBRARYNAME option
-LIBRARYNAME := $(strip $(LIBRARYNAME))
-
-LIBNAME_O := $(LIBRELEASE)/lib$(LIBRARYNAME).so
-LIBNAME_P := $(LIBPROFILE)/lib$(LIBRARYNAME).so
-LIBNAME_G := $(LIBDEBUG)/lib$(LIBRARYNAME).so
-LIBNAME_AO := $(LIBRELEASE)/lib$(LIBRARYNAME).a
-LIBNAME_AP := $(LIBPROFILE)/lib$(LIBRARYNAME).a
-LIBNAME_AG := $(LIBDEBUG)/lib$(LIBRARYNAME).a
-LIBNAME_OBJO := $(LIBRELEASE)/$(LIBRARYNAME).o
-LIBNAME_OBJP := $(LIBPROFILE)/$(LIBRARYNAME).o
-LIBNAME_OBJG := $(LIBDEBUG)/$(LIBRARYNAME).o
-
-
-ifndef ENABLE_OPTIMIZED
-BUILD_LIBNAME_G := $(LIBNAME_G)
-ifndef DONT_BUILD_RELINKED
-BUILD_LIBNAME_OBJG := $(LIBNAME_OBJG)
-endif
-ifdef BUILD_ARCHIVE
-BUILD_LIBNAME_AG := $(LIBNAME_AG)
-endif
-endif
-
-# If optimized builds are enabled...
-ifdef ENABLE_OPTIMIZED
- ifdef ENABLE_PROFILING
- BUILD_LIBNAME_O := $(LIBNAME_P)
- ifndef DONT_BUILD_RELINKED
- BUILD_LIBNAME_OBJO := $(LIBNAME_OBJP)
- endif
- ifdef BUILD_ARCHIVE
- BUILD_LIBNAME_AO := $(LIBNAME_AP)
- endif
- else
- BUILD_LIBNAME_O := $(LIBNAME_O)
- ifndef DONT_BUILD_RELINKED
- BUILD_LIBNAME_OBJO := $(LIBNAME_OBJO)
- endif
- ifdef BUILD_ARCHIVE
- BUILD_LIBNAME_AO := $(LIBNAME_AO)
- endif
- endif
-endif
-
-all:: $(BUILD_LIBNAME_AG) $(BUILD_LIBNAME_OBJG) # Debug
-all:: $(BUILD_LIBNAME_AO) $(BUILD_LIBNAME_OBJO) # Release
-all:: $(BUILD_LIBNAME_AP) $(BUILD_LIBNAME_OBJP) # Profile
-dynamic:: $(BUILD_LIBNAME_G) $(BUILD_LIBNAME_O) $(BUILD_LIBNAME_P) # .so files
-
-$(LIBNAME_O): $(ObjectsO) $(LibSubDirs) $(LIBRELEASE)/.dir
- @echo ======= Linking $(LIBRARYNAME) release library =======
- $(VERB) $(MakeSOO) -o $@ $(ObjectsO) $(LibSubDirs) $(LibLinkOpts)
-
-$(LIBNAME_P): $(ObjectsP) $(LibSubDirs) $(LIBPROFILE)/.dir
- @echo ======= Linking $(LIBRARYNAME) profile library =======
- $(VERB) $(MakeSOP) -o $@ $(ObjectsP) $(LibSubDirs) $(LibLinkOpts)
-
-$(LIBNAME_G): $(ObjectsG) $(LibSubDirs) $(LIBDEBUG)/.dir
- @echo ======= Linking $(LIBRARYNAME) debug library =======
- $(VERB) $(MakeSO) -g -o $@ $(ObjectsG) $(LibSubDirs) $(LibLinkOpts)
-
-$(LIBNAME_AO): $(ObjectsO) $(LibSubDirs) $(LIBRELEASE)/.dir
- @echo ======= Linking $(LIBRARYNAME) release library =======
- @rm -f $@
- $(VERB) $(AR) $@ $(ObjectsO) $(LibSubDirs)
-
-$(LIBNAME_AP): $(ObjectsP) $(LibSubDirs) $(LIBPROFILE)/.dir
- @echo ======= Linking $(LIBRARYNAME) profile library =======
- @rm -f $@
- $(VERB) $(AR) $@ $(ObjectsP) $(LibSubDirs)
-
-$(LIBNAME_AG): $(ObjectsG) $(LibSubDirs) $(LIBDEBUG)/.dir
- @echo ======= Linking $(LIBRARYNAME) debug library =======
- @rm -f $@
- $(VERB) $(AR) $@ $(ObjectsG) $(LibSubDirs)
-
-$(LIBNAME_OBJO): $(ObjectsO) $(LibSubDirs) $(LIBRELEASE)/.dir
- @echo "Linking $@"
- $(VERB) $(Relink) -o $@ $(ObjectsO) $(LibSubDirs)
-
-$(LIBNAME_OBJP): $(ObjectsP) $(LibSubDirs) $(LIBPROFILE)/.dir
- @echo "Linking $@"
- $(VERB) $(Relink) -o $@ $(ObjectsP) $(LibSubDirs)
-
-$(LIBNAME_OBJG): $(ObjectsG) $(LibSubDirs) $(LIBDEBUG)/.dir
- @echo "Linking $@"
- $(VERB) $(Relink) -o $@ $(ObjectsG) $(LibSubDirs)
-
-endif
-
-#------------------------------------------------------------------------
-# Create a TAGS database for emacs
-#------------------------------------------------------------------------
-
-ifeq ($(LEVEL), .)
-tags:
- etags -l c++ `find include lib tools -name '*.cpp' -o -name '*.h'`
-all:: tags
-endif
+#===-----------------------------------------------------------------------====
-#------------------------------------------------------------------------
-# Handle the TOOLNAME option - used when building tool executables...
-#------------------------------------------------------------------------
#
-# The TOOLNAME option should be used with a USEDLIBS variable that tells the
-# libraries (and the order of the libs) that should be linked to the
-# tool. USEDLIBS should contain a list of library names (some with .a extension)
-# that are automatically linked in as .o files unless the .a suffix is added.
+# Configuration file to set paths specific to local installation of LLVM
#
-ifdef TOOLNAME
-
-# TOOLEXENAME* - These compute the output filenames to generate...
-TOOLEXENAME_G := $(BUILD_ROOT_TOP)/tools/Debug/$(TOOLNAME)
-TOOLEXENAME_O := $(BUILD_ROOT_TOP)/tools/Release/$(TOOLNAME)
-TOOLEXENAME_P := $(BUILD_ROOT_TOP)/tools/Profile/$(TOOLNAME)
-
-ifndef ENABLE_OPTIMIZED
- TOOLEXENAMES := $(TOOLEXENAME_G)
+ifndef LLVM_OBJ_ROOT
+include $(LEVEL)/Makefile.config
else
- ifdef ENABLE_PROFILING
- TOOLEXENAMES := $(TOOLEXENAME_P)
- else
- TOOLEXENAMES := $(TOOLEXENAME_O)
- endif
+include $(LLVM_OBJ_ROOT)/Makefile.config
endif
-# USED_LIBS_OPTIONS - Compute the options line that add -llib1 -llib2, etc.
-USED_LIBS_OPTIONS := $(patsubst %.a.o, -l%, $(addsuffix .o, $(USEDLIBS)))
-USED_LIBS_OPTIONS_G := $(patsubst %.o, $(LIBDEBUG)/%.o, $(USED_LIBS_OPTIONS))
-USED_LIBS_OPTIONS_O := $(patsubst %.o, $(LIBRELEASE)/%.o,$(USED_LIBS_OPTIONS))
-USED_LIBS_OPTIONS_P := $(patsubst %.o, $(LIBPROFILE)/%.o,$(USED_LIBS_OPTIONS))
-
-
-# USED_LIB_PATHS - Compute the path of the libraries used so that tools are
-# rebuilt if libraries change. This has to make sure to handle .a/.so and .o
-# files seperately.
#
-STATICUSEDLIBS := $(patsubst %.a.o, lib%.a, $(addsuffix .o, $(USEDLIBS)))
-USED_LIB_PATHS_G := $(addprefix $(LIBDEBUG)/, $(STATICUSEDLIBS))
-USED_LIB_PATHS_O := $(addprefix $(LIBRELEASE)/, $(STATICUSEDLIBS))
-USED_LIB_PATHS_P := $(addprefix $(LIBPROFILE)/, $(STATICUSEDLIBS))
-
-all:: $(TOOLEXENAMES)
-clean::
- $(VERB) rm -f $(TOOLEXENAMES)
-
-$(TOOLEXENAME_G): $(ObjectsG) $(USED_LIB_PATHS_G) $(BUILD_ROOT_TOP)/tools/Debug/.dir
- @echo ======= Linking $(TOOLNAME) debug executable =======
- $(VERB) $(LinkG) -o $@ $(ObjectsG) $(USED_LIBS_OPTIONS_G) $(TOOLLINKOPTS)
-
-$(TOOLEXENAME_O): $(ObjectsO) $(USED_LIB_PATHS_O) $(BUILD_ROOT_TOP)/tools/Release/.dir
- @echo ======= Linking $(TOOLNAME) release executable =======
- $(VERB) $(LinkO) -o $@ $(ObjectsG) $(USED_LIBS_OPTIONS_O) $(TOOLLINKOPTS)
-
-$(TOOLEXENAME_P): $(ObjectsP) $(USED_LIB_PATHS_P) $(BUILD_ROOT_TOP)/tools/Profile/.dir
- @echo ======= Linking $(TOOLNAME) profile executable =======
- $(VERB) $(LinkP) -o $@ $(ObjectsP) $(USED_LIBS_OPTIONS_P) $(TOOLLINKOPTS)
-
-endif
-
-
-
-#---------------------------------------------------------
-.PRECIOUS: $(BUILD_ROOT)/Depend/.dir
-.PRECIOUS: $(BUILD_ROOT)/Debug/.dir $(BUILD_ROOT)/Release/.dir
-
-# Create dependencies for the *.cpp files...
-$(BUILD_ROOT)/Depend/%.d: %.cpp $(BUILD_ROOT)/Depend/.dir
- $(VERB) $(Depend) $< | sed 's|$*\.o *|$(BUILD_ROOT)/Release/& $(BUILD_ROOT)/Profile/& $(BUILD_ROOT)/Debug/& $(BUILD_ROOT)/Depend/$(@F)|g' > $@
-
-# Create dependencies for the *.c files...
-$(BUILD_ROOT)/Depend/%.d: %.c $(BUILD_ROOT)/Depend/.dir
- $(VERB) $(DependC) $< | sed 's|$*\.o *|Release/& Profile/& Debug/& Depend/$(@F)|g' > $@
-
-# Create .o files in the ObjectFiles directory from the .cpp and .c files...
-$(BUILD_ROOT)/Release/%.o: %.cpp $(BUILD_ROOT)/Release/.dir
- @echo "Compiling $<"
- $(VERB) $(CompileO) $< -o $@
-
-$(BUILD_ROOT)/Release/%.o: %.c $(BUILD_ROOT)/Release/.dir
- $(VERB) $(CompileOC) $< -o $@
-
-$(BUILD_ROOT)/Profile/%.o: %.cpp $(BUILD_ROOT)/Profile/.dir
- @echo "Compiling $<"
- $(VERB) $(CompileP) $< -o $@
-
-$(BUILD_ROOT)/Profile/%.o: %.c $(BUILD_ROOT)/Profile/.dir
- @echo "Compiling $<"
- $(VERB) $(CompileCP) $< -o $@
-
-$(BUILD_ROOT)/Debug/%.o: %.cpp $(BUILD_ROOT)/Debug/.dir
- @echo "Compiling $<"
- $(VERB) $(CompileG) $< -o $@
-
-$(BUILD_ROOT)/Debug/%.o: %.c $(BUILD_ROOT)/Debug/.dir
- $(VERB) $(CompileCG) $< -o $@
-
-# Create a .cpp source file from a flex input file... this uses sed to cut down
-# on the warnings emited by GCC...
-%.cpp: %.l
- flex -t $< | sed '/^find_rule/d' | sed 's/void yyunput/inline void yyunput/' | sed 's/void \*yy_flex_realloc/inline void *yy_flex_realloc/' > $@
-
-# Rule for building the bison parsers...
-
-%.cpp %.h : %.y
- $(VERB) $(BISON) -v -d -p $(<:%Parser.y=%) $(basename $@).y
- $(VERB) mv -f $(basename $@).tab.c $(basename $@).cpp
- $(VERB) mv -f $(basename $@).tab.h $(basename $@).h
-
-# To create the directories...
-%/.dir:
- $(VERB) mkdir -p $(@D)
- @date > $@
-
-# 'make clean' nukes the tree
-clean::
- $(VERB) rm -rf $(BUILD_ROOT)/Debug $(BUILD_ROOT)/Release $(BUILD_ROOT)/Profile $(BUILD_ROOT)/Depend
- $(VERB) rm -f core *.o *.d *.so *~ *.flc
-
-# If dependancies were generated for the file that included this file,
-# include the dependancies now...
+# Include all of the build rules used for making LLVM
#
-SourceDepend := $(addsuffix .d,$(addprefix $(BUILD_ROOT)/Depend/,$(basename $(filter-out Debug/%, $(Source)))))
-ifneq ($(SourceDepend),)
-include $(SourceDepend)
-endif
+include $(LLVM_SRC_ROOT)/Makefile.rules
+