diff --git a/Makefile.config.in b/Makefile.config.in
index 0fa41f7989be93980df778844f0e787d6fd6f22e..d34a2d51a933d9efd2c352cce5e0f1c6776a1785 100644 (file)
--- a/Makefile.config.in
+++ b/Makefile.config.in
#===------------------------------------------------------------------------===#
# Define LLVM specific info and directories based on the autoconf variables
-LLVMPackageName := @PACKAGE_NAME@
+LLVMPackageName := @PACKAGE_TARNAME@
LLVMVersion := @PACKAGE_VERSION@
+LLVM_VERSION_MAJOR := @LLVM_VERSION_MAJOR@
+LLVM_VERSION_MINOR := @LLVM_VERSION_MINOR@
+LLVM_VERSION_PATCH := @LLVM_VERSION_PATCH@
+LLVM_VERSION_SUFFIX := @LLVM_VERSION_SUFFIX@
LLVM_CONFIGTIME := @LLVM_CONFIGTIME@
###########################################################################
PROJECT_NAME := $(LLVMPackageName)
endif
-PROJ_OBJ_DIR := $(shell $(PWD))
-PROJ_OBJ_ROOT := $(shell cd $(PROJ_OBJ_DIR)/$(LEVEL); $(PWD))
+# The macro below is expanded when 'realpath' is not built-in.
+# Built-in 'realpath' is available on GNU Make 3.81.
+realpath = $(shell cd $(1); $(PWD))
+
+PROJ_OBJ_DIR := $(call realpath, .)
+PROJ_OBJ_ROOT := $(call realpath, $(PROJ_OBJ_DIR)/$(LEVEL))
+
+CLANG_SRC_ROOT := @CLANG_SRC_ROOT@
+
+ifeq ($(PROJECT_NAME),$(LLVMPackageName))
+LLVM_SRC_ROOT := $(call realpath, @abs_top_srcdir@)
+LLVM_OBJ_ROOT := $(call realpath, @abs_top_builddir@)
+PROJ_SRC_ROOT := $(LLVM_SRC_ROOT)
+PROJ_SRC_DIR := $(LLVM_SRC_ROOT)$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR))
+
+ifneq ($(CLANG_SRC_ROOT),)
+ CLANG_SRC_ROOT:= $(call realpath, $(CLANG_SRC_ROOT))
+ PROJ_SRC_DIR := $(patsubst $(LLVM_SRC_ROOT)/tools/clang%,$(CLANG_SRC_ROOT)%,$(PROJ_SRC_DIR))
+endif
-ifeq ($(PROJECT_NAME),llvm)
-LLVM_SRC_ROOT := $(shell cd @abs_top_srcdir@; $(PWD))
-LLVM_OBJ_ROOT := $(shell cd @abs_top_builddir@; $(PWD))
-PROJ_SRC_ROOT := $(shell cd $(LLVM_SRC_ROOT); $(PWD))
-PROJ_SRC_DIR := $(shell cd $(LLVM_SRC_ROOT)/$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR)); $(PWD))
prefix := @prefix@
PROJ_prefix := $(prefix)
+program_prefix := @program_prefix@
PROJ_VERSION := $(LLVMVersion)
else
ifndef PROJ_SRC_ROOT
ifndef LLVM_OBJ_ROOT
$(error Projects must define LLVM_OBJ_ROOT)
endif
-PROJ_SRC_DIR := $(shell cd $(PROJ_SRC_ROOT)/$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR)); $(PWD))
+PROJ_SRC_DIR := $(call realpath, $(PROJ_SRC_ROOT)/$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR)))
prefix := $(PROJ_INSTALL_ROOT)
PROJ_prefix := $(prefix)
ifndef PROJ_VERSION
endif
endif
-LLVMMAKE := $(LLVM_SRC_ROOT)/make
+INTERNAL_PREFIX := @INTERNAL_PREFIX@
+ifneq ($(INTERNAL_PREFIX),)
+PROJ_internal_prefix := $(INTERNAL_PREFIX)
+else
+PROJ_internal_prefix := $(prefix)
+endif
-PROJ_bindir := $(DESTDIR)$(PROJ_prefix)/bin
-PROJ_libdir := $(DESTDIR)$(PROJ_prefix)/lib
-PROJ_datadir := $(DESTDIR)$(PROJ_prefix)/share
-PROJ_docsdir := $(DESTDIR)$(PROJ_prefix)/docs/llvm
-PROJ_etcdir := $(DESTDIR)$(PROJ_prefix)/etc/llvm
-PROJ_includedir := $(DESTDIR)$(PROJ_prefix)/include
-PROJ_infodir := $(DESTDIR)$(PROJ_prefix)/info
-PROJ_mandir := $(DESTDIR)$(PROJ_prefix)/share/man
+PROJ_bindir := $(PROJ_prefix)/bin
+PROJ_libdir := $(PROJ_prefix)/lib
+PROJ_datadir := $(PROJ_prefix)/share
+PROJ_docsdir := $(PROJ_prefix)/docs/llvm
+PROJ_etcdir := $(PROJ_prefix)/etc/llvm
+PROJ_includedir := $(PROJ_prefix)/include
+PROJ_infodir := $(PROJ_prefix)/info
+PROJ_mandir := $(PROJ_prefix)/share/man
# Determine if we're on a unix type operating system
LLVM_ON_UNIX:=@LLVM_ON_UNIX@
# Target operating system for which LLVM will compile for.
TARGET_OS=@TARGET_OS@
+# Host hardware architecture
+HOST_ARCH=@HOST_ARCH@
# Target hardware architecture
ARCH=@ARCH@
+TARGET_NATIVE_ARCH := $(ARCH)
+LLVM_NATIVE_ARCH := @LLVM_NATIVE_ARCH@
# Indicates, whether we're cross-compiling LLVM or not
LLVM_CROSS_COMPILING=@LLVM_CROSS_COMPILING@
# Triple for configuring build tools when cross-compiling
BUILD_TRIPLE=@build@
+# Target triple (cpu-vendor-os) which LLVM is compiled for
+HOST_TRIPLE=@host@
+
# Target triple (cpu-vendor-os) for which we should generate code
TARGET_TRIPLE=@target@
# Extra options to compile LLVM with
EXTRA_OPTIONS=@EXTRA_OPTIONS@
+# Extra options to link LLVM with
+EXTRA_LD_OPTIONS=@EXTRA_LD_OPTIONS@
+
# Endian-ness of the target
ENDIAN=@ENDIAN@
# Path to the CC binary, which use used by testcases for native builds.
CC := @CC@
+# C/C++ preprocessor flags.
+CPPFLAGS += @CPPFLAGS@
+
+# C compiler flags.
+CFLAGS += @CFLAGS@
+
+# C++ compiler flags.
+CXXFLAGS += @CXXFLAGS@
+
# Linker flags.
-LDFLAGS+=@LDFLAGS@
+LDFLAGS += @LDFLAGS@
# Path to the library archiver program.
AR_PATH = @AR@
RM := @RM@
SED := @SED@
TAR := @TAR@
+PYTHON := @PYTHON@
# Paths to miscellaneous programs we hope are present but might not be
-PERL := @PERL@
BZIP2 := @BZIP2@
+CAT := @CAT@
DOT := @DOT@
DOXYGEN := @DOXYGEN@
GROFF := @GROFF@
-GZIP := @GZIP@
-OCAMLC := @OCAMLC@
-OCAMLOPT := @OCAMLOPT@
-OCAMLDEP := @OCAMLDEP@
-OCAMLDOC := @OCAMLDOC@
+GZIPBIN := @GZIPBIN@
+GO := @GO@
+OCAMLFIND := @OCAMLFIND@
GAS := @GAS@
POD2HTML := @POD2HTML@
POD2MAN := @POD2MAN@
-RUNTEST := @RUNTEST@
-TCLSH := @TCLSH@
+PDFROFF := @PDFROFF@
ZIP := @ZIP@
-HAVE_PERL := @HAVE_PERL@
+HAVE_LIBZ := @HAVE_LIBZ@
+HAVE_DLOPEN := @HAVE_DLOPEN@
HAVE_PTHREAD := @HAVE_PTHREAD@
+HAVE_TERMINFO := @HAVE_TERMINFO@
+
+HAVE_OCAMLOPT := @HAVE_OCAMLOPT@
+HAVE_OCAML_OUNIT := @HAVE_OCAML_OUNIT@
LIBS := @LIBS@
+# Targets that are possible to build
+ALL_TARGETS := @ALL_TARGETS@
+
# Targets that we should build
TARGETS_TO_BUILD=@TARGETS_TO_BUILD@
-# Path to location for LLVM C/C++ front-end. You can modify this if you
-# want to override the value set by configure.
-LLVMGCCDIR := @LLVMGCCDIR@
-
-# Determine the target for which LLVM should generate code.
-LLVMGCCARCH := @target@/@LLVMGCC_VERSION@
-
-# Determine the path where the library executables are
-LLVMGCCLIBEXEC := @LLVMGCCLIBEXEC@
-
-# Full pathnames of LLVM C/C++ front-end 'cc1' and 'cc1plus' binaries:
-LLVMGCC := @LLVMGCC@
-LLVMGXX := @LLVMGXX@
-LLVMCC1 := @LLVMCC1@
-LLVMCC1PLUS := @LLVMCC1PLUS@
-LLVMGCC_VERSION := @LLVMGCC_VERSION@
-LLVMGCC_LANGS := @LLVMGCC_LANGS@
+# Targets supporting JIT
+TARGETS_WITH_JIT := @TARGETS_WITH_JIT@
# Path to directory where object files should be stored during a build.
# Set OBJ_ROOT to "." if you do not want to use a separate place for
# These are options that can either be enabled here, or can be enabled on the
# make command line (ie, make ENABLE_PROFILING=1):
+# When ENABLE_LIBCPP is enabled, LLVM uses libc++ by default to build.
+#ENABLE_LIBCPP = 0
+ENABLE_LIBCPP = @ENABLE_LIBCPP@
+
+# When ENABLE_CXX1Y is enabled, LLVM uses c++1y mode by default to build.
+# Otherwise it uses the baseline c++11.
+ENABLE_CXX1Y = @ENABLE_CXX1Y@
+
+# When ENABLE_SPLIT_DWARF is enabled, LLVM uses -gfission to build in debug mode.
+ENABLE_SPLIT_DWARF = @ENABLE_SPLIT_DWARF@
+
+# When enabled, clang will have plugin support.
+CLANG_PLUGIN_SUPPORT = @CLANG_PLUGIN_SUPPORT@
+
+# When ENABLE_CLANG_ARCMT is enabled, clang will have ARCMigrationTool.
+ENABLE_CLANG_ARCMT = @ENABLE_CLANG_ARCMT@
+
+# When ENABLE_CLANG_STATIC_ANALYZER is enabled, clang will have StaticAnalyzer.
+ENABLE_CLANG_STATIC_ANALYZER = @ENABLE_CLANG_STATIC_ANALYZER@
+
+# When ENABLE_WERROR is enabled, we'll pass -Werror on the command line
+ENABLE_WERROR = @ENABLE_WERROR@
+
+# When ENABLE_TERMINFO is enabled, we use terminfo.
+ENABLE_TERMINFO = @ENABLE_TERMINFO@
+
# When ENABLE_OPTIMIZED is enabled, LLVM code is optimized and output is put
# into the "Release" directories. Otherwise, LLVM code is not optimized and
# output is put in the "Debug" directories.
# When ENABLE_PROFILING is enabled, profile instrumentation is done
# and output is put into the "<Flavor>+Profile" directories, where
-# <Flavor> is either Debug or Release depending on how other builkd
-# flags are set.. Otherwise, output is put in the <Flavor>
+# <Flavor> is either Debug or Release depending on how other build
+# flags are set. Otherwise, output is put in the <Flavor>
# directories.
#ENABLE_PROFILING = 1
@ENABLE_PROFILING@
#DEBUG_SYMBOLS = 1
@DEBUG_SYMBOLS@
+# When KEEP_SYMBOLS is enabled, installed executables will never have their
+# symbols stripped.
+#KEEP_SYMBOLS = 1
+@KEEP_SYMBOLS@
+
# The compiler flags to use for optimized builds.
OPTIMIZE_OPTION := @OPTIMIZE_OPTION@
# information to allow gprof to be used to get execution frequencies.
#ENABLE_PROFILING = 1
+# When ENABLE_DOCS is disabled, docs/ will not be built.
+ENABLE_DOCS = @ENABLE_DOCS@
+
# When ENABLE_DOXYGEN is enabled, the doxygen documentation will be built
ENABLE_DOXYGEN = @ENABLE_DOXYGEN@
# Do we want to enable threads?
-ENABLE_THREADS := @ENABLE_THREADS@
+ENABLE_THREADS := @LLVM_ENABLE_THREADS@
+
+# Do we want to enable zlib?
+ENABLE_ZLIB := @LLVM_ENABLE_ZLIB@
# Do we want to build with position independent code?
ENABLE_PIC := @ENABLE_PIC@
+# Do we want to build a shared library and link the tools with it?
+ENABLE_SHARED := @ENABLE_SHARED@
+
+# Do we want to link the stdc++ into a shared library? (Cygming)
+ENABLE_EMBED_STDCXX := @ENABLE_EMBED_STDCXX@
+
# Use -fvisibility-inlines-hidden?
ENABLE_VISIBILITY_INLINES_HIDDEN := @ENABLE_VISIBILITY_INLINES_HIDDEN@
+# Do we want to allow timestamping information into builds?
+ENABLE_TIMESTAMPS := @ENABLE_TIMESTAMPS@
+
# This option tells the Makefiles to produce verbose output.
# It essentially prints the commands that make is executing
#VERBOSE = 1
# Bindings that we should build
BINDINGS_TO_BUILD := @BINDINGS_TO_BUILD@
-ALL_BINDINGS := @ALL_BINDINGS@
OCAML_LIBDIR := @OCAML_LIBDIR@
# When compiling under Mingw/Cygwin, executables such as tblgen
# Location of the plugin header file for gold.
BINUTILS_INCDIR := @BINUTILS_INCDIR@
-C_INCLUDE_DIRS := @C_INCLUDE_DIRS@
-CXX_INCLUDE_ROOT := @CXX_INCLUDE_ROOT@
-CXX_INCLUDE_ARCH := @CXX_INCLUDE_ARCH@
-CXX_INCLUDE_32BIT_DIR = @CXX_INCLUDE_32BIT_DIR@
-CXX_INCLUDE_64BIT_DIR = @CXX_INCLUDE_64BIT_DIR@
-
-# When ENABLE_LLVMC_DYNAMIC is enabled, LLVMC will link libCompilerDriver
-# dynamically. This is needed to make dynamic plugins work on some targets
-# (Windows).
-ENABLE_LLVMC_DYNAMIC = 0
-#@ENABLE_LLVMC_DYNAMIC@
-
-# When ENABLE_LLVMC_DYNAMIC_PLUGINS is enabled, LLVMC will have dynamic plugin
-# support (via the -load option).
-ENABLE_LLVMC_DYNAMIC_PLUGINS = 1
-#@ENABLE_LLVMC_DYNAMIC_PLUGINS@
-
# Optional flags supported by the compiler
# -Wno-missing-field-initializers
NO_MISSING_FIELD_INITIALIZERS = @NO_MISSING_FIELD_INITIALIZERS@
# -Wno-variadic-macros
NO_VARIADIC_MACROS = @NO_VARIADIC_MACROS@
+# -Wcovered-switch-default
+COVERED_SWITCH_DEFAULT = @COVERED_SWITCH_DEFAULT@
+# -Wno-uninitialized
+NO_UNINITIALIZED = @NO_UNINITIALIZED@
+# -Wno-maybe-uninitialized
+NO_MAYBE_UNINITIALIZED = @NO_MAYBE_UNINITIALIZED@
+# -Wno-comment
+NO_COMMENT = @NO_COMMENT@
+
+# Was polly found in tools/polly?
+LLVM_HAS_POLLY = @LLVM_HAS_POLLY@
+# Flags supported by the linker.
+# bfd ld / gold --version-script=file
+HAVE_LINK_VERSION_SCRIPT = @HAVE_LINK_VERSION_SCRIPT@
+
+# Flags to control using libxml2
+LIBXML2_LIBS := @LIBXML2_LIBS@
+LIBXML2_INC := @LIBXML2_INC@
+
+# Flags to control building support for Intel JIT Events API
+USE_INTEL_JITEVENTS := @USE_INTEL_JITEVENTS@
+INTEL_JITEVENTS_INCDIR := @INTEL_JITEVENTS_INCDIR@
+INTEL_JITEVENTS_LIBDIR := @INTEL_JITEVENTS_LIBDIR@
+
+# Flags to control building support for OProfile JIT API
+USE_OPROFILE := @USE_OPROFILE@
+
+ifeq ($(USE_INTEL_JITEVENTS), 1)
+ OPTIONAL_COMPONENTS += IntelJITEvents
+endif
+ifeq ($(USE_OPROFILE), 1)
+ OPTIONAL_COMPONENTS += OProfileJIT
+endif