]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - Makefile
Updates to sync with changes in upstream.
[opencl/llvm.git] / Makefile
index 03ab0446522a55dff64c73aa62b687fb16474cce..2b9468af205381d5b7e25d4dd8873ed560819006 100644 (file)
--- a/Makefile
+++ b/Makefile
 LEVEL := .
 
 # Top-Level LLVM Build Stages:
-#   1. Build lib/System and lib/Support, which are used by utils (tblgen).
-#   2. Build utils, which is used by VMCore.
-#   3. Build VMCore, which builds the Intrinsics.inc file used by libs.
+#   1. Build lib/Support and lib/TableGen, which are used by utils (tblgen).
+#   2. Build utils, which is used by IR.
+#   3. Build IR, which builds the Intrinsics.inc file used by libs.
 #   4. Build libs, which are needed by llvm-config.
 #   5. Build llvm-config, which determines inter-lib dependencies for tools.
-#   6. Build tools, runtime, docs.
+#   6. Build tools, docs, and cmake modules.
 #
 # When cross-compiling, there are some things (tablegen) that need to
 # be build for the build system first.
+
+# If "RC_ProjectName" exists in the environment, and its value is
+# "llvmCore", then this is an "Apple-style" build; search for
+# "Apple-style" in the comments for more info.  Anything else is a
+# normal build.
+ifneq ($(findstring llvmCore, $(RC_ProjectName)),llvmCore)  # Normal build (not "Apple-style").
+
 ifeq ($(BUILD_DIRS_ONLY),1)
-  DIRS := lib/System lib/Support utils
-  OPTIONAL_DIRS :=
+  DIRS := lib/Support lib/TableGen utils tools/llvm-config
+  OPTIONAL_DIRS := tools/clang/utils/TableGen
 else
-  DIRS := lib/System lib/Support utils lib/VMCore lib tools/llvm-config \
-          tools runtime docs unittests
-  OPTIONAL_DIRS := examples projects bindings
+  DIRS := lib/Support lib/TableGen utils lib/IR lib tools/llvm-shlib \
+          tools/llvm-config tools docs cmake unittests
+  OPTIONAL_DIRS := projects bindings
+endif
+
+ifeq ($(BUILD_EXAMPLES),1)
+  OPTIONAL_DIRS += examples
 endif
 
 EXTRA_DIST := test unittests llvm.spec include win32 Xcode
 
 include $(LEVEL)/Makefile.config
 
-# llvm-gcc4 doesn't need runtime libs.  llvm-gcc4 is the only supported one.
-# FIXME: Remove runtime entirely once we have an understanding of where
-# libprofile etc should go.
-#ifeq ($(LLVMGCC_MAJVERS),4)
-#  DIRS := $(filter-out runtime, $(DIRS))
-#endif
+ifneq ($(ENABLE_SHARED),1)
+  DIRS := $(filter-out tools/llvm-shlib, $(DIRS))
+endif
+
+ifneq ($(ENABLE_DOCS),1)
+  DIRS := $(filter-out docs, $(DIRS))
+endif
 
 ifeq ($(MAKECMDGOALS),libs-only)
-  DIRS := $(filter-out tools runtime docs, $(DIRS))
+  DIRS := $(filter-out tools docs, $(DIRS))
   OPTIONAL_DIRS :=
 endif
 
 ifeq ($(MAKECMDGOALS),install-libs)
-  DIRS := $(filter-out tools runtime docs, $(DIRS))
+  DIRS := $(filter-out tools docs, $(DIRS))
   OPTIONAL_DIRS := $(filter bindings, $(OPTIONAL_DIRS))
 endif
 
 ifeq ($(MAKECMDGOALS),tools-only)
-  DIRS := $(filter-out runtime docs, $(DIRS))
+  DIRS := $(filter-out docs, $(DIRS))
   OPTIONAL_DIRS :=
 endif
 
 ifeq ($(MAKECMDGOALS),install-clang)
-  DIRS := tools/clang/tools/driver tools/clang/tools/clang-cc \
-       tools/clang/lib/Headers tools/clang/docs
+  DIRS := tools/clang/tools/driver tools/clang/lib/Headers \
+          tools/clang/tools/libclang \
+          tools/clang/tools/c-index-test \
+          tools/clang/include/clang-c \
+          tools/clang/runtime tools/clang/docs \
+          tools/lto
   OPTIONAL_DIRS :=
   NO_INSTALL = 1
 endif
 
 ifeq ($(MAKECMDGOALS),clang-only)
-  DIRS := $(filter-out tools runtime docs, $(DIRS)) tools/clang
+  DIRS := $(filter-out tools docs unittests, $(DIRS)) \
+          tools/clang tools/lto
   OPTIONAL_DIRS :=
 endif
 
 ifeq ($(MAKECMDGOALS),unittests)
-  DIRS := $(filter-out tools runtime docs, $(DIRS)) utils unittests
+  DIRS := $(filter-out tools docs, $(DIRS)) utils unittests
   OPTIONAL_DIRS :=
 endif
 
@@ -77,6 +94,11 @@ ifeq ($(MAKECMDGOALS),install)
   OPTIONAL_DIRS := $(filter bindings, $(OPTIONAL_DIRS))
 endif
 
+# Don't build unittests when ONLY_TOOLS is set.
+ifneq ($(ONLY_TOOLS),)
+  DIRS := $(filter-out unittests, $(DIRS))
+endif
+
 # If we're cross-compiling, build the build-hosted tools first
 ifeq ($(LLVM_CROSS_COMPILING),1)
 all:: cross-compile-build-tools
@@ -88,18 +110,40 @@ cross-compile-build-tools:
        $(Verb) if [ ! -f BuildTools/Makefile ]; then \
           $(MKDIR) BuildTools; \
          cd BuildTools ; \
+         unset CFLAGS ; \
+         unset CXXFLAGS ; \
+         AR=$(BUILD_AR) ; \
+         AS=$(BUILD_AS) ; \
+         LD=$(BUILD_LD) ; \
+         CC=$(BUILD_CC) ; \
+         CXX=$(BUILD_CXX) ; \
+         unset SDKROOT ; \
+         unset UNIVERSAL_SDK_PATH ; \
+         configure_opts= ; \
+         if test "$(ENABLE_LIBCPP)" -ne 0 ; then \
+           configure_opts="$$configure_opts --enable-libcpp"; \
+         fi; \
          $(PROJ_SRC_DIR)/configure --build=$(BUILD_TRIPLE) \
-               --host=$(BUILD_TRIPLE) --target=$(BUILD_TRIPLE); \
+               --host=$(BUILD_TRIPLE) --target=$(BUILD_TRIPLE) \
+               --disable-polly $$configure_opts; \
          cd .. ; \
        fi; \
-        ($(MAKE) -C BuildTools \
+       ($(MAKE) -C BuildTools \
          BUILD_DIRS_ONLY=1 \
          UNIVERSAL= \
+         UNIVERSAL_SDK_PATH= \
+         SDKROOT= \
+         TARGET_NATIVE_ARCH="$(TARGET_NATIVE_ARCH)" \
+         TARGETS_TO_BUILD="$(TARGETS_TO_BUILD)" \
+         TARGET_LIBS="$(LIBS)" \
          ENABLE_OPTIMIZED=$(ENABLE_OPTIMIZED) \
          ENABLE_PROFILING=$(ENABLE_PROFILING) \
          ENABLE_COVERAGE=$(ENABLE_COVERAGE) \
          DISABLE_ASSERTIONS=$(DISABLE_ASSERTIONS) \
          ENABLE_EXPENSIVE_CHECKS=$(ENABLE_EXPENSIVE_CHECKS) \
+         ENABLE_LIBCPP=$(ENABLE_LIBCPP) \
+         CFLAGS= \
+         CXXFLAGS= \
        ) || exit 1;
 endif
 
@@ -127,8 +171,7 @@ dist-hook::
        $(Echo) Eliminating files constructed by configure
        $(Verb) $(RM) -f \
          $(TopDistDir)/include/llvm/Config/config.h  \
-         $(TopDistDir)/include/llvm/Support/DataTypes.h  \
-         $(TopDistDir)/include/llvm/Support/ThreadSupport.h
+         $(TopDistDir)/include/llvm/Support/DataTypes.h
 
 clang-only: all
 tools-only: all
@@ -136,14 +179,32 @@ libs-only: all
 install-clang: install
 install-libs: install
 
+# If SHOW_DIAGNOSTICS is enabled, clear the diagnostics file first.
+ifeq ($(SHOW_DIAGNOSTICS),1)
+clean-diagnostics:
+       $(Verb) rm -f $(LLVM_OBJ_ROOT)/$(BuildMode)/diags
+.PHONY: clean-diagnostics
+
+all-local:: clean-diagnostics
+endif
+
 #------------------------------------------------------------------------
-# Make sure the generated headers are up-to-date. This must be kept in
-# sync with the AC_CONFIG_HEADER invocations in autoconf/configure.ac
+# Make sure the generated files are up-to-date. This must be kept in
+# sync with the AC_CONFIG_HEADER and AC_CONFIG_FILE invocations in
+# autoconf/configure.ac.
+# Note that Makefile.config is covered by its own separate rule
+# in Makefile.rules where it can be reused by sub-projects.
 #------------------------------------------------------------------------
 FilesToConfig := \
+  bindings/ocaml/llvm/META.llvm \
+  docs/doxygen.cfg \
+  llvm.spec \
   include/llvm/Config/config.h \
+  include/llvm/Config/llvm-config.h \
   include/llvm/Config/Targets.def \
-       include/llvm/Config/AsmPrinters.def \
+  include/llvm/Config/AsmPrinters.def \
+  include/llvm/Config/AsmParsers.def \
+  include/llvm/Config/Disassemblers.def \
   include/llvm/Support/DataTypes.h
 FilesToConfigPATH  := $(addprefix $(LLVM_OBJ_ROOT)/,$(FilesToConfig))
 
@@ -157,21 +218,24 @@ $(FilesToConfigPATH) : $(LLVM_OBJ_ROOT)/% : $(LLVM_SRC_ROOT)/%.in
 # that it gets executed last.
 ifneq ($(BUILD_DIRS_ONLY),1)
 all::
-       $(Echo) '*****' Completed $(BuildMode)$(AssertMode) Build
-ifeq ($(BuildMode),Debug)
+       $(Echo) '*****' Completed $(BuildMode) Build
+ifneq ($(ENABLE_OPTIMIZED),1)
        $(Echo) '*****' Note: Debug build can be 10 times slower than an
        $(Echo) '*****' optimized build. Use 'make ENABLE_OPTIMIZED=1' to
        $(Echo) '*****' make an optimized build. Alternatively you can
        $(Echo) '*****' configure with --enable-optimized.
+ifeq ($(SHOW_DIAGNOSTICS),1)
+       $(Verb) if test -s $(LLVM_OBJ_ROOT)/$(BuildMode)/diags; then \
+         $(LLVM_SRC_ROOT)/utils/clang-parse-diagnostics-file -a \
+           $(LLVM_OBJ_ROOT)/$(BuildMode)/diags; \
+       fi
+endif
 endif
 endif
 
 check-llvm2cpp:
        $(Verb)$(MAKE) check TESTSUITE=Feature RUNLLVM2CPP=1
 
-check-one:
-       $(Verb)$(MAKE) -C test check-one TESTONE=$(TESTONE)
-
 srpm: $(LLVM_OBJ_ROOT)/llvm.spec
        rpmbuild -bs $(LLVM_OBJ_ROOT)/llvm.spec
 
@@ -194,15 +258,28 @@ build-for-llvm-top:
 SVN = svn
 SVN-UPDATE-OPTIONS =
 AWK = awk
-SUB-SVN-DIRS = $(AWK) '/\?\ \ \ \ \ \ / {print $$2}'   \
-               | LC_ALL=C xargs $(SVN) info 2>/dev/null \
-               | $(AWK) '/Path:\ / {print $$2}'
+
+# Multiline variable defining a recursive function for finding svn repos rooted at
+# a given path. svnup() requires one argument: the root to search from.
+define SUB_SVN_DIRS
+svnup() {
+  dirs=`svn status --no-ignore $$1 | awk '/^(I|\?) / {print $$2}' | LC_ALL=C xargs svn info 2>/dev/null | awk '/^Path:\ / {print $$2}'`;
+  if [ "$$dirs" = "" ]; then
+    return;
+  fi;
+  for f in $$dirs; do
+         echo $$f;
+    svnup $$f;
+  done
+}
+endef
+export SUB_SVN_DIRS
 
 update:
        $(SVN) $(SVN-UPDATE-OPTIONS) update $(LLVM_SRC_ROOT)
-       @ $(SVN) status $(LLVM_SRC_ROOT) | $(SUB-SVN-DIRS) | xargs $(SVN) $(SVN-UPDATE-OPTIONS) update
+       @eval $$SUB_SVN_DIRS; $(SVN) status --no-ignore $(LLVM_SRC_ROOT) | svnup $(LLVM_SRC_ROOT) | xargs $(SVN) $(SVN-UPDATE-OPTIONS) update
 
-happiness: update all check unittests
+happiness: update all check-all
 
 .PHONY: srpm rpm update happiness
 
@@ -210,3 +287,9 @@ happiness: update all check unittests
 
 .NOTPARALLEL:
 
+else # Building "Apple-style."
+# In an Apple-style build, once configuration is done, lines marked
+# "Apple-style" are removed with sed!  Please don't remove these!
+# Look for the string "Apple-style" in utils/buildit/build_llvm.
+include $(shell find . -name GNUmakefile) # Building "Apple-style."
+endif # Building "Apple-style."