]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - cmake/config-ix.cmake
Don't pass -Wl,z,defs for now.
[opencl/llvm.git] / cmake / config-ix.cmake
index 93aeae1003206ef99635e92b4d6bf6ed71272f97..f806d9c54ed93506498281e7c5f1463881879f3d 100755 (executable)
@@ -17,6 +17,11 @@ if( UNIX AND NOT BEOS )
   # Used by check_symbol_exists:
   set(CMAKE_REQUIRED_LIBRARIES m)
 endif()
+# x86_64 FreeBSD 9.2 requires libcxxrt to be specified explicitly.
+if( CMAKE_SYSTEM MATCHES "FreeBSD-9.2-RELEASE" AND
+    CMAKE_SIZEOF_VOID_P EQUAL 8 )
+  list(APPEND CMAKE_REQUIRED_LIBRARIES "cxxrt")
+endif()
 
 # Helper macros and functions
 macro(add_cxx_include result files)
@@ -37,7 +42,6 @@ function(check_type_exists type files variable)
 endfunction()
 
 # include checks
-check_include_file_cxx(cxxabi.h HAVE_CXXABI_H)
 check_include_file(dirent.h HAVE_DIRENT_H)
 check_include_file(dlfcn.h HAVE_DLFCN_H)
 check_include_file(errno.h HAVE_ERRNO_H)
@@ -45,13 +49,13 @@ check_include_file(execinfo.h HAVE_EXECINFO_H)
 check_include_file(fcntl.h HAVE_FCNTL_H)
 check_include_file(inttypes.h HAVE_INTTYPES_H)
 check_include_file(limits.h HAVE_LIMITS_H)
+check_include_file(link.h HAVE_LINK_H)
 check_include_file(malloc.h HAVE_MALLOC_H)
 check_include_file(malloc/malloc.h HAVE_MALLOC_MALLOC_H)
 check_include_file(ndir.h HAVE_NDIR_H)
 if( NOT PURE_WINDOWS )
   check_include_file(pthread.h HAVE_PTHREAD_H)
 endif()
-check_include_file(sanitizer/msan_interface.h HAVE_SANITIZER_MSAN_INTERFACE_H)
 check_include_file(signal.h HAVE_SIGNAL_H)
 check_include_file(stdint.h HAVE_STDINT_H)
 check_include_file(sys/dir.h HAVE_SYS_DIR_H)
@@ -76,6 +80,13 @@ check_symbol_exists(FE_INEXACT "fenv.h" HAVE_DECL_FE_INEXACT)
 check_include_file(mach/mach.h HAVE_MACH_MACH_H)
 check_include_file(mach-o/dyld.h HAVE_MACH_O_DYLD_H)
 
+# size_t must be defined before including cxxabi.h on FreeBSD 10.0.
+check_cxx_source_compiles("
+#include <stddef.h>
+#include <cxxabi.h>
+int main() { return 0; }
+" HAVE_CXXABI_H)
+
 # library checks
 if( NOT PURE_WINDOWS )
   check_library_exists(pthread pthread_create "" HAVE_LIBPTHREAD)
@@ -248,24 +259,18 @@ function(llvm_find_program name)
   endif(LLVM_PATH_${NAME})
 endfunction()
 
-llvm_find_program(gv)
-llvm_find_program(circo)
-llvm_find_program(twopi)
-llvm_find_program(neato)
-llvm_find_program(fdp)
-llvm_find_program(dot)
-llvm_find_program(dotty)
-llvm_find_program(xdot xdot.py)
-llvm_find_program(Graphviz)
+if (LLVM_ENABLE_DOXYGEN)
+  llvm_find_program(dot)
+endif ()
 
 if( LLVM_ENABLE_FFI )
   find_path(FFI_INCLUDE_PATH ffi.h PATHS ${FFI_INCLUDE_DIR})
-  if( FFI_INCLUDE_PATH )
+  if( EXISTS "${FFI_INCLUDE_PATH}/ffi.h" )
     set(FFI_HEADER ffi.h CACHE INTERNAL "")
     set(HAVE_FFI_H 1 CACHE INTERNAL "")
   else()
     find_path(FFI_INCLUDE_PATH ffi/ffi.h PATHS ${FFI_INCLUDE_DIR})
-    if( FFI_INCLUDE_PATH )
+    if( EXISTS "${FFI_INCLUDE_PATH}/ffi/ffi.h" )
       set(FFI_HEADER ffi/ffi.h CACHE INTERNAL "")
       set(HAVE_FFI_FFI_H 1 CACHE INTERNAL "")
     endif()
@@ -300,25 +305,6 @@ else()
   set(ENABLE_PIC 0)
 endif()
 
-find_package(LibXml2)
-if (LIBXML2_FOUND)
-  set(CLANG_HAVE_LIBXML 1)
-  # When cross-compiling, liblzma is not detected as a dependency for libxml2,
-  # which makes linking c-index-test fail. But for native builds, all libraries
-  # are installed and checked by CMake before Makefiles are generated and everything
-  # works according to the plan. However, if a -llzma is added to native builds,
-  # an additional requirement on the static liblzma.a is required, but will not
-  # be checked by CMake, breaking native compilation.
-  # Since this is only pertinent to cross-compilations, and there's no way CMake
-  # can check for every foreign library on every OS, we add the dep and warn the dev.
-  if ( CMAKE_CROSSCOMPILING )
-    if (NOT PC_LIBXML_VERSION VERSION_LESS "2.8.0")
-      message(STATUS "Adding LZMA as a dep to XML2 for cross-compilation, make sure liblzma.a is available.")
-      set(LIBXML2_LIBRARIES ${LIBXML2_LIBRARIES} "-llzma")
-    endif ()
-  endif ()
-endif ()
-
 check_cxx_compiler_flag("-Wno-variadic-macros" SUPPORTS_NO_VARIADIC_MACROS_FLAG)
 
 set(USE_NO_MAYBE_UNINITIALIZED 0)
@@ -367,6 +353,8 @@ elseif (LLVM_NATIVE_ARCH MATCHES "powerpc")
   set(LLVM_NATIVE_ARCH PowerPC)
 elseif (LLVM_NATIVE_ARCH MATCHES "aarch64")
   set(LLVM_NATIVE_ARCH AArch64)
+elseif (LLVM_NATIVE_ARCH MATCHES "arm64")
+  set(LLVM_NATIVE_ARCH AArch64)
 elseif (LLVM_NATIVE_ARCH MATCHES "arm")
   set(LLVM_NATIVE_ARCH ARM)
 elseif (LLVM_NATIVE_ARCH MATCHES "mips")
@@ -480,7 +468,7 @@ set(LLVM_PREFIX ${CMAKE_INSTALL_PREFIX})
 
 if (LLVM_ENABLE_DOXYGEN)
   message(STATUS "Doxygen enabled.")
-  find_package(Doxygen)
+  find_package(Doxygen REQUIRED)
 
   if (DOXYGEN_FOUND)
     # If we find doxygen and we want to enable doxygen by default create a
@@ -499,3 +487,58 @@ if (LLVM_ENABLE_DOXYGEN)
 else()
   message(STATUS "Doxygen disabled.")
 endif()
+
+if (LLVM_ENABLE_SPHINX)
+  message(STATUS "Sphinx enabled.")
+  find_package(Sphinx REQUIRED)
+  if (LLVM_BUILD_DOCS)
+    add_custom_target(sphinx ALL)
+  endif()
+else()
+  message(STATUS "Sphinx disabled.")
+endif()
+
+set(LLVM_BINDINGS "")
+if(WIN32)
+  message(STATUS "Go bindings disabled.")
+else()
+  find_program(GO_EXECUTABLE NAMES go DOC "go executable")
+  if(GO_EXECUTABLE STREQUAL "GO_EXECUTABLE-NOTFOUND")
+    message(STATUS "Go bindings disabled.")
+  else()
+    execute_process(COMMAND ${GO_EXECUTABLE} run ${CMAKE_SOURCE_DIR}/bindings/go/conftest.go
+                    RESULT_VARIABLE GO_CONFTEST)
+    if(GO_CONFTEST STREQUAL "0")
+      set(LLVM_BINDINGS "${LLVM_BINDINGS} go")
+      message(STATUS "Go bindings enabled.")
+    else()
+      message(STATUS "Go bindings disabled, need at least Go 1.2.")
+    endif()
+  endif()
+endif()
+
+include(FindOCaml)
+include(AddOCaml)
+if(WIN32)
+  message(STATUS "OCaml bindings disabled.")
+else()
+  find_package(OCaml)
+  if( NOT OCAML_FOUND )
+    message(STATUS "OCaml bindings disabled.")
+  else()
+    if( OCAML_VERSION VERSION_LESS "4.00.0" )
+      message(STATUS "OCaml bindings disabled, need OCaml >=4.00.0.")
+    else()
+      find_ocamlfind_package(ctypes VERSION 0.3 OPTIONAL)
+      if( HAVE_OCAML_CTYPES )
+        message(STATUS "OCaml bindings enabled.")
+        find_ocamlfind_package(oUnit VERSION 2 OPTIONAL)
+        set(LLVM_BINDINGS "${LLVM_BINDINGS} ocaml")
+      else()
+        message(STATUS "OCaml bindings disabled, need ctypes >=0.3.")
+      endif()
+    endif()
+  endif()
+endif()
+
+string(REPLACE " " ";" LLVM_BINDINGS_LIST "${LLVM_BINDINGS}")