index b129e67963283acb784797aa7b50040c51ebe8f6..fc1393fc47a2b1efdc1a063591d27c5203a13460 100644 (file)
namespace llvm {
+// FIXME: Replace this brittle forward declaration with the include of the new
+// PassManager.h when doing so doesn't break the PassManagerBuilder.
+template <typename IRUnitT> class AnalysisManager;
+class PreservedAnalyses;
+
/// \brief A cache of @llvm.assume calls within a function.
///
/// This cache provides fast lookup of assumptions within a function by caching
}
};
+/// \brief A function analysis which provides an \c AssumptionCache.
+///
+/// This analysis is intended for use with the new pass manager and will vend
+/// assumption caches for a given function.
+class AssumptionAnalysis {
+ static char PassID;
+
+public:
+ typedef AssumptionCache Result;
+
+ /// \brief Opaque, unique identifier for this analysis pass.
+ static void *ID() { return (void *)&PassID; }
+
+ /// \brief Provide a name for the analysis for debugging and logging.
+ static StringRef name() { return "AssumptionAnalysis"; }
+
+ AssumptionAnalysis() {}
+ AssumptionAnalysis(const AssumptionAnalysis &Arg) {}
+ AssumptionAnalysis(AssumptionAnalysis &&Arg) {}
+ AssumptionAnalysis &operator=(const AssumptionAnalysis &RHS) { return *this; }
+ AssumptionAnalysis &operator=(AssumptionAnalysis &&RHS) { return *this; }
+
+ AssumptionCache run(Function &F) { return AssumptionCache(F); }
+};
+
+/// \brief Printer pass for the \c AssumptionAnalysis results.
+class AssumptionPrinterPass {
+ raw_ostream &OS;
+
+public:
+ explicit AssumptionPrinterPass(raw_ostream &OS) : OS(OS) {}
+ PreservedAnalyses run(Function &F, AnalysisManager<Function> *AM);
+
+ static StringRef name() { return "AssumptionPrinterPass"; }
+};
+
/// \brief An immutable pass that tracks lazily created \c AssumptionCache
/// objects.
///