diff --git a/include/llvm/CodeGen/LiveIntervalAnalysis.h b/include/llvm/CodeGen/LiveIntervalAnalysis.h
index 70f570212a073b47145ec7bdfba19bf34537ba10..61c705e04d29be4b028c2dc54e5eec2c040a29b3 100644 (file)
//
//===----------------------------------------------------------------------===//
-#ifndef LLVM_CODEGEN_LIVEINTERVAL_ANALYSIS_H
-#define LLVM_CODEGEN_LIVEINTERVAL_ANALYSIS_H
+#ifndef LLVM_CODEGEN_LIVEINTERVALANALYSIS_H
+#define LLVM_CODEGEN_LIVEINTERVALANALYSIS_H
+#include "llvm/ADT/IndexedMap.h"
+#include "llvm/ADT/SmallVector.h"
+#include "llvm/CodeGen/LiveInterval.h"
#include "llvm/CodeGen/MachineBasicBlock.h"
#include "llvm/CodeGen/MachineFunctionPass.h"
-#include "llvm/CodeGen/LiveInterval.h"
#include "llvm/CodeGen/SlotIndexes.h"
-#include "llvm/ADT/BitVector.h"
-#include "llvm/ADT/DenseMap.h"
-#include "llvm/ADT/SmallPtrSet.h"
-#include "llvm/ADT/SmallVector.h"
#include "llvm/Support/Allocator.h"
+#include "llvm/Target/TargetRegisterInfo.h"
#include <cmath>
#include <iterator>
namespace llvm {
class AliasAnalysis;
+ class BitVector;
+ class BlockFrequency;
+ class LiveRangeCalc;
class LiveVariables;
+ class MachineDominatorTree;
class MachineLoopInfo;
class TargetRegisterInfo;
class MachineRegisterInfo;
class TargetInstrInfo;
class TargetRegisterClass;
class VirtRegMap;
+ class MachineBlockFrequencyInfo;
class LiveIntervals : public MachineFunctionPass {
- MachineFunction* mf_;
- MachineRegisterInfo* mri_;
- const TargetMachine* tm_;
- const TargetRegisterInfo* tri_;
- const TargetInstrInfo* tii_;
- AliasAnalysis *aa_;
- LiveVariables* lv_;
- SlotIndexes* indexes_;
+ MachineFunction* MF;
+ MachineRegisterInfo* MRI;
+ const TargetRegisterInfo* TRI;
+ const TargetInstrInfo* TII;
+ AliasAnalysis *AA;
+ SlotIndexes* Indexes;
+ MachineDominatorTree *DomTree;
+ LiveRangeCalc *LRCalc;
/// Special pool allocator for VNInfo's (LiveInterval val#).
///
VNInfo::Allocator VNInfoAllocator;
- typedef DenseMap<unsigned, LiveInterval*> Reg2IntervalMap;
- Reg2IntervalMap r2iMap_;
+ /// Live interval pointers for all the virtual registers.
+ IndexedMap<LiveInterval*, VirtReg2IndexFunctor> VirtRegIntervals;
- /// allocatableRegs_ - A bit vector of allocatable registers.
- BitVector allocatableRegs_;
+ /// RegMaskSlots - Sorted list of instructions with register mask operands.
+ /// Always use the 'r' slot, RegMasks are normal clobbers, not early
+ /// clobbers.
+ SmallVector<SlotIndex, 8> RegMaskSlots;
- /// CloneMIs - A list of clones as result of re-materialization.
- std::vector<MachineInstr*> CloneMIs;
+ /// RegMaskBits - This vector is parallel to RegMaskSlots, it holds a
+ /// pointer to the corresponding register mask. This pointer can be
+ /// recomputed as:
+ ///
+ /// MI = Indexes->getInstructionFromIndex(RegMaskSlot[N]);
+ /// unsigned OpNum = findRegMaskOperand(MI);
+ /// RegMaskBits[N] = MI->getOperand(OpNum).getRegMask();
+ ///
+ /// This is kept in a separate vector partly because some standard
+ /// libraries don't support lower_bound() with mixed objects, partly to
+ /// improve locality when searching in RegMaskSlots.
+ /// Also see the comment in LiveInterval::find().
+ SmallVector<const uint32_t*, 8> RegMaskBits;
+
+ /// For each basic block number, keep (begin, size) pairs indexing into the
+ /// RegMaskSlots and RegMaskBits arrays.
+ /// Note that basic block numbers may not be layout contiguous, that's why
+ /// we can't just keep track of the first register mask in each basic
+ /// block.
+ SmallVector<std::pair<unsigned, unsigned>, 8> RegMaskBlocks;
+
+ /// Keeps a live range set for each register unit to track fixed physreg
+ /// interference.
+ SmallVector<LiveRange*, 0> RegUnitRanges;
public:
static char ID; // Pass identification, replacement for typeid
- LiveIntervals() : MachineFunctionPass(ID) {
- initializeLiveIntervalsPass(*PassRegistry::getPassRegistry());
- }
+ LiveIntervals();
+ virtual ~LiveIntervals();
// Calculate the spill weight to assign to a single instruction.
- static float getSpillWeight(bool isDef, bool isUse, unsigned loopDepth);
-
- // After summing the spill weights of all defs and uses, the final weight
- // should be normalized, dividing the weight of the interval by its size.
- // This encourages spilling of intervals that are large and have few uses,
- // and discourages spilling of small intervals with many uses.
- void normalizeSpillWeight(LiveInterval &li) {
- li.weight /= getApproximateInstructionCount(li) + 25;
+ static float getSpillWeight(bool isDef, bool isUse,
+ const MachineBlockFrequencyInfo *MBFI,
+ const MachineInstr *Instr);
+
+ LiveInterval &getInterval(unsigned Reg) {
+ if (hasInterval(Reg))
+ return *VirtRegIntervals[Reg];
+ else
+ return createAndComputeVirtRegInterval(Reg);
}
- typedef Reg2IntervalMap::iterator iterator;
- typedef Reg2IntervalMap::const_iterator const_iterator;
- const_iterator begin() const { return r2iMap_.begin(); }
- const_iterator end() const { return r2iMap_.end(); }
- iterator begin() { return r2iMap_.begin(); }
- iterator end() { return r2iMap_.end(); }
- unsigned getNumIntervals() const { return (unsigned)r2iMap_.size(); }
-
- LiveInterval &getInterval(unsigned reg) {
- Reg2IntervalMap::iterator I = r2iMap_.find(reg);
- assert(I != r2iMap_.end() && "Interval does not exist for register");
- return *I->second;
+ const LiveInterval &getInterval(unsigned Reg) const {
+ return const_cast<LiveIntervals*>(this)->getInterval(Reg);
}
- const LiveInterval &getInterval(unsigned reg) const {
- Reg2IntervalMap::const_iterator I = r2iMap_.find(reg);
- assert(I != r2iMap_.end() && "Interval does not exist for register");
- return *I->second;
+ bool hasInterval(unsigned Reg) const {
+ return VirtRegIntervals.inBounds(Reg) && VirtRegIntervals[Reg];
}
- bool hasInterval(unsigned reg) const {
- return r2iMap_.count(reg);
+ // Interval creation.
+ LiveInterval &createEmptyInterval(unsigned Reg) {
+ assert(!hasInterval(Reg) && "Interval already exists!");
+ VirtRegIntervals.grow(Reg);
+ VirtRegIntervals[Reg] = createInterval(Reg);
+ return *VirtRegIntervals[Reg];
}
- /// isAllocatable - is the physical register reg allocatable in the current
- /// function?
- bool isAllocatable(unsigned reg) const {
- return allocatableRegs_.test(reg);
+ LiveInterval &createAndComputeVirtRegInterval(unsigned Reg) {
+ LiveInterval &LI = createEmptyInterval(Reg);
+ computeVirtRegInterval(LI);
+ return LI;
}
- /// getScaledIntervalSize - get the size of an interval in "units,"
- /// where every function is composed of one thousand units. This
- /// measure scales properly with empty index slots in the function.
- double getScaledIntervalSize(LiveInterval& I) {
- return (1000.0 * I.getSize()) / indexes_->getIndexesLength();
- }
-
- /// getFuncInstructionCount - Return the number of instructions in the
- /// current function.
- unsigned getFuncInstructionCount() {
- return indexes_->getFunctionSize();
- }
-
- /// getApproximateInstructionCount - computes an estimate of the number
- /// of instructions in a given LiveInterval.
- unsigned getApproximateInstructionCount(LiveInterval& I) {
- double IntervalPercentage = getScaledIntervalSize(I) / 1000.0;
- return (unsigned)(IntervalPercentage * indexes_->getFunctionSize());
- }
-
- /// conflictsWithPhysReg - Returns true if the specified register is used or
- /// defined during the duration of the specified interval. Copies to and
- /// from li.reg are allowed. This method is only able to analyze simple
- /// ranges that stay within a single basic block. Anything else is
- /// considered a conflict.
- bool conflictsWithPhysReg(const LiveInterval &li, VirtRegMap &vrm,
- unsigned reg);
-
- /// conflictsWithAliasRef - Similar to conflictsWithPhysRegRef except
- /// it checks for alias uses and defs.
- bool conflictsWithAliasRef(LiveInterval &li, unsigned Reg,
- SmallPtrSet<MachineInstr*,32> &JoinedCopies);
-
- // Interval creation
- LiveInterval &getOrCreateInterval(unsigned reg) {
- Reg2IntervalMap::iterator I = r2iMap_.find(reg);
- if (I == r2iMap_.end())
- I = r2iMap_.insert(std::make_pair(reg, createInterval(reg))).first;
- return *I->second;
+ // Interval removal.
+ void removeInterval(unsigned Reg) {
+ delete VirtRegIntervals[Reg];
+ VirtRegIntervals[Reg] = nullptr;
}
- /// dupInterval - Duplicate a live interval. The caller is responsible for
- /// managing the allocated memory.
- LiveInterval *dupInterval(LiveInterval *li);
-
- /// addLiveRangeToEndOfBlock - Given a register and an instruction,
- /// adds a live range from that instruction to the end of its MBB.
- LiveRange addLiveRangeToEndOfBlock(unsigned reg,
- MachineInstr* startInst);
+ /// Given a register and an instruction, adds a live segment from that
+ /// instruction to the end of its MBB.
+ LiveInterval::Segment addSegmentToEndOfBlock(unsigned reg,
+ MachineInstr* startInst);
+
+ /// shrinkToUses - After removing some uses of a register, shrink its live
+ /// range to just the remaining uses. This method does not compute reaching
+ /// defs for new uses, and it doesn't remove dead defs.
+ /// Dead PHIDef values are marked as unused.
+ /// New dead machine instructions are added to the dead vector.
+ /// Return true if the interval may have been separated into multiple
+ /// connected components.
+ bool shrinkToUses(LiveInterval *li,
+ SmallVectorImpl<MachineInstr*> *dead = nullptr);
+
+ /// Specialized version of
+ /// shrinkToUses(LiveInterval *li, SmallVectorImpl<MachineInstr*> *dead)
+ /// that works on a subregister live range and only looks at uses matching
+ /// the lane mask of the subregister range.
+ void shrinkToUses(LiveInterval::SubRange &SR, unsigned Reg);
+
+ /// extendToIndices - Extend the live range of LI to reach all points in
+ /// Indices. The points in the Indices array must be jointly dominated by
+ /// existing defs in LI. PHI-defs are added as needed to maintain SSA form.
+ ///
+ /// If a SlotIndex in Indices is the end index of a basic block, LI will be
+ /// extended to be live out of the basic block.
+ ///
+ /// See also LiveRangeCalc::extend().
+ void extendToIndices(LiveRange &LR, ArrayRef<SlotIndex> Indices);
- // Interval removal
- void removeInterval(unsigned Reg) {
- DenseMap<unsigned, LiveInterval*>::iterator I = r2iMap_.find(Reg);
- delete I->second;
- r2iMap_.erase(I);
- }
+ /// If @p LR has a live value at @p Kill, prune its live range by removing
+ /// any liveness reachable from Kill. Add live range end points to
+ /// EndPoints such that extendToIndices(LI, EndPoints) will reconstruct the
+ /// value's live range.
+ ///
+ /// Calling pruneValue() and extendToIndices() can be used to reconstruct
+ /// SSA form after adding defs to a virtual register.
+ void pruneValue(LiveRange &LR, SlotIndex Kill,
+ SmallVectorImpl<SlotIndex> *EndPoints);
SlotIndexes *getSlotIndexes() const {
- return indexes_;
- }
-
- SlotIndex getZeroIndex() const {
- return indexes_->getZeroIndex();
+ return Indexes;
}
- SlotIndex getInvalidIndex() const {
- return indexes_->getInvalidIndex();
+ AliasAnalysis *getAliasAnalysis() const {
+ return AA;
}
/// isNotInMIMap - returns true if the specified machine instr has been
/// removed or was never entered in the map.
bool isNotInMIMap(const MachineInstr* Instr) const {
- return !indexes_->hasIndex(Instr);
+ return !Indexes->hasIndex(Instr);
}
/// Returns the base index of the given instruction.
SlotIndex getInstructionIndex(const MachineInstr *instr) const {
- return indexes_->getInstructionIndex(instr);
+ return Indexes->getInstructionIndex(instr);
}
/// Returns the instruction associated with the given index.
MachineInstr* getInstructionFromIndex(SlotIndex index) const {
- return indexes_->getInstructionFromIndex(index);
+ return Indexes->getInstructionFromIndex(index);
}
/// Return the first index in the given basic block.
SlotIndex getMBBStartIdx(const MachineBasicBlock *mbb) const {
- return indexes_->getMBBStartIdx(mbb);
+ return Indexes->getMBBStartIdx(mbb);
}
/// Return the last index in the given basic block.
SlotIndex getMBBEndIdx(const MachineBasicBlock *mbb) const {
- return indexes_->getMBBEndIdx(mbb);
+ return Indexes->getMBBEndIdx(mbb);
}
- bool isLiveInToMBB(const LiveInterval &li,
+ bool isLiveInToMBB(const LiveRange &LR,
const MachineBasicBlock *mbb) const {
- return li.liveAt(getMBBStartIdx(mbb));
+ return LR.liveAt(getMBBStartIdx(mbb));
}
- LiveRange* findEnteringRange(LiveInterval &li,
- const MachineBasicBlock *mbb) {
- return li.getLiveRangeContaining(getMBBStartIdx(mbb));
- }
-
- bool isLiveOutOfMBB(const LiveInterval &li,
+ bool isLiveOutOfMBB(const LiveRange &LR,
const MachineBasicBlock *mbb) const {
- return li.liveAt(getMBBEndIdx(mbb).getPrevSlot());
+ return LR.liveAt(getMBBEndIdx(mbb).getPrevSlot());
}
- LiveRange* findExitingRange(LiveInterval &li,
- const MachineBasicBlock *mbb) {
- return li.getLiveRangeContaining(getMBBEndIdx(mbb).getPrevSlot());
+ MachineBasicBlock* getMBBFromIndex(SlotIndex index) const {
+ return Indexes->getMBBFromIndex(index);
}
- MachineBasicBlock* getMBBFromIndex(SlotIndex index) const {
- return indexes_->getMBBFromIndex(index);
+ void insertMBBInMaps(MachineBasicBlock *MBB) {
+ Indexes->insertMBBInMaps(MBB);
+ assert(unsigned(MBB->getNumber()) == RegMaskBlocks.size() &&
+ "Blocks must be added in order.");
+ RegMaskBlocks.push_back(std::make_pair(RegMaskSlots.size(), 0));
}
SlotIndex InsertMachineInstrInMaps(MachineInstr *MI) {
- return indexes_->insertMachineInstrInMaps(MI);
+ return Indexes->insertMachineInstrInMaps(MI);
}
- void RemoveMachineInstrFromMaps(MachineInstr *MI) {
- indexes_->removeMachineInstrFromMaps(MI);
+ void InsertMachineInstrRangeInMaps(MachineBasicBlock::iterator B,
+ MachineBasicBlock::iterator E) {
+ for (MachineBasicBlock::iterator I = B; I != E; ++I)
+ Indexes->insertMachineInstrInMaps(I);
}
- void ReplaceMachineInstrInMaps(MachineInstr *MI, MachineInstr *NewMI) {
- indexes_->replaceMachineInstrInMaps(MI, NewMI);
+ void RemoveMachineInstrFromMaps(MachineInstr *MI) {
+ Indexes->removeMachineInstrFromMaps(MI);
}
- void InsertMBBInMaps(MachineBasicBlock *MBB) {
- indexes_->insertMBBInMaps(MBB);
+ void ReplaceMachineInstrInMaps(MachineInstr *MI, MachineInstr *NewMI) {
+ Indexes->replaceMachineInstrInMaps(MI, NewMI);
}
bool findLiveInMBBs(SlotIndex Start, SlotIndex End,
SmallVectorImpl<MachineBasicBlock*> &MBBs) const {
- return indexes_->findLiveInMBBs(Start, End, MBBs);
- }
-
- void renumber() {
- indexes_->renumberIndexes();
+ return Indexes->findLiveInMBBs(Start, End, MBBs);
}
VNInfo::Allocator& getVNInfoAllocator() { return VNInfoAllocator; }
- virtual void getAnalysisUsage(AnalysisUsage &AU) const;
- virtual void releaseMemory();
+ void getAnalysisUsage(AnalysisUsage &AU) const override;
+ void releaseMemory() override;
/// runOnMachineFunction - pass entry point
- virtual bool runOnMachineFunction(MachineFunction&);
+ bool runOnMachineFunction(MachineFunction&) override;
/// print - Implement the dump method.
- virtual void print(raw_ostream &O, const Module* = 0) const;
-
- /// addIntervalsForSpills - Create new intervals for spilled defs / uses of
- /// the given interval. FIXME: It also returns the weight of the spill slot
- /// (if any is created) by reference. This is temporary.
- std::vector<LiveInterval*>
- addIntervalsForSpills(const LiveInterval& i,
- const SmallVectorImpl<LiveInterval*> &SpillIs,
- const MachineLoopInfo *loopInfo, VirtRegMap& vrm);
-
- /// spillPhysRegAroundRegDefsUses - Spill the specified physical register
- /// around all defs and uses of the specified interval. Return true if it
- /// was able to cut its interval.
- bool spillPhysRegAroundRegDefsUses(const LiveInterval &li,
- unsigned PhysReg, VirtRegMap &vrm);
-
- /// isReMaterializable - Returns true if every definition of MI of every
- /// val# of the specified interval is re-materializable. Also returns true
- /// by reference if all of the defs are load instructions.
- bool isReMaterializable(const LiveInterval &li,
- const SmallVectorImpl<LiveInterval*> &SpillIs,
- bool &isLoad);
-
- /// isReMaterializable - Returns true if the definition MI of the specified
- /// val# of the specified interval is re-materializable.
- bool isReMaterializable(const LiveInterval &li, const VNInfo *ValNo,
- MachineInstr *MI);
-
- /// getRepresentativeReg - Find the largest super register of the specified
- /// physical register.
- unsigned getRepresentativeReg(unsigned Reg) const;
-
- /// getNumConflictsWithPhysReg - Return the number of uses and defs of the
- /// specified interval that conflicts with the specified physical register.
- unsigned getNumConflictsWithPhysReg(const LiveInterval &li,
- unsigned PhysReg) const;
-
- /// intervalIsInOneMBB - Returns true if the specified interval is entirely
- /// within a single basic block.
- bool intervalIsInOneMBB(const LiveInterval &li) const;
-
- /// getLastSplitPoint - Return the last possible insertion point in mbb for
- /// spilling and splitting code. This is the first terminator, or the call
- /// instruction if li is live into a landing pad successor.
- MachineBasicBlock::iterator getLastSplitPoint(const LiveInterval &li,
- MachineBasicBlock *mbb);
+ void print(raw_ostream &O, const Module* = nullptr) const override;
+
+ /// intervalIsInOneMBB - If LI is confined to a single basic block, return
+ /// a pointer to that block. If LI is live in to or out of any block,
+ /// return NULL.
+ MachineBasicBlock *intervalIsInOneMBB(const LiveInterval &LI) const;
+
+ /// Returns true if VNI is killed by any PHI-def values in LI.
+ /// This may conservatively return true to avoid expensive computations.
+ bool hasPHIKill(const LiveInterval &LI, const VNInfo *VNI) const;
+
+ /// addKillFlags - Add kill flags to any instruction that kills a virtual
+ /// register.
+ void addKillFlags(const VirtRegMap*);
+
+ /// handleMove - call this method to notify LiveIntervals that
+ /// instruction 'mi' has been moved within a basic block. This will update
+ /// the live intervals for all operands of mi. Moves between basic blocks
+ /// are not supported.
+ ///
+ /// \param UpdateFlags Update live intervals for nonallocatable physregs.
+ void handleMove(MachineInstr* MI, bool UpdateFlags = false);
+
+ /// moveIntoBundle - Update intervals for operands of MI so that they
+ /// begin/end on the SlotIndex for BundleStart.
+ ///
+ /// \param UpdateFlags Update live intervals for nonallocatable physregs.
+ ///
+ /// Requires MI and BundleStart to have SlotIndexes, and assumes
+ /// existing liveness is accurate. BundleStart should be the first
+ /// instruction in the Bundle.
+ void handleMoveIntoBundle(MachineInstr* MI, MachineInstr* BundleStart,
+ bool UpdateFlags = false);
+
+ /// repairIntervalsInRange - Update live intervals for instructions in a
+ /// range of iterators. It is intended for use after target hooks that may
+ /// insert or remove instructions, and is only efficient for a small number
+ /// of instructions.
+ ///
+ /// OrigRegs is a vector of registers that were originally used by the
+ /// instructions in the range between the two iterators.
+ ///
+ /// Currently, the only only changes that are supported are simple removal
+ /// and addition of uses.
+ void repairIntervalsInRange(MachineBasicBlock *MBB,
+ MachineBasicBlock::iterator Begin,
+ MachineBasicBlock::iterator End,
+ ArrayRef<unsigned> OrigRegs);
+
+ // Register mask functions.
+ //
+ // Machine instructions may use a register mask operand to indicate that a
+ // large number of registers are clobbered by the instruction. This is
+ // typically used for calls.
+ //
+ // For compile time performance reasons, these clobbers are not recorded in
+ // the live intervals for individual physical registers. Instead,
+ // LiveIntervalAnalysis maintains a sorted list of instructions with
+ // register mask operands.
+
+ /// getRegMaskSlots - Returns a sorted array of slot indices of all
+ /// instructions with register mask operands.
+ ArrayRef<SlotIndex> getRegMaskSlots() const { return RegMaskSlots; }
+
+ /// getRegMaskSlotsInBlock - Returns a sorted array of slot indices of all
+ /// instructions with register mask operands in the basic block numbered
+ /// MBBNum.
+ ArrayRef<SlotIndex> getRegMaskSlotsInBlock(unsigned MBBNum) const {
+ std::pair<unsigned, unsigned> P = RegMaskBlocks[MBBNum];
+ return getRegMaskSlots().slice(P.first, P.second);
+ }
+
+ /// getRegMaskBits() - Returns an array of register mask pointers
+ /// corresponding to getRegMaskSlots().
+ ArrayRef<const uint32_t*> getRegMaskBits() const { return RegMaskBits; }
+
+ /// getRegMaskBitsInBlock - Returns an array of mask pointers corresponding
+ /// to getRegMaskSlotsInBlock(MBBNum).
+ ArrayRef<const uint32_t*> getRegMaskBitsInBlock(unsigned MBBNum) const {
+ std::pair<unsigned, unsigned> P = RegMaskBlocks[MBBNum];
+ return getRegMaskBits().slice(P.first, P.second);
+ }
+
+ /// checkRegMaskInterference - Test if LI is live across any register mask
+ /// instructions, and compute a bit mask of physical registers that are not
+ /// clobbered by any of them.
+ ///
+ /// Returns false if LI doesn't cross any register mask instructions. In
+ /// that case, the bit vector is not filled in.
+ bool checkRegMaskInterference(LiveInterval &LI,
+ BitVector &UsableRegs);
+
+ // Register unit functions.
+ //
+ // Fixed interference occurs when MachineInstrs use physregs directly
+ // instead of virtual registers. This typically happens when passing
+ // arguments to a function call, or when instructions require operands in
+ // fixed registers.
+ //
+ // Each physreg has one or more register units, see MCRegisterInfo. We
+ // track liveness per register unit to handle aliasing registers more
+ // efficiently.
+
+ /// getRegUnit - Return the live range for Unit.
+ /// It will be computed if it doesn't exist.
+ LiveRange &getRegUnit(unsigned Unit) {
+ LiveRange *LR = RegUnitRanges[Unit];
+ if (!LR) {
+ // Compute missing ranges on demand.
+ RegUnitRanges[Unit] = LR = new LiveRange();
+ computeRegUnitRange(*LR, Unit);
+ }
+ return *LR;
+ }
+
+ /// getCachedRegUnit - Return the live range for Unit if it has already
+ /// been computed, or NULL if it hasn't been computed yet.
+ LiveRange *getCachedRegUnit(unsigned Unit) {
+ return RegUnitRanges[Unit];
+ }
+
+ const LiveRange *getCachedRegUnit(unsigned Unit) const {
+ return RegUnitRanges[Unit];
+ }
private:
- /// computeIntervals - Compute live intervals.
- void computeIntervals();
-
- /// handleRegisterDef - update intervals for a register def
- /// (calls handlePhysicalRegisterDef and
- /// handleVirtualRegisterDef)
- void handleRegisterDef(MachineBasicBlock *MBB,
- MachineBasicBlock::iterator MI,
- SlotIndex MIIdx,
- MachineOperand& MO, unsigned MOIdx);
-
- /// isPartialRedef - Return true if the specified def at the specific index
- /// is partially re-defining the specified live interval. A common case of
- /// this is a definition of the sub-register.
- bool isPartialRedef(SlotIndex MIIdx, MachineOperand &MO,
- LiveInterval &interval);
-
- /// handleVirtualRegisterDef - update intervals for a virtual
- /// register def
- void handleVirtualRegisterDef(MachineBasicBlock *MBB,
- MachineBasicBlock::iterator MI,
- SlotIndex MIIdx, MachineOperand& MO,
- unsigned MOIdx,
- LiveInterval& interval);
-
- /// handlePhysicalRegisterDef - update intervals for a physical register
- /// def.
- void handlePhysicalRegisterDef(MachineBasicBlock* mbb,
- MachineBasicBlock::iterator mi,
- SlotIndex MIIdx, MachineOperand& MO,
- LiveInterval &interval,
- MachineInstr *CopyMI);
-
- /// handleLiveInRegister - Create interval for a livein register.
- void handleLiveInRegister(MachineBasicBlock* mbb,
- SlotIndex MIIdx,
- LiveInterval &interval, bool isAlias = false);
-
- /// getReMatImplicitUse - If the remat definition MI has one (for now, we
- /// only allow one) virtual register operand, then its uses are implicitly
- /// using the register. Returns the virtual register.
- unsigned getReMatImplicitUse(const LiveInterval &li,
- MachineInstr *MI) const;
-
- /// isValNoAvailableAt - Return true if the val# of the specified interval
- /// which reaches the given instruction also reaches the specified use
- /// index.
- bool isValNoAvailableAt(const LiveInterval &li, MachineInstr *MI,
- SlotIndex UseIdx) const;
-
- /// isReMaterializable - Returns true if the definition MI of the specified
- /// val# of the specified interval is re-materializable. Also returns true
- /// by reference if the def is a load.
- bool isReMaterializable(const LiveInterval &li, const VNInfo *ValNo,
- MachineInstr *MI,
- const SmallVectorImpl<LiveInterval*> &SpillIs,
- bool &isLoad);
-
- /// tryFoldMemoryOperand - Attempts to fold either a spill / restore from
- /// slot / to reg or any rematerialized load into ith operand of specified
- /// MI. If it is successul, MI is updated with the newly created MI and
- /// returns true.
- bool tryFoldMemoryOperand(MachineInstr* &MI, VirtRegMap &vrm,
- MachineInstr *DefMI, SlotIndex InstrIdx,
- SmallVector<unsigned, 2> &Ops,
- bool isSS, int FrameIndex, unsigned Reg);
-
- /// canFoldMemoryOperand - Return true if the specified load / store
- /// folding is possible.
- bool canFoldMemoryOperand(MachineInstr *MI,
- SmallVector<unsigned, 2> &Ops,
- bool ReMatLoadSS) const;
-
- /// anyKillInMBBAfterIdx - Returns true if there is a kill of the specified
- /// VNInfo that's after the specified index but is within the basic block.
- bool anyKillInMBBAfterIdx(const LiveInterval &li, const VNInfo *VNI,
- MachineBasicBlock *MBB,
- SlotIndex Idx) const;
-
- /// hasAllocatableSuperReg - Return true if the specified physical register
- /// has any super register that's allocatable.
- bool hasAllocatableSuperReg(unsigned Reg) const;
-
- /// SRInfo - Spill / restore info.
- struct SRInfo {
- SlotIndex index;
- unsigned vreg;
- bool canFold;
- SRInfo(SlotIndex i, unsigned vr, bool f)
- : index(i), vreg(vr), canFold(f) {}
- };
-
- bool alsoFoldARestore(int Id, SlotIndex index, unsigned vr,
- BitVector &RestoreMBBs,
- DenseMap<unsigned,std::vector<SRInfo> >&RestoreIdxes);
- void eraseRestoreInfo(int Id, SlotIndex index, unsigned vr,
- BitVector &RestoreMBBs,
- DenseMap<unsigned,std::vector<SRInfo> >&RestoreIdxes);
-
- /// handleSpilledImpDefs - Remove IMPLICIT_DEF instructions which are being
- /// spilled and create empty intervals for their uses.
- void handleSpilledImpDefs(const LiveInterval &li, VirtRegMap &vrm,
- const TargetRegisterClass* rc,
- std::vector<LiveInterval*> &NewLIs);
-
- /// rewriteImplicitOps - Rewrite implicit use operands of MI (i.e. uses of
- /// interval on to-be re-materialized operands of MI) with new register.
- void rewriteImplicitOps(const LiveInterval &li,
- MachineInstr *MI, unsigned NewVReg, VirtRegMap &vrm);
-
- /// rewriteInstructionForSpills, rewriteInstructionsForSpills - Helper
- /// functions for addIntervalsForSpills to rewrite uses / defs for the given
- /// live range.
- bool rewriteInstructionForSpills(const LiveInterval &li, const VNInfo *VNI,
- bool TrySplit, SlotIndex index, SlotIndex end,
- MachineInstr *MI, MachineInstr *OrigDefMI, MachineInstr *DefMI,
- unsigned Slot, int LdSlot,
- bool isLoad, bool isLoadSS, bool DefIsReMat, bool CanDelete,
- VirtRegMap &vrm, const TargetRegisterClass* rc,
- SmallVector<int, 4> &ReMatIds, const MachineLoopInfo *loopInfo,
- unsigned &NewVReg, unsigned ImpUse, bool &HasDef, bool &HasUse,
- DenseMap<unsigned,unsigned> &MBBVRegsMap,
- std::vector<LiveInterval*> &NewLIs);
- void rewriteInstructionsForSpills(const LiveInterval &li, bool TrySplit,
- LiveInterval::Ranges::const_iterator &I,
- MachineInstr *OrigDefMI, MachineInstr *DefMI, unsigned Slot, int LdSlot,
- bool isLoad, bool isLoadSS, bool DefIsReMat, bool CanDelete,
- VirtRegMap &vrm, const TargetRegisterClass* rc,
- SmallVector<int, 4> &ReMatIds, const MachineLoopInfo *loopInfo,
- BitVector &SpillMBBs,
- DenseMap<unsigned,std::vector<SRInfo> > &SpillIdxes,
- BitVector &RestoreMBBs,
- DenseMap<unsigned,std::vector<SRInfo> > &RestoreIdxes,
- DenseMap<unsigned,unsigned> &MBBVRegsMap,
- std::vector<LiveInterval*> &NewLIs);
-
- // Normalize the spill weight of all the intervals in NewLIs.
- void normalizeSpillWeights(std::vector<LiveInterval*> &NewLIs);
+ /// Compute live intervals for all virtual registers.
+ void computeVirtRegs();
+
+ /// Compute RegMaskSlots and RegMaskBits.
+ void computeRegMasks();
+
+ /// Walk the values in @p LI and check for dead values:
+ /// - Dead PHIDef values are marked as unused.
+ /// - Dead operands are marked as such.
+ /// - Completely dead machine instructions are added to the @p dead vector
+ /// if it is not nullptr.
+ /// Returns true if any PHI value numbers have been removed which may
+ /// have separated the interval into multiple connected components.
+ bool computeDeadValues(LiveInterval &LI,
+ SmallVectorImpl<MachineInstr*> *dead);
static LiveInterval* createInterval(unsigned Reg);
void printInstrs(raw_ostream &O) const;
void dumpInstrs() const;
+
+ void computeLiveInRegUnits();
+ void computeRegUnitRange(LiveRange&, unsigned Unit);
+ void computeVirtRegInterval(LiveInterval&);
+
+
+ /// Helper function for repairIntervalsInRange(), walks backwards and
+ /// creates/modifies live segments in @p LR to match the operands found.
+ /// Only full operands or operands with subregisters matching @p LaneMask
+ /// are considered.
+ void repairOldRegInRange(MachineBasicBlock::iterator Begin,
+ MachineBasicBlock::iterator End,
+ const SlotIndex endIdx, LiveRange &LR,
+ unsigned Reg, unsigned LaneMask = ~0u);
+
+ class HMEditor;
};
} // End llvm namespace