diff --git a/include/llvm/CodeGen/LiveIntervalAnalysis.h b/include/llvm/CodeGen/LiveIntervalAnalysis.h
index 74e47413d8e33e786901d31b1264a70f99f5bfb4..61c705e04d29be4b028c2dc54e5eec2c040a29b3 100644 (file)
//
//===----------------------------------------------------------------------===//
-#ifndef LLVM_CODEGEN_LIVEINTERVAL_ANALYSIS_H
-#define LLVM_CODEGEN_LIVEINTERVAL_ANALYSIS_H
+#ifndef LLVM_CODEGEN_LIVEINTERVALANALYSIS_H
+#define LLVM_CODEGEN_LIVEINTERVALANALYSIS_H
#include "llvm/ADT/IndexedMap.h"
#include "llvm/ADT/SmallVector.h"
class LiveIntervals : public MachineFunctionPass {
MachineFunction* MF;
MachineRegisterInfo* MRI;
- const TargetMachine* TM;
const TargetRegisterInfo* TRI;
const TargetInstrInfo* TII;
AliasAnalysis *AA;
// Interval removal.
void removeInterval(unsigned Reg) {
delete VirtRegIntervals[Reg];
- VirtRegIntervals[Reg] = 0;
+ VirtRegIntervals[Reg] = nullptr;
}
/// Given a register and an instruction, adds a live segment from that
/// Return true if the interval may have been separated into multiple
/// connected components.
bool shrinkToUses(LiveInterval *li,
- SmallVectorImpl<MachineInstr*> *dead = 0);
+ SmallVectorImpl<MachineInstr*> *dead = nullptr);
+
+ /// Specialized version of
+ /// shrinkToUses(LiveInterval *li, SmallVectorImpl<MachineInstr*> *dead)
+ /// that works on a subregister live range and only looks at uses matching
+ /// the lane mask of the subregister range.
+ void shrinkToUses(LiveInterval::SubRange &SR, unsigned Reg);
/// extendToIndices - Extend the live range of LI to reach all points in
/// Indices. The points in the Indices array must be jointly dominated by
/// See also LiveRangeCalc::extend().
void extendToIndices(LiveRange &LR, ArrayRef<SlotIndex> Indices);
- /// pruneValue - If an LI value is live at Kill, prune its live range by
- /// removing any liveness reachable from Kill. Add live range end points to
+
+ /// If @p LR has a live value at @p Kill, prune its live range by removing
+ /// any liveness reachable from Kill. Add live range end points to
/// EndPoints such that extendToIndices(LI, EndPoints) will reconstruct the
/// value's live range.
///
/// Calling pruneValue() and extendToIndices() can be used to reconstruct
/// SSA form after adding defs to a virtual register.
- void pruneValue(LiveInterval *LI, SlotIndex Kill,
+ void pruneValue(LiveRange &LR, SlotIndex Kill,
SmallVectorImpl<SlotIndex> *EndPoints);
SlotIndexes *getSlotIndexes() const {
VNInfo::Allocator& getVNInfoAllocator() { return VNInfoAllocator; }
- virtual void getAnalysisUsage(AnalysisUsage &AU) const;
- virtual void releaseMemory();
+ void getAnalysisUsage(AnalysisUsage &AU) const override;
+ void releaseMemory() override;
/// runOnMachineFunction - pass entry point
- virtual bool runOnMachineFunction(MachineFunction&);
+ bool runOnMachineFunction(MachineFunction&) override;
/// print - Implement the dump method.
- virtual void print(raw_ostream &O, const Module* = 0) const;
+ void print(raw_ostream &O, const Module* = nullptr) const override;
/// intervalIsInOneMBB - If LI is confined to a single basic block, return
/// a pointer to that block. If LI is live in to or out of any block,
/// Compute RegMaskSlots and RegMaskBits.
void computeRegMasks();
+ /// Walk the values in @p LI and check for dead values:
+ /// - Dead PHIDef values are marked as unused.
+ /// - Dead operands are marked as such.
+ /// - Completely dead machine instructions are added to the @p dead vector
+ /// if it is not nullptr.
+ /// Returns true if any PHI value numbers have been removed which may
+ /// have separated the interval into multiple connected components.
+ bool computeDeadValues(LiveInterval &LI,
+ SmallVectorImpl<MachineInstr*> *dead);
+
static LiveInterval* createInterval(unsigned Reg);
void printInstrs(raw_ostream &O) const;
void computeRegUnitRange(LiveRange&, unsigned Unit);
void computeVirtRegInterval(LiveInterval&);
+
+ /// Helper function for repairIntervalsInRange(), walks backwards and
+ /// creates/modifies live segments in @p LR to match the operands found.
+ /// Only full operands or operands with subregisters matching @p LaneMask
+ /// are considered.
+ void repairOldRegInRange(MachineBasicBlock::iterator Begin,
+ MachineBasicBlock::iterator End,
+ const SlotIndex endIdx, LiveRange &LR,
+ unsigned Reg, unsigned LaneMask = ~0u);
+
class HMEditor;
};
} // End llvm namespace