index 244006445b7c6a7083742ff7f9e944e394afcb3e..44f40819c71900436646d96da5f7fdfffdb1c8c4 100644 (file)
--- a/include/llvm/DIBuilder.h
+++ b/include/llvm/DIBuilder.h
#include "llvm/ADT/ArrayRef.h"
#include "llvm/ADT/StringRef.h"
+#include "llvm/DebugInfo.h"
#include "llvm/Support/DataTypes.h"
+#include "llvm/Support/ValueHandle.h"
namespace llvm {
class BasicBlock;
class MDNode;
class StringRef;
class DIBasicType;
+ class DICompileUnit;
class DICompositeType;
class DIDerivedType;
class DIDescriptor;
private:
Module &M;
LLVMContext & VMContext;
- MDNode *TheCU;
MDNode *TempEnumTypes;
MDNode *TempRetainTypes;
Function *ValueFn; // llvm.dbg.value
SmallVector<Value *, 4> AllEnumTypes;
- SmallVector<Value *, 4> AllRetainTypes;
+ /// Use TrackingVH to collect RetainTypes, since they can be updated
+ /// later on.
+ SmallVector<TrackingVH<MDNode>, 4> AllRetainTypes;
SmallVector<Value *, 4> AllSubprograms;
SmallVector<Value *, 4> AllGVs;
SmallVector<Value *, 4> AllImportedModules;
+ DITemplateValueParameter
+ createTemplateValueParameter(unsigned Tag, DIDescriptor Scope,
+ StringRef Name, DIType Ty, Value *Val,
+ MDNode *File = 0, unsigned LineNo = 0,
+ unsigned ColumnNo = 0);
+
DIBuilder(const DIBuilder &) LLVM_DELETED_FUNCTION;
void operator=(const DIBuilder &) LLVM_DELETED_FUNCTION;
public:
explicit DIBuilder(Module &M);
- const MDNode *getCU() { return TheCU; }
enum ComplexAddrKind { OpPlus=1, OpDeref };
/// finalize - Construct any deferred debug info descriptors.
/// Objective-C.
/// @param SplitName The name of the file that we'll split debug info out
/// into.
- void createCompileUnit(unsigned Lang, StringRef File, StringRef Dir,
- StringRef Producer, bool isOptimized,
- StringRef Flags, unsigned RV,
- StringRef SplitName = StringRef());
+ DICompileUnit createCompileUnit(unsigned Lang, StringRef File,
+ StringRef Dir, StringRef Producer,
+ bool isOptimized, StringRef Flags,
+ unsigned RV,
+ StringRef SplitName = StringRef());
/// createFile - Create a file descriptor to hold debugging information
/// for a file.
DIFile createFile(StringRef Filename, StringRef Directory);
/// createEnumerator - Create a single enumerator value.
- DIEnumerator createEnumerator(StringRef Name, uint64_t Val);
+ DIEnumerator createEnumerator(StringRef Name, int64_t Val);
- /// createNullPtrType - Create C++0x nullptr type.
- DIBasicType createNullPtrType(StringRef Name);
+ /// \brief Create a DWARF unspecified type.
+ DIBasicType createUnspecifiedType(StringRef Name);
+
+ /// \brief Create C++11 nullptr type.
+ DIBasicType createNullPtrType();
/// createBasicType - Create debugging information entry for a basic
/// type.
/// DW_AT_containing_type. See DWARF documentation
/// for more info.
/// @param TemplateParms Template type parameters.
+ /// @param UniqueIdentifier A unique identifier for the class.
DICompositeType createClassType(DIDescriptor Scope, StringRef Name,
DIFile File, unsigned LineNumber,
uint64_t SizeInBits, uint64_t AlignInBits,
uint64_t OffsetInBits, unsigned Flags,
DIType DerivedFrom, DIArray Elements,
- MDNode *VTableHolder = 0,
- MDNode *TemplateParms = 0);
+ DIType VTableHolder = DIType(),
+ MDNode *TemplateParms = 0,
+ StringRef UniqueIdentifier = StringRef());
/// createStructType - Create debugging information entry for a struct.
/// @param Scope Scope in which this struct is defined.
/// @param Flags Flags to encode member attribute, e.g. private
/// @param Elements Struct elements.
/// @param RunTimeLang Optional parameter, Objective-C runtime version.
+ /// @param UniqueIdentifier A unique identifier for the struct.
DICompositeType createStructType(DIDescriptor Scope, StringRef Name,
DIFile File, unsigned LineNumber,
uint64_t SizeInBits, uint64_t AlignInBits,
unsigned Flags, DIType DerivedFrom,
DIArray Elements, unsigned RunTimeLang = 0,
- MDNode *VTableHolder = 0);
+ DIType VTableHolder = DIType(),
+ StringRef UniqueIdentifier = StringRef());
/// createUnionType - Create debugging information entry for an union.
/// @param Scope Scope in which this union is defined.
/// @param Flags Flags to encode member attribute, e.g. private
/// @param Elements Union elements.
/// @param RunTimeLang Optional parameter, Objective-C runtime version.
+ /// @param UniqueIdentifier A unique identifier for the union.
DICompositeType createUnionType(
DIDescriptor Scope, StringRef Name, DIFile File, unsigned LineNumber,
uint64_t SizeInBits, uint64_t AlignInBits, unsigned Flags,
- DIArray Elements, unsigned RunTimeLang = 0);
+ DIArray Elements, unsigned RunTimeLang = 0,
+ StringRef UniqueIdentifier = StringRef());
/// createTemplateTypeParameter - Create debugging information for template
/// type parameter.
DIType Ty, Value *Val, MDNode *File = 0,
unsigned LineNo = 0, unsigned ColumnNo = 0);
+ /// \brief Create debugging information for a template template parameter.
+ /// @param Scope Scope in which this type is defined.
+ /// @param Name Value parameter name.
+ /// @param Ty Parameter type.
+ /// @param Val The fully qualified name of the template.
+ /// @param File File where this type parameter is defined.
+ /// @param LineNo Line number.
+ /// @param ColumnNo Column Number.
+ DITemplateValueParameter
+ createTemplateTemplateParameter(DIDescriptor Scope, StringRef Name,
+ DIType Ty, StringRef Val, MDNode *File = 0,
+ unsigned LineNo = 0, unsigned ColumnNo = 0);
+
+ /// \brief Create debugging information for a template parameter pack.
+ /// @param Scope Scope in which this type is defined.
+ /// @param Name Value parameter name.
+ /// @param Ty Parameter type.
+ /// @param Val An array of types in the pack.
+ /// @param File File where this type parameter is defined.
+ /// @param LineNo Line number.
+ /// @param ColumnNo Column Number.
+ DITemplateValueParameter
+ createTemplateParameterPack(DIDescriptor Scope, StringRef Name,
+ DIType Ty, DIArray Val, MDNode *File = 0,
+ unsigned LineNo = 0, unsigned ColumnNo = 0);
+
/// createArrayType - Create debugging information entry for an array.
/// @param Size Array size.
/// @param AlignInBits Alignment.
/// @param AlignInBits Member alignment.
/// @param Elements Enumeration elements.
/// @param UnderlyingType Underlying type of a C++11/ObjC fixed enum.
+ /// @param UniqueIdentifier A unique identifier for the enum.
DICompositeType createEnumerationType(DIDescriptor Scope, StringRef Name,
- DIFile File, unsigned LineNumber,
- uint64_t SizeInBits,
- uint64_t AlignInBits,
- DIArray Elements,
- DIType UnderlyingType);
+ DIFile File, unsigned LineNumber, uint64_t SizeInBits,
+ uint64_t AlignInBits, DIArray Elements, DIType UnderlyingType,
+ StringRef UniqueIdentifier = StringRef());
/// createSubroutineType - Create subroutine type.
- /// @param File File in which this subroutine is defined.
- /// @param ParameterTypes An array of subroutine parameter types. This
- /// includes return type at 0th index.
- DICompositeType createSubroutineType(DIFile File, DIArray ParameterTypes);
+ /// @param File File in which this subroutine is defined.
+ /// @param ParameterTypes An array of subroutine parameter types. This
+ /// includes return type at 0th index.
+ /// @param Flags E.g.: LValueReference.
+ /// These flags are used to emit dwarf attributes.
+ DICompositeType createSubroutineType(DIFile File, DIArray ParameterTypes,
+ unsigned Flags = 0);
/// createArtificialType - Create a new DIType with "artificial" flag set.
DIType createArtificialType(DIType Ty);
DIType createObjectPointerType(DIType Ty);
/// createForwardDecl - Create a temporary forward-declared type.
- DIType createForwardDecl(unsigned Tag, StringRef Name, DIDescriptor Scope,
- DIFile F, unsigned Line, unsigned RuntimeLang = 0,
- uint64_t SizeInBits = 0, uint64_t AlignInBits = 0);
+ DICompositeType createForwardDecl(unsigned Tag, StringRef Name,
+ DIDescriptor Scope, DIFile F,
+ unsigned Line, unsigned RuntimeLang = 0,
+ uint64_t SizeInBits = 0,
+ uint64_t AlignInBits = 0,
+ StringRef UniqueIdentifier = StringRef());
/// retainType - Retain DIType in a module even if it is not referenced
/// through debug info anchors.
/// @param Ty Variable Type
/// @param AlwaysPreserve Boolean. Set to true if debug info for this
/// variable should be preserved in optimized build.
- /// @param Flags Flags, e.g. artificial variable.
- /// @param ArgNo If this variable is an arugment then this argument's
+ /// @param Flags Flags, e.g. artificial variable.
+ /// @param ArgNo If this variable is an argument then this argument's
/// number. 1 indicates 1st argument.
DIVariable createLocalVariable(unsigned Tag, DIDescriptor Scope,
StringRef Name,
/// @param LineNo Line number.
/// @param Ty Variable Type
/// @param Addr An array of complex address operations.
- /// @param ArgNo If this variable is an arugment then this argument's
+ /// @param ArgNo If this variable is an argument then this argument's
/// number. 1 indicates 1st argument.
DIVariable createComplexVariable(unsigned Tag, DIDescriptor Scope,
StringRef Name, DIFile F, unsigned LineNo,
/// @param isDefinition True if this is a function definition.
/// @param ScopeLine Set to the beginning of the scope this starts
/// @param Flags e.g. is this function prototyped or not.
- /// This flags are used to emit dwarf attributes.
+ /// These flags are used to emit dwarf attributes.
/// @param isOptimized True if optimization is ON.
/// @param Fn llvm::Function pointer.
/// @param TParam Function template parameters.
MDNode *TParam = 0,
MDNode *Decl = 0);
+ /// FIXME: this is added for dragonegg. Once we update dragonegg
+ /// to call resolve function, this will be removed.
+ DISubprogram createFunction(DIScopeRef Scope, StringRef Name,
+ StringRef LinkageName,
+ DIFile File, unsigned LineNo,
+ DICompositeType Ty, bool isLocalToUnit,
+ bool isDefinition,
+ unsigned ScopeLine,
+ unsigned Flags = 0,
+ bool isOptimized = false,
+ Function *Fn = 0,
+ MDNode *TParam = 0,
+ MDNode *Decl = 0);
+
/// createMethod - Create a new descriptor for the specified C++ method.
/// See comments in DISubprogram for descriptions of these fields.
/// @param Scope Function scope.
DICompositeType Ty, bool isLocalToUnit,
bool isDefinition,
unsigned Virtuality = 0, unsigned VTableIndex = 0,
- MDNode *VTableHolder = 0,
+ DIType VTableHolder = DIType(),
unsigned Flags = 0,
bool isOptimized = false,
Function *Fn = 0,