index 1b97f6254215ad1dcc46c7223cb7560dd0b05fb8..ebdd32682393f750c97b1462b36c39b9b1e9f752 100644 (file)
#define LLVM_IR_DEBUGINFO_H
#include "llvm/ADT/DenseMap.h"
-#include "llvm/ADT/iterator_range.h"
#include "llvm/ADT/SmallPtrSet.h"
#include "llvm/ADT/SmallVector.h"
#include "llvm/ADT/StringRef.h"
+#include "llvm/ADT/iterator_range.h"
#include "llvm/IR/Metadata.h"
#include "llvm/Support/Casting.h"
#include "llvm/Support/Dwarf.h"
+#include "llvm/Support/ErrorHandling.h"
+#include <iterator>
namespace llvm {
class BasicBlock;
class DbgDeclareInst;
class DbgValueInst;
class Instruction;
+class Metadata;
class MDNode;
class MDString;
class NamedMDNode;
class DIScope;
class DIObjCProperty;
-/// Maps from type identifier to the actual MDNode.
+/// \brief Maps from type identifier to the actual MDNode.
typedef DenseMap<const MDString *, MDNode *> DITypeIdentifierMap;
-/// DIDescriptor - A thin wraper around MDNode to access encoded debug info.
-/// This should not be stored in a container, because the underlying MDNode
-/// may change in certain situations.
+class DIHeaderFieldIterator
+ : public std::iterator<std::forward_iterator_tag, StringRef, std::ptrdiff_t,
+ const StringRef *, StringRef> {
+ StringRef Header;
+ StringRef Current;
+
+public:
+ DIHeaderFieldIterator() {}
+ explicit DIHeaderFieldIterator(StringRef Header)
+ : Header(Header), Current(Header.slice(0, Header.find('\0'))) {}
+ StringRef operator*() const { return Current; }
+ const StringRef * operator->() const { return &Current; }
+ DIHeaderFieldIterator &operator++() {
+ increment();
+ return *this;
+ }
+ DIHeaderFieldIterator operator++(int) {
+ DIHeaderFieldIterator X(*this);
+ increment();
+ return X;
+ }
+ bool operator==(const DIHeaderFieldIterator &X) const {
+ return Current.data() == X.Current.data();
+ }
+ bool operator!=(const DIHeaderFieldIterator &X) const {
+ return !(*this == X);
+ }
+
+ StringRef getHeader() const { return Header; }
+ StringRef getCurrent() const { return Current; }
+ StringRef getPrefix() const {
+ if (Current.begin() == Header.begin())
+ return StringRef();
+ return Header.slice(0, Current.begin() - Header.begin() - 1);
+ }
+ StringRef getSuffix() const {
+ if (Current.end() == Header.end())
+ return StringRef();
+ return Header.slice(Current.end() - Header.begin() + 1, StringRef::npos);
+ }
+
+ /// \brief Get the current field as a number.
+ ///
+ /// Convert the current field into a number. Return \c 0 on error.
+ template <class T> T getNumber() const {
+ T Int;
+ if (getCurrent().getAsInteger(0, Int))
+ return 0;
+ return Int;
+ }
+
+private:
+ void increment() {
+ assert(Current.data() != nullptr && "Cannot increment past the end");
+ StringRef Suffix = getSuffix();
+ Current = Suffix.slice(0, Suffix.find('\0'));
+ }
+};
+
+/// \brief A thin wraper around MDNode to access encoded debug info.
+///
+/// This should not be stored in a container, because the underlying MDNode may
+/// change in certain situations.
class DIDescriptor {
// Befriends DIRef so DIRef can befriend the protected member
// function: getFieldAs<DIRef>.
template <typename T> friend class DIRef;
public:
+ /// \brief Accessibility flags.
+ ///
+ /// The three accessibility flags are mutually exclusive and rolled together
+ /// in the first two bits.
enum {
- FlagPrivate = 1 << 0,
- FlagProtected = 1 << 1,
+ FlagAccessibility = 1 << 0 | 1 << 1,
+ FlagPrivate = 1,
+ FlagProtected = 2,
+ FlagPublic = 3,
+
FlagFwdDecl = 1 << 2,
FlagAppleBlock = 1 << 3,
FlagBlockByrefStruct = 1 << 4,
FlagObjectPointer = 1 << 10,
FlagVector = 1 << 11,
FlagStaticMember = 1 << 12,
- FlagIndirectVariable = 1 << 13,
- FlagLValueReference = 1 << 14,
- FlagRValueReference = 1 << 15
+ FlagLValueReference = 1 << 13,
+ FlagRValueReference = 1 << 14
};
protected:
bool Verify() const;
- operator MDNode *() const { return const_cast<MDNode *>(DbgNode); }
- MDNode *operator->() const { return const_cast<MDNode *>(DbgNode); }
+ MDNode *get() const { return const_cast<MDNode *>(DbgNode); }
+ operator MDNode *() const { return get(); }
+ MDNode *operator->() const { return get(); }
// An explicit operator bool so that we can do testing of DI values
// easily.
bool operator==(DIDescriptor Other) const { return DbgNode == Other.DbgNode; }
bool operator!=(DIDescriptor Other) const { return !operator==(Other); }
- uint16_t getTag() const {
- return getUnsignedField(0) & ~LLVMDebugVersionMask;
+ StringRef getHeader() const {
+ return getStringField(0);
+ }
+
+ size_t getNumHeaderFields() const {
+ return std::distance(DIHeaderFieldIterator(getHeader()),
+ DIHeaderFieldIterator());
+ }
+
+ DIHeaderFieldIterator header_begin() const {
+ return DIHeaderFieldIterator(getHeader());
+ }
+ DIHeaderFieldIterator header_end() const { return DIHeaderFieldIterator(); }
+
+ DIHeaderFieldIterator getHeaderIterator(unsigned Index) const {
+ // Since callers expect an empty string for out-of-range accesses, we can't
+ // use std::advance() here.
+ for (auto I = header_begin(), E = header_end(); I != E; ++I, --Index)
+ if (!Index)
+ return I;
+ return header_end();
+ }
+
+ StringRef getHeaderField(unsigned Index) const {
+ return *getHeaderIterator(Index);
}
+ template <class T> T getHeaderFieldAs(unsigned Index) const {
+ return getHeaderIterator(Index).getNumber<T>();
+ }
+
+ uint16_t getTag() const { return getHeaderFieldAs<uint16_t>(0); }
+
bool isDerivedType() const;
bool isCompositeType() const;
+ bool isSubroutineType() const;
bool isBasicType() const;
bool isVariable() const;
bool isSubprogram() const;
bool isSubrange() const;
bool isEnumerator() const;
bool isType() const;
- bool isUnspecifiedParameter() const;
bool isTemplateTypeParameter() const;
bool isTemplateValueParameter() const;
bool isObjCProperty() const;
bool isImportedEntity() const;
+ bool isExpression() const;
- /// print - print descriptor.
void print(raw_ostream &OS) const;
-
- /// dump - print descriptor to dbgs() with a newline.
void dump() const;
+
+ /// \brief Replace all uses of debug info referenced by this descriptor.
+ void replaceAllUsesWith(LLVMContext &VMContext, DIDescriptor D);
+ void replaceAllUsesWith(MDNode *D);
};
-/// DISubrange - This is used to represent ranges, for array bounds.
+/// \brief This is used to represent ranges, for array bounds.
class DISubrange : public DIDescriptor {
friend class DIDescriptor;
void printInternal(raw_ostream &OS) const;
public:
explicit DISubrange(const MDNode *N = nullptr) : DIDescriptor(N) {}
- int64_t getLo() const { return getInt64Field(1); }
- int64_t getCount() const { return getInt64Field(2); }
+ int64_t getLo() const { return getHeaderFieldAs<int64_t>(1); }
+ int64_t getCount() const { return getHeaderFieldAs<int64_t>(2); }
bool Verify() const;
};
-/// DIArray - This descriptor holds an array of descriptors.
-class DIArray : public DIDescriptor {
+/// \brief This descriptor holds an array of nodes with type T.
+template <typename T> class DITypedArray : public DIDescriptor {
public:
- explicit DIArray(const MDNode *N = nullptr) : DIDescriptor(N) {}
-
- unsigned getNumElements() const;
- DIDescriptor getElement(unsigned Idx) const {
- return getDescriptorField(Idx);
+ explicit DITypedArray(const MDNode *N = nullptr) : DIDescriptor(N) {}
+ unsigned getNumElements() const {
+ return DbgNode ? DbgNode->getNumOperands() : 0;
+ }
+ T getElement(unsigned Idx) const {
+ return getFieldAs<T>(Idx);
}
};
-/// DIEnumerator - A wrapper for an enumerator (e.g. X and Y in 'enum {X,Y}').
+typedef DITypedArray<DIDescriptor> DIArray;
+
+/// \brief A wrapper for an enumerator (e.g. X and Y in 'enum {X,Y}').
+///
/// FIXME: it seems strange that this doesn't have either a reference to the
/// type/precision or a file/line pair for location info.
class DIEnumerator : public DIDescriptor {
public:
explicit DIEnumerator(const MDNode *N = nullptr) : DIDescriptor(N) {}
- StringRef getName() const { return getStringField(1); }
- int64_t getEnumValue() const { return getInt64Field(2); }
+ StringRef getName() const { return getHeaderField(1); }
+ int64_t getEnumValue() const { return getHeaderFieldAs<int64_t>(2); }
bool Verify() const;
};
template <typename T> class DIRef;
typedef DIRef<DIScope> DIScopeRef;
typedef DIRef<DIType> DITypeRef;
+typedef DITypedArray<DITypeRef> DITypeArray;
-/// DIScope - A base class for various scopes.
+/// \brief A base class for various scopes.
///
/// Although, implementation-wise, DIScope is the parent class of most
/// other DIxxx classes, including DIType and its descendants, most of
public:
explicit DIScope(const MDNode *N = nullptr) : DIDescriptor(N) {}
- /// Gets the parent scope for this scope node or returns a
- /// default constructed scope.
+ /// \brief Get the parent scope.
+ ///
+ /// Gets the parent scope for this scope node or returns a default
+ /// constructed scope.
DIScopeRef getContext() const;
+ /// \brief Get the scope name.
+ ///
/// If the scope node has a name, return that, else return an empty string.
StringRef getName() const;
StringRef getFilename() const;
StringRef getDirectory() const;
- /// Generate a reference to this DIScope. Uses the type identifier instead
- /// of the actual MDNode if possible, to help type uniquing.
+ /// \brief Generate a reference to this DIScope.
+ ///
+ /// Uses the type identifier instead of the actual MDNode if possible, to
+ /// help type uniquing.
DIScopeRef getRef() const;
};
-/// Represents reference to a DIDescriptor, abstracts over direct and
-/// identifier-based metadata references.
+/// \brief Represents reference to a DIDescriptor.
+///
+/// Abstracts over direct and identifier-based metadata references.
template <typename T> class DIRef {
template <typename DescTy>
friend DescTy DIDescriptor::getFieldAs(unsigned Elt) const;
friend DIScopeRef DIScope::getRef() const;
friend class DIType;
- /// Val can be either a MDNode or a MDString, in the latter,
- /// MDString specifies the type identifier.
- const Value *Val;
- explicit DIRef(const Value *V);
+ /// \brief Val can be either a MDNode or a MDString.
+ ///
+ /// In the latter, MDString specifies the type identifier.
+ const Metadata *Val;
+ explicit DIRef(const Metadata *V);
public:
T resolve(const DITypeIdentifierMap &Map) const;
StringRef getName() const;
- operator Value *() const { return const_cast<Value *>(Val); }
+ operator Metadata *() const { return const_cast<Metadata *>(Val); }
};
template <typename T>
return MS->getString();
}
-/// Specialize getFieldAs to handle fields that are references to DIScopes.
+/// \brief Handle fields that are references to DIScopes.
template <> DIScopeRef DIDescriptor::getFieldAs<DIScopeRef>(unsigned Elt) const;
-/// Specialize DIRef constructor for DIScopeRef.
-template <> DIRef<DIScope>::DIRef(const Value *V);
+/// \brief Specialize DIRef constructor for DIScopeRef.
+template <> DIRef<DIScope>::DIRef(const Metadata *V);
-/// Specialize getFieldAs to handle fields that are references to DITypes.
+/// \brief Handle fields that are references to DITypes.
template <> DITypeRef DIDescriptor::getFieldAs<DITypeRef>(unsigned Elt) const;
-/// Specialize DIRef constructor for DITypeRef.
-template <> DIRef<DIType>::DIRef(const Value *V);
+/// \brief Specialize DIRef constructor for DITypeRef.
+template <> DIRef<DIType>::DIRef(const Metadata *V);
-/// DIType - This is a wrapper for a type.
+/// \brief This is a wrapper for a type.
+///
/// FIXME: Types should be factored much better so that CV qualifiers and
/// others do not require a huge and empty descriptor full of zeros.
class DIType : public DIScope {
return DITypeRef(&*getRef());
}
- /// Verify - Verify that a type descriptor is well formed.
bool Verify() const;
DIScopeRef getContext() const { return getFieldAs<DIScopeRef>(2); }
- StringRef getName() const { return getStringField(3); }
- unsigned getLineNumber() const { return getUnsignedField(4); }
- uint64_t getSizeInBits() const { return getUInt64Field(5); }
- uint64_t getAlignInBits() const { return getUInt64Field(6); }
+ StringRef getName() const { return getHeaderField(1); }
+ unsigned getLineNumber() const {
+ return getHeaderFieldAs<unsigned>(2);
+ }
+ uint64_t getSizeInBits() const {
+ return getHeaderFieldAs<unsigned>(3);
+ }
+ uint64_t getAlignInBits() const {
+ return getHeaderFieldAs<unsigned>(4);
+ }
// FIXME: Offset is only used for DW_TAG_member nodes. Making every type
// carry this is just plain insane.
- uint64_t getOffsetInBits() const { return getUInt64Field(7); }
- unsigned getFlags() const { return getUnsignedField(8); }
- bool isPrivate() const { return (getFlags() & FlagPrivate) != 0; }
- bool isProtected() const { return (getFlags() & FlagProtected) != 0; }
+ uint64_t getOffsetInBits() const {
+ return getHeaderFieldAs<unsigned>(5);
+ }
+ unsigned getFlags() const { return getHeaderFieldAs<unsigned>(6); }
+ bool isPrivate() const {
+ return (getFlags() & FlagAccessibility) == FlagPrivate;
+ }
+ bool isProtected() const {
+ return (getFlags() & FlagAccessibility) == FlagProtected;
+ }
+ bool isPublic() const {
+ return (getFlags() & FlagAccessibility) == FlagPublic;
+ }
bool isForwardDecl() const { return (getFlags() & FlagFwdDecl) != 0; }
- // isAppleBlock - Return true if this is the Apple Blocks extension.
bool isAppleBlockExtension() const {
return (getFlags() & FlagAppleBlock) != 0;
}
return (getFlags() & FlagRValueReference) != 0;
}
bool isValid() const { return DbgNode && isType(); }
-
- /// replaceAllUsesWith - Replace all uses of debug info referenced by
- /// this descriptor.
- void replaceAllUsesWith(LLVMContext &VMContext, DIDescriptor D);
- void replaceAllUsesWith(MDNode *D);
};
-/// DIBasicType - A basic type, like 'int' or 'float'.
+/// \brief A basic type, like 'int' or 'float'.
class DIBasicType : public DIType {
public:
explicit DIBasicType(const MDNode *N = nullptr) : DIType(N) {}
- unsigned getEncoding() const { return getUnsignedField(9); }
+ unsigned getEncoding() const { return getHeaderFieldAs<unsigned>(7); }
- /// Verify - Verify that a basic type descriptor is well formed.
bool Verify() const;
};
-/// DIDerivedType - A simple derived type, like a const qualified type,
-/// a typedef, a pointer or reference, et cetera. Or, a data member of
-/// a class/struct/union.
+/// \brief A simple derived type
+///
+/// Like a const qualified type, a typedef, a pointer or reference, et cetera.
+/// Or, a data member of a class/struct/union.
class DIDerivedType : public DIType {
friend class DIDescriptor;
void printInternal(raw_ostream &OS) const;
public:
explicit DIDerivedType(const MDNode *N = nullptr) : DIType(N) {}
- DITypeRef getTypeDerivedFrom() const { return getFieldAs<DITypeRef>(9); }
+ DITypeRef getTypeDerivedFrom() const { return getFieldAs<DITypeRef>(3); }
- /// getObjCProperty - Return property node, if this ivar is
- /// associated with one.
+ /// \brief Return property node, if this ivar is associated with one.
MDNode *getObjCProperty() const;
DITypeRef getClassType() const {
assert(getTag() == dwarf::DW_TAG_ptr_to_member_type);
- return getFieldAs<DITypeRef>(10);
+ return getFieldAs<DITypeRef>(4);
}
Constant *getConstant() const {
assert((getTag() == dwarf::DW_TAG_member) && isStaticMember());
- return getConstantField(10);
+ return getConstantField(4);
}
- /// Verify - Verify that a derived type descriptor is well formed.
bool Verify() const;
};
-/// DICompositeType - This descriptor holds a type that can refer to multiple
-/// other types, like a function or struct.
+/// \brief Types that refer to multiple other types.
+///
+/// This descriptor holds a type that can refer to multiple other types, like a
+/// function or struct.
+///
/// DICompositeType is derived from DIDerivedType because some
/// composite types (such as enums) can be derived from basic types
// FIXME: Make this derive from DIType directly & just store the
// base type in a single DIType field.
class DICompositeType : public DIDerivedType {
+ friend class DIBuilder;
friend class DIDescriptor;
void printInternal(raw_ostream &OS) const;
+ /// \brief Set the array of member DITypes.
+ void setArraysHelper(MDNode *Elements, MDNode *TParams);
+
public:
explicit DICompositeType(const MDNode *N = nullptr) : DIDerivedType(N) {}
- DIArray getTypeArray() const { return getFieldAs<DIArray>(10); }
- void setTypeArray(DIArray Elements, DIArray TParams = DIArray());
- unsigned getRunTimeLang() const { return getUnsignedField(11); }
- DITypeRef getContainingType() const { return getFieldAs<DITypeRef>(12); }
+ DIArray getElements() const {
+ assert(!isSubroutineType() && "no elements for DISubroutineType");
+ return getFieldAs<DIArray>(4);
+ }
+
+private:
+ template <typename T>
+ void setArrays(DITypedArray<T> Elements, DIArray TParams = DIArray()) {
+ assert((!TParams || DbgNode->getNumOperands() == 8) &&
+ "If you're setting the template parameters this should include a slot "
+ "for that!");
+ setArraysHelper(Elements, TParams);
+ }
+
+public:
+ unsigned getRunTimeLang() const {
+ return getHeaderFieldAs<unsigned>(7);
+ }
+ DITypeRef getContainingType() const { return getFieldAs<DITypeRef>(5); }
+
+private:
+ /// \brief Set the containing type.
void setContainingType(DICompositeType ContainingType);
- DIArray getTemplateParams() const { return getFieldAs<DIArray>(13); }
+
+public:
+ DIArray getTemplateParams() const { return getFieldAs<DIArray>(6); }
MDString *getIdentifier() const;
- /// Verify - Verify that a composite type descriptor is well formed.
bool Verify() const;
};
-/// DIFile - This is a wrapper for a file.
+class DISubroutineType : public DICompositeType {
+public:
+ explicit DISubroutineType(const MDNode *N = nullptr) : DICompositeType(N) {}
+ DITypedArray<DITypeRef> getTypeArray() const {
+ return getFieldAs<DITypedArray<DITypeRef>>(4);
+ }
+};
+
+/// \brief This is a wrapper for a file.
class DIFile : public DIScope {
friend class DIDescriptor;
public:
explicit DIFile(const MDNode *N = nullptr) : DIScope(N) {}
+
+ /// \brief Retrieve the MDNode for the directory/file pair.
MDNode *getFileNode() const;
bool Verify() const;
};
-/// DICompileUnit - A wrapper for a compile unit.
+/// \brief A wrapper for a compile unit.
class DICompileUnit : public DIScope {
friend class DIDescriptor;
void printInternal(raw_ostream &OS) const;
public:
explicit DICompileUnit(const MDNode *N = nullptr) : DIScope(N) {}
- unsigned getLanguage() const { return getUnsignedField(2); }
- StringRef getProducer() const { return getStringField(3); }
+ dwarf::SourceLanguage getLanguage() const {
+ return static_cast<dwarf::SourceLanguage>(getHeaderFieldAs<unsigned>(1));
+ }
+ StringRef getProducer() const { return getHeaderField(2); }
- bool isOptimized() const { return getUnsignedField(4) != 0; }
- StringRef getFlags() const { return getStringField(5); }
- unsigned getRunTimeVersion() const { return getUnsignedField(6); }
+ bool isOptimized() const { return getHeaderFieldAs<bool>(3) != 0; }
+ StringRef getFlags() const { return getHeaderField(4); }
+ unsigned getRunTimeVersion() const { return getHeaderFieldAs<unsigned>(5); }
DIArray getEnumTypes() const;
DIArray getRetainedTypes() const;
DIArray getGlobalVariables() const;
DIArray getImportedEntities() const;
- StringRef getSplitDebugFilename() const { return getStringField(12); }
- unsigned getEmissionKind() const { return getUnsignedField(13); }
+ void replaceSubprograms(DIArray Subprograms);
+ void replaceGlobalVariables(DIArray GlobalVariables);
+
+ StringRef getSplitDebugFilename() const { return getHeaderField(6); }
+ unsigned getEmissionKind() const { return getHeaderFieldAs<unsigned>(7); }
- /// Verify - Verify that a compile unit is well formed.
bool Verify() const;
};
-/// DISubprogram - This is a wrapper for a subprogram (e.g. a function).
+/// \brief This is a wrapper for a subprogram (e.g. a function).
class DISubprogram : public DIScope {
friend class DIDescriptor;
void printInternal(raw_ostream &OS) const;
public:
explicit DISubprogram(const MDNode *N = nullptr) : DIScope(N) {}
- DIScopeRef getContext() const { return getFieldAs<DIScopeRef>(2); }
- StringRef getName() const { return getStringField(3); }
- StringRef getDisplayName() const { return getStringField(4); }
- StringRef getLinkageName() const { return getStringField(5); }
- unsigned getLineNumber() const { return getUnsignedField(6); }
- DICompositeType getType() const { return getFieldAs<DICompositeType>(7); }
-
- /// isLocalToUnit - Return true if this subprogram is local to the current
- /// compile unit, like 'static' in C.
- unsigned isLocalToUnit() const { return getUnsignedField(8); }
- unsigned isDefinition() const { return getUnsignedField(9); }
+ StringRef getName() const { return getHeaderField(1); }
+ StringRef getDisplayName() const { return getHeaderField(2); }
+ StringRef getLinkageName() const { return getHeaderField(3); }
+ unsigned getLineNumber() const { return getHeaderFieldAs<unsigned>(4); }
- unsigned getVirtuality() const { return getUnsignedField(10); }
- unsigned getVirtualIndex() const { return getUnsignedField(11); }
+ /// \brief Check if this is local (like 'static' in C).
+ unsigned isLocalToUnit() const { return getHeaderFieldAs<unsigned>(5); }
+ unsigned isDefinition() const { return getHeaderFieldAs<unsigned>(6); }
- DITypeRef getContainingType() const { return getFieldAs<DITypeRef>(12); }
+ unsigned getVirtuality() const { return getHeaderFieldAs<unsigned>(7); }
+ unsigned getVirtualIndex() const { return getHeaderFieldAs<unsigned>(8); }
- unsigned getFlags() const { return getUnsignedField(13); }
+ unsigned getFlags() const { return getHeaderFieldAs<unsigned>(9); }
- unsigned isArtificial() const {
- return (getUnsignedField(13) & FlagArtificial) != 0;
- }
- /// isPrivate - Return true if this subprogram has "private"
- /// access specifier.
- bool isPrivate() const { return (getUnsignedField(13) & FlagPrivate) != 0; }
- /// isProtected - Return true if this subprogram has "protected"
- /// access specifier.
- bool isProtected() const {
- return (getUnsignedField(13) & FlagProtected) != 0;
- }
- /// isExplicit - Return true if this subprogram is marked as explicit.
- bool isExplicit() const { return (getUnsignedField(13) & FlagExplicit) != 0; }
- /// isPrototyped - Return true if this subprogram is prototyped.
- bool isPrototyped() const {
- return (getUnsignedField(13) & FlagPrototyped) != 0;
- }
+ unsigned isOptimized() const { return getHeaderFieldAs<bool>(10); }
- /// Return true if this subprogram is a C++11 reference-qualified
- /// non-static member function (void foo() &).
- unsigned isLValueReference() const {
- return (getUnsignedField(13) & FlagLValueReference) != 0;
- }
+ /// \brief Get the beginning of the scope of the function (not the name).
+ unsigned getScopeLineNumber() const { return getHeaderFieldAs<unsigned>(11); }
- /// Return true if this subprogram is a C++11
- /// rvalue-reference-qualified non-static member function
- /// (void foo() &&).
- unsigned isRValueReference() const {
- return (getUnsignedField(13) & FlagRValueReference) != 0;
- }
+ DIScopeRef getContext() const { return getFieldAs<DIScopeRef>(2); }
+ DISubroutineType getType() const { return getFieldAs<DISubroutineType>(3); }
- unsigned isOptimized() const;
+ DITypeRef getContainingType() const { return getFieldAs<DITypeRef>(4); }
- /// Verify - Verify that a subprogram descriptor is well formed.
bool Verify() const;
- /// describes - Return true if this subprogram provides debugging
- /// information for the function F.
+ /// \brief Check if this provides debugging information for the function F.
bool describes(const Function *F);
- Function *getFunction() const { return getFunctionField(15); }
- void replaceFunction(Function *F) { replaceFunctionField(15, F); }
- DIArray getTemplateParams() const { return getFieldAs<DIArray>(16); }
+ Function *getFunction() const { return getFunctionField(5); }
+ void replaceFunction(Function *F) { replaceFunctionField(5, F); }
+ DIArray getTemplateParams() const { return getFieldAs<DIArray>(6); }
DISubprogram getFunctionDeclaration() const {
- return getFieldAs<DISubprogram>(17);
+ return getFieldAs<DISubprogram>(7);
}
MDNode *getVariablesNodes() const;
DIArray getVariables() const;
- /// getScopeLineNumber - Get the beginning of the scope of the
- /// function, not necessarily where the name of the program
- /// starts.
- unsigned getScopeLineNumber() const { return getUnsignedField(19); }
+ unsigned isArtificial() const { return (getFlags() & FlagArtificial) != 0; }
+ /// \brief Check for the "private" access specifier.
+ bool isPrivate() const {
+ return (getFlags() & FlagAccessibility) == FlagPrivate;
+ }
+ /// \brief Check for the "protected" access specifier.
+ bool isProtected() const {
+ return (getFlags() & FlagAccessibility) == FlagProtected;
+ }
+ /// \brief Check for the "public" access specifier.
+ bool isPublic() const {
+ return (getFlags() & FlagAccessibility) == FlagPublic;
+ }
+ /// \brief Check for "explicit".
+ bool isExplicit() const { return (getFlags() & FlagExplicit) != 0; }
+ /// \brief Check if this is prototyped.
+ bool isPrototyped() const { return (getFlags() & FlagPrototyped) != 0; }
+
+ /// \brief Check if this is reference-qualified.
+ ///
+ /// Return true if this subprogram is a C++11 reference-qualified non-static
+ /// member function (void foo() &).
+ unsigned isLValueReference() const {
+ return (getFlags() & FlagLValueReference) != 0;
+ }
+
+ /// \brief Check if this is rvalue-reference-qualified.
+ ///
+ /// Return true if this subprogram is a C++11 rvalue-reference-qualified
+ /// non-static member function (void foo() &&).
+ unsigned isRValueReference() const {
+ return (getFlags() & FlagRValueReference) != 0;
+ }
+
};
-/// DILexicalBlock - This is a wrapper for a lexical block.
+/// \brief This is a wrapper for a lexical block.
class DILexicalBlock : public DIScope {
public:
explicit DILexicalBlock(const MDNode *N = nullptr) : DIScope(N) {}
DIScope getContext() const { return getFieldAs<DIScope>(2); }
- unsigned getLineNumber() const { return getUnsignedField(3); }
- unsigned getColumnNumber() const { return getUnsignedField(4); }
- unsigned getDiscriminator() const { return getUnsignedField(5); }
+ unsigned getLineNumber() const {
+ return getHeaderFieldAs<unsigned>(1);
+ }
+ unsigned getColumnNumber() const {
+ return getHeaderFieldAs<unsigned>(2);
+ }
bool Verify() const;
};
-/// DILexicalBlockFile - This is a wrapper for a lexical block with
-/// a filename change.
+/// \brief This is a wrapper for a lexical block with a filename change.
class DILexicalBlockFile : public DIScope {
public:
explicit DILexicalBlockFile(const MDNode *N = nullptr) : DIScope(N) {}
unsigned getLineNumber() const { return getScope().getLineNumber(); }
unsigned getColumnNumber() const { return getScope().getColumnNumber(); }
DILexicalBlock getScope() const { return getFieldAs<DILexicalBlock>(2); }
+ unsigned getDiscriminator() const { return getHeaderFieldAs<unsigned>(1); }
bool Verify() const;
};
-/// DINameSpace - A wrapper for a C++ style name space.
+/// \brief A wrapper for a C++ style name space.
class DINameSpace : public DIScope {
friend class DIDescriptor;
void printInternal(raw_ostream &OS) const;
public:
explicit DINameSpace(const MDNode *N = nullptr) : DIScope(N) {}
+ StringRef getName() const { return getHeaderField(1); }
+ unsigned getLineNumber() const { return getHeaderFieldAs<unsigned>(2); }
DIScope getContext() const { return getFieldAs<DIScope>(2); }
- StringRef getName() const { return getStringField(3); }
- unsigned getLineNumber() const { return getUnsignedField(4); }
- bool Verify() const;
-};
-
-/// DIUnspecifiedParameter - This is a wrapper for unspecified parameters.
-class DIUnspecifiedParameter : public DIDescriptor {
-public:
- explicit DIUnspecifiedParameter(const MDNode *N = nullptr)
- : DIDescriptor(N) {}
bool Verify() const;
};
-/// DITemplateTypeParameter - This is a wrapper for template type parameter.
+/// \brief This is a wrapper for template type parameter.
class DITemplateTypeParameter : public DIDescriptor {
public:
explicit DITemplateTypeParameter(const MDNode *N = nullptr)
: DIDescriptor(N) {}
+ StringRef getName() const { return getHeaderField(1); }
+ unsigned getLineNumber() const { return getHeaderFieldAs<unsigned>(2); }
+ unsigned getColumnNumber() const { return getHeaderFieldAs<unsigned>(3); }
+
DIScopeRef getContext() const { return getFieldAs<DIScopeRef>(1); }
- StringRef getName() const { return getStringField(2); }
- DITypeRef getType() const { return getFieldAs<DITypeRef>(3); }
- StringRef getFilename() const { return getFieldAs<DIFile>(4).getFilename(); }
+ DITypeRef getType() const { return getFieldAs<DITypeRef>(2); }
+ StringRef getFilename() const { return getFieldAs<DIFile>(3).getFilename(); }
StringRef getDirectory() const {
- return getFieldAs<DIFile>(4).getDirectory();
+ return getFieldAs<DIFile>(3).getDirectory();
}
- unsigned getLineNumber() const { return getUnsignedField(5); }
- unsigned getColumnNumber() const { return getUnsignedField(6); }
bool Verify() const;
};
-/// DITemplateValueParameter - This is a wrapper for template value parameter.
+/// \brief This is a wrapper for template value parameter.
class DITemplateValueParameter : public DIDescriptor {
public:
explicit DITemplateValueParameter(const MDNode *N = nullptr)
: DIDescriptor(N) {}
+ StringRef getName() const { return getHeaderField(1); }
+ unsigned getLineNumber() const { return getHeaderFieldAs<unsigned>(2); }
+ unsigned getColumnNumber() const { return getHeaderFieldAs<unsigned>(3); }
+
DIScopeRef getContext() const { return getFieldAs<DIScopeRef>(1); }
- StringRef getName() const { return getStringField(2); }
- DITypeRef getType() const { return getFieldAs<DITypeRef>(3); }
- Value *getValue() const;
- StringRef getFilename() const { return getFieldAs<DIFile>(5).getFilename(); }
+ DITypeRef getType() const { return getFieldAs<DITypeRef>(2); }
+ Metadata *getValue() const;
+ StringRef getFilename() const { return getFieldAs<DIFile>(4).getFilename(); }
StringRef getDirectory() const {
- return getFieldAs<DIFile>(5).getDirectory();
+ return getFieldAs<DIFile>(4).getDirectory();
}
- unsigned getLineNumber() const { return getUnsignedField(6); }
- unsigned getColumnNumber() const { return getUnsignedField(7); }
bool Verify() const;
};
-/// DIGlobalVariable - This is a wrapper for a global variable.
+/// \brief This is a wrapper for a global variable.
class DIGlobalVariable : public DIDescriptor {
friend class DIDescriptor;
void printInternal(raw_ostream &OS) const;
public:
explicit DIGlobalVariable(const MDNode *N = nullptr) : DIDescriptor(N) {}
- DIScope getContext() const { return getFieldAs<DIScope>(2); }
- StringRef getName() const { return getStringField(3); }
- StringRef getDisplayName() const { return getStringField(4); }
- StringRef getLinkageName() const { return getStringField(5); }
- StringRef getFilename() const { return getFieldAs<DIFile>(6).getFilename(); }
+ StringRef getName() const { return getHeaderField(1); }
+ StringRef getDisplayName() const { return getHeaderField(2); }
+ StringRef getLinkageName() const { return getHeaderField(3); }
+ unsigned getLineNumber() const { return getHeaderFieldAs<unsigned>(4); }
+ unsigned isLocalToUnit() const { return getHeaderFieldAs<bool>(5); }
+ unsigned isDefinition() const { return getHeaderFieldAs<bool>(6); }
+
+ DIScope getContext() const { return getFieldAs<DIScope>(1); }
+ StringRef getFilename() const { return getFieldAs<DIFile>(2).getFilename(); }
StringRef getDirectory() const {
- return getFieldAs<DIFile>(6).getDirectory();
+ return getFieldAs<DIFile>(2).getDirectory();
}
+ DITypeRef getType() const { return getFieldAs<DITypeRef>(3); }
- unsigned getLineNumber() const { return getUnsignedField(7); }
- DITypeRef getType() const { return getFieldAs<DITypeRef>(8); }
- unsigned isLocalToUnit() const { return getUnsignedField(9); }
- unsigned isDefinition() const { return getUnsignedField(10); }
-
- GlobalVariable *getGlobal() const { return getGlobalVariableField(11); }
- Constant *getConstant() const { return getConstantField(11); }
+ GlobalVariable *getGlobal() const { return getGlobalVariableField(4); }
+ Constant *getConstant() const { return getConstantField(4); }
DIDerivedType getStaticDataMemberDeclaration() const {
- return getFieldAs<DIDerivedType>(12);
+ return getFieldAs<DIDerivedType>(5);
}
- /// Verify - Verify that a global variable descriptor is well formed.
bool Verify() const;
};
-/// DIVariable - This is a wrapper for a variable (e.g. parameter, local,
-/// global etc).
+/// \brief This is a wrapper for a variable (e.g. parameter, local, global etc).
class DIVariable : public DIDescriptor {
friend class DIDescriptor;
void printInternal(raw_ostream &OS) const;
public:
explicit DIVariable(const MDNode *N = nullptr) : DIDescriptor(N) {}
- DIScope getContext() const { return getFieldAs<DIScope>(1); }
- StringRef getName() const { return getStringField(2); }
- DIFile getFile() const { return getFieldAs<DIFile>(3); }
- unsigned getLineNumber() const { return (getUnsignedField(4) << 8) >> 8; }
- unsigned getArgNumber() const {
- unsigned L = getUnsignedField(4);
- return L >> 24;
+ StringRef getName() const { return getHeaderField(1); }
+ unsigned getLineNumber() const {
+ // FIXME: Line number and arg number shouldn't be merged together like this.
+ return (getHeaderFieldAs<unsigned>(2) << 8) >> 8;
}
- DITypeRef getType() const { return getFieldAs<DITypeRef>(5); }
+ unsigned getArgNumber() const { return getHeaderFieldAs<unsigned>(2) >> 24; }
+
+ DIScope getContext() const { return getFieldAs<DIScope>(1); }
+ DIFile getFile() const { return getFieldAs<DIFile>(2); }
+ DITypeRef getType() const { return getFieldAs<DITypeRef>(3); }
- /// isArtificial - Return true if this variable is marked as "artificial".
+ /// \brief Return true if this variable is marked as "artificial".
bool isArtificial() const {
- return (getUnsignedField(6) & FlagArtificial) != 0;
+ return (getHeaderFieldAs<unsigned>(3) & FlagArtificial) != 0;
}
bool isObjectPointer() const {
- return (getUnsignedField(6) & FlagObjectPointer) != 0;
- }
-
- /// \brief Return true if this variable is represented as a pointer.
- bool isIndirect() const {
- return (getUnsignedField(6) & FlagIndirectVariable) != 0;
+ return (getHeaderFieldAs<unsigned>(3) & FlagObjectPointer) != 0;
}
- /// getInlinedAt - If this variable is inlined then return inline location.
+ /// \brief If this variable is inlined then return inline location.
MDNode *getInlinedAt() const;
- /// Verify - Verify that a variable descriptor is well formed.
bool Verify() const;
- /// HasComplexAddr - Return true if the variable has a complex address.
- bool hasComplexAddress() const { return getNumAddrElements() > 0; }
-
- unsigned getNumAddrElements() const;
-
- uint64_t getAddrElement(unsigned Idx) const {
- return getUInt64Field(Idx + 8);
- }
-
- /// isBlockByrefVariable - Return true if the variable was declared as
- /// a "__block" variable (Apple Blocks).
+ /// \brief Check if this is a "__block" variable (Apple Blocks).
bool isBlockByrefVariable(const DITypeIdentifierMap &Map) const {
return (getType().resolve(Map)).isBlockByrefStruct();
}
- /// isInlinedFnArgument - Return true if this variable provides debugging
- /// information for an inlined function arguments.
+ /// \brief Check if this is an inlined function argument.
bool isInlinedFnArgument(const Function *CurFn);
+ /// \brief Return the size reported by the variable's type.
+ unsigned getSizeInBits(const DITypeIdentifierMap &Map);
+
void printExtendedName(raw_ostream &OS) const;
};
-/// DILocation - This object holds location information. This object
-/// is not associated with any DWARF tag.
+/// \brief A complex location expression.
+class DIExpression : public DIDescriptor {
+ friend class DIDescriptor;
+ void printInternal(raw_ostream &OS) const;
+
+public:
+ explicit DIExpression(const MDNode *N = nullptr) : DIDescriptor(N) {}
+
+ bool Verify() const;
+
+ /// \brief Return the number of elements in the complex expression.
+ unsigned getNumElements() const {
+ if (!DbgNode)
+ return 0;
+ unsigned N = getNumHeaderFields();
+ assert(N > 0 && "missing tag");
+ return N - 1;
+ }
+
+ /// \brief return the Idx'th complex address element.
+ uint64_t getElement(unsigned Idx) const;
+
+ /// \brief Return whether this is a piece of an aggregate variable.
+ bool isVariablePiece() const;
+ /// \brief Return the offset of this piece in bytes.
+ uint64_t getPieceOffset() const;
+ /// \brief Return the size of this piece in bytes.
+ uint64_t getPieceSize() const;
+
+ /// \brief An iterator for DIExpression elements.
+ class iterator
+ : public std::iterator<std::forward_iterator_tag, StringRef, unsigned,
+ const uint64_t *, uint64_t> {
+ DIHeaderFieldIterator I;
+ iterator(DIHeaderFieldIterator I) : I(I) {}
+ public:
+ iterator() {}
+ iterator(const DIExpression &Expr) : I(++Expr.header_begin()) {}
+ uint64_t operator*() const { return I.getNumber<uint64_t>(); }
+ iterator &operator++() {
+ increment();
+ return *this;
+ }
+ iterator operator++(int) {
+ iterator X(*this);
+ increment();
+ return X;
+ }
+ bool operator==(const iterator &X) const {
+ return I == X.I;
+ }
+ bool operator!=(const iterator &X) const {
+ return !(*this == X);
+ }
+
+ uint64_t getArg(unsigned N) const {
+ auto In = I;
+ std::advance(In, N);
+ return In.getNumber<uint64_t>();
+ }
+
+ const DIHeaderFieldIterator& getBase() const { return I; }
+
+ private:
+ void increment() {
+ switch (**this) {
+ case dwarf::DW_OP_piece: std::advance(I, 3); break;
+ case dwarf::DW_OP_plus: std::advance(I, 2); break;
+ case dwarf::DW_OP_deref: std::advance(I, 1); break;
+ default:
+ assert("unsupported operand");
+ }
+ }
+ };
+
+ iterator begin() const;
+ iterator end() const;
+};
+
+/// \brief This object holds location information.
+///
+/// This object is not associated with any DWARF tag.
class DILocation : public DIDescriptor {
public:
explicit DILocation(const MDNode *N) : DIDescriptor(N) {}
- unsigned getLineNumber() const { return getUnsignedField(0); }
- unsigned getColumnNumber() const { return getUnsignedField(1); }
- DIScope getScope() const { return getFieldAs<DIScope>(2); }
- DILocation getOrigLocation() const { return getFieldAs<DILocation>(3); }
+ unsigned getLineNumber() const {
+ if (auto *L = dyn_cast_or_null<MDLocation>(DbgNode))
+ return L->getLine();
+ return 0;
+ }
+ unsigned getColumnNumber() const {
+ if (auto *L = dyn_cast_or_null<MDLocation>(DbgNode))
+ return L->getColumn();
+ return 0;
+ }
+ DIScope getScope() const {
+ if (auto *L = dyn_cast_or_null<MDLocation>(DbgNode))
+ return DIScope(dyn_cast_or_null<MDNode>(L->getScope()));
+ return DIScope(nullptr);
+ }
+ DILocation getOrigLocation() const {
+ if (auto *L = dyn_cast_or_null<MDLocation>(DbgNode))
+ return DILocation(dyn_cast_or_null<MDNode>(L->getInlinedAt()));
+ return DILocation(nullptr);
+ }
StringRef getFilename() const { return getScope().getFilename(); }
StringRef getDirectory() const { return getScope().getDirectory(); }
bool Verify() const;
return (getLineNumber() == Other.getLineNumber() &&
getFilename() == Other.getFilename());
}
- /// getDiscriminator - DWARF discriminators are used to distinguish
- /// identical file locations for instructions that are on different
- /// basic blocks. If two instructions are inside the same lexical block
- /// and are in different basic blocks, we create a new lexical block
- /// with identical location as the original but with a different
- /// discriminator value (lib/Transforms/Util/AddDiscriminators.cpp
- /// for details).
+ /// \brief Get the DWAF discriminator.
+ ///
+ /// DWARF discriminators are used to distinguish identical file locations for
+ /// instructions that are on different basic blocks. If two instructions are
+ /// inside the same lexical block and are in different basic blocks, we
+ /// create a new lexical block with identical location as the original but
+ /// with a different discriminator value
+ /// (lib/Transforms/Util/AddDiscriminators.cpp for details).
unsigned getDiscriminator() const {
// Since discriminators are associated with lexical blocks, make
// sure this location is a lexical block before retrieving its
// value.
- return getScope().isLexicalBlock()
- ? getFieldAs<DILexicalBlock>(2).getDiscriminator()
+ return getScope().isLexicalBlockFile()
+ ? DILexicalBlockFile(
+ cast<MDNode>(cast<MDLocation>(DbgNode)->getScope()))
+ .getDiscriminator()
: 0;
}
+
+ /// \brief Generate a new discriminator value for this location.
unsigned computeNewDiscriminator(LLVMContext &Ctx);
- DILocation copyWithNewScope(LLVMContext &Ctx, DILexicalBlock NewScope);
+
+ /// \brief Return a copy of this location with a different scope.
+ DILocation copyWithNewScope(LLVMContext &Ctx, DILexicalBlockFile NewScope);
};
class DIObjCProperty : public DIDescriptor {
public:
explicit DIObjCProperty(const MDNode *N) : DIDescriptor(N) {}
- StringRef getObjCPropertyName() const { return getStringField(1); }
- DIFile getFile() const { return getFieldAs<DIFile>(2); }
- unsigned getLineNumber() const { return getUnsignedField(3); }
+ StringRef getObjCPropertyName() const { return getHeaderField(1); }
+ DIFile getFile() const { return getFieldAs<DIFile>(1); }
+ unsigned getLineNumber() const { return getHeaderFieldAs<unsigned>(2); }
- StringRef getObjCPropertyGetterName() const { return getStringField(4); }
- StringRef getObjCPropertySetterName() const { return getStringField(5); }
+ StringRef getObjCPropertyGetterName() const { return getHeaderField(3); }
+ StringRef getObjCPropertySetterName() const { return getHeaderField(4); }
+ unsigned getAttributes() const { return getHeaderFieldAs<unsigned>(5); }
bool isReadOnlyObjCProperty() const {
- return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_readonly) != 0;
+ return (getAttributes() & dwarf::DW_APPLE_PROPERTY_readonly) != 0;
}
bool isReadWriteObjCProperty() const {
- return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_readwrite) != 0;
+ return (getAttributes() & dwarf::DW_APPLE_PROPERTY_readwrite) != 0;
}
bool isAssignObjCProperty() const {
- return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_assign) != 0;
+ return (getAttributes() & dwarf::DW_APPLE_PROPERTY_assign) != 0;
}
bool isRetainObjCProperty() const {
- return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_retain) != 0;
+ return (getAttributes() & dwarf::DW_APPLE_PROPERTY_retain) != 0;
}
bool isCopyObjCProperty() const {
- return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_copy) != 0;
+ return (getAttributes() & dwarf::DW_APPLE_PROPERTY_copy) != 0;
}
bool isNonAtomicObjCProperty() const {
- return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_nonatomic) != 0;
+ return (getAttributes() & dwarf::DW_APPLE_PROPERTY_nonatomic) != 0;
}
- /// Objective-C doesn't have an ODR, so there is no benefit in storing
+ /// \brief Get the type.
+ ///
+ /// \note Objective-C doesn't have an ODR, so there is no benefit in storing
/// the type as a DITypeRef here.
- DIType getType() const { return getFieldAs<DIType>(7); }
+ DIType getType() const { return getFieldAs<DIType>(2); }
- /// Verify - Verify that a derived type descriptor is well formed.
bool Verify() const;
};
explicit DIImportedEntity(const MDNode *N) : DIDescriptor(N) {}
DIScope getContext() const { return getFieldAs<DIScope>(1); }
DIScopeRef getEntity() const { return getFieldAs<DIScopeRef>(2); }
- unsigned getLineNumber() const { return getUnsignedField(3); }
- StringRef getName() const { return getStringField(4); }
+ unsigned getLineNumber() const { return getHeaderFieldAs<unsigned>(1); }
+ StringRef getName() const { return getHeaderField(2); }
bool Verify() const;
};
-/// getDISubprogram - Find subprogram that is enclosing this scope.
+/// \brief Find subprogram that is enclosing this scope.
DISubprogram getDISubprogram(const MDNode *Scope);
-/// getDICompositeType - Find underlying composite type.
-DICompositeType getDICompositeType(DIType T);
-
-/// getOrInsertFnSpecificMDNode - Return a NameMDNode that is suitable
-/// to hold function specific information.
-NamedMDNode *getOrInsertFnSpecificMDNode(Module &M, DISubprogram SP);
+/// \brief Find debug info for a given function.
+/// \returns a valid DISubprogram, if found. Otherwise, it returns an empty
+/// DISubprogram.
+DISubprogram getDISubprogram(const Function *F);
-/// getFnSpecificMDNode - Return a NameMDNode, if available, that is
-/// suitable to hold function specific information.
-NamedMDNode *getFnSpecificMDNode(const Module &M, DISubprogram SP);
+/// \brief Find underlying composite type.
+DICompositeType getDICompositeType(DIType T);
-/// createInlinedVariable - Create a new inlined variable based on current
-/// variable.
+/// \brief Create a new inlined variable based on current variable.
+///
/// @param DV Current Variable.
/// @param InlinedScope Location at current variable is inlined.
DIVariable createInlinedVariable(MDNode *DV, MDNode *InlinedScope,
LLVMContext &VMContext);
-/// cleanseInlinedVariable - Remove inlined scope from the variable.
+/// \brief Remove inlined scope from the variable.
DIVariable cleanseInlinedVariable(MDNode *DV, LLVMContext &VMContext);
-/// Construct DITypeIdentifierMap by going through retained types of each CU.
+/// \brief Generate map by visiting all retained types.
DITypeIdentifierMap generateDITypeIdentifierMap(const NamedMDNode *CU_Nodes);
-/// Strip debug info in the module if it exists.
+/// \brief Strip debug info in the module if it exists.
+///
/// To do this, we remove all calls to the debugger intrinsics and any named
/// metadata for debugging. We also remove debug locations for instructions.
/// Return true if module is modified.
bool StripDebugInfo(Module &M);
-/// Return Debug Info Metadata Version by checking module flags.
+/// \brief Return Debug Info Metadata Version by checking module flags.
unsigned getDebugMetadataVersionFromModule(const Module &M);
+/// \brief Utility to find all debug info in a module.
+///
/// DebugInfoFinder tries to list all debug info MDNodes used in a module. To
/// list debug info MDNodes used by an instruction, DebugInfoFinder uses
/// processDeclare, processValue and processLocation to handle DbgDeclareInst,
public:
DebugInfoFinder() : TypeMapInitialized(false) {}
- /// processModule - Process entire module and collect debug info
- /// anchors.
+ /// \brief Process entire module and collect debug info anchors.
void processModule(const Module &M);
- /// processDeclare - Process DbgDeclareInst.
+ /// \brief Process DbgDeclareInst.
void processDeclare(const Module &M, const DbgDeclareInst *DDI);
- /// Process DbgValueInst.
+ /// \brief Process DbgValueInst.
void processValue(const Module &M, const DbgValueInst *DVI);
- /// processLocation - Process DILocation.
+ /// \brief Process DILocation.
void processLocation(const Module &M, DILocation Loc);
- /// Clear all lists.
+ /// \brief Process DIExpression.
+ void processExpression(DIExpression Expr);
+
+ /// \brief Clear all lists.
void reset();
private:
- /// Initialize TypeIdentifierMap.
void InitializeTypeMap(const Module &M);
- /// processType - Process DIType.
void processType(DIType DT);
-
- /// processSubprogram - Process DISubprogram.
void processSubprogram(DISubprogram SP);
-
void processScope(DIScope Scope);
-
- /// addCompileUnit - Add compile unit into CUs.
bool addCompileUnit(DICompileUnit CU);
-
- /// addGlobalVariable - Add global variable into GVs.
bool addGlobalVariable(DIGlobalVariable DIG);
-
- // addSubprogram - Add subprogram into SPs.
bool addSubprogram(DISubprogram SP);
-
- /// addType - Add type into Tys.
bool addType(DIType DT);
-
bool addScope(DIScope Scope);
public:
unsigned scope_count() const { return Scopes.size(); }
private:
- SmallVector<DICompileUnit, 8> CUs; // Compile Units
- SmallVector<DISubprogram, 8> SPs; // Subprograms
- SmallVector<DIGlobalVariable, 8> GVs; // Global Variables;
- SmallVector<DIType, 8> TYs; // Types
- SmallVector<DIScope, 8> Scopes; // Scopes
+ SmallVector<DICompileUnit, 8> CUs;
+ SmallVector<DISubprogram, 8> SPs;
+ SmallVector<DIGlobalVariable, 8> GVs;
+ SmallVector<DIType, 8> TYs;
+ SmallVector<DIScope, 8> Scopes;
SmallPtrSet<MDNode *, 64> NodesSeen;
DITypeIdentifierMap TypeIdentifierMap;
- /// Specify if TypeIdentifierMap is initialized.
+
+ /// \brief Specify if TypeIdentifierMap is initialized.
bool TypeMapInitialized;
};
+
+DenseMap<const Function *, DISubprogram> makeSubprogramMap(const Module &M);
+
} // end namespace llvm
#endif