index 9738be02c1ea59f8ba76835c48242534d7d9aa83..a010341305c18b1172922f31b0483480a483b545 100644 (file)
#include "llvm/ADT/ArrayRef.h"
#include "llvm/ADT/DenseMap.h"
-#include "llvm/ADT/FoldingSet.h"
#include "llvm/ADT/ilist_node.h"
#include "llvm/ADT/iterator_range.h"
+#include "llvm/IR/Constant.h"
+#include "llvm/IR/MetadataTracking.h"
#include "llvm/IR/Value.h"
+#include "llvm/Support/ErrorHandling.h"
+#include <type_traits>
namespace llvm {
class LLVMContext;
DEBUG_METADATA_VERSION = 2 // Current debug info version number.
};
+/// \brief Root of the metadata hierarchy.
+///
+/// This is a root class for typeless data in the IR.
+class Metadata {
+ friend class ReplaceableMetadataImpl;
+
+ /// \brief RTTI.
+ const unsigned char SubclassID;
+
+protected:
+ /// \brief Storage flag for non-uniqued, otherwise unowned, metadata.
+ bool IsDistinctInContext : 1;
+ bool InRAUW : 1;
+ // TODO: expose remaining bits to subclasses.
+
+ unsigned short SubclassData16;
+ unsigned SubclassData32;
+
+public:
+ enum MetadataKind {
+ GenericMDNodeKind,
+ MDNodeFwdDeclKind,
+ ConstantAsMetadataKind,
+ LocalAsMetadataKind,
+ MDStringKind
+ };
+
+protected:
+ Metadata(unsigned ID)
+ : SubclassID(ID), IsDistinctInContext(false), InRAUW(false),
+ SubclassData16(0), SubclassData32(0) {}
+ ~Metadata() {}
+
+ /// \brief Store this in a big non-uniqued untyped bucket.
+ bool isStoredDistinctInContext() const { return IsDistinctInContext; }
+
+ /// \brief Default handling of a changed operand, which asserts.
+ ///
+ /// If subclasses pass themselves in as owners to a tracking node reference,
+ /// they must provide an implementation of this method.
+ void handleChangedOperand(void *, Metadata *) {
+ llvm_unreachable("Unimplemented in Metadata subclass");
+ }
+
+public:
+ unsigned getMetadataID() const { return SubclassID; }
+
+ /// \brief User-friendly dump.
+ void dump() const;
+ void print(raw_ostream &OS) const;
+ void printAsOperand(raw_ostream &OS, bool PrintType = true,
+ const Module *M = nullptr) const;
+};
+
+#define HANDLE_METADATA(CLASS) class CLASS;
+#include "llvm/IR/Metadata.def"
+
+inline raw_ostream &operator<<(raw_ostream &OS, const Metadata &MD) {
+ MD.print(OS);
+ return OS;
+}
+
+/// \brief Metadata wrapper in the Value hierarchy.
+///
+/// A member of the \a Value hierarchy to represent a reference to metadata.
+/// This allows, e.g., instrinsics to have metadata as operands.
+///
+/// Notably, this is the only thing in either hierarchy that is allowed to
+/// reference \a LocalAsMetadata.
+class MetadataAsValue : public Value {
+ friend class ReplaceableMetadataImpl;
+ friend class LLVMContextImpl;
+
+ Metadata *MD;
+
+ MetadataAsValue(Type *Ty, Metadata *MD);
+ ~MetadataAsValue();
+
+public:
+ static MetadataAsValue *get(LLVMContext &Context, Metadata *MD);
+ static MetadataAsValue *getIfExists(LLVMContext &Context, Metadata *MD);
+ Metadata *getMetadata() const { return MD; }
+
+ static bool classof(const Value *V) {
+ return V->getValueID() == MetadataAsValueVal;
+ }
+
+private:
+ void handleChangedMetadata(Metadata *MD);
+ void track();
+ void untrack();
+};
+
+/// \brief Shared implementation of use-lists for replaceable metadata.
+///
+/// Most metadata cannot be RAUW'ed. This is a shared implementation of
+/// use-lists and associated API for the two that support it (\a ValueAsMetadata
+/// and \a TempMDNode).
+class ReplaceableMetadataImpl {
+ friend class MetadataTracking;
+
+public:
+ typedef MetadataTracking::OwnerTy OwnerTy;
+
+private:
+ uint64_t NextIndex;
+ SmallDenseMap<void *, std::pair<OwnerTy, uint64_t>, 4> UseMap;
+
+public:
+ ReplaceableMetadataImpl() : NextIndex(0) {}
+ ~ReplaceableMetadataImpl() {
+ assert(UseMap.empty() && "Cannot destroy in-use replaceable metadata");
+ }
+
+ /// \brief Replace all uses of this with MD.
+ ///
+ /// Replace all uses of this with \c MD, which is allowed to be null.
+ void replaceAllUsesWith(Metadata *MD);
+
+ /// \brief Resolve all uses of this.
+ ///
+ /// Resolve all uses of this, turning off RAUW permanently. If \c
+ /// ResolveUsers, call \a GenericMDNode::resolve() on any users whose last
+ /// operand is resolved.
+ void resolveAllUses(bool ResolveUsers = true);
+
+private:
+ void addRef(void *Ref, OwnerTy Owner);
+ void dropRef(void *Ref);
+ void moveRef(void *Ref, void *New, const Metadata &MD);
+
+ static ReplaceableMetadataImpl *get(Metadata &MD);
+};
+
+/// \brief Value wrapper in the Metadata hierarchy.
+///
+/// This is a custom value handle that allows other metadata to refer to
+/// classes in the Value hierarchy.
+///
+/// Because of full uniquing support, each value is only wrapped by a single \a
+/// ValueAsMetadata object, so the lookup maps are far more efficient than
+/// those using ValueHandleBase.
+class ValueAsMetadata : public Metadata, ReplaceableMetadataImpl {
+ friend class ReplaceableMetadataImpl;
+ friend class LLVMContextImpl;
+
+ Value *V;
+
+protected:
+ ValueAsMetadata(unsigned ID, Value *V)
+ : Metadata(ID), V(V) {
+ assert(V && "Expected valid value");
+ }
+ ~ValueAsMetadata() {}
+
+public:
+ static ValueAsMetadata *get(Value *V);
+ static ConstantAsMetadata *getConstant(Value *C) {
+ return cast<ConstantAsMetadata>(get(C));
+ }
+ static LocalAsMetadata *getLocal(Value *Local) {
+ return cast<LocalAsMetadata>(get(Local));
+ }
+
+ static ValueAsMetadata *getIfExists(Value *V);
+ static ConstantAsMetadata *getConstantIfExists(Value *C) {
+ return cast_or_null<ConstantAsMetadata>(getIfExists(C));
+ }
+ static LocalAsMetadata *getLocalIfExists(Value *Local) {
+ return cast_or_null<LocalAsMetadata>(getIfExists(Local));
+ }
+
+ Value *getValue() const { return V; }
+ Type *getType() const { return V->getType(); }
+ LLVMContext &getContext() const { return V->getContext(); }
+
+ static void handleDeletion(Value *V);
+ static void handleRAUW(Value *From, Value *To);
+
+protected:
+ /// \brief Handle collisions after \a Value::replaceAllUsesWith().
+ ///
+ /// RAUW isn't supported directly for \a ValueAsMetadata, but if the wrapped
+ /// \a Value gets RAUW'ed and the target already exists, this is used to
+ /// merge the two metadata nodes.
+ void replaceAllUsesWith(Metadata *MD) {
+ ReplaceableMetadataImpl::replaceAllUsesWith(MD);
+ }
+
+public:
+ static bool classof(const Metadata *MD) {
+ return MD->getMetadataID() == LocalAsMetadataKind ||
+ MD->getMetadataID() == ConstantAsMetadataKind;
+ }
+};
+
+class ConstantAsMetadata : public ValueAsMetadata {
+ friend class ValueAsMetadata;
+
+ ConstantAsMetadata(Constant *C)
+ : ValueAsMetadata(ConstantAsMetadataKind, C) {}
+
+public:
+ static ConstantAsMetadata *get(Constant *C) {
+ return ValueAsMetadata::getConstant(C);
+ }
+ static ConstantAsMetadata *getIfExists(Constant *C) {
+ return ValueAsMetadata::getConstantIfExists(C);
+ }
+
+ Constant *getValue() const {
+ return cast<Constant>(ValueAsMetadata::getValue());
+ }
+
+ static bool classof(const Metadata *MD) {
+ return MD->getMetadataID() == ConstantAsMetadataKind;
+ }
+};
+
+class LocalAsMetadata : public ValueAsMetadata {
+ friend class ValueAsMetadata;
+
+ LocalAsMetadata(Value *Local)
+ : ValueAsMetadata(LocalAsMetadataKind, Local) {
+ assert(!isa<Constant>(Local) && "Expected local value");
+ }
+
+public:
+ static LocalAsMetadata *get(Value *Local) {
+ return ValueAsMetadata::getLocal(Local);
+ }
+ static LocalAsMetadata *getIfExists(Value *Local) {
+ return ValueAsMetadata::getLocalIfExists(Local);
+ }
+
+ static bool classof(const Metadata *MD) {
+ return MD->getMetadataID() == LocalAsMetadataKind;
+ }
+};
+
+/// \brief Transitional API for extracting constants from Metadata.
+///
+/// This namespace contains transitional functions for metadata that points to
+/// \a Constants.
+///
+/// In prehistory -- when metadata was a subclass of \a Value -- \a MDNode
+/// operands could refer to any \a Value. There's was a lot of code like this:
+///
+/// \code
+/// MDNode *N = ...;
+/// auto *CI = dyn_cast<ConstantInt>(N->getOperand(2));
+/// \endcode
+///
+/// Now that \a Value and \a Metadata are in separate hierarchies, maintaining
+/// the semantics for \a isa(), \a cast(), \a dyn_cast() (etc.) requires three
+/// steps: cast in the \a Metadata hierarchy, extraction of the \a Value, and
+/// cast in the \a Value hierarchy. Besides creating boiler-plate, this
+/// requires subtle control flow changes.
+///
+/// The end-goal is to create a new type of metadata, called (e.g.) \a MDInt,
+/// so that metadata can refer to numbers without traversing a bridge to the \a
+/// Value hierarchy. In this final state, the code above would look like this:
+///
+/// \code
+/// MDNode *N = ...;
+/// auto *MI = dyn_cast<MDInt>(N->getOperand(2));
+/// \endcode
+///
+/// The API in this namespace supports the transition. \a MDInt doesn't exist
+/// yet, and even once it does, changing each metadata schema to use it is its
+/// own mini-project. In the meantime this API prevents us from introducing
+/// complex and bug-prone control flow that will disappear in the end. In
+/// particular, the above code looks like this:
+///
+/// \code
+/// MDNode *N = ...;
+/// auto *CI = mdconst::dyn_extract<ConstantInt>(N->getOperand(2));
+/// \endcode
+///
+/// The full set of provided functions includes:
+///
+/// mdconst::hasa <=> isa
+/// mdconst::extract <=> cast
+/// mdconst::extract_or_null <=> cast_or_null
+/// mdconst::dyn_extract <=> dyn_cast
+/// mdconst::dyn_extract_or_null <=> dyn_cast_or_null
+///
+/// The target of the cast must be a subclass of \a Constant.
+namespace mdconst {
+
+namespace detail {
+template <class T> T &make();
+template <class T, class Result> struct HasDereference {
+ typedef char Yes[1];
+ typedef char No[2];
+ template <size_t N> struct SFINAE {};
+
+ template <class U, class V>
+ static Yes &hasDereference(SFINAE<sizeof(static_cast<V>(*make<U>()))> * = 0);
+ template <class U, class V> static No &hasDereference(...);
+
+ static const bool value =
+ sizeof(hasDereference<T, Result>(nullptr)) == sizeof(Yes);
+};
+template <class V, class M> struct IsValidPointer {
+ static const bool value = std::is_base_of<Constant, V>::value &&
+ HasDereference<M, const Metadata &>::value;
+};
+template <class V, class M> struct IsValidReference {
+ static const bool value = std::is_base_of<Constant, V>::value &&
+ std::is_convertible<M, const Metadata &>::value;
+};
+} // end namespace detail
+
+/// \brief Check whether Metadata has a Value.
+///
+/// As an analogue to \a isa(), check whether \c MD has an \a Value inside of
+/// type \c X.
+template <class X, class Y>
+inline typename std::enable_if<detail::IsValidPointer<X, Y>::value, bool>::type
+hasa(Y &&MD) {
+ assert(MD && "Null pointer sent into hasa");
+ if (auto *V = dyn_cast<ConstantAsMetadata>(MD))
+ return isa<X>(V->getValue());
+ return false;
+}
+template <class X, class Y>
+inline
+ typename std::enable_if<detail::IsValidReference<X, Y &>::value, bool>::type
+ hasa(Y &MD) {
+ return hasa(&MD);
+}
+
+/// \brief Extract a Value from Metadata.
+///
+/// As an analogue to \a cast(), extract the \a Value subclass \c X from \c MD.
+template <class X, class Y>
+inline typename std::enable_if<detail::IsValidPointer<X, Y>::value, X *>::type
+extract(Y &&MD) {
+ return cast<X>(cast<ConstantAsMetadata>(MD)->getValue());
+}
+template <class X, class Y>
+inline
+ typename std::enable_if<detail::IsValidReference<X, Y &>::value, X *>::type
+ extract(Y &MD) {
+ return extract(&MD);
+}
+
+/// \brief Extract a Value from Metadata, allowing null.
+///
+/// As an analogue to \a cast_or_null(), extract the \a Value subclass \c X
+/// from \c MD, allowing \c MD to be null.
+template <class X, class Y>
+inline typename std::enable_if<detail::IsValidPointer<X, Y>::value, X *>::type
+extract_or_null(Y &&MD) {
+ if (auto *V = cast_or_null<ConstantAsMetadata>(MD))
+ return cast<X>(V->getValue());
+ return nullptr;
+}
+
+/// \brief Extract a Value from Metadata, if any.
+///
+/// As an analogue to \a dyn_cast_or_null(), extract the \a Value subclass \c X
+/// from \c MD, return null if \c MD doesn't contain a \a Value or if the \a
+/// Value it does contain is of the wrong subclass.
+template <class X, class Y>
+inline typename std::enable_if<detail::IsValidPointer<X, Y>::value, X *>::type
+dyn_extract(Y &&MD) {
+ if (auto *V = dyn_cast<ConstantAsMetadata>(MD))
+ return dyn_cast<X>(V->getValue());
+ return nullptr;
+}
+
+/// \brief Extract a Value from Metadata, if any, allowing null.
+///
+/// As an analogue to \a dyn_cast_or_null(), extract the \a Value subclass \c X
+/// from \c MD, return null if \c MD doesn't contain a \a Value or if the \a
+/// Value it does contain is of the wrong subclass, allowing \c MD to be null.
+template <class X, class Y>
+inline typename std::enable_if<detail::IsValidPointer<X, Y>::value, X *>::type
+dyn_extract_or_null(Y &&MD) {
+ if (auto *V = dyn_cast_or_null<ConstantAsMetadata>(MD))
+ return dyn_cast<X>(V->getValue());
+ return nullptr;
+}
+
+} // end namespace mdconst
+
//===----------------------------------------------------------------------===//
-/// MDString - a single uniqued string.
+/// \brief A single uniqued string.
+///
/// These are used to efficiently contain a byte sequence for metadata.
/// MDString is always unnamed.
-class MDString : public Value {
- virtual void anchor();
+class MDString : public Metadata {
+ friend class StringMapEntry<MDString>;
+
MDString(const MDString &) LLVM_DELETED_FUNCTION;
+ MDString &operator=(MDString &&) LLVM_DELETED_FUNCTION;
+ MDString &operator=(const MDString &) LLVM_DELETED_FUNCTION;
+
+ StringMapEntry<MDString> *Entry;
+ MDString() : Metadata(MDStringKind), Entry(nullptr) {}
+ MDString(MDString &&) : Metadata(MDStringKind) {}
- explicit MDString(LLVMContext &C);
public:
static MDString *get(LLVMContext &Context, StringRef Str);
static MDString *get(LLVMContext &Context, const char *Str) {
return get(Context, Str ? StringRef(Str) : StringRef());
}
- StringRef getString() const { return getName(); }
+ StringRef getString() const;
- unsigned getLength() const { return (unsigned)getName().size(); }
+ unsigned getLength() const { return (unsigned)getString().size(); }
typedef StringRef::iterator iterator;
- /// begin() - Pointer to the first byte of the string.
- iterator begin() const { return getName().begin(); }
+ /// \brief Pointer to the first byte of the string.
+ iterator begin() const { return getString().begin(); }
- /// end() - Pointer to one byte past the end of the string.
- iterator end() const { return getName().end(); }
+ /// \brief Pointer to one byte past the end of the string.
+ iterator end() const { return getString().end(); }
- /// Methods for support type inquiry through isa, cast, and dyn_cast:
- static bool classof(const Value *V) {
- return V->getValueID() == MDStringVal;
+ const unsigned char *bytes_begin() const { return getString().bytes_begin(); }
+ const unsigned char *bytes_end() const { return getString().bytes_end(); }
+
+ /// \brief Methods for support type inquiry through isa, cast, and dyn_cast.
+ static bool classof(const Metadata *MD) {
+ return MD->getMetadataID() == MDStringKind;
}
};
-/// AAMDNodes - A collection of metadata nodes that might be associated with a
+/// \brief A collection of metadata nodes that might be associated with a
/// memory access used by the alias-analysis infrastructure.
struct AAMDNodes {
explicit AAMDNodes(MDNode *T = nullptr, MDNode *S = nullptr,
LLVM_EXPLICIT operator bool() const { return TBAA || Scope || NoAlias; }
- /// TBAA - The tag for type-based alias analysis.
+ /// \brief The tag for type-based alias analysis.
MDNode *TBAA;
- /// Scope - The tag for alias scope specification (used with noalias).
+ /// \brief The tag for alias scope specification (used with noalias).
MDNode *Scope;
- /// NoAlias - The tag specifying the noalias scope.
+ /// \brief The tag specifying the noalias scope.
MDNode *NoAlias;
};
}
};
-class MDNodeOperand;
+/// \brief Tracking metadata reference owned by Metadata.
+///
+/// Similar to \a TrackingMDRef, but it's expected to be owned by an instance
+/// of \a Metadata, which has the option of registering itself for callbacks to
+/// re-unique itself.
+///
+/// In particular, this is used by \a MDNode.
+class MDOperand {
+ MDOperand(MDOperand &&) LLVM_DELETED_FUNCTION;
+ MDOperand(const MDOperand &) LLVM_DELETED_FUNCTION;
+ MDOperand &operator=(MDOperand &&) LLVM_DELETED_FUNCTION;
+ MDOperand &operator=(const MDOperand &) LLVM_DELETED_FUNCTION;
+
+ Metadata *MD;
+
+public:
+ MDOperand() : MD(nullptr) {}
+ ~MDOperand() { untrack(); }
+
+ Metadata *get() const { return MD; }
+ operator Metadata *() const { return get(); }
+ Metadata *operator->() const { return get(); }
+ Metadata &operator*() const { return *get(); }
+
+ void reset() {
+ untrack();
+ MD = nullptr;
+ }
+ void reset(Metadata *MD, Metadata *Owner) {
+ untrack();
+ this->MD = MD;
+ track(Owner);
+ }
+
+private:
+ void track(Metadata *Owner) {
+ if (MD) {
+ if (Owner)
+ MetadataTracking::track(this, *MD, *Owner);
+ else
+ MetadataTracking::track(MD);
+ }
+ }
+ void untrack() {
+ assert(static_cast<void *>(this) == &MD && "Expected same address");
+ if (MD)
+ MetadataTracking::untrack(MD);
+ }
+};
+
+template <> struct simplify_type<MDOperand> {
+ typedef Metadata *SimpleType;
+ static SimpleType getSimplifiedValue(MDOperand &MD) { return MD.get(); }
+};
+
+template <> struct simplify_type<const MDOperand> {
+ typedef Metadata *SimpleType;
+ static SimpleType getSimplifiedValue(const MDOperand &MD) { return MD.get(); }
+};
//===----------------------------------------------------------------------===//
-/// MDNode - a tuple of other values.
-class MDNode : public Value, public FoldingSetNode {
+/// \brief Tuple of metadata.
+class MDNode : public Metadata {
MDNode(const MDNode &) LLVM_DELETED_FUNCTION;
void operator=(const MDNode &) LLVM_DELETED_FUNCTION;
- friend class MDNodeOperand;
- friend class LLVMContextImpl;
- friend struct FoldingSetTrait<MDNode>;
-
- /// Hash - If the MDNode is uniqued cache the hash to speed up lookup.
- unsigned Hash;
+ void *operator new(size_t) LLVM_DELETED_FUNCTION;
- /// NumOperands - This many 'MDNodeOperand' items are co-allocated onto the
- /// end of this MDNode.
+ LLVMContext &Context;
unsigned NumOperands;
- // Subclass data enums.
- enum {
- /// FunctionLocalBit - This bit is set if this MDNode is function local.
- /// This is true when it (potentially transitively) contains a reference to
- /// something in a function, like an argument, basicblock, or instruction.
- FunctionLocalBit = 1 << 0,
+protected:
+ unsigned MDNodeSubclassData;
- /// NotUniquedBit - This is set on MDNodes that are not uniqued because they
- /// have a null operand.
- NotUniquedBit = 1 << 1,
+ void *operator new(size_t Size, unsigned NumOps);
- /// DestroyFlag - This bit is set by destroy() so the destructor can assert
- /// that the node isn't being destroyed with a plain 'delete'.
- DestroyFlag = 1 << 2
- };
+ /// \brief Required by std, but never called.
+ void operator delete(void *Mem);
- // FunctionLocal enums.
- enum FunctionLocalness {
- FL_Unknown = -1,
- FL_No = 0,
- FL_Yes = 1
- };
+ /// \brief Required by std, but never called.
+ void operator delete(void *, unsigned) {
+ llvm_unreachable("Constructor throws?");
+ }
+
+ /// \brief Required by std, but never called.
+ void operator delete(void *, unsigned, bool) {
+ llvm_unreachable("Constructor throws?");
+ }
+
+ MDNode(LLVMContext &Context, unsigned ID, ArrayRef<Metadata *> MDs);
+ ~MDNode() {}
- /// replaceOperand - Replace each instance of F from the operand list of this
- /// node with T.
- void replaceOperand(MDNodeOperand *Op, Value *NewVal);
- ~MDNode();
+ void dropAllReferences();
+ void storeDistinctInContext();
+
+ static MDNode *getMDNode(LLVMContext &C, ArrayRef<Metadata *> MDs,
+ bool Insert = true);
- MDNode(LLVMContext &C, ArrayRef<Value*> Vals, bool isFunctionLocal);
+ MDOperand *mutable_begin() { return mutable_end() - NumOperands; }
+ MDOperand *mutable_end() { return reinterpret_cast<MDOperand *>(this); }
- static MDNode *getMDNode(LLVMContext &C, ArrayRef<Value*> Vals,
- FunctionLocalness FL, bool Insert = true);
public:
- // Constructors and destructors.
- static MDNode *get(LLVMContext &Context, ArrayRef<Value*> Vals);
- // getWhenValsUnresolved - Construct MDNode determining function-localness
- // from isFunctionLocal argument, not by analyzing Vals.
- static MDNode *getWhenValsUnresolved(LLVMContext &Context,
- ArrayRef<Value*> Vals,
- bool isFunctionLocal);
-
- static MDNode *getIfExists(LLVMContext &Context, ArrayRef<Value*> Vals);
-
- /// getTemporary - Return a temporary MDNode, for use in constructing
- /// cyclic MDNode structures. A temporary MDNode is not uniqued,
- /// may be RAUW'd, and must be manually deleted with deleteTemporary.
- static MDNode *getTemporary(LLVMContext &Context, ArrayRef<Value*> Vals);
-
- /// deleteTemporary - Deallocate a node created by getTemporary. The
- /// node must not have any users.
+ static MDNode *get(LLVMContext &Context, ArrayRef<Metadata *> MDs) {
+ return getMDNode(Context, MDs, true);
+ }
+
+ static MDNode *getIfExists(LLVMContext &Context, ArrayRef<Metadata *> MDs) {
+ return getMDNode(Context, MDs, false);
+ }
+
+ /// \brief Return a temporary MDNode
+ ///
+ /// For use in constructing cyclic MDNode structures. A temporary MDNode is
+ /// not uniqued, may be RAUW'd, and must be manually deleted with
+ /// deleteTemporary.
+ static MDNodeFwdDecl *getTemporary(LLVMContext &Context,
+ ArrayRef<Metadata *> MDs);
+
+ /// \brief Deallocate a node created by getTemporary.
+ ///
+ /// The node must not have any users.
static void deleteTemporary(MDNode *N);
- /// replaceOperandWith - Replace a specific operand.
- void replaceOperandWith(unsigned i, Value *NewVal);
+ LLVMContext &getContext() const { return Context; }
- /// getOperand - Return specified operand.
- Value *getOperand(unsigned i) const LLVM_READONLY;
+ /// \brief Replace a specific operand.
+ void replaceOperandWith(unsigned I, Metadata *New);
- /// getNumOperands - Return number of MDNode operands.
- unsigned getNumOperands() const { return NumOperands; }
+ /// \brief Check if node is fully resolved.
+ bool isResolved() const;
+
+protected:
+ /// \brief Set an operand.
+ ///
+ /// Sets the operand directly, without worrying about uniquing.
+ void setOperand(unsigned I, Metadata *New);
+
+public:
+ typedef const MDOperand *op_iterator;
+ typedef iterator_range<op_iterator> op_range;
- /// isFunctionLocal - Return whether MDNode is local to a function.
- bool isFunctionLocal() const {
- return (getSubclassDataFromValue() & FunctionLocalBit) != 0;
+ op_iterator op_begin() const {
+ return const_cast<MDNode *>(this)->mutable_begin();
}
+ op_iterator op_end() const {
+ return const_cast<MDNode *>(this)->mutable_end();
+ }
+ op_range operands() const { return op_range(op_begin(), op_end()); }
- // getFunction - If this metadata is function-local and recursively has a
- // function-local operand, return the first such operand's parent function.
- // Otherwise, return null. getFunction() should not be used for performance-
- // critical code because it recursively visits all the MDNode's operands.
- const Function *getFunction() const;
+ const MDOperand &getOperand(unsigned I) const {
+ assert(I < NumOperands && "Out of range");
+ return op_begin()[I];
+ }
- /// Profile - calculate a unique identifier for this MDNode to collapse
- /// duplicates
- void Profile(FoldingSetNodeID &ID) const;
+ /// \brief Return number of MDNode operands.
+ unsigned getNumOperands() const { return NumOperands; }
- /// Methods for support type inquiry through isa, cast, and dyn_cast:
- static bool classof(const Value *V) {
- return V->getValueID() == MDNodeVal;
+ /// \brief Methods for support type inquiry through isa, cast, and dyn_cast:
+ static bool classof(const Metadata *MD) {
+ return MD->getMetadataID() == GenericMDNodeKind ||
+ MD->getMetadataID() == MDNodeFwdDeclKind;
}
- /// Check whether MDNode is a vtable access.
+ /// \brief Check whether MDNode is a vtable access.
bool isTBAAVtableAccess() const;
- /// Methods for metadata merging.
+ /// \brief Methods for metadata merging.
static MDNode *concatenate(MDNode *A, MDNode *B);
static MDNode *intersect(MDNode *A, MDNode *B);
static MDNode *getMostGenericTBAA(MDNode *A, MDNode *B);
static AAMDNodes getMostGenericAA(const AAMDNodes &A, const AAMDNodes &B);
static MDNode *getMostGenericFPMath(MDNode *A, MDNode *B);
static MDNode *getMostGenericRange(MDNode *A, MDNode *B);
-private:
- // destroy - Delete this node. Only when there are no uses.
- void destroy();
+};
+
+/// \brief Generic metadata node.
+///
+/// Generic metadata nodes, with opt-out support for uniquing.
+///
+/// Although nodes are uniqued by default, \a GenericMDNode has no support for
+/// RAUW. If an operand change (due to RAUW or otherwise) causes a uniquing
+/// collision, the uniquing bit is dropped.
+///
+/// TODO: Make uniquing opt-out (status: mandatory, sometimes dropped).
+class GenericMDNode : public MDNode {
+ friend class Metadata;
+ friend class MDNode;
+ friend class LLVMContextImpl;
+ friend class ReplaceableMetadataImpl;
+
+ /// \brief Support RAUW as long as one of its arguments is replaceable.
+ ///
+ /// If an operand is an \a MDNodeFwdDecl (or a replaceable \a GenericMDNode),
+ /// support RAUW to support uniquing as forward declarations are resolved.
+ /// As soon as operands have been resolved, drop support.
+ ///
+ /// FIXME: Save memory by storing this in a pointer union with the
+ /// LLVMContext, and adding an LLVMContext reference to RMI.
+ std::unique_ptr<ReplaceableMetadataImpl> ReplaceableUses;
- bool isNotUniqued() const {
- return (getSubclassDataFromValue() & NotUniquedBit) != 0;
+ GenericMDNode(LLVMContext &C, ArrayRef<Metadata *> Vals);
+ ~GenericMDNode();
+
+ void setHash(unsigned Hash) { MDNodeSubclassData = Hash; }
+
+public:
+ /// \brief Get the hash, if any.
+ unsigned getHash() const { return MDNodeSubclassData; }
+
+ static bool classof(const Metadata *MD) {
+ return MD->getMetadataID() == GenericMDNodeKind;
}
- void setIsNotUniqued();
- // Shadow Value::setValueSubclassData with a private forwarding method so that
- // any future subclasses cannot accidentally use it.
- void setValueSubclassData(unsigned short D) {
- Value::setValueSubclassData(D);
+ /// \brief Check whether any operands are forward declarations.
+ ///
+ /// Returns \c true as long as any operands (or their operands, etc.) are \a
+ /// MDNodeFwdDecl.
+ ///
+ /// As forward declarations are resolved, their containers should get
+ /// resolved automatically. However, if this (or one of its operands) is
+ /// involved in a cycle, \a resolveCycles() needs to be called explicitly.
+ bool isResolved() const { return !ReplaceableUses; }
+
+ /// \brief Resolve cycles.
+ ///
+ /// Once all forward declarations have been resolved, force cycles to be
+ /// resolved.
+ ///
+ /// \pre No operands (or operands' operands, etc.) are \a MDNodeFwdDecl.
+ void resolveCycles();
+
+private:
+ void handleChangedOperand(void *Ref, Metadata *New);
+
+ bool hasUnresolvedOperands() const { return SubclassData32; }
+ void incrementUnresolvedOperands() { ++SubclassData32; }
+ void decrementUnresolvedOperands() { --SubclassData32; }
+ void resolve();
+};
+
+/// \brief Forward declaration of metadata.
+///
+/// Forward declaration of metadata, in the form of a metadata node. Unlike \a
+/// GenericMDNode, this class has support for RAUW and is suitable for forward
+/// references.
+class MDNodeFwdDecl : public MDNode, ReplaceableMetadataImpl {
+ friend class Metadata;
+ friend class MDNode;
+ friend class ReplaceableMetadataImpl;
+
+ MDNodeFwdDecl(LLVMContext &C, ArrayRef<Metadata *> Vals)
+ : MDNode(C, MDNodeFwdDeclKind, Vals) {}
+ ~MDNodeFwdDecl() { dropAllReferences(); }
+
+public:
+ static bool classof(const Metadata *MD) {
+ return MD->getMetadataID() == MDNodeFwdDeclKind;
}
+
+ using ReplaceableMetadataImpl::replaceAllUsesWith;
};
//===----------------------------------------------------------------------===//
-/// NamedMDNode - a tuple of MDNodes. Despite its name, a NamedMDNode isn't
-/// itself an MDNode. NamedMDNodes belong to modules, have names, and contain
-/// lists of MDNodes.
+/// \brief A tuple of MDNodes.
+///
+/// Despite its name, a NamedMDNode isn't itself an MDNode. NamedMDNodes belong
+/// to modules, have names, and contain lists of MDNodes.
+///
+/// TODO: Inherit from Metadata.
class NamedMDNode : public ilist_node<NamedMDNode> {
friend class SymbolTableListTraits<NamedMDNode, Module>;
friend struct ilist_traits<NamedMDNode>;
std::string Name;
Module *Parent;
- void *Operands; // SmallVector<TrackingVH<MDNode>, 4>
+ void *Operands; // SmallVector<TrackingMDRef, 4>
void setParent(Module *M) { Parent = M; }
};
public:
- /// eraseFromParent - Drop all references and remove the node from parent
- /// module.
+ /// \brief Drop all references and remove the node from parent module.
void eraseFromParent();
- /// dropAllReferences - Remove all uses and clear node vector.
+ /// \brief Remove all uses and clear node vector.
void dropAllReferences();
- /// ~NamedMDNode - Destroy NamedMDNode.
~NamedMDNode();
- /// getParent - Get the module that holds this named metadata collection.
+ /// \brief Get the module that holds this named metadata collection.
inline Module *getParent() { return Parent; }
inline const Module *getParent() const { return Parent; }
- /// getOperand - Return specified operand.
MDNode *getOperand(unsigned i) const;
-
- /// getNumOperands - Return the number of NamedMDNode operands.
unsigned getNumOperands() const;
-
- /// addOperand - Add metadata operand.
void addOperand(MDNode *M);
-
- /// getName - Return a constant reference to this named metadata's name.
+ void setOperand(unsigned I, MDNode *New);
StringRef getName() const;
-
- /// print - Implement operator<< on NamedMDNode.
void print(raw_ostream &ROS) const;
-
- /// dump() - Allow printing of NamedMDNodes from the debugger.
void dump() const;
// ---------------------------------------------------------------------------
// Operand Iterator interface...
//
- typedef op_iterator_impl<MDNode*, MDNode> op_iterator;
+ typedef op_iterator_impl<MDNode *, MDNode> op_iterator;
op_iterator op_begin() { return op_iterator(this, 0); }
op_iterator op_end() { return op_iterator(this, getNumOperands()); }
- typedef op_iterator_impl<const MDNode*, MDNode> const_op_iterator;
+ typedef op_iterator_impl<const MDNode *, MDNode> const_op_iterator;
const_op_iterator op_begin() const { return const_op_iterator(this, 0); }
const_op_iterator op_end() const { return const_op_iterator(this, getNumOperands()); }