diff --git a/include/llvm/Transforms/Utils/SimplifyLibCalls.h b/include/llvm/Transforms/Utils/SimplifyLibCalls.h
index d2f096fd1efd4773274cf48904ab73d238004684..fb3beb2ab2d7a973b390321bd26de87990cb4953 100644 (file)
const DataLayout *DL;
const TargetLibraryInfo *TLI;
bool UnsafeFPShrink;
const DataLayout *DL;
const TargetLibraryInfo *TLI;
bool UnsafeFPShrink;
+ function_ref<void(Instruction *, Value *)> Replacer;
-protected:
- ~LibCallSimplifier() {}
+ /// \brief Internal wrapper for RAUW that is the default implementation.
+ ///
+ /// Other users may provide an alternate function with this signature instead
+ /// of this one.
+ static void replaceAllUsesWithDefault(Instruction *I, Value *With);
+
+ /// \brief Replace an instruction's uses with a value using our replacer.
+ void replaceAllUsesWith(Instruction *I, Value *With);
public:
public:
- LibCallSimplifier(const DataLayout *TD, const TargetLibraryInfo *TLI);
+ LibCallSimplifier(const DataLayout *TD, const TargetLibraryInfo *TLI,
+ function_ref<void(Instruction *, Value *)> Replacer =
+ &replaceAllUsesWithDefault);
/// optimizeCall - Take the given call instruction and return a more
/// optimal value to replace the instruction with or 0 if a more
/// optimizeCall - Take the given call instruction and return a more
/// optimal value to replace the instruction with or 0 if a more
/// The call must not be an indirect call.
Value *optimizeCall(CallInst *CI);
/// The call must not be an indirect call.
Value *optimizeCall(CallInst *CI);
- /// replaceAllUsesWith - This method is used when the library call
- /// simplifier needs to replace instructions other than the library
- /// call being modified.
- virtual void replaceAllUsesWith(Instruction *I, Value *With) const;
-
private:
// String and Memory Library Call Optimizations
Value *optimizeStrCat(CallInst *CI, IRBuilder<> &B);
private:
// String and Memory Library Call Optimizations
Value *optimizeStrCat(CallInst *CI, IRBuilder<> &B);