]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - lib/CodeGen/AsmPrinter/AsmPrinter.cpp
Debug info: Remove ARMAsmPrinter::EmitDwarfRegOp(). AsmPrinter can now
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / AsmPrinter.cpp
index 7422988e74a43c0ddd1e9f176b6b0a7b5c08da50..d59713c142eba2f84cc1dcee8bb9cfe4453bb033 100644 (file)
 #include "llvm/CodeGen/AsmPrinter.h"
 #include "DwarfDebug.h"
 #include "DwarfException.h"
+#include "llvm/ADT/SmallBitVector.h"
 #include "llvm/ADT/SmallString.h"
 #include "llvm/ADT/Statistic.h"
 #include "llvm/Analysis/ConstantFolding.h"
-#include "llvm/Assembly/Writer.h"
 #include "llvm/CodeGen/GCMetadataPrinter.h"
 #include "llvm/CodeGen/MachineConstantPool.h"
 #include "llvm/CodeGen/MachineFrameInfo.h"
 #include "llvm/CodeGen/MachineFunction.h"
+#include "llvm/CodeGen/MachineInstrBundle.h"
 #include "llvm/CodeGen/MachineJumpTableInfo.h"
 #include "llvm/CodeGen/MachineLoopInfo.h"
 #include "llvm/CodeGen/MachineModuleInfo.h"
 #include "llvm/DebugInfo.h"
 #include "llvm/IR/DataLayout.h"
+#include "llvm/IR/Mangler.h"
 #include "llvm/IR/Module.h"
 #include "llvm/IR/Operator.h"
 #include "llvm/MC/MCAsmInfo.h"
 #include "llvm/Support/Format.h"
 #include "llvm/Support/MathExtras.h"
 #include "llvm/Support/Timer.h"
-#include "llvm/Target/Mangler.h"
 #include "llvm/Target/TargetFrameLowering.h"
 #include "llvm/Target/TargetInstrInfo.h"
 #include "llvm/Target/TargetLowering.h"
 #include "llvm/Target/TargetLoweringObjectFile.h"
 #include "llvm/Target/TargetOptions.h"
 #include "llvm/Target/TargetRegisterInfo.h"
+#include "llvm/Target/TargetSubtargetInfo.h"
 #include "llvm/Transforms/Utils/GlobalStatus.h"
+#include "WinCodeViewLineTables.h"
 using namespace llvm;
 
 static const char *const DWARFGroupName = "DWARF Emission";
-static const char *const DbgTimerName = "DWARF Debug Writer";
+static const char *const DbgTimerName = "Debug Info Emission";
 static const char *const EHTimerName = "DWARF Exception Writer";
+static const char *const CodeViewLineTablesGroupName = "CodeView Line Tables";
 
 STATISTIC(EmittedInsts, "Number of machine instrs printed");
 
@@ -135,6 +139,14 @@ const DataLayout &AsmPrinter::getDataLayout() const {
   return *TM.getDataLayout();
 }
 
+const MCSubtargetInfo &AsmPrinter::getSubtargetInfo() const {
+  return TM.getSubtarget<MCSubtargetInfo>();
+}
+
+void AsmPrinter::EmitToStreamer(MCStreamer &S, const MCInst &Inst) {
+  S.EmitInstruction(Inst, getSubtargetInfo());
+}
+
 StringRef AsmPrinter::getTargetTriple() const {
   return TM.getTargetTriple();
 }
@@ -163,9 +175,9 @@ bool AsmPrinter::doInitialization(Module &M) {
   const_cast<TargetLoweringObjectFile&>(getObjFileLowering())
     .Initialize(OutContext, TM);
 
-  OutStreamer.InitStreamer();
+  OutStreamer.InitSections(false);
 
-  Mang = new Mangler(&TM);
+  Mang = new Mangler(TM.getDataLayout());
 
   // Allow the target to emit any magic that it wants at the start of the file.
   EmitStartOfAsmFile(M);
@@ -193,8 +205,14 @@ bool AsmPrinter::doInitialization(Module &M) {
   }
 
   if (MAI->doesSupportDebugInformation()) {
-    DD = new DwarfDebug(this, &M);
-    Handlers.push_back(HandlerInfo(DD, DbgTimerName, DWARFGroupName));
+    if (Triple(TM.getTargetTriple()).getOS() == Triple::Win32) {
+      Handlers.push_back(HandlerInfo(new WinCodeViewLineTables(this),
+                                     DbgTimerName,
+                                     CodeViewLineTablesGroupName));
+    } else {
+      DD = new DwarfDebug(this, &M);
+      Handlers.push_back(HandlerInfo(DD, DbgTimerName, DWARFGroupName));
+    }
   }
 
   DwarfException *DE = 0;
@@ -217,6 +235,36 @@ bool AsmPrinter::doInitialization(Module &M) {
   return false;
 }
 
+static bool canBeHidden(const GlobalValue *GV, const MCAsmInfo &MAI) {
+  GlobalValue::LinkageTypes Linkage = GV->getLinkage();
+  if (Linkage != GlobalValue::LinkOnceODRLinkage)
+    return false;
+
+  if (!MAI.hasWeakDefCanBeHiddenDirective())
+    return false;
+
+  if (GV->hasUnnamedAddr())
+    return true;
+
+  // This is only used for MachO, so right now it doesn't really matter how
+  // we handle alias. Revisit this once the MachO linker implements aliases.
+  if (isa<GlobalAlias>(GV))
+    return false;
+
+  // If it is a non constant variable, it needs to be uniqued across shared
+  // objects.
+  if (const GlobalVariable *Var = dyn_cast<GlobalVariable>(GV)) {
+    if (!Var->isConstant())
+      return false;
+  }
+
+  GlobalStatus GS;
+  if (!GlobalStatus::analyzeGlobal(GV, GS) && !GS.IsCompared)
+    return true;
+
+  return false;
+}
+
 void AsmPrinter::EmitLinkage(const GlobalValue *GV, MCSymbol *GVSym) const {
   GlobalValue::LinkageTypes Linkage = GV->getLinkage();
   switch (Linkage) {
@@ -230,19 +278,7 @@ void AsmPrinter::EmitLinkage(const GlobalValue *GV, MCSymbol *GVSym) const {
       // .globl _foo
       OutStreamer.EmitSymbolAttribute(GVSym, MCSA_Global);
 
-      bool CanBeHidden = false;
-
-      if (Linkage == GlobalValue::LinkOnceODRLinkage) {
-        if (GV->hasUnnamedAddr()) {
-          CanBeHidden = true;
-        } else {
-          GlobalStatus GS;
-          if (!GlobalStatus::analyzeGlobal(GV, GS) && !GS.IsCompared)
-            CanBeHidden = true;
-        }
-      }
-
-      if (!CanBeHidden)
+      if (!canBeHidden(GV, *MAI))
         // .weak_definition _foo
         OutStreamer.EmitSymbolAttribute(GVSym, MCSA_WeakDefinition);
       else
@@ -256,7 +292,6 @@ void AsmPrinter::EmitLinkage(const GlobalValue *GV, MCSymbol *GVSym) const {
       OutStreamer.EmitSymbolAttribute(GVSym, MCSA_Weak);
     }
     return;
-  case GlobalValue::DLLExportLinkage:
   case GlobalValue::AppendingLinkage:
     // FIXME: appending linkage variables should go into a section of
     // their name or something.  For now, just emit them as external.
@@ -271,15 +306,19 @@ void AsmPrinter::EmitLinkage(const GlobalValue *GV, MCSymbol *GVSym) const {
     return;
   case GlobalValue::AvailableExternallyLinkage:
     llvm_unreachable("Should never emit this");
-  case GlobalValue::DLLImportLinkage:
   case GlobalValue::ExternalWeakLinkage:
     llvm_unreachable("Don't know how to emit these");
   }
   llvm_unreachable("Unknown linkage type!");
 }
 
+void AsmPrinter::getNameWithPrefix(SmallVectorImpl<char> &Name,
+                                   const GlobalValue *GV) const {
+  TM.getNameWithPrefix(Name, GV, *Mang);
+}
+
 MCSymbol *AsmPrinter::getSymbol(const GlobalValue *GV) const {
-  return getObjFileLowering().getSymbol(*Mang, GV);
+  return TM.getSymbol(GV, *Mang);
 }
 
 /// EmitGlobalVariable - Emit the specified global variable to the .s file.
@@ -290,7 +329,7 @@ void AsmPrinter::EmitGlobalVariable(const GlobalVariable *GV) {
       return;
 
     if (isVerbose()) {
-      WriteAsOperand(OutStreamer.GetCommentOS(), GV,
+      GV->printAsOperand(OutStreamer.GetCommentOS(),
                      /*PrintType=*/false, GV->getParent());
       OutStreamer.GetCommentOS() << '\n';
     }
@@ -339,7 +378,7 @@ void AsmPrinter::EmitGlobalVariable(const GlobalVariable *GV) {
     // Handle local BSS symbols.
     if (MAI->hasMachoZeroFillDirective()) {
       const MCSection *TheSection =
-        getObjFileLowering().SectionForGlobal(GV, GVKind, Mang, TM);
+        getObjFileLowering().SectionForGlobal(GV, GVKind, *Mang, TM);
       // .zerofill __DATA, __bss, _foo, 400, 5
       OutStreamer.EmitZerofill(TheSection, GVSym, Size, Align);
       return;
@@ -368,7 +407,7 @@ void AsmPrinter::EmitGlobalVariable(const GlobalVariable *GV) {
   }
 
   const MCSection *TheSection =
-    getObjFileLowering().SectionForGlobal(GV, GVKind, Mang, TM);
+    getObjFileLowering().SectionForGlobal(GV, GVKind, *Mang, TM);
 
   // Handle the zerofill directive on darwin, which is a special form of BSS
   // emission.
@@ -459,7 +498,8 @@ void AsmPrinter::EmitFunctionHeader() {
   // Print the 'header' of function.
   const Function *F = MF->getFunction();
 
-  OutStreamer.SwitchSection(getObjFileLowering().SectionForGlobal(F, Mang, TM));
+  OutStreamer.SwitchSection(
+      getObjFileLowering().SectionForGlobal(F, *Mang, TM));
   EmitVisibility(CurrentFnSym, F->getVisibility());
 
   EmitLinkage(F, CurrentFnSym);
@@ -469,7 +509,7 @@ void AsmPrinter::EmitFunctionHeader() {
     OutStreamer.EmitSymbolAttribute(CurrentFnSym, MCSA_ELF_TypeFunction);
 
   if (isVerbose()) {
-    WriteAsOperand(OutStreamer.GetCommentOS(), F,
+    F->printAsOperand(OutStreamer.GetCommentOS(),
                    /*PrintType=*/false, F->getParent());
     OutStreamer.GetCommentOS() << '\n';
   }
@@ -580,7 +620,7 @@ static bool emitDebugValueComment(const MachineInstr *MI, AsmPrinter &AP) {
 
   SmallString<128> Str;
   raw_svector_ostream OS(Str);
-  OS << '\t' << AP.MAI->getCommentString() << "DEBUG_VALUE: ";
+  OS << "DEBUG_VALUE: ";
 
   DIVariable V(MI->getOperand(2).getMetadata());
   if (V.getContext().isSubprogram()) {
@@ -628,7 +668,7 @@ static bool emitDebugValueComment(const MachineInstr *MI, AsmPrinter &AP) {
       // Suppress offset, it is not meaningful here.
       OS << "undef";
       // NOTE: Want this comment at start of line, don't emit with AddComment.
-      AP.OutStreamer.EmitRawText(OS.str());
+      AP.OutStreamer.emitRawComment(OS.str());
       return true;
     }
     if (Deref)
@@ -640,7 +680,7 @@ static bool emitDebugValueComment(const MachineInstr *MI, AsmPrinter &AP) {
     OS << '+' << Offset << ']';
 
   // NOTE: Want this comment at start of line, don't emit with AddComment.
-  AP.OutStreamer.EmitRawText(OS.str());
+  AP.OutStreamer.emitRawComment(OS.str());
   return true;
 }
 
@@ -660,14 +700,13 @@ bool AsmPrinter::needsSEHMoves() {
     MF->getFunction()->needsUnwindTableEntry();
 }
 
-bool AsmPrinter::needsRelocationsForDwarfStringPool() const {
-  return MAI->doesDwarfUseRelocationsAcrossSections();
-}
-
 void AsmPrinter::emitPrologLabel(const MachineInstr &MI) {
   const MCSymbol *Label = MI.getOperand(0).getMCSymbol();
 
-  if (MAI->getExceptionHandlingType() != ExceptionHandling::DwarfCFI)
+  ExceptionHandling::ExceptionsType ExceptionHandlingType =
+      MAI->getExceptionHandlingType();
+  if (ExceptionHandlingType != ExceptionHandling::DwarfCFI &&
+      ExceptionHandlingType != ExceptionHandling::ARM)
     return;
 
   if (needsCFIMoves() == CFI_M_None)
@@ -753,9 +792,6 @@ void AsmPrinter::EmitFunctionBody() {
         if (isVerbose()) emitKill(II, *this);
         break;
       default:
-        if (!TM.hasMCUseLoc())
-          MCLineEntry::Make(&OutStreamer, getCurrentSection());
-
         EmitInstruction(II);
         break;
       }
@@ -786,7 +822,7 @@ void AsmPrinter::EmitFunctionBody() {
     TM.getInstrInfo()->getNoopForMachoTarget(Noop);
     if (Noop.getOpcode()) {
       OutStreamer.AddComment("avoids zero-length function");
-      OutStreamer.EmitInstruction(Noop);
+      OutStreamer.EmitInstruction(Noop, getSubtargetInfo());
     } else  // Target not mc-ized yet.
       OutStreamer.EmitRawText(StringRef("\tnop\n"));
   }
@@ -836,54 +872,157 @@ void AsmPrinter::EmitFunctionBody() {
   OutStreamer.AddBlankLine();
 }
 
-/// EmitDwarfRegOp - Emit dwarf register operation.
-void AsmPrinter::EmitDwarfRegOp(const MachineLocation &MLoc,
-                                bool Indirect) const {
-  const TargetRegisterInfo *TRI = TM.getRegisterInfo();
+/// Emit a dwarf register operation.
+static void emitDwarfRegOp(const AsmPrinter &AP, int Reg) {
+  assert(Reg >= 0);
+  if (Reg < 32) {
+    AP.OutStreamer.AddComment(dwarf::
+                              OperationEncodingString(dwarf::DW_OP_reg0 + Reg));
+    AP.EmitInt8(dwarf::DW_OP_reg0 + Reg);
+  } else {
+    AP.OutStreamer.AddComment("DW_OP_regx");
+    AP.EmitInt8(dwarf::DW_OP_regx);
+    AP.OutStreamer.AddComment(Twine(Reg));
+    AP.EmitULEB128(Reg);
+  }
+}
+
+/// Emit an (double-)indirect dwarf register operation.
+static void emitDwarfRegOpIndirect(const AsmPrinter &AP,
+                                   int Reg, int Offset, bool Deref) {
+  assert(Reg >= 0);
+  if (Reg < 32) {
+    AP.OutStreamer.AddComment(dwarf::
+                              OperationEncodingString(dwarf::DW_OP_breg0 + Reg));
+    AP.EmitInt8(dwarf::DW_OP_breg0 + Reg);
+  } else {
+    AP.OutStreamer.AddComment("DW_OP_bregx");
+    AP.EmitInt8(dwarf::DW_OP_bregx);
+    AP.OutStreamer.AddComment(Twine(Reg));
+    AP.EmitULEB128(Reg);
+  }
+  AP.EmitSLEB128(Offset);
+  if (Deref)
+    AP.EmitInt8(dwarf::DW_OP_deref);
+}
+
+/// Emit a dwarf register operation for describing
+/// - a small value occupying only part of a register or
+/// - a small register representing only part of a value.
+static void emitDwarfOpPiece(const AsmPrinter &AP,
+                                unsigned Size, unsigned Offset) {
+  assert(Size > 0);
+  if (Offset > 0) {
+    AP.OutStreamer.AddComment("DW_OP_bit_piece");
+    AP.EmitInt8(dwarf::DW_OP_bit_piece);
+    AP.OutStreamer.AddComment(Twine(Size));
+    AP.EmitULEB128(Size);
+    AP.OutStreamer.AddComment(Twine(Offset));
+    AP.EmitULEB128(Offset);
+  } else {
+    AP.OutStreamer.AddComment("DW_OP_piece");
+    AP.EmitInt8(dwarf::DW_OP_piece);
+    unsigned ByteSize = Size / 8; // Assuming 8 bits per byte.
+    AP.OutStreamer.AddComment(Twine(ByteSize));
+    AP.EmitULEB128(ByteSize);
+  }
+}
+
+/// Some targets do not provide a DWARF register number for every
+/// register.  This function attempts to emit a dwarf register by
+/// emitting a piece of a super-register or by piecing together
+/// multiple subregisters that alias the register.
+static void EmitDwarfRegOpPiece(const AsmPrinter &AP,
+                                const MachineLocation &MLoc) {
+  assert(!MLoc.isIndirect());
+  const TargetRegisterInfo *TRI = AP.TM.getRegisterInfo();
   int Reg = TRI->getDwarfRegNum(MLoc.getReg(), false);
 
-  for (MCSuperRegIterator SR(MLoc.getReg(), TRI); SR.isValid() && Reg < 0;
-       ++SR) {
+  // Walk up the super-register chain until we find a valid number.
+  // For example, EAX on x86_64 is a 32-bit piece of RAX with offset 0.
+  for (MCSuperRegIterator SR(MLoc.getReg(), TRI); SR.isValid(); ++SR) {
     Reg = TRI->getDwarfRegNum(*SR, false);
-    // FIXME: Get the bit range this register uses of the superregister
-    // so that we can produce a DW_OP_bit_piece
+    if (Reg >= 0) {
+      unsigned Idx = TRI->getSubRegIndex(*SR, MLoc.getReg());
+      unsigned Size = TRI->getSubRegIdxSize(Idx);
+      unsigned Offset = TRI->getSubRegIdxOffset(Idx);
+      AP.OutStreamer.AddComment("super-register");
+      emitDwarfRegOp(AP, Reg);
+      emitDwarfOpPiece(AP, Size, Offset);
+      return;
+    }
   }
 
-  // FIXME: Handle cases like a super register being encoded as
-  // DW_OP_reg 32 DW_OP_piece 4 DW_OP_reg 33
-
-  // FIXME: We have no reasonable way of handling errors in here. The
-  // caller might be in the middle of an dwarf expression. We should
-  // probably assert that Reg >= 0 once debug info generation is more mature.
+  // Otherwise, attempt to find a covering set of sub-register numbers.
+  // For example, Q0 on ARM is a composition of D0+D1.
+  //
+  // Keep track of the current position so we can emit the more
+  // efficient DW_OP_piece.
+  unsigned CurPos = 0;
+  // The size of the register in bits, assuming 8 bits per byte.
+  unsigned RegSize = TRI->getMinimalPhysRegClass(MLoc.getReg())->getSize()*8;
+  // Keep track of the bits in the register we already emitted, so we
+  // can avoid emitting redundant aliasing subregs.
+  SmallBitVector Coverage(RegSize, false);
+  for (MCSubRegIterator SR(MLoc.getReg(), TRI); SR.isValid(); ++SR) {
+    unsigned Idx = TRI->getSubRegIndex(MLoc.getReg(), *SR);
+    unsigned Size = TRI->getSubRegIdxSize(Idx);
+    unsigned Offset = TRI->getSubRegIdxOffset(Idx);
+    Reg = TRI->getDwarfRegNum(*SR, false);
 
-  if (MLoc.isIndirect() || Indirect) {
-    if (Reg < 32) {
-      OutStreamer.AddComment(
-        dwarf::OperationEncodingString(dwarf::DW_OP_breg0 + Reg));
-      EmitInt8(dwarf::DW_OP_breg0 + Reg);
-    } else {
-      OutStreamer.AddComment("DW_OP_bregx");
-      EmitInt8(dwarf::DW_OP_bregx);
-      OutStreamer.AddComment(Twine(Reg));
-      EmitULEB128(Reg);
+    // Intersection between the bits we already emitted and the bits
+    // covered by this subregister.
+    SmallBitVector Intersection(RegSize, false);
+    Intersection.set(Offset, Offset+Size);
+    Intersection ^= Coverage;
+
+    // If this sub-register has a DWARF number and we haven't covered
+    // its range, emit a DWARF piece for it.
+    if (Reg >= 0 && Intersection.any()) {
+      AP.OutStreamer.AddComment("sub-register");
+      emitDwarfRegOp(AP, Reg);
+      emitDwarfOpPiece(AP, Size, Offset == CurPos ? 0 : Offset);
+      CurPos = Offset+Size;
+
+      // Mark it as emitted.
+      Coverage.set(Offset, Offset+Size);
     }
-    EmitSLEB128(!MLoc.isIndirect() ? 0 : MLoc.getOffset());
-    if (MLoc.isIndirect() && Indirect)
-      EmitInt8(dwarf::DW_OP_deref);
-  } else {
-    if (Reg < 32) {
-      OutStreamer.AddComment(
-        dwarf::OperationEncodingString(dwarf::DW_OP_reg0 + Reg));
-      EmitInt8(dwarf::DW_OP_reg0 + Reg);
-    } else {
-      OutStreamer.AddComment("DW_OP_regx");
-      EmitInt8(dwarf::DW_OP_regx);
-      OutStreamer.AddComment(Twine(Reg));
-      EmitULEB128(Reg);
+  }
+
+  if (CurPos == 0) {
+    // FIXME: We have no reasonable way of handling errors in here.
+    AP.OutStreamer.AddComment("nop (could not find a dwarf register number)");
+    AP.EmitInt8(dwarf::DW_OP_nop);
+  }
+}
+
+/// EmitDwarfRegOp - Emit dwarf register operation.
+void AsmPrinter::EmitDwarfRegOp(const MachineLocation &MLoc,
+                                bool Indirect) const {
+  const TargetRegisterInfo *TRI = TM.getRegisterInfo();
+  int Reg = TRI->getDwarfRegNum(MLoc.getReg(), false);
+  if (Reg < 0) {
+    // We assume that pointers are always in an addressable register.
+    if (Indirect || MLoc.isIndirect()) {
+      // FIXME: We have no reasonable way of handling errors in here. The
+      // caller might be in the middle of a dwarf expression. We should
+      // probably assert that Reg >= 0 once debug info generation is more mature.
+      OutStreamer.AddComment("nop (invalid dwarf register number for indirect loc)");
+      EmitInt8(dwarf::DW_OP_nop);
+      return;
     }
+
+    // Attempt to find a valid super- or sub-register.
+    if (!Indirect && !MLoc.isIndirect())
+      return EmitDwarfRegOpPiece(*this, MLoc);
   }
 
-  // FIXME: Produce a DW_OP_bit_piece if we used a superregister
+  if (MLoc.isIndirect())
+    emitDwarfRegOpIndirect(*this, Reg, MLoc.getOffset(), Indirect);
+  else if (Indirect)
+    emitDwarfRegOpIndirect(*this, Reg, 0, false);
+  else
+    emitDwarfRegOp(*this, Reg);
 }
 
 bool AsmPrinter::doFinalization(Module &M) {
@@ -909,7 +1048,7 @@ bool AsmPrinter::doFinalization(Module &M) {
   SmallVector<Module::ModuleFlagEntry, 8> ModuleFlags;
   M.getModuleFlagsMetadata(ModuleFlags);
   if (!ModuleFlags.empty())
-    getObjFileLowering().emitModuleFlags(OutStreamer, ModuleFlags, Mang, TM);
+    getObjFileLowering().emitModuleFlags(OutStreamer, ModuleFlags, *Mang, TM);
 
   // Make sure we wrote out everything we need.
   OutStreamer.Flush();
@@ -1109,6 +1248,7 @@ void AsmPrinter::EmitConstantPool() {
 /// by the current function to the current output stream.
 ///
 void AsmPrinter::EmitJumpTableInfo() {
+  const DataLayout *DL = MF->getTarget().getDataLayout();
   const MachineJumpTableInfo *MJTI = MF->getJumpTableInfo();
   if (MJTI == 0) return;
   if (MJTI->getEntryKind() == MachineJumpTableInfo::EK_Inline) return;
@@ -1128,7 +1268,8 @@ void AsmPrinter::EmitJumpTableInfo() {
       // FIXME: this isn't the right predicate, should be based on the MCSection
       // for the function.
       F->isWeakForLinker()) {
-    OutStreamer.SwitchSection(getObjFileLowering().SectionForGlobal(F,Mang,TM));
+    OutStreamer.SwitchSection(
+        getObjFileLowering().SectionForGlobal(F, *Mang, TM));
   } else {
     // Otherwise, drop it in the readonly section.
     const MCSection *ReadOnlySection =
@@ -1174,7 +1315,7 @@ void AsmPrinter::EmitJumpTableInfo() {
     // before each jump table.  The first label is never referenced, but tells
     // the assembler and linker the extents of the jump table object.  The
     // second label is actually referenced by the code.
-    if (JTInDiffSection && MAI->getLinkerPrivateGlobalPrefix()[0])
+    if (JTInDiffSection && DL->hasLinkerPrivateGlobalPrefix())
       // FIXME: This doesn't have to have any specific name, just any randomly
       // named and numbered 'l' label would work.  Simplify GetJTISymbol.
       OutStreamer.EmitLabel(GetJTISymbol(JTI, true));
@@ -1312,7 +1453,7 @@ void AsmPrinter::EmitLLVMUsedList(const ConstantArray *InitList) {
   for (unsigned i = 0, e = InitList->getNumOperands(); i != e; ++i) {
     const GlobalValue *GV =
       dyn_cast<GlobalValue>(InitList->getOperand(i)->stripPointerCasts());
-    if (GV && getObjFileLowering().shouldEmitUsedDirectiveFor(GV, Mang))
+    if (GV && getObjFileLowering().shouldEmitUsedDirectiveFor(GV, *Mang, TM))
       OutStreamer.EmitSymbolAttribute(getSymbol(GV), MCSA_NoDeadStrip);
   }
 }
@@ -1369,7 +1510,7 @@ void AsmPrinter::EmitModuleIdents(Module &M) {
   if (const NamedMDNode *NMD = M.getNamedMetadata("llvm.ident")) {
     for (unsigned i = 0, e = NMD->getNumOperands(); i != e; ++i) {
       const MDNode *N = NMD->getOperand(i);
-      assert(N->getNumOperands() == 1 && 
+      assert(N->getNumOperands() == 1 &&
              "llvm.ident metadata entry can have only one operand");
       const MDString *S = cast<MDString>(N->getOperand(0));
       OutStreamer.EmitIdent(S->getString());
@@ -1487,7 +1628,7 @@ void AsmPrinter::EmitAlignment(unsigned NumBits, const GlobalValue *GV) const {
   if (getCurrentSection()->getKind().isText())
     OutStreamer.EmitCodeAlignment(1 << NumBits);
   else
-    OutStreamer.EmitValueToAlignment(1 << NumBits, 0, 1, 0);
+    OutStreamer.EmitValueToAlignment(1 << NumBits);
 }
 
 //===----------------------------------------------------------------------===//
@@ -1516,6 +1657,11 @@ static const MCExpr *lowerConstant(const Constant *CV, AsmPrinter &AP) {
     llvm_unreachable("Unknown constant value to lower!");
   }
 
+  if (const MCExpr *RelocExpr =
+          AP.getObjFileLowering().getExecutableRelativeSymbol(CE, *AP.Mang,
+                                                              AP.TM))
+    return RelocExpr;
+
   switch (CE->getOpcode()) {
   default:
     // If the code isn't optimized, there may be outstanding folding
@@ -1531,7 +1677,7 @@ static const MCExpr *lowerConstant(const Constant *CV, AsmPrinter &AP) {
       std::string S;
       raw_string_ostream OS(S);
       OS << "Unsupported expression in static initializer: ";
-      WriteAsOperand(OS, CE, /*PrintType=*/false,
+      CE->printAsOperand(OS, /*PrintType=*/false,
                      !AP.MF ? 0 : AP.MF->getFunction()->getParent());
       report_fatal_error(OS.str());
     }
@@ -1996,14 +2142,16 @@ void AsmPrinter::printOffset(int64_t Offset, raw_ostream &OS) const {
 /// GetTempSymbol - Return the MCSymbol corresponding to the assembler
 /// temporary label with the specified stem and unique ID.
 MCSymbol *AsmPrinter::GetTempSymbol(StringRef Name, unsigned ID) const {
-  return OutContext.GetOrCreateSymbol(Twine(MAI->getPrivateGlobalPrefix()) +
+  const DataLayout *DL = TM.getDataLayout();
+  return OutContext.GetOrCreateSymbol(Twine(DL->getPrivateGlobalPrefix()) +
                                       Name + Twine(ID));
 }
 
 /// GetTempSymbol - Return an assembler temporary label with the specified
 /// stem.
 MCSymbol *AsmPrinter::GetTempSymbol(StringRef Name) const {
-  return OutContext.GetOrCreateSymbol(Twine(MAI->getPrivateGlobalPrefix())+
+  const DataLayout *DL = TM.getDataLayout();
+  return OutContext.GetOrCreateSymbol(Twine(DL->getPrivateGlobalPrefix())+
                                       Name);
 }
 
@@ -2018,8 +2166,9 @@ MCSymbol *AsmPrinter::GetBlockAddressSymbol(const BasicBlock *BB) const {
 
 /// GetCPISymbol - Return the symbol for the specified constant pool entry.
 MCSymbol *AsmPrinter::GetCPISymbol(unsigned CPID) const {
+  const DataLayout *DL = TM.getDataLayout();
   return OutContext.GetOrCreateSymbol
-    (Twine(MAI->getPrivateGlobalPrefix()) + "CPI" + Twine(getFunctionNumber())
+    (Twine(DL->getPrivateGlobalPrefix()) + "CPI" + Twine(getFunctionNumber())
      + "_" + Twine(CPID));
 }
 
@@ -2031,14 +2180,16 @@ MCSymbol *AsmPrinter::GetJTISymbol(unsigned JTID, bool isLinkerPrivate) const {
 /// GetJTSetSymbol - Return the symbol for the specified jump table .set
 /// FIXME: privatize to AsmPrinter.
 MCSymbol *AsmPrinter::GetJTSetSymbol(unsigned UID, unsigned MBBID) const {
+  const DataLayout *DL = TM.getDataLayout();
   return OutContext.GetOrCreateSymbol
-  (Twine(MAI->getPrivateGlobalPrefix()) + Twine(getFunctionNumber()) + "_" +
+  (Twine(DL->getPrivateGlobalPrefix()) + Twine(getFunctionNumber()) + "_" +
    Twine(UID) + "_set_" + Twine(MBBID));
 }
 
 MCSymbol *AsmPrinter::getSymbolWithGlobalValueBase(const GlobalValue *GV,
                                                    StringRef Suffix) const {
-  return getObjFileLowering().getSymbolWithGlobalValueBase(*Mang, GV, Suffix);
+  return getObjFileLowering().getSymbolWithGlobalValueBase(GV, Suffix, *Mang,
+                                                           TM);
 }
 
 /// GetExternalSymbolSymbol - Return the MCSymbol for the specified
@@ -2149,10 +2300,9 @@ void AsmPrinter::EmitBasicBlockStart(const MachineBasicBlock *MBB) const {
 
   // Print the main label for the block.
   if (MBB->pred_empty() || isBlockOnlyReachableByFallthrough(MBB)) {
-    if (isVerbose() && OutStreamer.hasRawTextSupport()) {
+    if (isVerbose()) {
       // NOTE: Want this comment at start of line, don't emit with AddComment.
-      OutStreamer.EmitRawText(Twine(MAI->getCommentString()) + " BB#" +
-                              Twine(MBB->getNumber()) + ":");
+      OutStreamer.emitRawComment(" BB#" + Twine(MBB->getNumber()) + ":", false);
     }
   } else {
     OutStreamer.EmitLabel(MBB->getSymbol());
@@ -2215,14 +2365,13 @@ isBlockOnlyReachableByFallthrough(const MachineBasicBlock *MBB) const {
     if (!MI.isBranch() || MI.isIndirectBranch())
       return false;
 
-    // If we are the operands of one of the branches, this is not
-    // a fall through.
-    for (MachineInstr::mop_iterator OI = MI.operands_begin(),
-           OE = MI.operands_end(); OI != OE; ++OI) {
-      const MachineOperand& OP = *OI;
-      if (OP.isJTI())
+    // If we are the operands of one of the branches, this is not a fall
+    // through. Note that targets with delay slots will usually bundle
+    // terminators with the delay slot instruction.
+    for (ConstMIBundleOperands OP(&MI); OP.isValid(); ++OP) {
+      if (OP->isJTI())
         return false;
-      if (OP.isMBB() && OP.getMBB() == MBB)
+      if (OP->isMBB() && OP->getMBB() == MBB)
         return false;
     }
   }
@@ -2255,3 +2404,6 @@ GCMetadataPrinter *AsmPrinter::GetOrCreateGCPrinter(GCStrategy *S) {
 
   report_fatal_error("no GCMetadataPrinter registered for GC: " + Twine(Name));
 }
+
+/// Pin vtable to this file.
+AsmPrinterHandler::~AsmPrinterHandler() {}