diff --git a/lib/CodeGen/AsmPrinter/AsmPrinterDwarf.cpp b/lib/CodeGen/AsmPrinter/AsmPrinterDwarf.cpp
index 66606caa73dd174577220ccfc4c480c288e53b53..5d6a03080c4f92683052c90bcd544ebb731fb85e 100644 (file)
//===----------------------------------------------------------------------===//
#include "ByteStreamer.h"
+#include "DwarfExpression.h"
#include "llvm/CodeGen/AsmPrinter.h"
-#include "llvm/ADT/SmallBitVector.h"
#include "llvm/ADT/Twine.h"
#include "llvm/IR/DataLayout.h"
#include "llvm/MC/MCAsmInfo.h"
#include "llvm/Target/TargetLoweringObjectFile.h"
#include "llvm/Target/TargetMachine.h"
#include "llvm/Target/TargetRegisterInfo.h"
+#include "llvm/Target/TargetSubtargetInfo.h"
using namespace llvm;
#define DEBUG_TYPE "asm-printer"
+void DebugLocDwarfExpression::EmitOp(uint8_t Op, const char *Comment) {
+ BS.EmitInt8(
+ Op, Comment ? Twine(Comment) + " " + dwarf::OperationEncodingString(Op)
+ : dwarf::OperationEncodingString(Op));
+}
+
+void DebugLocDwarfExpression::EmitSigned(int Value) {
+ BS.EmitSLEB128(Value, Twine(Value));
+}
+
+void DebugLocDwarfExpression::EmitUnsigned(unsigned Value) {
+ BS.EmitULEB128(Value, Twine(Value));
+}
+
+unsigned DebugLocDwarfExpression::getFrameRegister() {
+ llvm_unreachable("not available");
+}
+
//===----------------------------------------------------------------------===//
// Dwarf Emission Helper Routines
//===----------------------------------------------------------------------===//
default:
llvm_unreachable("Invalid encoded value.");
case dwarf::DW_EH_PE_absptr:
- return TM.getDataLayout()->getPointerSize();
+ return TM.getSubtargetImpl()->getDataLayout()->getPointerSize();
case dwarf::DW_EH_PE_udata2:
return 2;
case dwarf::DW_EH_PE_udata4:
EmitLabelDifference(Label, SectionLabel, 4);
}
-/// Emit a dwarf register operation.
-static void emitDwarfRegOp(ByteStreamer &Streamer, int Reg) {
- assert(Reg >= 0);
- if (Reg < 32) {
- Streamer.EmitInt8(dwarf::DW_OP_reg0 + Reg,
- dwarf::OperationEncodingString(dwarf::DW_OP_reg0 + Reg));
- } else {
- Streamer.EmitInt8(dwarf::DW_OP_regx, "DW_OP_regx");
- Streamer.EmitULEB128(Reg, Twine(Reg));
- }
-}
-
-/// Emit an (double-)indirect dwarf register operation.
-static void emitDwarfRegOpIndirect(ByteStreamer &Streamer, int Reg, int Offset,
- bool Deref) {
- assert(Reg >= 0);
- if (Reg < 32) {
- Streamer.EmitInt8(dwarf::DW_OP_breg0 + Reg,
- dwarf::OperationEncodingString(dwarf::DW_OP_breg0 + Reg));
- } else {
- Streamer.EmitInt8(dwarf::DW_OP_bregx, "DW_OP_bregx");
- Streamer.EmitULEB128(Reg, Twine(Reg));
- }
- Streamer.EmitSLEB128(Offset);
- if (Deref)
- Streamer.EmitInt8(dwarf::DW_OP_deref, "DW_OP_deref");
-}
-
-/// Emit a dwarf register operation for describing
-/// - a small value occupying only part of a register or
-/// - a small register representing only part of a value.
-static void emitDwarfOpPiece(ByteStreamer &Streamer, unsigned SizeInBits,
- unsigned OffsetInBits) {
- assert(SizeInBits > 0 && "zero-sized piece");
- unsigned SizeOfByte = 8;
- if (OffsetInBits > 0 || SizeInBits % SizeOfByte) {
- Streamer.EmitInt8(dwarf::DW_OP_bit_piece, "DW_OP_bit_piece");
- Streamer.EmitULEB128(SizeInBits, Twine(SizeInBits));
- Streamer.EmitULEB128(OffsetInBits, Twine(OffsetInBits));
- } else {
- Streamer.EmitInt8(dwarf::DW_OP_piece, "DW_OP_piece");
- unsigned ByteSize = SizeInBits / SizeOfByte;
- Streamer.EmitULEB128(ByteSize, Twine(ByteSize));
- }
-}
-
-/// Emit a shift-right dwarf expression.
-static void emitDwarfOpShr(ByteStreamer &Streamer,
- unsigned ShiftBy) {
- Streamer.EmitInt8(dwarf::DW_OP_constu, "DW_OP_constu");
- Streamer.EmitULEB128(ShiftBy);
- Streamer.EmitInt8(dwarf::DW_OP_shr, "DW_OP_shr");
-}
-
-/// Some targets do not provide a DWARF register number for every
-/// register. This function attempts to emit a DWARF register by
-/// emitting a piece of a super-register or by piecing together
-/// multiple subregisters that alias the register.
+// Some targets do not provide a DWARF register number for every
+// register. This function attempts to emit a DWARF register by
+// emitting a piece of a super-register or by piecing together
+// multiple subregisters that alias the register.
void AsmPrinter::EmitDwarfRegOpPiece(ByteStreamer &Streamer,
const MachineLocation &MLoc,
unsigned PieceSizeInBits,
unsigned PieceOffsetInBits) const {
- assert(!MLoc.isIndirect());
- const TargetRegisterInfo *TRI = TM.getRegisterInfo();
- int Reg = TRI->getDwarfRegNum(MLoc.getReg(), false);
-
- // If this is a valid register number, emit it.
- if (Reg >= 0) {
- emitDwarfRegOp(Streamer, Reg);
- emitDwarfOpPiece(Streamer, PieceSizeInBits, PieceOffsetInBits);
- return;
- }
-
- // Walk up the super-register chain until we find a valid number.
- // For example, EAX on x86_64 is a 32-bit piece of RAX with offset 0.
- for (MCSuperRegIterator SR(MLoc.getReg(), TRI); SR.isValid(); ++SR) {
- Reg = TRI->getDwarfRegNum(*SR, false);
- if (Reg >= 0) {
- unsigned Idx = TRI->getSubRegIndex(*SR, MLoc.getReg());
- unsigned Size = TRI->getSubRegIdxSize(Idx);
- unsigned Offset = TRI->getSubRegIdxOffset(Idx);
- OutStreamer.AddComment("super-register");
- emitDwarfRegOp(Streamer, Reg);
- if (PieceOffsetInBits == Offset) {
- emitDwarfOpPiece(Streamer, Size, Offset);
- } else {
- // If this is part of a variable in a sub-register at a
- // non-zero offset, we need to manually shift the value into
- // place, since the DW_OP_piece describes the part of the
- // variable, not the position of the subregister.
- emitDwarfOpPiece(Streamer, Size, PieceOffsetInBits);
- if (Offset)
- emitDwarfOpShr(Streamer, Offset);
- }
- return;
- }
- }
-
- // Otherwise, attempt to find a covering set of sub-register numbers.
- // For example, Q0 on ARM is a composition of D0+D1.
- //
- // Keep track of the current position so we can emit the more
- // efficient DW_OP_piece.
- unsigned CurPos = PieceOffsetInBits;
- // The size of the register in bits, assuming 8 bits per byte.
- unsigned RegSize = TRI->getMinimalPhysRegClass(MLoc.getReg())->getSize() * 8;
- // Keep track of the bits in the register we already emitted, so we
- // can avoid emitting redundant aliasing subregs.
- SmallBitVector Coverage(RegSize, false);
- for (MCSubRegIterator SR(MLoc.getReg(), TRI); SR.isValid(); ++SR) {
- unsigned Idx = TRI->getSubRegIndex(MLoc.getReg(), *SR);
- unsigned Size = TRI->getSubRegIdxSize(Idx);
- unsigned Offset = TRI->getSubRegIdxOffset(Idx);
- Reg = TRI->getDwarfRegNum(*SR, false);
-
- // Intersection between the bits we already emitted and the bits
- // covered by this subregister.
- SmallBitVector Intersection(RegSize, false);
- Intersection.set(Offset, Offset + Size);
- Intersection ^= Coverage;
-
- // If this sub-register has a DWARF number and we haven't covered
- // its range, emit a DWARF piece for it.
- if (Reg >= 0 && Intersection.any()) {
- OutStreamer.AddComment("sub-register");
- emitDwarfRegOp(Streamer, Reg);
- emitDwarfOpPiece(Streamer, Size, Offset == CurPos ? 0 : Offset);
- CurPos = Offset + Size;
-
- // Mark it as emitted.
- Coverage.set(Offset, Offset + Size);
- }
- }
+ assert(MLoc.isReg() && "MLoc must be a register");
+ DebugLocDwarfExpression Expr(*this, Streamer);
+ Expr.AddMachineRegPiece(MLoc.getReg(), PieceSizeInBits, PieceOffsetInBits);
+}
- if (CurPos == PieceOffsetInBits) {
- // FIXME: We have no reasonable way of handling errors in here.
- Streamer.EmitInt8(dwarf::DW_OP_nop,
- "nop (could not find a dwarf register number)");
- }
+void AsmPrinter::EmitDwarfOpPiece(ByteStreamer &Streamer,
+ unsigned PieceSizeInBits,
+ unsigned PieceOffsetInBits) const {
+ DebugLocDwarfExpression Expr(*this, Streamer);
+ Expr.AddOpPiece(PieceSizeInBits, PieceOffsetInBits);
}
/// EmitDwarfRegOp - Emit dwarf register operation.
void AsmPrinter::EmitDwarfRegOp(ByteStreamer &Streamer,
const MachineLocation &MLoc,
bool Indirect) const {
- const TargetRegisterInfo *TRI = TM.getRegisterInfo();
+ DebugLocDwarfExpression Expr(*this, Streamer);
+ const TargetRegisterInfo *TRI = TM.getSubtargetImpl()->getRegisterInfo();
int Reg = TRI->getDwarfRegNum(MLoc.getReg(), false);
if (Reg < 0) {
// We assume that pointers are always in an addressable register.
- if (Indirect || MLoc.isIndirect()) {
+ if (Indirect || MLoc.isIndirect())
// FIXME: We have no reasonable way of handling errors in here. The
// caller might be in the middle of a dwarf expression. We should
// probably assert that Reg >= 0 once debug info generation is more
// mature.
- Streamer.EmitInt8(dwarf::DW_OP_nop,
- "nop (invalid dwarf register number for indirect loc)");
- return;
- }
+ return Expr.EmitOp(dwarf::DW_OP_nop,
+ "nop (could not find a dwarf register number)");
// Attempt to find a valid super- or sub-register.
- return EmitDwarfRegOpPiece(Streamer, MLoc, 0, 0);
+ return Expr.AddMachineRegPiece(MLoc.getReg());
}
if (MLoc.isIndirect())
- emitDwarfRegOpIndirect(Streamer, Reg, MLoc.getOffset(), Indirect);
+ Expr.AddRegIndirect(Reg, MLoc.getOffset(), Indirect);
else if (Indirect)
- emitDwarfRegOpIndirect(Streamer, Reg, 0, false);
+ Expr.AddRegIndirect(Reg, 0, false);
else
- emitDwarfRegOp(Streamer, Reg);
+ Expr.AddReg(Reg);
}
//===----------------------------------------------------------------------===//