]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - lib/CodeGen/AsmPrinter/AsmPrinterDwarf.cpp
Debug Info: Move support for constants into DwarfExpression.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / AsmPrinterDwarf.cpp
index 94198c4af1780fc631897ade119edf3ea58d7e3a..5d6a03080c4f92683052c90bcd544ebb731fb85e 100644 (file)
@@ -11,7 +11,8 @@
 //
 //===----------------------------------------------------------------------===//
 
-#define DEBUG_TYPE "asm-printer"
+#include "ByteStreamer.h"
+#include "DwarfExpression.h"
 #include "llvm/CodeGen/AsmPrinter.h"
 #include "llvm/ADT/Twine.h"
 #include "llvm/IR/DataLayout.h"
 #include "llvm/Target/TargetLoweringObjectFile.h"
 #include "llvm/Target/TargetMachine.h"
 #include "llvm/Target/TargetRegisterInfo.h"
+#include "llvm/Target/TargetSubtargetInfo.h"
 using namespace llvm;
 
+#define DEBUG_TYPE "asm-printer"
+
+void DebugLocDwarfExpression::EmitOp(uint8_t Op, const char *Comment) {
+  BS.EmitInt8(
+      Op, Comment ? Twine(Comment) + " " + dwarf::OperationEncodingString(Op)
+                  : dwarf::OperationEncodingString(Op));
+}
+
+void DebugLocDwarfExpression::EmitSigned(int Value) {
+  BS.EmitSLEB128(Value, Twine(Value));
+}
+
+void DebugLocDwarfExpression::EmitUnsigned(unsigned Value) {
+  BS.EmitULEB128(Value, Twine(Value));
+}
+
+unsigned DebugLocDwarfExpression::getFrameRegister() {
+ llvm_unreachable("not available");
+}
+
 //===----------------------------------------------------------------------===//
 // Dwarf Emission Helper Routines
 //===----------------------------------------------------------------------===//
@@ -127,7 +149,7 @@ unsigned AsmPrinter::GetSizeOfEncodedValue(unsigned Encoding) const {
   default:
     llvm_unreachable("Invalid encoded value.");
   case dwarf::DW_EH_PE_absptr:
-    return TM.getDataLayout()->getPointerSize();
+    return TM.getSubtargetImpl()->getDataLayout()->getPointerSize();
   case dwarf::DW_EH_PE_udata2:
     return 2;
   case dwarf::DW_EH_PE_udata4:
@@ -143,7 +165,7 @@ void AsmPrinter::EmitTTypeReference(const GlobalValue *GV,
     const TargetLoweringObjectFile &TLOF = getObjFileLowering();
 
     const MCExpr *Exp =
-        TLOF.getTTypeGlobalReference(GV, Encoding, *Mang, MMI, OutStreamer);
+        TLOF.getTTypeGlobalReference(GV, Encoding, *Mang, TM, MMI, OutStreamer);
     OutStreamer.EmitValue(Exp, GetSizeOfEncodedValue(Encoding));
   } else
     OutStreamer.EmitIntValue(0, GetSizeOfEncodedValue(Encoding));
@@ -183,6 +205,55 @@ void AsmPrinter::EmitSectionOffset(const MCSymbol *Label,
   EmitLabelDifference(Label, SectionLabel, 4);
 }
 
+// Some targets do not provide a DWARF register number for every
+// register.  This function attempts to emit a DWARF register by
+// emitting a piece of a super-register or by piecing together
+// multiple subregisters that alias the register.
+void AsmPrinter::EmitDwarfRegOpPiece(ByteStreamer &Streamer,
+                                     const MachineLocation &MLoc,
+                                     unsigned PieceSizeInBits,
+                                     unsigned PieceOffsetInBits) const {
+  assert(MLoc.isReg() && "MLoc must be a register");
+  DebugLocDwarfExpression Expr(*this, Streamer);
+  Expr.AddMachineRegPiece(MLoc.getReg(), PieceSizeInBits, PieceOffsetInBits);
+}
+
+void AsmPrinter::EmitDwarfOpPiece(ByteStreamer &Streamer,
+                                  unsigned PieceSizeInBits,
+                                  unsigned PieceOffsetInBits) const {
+  DebugLocDwarfExpression Expr(*this, Streamer);
+  Expr.AddOpPiece(PieceSizeInBits, PieceOffsetInBits);
+}
+
+/// EmitDwarfRegOp - Emit dwarf register operation.
+void AsmPrinter::EmitDwarfRegOp(ByteStreamer &Streamer,
+                                const MachineLocation &MLoc,
+                                bool Indirect) const {
+  DebugLocDwarfExpression Expr(*this, Streamer);
+  const TargetRegisterInfo *TRI = TM.getSubtargetImpl()->getRegisterInfo();
+  int Reg = TRI->getDwarfRegNum(MLoc.getReg(), false);
+  if (Reg < 0) {
+    // We assume that pointers are always in an addressable register.
+    if (Indirect || MLoc.isIndirect())
+      // FIXME: We have no reasonable way of handling errors in here. The
+      // caller might be in the middle of a dwarf expression. We should
+      // probably assert that Reg >= 0 once debug info generation is more
+      // mature.
+      return Expr.EmitOp(dwarf::DW_OP_nop,
+                         "nop (could not find a dwarf register number)");
+
+    // Attempt to find a valid super- or sub-register.
+    return Expr.AddMachineRegPiece(MLoc.getReg());
+  }
+
+  if (MLoc.isIndirect())
+    Expr.AddRegIndirect(Reg, MLoc.getOffset(), Indirect);
+  else if (Indirect)
+    Expr.AddRegIndirect(Reg, 0, false);
+  else
+    Expr.AddReg(Reg);
+}
+
 //===----------------------------------------------------------------------===//
 // Dwarf Lowering Routines
 //===----------------------------------------------------------------------===//
@@ -209,5 +280,8 @@ void AsmPrinter::emitCFIInstruction(const MCCFIInstruction &Inst) const {
   case MCCFIInstruction::OpWindowSave:
     OutStreamer.EmitCFIWindowSave();
     break;
+  case MCCFIInstruction::OpSameValue:
+    OutStreamer.EmitCFISameValue(Inst.getRegister());
+    break;
   }
 }