diff --git a/lib/CodeGen/AsmPrinter/DbgValueHistoryCalculator.cpp b/lib/CodeGen/AsmPrinter/DbgValueHistoryCalculator.cpp
index 998c396924bc38d5872653019485f7f0c09ec59b..a258d621a6a01470633d2ee77615f5a26f62fec8 100644 (file)
// In the other case, returns 0.
static unsigned isDescribedByReg(const MachineInstr &MI) {
assert(MI.isDebugValue());
- assert(MI.getNumOperands() == 3);
+ assert(MI.getNumOperands() == 4);
// If location of variable is described using a register (directly or
// indirecltly), this register is always a first operand.
return MI.getOperand(0).isReg() ? MI.getOperand(0).getReg() : 0;
const MachineInstr &MI) {
// Instruction range should start with a DBG_VALUE instruction for the
// variable.
- assert(MI.isDebugValue() && getEntireVariable(MI.getDebugVariable()) == Var);
+ assert(MI.isDebugValue() && "not a DBG_VALUE");
auto &Ranges = VarInstrRanges[Var];
if (!Ranges.empty() && Ranges.back().second == nullptr &&
Ranges.back().first->isIdenticalTo(&MI)) {
// Use the base variable (without any DW_OP_piece expressions)
// as index into History. The full variables including the
// piece expressions are attached to the MI.
- DIVariable Var = getEntireVariable(MI.getDebugVariable());
+ DIVariable Var = MI.getDebugVariable();
if (unsigned PrevReg = Result.getRegisterForVar(Var))
dropRegDescribedVar(RegVars, PrevReg, Var);