]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - lib/CodeGen/AsmPrinter/DwarfCompileUnit.cpp
Debug Info: Don't bother emitting DW_AT_frame_base if the function has
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfCompileUnit.cpp
index 1bb546e54b2e9ba8a19b4a63e2f018cffc0cbced..fe01980c812f71b68ee1305ec9ecad0fe99a57ed 100644 (file)
@@ -283,7 +283,7 @@ void DwarfCompileUnit::attachLowHighPC(DIE &D, const MCSymbol *Begin,
 // and DW_AT_high_pc attributes. If there are global variables in this
 // scope then create and insert DIEs for these variables.
 DIE &DwarfCompileUnit::updateSubprogramScopeDIE(DISubprogram SP) {
-  DIE *SPDie = getOrCreateSubprogramDIE(SP);
+  DIE *SPDie = getOrCreateSubprogramDIE(SP, includeMinimalInlineScopes());
 
   attachLowHighPC(*SPDie, DD->getFunctionBeginSym(), DD->getFunctionEndSym());
   if (!DD->getCurrentFunction()->getTarget().Options.DisableFramePointerElim(
@@ -291,11 +291,12 @@ DIE &DwarfCompileUnit::updateSubprogramScopeDIE(DISubprogram SP) {
     addFlag(*SPDie, dwarf::DW_AT_APPLE_omit_frame_ptr);
 
   // Only include DW_AT_frame_base in full debug info
-  if (getCUNode().getEmissionKind() != DIBuilder::LineTablesOnly) {
+  if (!includeMinimalInlineScopes()) {
     const TargetRegisterInfo *RI =
         Asm->TM.getSubtargetImpl()->getRegisterInfo();
     MachineLocation Location(RI->getFrameRegister(*Asm->MF));
-    addAddress(*SPDie, dwarf::DW_AT_frame_base, Location);
+    if (RI->isPhysicalRegister(Location.getReg()))
+      addAddress(*SPDie, dwarf::DW_AT_frame_base, Location);
   }
 
   // Add name to the name table, we do this here because we're guaranteed
@@ -341,10 +342,14 @@ void DwarfCompileUnit::constructScopeDIE(
     // null and the children will be added to the scope DIE.
     createScopeChildrenDIE(Scope, Children, &ChildScopeCount);
 
-    // There is no need to emit empty lexical block DIE.
-    for (const auto &E : DD->findImportedEntitiesForScope(DS))
-      Children.push_back(
-          constructImportedEntityDIE(DIImportedEntity(E.second)));
+    // Skip imported directives in gmlt-like data.
+    if (!includeMinimalInlineScopes()) {
+      // There is no need to emit empty lexical block DIE.
+      for (const auto &E : DD->findImportedEntitiesForScope(DS))
+        Children.push_back(
+            constructImportedEntityDIE(DIImportedEntity(E.second)));
+    }
+
     // If there are only other scopes as children, put them directly in the
     // parent instead, as this scope would serve no purpose.
     if (Children.size() == ChildScopeCount) {
@@ -372,40 +377,46 @@ void DwarfCompileUnit::addSectionDelta(DIE &Die, dwarf::Attribute Attribute,
                Value);
 }
 
-void
-DwarfCompileUnit::addScopeRangeList(DIE &ScopeDIE,
-                                    const SmallVectorImpl<InsnRange> &Range) {
+void DwarfCompileUnit::addScopeRangeList(DIE &ScopeDIE,
+                                         SmallVector<RangeSpan, 2> Range) {
   // Emit offset in .debug_range as a relocatable label. emitDIE will handle
   // emitting it appropriately.
-  MCSymbol *RangeSym =
-      Asm->GetTempSymbol("debug_ranges", DD->getNextRangeNumber());
-
   auto *RangeSectionSym = DD->getRangeSectionSym();
 
+  RangeSpanList List(
+      Asm->GetTempSymbol("debug_ranges", DD->getNextRangeNumber()),
+      std::move(Range));
+
   // Under fission, ranges are specified by constant offsets relative to the
   // CU's DW_AT_GNU_ranges_base.
-  if (DD->useSplitDwarf())
-    addSectionDelta(ScopeDIE, dwarf::DW_AT_ranges, RangeSym, RangeSectionSym);
+  if (isDwoUnit())
+    addSectionDelta(ScopeDIE, dwarf::DW_AT_ranges, List.getSym(),
+                    RangeSectionSym);
   else
-    addSectionLabel(ScopeDIE, dwarf::DW_AT_ranges, RangeSym, RangeSectionSym);
-
-  RangeSpanList List(RangeSym);
-  for (const InsnRange &R : Range)
-    List.addRange(RangeSpan(DD->getLabelBeforeInsn(R.first),
-                            DD->getLabelAfterInsn(R.second)));
+    addSectionLabel(ScopeDIE, dwarf::DW_AT_ranges, List.getSym(),
+                    RangeSectionSym);
 
   // Add the range list to the set of ranges to be emitted.
   (Skeleton ? Skeleton : this)->CURangeLists.push_back(std::move(List));
 }
 
+void DwarfCompileUnit::attachRangesOrLowHighPC(
+    DIE &Die, SmallVector<RangeSpan, 2> Ranges) {
+  if (Ranges.size() == 1) {
+    const auto &single = Ranges.front();
+    attachLowHighPC(Die, single.getStart(), single.getEnd());
+  } else
+    addScopeRangeList(Die, std::move(Ranges));
+}
+
 void DwarfCompileUnit::attachRangesOrLowHighPC(
     DIE &Die, const SmallVectorImpl<InsnRange> &Ranges) {
-  assert(!Ranges.empty());
-  if (Ranges.size() == 1)
-    attachLowHighPC(Die, DD->getLabelBeforeInsn(Ranges.front().first),
-                    DD->getLabelAfterInsn(Ranges.front().second));
-  else
-    addScopeRangeList(Die, Ranges);
+  SmallVector<RangeSpan, 2> List;
+  List.reserve(Ranges.size());
+  for (const InsnRange &R : Ranges)
+    List.push_back(RangeSpan(DD->getLabelBeforeInsn(R.first),
+                             DD->getLabelAfterInsn(R.second)));
+  attachRangesOrLowHighPC(Die, std::move(List));
 }
 
 // This scope represents inlined body of a function. Construct DIE to
@@ -570,7 +581,8 @@ void DwarfCompileUnit::constructSubprogramScopeDIE(LexicalScope *Scope) {
   // If we have more than one elements and the last one is null, it is a
   // variadic function.
   if (FnArgs.getNumElements() > 1 &&
-      !FnArgs.getElement(FnArgs.getNumElements() - 1))
+      !FnArgs.getElement(FnArgs.getNumElements() - 1) &&
+      !includeMinimalInlineScopes())
     ScopeDIE.addChild(make_unique<DIE>(dwarf::DW_TAG_unspecified_parameters));
 }
 
@@ -597,11 +609,13 @@ DwarfCompileUnit::constructAbstractSubprogramScopeDIE(LexicalScope *Scope) {
 
   DIE *ContextDIE;
 
+  if (includeMinimalInlineScopes())
+    ContextDIE = &getUnitDie();
   // Some of this is duplicated from DwarfUnit::getOrCreateSubprogramDIE, with
   // the important distinction that the DIDescriptor is not associated with the
   // DIE (since the DIDescriptor will be associated with the concrete DIE, if
   // any). It could be refactored to some common utility function.
-  if (DISubprogram SPDecl = SP.getFunctionDeclaration()) {
+  else if (DISubprogram SPDecl = SP.getFunctionDeclaration()) {
     ContextDIE = &getUnitDie();
     getOrCreateSubprogramDIE(SPDecl);
   } else
@@ -613,7 +627,7 @@ DwarfCompileUnit::constructAbstractSubprogramScopeDIE(LexicalScope *Scope) {
       &createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE, DIDescriptor());
   applySubprogramAttributesToDefinition(SP, *AbsDef);
 
-  if (getCUNode().getEmissionKind() != DIBuilder::LineTablesOnly)
+  if (!includeMinimalInlineScopes())
     addUInt(*AbsDef, dwarf::DW_AT_inline, None, dwarf::DW_INL_inlined);
   if (DIE *ObjectPointer = createAndAddScopeChildren(Scope, *AbsDef))
     addDIEEntry(*AbsDef, dwarf::DW_AT_object_pointer, *ObjectPointer);
@@ -633,6 +647,8 @@ DwarfCompileUnit::constructImportedEntityDIE(const DIImportedEntity &Module) {
     EntityDie = getOrCreateSubprogramDIE(DISubprogram(Entity));
   else if (Entity.isType())
     EntityDie = getOrCreateTypeDIE(DIType(Entity));
+  else if (Entity.isGlobalVariable())
+    EntityDie = getOrCreateGlobalVariableDIE(DIGlobalVariable(Entity));
   else
     EntityDie = getDIE(Entity);
   assert(EntityDie);
@@ -654,7 +670,7 @@ void DwarfCompileUnit::finishSubprogramDefinition(DISubprogram SP) {
       // If this subprogram has an abstract definition, reference that
       addDIEEntry(*D, dwarf::DW_AT_abstract_origin, *AbsSPDIE);
   } else {
-    if (!D && getCUNode().getEmissionKind() != DIBuilder::LineTablesOnly)
+    if (!D && !includeMinimalInlineScopes())
       // Lazily construct the subprogram if we didn't see either concrete or
       // inlined versions during codegen. (except in -gmlt ^ where we want
       // to omit these entirely)
@@ -697,7 +713,7 @@ void DwarfCompileUnit::emitHeader(const MCSymbol *ASectionSym) const {
 /// addGlobalName - Add a new global name to the compile unit.
 void DwarfCompileUnit::addGlobalName(StringRef Name, DIE &Die,
                                      DIScope Context) {
-  if (getCUNode().getEmissionKind() == DIBuilder::LineTablesOnly)
+  if (includeMinimalInlineScopes())
     return;
   std::string FullName = getParentContextString(Context) + Name.str();
   GlobalNames[FullName] = &Die;
@@ -706,7 +722,7 @@ void DwarfCompileUnit::addGlobalName(StringRef Name, DIE &Die,
 /// Add a new global type to the unit.
 void DwarfCompileUnit::addGlobalType(DIType Ty, const DIE &Die,
                                      DIScope Context) {
-  if (getCUNode().getEmissionKind() == DIBuilder::LineTablesOnly)
+  if (includeMinimalInlineScopes())
     return;
   std::string FullName = getParentContextString(Context) + Ty.getName().str();
   GlobalTypes[FullName] = &Die;
@@ -731,14 +747,17 @@ void DwarfCompileUnit::addAddress(DIE &Die, dwarf::Attribute Attribute,
                                   bool Indirect) {
   DIELoc *Loc = new (DIEValueAllocator) DIELoc();
 
+  bool validReg;
   if (Location.isReg() && !Indirect)
-    addRegisterOpPiece(*Loc, Location.getReg());
-  else {
-    addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
-    if (Indirect && !Location.isReg()) {
-      addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
-    }
-  }
+    validReg = addRegisterOpPiece(*Loc, Location.getReg());
+  else
+    validReg = addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
+
+  if (!validReg)
+    return;
+
+  if (!Location.isReg() && Indirect)
+    addUInt(*Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
 
   // Now attach the location information to the DIE.
   addBlock(Die, Attribute, Loc);
@@ -754,25 +773,29 @@ void DwarfCompileUnit::addComplexAddress(const DbgVariable &DV, DIE &Die,
   DIELoc *Loc = new (DIEValueAllocator) DIELoc();
   unsigned N = DV.getNumAddrElements();
   unsigned i = 0;
+  bool validReg;
   if (Location.isReg()) {
     if (N >= 2 && DV.getAddrElement(0) == dwarf::DW_OP_plus) {
       assert(!DV.getVariable().isIndirect() &&
              "double indirection not handled");
       // If first address element is OpPlus then emit
       // DW_OP_breg + Offset instead of DW_OP_reg + Offset.
-      addRegisterOffset(*Loc, Location.getReg(), DV.getAddrElement(1));
+      validReg = addRegisterOffset(*Loc, Location.getReg(), DV.getAddrElement(1));
       i = 2;
     } else if (N >= 2 && DV.getAddrElement(0) == dwarf::DW_OP_deref) {
       assert(!DV.getVariable().isIndirect() &&
              "double indirection not handled");
-      addRegisterOpPiece(*Loc, Location.getReg(),
-                         DV.getExpression().getPieceSize(),
-                         DV.getExpression().getPieceOffset());
+      validReg = addRegisterOpPiece(*Loc, Location.getReg(),
+                                 DV.getExpression().getPieceSize(),
+                                 DV.getExpression().getPieceOffset());
       i = 3;
     } else
-      addRegisterOpPiece(*Loc, Location.getReg());
+      validReg = addRegisterOpPiece(*Loc, Location.getReg());
   } else
-    addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
+    validReg = addRegisterOffset(*Loc, Location.getReg(), Location.getOffset());
+
+  if (!validReg)
+    return;
 
   for (; i < N; ++i) {
     uint64_t Element = DV.getAddrElement(i);
@@ -832,12 +855,16 @@ void DwarfCompileUnit::applySubprogramAttributesToDefinition(DISubprogram SP,
                                                              DIE &SPDie) {
   DISubprogram SPDecl = SP.getFunctionDeclaration();
   DIScope Context = resolve(SPDecl ? SPDecl.getContext() : SP.getContext());
-  applySubprogramAttributes(SP, SPDie, getCUNode().getEmissionKind() ==
-                                           DIBuilder::LineTablesOnly);
+  applySubprogramAttributes(SP, SPDie, includeMinimalInlineScopes());
   addGlobalName(SP.getName(), SPDie, Context);
 }
 
 bool DwarfCompileUnit::isDwoUnit() const {
   return DD->useSplitDwarf() && Skeleton;
 }
+
+bool DwarfCompileUnit::includeMinimalInlineScopes() const {
+  return getCUNode().getEmissionKind() == DIBuilder::LineTablesOnly ||
+         (DD->useSplitDwarf() && !Skeleton);
+}
 } // end llvm namespace