index afd53293fe3feb54cb1d524b4df29f8033f5712a..967c7b1b5964228e04983602962e33e1201eb909 100644 (file)
// scope then create and insert DIEs for these variables.
DIE &DwarfDebug::updateSubprogramScopeDIE(DwarfCompileUnit &SPCU,
DISubprogram SP) {
- DIE *SPDie = SPCU.getDIE(SP);
-
- assert(SPDie && "Unable to find subprogram DIE!");
-
- // If we're updating an abstract DIE, then we will be adding the children and
- // object pointer later on. But what we don't want to do is process the
- // concrete DIE twice.
- if (DIE *AbsSPDIE = AbstractSPDies.lookup(SP)) {
- // Pick up abstract subprogram DIE.
- SPDie = &SPCU.createAndAddDIE(dwarf::DW_TAG_subprogram, SPCU.getUnitDie());
- SPCU.addDIEEntry(*SPDie, dwarf::DW_AT_abstract_origin, *AbsSPDIE);
- } else if (!SP.getFunctionDeclaration()) {
- // There is not any need to generate specification DIE for a function
- // defined at compile unit level. If a function is defined inside another
- // function then gdb prefers the definition at top level and but does not
- // expect specification DIE in parent function. So avoid creating
- // specification DIE for a function defined inside a function.
- DIScope SPContext = resolve(SP.getContext());
- if (SP.isDefinition() && !SPContext.isCompileUnit() &&
- !SPContext.isFile() && !isSubprogramContext(SPContext)) {
- SPCU.addFlag(*SPDie, dwarf::DW_AT_declaration);
-
- // Add arguments.
- DICompositeType SPTy = SP.getType();
- DIArray Args = SPTy.getTypeArray();
- uint16_t SPTag = SPTy.getTag();
- if (SPTag == dwarf::DW_TAG_subroutine_type)
- SPCU.constructSubprogramArguments(*SPDie, Args);
- DIE *SPDeclDie = SPDie;
- SPDie =
- &SPCU.createAndAddDIE(dwarf::DW_TAG_subprogram, SPCU.getUnitDie());
- SPCU.addDIEEntry(*SPDie, dwarf::DW_AT_specification, *SPDeclDie);
- }
- }
+ DIE *SPDie = SPCU.getOrCreateSubprogramDIE(SP);
attachLowHighPC(SPCU, *SPDie, FunctionBeginSym, FunctionEndSym);
assert(Scope->getScopeNode());
DIScope DS(Scope->getScopeNode());
DISubprogram InlinedSP = getDISubprogram(DS);
- DIE *OriginDIE = TheCU.getDIE(InlinedSP);
- // FIXME: This should be an assert (or possibly a
- // getOrCreateSubprogram(InlinedSP)) otherwise we're just failing to emit
- // inlining information.
- if (!OriginDIE) {
- DEBUG(dbgs() << "Unable to find original DIE for an inlined subprogram.");
- return nullptr;
- }
+ // Find the subprogram's DwarfCompileUnit in the SPMap in case the subprogram
+ // was inlined from another compile unit.
+ DIE *OriginDIE = AbstractSPDies[InlinedSP];
+ assert(OriginDIE && "Unable to find original DIE for an inlined subprogram.");
auto ScopeDIE = make_unique<DIE>(dwarf::DW_TAG_inlined_subroutine);
TheCU.addDIEEntry(*ScopeDIE, dwarf::DW_AT_abstract_origin, *OriginDIE);
attachRangesOrLowHighPC(TheCU, *ScopeDIE, Scope->getRanges());
InlinedSubprogramDIEs.insert(OriginDIE);
- TheCU.addUInt(*OriginDIE, dwarf::DW_AT_inline, None, dwarf::DW_INL_inlined);
// Add the call site information to the DIE.
DILocation DL(Scope->getInlinedAt());
DbgVariable &DV,
const LexicalScope &Scope,
DIE *&ObjectPointer) {
- AbstractOrInlined AOI = AOI_None;
- if (Scope.isAbstractScope())
- AOI = AOI_Abstract;
- else if (Scope.getInlinedAt())
- AOI = AOI_Inlined;
- auto Var = TheCU.constructVariableDIE(DV, AOI);
+ auto Var = TheCU.constructVariableDIE(DV, Scope.isAbstractScope());
if (DV.isObjectPointer())
ObjectPointer = Var.get();
return Var;
assert(Scope->isAbstractScope());
assert(!Scope->getInlinedAt());
- DISubprogram Sub(Scope->getScopeNode());
+ DISubprogram SP(Scope->getScopeNode());
+
+ ProcessedSPNodes.insert(SP);
- if (!ProcessedSPNodes.insert(Sub))
+ DIE *&AbsDef = AbstractSPDies[SP];
+ if (AbsDef)
return;
- if (DIE *ScopeDIE = TheCU.getDIE(Sub)) {
- AbstractSPDies.insert(std::make_pair(Sub, ScopeDIE));
- TheCU.addUInt(*ScopeDIE, dwarf::DW_AT_inline, None, dwarf::DW_INL_inlined);
- createAndAddScopeChildren(TheCU, Scope, *ScopeDIE);
- }
+ // Find the subprogram's DwarfCompileUnit in the SPMap in case the subprogram
+ // was inlined from another compile unit.
+ DwarfCompileUnit &SPCU = *SPMap[SP];
+ DIE *ContextDIE;
+
+ // Some of this is duplicated from DwarfUnit::getOrCreateSubprogramDIE, with
+ // the important distinction that the DIDescriptor is not associated with the
+ // DIE (since the DIDescriptor will be associated with the concrete DIE, if
+ // any). It could be refactored to some common utility function.
+ if (DISubprogram SPDecl = SP.getFunctionDeclaration()) {
+ ContextDIE = &SPCU.getUnitDie();
+ SPCU.getOrCreateSubprogramDIE(SPDecl);
+ } else
+ ContextDIE = SPCU.getOrCreateContextDIE(resolve(SP.getContext()));
+
+ // Passing null as the associated DIDescriptor because the abstract definition
+ // shouldn't be found by lookup.
+ AbsDef = &SPCU.createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE,
+ DIDescriptor());
+ SPCU.applySubprogramAttributes(SP, *AbsDef);
+ SPCU.addGlobalName(SP.getName(), *AbsDef, resolve(SP.getContext()));
+
+ SPCU.addUInt(*AbsDef, dwarf::DW_AT_inline, None, dwarf::DW_INL_inlined);
+ createAndAddScopeChildren(SPCU, Scope, *AbsDef);
}
DIE &DwarfDebug::constructSubprogramScopeDIE(DwarfCompileUnit &TheCU,
// avoid creating un-used children then removing them later when we find out
// the scope DIE is null.
std::unique_ptr<DIE> ScopeDIE;
- if (DS.getContext() && DS.isSubprogram()) {
+ if (Scope->getParent() && DS.isSubprogram()) {
ScopeDIE = constructInlinedScopeDIE(TheCU, Scope);
if (!ScopeDIE)
return nullptr;
@@ -704,31 +683,6 @@ DwarfCompileUnit &DwarfDebug::constructDwarfCompileUnit(DICompileUnit DIUnit) {
return NewCU;
}
-// Construct subprogram DIE.
-void DwarfDebug::constructSubprogramDIE(DwarfCompileUnit &TheCU,
- const MDNode *N) {
- // FIXME: We should only call this routine once, however, during LTO if a
- // program is defined in multiple CUs we could end up calling it out of
- // beginModule as we walk the CUs.
-
- DwarfCompileUnit *&CURef = SPMap[N];
- if (CURef)
- return;
- CURef = &TheCU;
-
- DISubprogram SP(N);
- assert(SP.isSubprogram());
- if (!SP.isDefinition())
- // This is a method declaration which will be handled while constructing
- // class type.
- return;
-
- DIE &SubprogramDie = *TheCU.getOrCreateSubprogramDIE(SP);
-
- // Expose as a global name.
- TheCU.addGlobalName(SP.getName(), SubprogramDie, resolve(SP.getContext()));
-}
-
void DwarfDebug::constructImportedEntityDIE(DwarfCompileUnit &TheCU,
const MDNode *N) {
DIImportedEntity Module(N);
CU.createGlobalVariableDIE(DIGlobalVariable(GVs.getElement(i)));
DIArray SPs = CUNode.getSubprograms();
for (unsigned i = 0, e = SPs.getNumElements(); i != e; ++i)
- constructSubprogramDIE(CU, SPs.getElement(i));
+ SPMap.insert(std::make_pair(SPs.getElement(i), &CU));
DIArray EnumTypes = CUNode.getEnumTypes();
for (unsigned i = 0, e = EnumTypes.getNumElements(); i != e; ++i)
CU.getOrCreateTypeDIE(EnumTypes.getElement(i));
SectionMap[Asm->getObjFileLowering().getTextSection()];
}
+void DwarfDebug::finishSubprogramDefinitions() {
+ const Module *M = MMI->getModule();
+
+ NamedMDNode *CU_Nodes = M->getNamedMetadata("llvm.dbg.cu");
+ for (MDNode *N : CU_Nodes->operands()) {
+ DICompileUnit TheCU(N);
+ // Construct subprogram DIE and add variables DIEs.
+ DwarfCompileUnit *SPCU =
+ static_cast<DwarfCompileUnit *>(CUMap.lookup(TheCU));
+ DIArray Subprograms = TheCU.getSubprograms();
+ for (unsigned i = 0, e = Subprograms.getNumElements(); i != e; ++i) {
+ DISubprogram SP(Subprograms.getElement(i));
+ // Perhaps the subprogram is in another CU (such as due to comdat
+ // folding, etc), in which case ignore it here.
+ if (SPMap[SP] != SPCU)
+ continue;
+ DIE *D = SPCU->getDIE(SP);
+ if (DIE *AbsSPDIE = AbstractSPDies.lookup(SP)) {
+ if (D)
+ // If this subprogram has an abstract definition, reference that
+ SPCU->addDIEEntry(*D, dwarf::DW_AT_abstract_origin, *AbsSPDIE);
+ } else {
+ if (!D)
+ // Lazily construct the subprogram if we didn't see either concrete or
+ // inlined versions during codegen.
+ D = SPCU->getOrCreateSubprogramDIE(SP);
+ // And attach the attributes
+ SPCU->applySubprogramAttributes(SP, *D);
+ SPCU->addGlobalName(SP.getName(), *D, resolve(SP.getContext()));
+ }
+ }
+ }
+}
+
+
// Collect info for variables that were optimized out.
void DwarfDebug::collectDeadVariables() {
const Module *M = MMI->getModule();
continue;
assert(SP.isSubprogram() &&
"CU's subprogram list contains a non-subprogram");
- if (!SP.isDefinition())
- continue;
+ assert(SP.isDefinition() &&
+ "CU's subprogram list contains a subprogram declaration");
DIArray Variables = SP.getVariables();
if (Variables.getNumElements() == 0)
continue;
- // FIXME: See the comment in constructSubprogramDIE about duplicate
- // subprogram DIEs.
- constructSubprogramDIE(*SPCU, SP);
- DIE *SPDIE = SPCU->getDIE(SP);
+ DIE *SPDIE = AbstractSPDies.lookup(SP);
+ if (!SPDIE)
+ SPDIE = SPCU->getDIE(SP);
+ assert(SPDIE);
for (unsigned vi = 0, ve = Variables.getNumElements(); vi != ve; ++vi) {
DIVariable DV(Variables.getElement(vi));
assert(DV.isVariable());
}
void DwarfDebug::finalizeModuleInfo() {
+ finishSubprogramDefinitions();
+
// Collect info for variables that were optimized out.
collectDeadVariables();
// clean up.
SPMap.clear();
+ AbstractVariables.clear();
// Reset these for the next Module if we have one.
FirstCU = nullptr;
// Find abstract variable, if any, associated with Var.
DbgVariable *DwarfDebug::findAbstractVariable(DIVariable &DV,
DebugLoc ScopeLoc) {
+ return findAbstractVariable(DV, ScopeLoc.getScope(DV->getContext()));
+}
+
+DbgVariable *DwarfDebug::findAbstractVariable(DIVariable &DV,
+ const MDNode *ScopeNode) {
LLVMContext &Ctx = DV->getContext();
// More then one inlined variable corresponds to one abstract variable.
DIVariable Var = cleanseInlinedVariable(DV, Ctx);
- DbgVariable *AbsDbgVariable = AbstractVariables.lookup(Var);
- if (AbsDbgVariable)
- return AbsDbgVariable;
+ auto I = AbstractVariables.find(Var);
+ if (I != AbstractVariables.end())
+ return I->second.get();
- LexicalScope *Scope = LScopes.findAbstractScope(ScopeLoc.getScope(Ctx));
+ LexicalScope *Scope = LScopes.findAbstractScope(ScopeNode);
if (!Scope)
return nullptr;
- AbsDbgVariable = new DbgVariable(Var, nullptr, this);
- addScopeVariable(Scope, AbsDbgVariable);
- AbstractVariables[Var] = AbsDbgVariable;
- return AbsDbgVariable;
+ auto AbsDbgVariable = make_unique<DbgVariable>(Var, nullptr, this);
+ addScopeVariable(Scope, AbsDbgVariable.get());
+ return (AbstractVariables[Var] = std::move(AbsDbgVariable)).get();
}
// If Var is a current function argument then add it to CurrentFnArguments list.
@@ -1226,10 +1222,10 @@ DwarfDebug::collectVariableInfo(SmallPtrSet<const MDNode *, 16> &Processed) {
const MachineInstr *End = HI[1];
DEBUG(dbgs() << "DotDebugLoc Pair:\n"
<< "\t" << *Begin << "\t" << *End << "\n");
- if (End->isDebugValue())
+ if (End->isDebugValue() && End->getDebugVariable() == DV)
SLabel = getLabelBeforeInsn(End);
else {
- // End is a normal instruction clobbering the range.
+ // End is clobbering the range.
SLabel = getLabelAfterInsn(End);
assert(SLabel && "Forgot label after clobber instruction");
++HI;
@@ -1251,7 +1247,10 @@ DwarfDebug::collectVariableInfo(SmallPtrSet<const MDNode *, 16> &Processed) {
if (!Processed.insert(DV))
continue;
if (LexicalScope *Scope = LScopes.findLexicalScope(DV.getContext()))
- addScopeVariable(Scope, new DbgVariable(DV, nullptr, this));
+ addScopeVariable(
+ Scope,
+ new DbgVariable(DV, findAbstractVariable(DV, Scope->getScopeNode()),
+ this));
}
}
LabelsBeforeInsn[History.front()] = FunctionBeginSym;
for (const MachineInstr *MI : History) {
- if (MI->isDebugValue())
+ if (MI->isDebugValue() && MI->getDebugVariable() == DV)
requestLabelBeforeInsn(MI);
else
requestLabelAfterInsn(MI);
assert(DV && DV.isVariable());
if (!ProcessedVars.insert(DV))
continue;
- // Check that DbgVariable for DV wasn't created earlier, when
- // findAbstractVariable() was called for inlined instance of DV.
- LLVMContext &Ctx = DV->getContext();
- DIVariable CleanDV = cleanseInlinedVariable(DV, Ctx);
- if (AbstractVariables.lookup(CleanDV))
- continue;
- if (LexicalScope *Scope = LScopes.findAbstractScope(DV.getContext()))
- addScopeVariable(Scope, new DbgVariable(DV, nullptr, this));
+ findAbstractVariable(DV, DV.getContext());
}
constructAbstractSubprogramScopeDIE(TheCU, AScope);
}
PrevCU = &TheCU;
// Clear debug info
- for (auto &I : ScopeVariables)
- DeleteContainerPointers(I.second);
+ // Ownership of DbgVariables is a bit subtle - ScopeVariables owns all the
+ // DbgVariables except those that are also in AbstractVariables (since they
+ // can be used cross-function)
+ for (const auto &I : ScopeVariables)
+ for (const auto *Var : I.second)
+ if (!AbstractVariables.count(Var->getVariable()) || Var->getAbstractVariable())
+ delete Var;
ScopeVariables.clear();
DeleteContainerPointers(CurrentFnArguments);
DbgValues.clear();
- AbstractVariables.clear();
LabelsBeforeInsn.clear();
LabelsAfterInsn.clear();
PrevLabel = nullptr;
// Dwarf sections base addresses.
DwarfInfoSectionSym =
emitSectionSym(Asm, TLOF.getDwarfInfoSection(), "section_info");
- if (useSplitDwarf()) {
+ if (useSplitDwarf())
DwarfInfoDWOSectionSym =
emitSectionSym(Asm, TLOF.getDwarfInfoDWOSection(), "section_info_dwo");
- DwarfTypesDWOSectionSym =
- emitSectionSym(Asm, TLOF.getDwarfTypesDWOSection(), "section_types_dwo");
- }
DwarfAbbrevSectionSym =
emitSectionSym(Asm, TLOF.getDwarfAbbrevSection(), "section_abbrev");
if (useSplitDwarf())
bool TopLevelType = TypeUnitsUnderConstruction.empty();
AddrPool.resetUsedFlag();
- auto OwnedUnit = make_unique<DwarfTypeUnit>(
- InfoHolder.getUnits().size() + TypeUnitsUnderConstruction.size(), CU, Asm,
- this, &InfoHolder, getDwoLineTable(CU));
+ auto OwnedUnit =
+ make_unique<DwarfTypeUnit>(InfoHolder.getUnits().size(), CU, Asm, this,
+ &InfoHolder, getDwoLineTable(CU));
DwarfTypeUnit &NewTU = *OwnedUnit;
DIE &UnitDie = NewTU.getUnitDie();
TU = &NewTU;
uint64_t Signature = makeTypeSignature(Identifier);
NewTU.setTypeSignature(Signature);
- if (useSplitDwarf())
- NewTU.initSection(Asm->getObjFileLowering().getDwarfTypesDWOSection(),
- DwarfTypesDWOSectionSym);
- else {
+ if (!useSplitDwarf())
CU.applyStmtList(UnitDie);
- NewTU.initSection(
- Asm->getObjFileLowering().getDwarfTypesSection(Signature));
- }
+
+ // FIXME: Skip using COMDAT groups for type units in the .dwo file once tools
+ // such as DWP ( http://gcc.gnu.org/wiki/DebugFissionDWP ) can cope with it.
+ NewTU.initSection(
+ useSplitDwarf()
+ ? Asm->getObjFileLowering().getDwarfTypesDWOSection(Signature)
+ : Asm->getObjFileLowering().getDwarfTypesSection(Signature));
NewTU.setType(NewTU.createTypeDIE(CTy));