index 5f2d15e257ec9d979fd029a2a849d7b6b369bc86..99f4d1c5d446545cb4e633dca88ce58d75744ced 100644 (file)
#include "DwarfDebug.h"
#include "ByteStreamer.h"
+#include "DwarfExpression.h"
#include "DwarfCompileUnit.h"
-#include "DIE.h"
#include "DIEHash.h"
#include "DwarfUnit.h"
#include "llvm/ADT/STLExtras.h"
#include "llvm/ADT/Statistic.h"
#include "llvm/ADT/StringExtras.h"
#include "llvm/ADT/Triple.h"
+#include "llvm/CodeGen/DIE.h"
#include "llvm/CodeGen/MachineFunction.h"
#include "llvm/CodeGen/MachineModuleInfo.h"
#include "llvm/IR/Constants.h"
DwarfAccelTable::Atom(dwarf::DW_ATOM_type_flags, dwarf::DW_FORM_data1)};
DwarfDebug::DwarfDebug(AsmPrinter *A, Module *M)
- : Asm(A), MMI(Asm->MMI), FirstCU(nullptr), PrevLabel(nullptr),
- GlobalRangeCount(0), InfoHolder(A, "info_string", DIEValueAllocator),
+ : Asm(A), MMI(Asm->MMI), PrevLabel(nullptr), GlobalRangeCount(0),
+ InfoHolder(A, *this, "info_string", DIEValueAllocator),
UsedNonDefaultText(false),
- SkeletonHolder(A, "skel_string", DIEValueAllocator),
+ SkeletonHolder(A, *this, "skel_string", DIEValueAllocator),
IsDarwin(Triple(A->getTargetTriple()).isOSDarwin()),
AccelNames(DwarfAccelTable::Atom(dwarf::DW_ATOM_die_offset,
dwarf::DW_FORM_data4)),
return false;
}
-// Find DIE for the given subprogram and attach appropriate DW_AT_low_pc
-// and DW_AT_high_pc attributes. If there are global variables in this
-// scope then create and insert DIEs for these variables.
-DIE &DwarfDebug::updateSubprogramScopeDIE(DwarfCompileUnit &SPCU,
- DISubprogram SP) {
- DIE *SPDie = SPCU.getOrCreateSubprogramDIE(SP);
-
- SPCU.attachLowHighPC(*SPDie, FunctionBeginSym, FunctionEndSym);
- if (!CurFn->getTarget().Options.DisableFramePointerElim(*CurFn))
- SPCU.addFlag(*SPDie, dwarf::DW_AT_APPLE_omit_frame_ptr);
-
- // Only include DW_AT_frame_base in full debug info
- if (SPCU.getCUNode().getEmissionKind() != DIBuilder::LineTablesOnly) {
- const TargetRegisterInfo *RI =
- Asm->TM.getSubtargetImpl()->getRegisterInfo();
- MachineLocation Location(RI->getFrameRegister(*Asm->MF));
- SPCU.addAddress(*SPDie, dwarf::DW_AT_frame_base, Location);
- }
-
- // Add name to the name table, we do this here because we're guaranteed
- // to have concrete versions of our DW_TAG_subprogram nodes.
- addSubprogramNames(SP, *SPDie);
-
- return *SPDie;
-}
-
/// Check whether we should create a DIE for the given Scope, return true
/// if we don't create a DIE (the corresponding DIE is null).
bool DwarfDebug::isLexicalScopeDIENull(LexicalScope *Scope) {
return !getLabelAfterInsn(Ranges.front().second);
}
-static void addSectionLabel(AsmPrinter &Asm, DwarfUnit &U, DIE &D,
- dwarf::Attribute A, const MCSymbol *L,
- const MCSymbol *Sec) {
- if (Asm.MAI->doesDwarfUseRelocationsAcrossSections())
- U.addSectionLabel(D, A, L);
- else
- U.addSectionDelta(D, A, L, Sec);
-}
-
-void DwarfDebug::addScopeRangeList(DwarfCompileUnit &TheCU, DIE &ScopeDIE,
- const SmallVectorImpl<InsnRange> &Range) {
- // Emit offset in .debug_range as a relocatable label. emitDIE will handle
- // emitting it appropriately.
- MCSymbol *RangeSym = Asm->GetTempSymbol("debug_ranges", GlobalRangeCount++);
-
- // Under fission, ranges are specified by constant offsets relative to the
- // CU's DW_AT_GNU_ranges_base.
- if (useSplitDwarf())
- TheCU.addSectionDelta(ScopeDIE, dwarf::DW_AT_ranges, RangeSym,
- DwarfDebugRangeSectionSym);
- else
- addSectionLabel(*Asm, TheCU, ScopeDIE, dwarf::DW_AT_ranges, RangeSym,
- DwarfDebugRangeSectionSym);
-
- RangeSpanList List(RangeSym);
- for (const InsnRange &R : Range) {
- RangeSpan Span(getLabelBeforeInsn(R.first), getLabelAfterInsn(R.second));
- List.addRange(std::move(Span));
- }
-
- // Add the range list to the set of ranges to be emitted.
- TheCU.addRangeList(std::move(List));
-}
-
-void DwarfDebug::attachRangesOrLowHighPC(DwarfCompileUnit &TheCU, DIE &Die,
- const SmallVectorImpl<InsnRange> &Ranges) {
- assert(!Ranges.empty());
- if (Ranges.size() == 1)
- TheCU.attachLowHighPC(Die, getLabelBeforeInsn(Ranges.front().first),
- getLabelAfterInsn(Ranges.front().second));
- else
- addScopeRangeList(TheCU, Die, Ranges);
-}
-
-// Construct new DW_TAG_lexical_block for this scope and attach
-// DW_AT_low_pc/DW_AT_high_pc labels.
-std::unique_ptr<DIE>
-DwarfDebug::constructLexicalScopeDIE(DwarfCompileUnit &TheCU,
- LexicalScope *Scope) {
- if (isLexicalScopeDIENull(Scope))
- return nullptr;
-
- auto ScopeDIE = make_unique<DIE>(dwarf::DW_TAG_lexical_block);
- if (Scope->isAbstractScope())
- return ScopeDIE;
-
- attachRangesOrLowHighPC(TheCU, *ScopeDIE, Scope->getRanges());
-
- return ScopeDIE;
-}
-
-// This scope represents inlined body of a function. Construct DIE to
-// represent this concrete inlined copy of the function.
-std::unique_ptr<DIE>
-DwarfDebug::constructInlinedScopeDIE(DwarfCompileUnit &TheCU,
- LexicalScope *Scope) {
- assert(Scope->getScopeNode());
- DIScope DS(Scope->getScopeNode());
- DISubprogram InlinedSP = getDISubprogram(DS);
- // Find the subprogram's DwarfCompileUnit in the SPMap in case the subprogram
- // was inlined from another compile unit.
- DIE *OriginDIE = AbstractSPDies[InlinedSP];
- assert(OriginDIE && "Unable to find original DIE for an inlined subprogram.");
-
- auto ScopeDIE = make_unique<DIE>(dwarf::DW_TAG_inlined_subroutine);
- TheCU.addDIEEntry(*ScopeDIE, dwarf::DW_AT_abstract_origin, *OriginDIE);
-
- attachRangesOrLowHighPC(TheCU, *ScopeDIE, Scope->getRanges());
-
- InlinedSubprogramDIEs.insert(OriginDIE);
-
- // Add the call site information to the DIE.
- DILocation DL(Scope->getInlinedAt());
- TheCU.addUInt(*ScopeDIE, dwarf::DW_AT_call_file, None,
- TheCU.getOrCreateSourceID(DL.getFilename(), DL.getDirectory()));
- TheCU.addUInt(*ScopeDIE, dwarf::DW_AT_call_line, None, DL.getLineNumber());
-
- // Add name to the name table, we do this here because we're guaranteed
- // to have concrete versions of our DW_TAG_inlined_subprogram nodes.
- addSubprogramNames(InlinedSP, *ScopeDIE);
-
- return ScopeDIE;
-}
-
-static std::unique_ptr<DIE> constructVariableDIE(DwarfCompileUnit &TheCU,
- DbgVariable &DV,
- const LexicalScope &Scope,
- DIE *&ObjectPointer) {
- auto Var = TheCU.constructVariableDIE(DV, Scope.isAbstractScope());
- if (DV.isObjectPointer())
- ObjectPointer = Var.get();
- return Var;
+template <typename Func> void forBothCUs(DwarfCompileUnit &CU, Func F) {
+ F(CU);
+ if (auto *SkelCU = CU.getSkeleton())
+ F(*SkelCU);
}
-DIE *DwarfDebug::createScopeChildrenDIE(
- DwarfCompileUnit &TheCU, LexicalScope *Scope,
- SmallVectorImpl<std::unique_ptr<DIE>> &Children,
- unsigned *ChildScopeCount) {
- DIE *ObjectPointer = nullptr;
-
- for (DbgVariable *DV : ScopeVariables.lookup(Scope))
- Children.push_back(constructVariableDIE(TheCU, *DV, *Scope, ObjectPointer));
-
- unsigned ChildCountWithoutScopes = Children.size();
-
- for (LexicalScope *LS : Scope->getChildren())
- constructScopeDIE(TheCU, LS, Children);
-
- if (ChildScopeCount)
- *ChildScopeCount = Children.size() - ChildCountWithoutScopes;
-
- return ObjectPointer;
-}
-
-DIE *DwarfDebug::createAndAddScopeChildren(DwarfCompileUnit &TheCU,
- LexicalScope *Scope, DIE &ScopeDIE) {
- // We create children when the scope DIE is not null.
- SmallVector<std::unique_ptr<DIE>, 8> Children;
- DIE *ObjectPointer = createScopeChildrenDIE(TheCU, Scope, Children);
-
- // Add children
- for (auto &I : Children)
- ScopeDIE.addChild(std::move(I));
-
- return ObjectPointer;
-}
-
-void DwarfDebug::constructAbstractSubprogramScopeDIE(DwarfCompileUnit &TheCU,
- LexicalScope *Scope) {
+void DwarfDebug::constructAbstractSubprogramScopeDIE(LexicalScope *Scope) {
assert(Scope && Scope->getScopeNode());
assert(Scope->isAbstractScope());
assert(!Scope->getInlinedAt());
- DISubprogram SP(Scope->getScopeNode());
+ const MDNode *SP = Scope->getScopeNode();
ProcessedSPNodes.insert(SP);
- DIE *&AbsDef = AbstractSPDies[SP];
- if (AbsDef)
- return;
-
// Find the subprogram's DwarfCompileUnit in the SPMap in case the subprogram
// was inlined from another compile unit.
- DwarfCompileUnit &SPCU = *SPMap[SP];
- DIE *ContextDIE;
-
- // Some of this is duplicated from DwarfUnit::getOrCreateSubprogramDIE, with
- // the important distinction that the DIDescriptor is not associated with the
- // DIE (since the DIDescriptor will be associated with the concrete DIE, if
- // any). It could be refactored to some common utility function.
- if (DISubprogram SPDecl = SP.getFunctionDeclaration()) {
- ContextDIE = &SPCU.getUnitDie();
- SPCU.getOrCreateSubprogramDIE(SPDecl);
- } else
- ContextDIE = SPCU.getOrCreateContextDIE(resolve(SP.getContext()));
-
- // Passing null as the associated DIDescriptor because the abstract definition
- // shouldn't be found by lookup.
- AbsDef = &SPCU.createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE,
- DIDescriptor());
- SPCU.applySubprogramAttributesToDefinition(SP, *AbsDef);
-
- if (TheCU.getCUNode().getEmissionKind() != DIBuilder::LineTablesOnly)
- SPCU.addUInt(*AbsDef, dwarf::DW_AT_inline, None, dwarf::DW_INL_inlined);
- if (DIE *ObjectPointer = createAndAddScopeChildren(SPCU, Scope, *AbsDef))
- SPCU.addDIEEntry(*AbsDef, dwarf::DW_AT_object_pointer, *ObjectPointer);
-}
-
-void DwarfDebug::constructSubprogramScopeDIE(DwarfCompileUnit &TheCU,
- LexicalScope *Scope) {
- assert(Scope && Scope->getScopeNode());
- assert(!Scope->getInlinedAt());
- assert(!Scope->isAbstractScope());
- DISubprogram Sub(Scope->getScopeNode());
-
- assert(Sub.isSubprogram());
-
- ProcessedSPNodes.insert(Sub);
-
- DIE &ScopeDIE = updateSubprogramScopeDIE(TheCU, Sub);
-
- // Collect arguments for current function.
- assert(LScopes.isCurrentFunctionScope(Scope));
- DIE *ObjectPointer = nullptr;
- for (DbgVariable *ArgDV : CurrentFnArguments)
- if (ArgDV)
- ScopeDIE.addChild(
- constructVariableDIE(TheCU, *ArgDV, *Scope, ObjectPointer));
-
- // If this is a variadic function, add an unspecified parameter.
- DITypeArray FnArgs = Sub.getType().getTypeArray();
- // If we have a single element of null, it is a function that returns void.
- // If we have more than one elements and the last one is null, it is a
- // variadic function.
- if (FnArgs.getNumElements() > 1 &&
- !FnArgs.getElement(FnArgs.getNumElements() - 1))
- ScopeDIE.addChild(make_unique<DIE>(dwarf::DW_TAG_unspecified_parameters));
-
- // Collect lexical scope children first.
- // ObjectPointer might be a local (non-argument) local variable if it's a
- // block's synthetic this pointer.
- if (DIE *BlockObjPtr = createAndAddScopeChildren(TheCU, Scope, ScopeDIE)) {
- assert(!ObjectPointer && "multiple object pointers can't be described");
- ObjectPointer = BlockObjPtr;
- }
-
- if (ObjectPointer)
- TheCU.addDIEEntry(ScopeDIE, dwarf::DW_AT_object_pointer, *ObjectPointer);
-}
-
-// Construct a DIE for this scope.
-void DwarfDebug::constructScopeDIE(
- DwarfCompileUnit &TheCU, LexicalScope *Scope,
- SmallVectorImpl<std::unique_ptr<DIE>> &FinalChildren) {
- if (!Scope || !Scope->getScopeNode())
- return;
-
- DIScope DS(Scope->getScopeNode());
-
- assert((Scope->getInlinedAt() || !DS.isSubprogram()) &&
- "Only handle inlined subprograms here, use "
- "constructSubprogramScopeDIE for non-inlined "
- "subprograms");
-
- SmallVector<std::unique_ptr<DIE>, 8> Children;
-
- // We try to create the scope DIE first, then the children DIEs. This will
- // avoid creating un-used children then removing them later when we find out
- // the scope DIE is null.
- std::unique_ptr<DIE> ScopeDIE;
- if (Scope->getParent() && DS.isSubprogram()) {
- ScopeDIE = constructInlinedScopeDIE(TheCU, Scope);
- if (!ScopeDIE)
- return;
- // We create children when the scope DIE is not null.
- createScopeChildrenDIE(TheCU, Scope, Children);
- } else {
- // Early exit when we know the scope DIE is going to be null.
- if (isLexicalScopeDIENull(Scope))
- return;
-
- unsigned ChildScopeCount;
-
- // We create children here when we know the scope DIE is not going to be
- // null and the children will be added to the scope DIE.
- createScopeChildrenDIE(TheCU, Scope, Children, &ChildScopeCount);
-
- // There is no need to emit empty lexical block DIE.
- std::pair<ImportedEntityMap::const_iterator,
- ImportedEntityMap::const_iterator> Range =
- std::equal_range(ScopesWithImportedEntities.begin(),
- ScopesWithImportedEntities.end(),
- std::pair<const MDNode *, const MDNode *>(DS, nullptr),
- less_first());
- for (ImportedEntityMap::const_iterator i = Range.first; i != Range.second;
- ++i)
- Children.push_back(
- constructImportedEntityDIE(TheCU, DIImportedEntity(i->second)));
- // If there are only other scopes as children, put them directly in the
- // parent instead, as this scope would serve no purpose.
- if (Children.size() == ChildScopeCount) {
- FinalChildren.insert(FinalChildren.end(),
- std::make_move_iterator(Children.begin()),
- std::make_move_iterator(Children.end()));
- return;
- }
- ScopeDIE = constructLexicalScopeDIE(TheCU, Scope);
- assert(ScopeDIE && "Scope DIE should not be null.");
- }
-
- // Add children
- for (auto &I : Children)
- ScopeDIE->addChild(std::move(I));
-
- FinalChildren.push_back(std::move(ScopeDIE));
+ auto &CU = SPMap[SP];
+ forBothCUs(*CU, [&](DwarfCompileUnit &CU) {
+ CU.constructAbstractSubprogramScopeDIE(Scope);
+ });
}
void DwarfDebug::addGnuPubAttributes(DwarfUnit &U, DIE &D) const {
DwarfCompileUnit &NewCU = *OwnedUnit;
DIE &Die = NewCU.getUnitDie();
InfoHolder.addUnit(std::move(OwnedUnit));
+ if (useSplitDwarf())
+ NewCU.setSkeleton(constructSkeletonCU(NewCU));
// LTO with assembly output shares a single line table amongst multiple CUs.
// To avoid the compilation directory being ambiguous, let the line table
@@ -697,14 +410,10 @@ DwarfCompileUnit &DwarfDebug::constructDwarfCompileUnit(DICompileUnit DIUnit) {
NewCU.addUInt(Die, dwarf::DW_AT_APPLE_major_runtime_vers,
dwarf::DW_FORM_data1, RVer);
- if (!FirstCU)
- FirstCU = &NewCU;
-
- if (useSplitDwarf()) {
+ if (useSplitDwarf())
NewCU.initSection(Asm->getObjFileLowering().getDwarfInfoDWOSection(),
DwarfInfoDWOSectionSym);
- NewCU.setSkeleton(constructSkeletonCU(NewCU));
- } else
+ else
NewCU.initSection(Asm->getObjFileLowering().getDwarfInfoSection(),
DwarfInfoSectionSym);
DIImportedEntity Module(N);
assert(Module.Verify());
if (DIE *D = TheCU.getOrCreateContextDIE(Module.getContext()))
- D->addChild(constructImportedEntityDIE(TheCU, Module));
-}
-
-std::unique_ptr<DIE>
-DwarfDebug::constructImportedEntityDIE(DwarfCompileUnit &TheCU,
- const DIImportedEntity &Module) {
- assert(Module.Verify() &&
- "Use one of the MDNode * overloads to handle invalid metadata");
- std::unique_ptr<DIE> IMDie = make_unique<DIE>((dwarf::Tag)Module.getTag());
- TheCU.insertDIE(Module, IMDie.get());
- DIE *EntityDie;
- DIDescriptor Entity = resolve(Module.getEntity());
- if (Entity.isNameSpace())
- EntityDie = TheCU.getOrCreateNameSpace(DINameSpace(Entity));
- else if (Entity.isSubprogram())
- EntityDie = TheCU.getOrCreateSubprogramDIE(DISubprogram(Entity));
- else if (Entity.isType())
- EntityDie = TheCU.getOrCreateTypeDIE(DIType(Entity));
- else
- EntityDie = TheCU.getDIE(Entity);
- assert(EntityDie);
- TheCU.addSourceLine(*IMDie, Module.getLineNumber(),
- Module.getContext().getFilename(),
- Module.getContext().getDirectory());
- TheCU.addDIEEntry(*IMDie, dwarf::DW_AT_import, *EntityDie);
- StringRef Name = Module.getName();
- if (!Name.empty())
- TheCU.addString(*IMDie, dwarf::DW_AT_name, Name);
-
- return IMDie;
+ D->addChild(TheCU.constructImportedEntityDIE(Module));
}
// Emit all Dwarf sections that should come prior to the content. Create
FunctionDIs = makeSubprogramMap(*M);
- // If module has named metadata anchors then use them, otherwise scan the
- // module using debug info finder to collect debug info.
NamedMDNode *CU_Nodes = M->getNamedMetadata("llvm.dbg.cu");
if (!CU_Nodes)
return;
}
void DwarfDebug::finishSubprogramDefinitions() {
- const Module *M = MMI->getModule();
-
- NamedMDNode *CU_Nodes = M->getNamedMetadata("llvm.dbg.cu");
- for (MDNode *N : CU_Nodes->operands()) {
- DICompileUnit TheCU(N);
- // Construct subprogram DIE and add variables DIEs.
- DwarfCompileUnit *SPCU =
- static_cast<DwarfCompileUnit *>(CUMap.lookup(TheCU));
- DIArray Subprograms = TheCU.getSubprograms();
- for (unsigned i = 0, e = Subprograms.getNumElements(); i != e; ++i) {
- DISubprogram SP(Subprograms.getElement(i));
- // Perhaps the subprogram is in another CU (such as due to comdat
- // folding, etc), in which case ignore it here.
- if (SPMap[SP] != SPCU)
- continue;
- DIE *D = SPCU->getDIE(SP);
- if (DIE *AbsSPDIE = AbstractSPDies.lookup(SP)) {
- if (D)
- // If this subprogram has an abstract definition, reference that
- SPCU->addDIEEntry(*D, dwarf::DW_AT_abstract_origin, *AbsSPDIE);
- } else {
- if (!D && TheCU.getEmissionKind() != DIBuilder::LineTablesOnly)
- // Lazily construct the subprogram if we didn't see either concrete or
- // inlined versions during codegen. (except in -gmlt ^ where we want
- // to omit these entirely)
- D = SPCU->getOrCreateSubprogramDIE(SP);
- if (D)
- // And attach the attributes
- SPCU->applySubprogramAttributesToDefinition(SP, *D);
- }
- }
- }
+ for (const auto &P : SPMap)
+ forBothCUs(*P.second, [&](DwarfCompileUnit &CU) {
+ CU.finishSubprogramDefinition(DISubprogram(P.first));
+ });
}
DISubprogram SP(Subprograms.getElement(i));
if (ProcessedSPNodes.count(SP) != 0)
continue;
- assert(SP.isSubprogram() &&
- "CU's subprogram list contains a non-subprogram");
- assert(SP.isDefinition() &&
- "CU's subprogram list contains a subprogram declaration");
- DIArray Variables = SP.getVariables();
- if (Variables.getNumElements() == 0)
- continue;
-
- DIE *SPDIE = AbstractSPDies.lookup(SP);
- if (!SPDIE)
- SPDIE = SPCU->getDIE(SP);
- assert(SPDIE);
- for (unsigned vi = 0, ve = Variables.getNumElements(); vi != ve; ++vi) {
- DIVariable DV(Variables.getElement(vi));
- assert(DV.isVariable());
- DbgVariable NewVar(DV, DIExpression(nullptr), this);
- auto VariableDie = SPCU->constructVariableDIE(NewVar);
- SPCU->applyVariableAttributes(NewVar, *VariableDie);
- SPDIE->addChild(std::move(VariableDie));
- }
+ SPCU->collectDeadVariables(SP);
}
}
}
// Handle anything that needs to be done on a per-unit basis after
// all other generation.
- for (const auto &TheU : getUnits()) {
+ for (const auto &P : CUMap) {
+ auto &TheCU = *P.second;
// Emit DW_AT_containing_type attribute to connect types with their
// vtable holding type.
- TheU->constructContainingTypeDIEs();
+ TheCU.constructContainingTypeDIEs();
// Add CU specific attributes if we need to add any.
- if (TheU->getUnitDie().getTag() == dwarf::DW_TAG_compile_unit) {
- // If we're splitting the dwarf out now that we've got the entire
- // CU then add the dwo id to it.
- DwarfCompileUnit *SkCU =
- static_cast<DwarfCompileUnit *>(TheU->getSkeleton());
- if (useSplitDwarf()) {
- // Emit a unique identifier for this CU.
- uint64_t ID = DIEHash(Asm).computeCUSignature(TheU->getUnitDie());
- TheU->addUInt(TheU->getUnitDie(), dwarf::DW_AT_GNU_dwo_id,
- dwarf::DW_FORM_data8, ID);
- SkCU->addUInt(SkCU->getUnitDie(), dwarf::DW_AT_GNU_dwo_id,
- dwarf::DW_FORM_data8, ID);
-
- // We don't keep track of which addresses are used in which CU so this
- // is a bit pessimistic under LTO.
- if (!AddrPool.isEmpty())
- addSectionLabel(*Asm, *SkCU, SkCU->getUnitDie(),
- dwarf::DW_AT_GNU_addr_base, DwarfAddrSectionSym,
- DwarfAddrSectionSym);
- if (!TheU->getRangeLists().empty())
- addSectionLabel(*Asm, *SkCU, SkCU->getUnitDie(),
- dwarf::DW_AT_GNU_ranges_base,
- DwarfDebugRangeSectionSym, DwarfDebugRangeSectionSym);
- }
+ // If we're splitting the dwarf out now that we've got the entire
+ // CU then add the dwo id to it.
+ auto *SkCU = TheCU.getSkeleton();
+ if (useSplitDwarf()) {
+ // Emit a unique identifier for this CU.
+ uint64_t ID = DIEHash(Asm).computeCUSignature(TheCU.getUnitDie());
+ TheCU.addUInt(TheCU.getUnitDie(), dwarf::DW_AT_GNU_dwo_id,
+ dwarf::DW_FORM_data8, ID);
+ SkCU->addUInt(SkCU->getUnitDie(), dwarf::DW_AT_GNU_dwo_id,
+ dwarf::DW_FORM_data8, ID);
+
+ // We don't keep track of which addresses are used in which CU so this
+ // is a bit pessimistic under LTO.
+ if (!AddrPool.isEmpty())
+ SkCU->addSectionLabel(SkCU->getUnitDie(), dwarf::DW_AT_GNU_addr_base,
+ DwarfAddrSectionSym, DwarfAddrSectionSym);
+ if (!SkCU->getRangeLists().empty())
+ SkCU->addSectionLabel(SkCU->getUnitDie(), dwarf::DW_AT_GNU_ranges_base,
+ DwarfDebugRangeSectionSym,
+ DwarfDebugRangeSectionSym);
+ }
- // If we have code split among multiple sections or non-contiguous
- // ranges of code then emit a DW_AT_ranges attribute on the unit that will
- // remain in the .o file, otherwise add a DW_AT_low_pc.
- // FIXME: We should use ranges allow reordering of code ala
- // .subsections_via_symbols in mach-o. This would mean turning on
- // ranges for all subprogram DIEs for mach-o.
- DwarfCompileUnit &U =
- SkCU ? *SkCU : static_cast<DwarfCompileUnit &>(*TheU);
- unsigned NumRanges = TheU->getRanges().size();
- if (NumRanges) {
- if (NumRanges > 1) {
- addSectionLabel(*Asm, U, U.getUnitDie(), dwarf::DW_AT_ranges,
- Asm->GetTempSymbol("cu_ranges", U.getUniqueID()),
- DwarfDebugRangeSectionSym);
-
- // A DW_AT_low_pc attribute may also be specified in combination with
- // DW_AT_ranges to specify the default base address for use in
- // location lists (see Section 2.6.2) and range lists (see Section
- // 2.17.3).
- U.addUInt(U.getUnitDie(), dwarf::DW_AT_low_pc, dwarf::DW_FORM_addr,
- 0);
- } else {
- RangeSpan &Range = TheU->getRanges().back();
- U.attachLowHighPC(U.getUnitDie(), Range.getStart(), Range.getEnd());
- }
- }
+ // If we have code split among multiple sections or non-contiguous
+ // ranges of code then emit a DW_AT_ranges attribute on the unit that will
+ // remain in the .o file, otherwise add a DW_AT_low_pc.
+ // FIXME: We should use ranges allow reordering of code ala
+ // .subsections_via_symbols in mach-o. This would mean turning on
+ // ranges for all subprogram DIEs for mach-o.
+ DwarfCompileUnit &U = SkCU ? *SkCU : TheCU;
+ if (unsigned NumRanges = TheCU.getRanges().size()) {
+ if (NumRanges > 1)
+ // A DW_AT_low_pc attribute may also be specified in combination with
+ // DW_AT_ranges to specify the default base address for use in
+ // location lists (see Section 2.6.2) and range lists (see Section
+ // 2.17.3).
+ U.addUInt(U.getUnitDie(), dwarf::DW_AT_low_pc, dwarf::DW_FORM_addr, 0);
+ else
+ TheCU.setBaseAddress(TheCU.getRanges().front().getStart());
+ U.attachRangesOrLowHighPC(U.getUnitDie(), TheCU.takeRanges());
}
}
assert(CurFn == nullptr);
assert(CurMI == nullptr);
- if (!FirstCU)
+ // If we aren't actually generating debug info (check beginModule -
+ // conditionalized on !DisableDebugInfoPrinting and the presence of the
+ // llvm.dbg.cu metadata node)
+ if (!DwarfInfoSectionSym)
return;
// End any existing sections.
// clean up.
SPMap.clear();
AbstractVariables.clear();
-
- // Reset these for the next Module if we have one.
- FirstCU = nullptr;
}
// Find abstract variable, if any, associated with Var.
void DwarfDebug::createAbstractVariable(const DIVariable &Var,
LexicalScope *Scope) {
auto AbsDbgVariable = make_unique<DbgVariable>(Var, DIExpression(), this);
- addScopeVariable(Scope, AbsDbgVariable.get());
+ InfoHolder.addScopeVariable(Scope, AbsDbgVariable.get());
AbstractVariables[Var] = std::move(AbsDbgVariable);
}
createAbstractVariable(Cleansed, Scope);
}
-// If Var is a current function argument then add it to CurrentFnArguments list.
-bool DwarfDebug::addCurrentFnArgument(DbgVariable *Var, LexicalScope *Scope) {
- if (!LScopes.isCurrentFunctionScope(Scope))
- return false;
- DIVariable DV = Var->getVariable();
- if (DV.getTag() != dwarf::DW_TAG_arg_variable)
- return false;
- unsigned ArgNo = DV.getArgNumber();
- if (ArgNo == 0)
- return false;
-
- size_t Size = CurrentFnArguments.size();
- if (Size == 0)
- CurrentFnArguments.resize(CurFn->getFunction()->arg_size());
- // llvm::Function argument size is not good indicator of how many
- // arguments does the function have at source level.
- if (ArgNo > Size)
- CurrentFnArguments.resize(ArgNo * 2);
- assert(!CurrentFnArguments[ArgNo - 1]);
- CurrentFnArguments[ArgNo - 1] = Var;
- return true;
-}
-
// Collect variable information from side table maintained by MMI.
void DwarfDebug::collectVariableInfoFromMMITable(
SmallPtrSetImpl<const MDNode *> &Processed) {
if (!VI.Var)
continue;
Processed.insert(VI.Var);
- DIVariable DV(VI.Var);
- DIExpression Expr(VI.Expr);
LexicalScope *Scope = LScopes.findLexicalScope(VI.Loc);
// If variable scope is not found then skip this variable.
if (!Scope)
continue;
+ DIVariable DV(VI.Var);
+ DIExpression Expr(VI.Expr);
ensureAbstractVariableIsCreatedIfScoped(DV, Scope->getScopeNode());
ConcreteVariables.push_back(make_unique<DbgVariable>(DV, Expr, this));
DbgVariable *RegVar = ConcreteVariables.back().get();
RegVar->setFrameIndex(VI.Slot);
- addScopeVariable(Scope, RegVar);
+ InfoHolder.addScopeVariable(Scope, RegVar);
}
}
// Find variables for each lexical scope.
void
-DwarfDebug::collectVariableInfo(SmallPtrSetImpl<const MDNode *> &Processed) {
- LexicalScope *FnScope = LScopes.getCurrentFunctionScope();
- DwarfCompileUnit *TheCU = SPMap.lookup(FnScope->getScopeNode());
-
+DwarfDebug::collectVariableInfo(DwarfCompileUnit &TheCU, DISubprogram SP,
+ SmallPtrSetImpl<const MDNode *> &Processed) {
// Grab the variable info that was squirreled away in the MMI side-table.
collectVariableInfoFromMMITable(Processed);
ensureAbstractVariableIsCreatedIfScoped(DV, Scope->getScopeNode());
ConcreteVariables.push_back(make_unique<DbgVariable>(MInsn, this));
DbgVariable *RegVar = ConcreteVariables.back().get();
- addScopeVariable(Scope, RegVar);
+ InfoHolder.addScopeVariable(Scope, RegVar);
// Check if the first DBG_VALUE is valid for the rest of the function.
if (Ranges.size() == 1 && Ranges.front().second == nullptr)
DotDebugLocEntries.resize(DotDebugLocEntries.size() + 1);
DebugLocList &LocList = DotDebugLocEntries.back();
- LocList.CU = TheCU;
+ LocList.CU = &TheCU;
LocList.Label =
Asm->GetTempSymbol("debug_loc", DotDebugLocEntries.size() - 1);
@@ -1392,17 +987,17 @@ DwarfDebug::collectVariableInfo(SmallPtrSetImpl<const MDNode *> &Processed) {
}
// Collect info for variables that were optimized out.
- DIArray Variables = DISubprogram(FnScope->getScopeNode()).getVariables();
+ DIArray Variables = SP.getVariables();
for (unsigned i = 0, e = Variables.getNumElements(); i != e; ++i) {
DIVariable DV(Variables.getElement(i));
assert(DV.isVariable());
- if (!Processed.insert(DV))
+ if (!Processed.insert(DV).second)
continue;
if (LexicalScope *Scope = LScopes.findLexicalScope(DV.getContext())) {
ensureAbstractVariableIsCreatedIfScoped(DV, Scope->getScopeNode());
DIExpression NoExpr;
ConcreteVariables.push_back(make_unique<DbgVariable>(DV, NoExpr, this));
- addScopeVariable(Scope, ConcreteVariables.back().get());
+ InfoHolder.addScopeVariable(Scope, ConcreteVariables.back().get());
}
}
}
if (DL == PrologEndLoc) {
Flags |= DWARF2_FLAG_PROLOGUE_END;
PrologEndLoc = DebugLoc();
+ Flags |= DWARF2_FLAG_IS_STMT;
}
- if (PrologEndLoc.isUnknown())
+ if (DL.getLine() !=
+ Asm->OutStreamer.getContext().getCurrentDwarfLoc().getLine())
Flags |= DWARF2_FLAG_IS_STMT;
if (!DL.isUnknown()) {
for (const auto &MBB : *MF)
for (const auto &MI : MBB)
if (!MI.isDebugValue() && !MI.getFlag(MachineInstr::FrameSetup) &&
- !MI.getDebugLoc().isUnknown())
+ !MI.getDebugLoc().isUnknown()) {
+ // Did the target forget to set the FrameSetup flag for CFI insns?
+ assert(!MI.isCFIInstruction() &&
+ "First non-frame-setup instruction is a CFI instruction.");
return MI.getDebugLoc();
+ }
return DebugLoc();
}
}
}
-void DwarfDebug::addScopeVariable(LexicalScope *LS, DbgVariable *Var) {
- if (addCurrentFnArgument(Var, LS))
- return;
- SmallVectorImpl<DbgVariable *> &Vars = ScopeVariables[LS];
- DIVariable DV = Var->getVariable();
- // Variables with positive arg numbers are parameters.
- if (unsigned ArgNum = DV.getArgNumber()) {
- // Keep all parameters in order at the start of the variable list to ensure
- // function types are correct (no out-of-order parameters)
- //
- // This could be improved by only doing it for optimized builds (unoptimized
- // builds have the right order to begin with), searching from the back (this
- // would catch the unoptimized case quickly), or doing a binary search
- // rather than linear search.
- SmallVectorImpl<DbgVariable *>::iterator I = Vars.begin();
- while (I != Vars.end()) {
- unsigned CurNum = (*I)->getVariable().getArgNumber();
- // A local (non-parameter) variable has been found, insert immediately
- // before it.
- if (CurNum == 0)
- break;
- // A later indexed parameter has been found, insert immediately before it.
- if (CurNum > ArgNum)
- break;
- ++I;
- }
- Vars.insert(I, Var);
- return;
- }
-
- Vars.push_back(Var);
-}
-
// Gather and emit post-function debug information.
void DwarfDebug::endFunction(const MachineFunction *MF) {
- // Every beginFunction(MF) call should be followed by an endFunction(MF) call,
- // though the beginFunction may not be called at all.
- // We should handle both cases.
- if (!CurFn)
- CurFn = MF;
- else
- assert(CurFn == MF);
- assert(CurFn != nullptr);
+ assert(CurFn == MF &&
+ "endFunction should be called with the same function as beginFunction");
if (!MMI->hasDebugInfo() || LScopes.empty() ||
!FunctionDIs.count(MF->getFunction())) {
// Set DwarfDwarfCompileUnitID in MCContext to default value.
Asm->OutStreamer.getContext().setDwarfCompileUnitID(0);
- SmallPtrSet<const MDNode *, 16> ProcessedVars;
- collectVariableInfo(ProcessedVars);
-
LexicalScope *FnScope = LScopes.getCurrentFunctionScope();
- DwarfCompileUnit &TheCU = *SPMap.lookup(FnScope->getScopeNode());
+ DISubprogram SP(FnScope->getScopeNode());
+ DwarfCompileUnit &TheCU = *SPMap.lookup(SP);
+
+ SmallPtrSet<const MDNode *, 16> ProcessedVars;
+ collectVariableInfo(TheCU, SP, ProcessedVars);
// Add the range of this function to the list of ranges for the CU.
TheCU.addRange(RangeSpan(FunctionBeginSym, FunctionEndSym));
// subroutines inside it.
if (TheCU.getCUNode().getEmissionKind() == DIBuilder::LineTablesOnly &&
LScopes.getAbstractScopesList().empty() && !IsDarwin) {
- assert(ScopeVariables.empty());
- assert(CurrentFnArguments.empty());
+ assert(InfoHolder.getScopeVariables().empty());
assert(DbgValues.empty());
+ // FIXME: This wouldn't be true in LTO with a -g (with inlining) CU followed
+ // by a -gmlt CU. Add a test and remove this assertion.
assert(AbstractVariables.empty());
LabelsBeforeInsn.clear();
LabelsAfterInsn.clear();
return;
}
+#ifndef NDEBUG
+ size_t NumAbstractScopes = LScopes.getAbstractScopesList().size();
+#endif
// Construct abstract scopes.
for (LexicalScope *AScope : LScopes.getAbstractScopesList()) {
DISubprogram SP(AScope->getScopeNode());
for (unsigned i = 0, e = Variables.getNumElements(); i != e; ++i) {
DIVariable DV(Variables.getElement(i));
assert(DV && DV.isVariable());
- if (!ProcessedVars.insert(DV))
+ if (!ProcessedVars.insert(DV).second)
continue;
ensureAbstractVariableIsCreated(DV, DV.getContext());
+ assert(LScopes.getAbstractScopesList().size() == NumAbstractScopes
+ && "ensureAbstractVariableIsCreated inserted abstract scopes");
}
- constructAbstractSubprogramScopeDIE(TheCU, AScope);
+ constructAbstractSubprogramScopeDIE(AScope);
}
- constructSubprogramScopeDIE(TheCU, FnScope);
+ TheCU.constructSubprogramScopeDIE(FnScope);
+ if (auto *SkelCU = TheCU.getSkeleton())
+ if (!LScopes.getAbstractScopesList().empty())
+ SkelCU->constructSubprogramScopeDIE(FnScope);
// Clear debug info
// Ownership of DbgVariables is a bit subtle - ScopeVariables owns all the
// DbgVariables except those that are also in AbstractVariables (since they
// can be used cross-function)
- ScopeVariables.clear();
- CurrentFnArguments.clear();
+ InfoHolder.getScopeVariables().clear();
DbgValues.clear();
LabelsBeforeInsn.clear();
LabelsAfterInsn.clear();
void DwarfDebug::emitDebugInfo() {
DwarfFile &Holder = useSplitDwarf() ? SkeletonHolder : InfoHolder;
- Holder.emitUnits(this, DwarfAbbrevSectionSym);
+ Holder.emitUnits(DwarfAbbrevSectionSym);
}
// Emit the abbreviation section.
Asm->OutStreamer.EmitLabel(SectionBegin);
// Emit the full data.
- Accel.Emit(Asm, SectionBegin, &InfoHolder, DwarfStrSectionSym);
+ Accel.Emit(Asm, SectionBegin, this, DwarfStrSectionSym);
}
// Emit visible names into a hashed accelerator table section.
GnuStyle ? Asm->getObjFileLowering().getDwarfGnuPubNamesSection()
: Asm->getObjFileLowering().getDwarfPubNamesSection();
- emitDebugPubSection(GnuStyle, PSec, "Names", &DwarfUnit::getGlobalNames);
+ emitDebugPubSection(GnuStyle, PSec, "Names",
+ &DwarfCompileUnit::getGlobalNames);
}
void DwarfDebug::emitDebugPubSection(
bool GnuStyle, const MCSection *PSec, StringRef Name,
- const StringMap<const DIE *> &(DwarfUnit::*Accessor)() const) {
+ const StringMap<const DIE *> &(DwarfCompileUnit::*Accessor)() const) {
for (const auto &NU : CUMap) {
DwarfCompileUnit *TheU = NU.second;
if (Globals.empty())
continue;
- if (auto Skeleton = static_cast<DwarfCompileUnit *>(TheU->getSkeleton()))
+ if (auto *Skeleton = TheU->getSkeleton())
TheU = Skeleton;
unsigned ID = TheU->getUniqueID();
Asm->EmitSectionOffset(TheU->getLabelBegin(), TheU->getSectionSym());
Asm->OutStreamer.AddComment("Compilation Unit Length");
- Asm->EmitLabelDifference(TheU->getLabelEnd(), TheU->getLabelBegin(), 4);
+ Asm->EmitInt32(TheU->getLength());
// Emit the pubnames for this compilation unit.
for (const auto &GI : Globals) {
GnuStyle ? Asm->getObjFileLowering().getDwarfGnuPubTypesSection()
: Asm->getObjFileLowering().getDwarfPubTypesSection();
- emitDebugPubSection(GnuStyle, PSec, "Types", &DwarfUnit::getGlobalTypes);
+ emitDebugPubSection(GnuStyle, PSec, "Types",
+ &DwarfCompileUnit::getGlobalTypes);
}
// Emit visible names into a debug str section.
void DwarfDebug::emitDebugLocValue(ByteStreamer &Streamer,
const DebugLocEntry::Value &Value) {
DIVariable DV = Value.getVariable();
+ DebugLocDwarfExpression Expr(*Asm, Streamer);
// Regular entry.
if (Value.isInt()) {
DIBasicType BTy(resolve(DV.getType()));
if (BTy.Verify() && (BTy.getEncoding() == dwarf::DW_ATE_signed ||
- BTy.getEncoding() == dwarf::DW_ATE_signed_char)) {
- Streamer.EmitInt8(dwarf::DW_OP_consts, "DW_OP_consts");
- Streamer.EmitSLEB128(Value.getInt());
- } else {
- Streamer.EmitInt8(dwarf::DW_OP_constu, "DW_OP_constu");
- Streamer.EmitULEB128(Value.getInt());
- }
+ BTy.getEncoding() == dwarf::DW_ATE_signed_char))
+ Expr.AddSignedConstant(Value.getInt());
+ else
+ Expr.AddUnsignedConstant(Value.getInt());
} else if (Value.isLocation()) {
MachineLocation Loc = Value.getLoc();
DIExpression Expr = Value.getExpression();
for (const auto &DebugLoc : DotDebugLocEntries) {
Asm->OutStreamer.EmitLabel(DebugLoc.Label);
const DwarfCompileUnit *CU = DebugLoc.CU;
- assert(!CU->getRanges().empty());
for (const auto &Entry : DebugLoc.List) {
// Set up the range. This range is relative to the entry point of the
// compile unit. This is a hard coded 0 for low_pc when we're emitting
// ranges, or the DW_AT_low_pc on the compile unit otherwise.
- if (CU->getRanges().size() == 1) {
- // Grab the begin symbol from the first range as our base.
- const MCSymbol *Base = CU->getRanges()[0].getStart();
+ if (auto *Base = CU->getBaseAddress()) {
Asm->EmitLabelDifference(Entry.getBeginSym(), Base, Size);
Asm->EmitLabelDifference(Entry.getEndSym(), Base, Size);
} else {
for (DwarfCompileUnit *CU : CUs) {
std::vector<ArangeSpan> &List = Spans[CU];
+ // Describe the skeleton CU's offset and length, not the dwo file's.
+ if (auto *Skel = CU->getSkeleton())
+ CU = Skel;
+
// Emit size of content not including length itself.
unsigned ContentSize =
sizeof(int16_t) + // DWARF ARange version number
Asm->OutStreamer.AddComment("DWARF Arange version number");
Asm->EmitInt16(dwarf::DW_ARANGES_VERSION);
Asm->OutStreamer.AddComment("Offset Into Debug Info Section");
- Asm->EmitSectionOffset(CU->getLocalLabelBegin(), CU->getLocalSectionSym());
+ Asm->EmitSectionOffset(CU->getLabelBegin(), CU->getSectionSym());
Asm->OutStreamer.AddComment("Address Size (in bytes)");
Asm->EmitInt8(PtrSize);
Asm->OutStreamer.AddComment("Segment Size (in bytes)");
for (const auto &I : CUMap) {
DwarfCompileUnit *TheCU = I.second;
+ if (auto *Skel = TheCU->getSkeleton())
+ TheCU = Skel;
+
// Iterate over the misc ranges for the compile units in the module.
for (const RangeSpanList &List : TheCU->getRangeLists()) {
// Emit our symbol so we can find the beginning of the range.
const MCSymbol *End = Range.getEnd();
assert(Begin && "Range without a begin symbol?");
assert(End && "Range without an end symbol?");
- if (TheCU->getRanges().size() == 1) {
- // Grab the begin symbol from the first range as our base.
- const MCSymbol *Base = TheCU->getRanges()[0].getStart();
+ if (auto *Base = TheCU->getBaseAddress()) {
Asm->EmitLabelDifference(Begin, Base, Size);
Asm->EmitLabelDifference(End, Base, Size);
} else {
Asm->OutStreamer.EmitIntValue(0, Size);
Asm->OutStreamer.EmitIntValue(0, Size);
}
-
- // Now emit a range for the CU itself.
- if (TheCU->getRanges().size() > 1) {
- Asm->OutStreamer.EmitLabel(
- Asm->GetTempSymbol("cu_ranges", TheCU->getUniqueID()));
- for (const RangeSpan &Range : TheCU->getRanges()) {
- const MCSymbol *Begin = Range.getStart();
- const MCSymbol *End = Range.getEnd();
- assert(Begin && "Range without a begin symbol?");
- assert(End && "Range without an end symbol?");
- Asm->OutStreamer.EmitSymbolValue(Begin, Size);
- Asm->OutStreamer.EmitSymbolValue(End, Size);
- }
- // And terminate the list with two 0 values.
- Asm->OutStreamer.EmitIntValue(0, Size);
- Asm->OutStreamer.EmitIntValue(0, Size);
- }
}
}
void DwarfDebug::initSkeletonUnit(const DwarfUnit &U, DIE &Die,
std::unique_ptr<DwarfUnit> NewU) {
- NewU->addLocalString(Die, dwarf::DW_AT_GNU_dwo_name,
- U.getCUNode().getSplitDebugFilename());
+ NewU->addString(Die, dwarf::DW_AT_GNU_dwo_name,
+ U.getCUNode().getSplitDebugFilename());
if (!CompilationDir.empty())
- NewU->addLocalString(Die, dwarf::DW_AT_comp_dir, CompilationDir);
+ NewU->addString(Die, dwarf::DW_AT_comp_dir, CompilationDir);
addGnuPubAttributes(*NewU, Die);
assert(useSplitDwarf() && "No split dwarf debug info?");
// Don't pass an abbrev symbol, using a constant zero instead so as not to
// emit relocations into the dwo file.
- InfoHolder.emitUnits(this, /* AbbrevSymbol */ nullptr);
+ InfoHolder.emitUnits(/* AbbrevSymbol */ nullptr);
}
// Emit the .debug_abbrev.dwo section for separated dwarf. This contains the
NewTU.setTypeSignature(Signature);
if (useSplitDwarf())
- NewTU.initSection(Asm->getObjFileLowering().getDwarfTypesDWOSection(),
- DwarfTypesDWOSectionSym);
+ NewTU.initSection(Asm->getObjFileLowering().getDwarfTypesDWOSection());
else {
CU.applyStmtList(UnitDie);
NewTU.initSection(