index decc434598f8af5080132761702b72b4a1b073a8..99f4d1c5d446545cb4e633dca88ce58d75744ced 100644 (file)
#include "DwarfDebug.h"
#include "ByteStreamer.h"
+#include "DwarfExpression.h"
#include "DwarfCompileUnit.h"
-#include "DIE.h"
#include "DIEHash.h"
#include "DwarfUnit.h"
#include "llvm/ADT/STLExtras.h"
#include "llvm/ADT/Statistic.h"
#include "llvm/ADT/StringExtras.h"
#include "llvm/ADT/Triple.h"
+#include "llvm/CodeGen/DIE.h"
#include "llvm/CodeGen/MachineFunction.h"
#include "llvm/CodeGen/MachineModuleInfo.h"
#include "llvm/IR/Constants.h"
return !getLabelAfterInsn(Ranges.front().second);
}
+template <typename Func> void forBothCUs(DwarfCompileUnit &CU, Func F) {
+ F(CU);
+ if (auto *SkelCU = CU.getSkeleton())
+ F(*SkelCU);
+}
+
void DwarfDebug::constructAbstractSubprogramScopeDIE(LexicalScope *Scope) {
assert(Scope && Scope->getScopeNode());
assert(Scope->isAbstractScope());
// Find the subprogram's DwarfCompileUnit in the SPMap in case the subprogram
// was inlined from another compile unit.
- SPMap[SP]->constructAbstractSubprogramScopeDIE(Scope);
+ auto &CU = SPMap[SP];
+ forBothCUs(*CU, [&](DwarfCompileUnit &CU) {
+ CU.constructAbstractSubprogramScopeDIE(Scope);
+ });
}
void DwarfDebug::addGnuPubAttributes(DwarfUnit &U, DIE &D) const {
DwarfCompileUnit &NewCU = *OwnedUnit;
DIE &Die = NewCU.getUnitDie();
InfoHolder.addUnit(std::move(OwnedUnit));
+ if (useSplitDwarf())
+ NewCU.setSkeleton(constructSkeletonCU(NewCU));
// LTO with assembly output shares a single line table amongst multiple CUs.
// To avoid the compilation directory being ambiguous, let the line table
@@ -398,11 +410,10 @@ DwarfCompileUnit &DwarfDebug::constructDwarfCompileUnit(DICompileUnit DIUnit) {
NewCU.addUInt(Die, dwarf::DW_AT_APPLE_major_runtime_vers,
dwarf::DW_FORM_data1, RVer);
- if (useSplitDwarf()) {
+ if (useSplitDwarf())
NewCU.initSection(Asm->getObjFileLowering().getDwarfInfoDWOSection(),
DwarfInfoDWOSectionSym);
- NewCU.setSkeleton(constructSkeletonCU(NewCU));
- } else
+ else
NewCU.initSection(Asm->getObjFileLowering().getDwarfInfoSection(),
DwarfInfoSectionSym);
void DwarfDebug::finishSubprogramDefinitions() {
for (const auto &P : SPMap)
- P.second->finishSubprogramDefinition(DISubprogram(P.first));
+ forBothCUs(*P.second, [&](DwarfCompileUnit &CU) {
+ CU.finishSubprogramDefinition(DISubprogram(P.first));
+ });
}
// Handle anything that needs to be done on a per-unit basis after
// all other generation.
- for (const auto &TheU : getUnits()) {
+ for (const auto &P : CUMap) {
+ auto &TheCU = *P.second;
// Emit DW_AT_containing_type attribute to connect types with their
// vtable holding type.
- TheU->constructContainingTypeDIEs();
+ TheCU.constructContainingTypeDIEs();
// Add CU specific attributes if we need to add any.
- if (TheU->getUnitDie().getTag() == dwarf::DW_TAG_compile_unit) {
- // If we're splitting the dwarf out now that we've got the entire
- // CU then add the dwo id to it.
- DwarfCompileUnit *SkCU = TheU->getSkeleton();
- if (useSplitDwarf()) {
- // Emit a unique identifier for this CU.
- uint64_t ID = DIEHash(Asm).computeCUSignature(TheU->getUnitDie());
- TheU->addUInt(TheU->getUnitDie(), dwarf::DW_AT_GNU_dwo_id,
- dwarf::DW_FORM_data8, ID);
- SkCU->addUInt(SkCU->getUnitDie(), dwarf::DW_AT_GNU_dwo_id,
- dwarf::DW_FORM_data8, ID);
-
- // We don't keep track of which addresses are used in which CU so this
- // is a bit pessimistic under LTO.
- if (!AddrPool.isEmpty())
- SkCU->addSectionLabel(SkCU->getUnitDie(), dwarf::DW_AT_GNU_addr_base,
- DwarfAddrSectionSym, DwarfAddrSectionSym);
- if (!TheU->getRangeLists().empty())
- SkCU->addSectionLabel(
- SkCU->getUnitDie(), dwarf::DW_AT_GNU_ranges_base,
- DwarfDebugRangeSectionSym, DwarfDebugRangeSectionSym);
- }
+ // If we're splitting the dwarf out now that we've got the entire
+ // CU then add the dwo id to it.
+ auto *SkCU = TheCU.getSkeleton();
+ if (useSplitDwarf()) {
+ // Emit a unique identifier for this CU.
+ uint64_t ID = DIEHash(Asm).computeCUSignature(TheCU.getUnitDie());
+ TheCU.addUInt(TheCU.getUnitDie(), dwarf::DW_AT_GNU_dwo_id,
+ dwarf::DW_FORM_data8, ID);
+ SkCU->addUInt(SkCU->getUnitDie(), dwarf::DW_AT_GNU_dwo_id,
+ dwarf::DW_FORM_data8, ID);
+
+ // We don't keep track of which addresses are used in which CU so this
+ // is a bit pessimistic under LTO.
+ if (!AddrPool.isEmpty())
+ SkCU->addSectionLabel(SkCU->getUnitDie(), dwarf::DW_AT_GNU_addr_base,
+ DwarfAddrSectionSym, DwarfAddrSectionSym);
+ if (!SkCU->getRangeLists().empty())
+ SkCU->addSectionLabel(SkCU->getUnitDie(), dwarf::DW_AT_GNU_ranges_base,
+ DwarfDebugRangeSectionSym,
+ DwarfDebugRangeSectionSym);
+ }
- // If we have code split among multiple sections or non-contiguous
- // ranges of code then emit a DW_AT_ranges attribute on the unit that will
- // remain in the .o file, otherwise add a DW_AT_low_pc.
- // FIXME: We should use ranges allow reordering of code ala
- // .subsections_via_symbols in mach-o. This would mean turning on
- // ranges for all subprogram DIEs for mach-o.
- DwarfCompileUnit &U =
- SkCU ? *SkCU : static_cast<DwarfCompileUnit &>(*TheU);
- unsigned NumRanges = TheU->getRanges().size();
- if (NumRanges) {
- if (NumRanges > 1) {
- U.addSectionLabel(U.getUnitDie(), dwarf::DW_AT_ranges,
- Asm->GetTempSymbol("cu_ranges", U.getUniqueID()),
- DwarfDebugRangeSectionSym);
-
- // A DW_AT_low_pc attribute may also be specified in combination with
- // DW_AT_ranges to specify the default base address for use in
- // location lists (see Section 2.6.2) and range lists (see Section
- // 2.17.3).
- U.addUInt(U.getUnitDie(), dwarf::DW_AT_low_pc, dwarf::DW_FORM_addr,
- 0);
- } else {
- RangeSpan &Range = TheU->getRanges().back();
- U.attachLowHighPC(U.getUnitDie(), Range.getStart(), Range.getEnd());
- }
- }
+ // If we have code split among multiple sections or non-contiguous
+ // ranges of code then emit a DW_AT_ranges attribute on the unit that will
+ // remain in the .o file, otherwise add a DW_AT_low_pc.
+ // FIXME: We should use ranges allow reordering of code ala
+ // .subsections_via_symbols in mach-o. This would mean turning on
+ // ranges for all subprogram DIEs for mach-o.
+ DwarfCompileUnit &U = SkCU ? *SkCU : TheCU;
+ if (unsigned NumRanges = TheCU.getRanges().size()) {
+ if (NumRanges > 1)
+ // A DW_AT_low_pc attribute may also be specified in combination with
+ // DW_AT_ranges to specify the default base address for use in
+ // location lists (see Section 2.6.2) and range lists (see Section
+ // 2.17.3).
+ U.addUInt(U.getUnitDie(), dwarf::DW_AT_low_pc, dwarf::DW_FORM_addr, 0);
+ else
+ TheCU.setBaseAddress(TheCU.getRanges().front().getStart());
+ U.attachRangesOrLowHighPC(U.getUnitDie(), TheCU.takeRanges());
}
}
for (unsigned i = 0, e = Variables.getNumElements(); i != e; ++i) {
DIVariable DV(Variables.getElement(i));
assert(DV.isVariable());
- if (!Processed.insert(DV))
+ if (!Processed.insert(DV).second)
continue;
if (LexicalScope *Scope = LScopes.findLexicalScope(DV.getContext())) {
ensureAbstractVariableIsCreatedIfScoped(DV, Scope->getScopeNode());
if (DL == PrologEndLoc) {
Flags |= DWARF2_FLAG_PROLOGUE_END;
PrologEndLoc = DebugLoc();
+ Flags |= DWARF2_FLAG_IS_STMT;
}
- if (PrologEndLoc.isUnknown())
+ if (DL.getLine() !=
+ Asm->OutStreamer.getContext().getCurrentDwarfLoc().getLine())
Flags |= DWARF2_FLAG_IS_STMT;
if (!DL.isUnknown()) {
for (const auto &MBB : *MF)
for (const auto &MI : MBB)
if (!MI.isDebugValue() && !MI.getFlag(MachineInstr::FrameSetup) &&
- !MI.getDebugLoc().isUnknown())
+ !MI.getDebugLoc().isUnknown()) {
+ // Did the target forget to set the FrameSetup flag for CFI insns?
+ assert(!MI.isCFIInstruction() &&
+ "First non-frame-setup instruction is a CFI instruction.");
return MI.getDebugLoc();
+ }
return DebugLoc();
}
for (unsigned i = 0, e = Variables.getNumElements(); i != e; ++i) {
DIVariable DV(Variables.getElement(i));
assert(DV && DV.isVariable());
- if (!ProcessedVars.insert(DV))
+ if (!ProcessedVars.insert(DV).second)
continue;
ensureAbstractVariableIsCreated(DV, DV.getContext());
assert(LScopes.getAbstractScopesList().size() == NumAbstractScopes
}
TheCU.constructSubprogramScopeDIE(FnScope);
+ if (auto *SkelCU = TheCU.getSkeleton())
+ if (!LScopes.getAbstractScopesList().empty())
+ SkelCU->constructSubprogramScopeDIE(FnScope);
// Clear debug info
// Ownership of DbgVariables is a bit subtle - ScopeVariables owns all the
Asm->OutStreamer.EmitLabel(SectionBegin);
// Emit the full data.
- Accel.Emit(Asm, SectionBegin, &InfoHolder, DwarfStrSectionSym);
+ Accel.Emit(Asm, SectionBegin, this, DwarfStrSectionSym);
}
// Emit visible names into a hashed accelerator table section.
GnuStyle ? Asm->getObjFileLowering().getDwarfGnuPubNamesSection()
: Asm->getObjFileLowering().getDwarfPubNamesSection();
- emitDebugPubSection(GnuStyle, PSec, "Names", &DwarfUnit::getGlobalNames);
+ emitDebugPubSection(GnuStyle, PSec, "Names",
+ &DwarfCompileUnit::getGlobalNames);
}
void DwarfDebug::emitDebugPubSection(
bool GnuStyle, const MCSection *PSec, StringRef Name,
- const StringMap<const DIE *> &(DwarfUnit::*Accessor)() const) {
+ const StringMap<const DIE *> &(DwarfCompileUnit::*Accessor)() const) {
for (const auto &NU : CUMap) {
DwarfCompileUnit *TheU = NU.second;
Asm->EmitSectionOffset(TheU->getLabelBegin(), TheU->getSectionSym());
Asm->OutStreamer.AddComment("Compilation Unit Length");
- Asm->EmitLabelDifference(TheU->getLabelEnd(), TheU->getLabelBegin(), 4);
+ Asm->EmitInt32(TheU->getLength());
// Emit the pubnames for this compilation unit.
for (const auto &GI : Globals) {
GnuStyle ? Asm->getObjFileLowering().getDwarfGnuPubTypesSection()
: Asm->getObjFileLowering().getDwarfPubTypesSection();
- emitDebugPubSection(GnuStyle, PSec, "Types", &DwarfUnit::getGlobalTypes);
+ emitDebugPubSection(GnuStyle, PSec, "Types",
+ &DwarfCompileUnit::getGlobalTypes);
}
// Emit visible names into a debug str section.
void DwarfDebug::emitDebugLocValue(ByteStreamer &Streamer,
const DebugLocEntry::Value &Value) {
DIVariable DV = Value.getVariable();
+ DebugLocDwarfExpression Expr(*Asm, Streamer);
// Regular entry.
if (Value.isInt()) {
DIBasicType BTy(resolve(DV.getType()));
if (BTy.Verify() && (BTy.getEncoding() == dwarf::DW_ATE_signed ||
- BTy.getEncoding() == dwarf::DW_ATE_signed_char)) {
- Streamer.EmitInt8(dwarf::DW_OP_consts, "DW_OP_consts");
- Streamer.EmitSLEB128(Value.getInt());
- } else {
- Streamer.EmitInt8(dwarf::DW_OP_constu, "DW_OP_constu");
- Streamer.EmitULEB128(Value.getInt());
- }
+ BTy.getEncoding() == dwarf::DW_ATE_signed_char))
+ Expr.AddSignedConstant(Value.getInt());
+ else
+ Expr.AddUnsignedConstant(Value.getInt());
} else if (Value.isLocation()) {
MachineLocation Loc = Value.getLoc();
DIExpression Expr = Value.getExpression();
for (const auto &DebugLoc : DotDebugLocEntries) {
Asm->OutStreamer.EmitLabel(DebugLoc.Label);
const DwarfCompileUnit *CU = DebugLoc.CU;
- assert(!CU->getRanges().empty());
for (const auto &Entry : DebugLoc.List) {
// Set up the range. This range is relative to the entry point of the
// compile unit. This is a hard coded 0 for low_pc when we're emitting
// ranges, or the DW_AT_low_pc on the compile unit otherwise.
- if (CU->getRanges().size() == 1) {
- // Grab the begin symbol from the first range as our base.
- const MCSymbol *Base = CU->getRanges()[0].getStart();
+ if (auto *Base = CU->getBaseAddress()) {
Asm->EmitLabelDifference(Entry.getBeginSym(), Base, Size);
Asm->EmitLabelDifference(Entry.getEndSym(), Base, Size);
} else {
for (DwarfCompileUnit *CU : CUs) {
std::vector<ArangeSpan> &List = Spans[CU];
+ // Describe the skeleton CU's offset and length, not the dwo file's.
+ if (auto *Skel = CU->getSkeleton())
+ CU = Skel;
+
// Emit size of content not including length itself.
unsigned ContentSize =
sizeof(int16_t) + // DWARF ARange version number
Asm->OutStreamer.AddComment("DWARF Arange version number");
Asm->EmitInt16(dwarf::DW_ARANGES_VERSION);
Asm->OutStreamer.AddComment("Offset Into Debug Info Section");
- Asm->EmitSectionOffset(CU->getLocalLabelBegin(), CU->getLocalSectionSym());
+ Asm->EmitSectionOffset(CU->getLabelBegin(), CU->getSectionSym());
Asm->OutStreamer.AddComment("Address Size (in bytes)");
Asm->EmitInt8(PtrSize);
Asm->OutStreamer.AddComment("Segment Size (in bytes)");
for (const auto &I : CUMap) {
DwarfCompileUnit *TheCU = I.second;
+ if (auto *Skel = TheCU->getSkeleton())
+ TheCU = Skel;
+
// Iterate over the misc ranges for the compile units in the module.
for (const RangeSpanList &List : TheCU->getRangeLists()) {
// Emit our symbol so we can find the beginning of the range.
const MCSymbol *End = Range.getEnd();
assert(Begin && "Range without a begin symbol?");
assert(End && "Range without an end symbol?");
- if (TheCU->getRanges().size() == 1) {
- // Grab the begin symbol from the first range as our base.
- const MCSymbol *Base = TheCU->getRanges()[0].getStart();
+ if (auto *Base = TheCU->getBaseAddress()) {
Asm->EmitLabelDifference(Begin, Base, Size);
Asm->EmitLabelDifference(End, Base, Size);
} else {
Asm->OutStreamer.EmitIntValue(0, Size);
Asm->OutStreamer.EmitIntValue(0, Size);
}
-
- // Now emit a range for the CU itself.
- if (TheCU->getRanges().size() > 1) {
- Asm->OutStreamer.EmitLabel(
- Asm->GetTempSymbol("cu_ranges", TheCU->getUniqueID()));
- for (const RangeSpan &Range : TheCU->getRanges()) {
- const MCSymbol *Begin = Range.getStart();
- const MCSymbol *End = Range.getEnd();
- assert(Begin && "Range without a begin symbol?");
- assert(End && "Range without an end symbol?");
- Asm->OutStreamer.EmitSymbolValue(Begin, Size);
- Asm->OutStreamer.EmitSymbolValue(End, Size);
- }
- // And terminate the list with two 0 values.
- Asm->OutStreamer.EmitIntValue(0, Size);
- Asm->OutStreamer.EmitIntValue(0, Size);
- }
}
}
void DwarfDebug::initSkeletonUnit(const DwarfUnit &U, DIE &Die,
std::unique_ptr<DwarfUnit> NewU) {
- NewU->addLocalString(Die, dwarf::DW_AT_GNU_dwo_name,
- U.getCUNode().getSplitDebugFilename());
+ NewU->addString(Die, dwarf::DW_AT_GNU_dwo_name,
+ U.getCUNode().getSplitDebugFilename());
if (!CompilationDir.empty())
- NewU->addLocalString(Die, dwarf::DW_AT_comp_dir, CompilationDir);
+ NewU->addString(Die, dwarf::DW_AT_comp_dir, CompilationDir);
addGnuPubAttributes(*NewU, Die);
NewTU.setTypeSignature(Signature);
if (useSplitDwarf())
- NewTU.initSection(Asm->getObjFileLowering().getDwarfTypesDWOSection(),
- DwarfTypesDWOSectionSym);
+ NewTU.initSection(Asm->getObjFileLowering().getDwarfTypesDWOSection());
else {
CU.applyStmtList(UnitDie);
NewTU.initSection(