index c0b8044ba17fb4830c04bb299da949c319544df8..f78ca2c03b4ec247a29ce4e2ee141318da349244 100644 (file)
clEnumVal(Disable, "Disabled"), clEnumValEnd),
cl::init(Default));
-static cl::opt<unsigned>
-DwarfVersionNumber("dwarf-version", cl::Hidden,
- cl::desc("Generate DWARF for dwarf version."), cl::init(0));
-
static const char *const DWARFGroupName = "DWARF Emission";
static const char *const DbgTimerName = "DWARF Debug Writer";
return Var.isBlockByrefVariable(DD->getTypeIdentifierMap());
}
-
DIType DbgVariable::getType() const {
DIType Ty = Var.getType().resolve(DD->getTypeIdentifierMap());
// FIXME: isBlockByrefVariable should be reformulated in terms of complex
else
HasDwarfPubSections = DwarfPubSections == Enable;
- DwarfVersion = DwarfVersionNumber
- ? DwarfVersionNumber
- : MMI->getModule()->getDwarfVersion();
+ unsigned DwarfVersionNumber = Asm->TM.Options.MCOptions.DwarfVersion;
+ DwarfVersion = DwarfVersionNumber ? DwarfVersionNumber
+ : MMI->getModule()->getDwarfVersion();
+
+ Asm->OutStreamer.getContext().setDwarfVersion(DwarfVersion);
{
NamedRegionTimer T(DbgTimerName, DWARFGroupName, TimePassesIsEnabled);
}
}
+// Define out of line so we don't have to include DwarfUnit.h in DwarfDebug.h.
+DwarfDebug::~DwarfDebug() { }
+
// Switch to the specified MCSection and emit an assembler
// temporary label to it if SymbolStem is specified.
static MCSymbol *emitSectionSym(AsmPrinter *Asm, const MCSection *Section,
// Find DIE for the given subprogram and attach appropriate DW_AT_low_pc
// and DW_AT_high_pc attributes. If there are global variables in this
// scope then create and insert DIEs for these variables.
-DIE *DwarfDebug::updateSubprogramScopeDIE(DwarfCompileUnit &SPCU,
+DIE &DwarfDebug::updateSubprogramScopeDIE(DwarfCompileUnit &SPCU,
DISubprogram SP) {
- DIE *SPDie = SPCU.getDIE(SP);
-
- assert(SPDie && "Unable to find subprogram DIE!");
-
- // If we're updating an abstract DIE, then we will be adding the children and
- // object pointer later on. But what we don't want to do is process the
- // concrete DIE twice.
- if (DIE *AbsSPDIE = AbstractSPDies.lookup(SP)) {
- // Pick up abstract subprogram DIE.
- SPDie = &SPCU.createAndAddDIE(dwarf::DW_TAG_subprogram, SPCU.getUnitDie());
- SPCU.addDIEEntry(*SPDie, dwarf::DW_AT_abstract_origin, *AbsSPDIE);
- } else {
- DISubprogram SPDecl = SP.getFunctionDeclaration();
- if (!SPDecl.isSubprogram()) {
- // There is not any need to generate specification DIE for a function
- // defined at compile unit level. If a function is defined inside another
- // function then gdb prefers the definition at top level and but does not
- // expect specification DIE in parent function. So avoid creating
- // specification DIE for a function defined inside a function.
- DIScope SPContext = resolve(SP.getContext());
- if (SP.isDefinition() && !SPContext.isCompileUnit() &&
- !SPContext.isFile() && !isSubprogramContext(SPContext)) {
- SPCU.addFlag(*SPDie, dwarf::DW_AT_declaration);
-
- // Add arguments.
- DICompositeType SPTy = SP.getType();
- DIArray Args = SPTy.getTypeArray();
- uint16_t SPTag = SPTy.getTag();
- if (SPTag == dwarf::DW_TAG_subroutine_type)
- SPCU.constructSubprogramArguments(*SPDie, Args);
- DIE *SPDeclDie = SPDie;
- SPDie =
- &SPCU.createAndAddDIE(dwarf::DW_TAG_subprogram, SPCU.getUnitDie());
- SPCU.addDIEEntry(*SPDie, dwarf::DW_AT_specification, *SPDeclDie);
- }
- }
- }
+ DIE *SPDie = SPCU.getOrCreateSubprogramDIE(SP);
attachLowHighPC(SPCU, *SPDie, FunctionBeginSym, FunctionEndSym);
// to have concrete versions of our DW_TAG_subprogram nodes.
addSubprogramNames(SP, *SPDie);
- return SPDie;
+ return *SPDie;
}
/// Check whether we should create a DIE for the given Scope, return true
TheCU.addRangeList(std::move(List));
}
+void DwarfDebug::attachRangesOrLowHighPC(DwarfCompileUnit &TheCU, DIE &Die,
+ const SmallVectorImpl<InsnRange> &Ranges) {
+ assert(!Ranges.empty());
+ if (Ranges.size() == 1)
+ attachLowHighPC(TheCU, Die, getLabelBeforeInsn(Ranges.front().first),
+ getLabelAfterInsn(Ranges.front().second));
+ else
+ addScopeRangeList(TheCU, Die, Ranges);
+}
+
// Construct new DW_TAG_lexical_block for this scope and attach
// DW_AT_low_pc/DW_AT_high_pc labels.
-DIE *DwarfDebug::constructLexicalScopeDIE(DwarfCompileUnit &TheCU,
- LexicalScope *Scope) {
+std::unique_ptr<DIE>
+DwarfDebug::constructLexicalScopeDIE(DwarfCompileUnit &TheCU,
+ LexicalScope *Scope) {
if (isLexicalScopeDIENull(Scope))
return nullptr;
- DIE *ScopeDIE = new DIE(dwarf::DW_TAG_lexical_block);
+ auto ScopeDIE = make_unique<DIE>(dwarf::DW_TAG_lexical_block);
if (Scope->isAbstractScope())
return ScopeDIE;
- const SmallVectorImpl<InsnRange> &ScopeRanges = Scope->getRanges();
-
- // If we have multiple ranges, emit them into the range section.
- if (ScopeRanges.size() > 1) {
- addScopeRangeList(TheCU, *ScopeDIE, ScopeRanges);
- return ScopeDIE;
- }
-
- // Construct the address range for this DIE.
- SmallVectorImpl<InsnRange>::const_iterator RI = ScopeRanges.begin();
- MCSymbol *Start = getLabelBeforeInsn(RI->first);
- MCSymbol *End = getLabelAfterInsn(RI->second);
- assert(End && "End label should not be null!");
-
- assert(Start->isDefined() && "Invalid starting label for an inlined scope!");
- assert(End->isDefined() && "Invalid end label for an inlined scope!");
-
- attachLowHighPC(TheCU, *ScopeDIE, Start, End);
+ attachRangesOrLowHighPC(TheCU, *ScopeDIE, Scope->getRanges());
return ScopeDIE;
}
// This scope represents inlined body of a function. Construct DIE to
// represent this concrete inlined copy of the function.
-DIE *DwarfDebug::constructInlinedScopeDIE(DwarfCompileUnit &TheCU,
- LexicalScope *Scope) {
- const SmallVectorImpl<InsnRange> &ScopeRanges = Scope->getRanges();
- assert(!ScopeRanges.empty() &&
- "LexicalScope does not have instruction markers!");
-
- if (!Scope->getScopeNode())
- return nullptr;
+std::unique_ptr<DIE>
+DwarfDebug::constructInlinedScopeDIE(DwarfCompileUnit &TheCU,
+ LexicalScope *Scope) {
+ assert(Scope->getScopeNode());
DIScope DS(Scope->getScopeNode());
DISubprogram InlinedSP = getDISubprogram(DS);
- DIE *OriginDIE = TheCU.getDIE(InlinedSP);
- if (!OriginDIE) {
- DEBUG(dbgs() << "Unable to find original DIE for an inlined subprogram.");
- return nullptr;
- }
+ // Find the subprogram's DwarfCompileUnit in the SPMap in case the subprogram
+ // was inlined from another compile unit.
+ DIE *OriginDIE = AbstractSPDies[InlinedSP];
+ assert(OriginDIE && "Unable to find original DIE for an inlined subprogram.");
- DIE *ScopeDIE = new DIE(dwarf::DW_TAG_inlined_subroutine);
+ auto ScopeDIE = make_unique<DIE>(dwarf::DW_TAG_inlined_subroutine);
TheCU.addDIEEntry(*ScopeDIE, dwarf::DW_AT_abstract_origin, *OriginDIE);
- // If we have multiple ranges, emit them into the range section.
- if (ScopeRanges.size() > 1)
- addScopeRangeList(TheCU, *ScopeDIE, ScopeRanges);
- else {
- SmallVectorImpl<InsnRange>::const_iterator RI = ScopeRanges.begin();
- MCSymbol *StartLabel = getLabelBeforeInsn(RI->first);
- MCSymbol *EndLabel = getLabelAfterInsn(RI->second);
-
- if (!StartLabel || !EndLabel)
- llvm_unreachable("Unexpected Start and End labels for an inlined scope!");
-
- assert(StartLabel->isDefined() &&
- "Invalid starting label for an inlined scope!");
- assert(EndLabel->isDefined() && "Invalid end label for an inlined scope!");
-
- attachLowHighPC(TheCU, *ScopeDIE, StartLabel, EndLabel);
- }
+ attachRangesOrLowHighPC(TheCU, *ScopeDIE, Scope->getRanges());
InlinedSubprogramDIEs.insert(OriginDIE);
return ScopeDIE;
}
+static std::unique_ptr<DIE> constructVariableDIE(DwarfCompileUnit &TheCU,
+ DbgVariable &DV,
+ const LexicalScope &Scope,
+ DIE *&ObjectPointer) {
+ auto Var = TheCU.constructVariableDIE(DV, Scope.isAbstractScope());
+ if (DV.isObjectPointer())
+ ObjectPointer = Var.get();
+ return Var;
+}
+
DIE *DwarfDebug::createScopeChildrenDIE(
DwarfCompileUnit &TheCU, LexicalScope *Scope,
SmallVectorImpl<std::unique_ptr<DIE>> &Children) {
// Collect arguments for current function.
if (LScopes.isCurrentFunctionScope(Scope)) {
for (DbgVariable *ArgDV : CurrentFnArguments)
- if (ArgDV) {
+ if (ArgDV)
Children.push_back(
- TheCU.constructVariableDIE(*ArgDV, Scope->isAbstractScope()));
- if (ArgDV->isObjectPointer())
- ObjectPointer = Children.back().get();
- }
+ constructVariableDIE(TheCU, *ArgDV, *Scope, ObjectPointer));
// If this is a variadic function, add an unspecified parameter.
DISubprogram SP(Scope->getScopeNode());
}
// Collect lexical scope children first.
- for (DbgVariable *DV : ScopeVariables.lookup(Scope)) {
- Children.push_back(
- TheCU.constructVariableDIE(*DV, Scope->isAbstractScope()));
- if (DV->isObjectPointer())
- ObjectPointer = Children.back().get();
- }
+ for (DbgVariable *DV : ScopeVariables.lookup(Scope))
+ Children.push_back(constructVariableDIE(TheCU, *DV, *Scope, ObjectPointer));
+
for (LexicalScope *LS : Scope->getChildren())
- if (DIE *Nested = constructScopeDIE(TheCU, LS))
- Children.push_back(std::unique_ptr<DIE>(Nested));
+ if (std::unique_ptr<DIE> Nested = constructScopeDIE(TheCU, LS))
+ Children.push_back(std::move(Nested));
return ObjectPointer;
}
-DIE *DwarfDebug::constructSubprogramScopeDIE(DwarfCompileUnit &TheCU, LexicalScope *Scope) {
- assert(Scope && Scope->getScopeNode());
+void DwarfDebug::createAndAddScopeChildren(DwarfCompileUnit &TheCU,
+ LexicalScope *Scope, DIE &ScopeDIE) {
+ // We create children when the scope DIE is not null.
+ SmallVector<std::unique_ptr<DIE>, 8> Children;
+ if (DIE *ObjectPointer = createScopeChildrenDIE(TheCU, Scope, Children))
+ TheCU.addDIEEntry(ScopeDIE, dwarf::DW_AT_object_pointer, *ObjectPointer);
- DIScope DS(Scope->getScopeNode());
+ // Add children
+ for (auto &I : Children)
+ ScopeDIE.addChild(std::move(I));
+}
+void DwarfDebug::constructAbstractSubprogramScopeDIE(DwarfCompileUnit &TheCU,
+ LexicalScope *Scope) {
+ assert(Scope && Scope->getScopeNode());
+ assert(Scope->isAbstractScope());
assert(!Scope->getInlinedAt());
- assert(DS.isSubprogram());
- ProcessedSPNodes.insert(DS);
+ DISubprogram SP(Scope->getScopeNode());
- SmallVector<std::unique_ptr<DIE>, 8> Children;
- DIE *ScopeDIE;
+ ProcessedSPNodes.insert(SP);
- if (Scope->isAbstractScope()) {
- ScopeDIE = TheCU.getDIE(DS);
- // Note down abstract DIE.
- if (ScopeDIE)
- AbstractSPDies.insert(std::make_pair(DS, ScopeDIE));
- else {
- assert(Children.empty() &&
- "We create children only when the scope DIE is not null.");
- return nullptr;
- }
+ DIE *&AbsDef = AbstractSPDies[SP];
+ if (AbsDef)
+ return;
+
+ // Find the subprogram's DwarfCompileUnit in the SPMap in case the subprogram
+ // was inlined from another compile unit.
+ DwarfCompileUnit &SPCU = *SPMap[SP];
+ DIE *ContextDIE;
+
+ // Some of this is duplicated from DwarfUnit::getOrCreateSubprogramDIE, with
+ // the important distinction that the DIDescriptor is not associated with the
+ // DIE (since the DIDescriptor will be associated with the concrete DIE, if
+ // any). It could be refactored to some common utility function.
+ if (DISubprogram SPDecl = SP.getFunctionDeclaration()) {
+ ContextDIE = &SPCU.getUnitDie();
+ SPCU.getOrCreateSubprogramDIE(SPDecl);
} else
- ScopeDIE = updateSubprogramScopeDIE(TheCU, DISubprogram(DS));
+ ContextDIE = SPCU.getOrCreateContextDIE(resolve(SP.getContext()));
- // We create children when the scope DIE is not null.
- if (DIE *ObjectPointer = createScopeChildrenDIE(TheCU, Scope, Children))
- TheCU.addDIEEntry(*ScopeDIE, dwarf::DW_AT_object_pointer, *ObjectPointer);
+ // Passing null as the associated DIDescriptor because the abstract definition
+ // shouldn't be found by lookup.
+ AbsDef = &SPCU.createAndAddDIE(dwarf::DW_TAG_subprogram, *ContextDIE,
+ DIDescriptor());
+ SPCU.applySubprogramAttributesToDefinition(SP, *AbsDef);
- // Add children
- for (auto &I : Children)
- ScopeDIE->addChild(std::move(I));
+ SPCU.addUInt(*AbsDef, dwarf::DW_AT_inline, None, dwarf::DW_INL_inlined);
+ createAndAddScopeChildren(SPCU, Scope, *AbsDef);
+}
+
+DIE &DwarfDebug::constructSubprogramScopeDIE(DwarfCompileUnit &TheCU,
+ LexicalScope *Scope) {
+ assert(Scope && Scope->getScopeNode());
+ assert(!Scope->getInlinedAt());
+ assert(!Scope->isAbstractScope());
+ DISubprogram Sub(Scope->getScopeNode());
+
+ assert(Sub.isSubprogram());
+
+ ProcessedSPNodes.insert(Sub);
+
+ DIE &ScopeDIE = updateSubprogramScopeDIE(TheCU, Sub);
+
+ createAndAddScopeChildren(TheCU, Scope, ScopeDIE);
return ScopeDIE;
}
// Construct a DIE for this scope.
-DIE *DwarfDebug::constructScopeDIE(DwarfCompileUnit &TheCU,
- LexicalScope *Scope) {
+std::unique_ptr<DIE> DwarfDebug::constructScopeDIE(DwarfCompileUnit &TheCU,
+ LexicalScope *Scope) {
if (!Scope || !Scope->getScopeNode())
return nullptr;
DIScope DS(Scope->getScopeNode());
- assert(Scope->getInlinedAt() ||
- !DS.isSubprogram() && "Only handle inlined subprograms here, use "
- "constructSubprogramScopeDIE for non-inlined "
- "subprograms");
+ assert((Scope->getInlinedAt() || !DS.isSubprogram()) &&
+ "Only handle inlined subprograms here, use "
+ "constructSubprogramScopeDIE for non-inlined "
+ "subprograms");
SmallVector<std::unique_ptr<DIE>, 8> Children;
// We try to create the scope DIE first, then the children DIEs. This will
// avoid creating un-used children then removing them later when we find out
// the scope DIE is null.
- DIE *ScopeDIE = nullptr;
- if (Scope->getInlinedAt()) {
+ std::unique_ptr<DIE> ScopeDIE;
+ if (Scope->getParent() && DS.isSubprogram()) {
ScopeDIE = constructInlinedScopeDIE(TheCU, Scope);
if (!ScopeDIE)
return nullptr;
// There is no need to emit empty lexical block DIE.
std::pair<ImportedEntityMap::const_iterator,
ImportedEntityMap::const_iterator> Range =
- std::equal_range(
- ScopesWithImportedEntities.begin(),
- ScopesWithImportedEntities.end(),
- std::pair<const MDNode *, const MDNode *>(DS, nullptr),
- less_first());
+ std::equal_range(ScopesWithImportedEntities.begin(),
+ ScopesWithImportedEntities.end(),
+ std::pair<const MDNode *, const MDNode *>(DS, nullptr),
+ less_first());
if (Children.empty() && Range.first == Range.second)
return nullptr;
ScopeDIE = constructLexicalScopeDIE(TheCU, Scope);
assert(ScopeDIE && "Scope DIE should not be null.");
for (ImportedEntityMap::const_iterator i = Range.first; i != Range.second;
++i)
- constructImportedEntityDIE(TheCU, i->second, ScopeDIE);
-
+ constructImportedEntityDIE(TheCU, i->second, *ScopeDIE);
}
// Add children
@@ -653,10 +624,10 @@ DwarfCompileUnit &DwarfDebug::constructDwarfCompileUnit(DICompileUnit DIUnit) {
StringRef FN = DIUnit.getFilename();
CompilationDir = DIUnit.getDirectory();
- DIE *Die = new DIE(dwarf::DW_TAG_compile_unit);
auto OwnedUnit = make_unique<DwarfCompileUnit>(
- InfoHolder.getUnits().size(), Die, DIUnit, Asm, this, &InfoHolder);
+ InfoHolder.getUnits().size(), DIUnit, Asm, this, &InfoHolder);
DwarfCompileUnit &NewCU = *OwnedUnit;
+ DIE &Die = NewCU.getUnitDie();
InfoHolder.addUnit(std::move(OwnedUnit));
// LTO with assembly output shares a single line table amongst multiple CUs.
@@ -667,10 +638,10 @@ DwarfCompileUnit &DwarfDebug::constructDwarfCompileUnit(DICompileUnit DIUnit) {
Asm->OutStreamer.getContext().setMCLineTableCompilationDir(
NewCU.getUniqueID(), CompilationDir);
- NewCU.addString(*Die, dwarf::DW_AT_producer, DIUnit.getProducer());
- NewCU.addUInt(*Die, dwarf::DW_AT_language, dwarf::DW_FORM_data2,
+ NewCU.addString(Die, dwarf::DW_AT_producer, DIUnit.getProducer());
+ NewCU.addUInt(Die, dwarf::DW_AT_language, dwarf::DW_FORM_data2,
DIUnit.getLanguage());
- NewCU.addString(*Die, dwarf::DW_AT_name, FN);
+ NewCU.addString(Die, dwarf::DW_AT_name, FN);
if (!useSplitDwarf()) {
NewCU.initStmtList(DwarfLineSectionSym);
@@ -678,20 +649,20 @@ DwarfCompileUnit &DwarfDebug::constructDwarfCompileUnit(DICompileUnit DIUnit) {
// If we're using split dwarf the compilation dir is going to be in the
// skeleton CU and so we don't need to duplicate it here.
if (!CompilationDir.empty())
- NewCU.addString(*Die, dwarf::DW_AT_comp_dir, CompilationDir);
+ NewCU.addString(Die, dwarf::DW_AT_comp_dir, CompilationDir);
- addGnuPubAttributes(NewCU, *Die);
+ addGnuPubAttributes(NewCU, Die);
}
if (DIUnit.isOptimized())
- NewCU.addFlag(*Die, dwarf::DW_AT_APPLE_optimized);
+ NewCU.addFlag(Die, dwarf::DW_AT_APPLE_optimized);
StringRef Flags = DIUnit.getFlags();
if (!Flags.empty())
- NewCU.addString(*Die, dwarf::DW_AT_APPLE_flags, Flags);
+ NewCU.addString(Die, dwarf::DW_AT_APPLE_flags, Flags);
if (unsigned RVer = DIUnit.getRunTimeVersion())
- NewCU.addUInt(*Die, dwarf::DW_AT_APPLE_major_runtime_vers,
+ NewCU.addUInt(Die, dwarf::DW_AT_APPLE_major_runtime_vers,
dwarf::DW_FORM_data1, RVer);
if (!FirstCU)
@@ -706,44 +677,20 @@ DwarfCompileUnit &DwarfDebug::constructDwarfCompileUnit(DICompileUnit DIUnit) {
DwarfInfoSectionSym);
CUMap.insert(std::make_pair(DIUnit, &NewCU));
- CUDieMap.insert(std::make_pair(Die, &NewCU));
+ CUDieMap.insert(std::make_pair(&Die, &NewCU));
return NewCU;
}
-// Construct subprogram DIE.
-void DwarfDebug::constructSubprogramDIE(DwarfCompileUnit &TheCU,
- const MDNode *N) {
- // FIXME: We should only call this routine once, however, during LTO if a
- // program is defined in multiple CUs we could end up calling it out of
- // beginModule as we walk the CUs.
-
- DwarfCompileUnit *&CURef = SPMap[N];
- if (CURef)
- return;
- CURef = &TheCU;
-
- DISubprogram SP(N);
- if (!SP.isDefinition())
- // This is a method declaration which will be handled while constructing
- // class type.
- return;
-
- DIE &SubprogramDie = *TheCU.getOrCreateSubprogramDIE(SP);
-
- // Expose as a global name.
- TheCU.addGlobalName(SP.getName(), SubprogramDie, resolve(SP.getContext()));
-}
-
void DwarfDebug::constructImportedEntityDIE(DwarfCompileUnit &TheCU,
const MDNode *N) {
DIImportedEntity Module(N);
assert(Module.Verify());
if (DIE *D = TheCU.getOrCreateContextDIE(Module.getContext()))
- constructImportedEntityDIE(TheCU, Module, D);
+ constructImportedEntityDIE(TheCU, Module, *D);
}
void DwarfDebug::constructImportedEntityDIE(DwarfCompileUnit &TheCU,
- const MDNode *N, DIE *Context) {
+ const MDNode *N, DIE &Context) {
DIImportedEntity Module(N);
assert(Module.Verify());
return constructImportedEntityDIE(TheCU, Module, Context);
void DwarfDebug::constructImportedEntityDIE(DwarfCompileUnit &TheCU,
const DIImportedEntity &Module,
- DIE *Context) {
+ DIE &Context) {
assert(Module.Verify() &&
"Use one of the MDNode * overloads to handle invalid metadata");
- assert(Context && "Should always have a context for an imported_module");
- DIE &IMDie = TheCU.createAndAddDIE(Module.getTag(), *Context, Module);
+ DIE &IMDie = TheCU.createAndAddDIE(Module.getTag(), Context, Module);
DIE *EntityDie;
DIDescriptor Entity = resolve(Module.getEntity());
if (Entity.isNameSpace())
CU.createGlobalVariableDIE(DIGlobalVariable(GVs.getElement(i)));
DIArray SPs = CUNode.getSubprograms();
for (unsigned i = 0, e = SPs.getNumElements(); i != e; ++i)
- constructSubprogramDIE(CU, SPs.getElement(i));
+ SPMap.insert(std::make_pair(SPs.getElement(i), &CU));
DIArray EnumTypes = CUNode.getEnumTypes();
for (unsigned i = 0, e = EnumTypes.getNumElements(); i != e; ++i)
CU.getOrCreateTypeDIE(EnumTypes.getElement(i));
SectionMap[Asm->getObjFileLowering().getTextSection()];
}
-// Attach DW_AT_inline attribute with inlined subprogram DIEs.
-void DwarfDebug::computeInlinedDIEs() {
- // Attach DW_AT_inline attribute with inlined subprogram DIEs.
- for (DIE *ISP : InlinedSubprogramDIEs)
- FirstCU->addUInt(*ISP, dwarf::DW_AT_inline, None, dwarf::DW_INL_inlined);
-
- for (const auto &AI : AbstractSPDies) {
- DIE &ISP = *AI.second;
- if (InlinedSubprogramDIEs.count(&ISP))
+void DwarfDebug::finishVariableDefinitions() {
+ for (const auto &Var : ConcreteVariables) {
+ DIE *VariableDie = Var->getDIE();
+ // FIXME: There shouldn't be any variables without DIEs.
+ if (!VariableDie)
continue;
- FirstCU->addUInt(ISP, dwarf::DW_AT_inline, None, dwarf::DW_INL_inlined);
+ // FIXME: Consider the time-space tradeoff of just storing the unit pointer
+ // in the ConcreteVariables list, rather than looking it up again here.
+ // DIE::getUnit isn't simple - it walks parent pointers, etc.
+ DwarfCompileUnit *Unit = lookupUnit(VariableDie->getUnit());
+ assert(Unit);
+ DbgVariable *AbsVar = getExistingAbstractVariable(Var->getVariable());
+ if (AbsVar && AbsVar->getDIE()) {
+ Unit->addDIEEntry(*VariableDie, dwarf::DW_AT_abstract_origin,
+ *AbsVar->getDIE());
+ } else
+ Unit->applyVariableAttributes(*Var, *VariableDie);
+ }
+}
+
+void DwarfDebug::finishSubprogramDefinitions() {
+ const Module *M = MMI->getModule();
+
+ NamedMDNode *CU_Nodes = M->getNamedMetadata("llvm.dbg.cu");
+ for (MDNode *N : CU_Nodes->operands()) {
+ DICompileUnit TheCU(N);
+ // Construct subprogram DIE and add variables DIEs.
+ DwarfCompileUnit *SPCU =
+ static_cast<DwarfCompileUnit *>(CUMap.lookup(TheCU));
+ DIArray Subprograms = TheCU.getSubprograms();
+ for (unsigned i = 0, e = Subprograms.getNumElements(); i != e; ++i) {
+ DISubprogram SP(Subprograms.getElement(i));
+ // Perhaps the subprogram is in another CU (such as due to comdat
+ // folding, etc), in which case ignore it here.
+ if (SPMap[SP] != SPCU)
+ continue;
+ DIE *D = SPCU->getDIE(SP);
+ if (DIE *AbsSPDIE = AbstractSPDies.lookup(SP)) {
+ if (D)
+ // If this subprogram has an abstract definition, reference that
+ SPCU->addDIEEntry(*D, dwarf::DW_AT_abstract_origin, *AbsSPDIE);
+ } else {
+ if (!D)
+ // Lazily construct the subprogram if we didn't see either concrete or
+ // inlined versions during codegen.
+ D = SPCU->getOrCreateSubprogramDIE(SP);
+ // And attach the attributes
+ SPCU->applySubprogramAttributesToDefinition(SP, *D);
+ }
+ }
}
}
+
// Collect info for variables that were optimized out.
void DwarfDebug::collectDeadVariables() {
const Module *M = MMI->getModule();
if (NamedMDNode *CU_Nodes = M->getNamedMetadata("llvm.dbg.cu")) {
for (MDNode *N : CU_Nodes->operands()) {
DICompileUnit TheCU(N);
+ // Construct subprogram DIE and add variables DIEs.
+ DwarfCompileUnit *SPCU =
+ static_cast<DwarfCompileUnit *>(CUMap.lookup(TheCU));
+ assert(SPCU && "Unable to find Compile Unit!");
DIArray Subprograms = TheCU.getSubprograms();
for (unsigned i = 0, e = Subprograms.getNumElements(); i != e; ++i) {
DISubprogram SP(Subprograms.getElement(i));
if (ProcessedSPNodes.count(SP) != 0)
continue;
- if (!SP.isSubprogram())
- continue;
- if (!SP.isDefinition())
- continue;
+ assert(SP.isSubprogram() &&
+ "CU's subprogram list contains a non-subprogram");
+ assert(SP.isDefinition() &&
+ "CU's subprogram list contains a subprogram declaration");
DIArray Variables = SP.getVariables();
if (Variables.getNumElements() == 0)
continue;
- // Construct subprogram DIE and add variables DIEs.
- DwarfCompileUnit *SPCU =
- static_cast<DwarfCompileUnit *>(CUMap.lookup(TheCU));
- assert(SPCU && "Unable to find Compile Unit!");
- // FIXME: See the comment in constructSubprogramDIE about duplicate
- // subprogram DIEs.
- constructSubprogramDIE(*SPCU, SP);
- DIE *SPDIE = SPCU->getDIE(SP);
+ DIE *SPDIE = AbstractSPDies.lookup(SP);
+ if (!SPDIE)
+ SPDIE = SPCU->getDIE(SP);
+ assert(SPDIE);
for (unsigned vi = 0, ve = Variables.getNumElements(); vi != ve; ++vi) {
DIVariable DV(Variables.getElement(vi));
- if (!DV.isVariable())
- continue;
- DbgVariable NewVar(DV, nullptr, this);
- SPDIE->addChild(SPCU->constructVariableDIE(NewVar, false));
+ assert(DV.isVariable());
+ DbgVariable NewVar(DV, this);
+ auto VariableDie = SPCU->constructVariableDIE(NewVar);
+ SPCU->applyVariableAttributes(NewVar, *VariableDie);
+ SPDIE->addChild(std::move(VariableDie));
}
}
}
}
void DwarfDebug::finalizeModuleInfo() {
+ finishSubprogramDefinitions();
+
+ finishVariableDefinitions();
+
// Collect info for variables that were optimized out.
collectDeadVariables();
- // Attach DW_AT_inline attribute with inlined subprogram DIEs.
- computeInlinedDIEs();
-
// Handle anything that needs to be done on a per-unit basis after
// all other generation.
for (const auto &TheU : getUnits()) {
emitDebugInfoDWO();
emitDebugAbbrevDWO();
emitDebugLineDWO();
+ emitDebugLocDWO();
// Emit DWO addresses.
AddrPool.emit(*Asm, Asm->getObjFileLowering().getDwarfAddrSection());
- emitDebugLocDWO();
} else
// Emit info into a debug loc section.
emitDebugLoc();
// clean up.
SPMap.clear();
+ AbstractVariables.clear();
// Reset these for the next Module if we have one.
FirstCU = nullptr;
}
// Find abstract variable, if any, associated with Var.
-DbgVariable *DwarfDebug::findAbstractVariable(DIVariable &DV,
- DebugLoc ScopeLoc) {
+DbgVariable *DwarfDebug::getExistingAbstractVariable(const DIVariable &DV,
+ DIVariable &Cleansed) {
LLVMContext &Ctx = DV->getContext();
// More then one inlined variable corresponds to one abstract variable.
- DIVariable Var = cleanseInlinedVariable(DV, Ctx);
- DbgVariable *AbsDbgVariable = AbstractVariables.lookup(Var);
- if (AbsDbgVariable)
- return AbsDbgVariable;
+ // FIXME: This duplication of variables when inlining should probably be
+ // removed. It's done to allow each DIVariable to describe its location
+ // because the DebugLoc on the dbg.value/declare isn't accurate. We should
+ // make it accurate then remove this duplication/cleansing stuff.
+ Cleansed = cleanseInlinedVariable(DV, Ctx);
+ auto I = AbstractVariables.find(Cleansed);
+ if (I != AbstractVariables.end())
+ return I->second.get();
+ return nullptr;
+}
- LexicalScope *Scope = LScopes.findAbstractScope(ScopeLoc.getScope(Ctx));
- if (!Scope)
- return nullptr;
+DbgVariable *DwarfDebug::getExistingAbstractVariable(const DIVariable &DV) {
+ DIVariable Cleansed;
+ return getExistingAbstractVariable(DV, Cleansed);
+}
+
+void DwarfDebug::createAbstractVariable(const DIVariable &Var,
+ LexicalScope *Scope) {
+ auto AbsDbgVariable = make_unique<DbgVariable>(Var, this);
+ addScopeVariable(Scope, AbsDbgVariable.get());
+ AbstractVariables[Var] = std::move(AbsDbgVariable);
+}
+
+void DwarfDebug::ensureAbstractVariableIsCreated(const DIVariable &DV,
+ const MDNode *ScopeNode) {
+ DIVariable Cleansed = DV;
+ if (getExistingAbstractVariable(DV, Cleansed))
+ return;
+
+ createAbstractVariable(Cleansed, LScopes.getOrCreateAbstractScope(ScopeNode));
+}
+
+void
+DwarfDebug::ensureAbstractVariableIsCreatedIfScoped(const DIVariable &DV,
+ const MDNode *ScopeNode) {
+ DIVariable Cleansed = DV;
+ if (getExistingAbstractVariable(DV, Cleansed))
+ return;
- AbsDbgVariable = new DbgVariable(Var, nullptr, this);
- addScopeVariable(Scope, AbsDbgVariable);
- AbstractVariables[Var] = AbsDbgVariable;
- return AbsDbgVariable;
+ if (LexicalScope *Scope = LScopes.findAbstractScope(ScopeNode))
+ createAbstractVariable(Cleansed, Scope);
}
// If Var is a current function argument then add it to CurrentFnArguments list.
if (!Scope)
continue;
- DbgVariable *AbsDbgVariable = findAbstractVariable(DV, VI.Loc);
- DbgVariable *RegVar = new DbgVariable(DV, AbsDbgVariable, this);
+ ensureAbstractVariableIsCreatedIfScoped(DV, Scope->getScopeNode());
+ ConcreteVariables.push_back(make_unique<DbgVariable>(DV, this));
+ DbgVariable *RegVar = ConcreteVariables.back().get();
RegVar->setFrameIndex(VI.Slot);
- if (!addCurrentFnArgument(RegVar, Scope))
- addScopeVariable(Scope, RegVar);
- if (AbsDbgVariable)
- AbsDbgVariable->setFrameIndex(VI.Slot);
+ addScopeVariable(Scope, RegVar);
}
}
-// Return true if debug value, encoded by DBG_VALUE instruction, is in a
-// defined reg.
-static bool isDbgValueInDefinedReg(const MachineInstr *MI) {
- assert(MI->isDebugValue() && "Invalid DBG_VALUE machine instruction!");
- return MI->getNumOperands() == 3 && MI->getOperand(0).isReg() &&
- MI->getOperand(0).getReg() &&
- (MI->getOperand(1).isImm() ||
- (MI->getOperand(1).isReg() && MI->getOperand(1).getReg() == 0U));
-}
-
// Get .debug_loc entry for the instruction range starting at MI.
static DebugLocEntry::Value getDebugLocValue(const MachineInstr *MI) {
const MDNode *Var = MI->getDebugVariable();
@@ -1188,45 +1193,41 @@ DwarfDebug::collectVariableInfo(SmallPtrSet<const MDNode *, 16> &Processed) {
// Grab the variable info that was squirreled away in the MMI side-table.
collectVariableInfoFromMMITable(Processed);
- for (const MDNode *Var : UserVariables) {
- if (Processed.count(Var))
+ for (const auto &I : DbgValues) {
+ DIVariable DV(I.first);
+ if (Processed.count(DV))
continue;
- // History contains relevant DBG_VALUE instructions for Var and instructions
- // clobbering it.
- SmallVectorImpl<const MachineInstr *> &History = DbgValues[Var];
- if (History.empty())
+ // Instruction ranges, specifying where DV is accessible.
+ const auto &Ranges = I.second;
+ if (Ranges.empty())
continue;
- const MachineInstr *MInsn = History.front();
- DIVariable DV(Var);
LexicalScope *Scope = nullptr;
if (DV.getTag() == dwarf::DW_TAG_arg_variable &&
DISubprogram(DV.getContext()).describes(CurFn->getFunction()))
Scope = LScopes.getCurrentFunctionScope();
- else if (MDNode *IA = DV.getInlinedAt())
- Scope = LScopes.findInlinedScope(DebugLoc::getFromDILocation(IA));
- else
- Scope = LScopes.findLexicalScope(cast<MDNode>(DV->getOperand(1)));
+ else if (MDNode *IA = DV.getInlinedAt()) {
+ DebugLoc DL = DebugLoc::getFromDILocation(IA);
+ Scope = LScopes.findInlinedScope(DebugLoc::get(
+ DL.getLine(), DL.getCol(), DV.getContext(), IA));
+ } else
+ Scope = LScopes.findLexicalScope(DV.getContext());
// If variable scope is not found then skip this variable.
if (!Scope)
continue;
Processed.insert(DV);
+ const MachineInstr *MInsn = Ranges.front().first;
assert(MInsn->isDebugValue() && "History must begin with debug value");
- DbgVariable *AbsVar = findAbstractVariable(DV, MInsn->getDebugLoc());
- DbgVariable *RegVar = new DbgVariable(DV, AbsVar, this);
- if (!addCurrentFnArgument(RegVar, Scope))
- addScopeVariable(Scope, RegVar);
- if (AbsVar)
- AbsVar->setMInsn(MInsn);
-
- // Simplify ranges that are fully coalesced.
- if (History.size() <= 1 ||
- (History.size() == 2 && MInsn->isIdenticalTo(History.back()))) {
- RegVar->setMInsn(MInsn);
+ ensureAbstractVariableIsCreatedIfScoped(DV, Scope->getScopeNode());
+ ConcreteVariables.push_back(make_unique<DbgVariable>(MInsn, this));
+ DbgVariable *RegVar = ConcreteVariables.back().get();
+ addScopeVariable(Scope, RegVar);
+
+ // Check if the first DBG_VALUE is valid for the rest of the function.
+ if (Ranges.size() == 1 && Ranges.front().second == nullptr)
continue;
- }
// Handle multiple DBG_VALUE instructions describing one variable.
RegVar->setDotDebugLocOffset(DotDebugLocEntries.size());
@@ -1236,42 +1237,34 @@ DwarfDebug::collectVariableInfo(SmallPtrSet<const MDNode *, 16> &Processed) {
LocList.Label =
Asm->GetTempSymbol("debug_loc", DotDebugLocEntries.size() - 1);
SmallVector<DebugLocEntry, 4> &DebugLoc = LocList.List;
- for (SmallVectorImpl<const MachineInstr *>::const_iterator
- HI = History.begin(),
- HE = History.end();
- HI != HE; ++HI) {
- const MachineInstr *Begin = *HI;
+ for (auto I = Ranges.begin(), E = Ranges.end(); I != E; ++I) {
+ const MachineInstr *Begin = I->first;
+ const MachineInstr *End = I->second;
assert(Begin->isDebugValue() && "Invalid History entry");
- // Check if DBG_VALUE is truncating a range.
+ // Check if a variable is unaccessible in this range.
if (Begin->getNumOperands() > 1 && Begin->getOperand(0).isReg() &&
!Begin->getOperand(0).getReg())
continue;
+ DEBUG(dbgs() << "DotDebugLoc Pair:\n" << "\t" << *Begin);
+ if (End != nullptr)
+ DEBUG(dbgs() << "\t" << *End);
+ else
+ DEBUG(dbgs() << "\tNULL\n");
- // Compute the range for a register location.
- const MCSymbol *FLabel = getLabelBeforeInsn(Begin);
- const MCSymbol *SLabel = nullptr;
-
- if (HI + 1 == HE)
- // If Begin is the last instruction in History then its value is valid
- // until the end of the function.
- SLabel = FunctionEndSym;
- else {
- const MachineInstr *End = HI[1];
- DEBUG(dbgs() << "DotDebugLoc Pair:\n"
- << "\t" << *Begin << "\t" << *End << "\n");
- if (End->isDebugValue())
- SLabel = getLabelBeforeInsn(End);
- else {
- // End is a normal instruction clobbering the range.
- SLabel = getLabelAfterInsn(End);
- assert(SLabel && "Forgot label after clobber instruction");
- ++HI;
- }
- }
+ const MCSymbol *StartLabel = getLabelBeforeInsn(Begin);
+ assert(StartLabel && "Forgot label before DBG_VALUE starting a range!");
- // The value is valid until the next DBG_VALUE or clobber.
- DebugLocEntry Loc(FLabel, SLabel, getDebugLocValue(Begin), TheCU);
+ const MCSymbol *EndLabel;
+ if (End != nullptr)
+ EndLabel = getLabelAfterInsn(End);
+ else if (std::next(I) == Ranges.end())
+ EndLabel = FunctionEndSym;
+ else
+ EndLabel = getLabelBeforeInsn(std::next(I)->first);
+ assert(EndLabel && "Forgot label after instruction ending a range!");
+
+ DebugLocEntry Loc(StartLabel, EndLabel, getDebugLocValue(Begin), TheCU);
if (DebugLoc.empty() || !DebugLoc.back().Merge(Loc))
DebugLoc.push_back(std::move(Loc));
}
@@ -1281,10 +1274,14 @@ DwarfDebug::collectVariableInfo(SmallPtrSet<const MDNode *, 16> &Processed) {
DIArray Variables = DISubprogram(FnScope->getScopeNode()).getVariables();
for (unsigned i = 0, e = Variables.getNumElements(); i != e; ++i) {
DIVariable DV(Variables.getElement(i));
- if (!DV || !DV.isVariable() || !Processed.insert(DV))
+ assert(DV.isVariable());
+ if (!Processed.insert(DV))
continue;
- if (LexicalScope *Scope = LScopes.findLexicalScope(DV.getContext()))
- addScopeVariable(Scope, new DbgVariable(DV, nullptr, this));
+ if (LexicalScope *Scope = LScopes.findLexicalScope(DV.getContext())) {
+ ensureAbstractVariableIsCreatedIfScoped(DV, Scope->getScopeNode());
+ ConcreteVariables.push_back(make_unique<DbgVariable>(DV, this));
+ addScopeVariable(Scope, ConcreteVariables.back().get());
+ }
}
}
}
}
+static DebugLoc findPrologueEndLoc(const MachineFunction *MF) {
+ // First known non-DBG_VALUE and non-frame setup location marks
+ // the beginning of the function body.
+ for (const auto &MBB : *MF)
+ for (const auto &MI : MBB)
+ if (!MI.isDebugValue() && !MI.getFlag(MachineInstr::FrameSetup) &&
+ !MI.getDebugLoc().isUnknown())
+ return MI.getDebugLoc();
+ return DebugLoc();
+}
+
// Gather pre-function debug information. Assumes being called immediately
// after the function entry point has been emitted.
void DwarfDebug::beginFunction(const MachineFunction *MF) {
if (LScopes.empty())
return;
- assert(UserVariables.empty() && DbgValues.empty() && "Maps weren't cleaned");
+ assert(DbgValues.empty() && "DbgValues map wasn't cleaned!");
// Make sure that each lexical scope will have a begin/end label.
identifyScopeMarkers();
// Assumes in correct section after the entry point.
Asm->OutStreamer.EmitLabel(FunctionBeginSym);
- const TargetRegisterInfo *TRI = Asm->TM.getRegisterInfo();
- // LiveUserVar - Map physreg numbers to the MDNode they contain.
- std::vector<const MDNode *> LiveUserVar(TRI->getNumRegs());
-
- for (MachineFunction::const_iterator I = MF->begin(), E = MF->end(); I != E;
- ++I) {
- bool AtBlockEntry = true;
- for (MachineBasicBlock::const_iterator II = I->begin(), IE = I->end();
- II != IE; ++II) {
- const MachineInstr *MI = II;
-
- if (MI->isDebugValue()) {
- assert(MI->getNumOperands() > 1 && "Invalid machine instruction!");
-
- // Keep track of user variables.
- const MDNode *Var = MI->getDebugVariable();
-
- // Variable is in a register, we need to check for clobbers.
- if (isDbgValueInDefinedReg(MI))
- LiveUserVar[MI->getOperand(0).getReg()] = Var;
-
- // Check the history of this variable.
- SmallVectorImpl<const MachineInstr *> &History = DbgValues[Var];
- if (History.empty()) {
- UserVariables.push_back(Var);
- // The first mention of a function argument gets the FunctionBeginSym
- // label, so arguments are visible when breaking at function entry.
- DIVariable DV(Var);
- if (DV.isVariable() && DV.getTag() == dwarf::DW_TAG_arg_variable &&
- getDISubprogram(DV.getContext()).describes(MF->getFunction()))
- LabelsBeforeInsn[MI] = FunctionBeginSym;
- } else {
- // We have seen this variable before. Try to coalesce DBG_VALUEs.
- const MachineInstr *Prev = History.back();
- if (Prev->isDebugValue()) {
- // Coalesce identical entries at the end of History.
- if (History.size() >= 2 &&
- Prev->isIdenticalTo(History[History.size() - 2])) {
- DEBUG(dbgs() << "Coalescing identical DBG_VALUE entries:\n"
- << "\t" << *Prev << "\t"
- << *History[History.size() - 2] << "\n");
- History.pop_back();
- }
-
- // Terminate old register assignments that don't reach MI;
- MachineFunction::const_iterator PrevMBB = Prev->getParent();
- if (PrevMBB != I && (!AtBlockEntry || std::next(PrevMBB) != I) &&
- isDbgValueInDefinedReg(Prev)) {
- // Previous register assignment needs to terminate at the end of
- // its basic block.
- MachineBasicBlock::const_iterator LastMI =
- PrevMBB->getLastNonDebugInstr();
- if (LastMI == PrevMBB->end()) {
- // Drop DBG_VALUE for empty range.
- DEBUG(dbgs() << "Dropping DBG_VALUE for empty range:\n"
- << "\t" << *Prev << "\n");
- History.pop_back();
- } else if (std::next(PrevMBB) != PrevMBB->getParent()->end())
- // Terminate after LastMI.
- History.push_back(LastMI);
- }
- }
- }
- History.push_back(MI);
- } else {
- // Not a DBG_VALUE instruction.
- if (!MI->isPosition())
- AtBlockEntry = false;
-
- // First known non-DBG_VALUE and non-frame setup location marks
- // the beginning of the function body.
- if (!MI->getFlag(MachineInstr::FrameSetup) &&
- (PrologEndLoc.isUnknown() && !MI->getDebugLoc().isUnknown()))
- PrologEndLoc = MI->getDebugLoc();
-
- // Check if the instruction clobbers any registers with debug vars.
- for (const MachineOperand &MO : MI->operands()) {
- if (!MO.isReg() || !MO.isDef() || !MO.getReg())
- continue;
- for (MCRegAliasIterator AI(MO.getReg(), TRI, true); AI.isValid();
- ++AI) {
- unsigned Reg = *AI;
- const MDNode *Var = LiveUserVar[Reg];
- if (!Var)
- continue;
- // Reg is now clobbered.
- LiveUserVar[Reg] = nullptr;
-
- // Was MD last defined by a DBG_VALUE referring to Reg?
- DbgValueHistoryMap::iterator HistI = DbgValues.find(Var);
- if (HistI == DbgValues.end())
- continue;
- SmallVectorImpl<const MachineInstr *> &History = HistI->second;
- if (History.empty())
- continue;
- const MachineInstr *Prev = History.back();
- // Sanity-check: Register assignments are terminated at the end of
- // their block.
- if (!Prev->isDebugValue() || Prev->getParent() != MI->getParent())
- continue;
- // Is the variable still in Reg?
- if (!isDbgValueInDefinedReg(Prev) ||
- Prev->getOperand(0).getReg() != Reg)
- continue;
- // Var is clobbered. Make sure the next instruction gets a label.
- History.push_back(MI);
- }
- }
- }
- }
- }
+ // Calculate history for local variables.
+ calculateDbgValueHistory(MF, Asm->TM.getRegisterInfo(), DbgValues);
- for (auto &I : DbgValues) {
- SmallVectorImpl<const MachineInstr *> &History = I.second;
- if (History.empty())
+ // Request labels for the full history.
+ for (const auto &I : DbgValues) {
+ const auto &Ranges = I.second;
+ if (Ranges.empty())
continue;
- // Make sure the final register assignments are terminated.
- const MachineInstr *Prev = History.back();
- if (Prev->isDebugValue() && isDbgValueInDefinedReg(Prev)) {
- const MachineBasicBlock *PrevMBB = Prev->getParent();
- MachineBasicBlock::const_iterator LastMI =
- PrevMBB->getLastNonDebugInstr();
- if (LastMI == PrevMBB->end())
- // Drop DBG_VALUE for empty range.
- History.pop_back();
- else if (PrevMBB != &PrevMBB->getParent()->back()) {
- // Terminate after LastMI.
- History.push_back(LastMI);
- }
- }
- // Request labels for the full history.
- for (const MachineInstr *MI : History) {
- if (MI->isDebugValue())
- requestLabelBeforeInsn(MI);
- else
- requestLabelAfterInsn(MI);
+ // The first mention of a function argument gets the FunctionBeginSym
+ // label, so arguments are visible when breaking at function entry.
+ DIVariable DV(I.first);
+ if (DV.isVariable() && DV.getTag() == dwarf::DW_TAG_arg_variable &&
+ getDISubprogram(DV.getContext()).describes(MF->getFunction()))
+ LabelsBeforeInsn[Ranges.front().first] = FunctionBeginSym;
+
+ for (const auto &Range : Ranges) {
+ requestLabelBeforeInsn(Range.first);
+ if (Range.second)
+ requestLabelAfterInsn(Range.second);
}
}
PrevLabel = FunctionBeginSym;
// Record beginning of function.
+ PrologEndLoc = findPrologueEndLoc(MF);
if (!PrologEndLoc.isUnknown()) {
DebugLoc FnStartDL =
PrologEndLoc.getFnDebugLoc(MF->getFunction()->getContext());
}
void DwarfDebug::addScopeVariable(LexicalScope *LS, DbgVariable *Var) {
+ if (addCurrentFnArgument(Var, LS))
+ return;
SmallVectorImpl<DbgVariable *> &Vars = ScopeVariables[LS];
DIVariable DV = Var->getVariable();
// Variables with positive arg numbers are parameters.
// Construct abstract scopes.
for (LexicalScope *AScope : LScopes.getAbstractScopesList()) {
DISubprogram SP(AScope->getScopeNode());
- if (SP.isSubprogram()) {
- // Collect info for variables that were optimized out.
- DIArray Variables = SP.getVariables();
- for (unsigned i = 0, e = Variables.getNumElements(); i != e; ++i) {
- DIVariable DV(Variables.getElement(i));
- if (!DV || !DV.isVariable() || !ProcessedVars.insert(DV))
- continue;
- // Check that DbgVariable for DV wasn't created earlier, when
- // findAbstractVariable() was called for inlined instance of DV.
- LLVMContext &Ctx = DV->getContext();
- DIVariable CleanDV = cleanseInlinedVariable(DV, Ctx);
- if (AbstractVariables.lookup(CleanDV))
- continue;
- if (LexicalScope *Scope = LScopes.findAbstractScope(DV.getContext()))
- addScopeVariable(Scope, new DbgVariable(DV, nullptr, this));
- }
+ if (!SP.isSubprogram())
+ continue;
+ // Collect info for variables that were optimized out.
+ DIArray Variables = SP.getVariables();
+ for (unsigned i = 0, e = Variables.getNumElements(); i != e; ++i) {
+ DIVariable DV(Variables.getElement(i));
+ assert(DV && DV.isVariable());
+ if (!ProcessedVars.insert(DV))
+ continue;
+ ensureAbstractVariableIsCreated(DV, DV.getContext());
}
- if (ProcessedSPNodes.count(AScope->getScopeNode()) == 0)
- constructSubprogramScopeDIE(TheCU, AScope);
+ constructAbstractSubprogramScopeDIE(TheCU, AScope);
}
- DIE &CurFnDIE = *constructSubprogramScopeDIE(TheCU, FnScope);
+ DIE &CurFnDIE = constructSubprogramScopeDIE(TheCU, FnScope);
if (!CurFn->getTarget().Options.DisableFramePointerElim(*CurFn))
TheCU.addFlag(CurFnDIE, dwarf::DW_AT_APPLE_omit_frame_ptr);
PrevCU = &TheCU;
// Clear debug info
- for (auto &I : ScopeVariables)
- DeleteContainerPointers(I.second);
+ // Ownership of DbgVariables is a bit subtle - ScopeVariables owns all the
+ // DbgVariables except those that are also in AbstractVariables (since they
+ // can be used cross-function)
ScopeVariables.clear();
- DeleteContainerPointers(CurrentFnArguments);
- UserVariables.clear();
+ CurrentFnArguments.clear();
DbgValues.clear();
- AbstractVariables.clear();
LabelsBeforeInsn.clear();
LabelsAfterInsn.clear();
PrevLabel = nullptr;
@@ -1713,32 +1599,12 @@ void DwarfDebug::recordSourceLine(unsigned Line, unsigned Col, const MDNode *S,
StringRef Dir;
unsigned Src = 1;
unsigned Discriminator = 0;
- if (S) {
- DIDescriptor Scope(S);
-
- if (Scope.isCompileUnit()) {
- DICompileUnit CU(S);
- Fn = CU.getFilename();
- Dir = CU.getDirectory();
- } else if (Scope.isFile()) {
- DIFile F(S);
- Fn = F.getFilename();
- Dir = F.getDirectory();
- } else if (Scope.isSubprogram()) {
- DISubprogram SP(S);
- Fn = SP.getFilename();
- Dir = SP.getDirectory();
- } else if (Scope.isLexicalBlockFile()) {
- DILexicalBlockFile DBF(S);
- Fn = DBF.getFilename();
- Dir = DBF.getDirectory();
- } else if (Scope.isLexicalBlock()) {
- DILexicalBlock DB(S);
- Fn = DB.getFilename();
- Dir = DB.getDirectory();
- Discriminator = DB.getDiscriminator();
- } else
- llvm_unreachable("Unexpected scope info");
+ if (DIScope Scope = DIScope(S)) {
+ assert(Scope.isScope());
+ Fn = Scope.getFilename();
+ Dir = Scope.getDirectory();
+ if (Scope.isLexicalBlock())
+ Discriminator = DILexicalBlock(S).getDiscriminator();
unsigned CUID = Asm->OutStreamer.getContext().getDwarfCompileUnitID();
Src = static_cast<DwarfCompileUnit &>(*InfoHolder.getUnits()[CUID])
void DwarfDebug::emitDebugLocEntry(ByteStreamer &Streamer,
const DebugLocEntry &Entry) {
assert(Entry.getValues().size() == 1 &&
- "multi-value entries are not supported yet.");
+ "multi-value entries are not supported yet.");
const DebugLocEntry::Value Value = Entry.getValues()[0];
DIVariable DV(Value.getVariable());
if (Value.isInt()) {
Asm->OutStreamer.SwitchSection(
Asm->getObjFileLowering().getDwarfARangesSection());
- typedef DenseMap<DwarfCompileUnit *, std::vector<ArangeSpan> > SpansType;
+ typedef DenseMap<DwarfCompileUnit *, std::vector<ArangeSpan>> SpansType;
SpansType Spans;
for (const auto &I : CUMap) {
DwarfCompileUnit *TheCU = I.second;
- // Emit a symbol so we can find the beginning of our ranges.
- Asm->OutStreamer.EmitLabel(TheCU->getLabelRange());
-
// Iterate over the misc ranges for the compile units in the module.
for (const RangeSpanList &List : TheCU->getRangeLists()) {
// Emit our symbol so we can find the beginning of the range.
// DW_AT_addr_base, DW_AT_ranges_base.
DwarfCompileUnit &DwarfDebug::constructSkeletonCU(const DwarfCompileUnit &CU) {
- DIE *Die = new DIE(dwarf::DW_TAG_compile_unit);
auto OwnedUnit = make_unique<DwarfCompileUnit>(
- CU.getUniqueID(), Die, CU.getCUNode(), Asm, this, &SkeletonHolder);
+ CU.getUniqueID(), CU.getCUNode(), Asm, this, &SkeletonHolder);
DwarfCompileUnit &NewCU = *OwnedUnit;
NewCU.initSection(Asm->getObjFileLowering().getDwarfInfoSection(),
DwarfInfoSectionSym);
NewCU.initStmtList(DwarfLineSectionSym);
- initSkeletonUnit(CU, *Die, std::move(OwnedUnit));
+ initSkeletonUnit(CU, NewCU.getUnitDie(), std::move(OwnedUnit));
return NewCU;
}
DwarfCompileUnit &CU = static_cast<DwarfCompileUnit &>(
*SkeletonHolder.getUnits()[TU.getCU().getUniqueID()]);
- DIE *Die = new DIE(dwarf::DW_TAG_type_unit);
- auto OwnedUnit = make_unique<DwarfTypeUnit>(TU.getUniqueID(), Die, CU, Asm,
- this, &SkeletonHolder);
+ auto OwnedUnit = make_unique<DwarfTypeUnit>(TU.getUniqueID(), CU, Asm, this,
+ &SkeletonHolder);
DwarfTypeUnit &NewTU = *OwnedUnit;
NewTU.setTypeSignature(TU.getTypeSignature());
NewTU.setType(nullptr);
NewTU.initSection(
Asm->getObjFileLowering().getDwarfTypesSection(TU.getTypeSignature()));
- initSkeletonUnit(TU, *Die, std::move(OwnedUnit));
+ initSkeletonUnit(TU, NewTU.getUnitDie(), std::move(OwnedUnit));
return NewTU;
}
assert(useSplitDwarf() && "No split dwarf debug info?");
// Don't pass an abbrev symbol, using a constant zero instead so as not to
// emit relocations into the dwo file.
- InfoHolder.emitUnits(this, /* AbbrevSymbol */nullptr);
+ InfoHolder.emitUnits(this, /* AbbrevSymbol */ nullptr);
}
// Emit the .debug_abbrev.dwo section for separated dwarf. This contains the
bool TopLevelType = TypeUnitsUnderConstruction.empty();
AddrPool.resetUsedFlag();
- DIE *UnitDie = new DIE(dwarf::DW_TAG_type_unit);
auto OwnedUnit =
- make_unique<DwarfTypeUnit>(InfoHolder.getUnits().size(), UnitDie, CU, Asm,
- this, &InfoHolder, getDwoLineTable(CU));
+ make_unique<DwarfTypeUnit>(InfoHolder.getUnits().size(), CU, Asm, this,
+ &InfoHolder, getDwoLineTable(CU));
DwarfTypeUnit &NewTU = *OwnedUnit;
+ DIE &UnitDie = NewTU.getUnitDie();
TU = &NewTU;
- TypeUnitsUnderConstruction.push_back(std::make_pair(std::move(OwnedUnit), CTy));
+ TypeUnitsUnderConstruction.push_back(
+ std::make_pair(std::move(OwnedUnit), CTy));
- NewTU.addUInt(*UnitDie, dwarf::DW_AT_language, dwarf::DW_FORM_data2,
+ NewTU.addUInt(UnitDie, dwarf::DW_AT_language, dwarf::DW_FORM_data2,
CU.getLanguage());
uint64_t Signature = makeTypeSignature(Identifier);
NewTU.setTypeSignature(Signature);
if (!useSplitDwarf())
- CU.applyStmtList(*UnitDie);
+ CU.applyStmtList(UnitDie);
+ // FIXME: Skip using COMDAT groups for type units in the .dwo file once tools
+ // such as DWP ( http://gcc.gnu.org/wiki/DebugFissionDWP ) can cope with it.
NewTU.initSection(
useSplitDwarf()
? Asm->getObjFileLowering().getDwarfTypesDWOSection(Signature)
void DwarfDebug::attachLowHighPC(DwarfCompileUnit &Unit, DIE &D,
MCSymbol *Begin, MCSymbol *End) {
+ assert(Begin && "Begin label should not be null!");
+ assert(End && "End label should not be null!");
+ assert(Begin->isDefined() && "Invalid starting label");
+ assert(End->isDefined() && "Invalid end label");
+
Unit.addLabelAddress(D, dwarf::DW_AT_low_pc, Begin);
if (DwarfVersion < 4)
Unit.addLabelAddress(D, dwarf::DW_AT_high_pc, End);