]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - lib/CodeGen/AsmPrinter/DwarfDebug.h
Replace unnecessary #include directive with forward declarations.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfDebug.h
index 516def804d1533f577900bbc1ce55479d8ec5930..44eed9406fef639d35412700650730bd96835cd8 100644 (file)
 #include "DIE.h"
 #include "llvm/ADT/DenseMap.h"
 #include "llvm/ADT/FoldingSet.h"
+#include "llvm/ADT/MapVector.h"
 #include "llvm/ADT/SetVector.h"
 #include "llvm/ADT/SmallPtrSet.h"
 #include "llvm/ADT/StringMap.h"
-#include "llvm/CodeGen/AsmPrinter.h"
 #include "llvm/CodeGen/LexicalScopes.h"
-#include "llvm/DebugInfo.h"
+#include "llvm/IR/DebugInfo.h"
+#include "llvm/IR/DebugLoc.h"
 #include "llvm/MC/MachineLocation.h"
+#include "llvm/MC/MCDwarf.h"
 #include "llvm/Support/Allocator.h"
-#include "llvm/Support/DebugLoc.h"
 
 namespace llvm {
 
+class AsmPrinter;
+class ByteStreamer;
+class DwarfDebug;
 class DwarfUnit;
 class DwarfCompileUnit;
 class ConstantInt;
@@ -42,7 +46,7 @@ class MCAsmInfo;
 class MCObjectFileInfo;
 class DIEAbbrev;
 class DIE;
-class DIEBlock;
+class DIELoc;
 class DIEEntry;
 
 //===----------------------------------------------------------------------===//
@@ -65,18 +69,13 @@ public:
 
 /// \brief This struct describes location entries emitted in the .debug_loc
 /// section.
-class DotDebugLocEntry {
+class DebugLocEntry {
   // Begin and end symbols for the address range that this location is valid.
   const MCSymbol *Begin;
   const MCSymbol *End;
 
   // Type of entry that this represents.
-  enum EntryType {
-    E_Location,
-    E_Integer,
-    E_ConstantFP,
-    E_ConstantInt
-  };
+  enum EntryType { E_Location, E_Integer, E_ConstantFP, E_ConstantInt };
   enum EntryType EntryKind;
 
   union {
@@ -95,27 +94,26 @@ class DotDebugLocEntry {
   bool Merged;
 
 public:
-  DotDebugLocEntry() : Begin(0), End(0), Variable(0), Merged(false) {
+  DebugLocEntry() : Begin(0), End(0), Variable(0), Merged(false) {
     Constants.Int = 0;
   }
-  DotDebugLocEntry(const MCSymbol *B, const MCSymbol *E, MachineLocation &L,
-                   const MDNode *V)
+  DebugLocEntry(const MCSymbol *B, const MCSymbol *E, MachineLocation &L,
+                const MDNode *V)
       : Begin(B), End(E), Loc(L), Variable(V), Merged(false) {
     Constants.Int = 0;
     EntryKind = E_Location;
   }
-  DotDebugLocEntry(const MCSymbol *B, const MCSymbol *E, int64_t i)
+  DebugLocEntry(const MCSymbol *B, const MCSymbol *E, int64_t i)
       : Begin(B), End(E), Variable(0), Merged(false) {
     Constants.Int = i;
     EntryKind = E_Integer;
   }
-  DotDebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantFP *FPtr)
+  DebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantFP *FPtr)
       : Begin(B), End(E), Variable(0), Merged(false) {
     Constants.CFP = FPtr;
     EntryKind = E_ConstantFP;
   }
-  DotDebugLocEntry(const MCSymbol *B, const MCSymbol *E,
-                   const ConstantInt *IPtr)
+  DebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantInt *IPtr)
       : Begin(B), End(E), Variable(0), Merged(false) {
     Constants.CIP = IPtr;
     EntryKind = E_ConstantInt;
@@ -123,9 +121,9 @@ public:
 
   /// \brief Empty entries are also used as a trigger to emit temp label. Such
   /// labels are referenced is used to find debug_loc offset for a given DIE.
-  bool isEmpty() { return Begin == 0 && End == 0; }
-  bool isMerged() { return Merged; }
-  void Merge(DotDebugLocEntry *Next) {
+  bool isEmpty() const { return Begin == 0 && End == 0; }
+  bool isMerged() const { return Merged; }
+  void Merge(DebugLocEntry *Next) {
     if (!(Begin && Loc == Next->Loc && End == Next->Begin))
       return;
     Next->Begin = Begin;
@@ -243,10 +241,15 @@ class DwarfFile {
   unsigned NextStringPoolNumber;
   std::string StringPref;
 
+  struct AddressPoolEntry {
+    unsigned Number;
+    bool TLS;
+    AddressPoolEntry(unsigned Number, bool TLS) : Number(Number), TLS(TLS) {}
+  };
   // Collection of addresses for this unit and assorted labels.
   // A Symbol->unsigned mapping of addresses used by indirect
   // references.
-  typedef DenseMap<const MCExpr *, unsigned> AddrPool;
+  typedef DenseMap<const MCSymbol *, AddressPoolEntry> AddrPool;
   AddrPool AddressPool;
   unsigned NextAddrPoolNumber;
 
@@ -302,8 +305,7 @@ public:
 
   /// \brief Returns the index into the address pool with the given
   /// label/symbol.
-  unsigned getAddrPoolIndex(const MCExpr *Sym);
-  unsigned getAddrPoolIndex(const MCSymbol *Sym);
+  unsigned getAddrPoolIndex(const MCSymbol *Sym, bool TLS = false);
 
   /// \brief Returns the address pool.
   AddrPool *getAddrPool() { return &AddressPool; }
@@ -334,7 +336,7 @@ class DwarfDebug : public AsmPrinterHandler {
   DwarfCompileUnit *FirstCU;
 
   // Maps MDNode with its corresponding DwarfCompileUnit.
-  DenseMap<const MDNode *, DwarfCompileUnit *> CUMap;
+  MapVector<const MDNode *, DwarfCompileUnit *> CUMap;
 
   // Maps subprogram MDNode with its corresponding DwarfCompileUnit.
   DenseMap<const MDNode *, DwarfCompileUnit *> SPMap;
@@ -347,11 +349,8 @@ class DwarfDebug : public AsmPrinterHandler {
   /// of in DwarfCompileUnit.
   DenseMap<const MDNode *, DIE *> MDTypeNodeToDieMap;
 
-  // Stores the current file ID for a given compile unit.
-  DenseMap<unsigned, unsigned> FileIDCUMap;
-  // Source id map, i.e. CUID, source filename and directory,
-  // separated by a zero byte, mapped to a unique id.
-  StringMap<unsigned, BumpPtrAllocator &> SourceIdMap;
+  // Used to unique C++ member function declarations.
+  StringMap<const MDNode *> OdrMemberMap;
 
   // List of all labels used in aranges generation.
   std::vector<SymbolCU> ArangeLabels;
@@ -379,8 +378,8 @@ class DwarfDebug : public AsmPrinterHandler {
   // Collection of abstract variables.
   DenseMap<const MDNode *, DbgVariable *> AbstractVariables;
 
-  // Collection of DotDebugLocEntry.
-  SmallVector<DotDebugLocEntry, 4> DotDebugLocEntries;
+  // Collection of DebugLocEntry.
+  SmallVector<DebugLocEntry, 4> DotDebugLocEntries;
 
   // Collection of subprogram DIEs that are marked (at the end of the module)
   // as DW_AT_inline.
@@ -461,6 +460,10 @@ class DwarfDebug : public AsmPrinterHandler {
   // Whether or not to use AT_ranges for compilation units.
   bool HasCURanges;
 
+  // Whether we emitted a function into a section other than the default
+  // text.
+  bool UsedNonDefaultText;
+
   // Version of dwarf we're emitting.
   unsigned DwarfVersion;
 
@@ -479,6 +482,10 @@ class DwarfDebug : public AsmPrinterHandler {
   // Holder for the skeleton information.
   DwarfFile SkeletonHolder;
 
+  // Store file names for type units under fission in a line table header that
+  // will be emitted into debug_line.dwo.
+  MCDwarfDwoLineTable SplitTypeUnitFileTable;
+
   void addScopeVariable(LexicalScope *LS, DbgVariable *Var);
 
   const SmallVectorImpl<DwarfUnit *> &getUnits() {
@@ -575,6 +582,11 @@ class DwarfDebug : public AsmPrinterHandler {
   /// index.
   void emitDebugPubTypes(bool GnuStyle = false);
 
+  void
+  emitDebugPubSection(bool GnuStyle, const MCSection *PSec, StringRef Name,
+                      const StringMap<const DIE *> &(DwarfUnit::*Accessor)()
+                      const);
+
   /// \brief Emit visible names into a debug str section.
   void emitDebugStr();
 
@@ -601,7 +613,7 @@ class DwarfDebug : public AsmPrinterHandler {
 
   /// \brief Construct the split debug info compile unit for the debug info
   /// section.
-  DwarfTypeUnit *constructSkeletonTU(const DwarfTypeUnit *TU);
+  DwarfTypeUnit *constructSkeletonTU(DwarfTypeUnit *TU);
 
   /// \brief Emit the debug info dwo section.
   void emitDebugInfoDWO();
@@ -609,6 +621,9 @@ class DwarfDebug : public AsmPrinterHandler {
   /// \brief Emit the debug abbrev dwo section.
   void emitDebugAbbrevDWO();
 
+  /// \brief Emit the debug line dwo section.
+  void emitDebugLineDWO();
+
   /// \brief Emit the debug str dwo section.
   void emitDebugStrDWO();
 
@@ -618,7 +633,8 @@ class DwarfDebug : public AsmPrinterHandler {
 
   /// \brief Create new DwarfCompileUnit for the given metadata node with tag
   /// DW_TAG_compile_unit.
-  DwarfCompileUnit *constructDwarfCompileUnit(DICompileUnit DIUnit);
+  DwarfCompileUnit *constructDwarfCompileUnit(DICompileUnit DIUnit,
+                                              bool Singular);
 
   /// \brief Construct subprogram DIE.
   void constructSubprogramDIE(DwarfCompileUnit *TheCU, const MDNode *N);
@@ -671,6 +687,9 @@ class DwarfDebug : public AsmPrinterHandler {
   /// \brief Return Label immediately following the instruction.
   MCSymbol *getLabelAfterInsn(const MachineInstr *MI);
 
+  void attachLowHighPC(DwarfCompileUnit *Unit, DIE *D, MCSymbol *Begin,
+                       MCSymbol *End);
+
 public:
   //===--------------------------------------------------------------------===//
   // Main entry points.
@@ -684,28 +703,33 @@ public:
     return MDTypeNodeToDieMap.lookup(TypeMD);
   }
 
+  /// \brief Look up or create an entry in the OdrMemberMap.
+  const MDNode *&getOrCreateOdrMember(StringRef Key) {
+    return OdrMemberMap.GetOrCreateValue(Key).getValue();
+  }
+
   /// \brief Emit all Dwarf sections that should come prior to the
   /// content.
   void beginModule();
 
   /// \brief Emit all Dwarf sections that should come after the content.
-  void endModule();
+  void endModule() override;
 
   /// \brief Gather pre-function debug information.
-  void beginFunction(const MachineFunction *MF);
+  void beginFunction(const MachineFunction *MF) override;
 
   /// \brief Gather and emit post-function debug information.
-  void endFunction(const MachineFunction *MF);
+  void endFunction(const MachineFunction *MF) override;
 
   /// \brief Process beginning of an instruction.
-  void beginInstruction(const MachineInstr *MI);
+  void beginInstruction(const MachineInstr *MI) override;
 
   /// \brief Process end of an instruction.
-  void endInstruction();
+  void endInstruction() override;
 
   /// \brief Add a DIE to the set of types that we're going to pull into
   /// type units.
-  void addDwarfTypeUnitType(DICompileUnit CUNode, StringRef Identifier,
+  void addDwarfTypeUnitType(DwarfCompileUnit &CU, StringRef Identifier,
                             DIE *Die, DICompositeType CTy);
 
   /// \brief Add a label so that arange data can be generated for it.
@@ -713,16 +737,10 @@ public:
 
   /// \brief For symbols that have a size designated (e.g. common symbols),
   /// this tracks that size.
-  void setSymbolSize(const MCSymbol *Sym, uint64_t Size) {
+  void setSymbolSize(const MCSymbol *Sym, uint64_t Size) override {
     SymSize[Sym] = Size;
   }
 
-  /// \brief Look up the source id with the given directory and source file
-  /// names. If none currently exists, create a new id and insert it in the
-  /// SourceIds map.
-  unsigned getOrCreateSourceID(StringRef DirName, StringRef FullName,
-                               unsigned CUID);
-
   /// \brief Recursively Emits a debug information entry.
   void emitDIE(DIE *Die);
 
@@ -730,23 +748,39 @@ public:
 
   /// \brief Returns whether or not to emit tables that dwarf consumers can
   /// use to accelerate lookup.
-  bool useDwarfAccelTables() { return HasDwarfAccelTables; }
+  bool useDwarfAccelTables() const { return HasDwarfAccelTables; }
 
   /// \brief Returns whether or not to change the current debug info for the
   /// split dwarf proposal support.
-  bool useSplitDwarf() { return HasSplitDwarf; }
+  bool useSplitDwarf() const { return HasSplitDwarf; }
 
   /// \brief Returns whether or not to use AT_ranges for compilation units.
-  bool useCURanges() { return HasCURanges; }
+  bool useCURanges() const { return HasCURanges; }
 
   /// Returns the Dwarf Version.
   unsigned getDwarfVersion() const { return DwarfVersion; }
 
+  /// Returns the section symbol for the .debug_loc section.
+  MCSymbol *getDebugLocSym() const { return DwarfDebugLocSectionSym; }
+
+  /// Returns the entries for the .debug_loc section.
+  const SmallVectorImpl<DebugLocEntry> &getDebugLocEntries() const {
+    return DotDebugLocEntries;
+  }
+
+  /// \brief Emit an entry for the debug loc section. This can be used to
+  /// handle an entry that's going to be emitted into the debug loc section.
+  void emitDebugLocEntry(ByteStreamer &Streamer, const DebugLocEntry &Entry);
+
   /// Find the MDNode for the given reference.
   template <typename T> T resolve(DIRef<T> Ref) const {
     return Ref.resolve(TypeIdentifierMap);
   }
 
+  /// Find the DwarfCompileUnit for the given CU Die.
+  DwarfCompileUnit *lookupUnit(const DIE *CU) const {
+    return CUDieMap.lookup(CU);
+  }
   /// isSubprogramContext - Return true if Context is either a subprogram
   /// or another context nested inside a subprogram.
   bool isSubprogramContext(const MDNode *Context);