index e49b05b46c975202b3571439a67db5f175f74b8d..44eed9406fef639d35412700650730bd96835cd8 100644 (file)
#ifndef CODEGEN_ASMPRINTER_DWARFDEBUG_H__
#define CODEGEN_ASMPRINTER_DWARFDEBUG_H__
+#include "AsmPrinterHandler.h"
#include "DIE.h"
#include "llvm/ADT/DenseMap.h"
#include "llvm/ADT/FoldingSet.h"
+#include "llvm/ADT/MapVector.h"
#include "llvm/ADT/SetVector.h"
#include "llvm/ADT/SmallPtrSet.h"
#include "llvm/ADT/StringMap.h"
-#include "llvm/CodeGen/AsmPrinter.h"
#include "llvm/CodeGen/LexicalScopes.h"
-#include "llvm/DebugInfo.h"
+#include "llvm/IR/DebugInfo.h"
+#include "llvm/IR/DebugLoc.h"
#include "llvm/MC/MachineLocation.h"
+#include "llvm/MC/MCDwarf.h"
#include "llvm/Support/Allocator.h"
-#include "llvm/Support/DebugLoc.h"
namespace llvm {
-class Unit;
-class CompileUnit;
+class AsmPrinter;
+class ByteStreamer;
+class DwarfDebug;
+class DwarfUnit;
+class DwarfCompileUnit;
class ConstantInt;
class ConstantFP;
class DbgVariable;
class MCObjectFileInfo;
class DIEAbbrev;
class DIE;
-class DIEBlock;
+class DIELoc;
class DIEEntry;
//===----------------------------------------------------------------------===//
/// \brief This class is used to record source line correspondence.
class SrcLineInfo {
- unsigned Line; // Source line number.
- unsigned Column; // Source column.
- unsigned SourceID; // Source ID number.
- MCSymbol *Label; // Label in code ID number.
+ unsigned Line; // Source line number.
+ unsigned Column; // Source column.
+ unsigned SourceID; // Source ID number.
+ MCSymbol *Label; // Label in code ID number.
public:
SrcLineInfo(unsigned L, unsigned C, unsigned S, MCSymbol *label)
- : Line(L), Column(C), SourceID(S), Label(label) {}
+ : Line(L), Column(C), SourceID(S), Label(label) {}
// Accessors
unsigned getLine() const { return Line; }
/// \brief This struct describes location entries emitted in the .debug_loc
/// section.
-class DotDebugLocEntry {
+class DebugLocEntry {
// Begin and end symbols for the address range that this location is valid.
const MCSymbol *Begin;
const MCSymbol *End;
// Type of entry that this represents.
- enum EntryType {
- E_Location,
- E_Integer,
- E_ConstantFP,
- E_ConstantInt
- };
+ enum EntryType { E_Location, E_Integer, E_ConstantFP, E_ConstantInt };
enum EntryType EntryKind;
union {
bool Merged;
public:
- DotDebugLocEntry() : Begin(0), End(0), Variable(0), Merged(false) {
+ DebugLocEntry() : Begin(0), End(0), Variable(0), Merged(false) {
Constants.Int = 0;
}
- DotDebugLocEntry(const MCSymbol *B, const MCSymbol *E, MachineLocation &L,
- const MDNode *V)
+ DebugLocEntry(const MCSymbol *B, const MCSymbol *E, MachineLocation &L,
+ const MDNode *V)
: Begin(B), End(E), Loc(L), Variable(V), Merged(false) {
Constants.Int = 0;
EntryKind = E_Location;
}
- DotDebugLocEntry(const MCSymbol *B, const MCSymbol *E, int64_t i)
+ DebugLocEntry(const MCSymbol *B, const MCSymbol *E, int64_t i)
: Begin(B), End(E), Variable(0), Merged(false) {
Constants.Int = i;
EntryKind = E_Integer;
}
- DotDebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantFP *FPtr)
+ DebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantFP *FPtr)
: Begin(B), End(E), Variable(0), Merged(false) {
Constants.CFP = FPtr;
EntryKind = E_ConstantFP;
}
- DotDebugLocEntry(const MCSymbol *B, const MCSymbol *E,
- const ConstantInt *IPtr)
+ DebugLocEntry(const MCSymbol *B, const MCSymbol *E, const ConstantInt *IPtr)
: Begin(B), End(E), Variable(0), Merged(false) {
Constants.CIP = IPtr;
EntryKind = E_ConstantInt;
/// \brief Empty entries are also used as a trigger to emit temp label. Such
/// labels are referenced is used to find debug_loc offset for a given DIE.
- bool isEmpty() { return Begin == 0 && End == 0; }
- bool isMerged() { return Merged; }
- void Merge(DotDebugLocEntry *Next) {
+ bool isEmpty() const { return Begin == 0 && End == 0; }
+ bool isMerged() const { return Merged; }
+ void Merge(DebugLocEntry *Next) {
if (!(Begin && Loc == Next->Loc && End == Next->Begin))
return;
Next->Begin = Begin;
Merged = true;
}
- bool isLocation() const { return EntryKind == E_Location; }
- bool isInt() const { return EntryKind == E_Integer; }
- bool isConstantFP() const { return EntryKind == E_ConstantFP; }
+ bool isLocation() const { return EntryKind == E_Location; }
+ bool isInt() const { return EntryKind == E_Integer; }
+ bool isConstantFP() const { return EntryKind == E_ConstantFP; }
bool isConstantInt() const { return EntryKind == E_ConstantInt; }
- int64_t getInt() const { return Constants.Int; }
- const ConstantFP *getConstantFP() const { return Constants.CFP; }
+ int64_t getInt() const { return Constants.Int; }
+ const ConstantFP *getConstantFP() const { return Constants.CFP; }
const ConstantInt *getConstantInt() const { return Constants.CIP; }
const MDNode *getVariable() const { return Variable; }
const MCSymbol *getBeginSym() const { return Begin; }
//===----------------------------------------------------------------------===//
/// \brief This class is used to track local variable information.
class DbgVariable {
- DIVariable Var; // Variable Descriptor.
- DIE *TheDIE; // Variable DIE.
- unsigned DotDebugLocOffset; // Offset in DotDebugLocEntries.
- DbgVariable *AbsVar; // Corresponding Abstract variable, if any.
- const MachineInstr *MInsn; // DBG_VALUE instruction of the variable.
+ DIVariable Var; // Variable Descriptor.
+ DIE *TheDIE; // Variable DIE.
+ unsigned DotDebugLocOffset; // Offset in DotDebugLocEntries.
+ DbgVariable *AbsVar; // Corresponding Abstract variable, if any.
+ const MachineInstr *MInsn; // DBG_VALUE instruction of the variable.
int FrameIndex;
DwarfDebug *DD;
+
public:
// AbsVar may be NULL.
DbgVariable(DIVariable V, DbgVariable *AV, DwarfDebug *DD)
- : Var(V), TheDIE(0), DotDebugLocOffset(~0U), AbsVar(AV), MInsn(0),
- FrameIndex(~0), DD(DD) {}
+ : Var(V), TheDIE(0), DotDebugLocOffset(~0U), AbsVar(AV), MInsn(0),
+ FrameIndex(~0), DD(DD) {}
// Accessors.
- DIVariable getVariable() const { return Var; }
- void setDIE(DIE *D) { TheDIE = D; }
- DIE *getDIE() const { return TheDIE; }
- void setDotDebugLocOffset(unsigned O) { DotDebugLocOffset = O; }
- unsigned getDotDebugLocOffset() const { return DotDebugLocOffset; }
- StringRef getName() const { return Var.getName(); }
+ DIVariable getVariable() const { return Var; }
+ void setDIE(DIE *D) { TheDIE = D; }
+ DIE *getDIE() const { return TheDIE; }
+ void setDotDebugLocOffset(unsigned O) { DotDebugLocOffset = O; }
+ unsigned getDotDebugLocOffset() const { return DotDebugLocOffset; }
+ StringRef getName() const { return Var.getName(); }
DbgVariable *getAbstractVariable() const { return AbsVar; }
- const MachineInstr *getMInsn() const { return MInsn; }
- void setMInsn(const MachineInstr *M) { MInsn = M; }
- int getFrameIndex() const { return FrameIndex; }
- void setFrameIndex(int FI) { FrameIndex = FI; }
+ const MachineInstr *getMInsn() const { return MInsn; }
+ void setMInsn(const MachineInstr *M) { MInsn = M; }
+ int getFrameIndex() const { return FrameIndex; }
+ void setFrameIndex(int FI) { FrameIndex = FI; }
// Translate tag to proper Dwarf tag.
- uint16_t getTag() const {
+ uint16_t getTag() const {
if (Var.getTag() == dwarf::DW_TAG_arg_variable)
return dwarf::DW_TAG_formal_parameter;
return dwarf::DW_TAG_variable;
}
/// \brief Return true if DbgVariable is artificial.
- bool isArtificial() const {
+ bool isArtificial() const {
if (Var.isArtificial())
return true;
if (getType().isArtificial())
return false;
}
- bool isObjectPointer() const {
+ bool isObjectPointer() const {
if (Var.isObjectPointer())
return true;
if (getType().isObjectPointer())
return false;
}
- bool variableHasComplexAddress() const {
+ bool variableHasComplexAddress() const {
assert(Var.isVariable() && "Invalid complex DbgVariable!");
return Var.hasComplexAddress();
}
- bool isBlockByrefVariable() const {
+ bool isBlockByrefVariable() const {
assert(Var.isVariable() && "Invalid complex DbgVariable!");
return Var.isBlockByrefVariable();
}
- unsigned getNumAddrElements() const {
+ unsigned getNumAddrElements() const {
assert(Var.isVariable() && "Invalid complex DbgVariable!");
return Var.getNumAddrElements();
}
- uint64_t getAddrElement(unsigned i) const {
- return Var.getAddrElement(i);
- }
+ uint64_t getAddrElement(unsigned i) const { return Var.getAddrElement(i); }
DIType getType() const;
private:
};
/// \brief Collects and handles information specific to a particular
-/// collection of units.
-class DwarfUnits {
+/// collection of units. This collection represents all of the units
+/// that will be ultimately output into a single object file.
+class DwarfFile {
// Target of Dwarf emission, used for sizing of abbreviations.
AsmPrinter *Asm;
// Used to uniquely define abbreviations.
- FoldingSet<DIEAbbrev> *AbbreviationsSet;
+ FoldingSet<DIEAbbrev> AbbreviationsSet;
// A list of all the unique abbreviations in use.
- std::vector<DIEAbbrev *> &Abbreviations;
+ std::vector<DIEAbbrev *> Abbreviations;
// A pointer to all units in the section.
- SmallVector<Unit *, 1> CUs;
+ SmallVector<DwarfUnit *, 1> CUs;
// Collection of strings for this unit and assorted symbols.
// A String->Symbol mapping of strings used by indirect
// references.
- typedef StringMap<std::pair<MCSymbol*, unsigned>,
- BumpPtrAllocator&> StrPool;
+ typedef StringMap<std::pair<MCSymbol *, unsigned>, BumpPtrAllocator &>
+ StrPool;
StrPool StringPool;
unsigned NextStringPoolNumber;
std::string StringPref;
+ struct AddressPoolEntry {
+ unsigned Number;
+ bool TLS;
+ AddressPoolEntry(unsigned Number, bool TLS) : Number(Number), TLS(TLS) {}
+ };
// Collection of addresses for this unit and assorted labels.
// A Symbol->unsigned mapping of addresses used by indirect
// references.
- typedef DenseMap<const MCExpr *, unsigned> AddrPool;
+ typedef DenseMap<const MCSymbol *, AddressPoolEntry> AddrPool;
AddrPool AddressPool;
unsigned NextAddrPoolNumber;
public:
- DwarfUnits(AsmPrinter *AP, FoldingSet<DIEAbbrev> *AS,
- std::vector<DIEAbbrev *> &A, const char *Pref,
- BumpPtrAllocator &DA)
- : Asm(AP), AbbreviationsSet(AS), Abbreviations(A), StringPool(DA),
- NextStringPoolNumber(0), StringPref(Pref), AddressPool(),
- NextAddrPoolNumber(0) {}
+ DwarfFile(AsmPrinter *AP, const char *Pref, BumpPtrAllocator &DA)
+ : Asm(AP), StringPool(DA), NextStringPoolNumber(0), StringPref(Pref),
+ AddressPool(), NextAddrPoolNumber(0) {}
- ~DwarfUnits();
+ ~DwarfFile();
- const SmallVectorImpl<Unit *> &getUnits() { return CUs; }
+ const SmallVectorImpl<DwarfUnit *> &getUnits() { return CUs; }
/// \brief Compute the size and offset of a DIE given an incoming Offset.
unsigned computeSizeAndOffset(DIE *Die, unsigned Offset);
void assignAbbrevNumber(DIEAbbrev &Abbrev);
/// \brief Add a unit to the list of CUs.
- void addUnit(Unit *CU) { CUs.push_back(CU); }
+ void addUnit(DwarfUnit *CU) { CUs.push_back(CU); }
/// \brief Emit all of the units to the section listed with the given
/// abbreviation section.
- void emitUnits(DwarfDebug *DD, const MCSection *USection,
- const MCSection *ASection, const MCSymbol *ASectionSym);
+ void emitUnits(DwarfDebug *DD, const MCSection *ASection,
+ const MCSymbol *ASectionSym);
+
+ /// \brief Emit a set of abbreviations to the specific section.
+ void emitAbbrevs(const MCSection *);
/// \brief Emit all of the strings to the section given.
void emitStrings(const MCSection *StrSection, const MCSection *OffsetSection,
/// \brief Returns the index into the address pool with the given
/// label/symbol.
- unsigned getAddrPoolIndex(const MCExpr *Sym);
- unsigned getAddrPoolIndex(const MCSymbol *Sym);
+ unsigned getAddrPoolIndex(const MCSymbol *Sym, bool TLS = false);
/// \brief Returns the address pool.
AddrPool *getAddrPool() { return &AddressPool; }
/// \brief Helper used to pair up a symbol and its DWARF compile unit.
struct SymbolCU {
- SymbolCU(CompileUnit *CU, const MCSymbol *Sym) : Sym(Sym), CU(CU) {}
+ SymbolCU(DwarfCompileUnit *CU, const MCSymbol *Sym) : Sym(Sym), CU(CU) {}
const MCSymbol *Sym;
- CompileUnit *CU;
+ DwarfCompileUnit *CU;
};
/// \brief Collects and handles dwarf debug information.
-class DwarfDebug {
+class DwarfDebug : public AsmPrinterHandler {
// Target of Dwarf emission.
AsmPrinter *Asm;
// All DIEValues are allocated through this allocator.
BumpPtrAllocator DIEValueAllocator;
- // Handle to the a compile unit used for the inline extension handling.
- CompileUnit *FirstCU;
+ // Handle to the compile unit used for the inline extension handling,
+ // this is just so that the DIEValue allocator has a place to store
+ // the particular elements.
+ // FIXME: Store these off of DwarfDebug instead?
+ DwarfCompileUnit *FirstCU;
- // Maps MDNode with its corresponding CompileUnit.
- DenseMap <const MDNode *, CompileUnit *> CUMap;
+ // Maps MDNode with its corresponding DwarfCompileUnit.
+ MapVector<const MDNode *, DwarfCompileUnit *> CUMap;
- // Maps subprogram MDNode with its corresponding CompileUnit.
- DenseMap <const MDNode *, CompileUnit *> SPMap;
+ // Maps subprogram MDNode with its corresponding DwarfCompileUnit.
+ DenseMap<const MDNode *, DwarfCompileUnit *> SPMap;
- // Maps a CU DIE with its corresponding CompileUnit.
- DenseMap <const DIE *, CompileUnit *> CUDieMap;
+ // Maps a CU DIE with its corresponding DwarfCompileUnit.
+ DenseMap<const DIE *, DwarfCompileUnit *> CUDieMap;
/// Maps MDNodes for type sysstem with the corresponding DIEs. These DIEs can
/// be shared across CUs, that is why we keep the map here instead
- /// of in CompileUnit.
+ /// of in DwarfCompileUnit.
DenseMap<const MDNode *, DIE *> MDTypeNodeToDieMap;
- // Used to uniquely define abbreviations.
- FoldingSet<DIEAbbrev> AbbreviationsSet;
-
- // A list of all the unique abbreviations in use.
- std::vector<DIEAbbrev *> Abbreviations;
-
- // Stores the current file ID for a given compile unit.
- DenseMap <unsigned, unsigned> FileIDCUMap;
- // Source id map, i.e. CUID, source filename and directory,
- // separated by a zero byte, mapped to a unique id.
- StringMap<unsigned, BumpPtrAllocator&> SourceIdMap;
+ // Used to unique C++ member function declarations.
+ StringMap<const MDNode *> OdrMemberMap;
// List of all labels used in aranges generation.
std::vector<SymbolCU> ArangeLabels;
// Size of each symbol emitted (for those symbols that have a specific size).
- DenseMap <const MCSymbol *, uint64_t> SymSize;
+ DenseMap<const MCSymbol *, uint64_t> SymSize;
// Provides a unique id per text section.
typedef DenseMap<const MCSection *, SmallVector<SymbolCU, 8> > SectionMapType;
DenseMap<const MDNode *, DIE *> AbstractSPDies;
// Collection of dbg variables of a scope.
- typedef DenseMap<LexicalScope *,
- SmallVector<DbgVariable *, 8> > ScopeVariablesMap;
+ typedef DenseMap<LexicalScope *, SmallVector<DbgVariable *, 8> >
+ ScopeVariablesMap;
ScopeVariablesMap ScopeVariables;
// Collection of abstract variables.
DenseMap<const MDNode *, DbgVariable *> AbstractVariables;
- // Collection of DotDebugLocEntry.
- SmallVector<DotDebugLocEntry, 4> DotDebugLocEntries;
+ // Collection of DebugLocEntry.
+ SmallVector<DebugLocEntry, 4> DotDebugLocEntries;
// Collection of subprogram DIEs that are marked (at the end of the module)
// as DW_AT_inline.
// Every user variable mentioned by a DBG_VALUE instruction in order of
// appearance.
- SmallVector<const MDNode*, 8> UserVariables;
+ SmallVector<const MDNode *, 8> UserVariables;
// For each user variable, keep a list of DBG_VALUE instructions in order.
// The list can also contain normal instructions that clobber the previous
// DBG_VALUE.
- typedef DenseMap<const MDNode*, SmallVector<const MachineInstr*, 4> >
- DbgValueHistoryMap;
+ typedef DenseMap<const MDNode *, SmallVector<const MachineInstr *, 4> >
+ DbgValueHistoryMap;
DbgValueHistoryMap DbgValues;
// Previous instruction's location information. This is used to determine
// body.
DebugLoc PrologEndLoc;
+ // If nonnull, stores the current machine function we're processing.
+ const MachineFunction *CurFn;
+
+ // If nonnull, stores the current machine instruction we're processing.
+ const MachineInstr *CurMI;
+
// Section Symbols: these are assembler temporary labels that are emitted at
// the beginning of each supported dwarf section. These are used to form
// section offsets and are created by EmitSectionLabels.
MCSymbol *DwarfStrSectionSym, *TextSectionSym, *DwarfDebugRangeSectionSym;
MCSymbol *DwarfDebugLocSectionSym, *DwarfLineSectionSym, *DwarfAddrSectionSym;
MCSymbol *FunctionBeginSym, *FunctionEndSym;
- MCSymbol *DwarfAbbrevDWOSectionSym, *DwarfStrDWOSectionSym;
+ MCSymbol *DwarfInfoDWOSectionSym, *DwarfAbbrevDWOSectionSym;
+ MCSymbol *DwarfStrDWOSectionSym;
MCSymbol *DwarfGnuPubNamesSectionSym, *DwarfGnuPubTypesSectionSym;
// As an optimization, there is no need to emit an entry in the directory
// table for the same directory as DW_AT_comp_dir.
StringRef CompilationDir;
- // Counter for assigning globally unique IDs for CUs.
- unsigned GlobalCUIndexCount;
-
// Counter for assigning globally unique IDs for ranges.
unsigned GlobalRangeCount;
// Holder for the file specific debug information.
- DwarfUnits InfoHolder;
+ DwarfFile InfoHolder;
// Holders for the various debug information flags that we might need to
// have exposed. See accessor functions below for description.
// Holder for imported entities.
typedef SmallVector<std::pair<const MDNode *, const MDNode *>, 32>
- ImportedEntityMap;
+ ImportedEntityMap;
ImportedEntityMap ScopesWithImportedEntities;
- // Map from type MDNodes to a pair used as a union. If the pointer is
- // non-null, proxy DIEs in CUs meant to reference this type should be stored
- // in the vector. The hash will be added to these DIEs once it is computed. If
- // the pointer is null, the hash is immediately available in the uint64_t and
- // should be directly used for proxy DIEs.
- DenseMap<const MDNode *, std::pair<uint64_t, SmallVectorImpl<DIE *> *> >
- TypeUnits;
+ // Map from MDNodes for user-defined types to the type units that describe
+ // them.
+ DenseMap<const MDNode *, const DwarfTypeUnit *> DwarfTypeUnits;
// Whether to emit the pubnames/pubtypes sections.
bool HasDwarfPubSections;
+ // Whether or not to use AT_ranges for compilation units.
+ bool HasCURanges;
+
+ // Whether we emitted a function into a section other than the default
+ // text.
+ bool UsedNonDefaultText;
+
// Version of dwarf we're emitting.
unsigned DwarfVersion;
// original object file, rather than things that are meant
// to be in the .dwo sections.
- // Used to uniquely define abbreviations for the skeleton emission.
- FoldingSet<DIEAbbrev> SkeletonAbbrevSet;
-
- // A list of all the unique abbreviations in use.
- std::vector<DIEAbbrev *> SkeletonAbbrevs;
-
// Holder for the skeleton information.
- DwarfUnits SkeletonHolder;
+ DwarfFile SkeletonHolder;
+
+ // Store file names for type units under fission in a line table header that
+ // will be emitted into debug_line.dwo.
+ MCDwarfDwoLineTable SplitTypeUnitFileTable;
void addScopeVariable(LexicalScope *LS, DbgVariable *Var);
- const SmallVectorImpl<Unit *> &getUnits() { return InfoHolder.getUnits(); }
+ const SmallVectorImpl<DwarfUnit *> &getUnits() {
+ return InfoHolder.getUnits();
+ }
/// \brief Find abstract variable associated with Var.
DbgVariable *findAbstractVariable(DIVariable &Var, DebugLoc Loc);
/// DW_AT_low_pc and DW_AT_high_pc attributes. If there are global
/// variables in this scope then create and insert DIEs for these
/// variables.
- DIE *updateSubprogramScopeDIE(CompileUnit *SPCU, DISubprogram SP);
+ DIE *updateSubprogramScopeDIE(DwarfCompileUnit *SPCU, DISubprogram SP);
/// \brief A helper function to check whether the DIE for a given Scope is
/// going to be null.
/// \brief A helper function to construct a RangeSpanList for a given
/// lexical scope.
- void addScopeRangeList(CompileUnit *TheCU, DIE *ScopeDIE,
+ void addScopeRangeList(DwarfCompileUnit *TheCU, DIE *ScopeDIE,
const SmallVectorImpl<InsnRange> &Range);
/// \brief Construct new DW_TAG_lexical_block for this scope and
/// attach DW_AT_low_pc/DW_AT_high_pc labels.
- DIE *constructLexicalScopeDIE(CompileUnit *TheCU, LexicalScope *Scope);
+ DIE *constructLexicalScopeDIE(DwarfCompileUnit *TheCU, LexicalScope *Scope);
/// \brief This scope represents inlined body of a function. Construct
/// DIE to represent this concrete inlined copy of the function.
- DIE *constructInlinedScopeDIE(CompileUnit *TheCU, LexicalScope *Scope);
+ DIE *constructInlinedScopeDIE(DwarfCompileUnit *TheCU, LexicalScope *Scope);
/// \brief Construct a DIE for this scope.
- DIE *constructScopeDIE(CompileUnit *TheCU, LexicalScope *Scope);
+ DIE *constructScopeDIE(DwarfCompileUnit *TheCU, LexicalScope *Scope);
/// A helper function to create children of a Scope DIE.
- DIE *createScopeChildrenDIE(CompileUnit *TheCU, LexicalScope *Scope,
- SmallVectorImpl<DIE*> &Children);
+ DIE *createScopeChildrenDIE(DwarfCompileUnit *TheCU, LexicalScope *Scope,
+ SmallVectorImpl<DIE *> &Children);
/// \brief Emit initial Dwarf sections with a label at the start of each one.
void emitSectionLabels();
/// open.
void endSections();
- /// \brief Emit a set of abbreviations to the specific section.
- void emitAbbrevs(const MCSection *, std::vector<DIEAbbrev*> *);
-
/// \brief Emit the debug info section.
void emitDebugInfo();
/// index.
void emitDebugPubTypes(bool GnuStyle = false);
+ void
+ emitDebugPubSection(bool GnuStyle, const MCSection *PSec, StringRef Name,
+ const StringMap<const DIE *> &(DwarfUnit::*Accessor)()
+ const);
+
/// \brief Emit visible names into a debug str section.
void emitDebugStr();
/// \brief Emit visible names into a debug ranges section.
void emitDebugRanges();
- /// \brief Emit visible names into a debug macinfo section.
- void emitDebugMacInfo();
-
/// \brief Emit inline info using custom format.
void emitDebugInlineInfo();
/// DWARF 5 Experimental Split Dwarf Emitters
+ /// \brief Initialize common features of skeleton units.
+ void initSkeletonUnit(const DwarfUnit *U, DIE *Die, DwarfUnit *NewU);
+
/// \brief Construct the split debug info compile unit for the debug info
/// section.
- CompileUnit *constructSkeletonCU(const CompileUnit *CU);
+ DwarfCompileUnit *constructSkeletonCU(const DwarfCompileUnit *CU);
- /// \brief Emit the local split abbreviations.
- void emitSkeletonAbbrevs(const MCSection *);
+ /// \brief Construct the split debug info compile unit for the debug info
+ /// section.
+ DwarfTypeUnit *constructSkeletonTU(DwarfTypeUnit *TU);
/// \brief Emit the debug info dwo section.
void emitDebugInfoDWO();
/// \brief Emit the debug abbrev dwo section.
void emitDebugAbbrevDWO();
+ /// \brief Emit the debug line dwo section.
+ void emitDebugLineDWO();
+
/// \brief Emit the debug str dwo section.
void emitDebugStrDWO();
- /// \brief Create new CompileUnit for the given metadata node with tag
+ /// Flags to let the linker know we have emitted new style pubnames. Only
+ /// emit it here if we don't have a skeleton CU for split dwarf.
+ void addGnuPubAttributes(DwarfUnit *U, DIE *D) const;
+
+ /// \brief Create new DwarfCompileUnit for the given metadata node with tag
/// DW_TAG_compile_unit.
- CompileUnit *constructCompileUnit(DICompileUnit DIUnit);
+ DwarfCompileUnit *constructDwarfCompileUnit(DICompileUnit DIUnit,
+ bool Singular);
/// \brief Construct subprogram DIE.
- void constructSubprogramDIE(CompileUnit *TheCU, const MDNode *N);
+ void constructSubprogramDIE(DwarfCompileUnit *TheCU, const MDNode *N);
/// \brief Construct imported_module or imported_declaration DIE.
- void constructImportedEntityDIE(CompileUnit *TheCU, const MDNode *N);
+ void constructImportedEntityDIE(DwarfCompileUnit *TheCU, const MDNode *N);
/// \brief Construct import_module DIE.
- void constructImportedEntityDIE(CompileUnit *TheCU, const MDNode *N,
+ void constructImportedEntityDIE(DwarfCompileUnit *TheCU, const MDNode *N,
DIE *Context);
/// \brief Construct import_module DIE.
- void constructImportedEntityDIE(CompileUnit *TheCU,
- const DIImportedEntity &Module,
- DIE *Context);
+ void constructImportedEntityDIE(DwarfCompileUnit *TheCU,
+ const DIImportedEntity &Module, DIE *Context);
/// \brief Register a source line with debug info. Returns the unique
/// label that was emitted and which provides correspondence to the
/// \brief If Var is an current function argument that add it in
/// CurrentFnArguments list.
- bool addCurrentFnArgument(const MachineFunction *MF,
- DbgVariable *Var, LexicalScope *Scope);
+ bool addCurrentFnArgument(DbgVariable *Var, LexicalScope *Scope);
/// \brief Populate LexicalScope entries with variables' info.
- void collectVariableInfo(const MachineFunction *,
- SmallPtrSet<const MDNode *, 16> &ProcessedVars);
+ void collectVariableInfo(SmallPtrSet<const MDNode *, 16> &ProcessedVars);
/// \brief Collect variable information from the side table maintained
/// by MMI.
- void collectVariableInfoFromMMITable(const MachineFunction * MF,
- SmallPtrSet<const MDNode *, 16> &P);
+ void collectVariableInfoFromMMITable(SmallPtrSet<const MDNode *, 16> &P);
/// \brief Ensure that a label will be emitted before MI.
void requestLabelBeforeInsn(const MachineInstr *MI) {
- LabelsBeforeInsn.insert(std::make_pair(MI, (MCSymbol*)0));
+ LabelsBeforeInsn.insert(std::make_pair(MI, (MCSymbol *)0));
}
/// \brief Return Label preceding the instruction.
/// \brief Ensure that a label will be emitted after MI.
void requestLabelAfterInsn(const MachineInstr *MI) {
- LabelsAfterInsn.insert(std::make_pair(MI, (MCSymbol*)0));
+ LabelsAfterInsn.insert(std::make_pair(MI, (MCSymbol *)0));
}
/// \brief Return Label immediately following the instruction.
MCSymbol *getLabelAfterInsn(const MachineInstr *MI);
+ void attachLowHighPC(DwarfCompileUnit *Unit, DIE *D, MCSymbol *Begin,
+ MCSymbol *End);
+
public:
//===--------------------------------------------------------------------===//
// Main entry points.
return MDTypeNodeToDieMap.lookup(TypeMD);
}
+ /// \brief Look up or create an entry in the OdrMemberMap.
+ const MDNode *&getOrCreateOdrMember(StringRef Key) {
+ return OdrMemberMap.GetOrCreateValue(Key).getValue();
+ }
+
/// \brief Emit all Dwarf sections that should come prior to the
/// content.
void beginModule();
/// \brief Emit all Dwarf sections that should come after the content.
- void endModule();
+ void endModule() override;
/// \brief Gather pre-function debug information.
- void beginFunction(const MachineFunction *MF);
+ void beginFunction(const MachineFunction *MF) override;
/// \brief Gather and emit post-function debug information.
- void endFunction(const MachineFunction *MF);
+ void endFunction(const MachineFunction *MF) override;
/// \brief Process beginning of an instruction.
- void beginInstruction(const MachineInstr *MI);
+ void beginInstruction(const MachineInstr *MI) override;
/// \brief Process end of an instruction.
- void endInstruction(const MachineInstr *MI);
+ void endInstruction() override;
/// \brief Add a DIE to the set of types that we're going to pull into
/// type units.
- void addTypeUnitType(uint16_t Language, DIE *Die, DICompositeType CTy);
+ void addDwarfTypeUnitType(DwarfCompileUnit &CU, StringRef Identifier,
+ DIE *Die, DICompositeType CTy);
/// \brief Add a label so that arange data can be generated for it.
void addArangeLabel(SymbolCU SCU) { ArangeLabels.push_back(SCU); }
/// \brief For symbols that have a size designated (e.g. common symbols),
/// this tracks that size.
- void setSymbolSize(const MCSymbol *Sym, uint64_t Size) { SymSize[Sym] = Size;}
-
- /// \brief Look up the source id with the given directory and source file
- /// names. If none currently exists, create a new id and insert it in the
- /// SourceIds map.
- unsigned getOrCreateSourceID(StringRef DirName, StringRef FullName,
- unsigned CUID);
+ void setSymbolSize(const MCSymbol *Sym, uint64_t Size) override {
+ SymSize[Sym] = Size;
+ }
/// \brief Recursively Emits a debug information entry.
- void emitDIE(DIE *Die, ArrayRef<DIEAbbrev *> Abbrevs);
+ void emitDIE(DIE *Die);
// Experimental DWARF5 features.
/// \brief Returns whether or not to emit tables that dwarf consumers can
/// use to accelerate lookup.
- bool useDwarfAccelTables() { return HasDwarfAccelTables; }
+ bool useDwarfAccelTables() const { return HasDwarfAccelTables; }
/// \brief Returns whether or not to change the current debug info for the
/// split dwarf proposal support.
- bool useSplitDwarf() { return HasSplitDwarf; }
+ bool useSplitDwarf() const { return HasSplitDwarf; }
+
+ /// \brief Returns whether or not to use AT_ranges for compilation units.
+ bool useCURanges() const { return HasCURanges; }
/// Returns the Dwarf Version.
unsigned getDwarfVersion() const { return DwarfVersion; }
+ /// Returns the section symbol for the .debug_loc section.
+ MCSymbol *getDebugLocSym() const { return DwarfDebugLocSectionSym; }
+
+ /// Returns the entries for the .debug_loc section.
+ const SmallVectorImpl<DebugLocEntry> &getDebugLocEntries() const {
+ return DotDebugLocEntries;
+ }
+
+ /// \brief Emit an entry for the debug loc section. This can be used to
+ /// handle an entry that's going to be emitted into the debug loc section.
+ void emitDebugLocEntry(ByteStreamer &Streamer, const DebugLocEntry &Entry);
+
/// Find the MDNode for the given reference.
template <typename T> T resolve(DIRef<T> Ref) const {
return Ref.resolve(TypeIdentifierMap);
}
+ /// Find the DwarfCompileUnit for the given CU Die.
+ DwarfCompileUnit *lookupUnit(const DIE *CU) const {
+ return CUDieMap.lookup(CU);
+ }
/// isSubprogramContext - Return true if Context is either a subprogram
/// or another context nested inside a subprogram.
bool isSubprogramContext(const MDNode *Context);
-
};
} // End of namespace llvm