diff --git a/lib/CodeGen/AsmPrinter/DwarfExpression.cpp b/lib/CodeGen/AsmPrinter/DwarfExpression.cpp
index 01c9e2497dd841fc646c6eaca00841612de18e7f..eb101ca2dcbbeee70ee45ee63f284a560e39d43b 100644 (file)
//===----------------------------------------------------------------------===//
#include "DwarfExpression.h"
+#include "DwarfDebug.h"
#include "llvm/ADT/SmallBitVector.h"
+#include "llvm/CodeGen/AsmPrinter.h"
#include "llvm/Support/Dwarf.h"
#include "llvm/Target/TargetMachine.h"
#include "llvm/Target/TargetRegisterInfo.h"
#include "llvm/Target/TargetSubtargetInfo.h"
-
using namespace llvm;
-void DwarfExpression::AddReg(int DwarfReg, const char* Comment) {
+const TargetRegisterInfo *DwarfExpression::getTRI() const {
+ return AP.TM.getSubtargetImpl()->getRegisterInfo();
+}
+
+unsigned DwarfExpression::getDwarfVersion() const {
+ return AP.getDwarfDebug()->getDwarfVersion();
+}
+
+void DwarfExpression::AddReg(int DwarfReg, const char *Comment) {
assert(DwarfReg >= 0 && "invalid negative dwarf register number");
if (DwarfReg < 32) {
EmitOp(dwarf::DW_OP_reg0 + DwarfReg, Comment);
EmitOp(dwarf::DW_OP_deref);
}
-void DwarfExpression::AddOpPiece(unsigned SizeInBits,
- unsigned OffsetInBits) {
+void DwarfExpression::AddOpPiece(unsigned SizeInBits, unsigned OffsetInBits) {
assert(SizeInBits > 0 && "piece has size zero");
const unsigned SizeOfByte = 8;
if (OffsetInBits > 0 || SizeInBits % SizeOfByte) {
EmitOp(dwarf::DW_OP_shr);
}
-void DwarfExpression::AddMachineRegPiece(unsigned MachineReg,
+bool DwarfExpression::AddMachineRegIndirect(unsigned MachineReg, int Offset) {
+ int DwarfReg = getTRI()->getDwarfRegNum(MachineReg, false);
+ if (DwarfReg < 0)
+ return false;
+
+ if (isFrameRegister(MachineReg)) {
+ // If variable offset is based in frame register then use fbreg.
+ EmitOp(dwarf::DW_OP_fbreg);
+ EmitSigned(Offset);
+ } else {
+ AddRegIndirect(DwarfReg, Offset);
+ }
+ return true;
+}
+
+bool DwarfExpression::AddMachineRegPiece(unsigned MachineReg,
unsigned PieceSizeInBits,
unsigned PieceOffsetInBits) {
- const TargetRegisterInfo *TRI = TM.getSubtargetImpl()->getRegisterInfo();
+ const TargetRegisterInfo *TRI = getTRI();
int Reg = TRI->getDwarfRegNum(MachineReg, false);
// If this is a valid register number, emit it.
if (Reg >= 0) {
AddReg(Reg);
- AddOpPiece(PieceSizeInBits, PieceOffsetInBits);
- return;
+ if (PieceSizeInBits)
+ AddOpPiece(PieceSizeInBits, PieceOffsetInBits);
+ return true;
}
// Walk up the super-register chain until we find a valid number.
AddShr(RegOffset);
AddOpPiece(Size, PieceOffsetInBits);
}
- return;
+ return true;
}
}
}
}
- if (CurPos == PieceOffsetInBits)
- // FIXME: We have no reasonable way of handling errors in here.
- EmitOp(dwarf::DW_OP_nop, "nop (could not find a dwarf register number)");
+ return CurPos > PieceOffsetInBits;
+}
+
+void DwarfExpression::AddSignedConstant(int Value) {
+ EmitOp(dwarf::DW_OP_consts);
+ EmitSigned(Value);
+ // The proper way to describe a constant value is
+ // DW_OP_constu <const>, DW_OP_stack_value.
+ // Unfortunately, DW_OP_stack_value was not available until DWARF-4,
+ // so we will continue to generate DW_OP_constu <const> for DWARF-2
+ // and DWARF-3. Technically, this is incorrect since DW_OP_const <const>
+ // actually describes a value at a constant addess, not a constant value.
+ // However, in the past there was no better way to describe a constant
+ // value, so the producers and consumers started to rely on heuristics
+ // to disambiguate the value vs. location status of the expression.
+ // See PR21176 for more details.
+ if (getDwarfVersion() >= 4)
+ EmitOp(dwarf::DW_OP_stack_value);
+}
+
+void DwarfExpression::AddUnsignedConstant(unsigned Value) {
+ EmitOp(dwarf::DW_OP_constu);
+ EmitUnsigned(Value);
+ // cf. comment in DwarfExpression::AddSignedConstant().
+ if (getDwarfVersion() >= 4)
+ EmitOp(dwarf::DW_OP_stack_value);
+}
+
+static unsigned getOffsetOrZero(unsigned OffsetInBits,
+ unsigned PieceOffsetInBits) {
+ if (OffsetInBits == PieceOffsetInBits)
+ return 0;
+ assert(OffsetInBits >= PieceOffsetInBits && "overlapping pieces");
+ return OffsetInBits;
+}
+
+bool DwarfExpression::AddMachineRegExpression(DIExpression Expr,
+ unsigned MachineReg,
+ unsigned PieceOffsetInBits) {
+ auto I = Expr.begin();
+ // Pattern-match combinations for which more efficient representations exist
+ // first.
+ if (I == Expr.end())
+ return AddMachineRegPiece(MachineReg);
+
+ bool ValidReg = false;
+ switch (*I) {
+ case dwarf::DW_OP_piece: {
+ unsigned SizeOfByte = 8;
+ unsigned OffsetInBits = I.getArg(1) * SizeOfByte;
+ unsigned SizeInBits = I.getArg(2) * SizeOfByte;
+ // Piece always comes at the end of the expression.
+ return AddMachineRegPiece(MachineReg, SizeInBits,
+ getOffsetOrZero(OffsetInBits, PieceOffsetInBits));
+ }
+ case dwarf::DW_OP_plus:
+ // [DW_OP_reg,Offset,DW_OP_plus,DW_OP_deref] --> [DW_OP_breg,Offset].
+ if (*std::next(I) == dwarf::DW_OP_deref) {
+ unsigned Offset = I.getArg(1);
+ ValidReg = AddMachineRegIndirect(MachineReg, Offset);
+ std::advance(I, 2);
+ break;
+ } else
+ ValidReg = AddMachineRegPiece(MachineReg);
+ case dwarf::DW_OP_deref:
+ // [DW_OP_reg,DW_OP_deref] --> [DW_OP_breg].
+ ValidReg = AddMachineRegIndirect(MachineReg);
+ ++I;
+ break;
+ default:
+ llvm_unreachable("unsupported operand");
+ }
+
+ if (!ValidReg)
+ return false;
+
+ // Emit remaining elements of the expression.
+ AddExpression(I, PieceOffsetInBits);
+ return true;
+}
+
+void DwarfExpression::AddExpression(DIExpression::iterator I,
+ unsigned PieceOffsetInBits) {
+ for (; I != DIExpression::iterator(); ++I) {
+ switch (*I) {
+ case dwarf::DW_OP_piece: {
+ unsigned SizeOfByte = 8;
+ unsigned OffsetInBits = I.getArg(1) * SizeOfByte;
+ unsigned SizeInBits = I.getArg(2) * SizeOfByte;
+ AddOpPiece(SizeInBits, getOffsetOrZero(OffsetInBits, PieceOffsetInBits));
+ break;
+ }
+ case dwarf::DW_OP_plus:
+ EmitOp(dwarf::DW_OP_plus_uconst);
+ EmitUnsigned(I.getArg(1));
+ break;
+ case dwarf::DW_OP_deref:
+ EmitOp(dwarf::DW_OP_deref);
+ break;
+ default:
+ llvm_unreachable("unhandled opcode found in DIExpression");
+ }
+ }
}