Rename DIExpressionIterator to DIExpression::iterator.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfExpression.h
index 870b9716039d486965c66ef7c15d447ac1a0b28c..14e07fcdb98ba41b8b0b3c35a0a25ac93fc4401f 100644 (file)
@@ -14,6 +14,7 @@
 #ifndef LLVM_LIB_CODEGEN_ASMPRINTER_DWARFEXPRESSION_H
 #define LLVM_LIB_CODEGEN_ASMPRINTER_DWARFEXPRESSION_H
 
+#include "llvm/IR/DebugInfo.h"
 #include "llvm/Support/DataTypes.h"
 
 namespace llvm {
@@ -21,6 +22,8 @@ namespace llvm {
 class AsmPrinter;
 class ByteStreamer;
 class TargetRegisterInfo;
+class DwarfUnit;
+class DIELoc;
 
 /// Base class containing the logic for constructing DWARF expressions
 /// independently of whether they are emitted into a DIE or into a .debug_loc
@@ -59,7 +62,7 @@ public:
   void AddShr(unsigned ShiftBy);
 
   /// Emit an indirect dwarf register operation for the given machine register.
-  /// Returns false if no DWARF register exists for MachineReg.
+  /// \return false if no DWARF register exists for MachineReg.
   bool AddMachineRegIndirect(unsigned MachineReg, int Offset = 0);
 
   /// \brief Emit a partial DWARF register operation.
@@ -74,15 +77,27 @@ public:
   /// function will attempt to emit a DWARF register by emitting a
   /// piece of a super-register or by piecing together multiple
   /// subregisters that alias the register.
-  void AddMachineRegPiece(unsigned MachineReg, unsigned PieceSizeInBits = 0,
+  ///
+  /// \return false if no DWARF register exists for MachineReg.
+  bool AddMachineRegPiece(unsigned MachineReg, unsigned PieceSizeInBits = 0,
                           unsigned PieceOffsetInBits = 0);
 
   /// Emit a signed constant.
   void AddSignedConstant(int Value);
   /// Emit an unsigned constant.
   void AddUnsignedConstant(unsigned Value);
-};
 
+  /// Emit an entire DIExpression on top of a machine register location.
+  /// \param PieceOffsetInBits If this is one piece out of a fragmented
+  /// location, this is the offset of the piece inside the entire variable.
+  /// \return false if no DWARF register exists for MachineReg.
+  bool AddMachineRegExpression(DIExpression Expr, unsigned MachineReg,
+                               unsigned PieceOffsetInBits = 0);
+  /// Emit a the operations remaining the DIExpressionIterator I.
+  /// \param PieceOffsetInBits If this is one piece out of a fragmented
+  /// location, this is the offset of the piece inside the entire variable.
+void AddExpression(DIExpression::iterator I, unsigned PieceOffsetInBits = 0);
+};
 
 /// DwarfExpression implementation for .debug_loc entries.
 class DebugLocDwarfExpression : public DwarfExpression {
@@ -97,6 +112,21 @@ public:
   void EmitUnsigned(unsigned Value) override;
   bool isFrameRegister(unsigned MachineReg) override;
 };
+
+/// DwarfExpression implementation for singular DW_AT_location.
+class DIEDwarfExpression : public DwarfExpression {
+  DwarfUnit &DU;
+  DIELoc ¨
+
+public:
+  DIEDwarfExpression(const AsmPrinter &AP, DwarfUnit &DU, DIELoc &DIE)
+      : DwarfExpression(AP), DU(DU), DIE(DIE) {}
+
+  void EmitOp(uint8_t Op, const char *Comment = nullptr) override;
+  void EmitSigned(int Value) override;
+  void EmitUnsigned(unsigned Value) override;
+  bool isFrameRegister(unsigned MachineReg) override;
+};
 }
 
 #endif