Rename DIExpressionIterator to DIExpression::iterator.
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfExpression.h
index 92e4d5d8a2905b9d0f4a528a937b02a9d3950da8..14e07fcdb98ba41b8b0b3c35a0a25ac93fc4401f 100644 (file)
@@ -93,11 +93,10 @@ public:
   /// \return false if no DWARF register exists for MachineReg.
   bool AddMachineRegExpression(DIExpression Expr, unsigned MachineReg,
                                unsigned PieceOffsetInBits = 0);
-  /// Emit a the operations in a DIExpression, starting from element I.
+  /// Emit a the operations remaining the DIExpressionIterator I.
   /// \param PieceOffsetInBits If this is one piece out of a fragmented
   /// location, this is the offset of the piece inside the entire variable.
-  void AddExpression(DIExpression Expr, unsigned PieceOffsetInBits = 0,
-                     unsigned I = 0);
+void AddExpression(DIExpression::iterator I, unsigned PieceOffsetInBits = 0);
 };
 
 /// DwarfExpression implementation for .debug_loc entries.