index 193f4307d881a54e2f18b25d7517ce00bc09a135..f164f1c85133ba5bf58e530708a510614f79e015 100644 (file)
#define LLVM_LIB_CODEGEN_ASMPRINTER_DWARFEXPRESSION_H
#include "llvm/Support/DataTypes.h"
+#include "llvm/IR/DebugInfo.h"
namespace llvm {
-class TargetMachine;
+class AsmPrinter;
+class ByteStreamer;
+class TargetRegisterInfo;
/// Base class containing the logic for constructing DWARF expressions
/// independently of whether they are emitted into a DIE or into a .debug_loc
/// entry.
class DwarfExpression {
- TargetMachine &TM;
+protected:
+ const AsmPrinter ≈
+ // Various convenience accessors that extract things out of AsmPrinter.
+ const TargetRegisterInfo *getTRI() const;
+ unsigned getDwarfVersion() const;
+
public:
- DwarfExpression(TargetMachine &TM) : TM(TM) {}
+ DwarfExpression(const AsmPrinter &AP) : AP(AP) {}
+ virtual ~DwarfExpression() {}
- virtual void EmitOp(uint8_t Op, const char* Comment = nullptr) = 0;
+ /// Output a dwarf operand and an optional assembler comment.
+ virtual void EmitOp(uint8_t Op, const char *Comment = nullptr) = 0;
+ /// Emit a raw signed value.
virtual void EmitSigned(int Value) = 0;
+ /// Emit a raw unsigned value.
virtual void EmitUnsigned(unsigned Value) = 0;
+ /// Return whether the given machine register is the frame register in the
+ /// current function.
+ virtual bool isFrameRegister(unsigned MachineReg) = 0;
+
/// Emit a dwarf register operation.
- void AddReg(int DwarfReg, const char* Comment = nullptr);
+ void AddReg(int DwarfReg, const char *Comment = nullptr);
/// Emit an (double-)indirect dwarf register operation.
void AddRegIndirect(int DwarfReg, int Offset, bool Deref = false);
/// Emit a shift-right dwarf expression.
void AddShr(unsigned ShiftBy);
+ /// Emit an indirect dwarf register operation for the given machine register.
+ /// Returns false if no DWARF register exists for MachineReg.
+ bool AddMachineRegIndirect(unsigned MachineReg, int Offset = 0);
+
/// \brief Emit a partial DWARF register operation.
- /// \param MLoc the register
- /// \param PieceSize size and
- /// \param PieceOffset offset of the piece in bits, if this is one
- /// piece of an aggregate value.
+ /// \param MachineReg the register
+ /// \param PieceSizeInBits size and
+ /// \param PieceOffsetInBits offset of the piece in bits, if this is one
+ /// piece of an aggregate value.
///
/// If size and offset is zero an operation for the entire
/// register is emitted: Some targets do not provide a DWARF
/// function will attempt to emit a DWARF register by emitting a
/// piece of a super-register or by piecing together multiple
/// subregisters that alias the register.
- void AddMachineRegPiece(unsigned MachineReg,
- unsigned PieceSizeInBits = 0,
+ void AddMachineRegPiece(unsigned MachineReg, unsigned PieceSizeInBits = 0,
unsigned PieceOffsetInBits = 0);
+
+ /// Emit a signed constant.
+ void AddSignedConstant(int Value);
+ /// Emit an unsigned constant.
+ void AddUnsignedConstant(unsigned Value);
+
+ /// Emit an entire DIExpression on top of a machine register location.
+ /// \param PieceOffsetInBits If this is one piece out of a fragmented
+ /// location, this is the offset of the piece inside the entire variable.
+ void AddMachineRegExpression(DIExpression Expr, unsigned MachineReg,
+ unsigned PieceOffsetInBits = 0);
+ /// Emit a the operations in a DIExpression, starting from element I.
+ /// \param PieceOffsetInBits If this is one piece out of a fragmented
+ /// location, this is the offset of the piece inside the entire variable.
+ void AddExpression(DIExpression Expr, unsigned PieceOffsetInBits = 0,
+ unsigned I = 0);
};
+/// DwarfExpression implementation for .debug_loc entries.
+class DebugLocDwarfExpression : public DwarfExpression {
+ ByteStreamer &BS;
+
+public:
+ DebugLocDwarfExpression(const AsmPrinter &AP, ByteStreamer &BS)
+ : DwarfExpression(AP), BS(BS) {}
+
+ void EmitOp(uint8_t Op, const char *Comment = nullptr) override;
+ void EmitSigned(int Value) override;
+ void EmitUnsigned(unsigned Value) override;
+ bool isFrameRegister(unsigned MachineReg) override;
+};
}
#endif