Debug Info: Move the complex expression handling (=the remainder) of
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfExpression.h
index 193f4307d881a54e2f18b25d7517ce00bc09a135..f164f1c85133ba5bf58e530708a510614f79e015 100644 (file)
 #define LLVM_LIB_CODEGEN_ASMPRINTER_DWARFEXPRESSION_H
 
 #include "llvm/Support/DataTypes.h"
 #define LLVM_LIB_CODEGEN_ASMPRINTER_DWARFEXPRESSION_H
 
 #include "llvm/Support/DataTypes.h"
+#include "llvm/IR/DebugInfo.h"
 
 namespace llvm {
 
 
 namespace llvm {
 
-class TargetMachine;
+class AsmPrinter;
+class ByteStreamer;
+class TargetRegisterInfo;
 
 /// Base class containing the logic for constructing DWARF expressions
 /// independently of whether they are emitted into a DIE or into a .debug_loc
 /// entry.
 class DwarfExpression {
 
 /// Base class containing the logic for constructing DWARF expressions
 /// independently of whether they are emitted into a DIE or into a .debug_loc
 /// entry.
 class DwarfExpression {
-  TargetMachine &TM;
+protected:
+  const AsmPrinter ≈
+  // Various convenience accessors that extract things out of AsmPrinter.
+  const TargetRegisterInfo *getTRI() const;
+  unsigned getDwarfVersion() const;
+
 public:
 public:
-  DwarfExpression(TargetMachine &TM) : TM(TM) {}
+  DwarfExpression(const AsmPrinter &AP) : AP(AP) {}
+  virtual ~DwarfExpression() {}
 
 
-  virtual void EmitOp(uint8_t Op, const char* Comment = nullptr) = 0;
+  /// Output a dwarf operand and an optional assembler comment.
+  virtual void EmitOp(uint8_t Op, const char *Comment = nullptr) = 0;
+  /// Emit a raw signed value.
   virtual void EmitSigned(int Value) = 0;
   virtual void EmitSigned(int Value) = 0;
+  /// Emit a raw unsigned value.
   virtual void EmitUnsigned(unsigned Value) = 0;
   virtual void EmitUnsigned(unsigned Value) = 0;
+  /// Return whether the given machine register is the frame register in the
+  /// current function.
+  virtual bool isFrameRegister(unsigned MachineReg) = 0;
+
   /// Emit a dwarf register operation.
   /// Emit a dwarf register operation.
-  void AddReg(int DwarfReg, const charComment = nullptr);
+  void AddReg(int DwarfReg, const char *Comment = nullptr);
   /// Emit an (double-)indirect dwarf register operation.
   void AddRegIndirect(int DwarfReg, int Offset, bool Deref = false);
 
   /// Emit an (double-)indirect dwarf register operation.
   void AddRegIndirect(int DwarfReg, int Offset, bool Deref = false);
 
@@ -43,11 +59,15 @@ public:
   /// Emit a shift-right dwarf expression.
   void AddShr(unsigned ShiftBy);
 
   /// Emit a shift-right dwarf expression.
   void AddShr(unsigned ShiftBy);
 
+  /// Emit an indirect dwarf register operation for the given machine register.
+  /// Returns false if no DWARF register exists for MachineReg.
+  bool AddMachineRegIndirect(unsigned MachineReg, int Offset = 0);
+
   /// \brief Emit a partial DWARF register operation.
   /// \brief Emit a partial DWARF register operation.
-  /// \param MLoc             the register
-  /// \param PieceSize        size and
-  /// \param PieceOffset      offset of the piece in bits, if this is one
-  ///                         piece of an aggregate value.
+  /// \param MachineReg        the register
+  /// \param PieceSizeInBits   size and
+  /// \param PieceOffsetInBits offset of the piece in bits, if this is one
+  ///                          piece of an aggregate value.
   ///
   /// If size and offset is zero an operation for the entire
   /// register is emitted: Some targets do not provide a DWARF
   ///
   /// If size and offset is zero an operation for the entire
   /// register is emitted: Some targets do not provide a DWARF
@@ -55,11 +75,39 @@ public:
   /// function will attempt to emit a DWARF register by emitting a
   /// piece of a super-register or by piecing together multiple
   /// subregisters that alias the register.
   /// function will attempt to emit a DWARF register by emitting a
   /// piece of a super-register or by piecing together multiple
   /// subregisters that alias the register.
-  void AddMachineRegPiece(unsigned MachineReg,
-                          unsigned PieceSizeInBits = 0,
+  void AddMachineRegPiece(unsigned MachineReg, unsigned PieceSizeInBits = 0,
                           unsigned PieceOffsetInBits = 0);
                           unsigned PieceOffsetInBits = 0);
+
+  /// Emit a signed constant.
+  void AddSignedConstant(int Value);
+  /// Emit an unsigned constant.
+  void AddUnsignedConstant(unsigned Value);
+
+  /// Emit an entire DIExpression on top of a machine register location.
+  /// \param PieceOffsetInBits If this is one piece out of a fragmented
+  /// location, this is the offset of the piece inside the entire variable.
+  void AddMachineRegExpression(DIExpression Expr, unsigned MachineReg,
+                               unsigned PieceOffsetInBits = 0);
+  /// Emit a the operations in a DIExpression, starting from element I.
+  /// \param PieceOffsetInBits If this is one piece out of a fragmented
+  /// location, this is the offset of the piece inside the entire variable.
+  void AddExpression(DIExpression Expr, unsigned PieceOffsetInBits = 0,
+                     unsigned I = 0);
 };
 
 };
 
+/// DwarfExpression implementation for .debug_loc entries.
+class DebugLocDwarfExpression : public DwarfExpression {
+  ByteStreamer &BS;
+
+public:
+  DebugLocDwarfExpression(const AsmPrinter &AP, ByteStreamer &BS)
+      : DwarfExpression(AP), BS(BS) {}
+
+  void EmitOp(uint8_t Op, const char *Comment = nullptr) override;
+  void EmitSigned(int Value) override;
+  void EmitUnsigned(unsigned Value) override;
+  bool isFrameRegister(unsigned MachineReg) override;
+};
 }
 
 #endif
 }
 
 #endif