]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blobdiff - lib/CodeGen/AsmPrinter/DwarfUnit.cpp
Debug info: Implement (rvalue) reference qualifiers for C++11 non-static
[opencl/llvm.git] / lib / CodeGen / AsmPrinter / DwarfUnit.cpp
index 663bc0c4d4a378807b99e6c5def1caf57ac06116..69240f870f9e581661b7d18f8da9614d7005e5e9 100644 (file)
 
 using namespace llvm;
 
-static cl::opt<bool> GenerateTypeUnits("generate-type-units", cl::Hidden,
-                                       cl::desc("Generate DWARF4 type units."),
-                                       cl::init(false));
+static cl::opt<bool>
+GenerateDwarfTypeUnits("generate-type-units", cl::Hidden,
+                       cl::desc("Generate DWARF4 type units."),
+                       cl::init(false));
 
 /// Unit - Unit constructor.
-Unit::Unit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
-           DwarfDebug *DW, DwarfUnits *DWU)
+DwarfUnit::DwarfUnit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
+                     DwarfDebug *DW, DwarfFile *DWU)
     : UniqueID(UID), Node(Node), UnitDie(D), DebugInfoOffset(0), Asm(A), DD(DW),
-      DU(DWU), IndexTyDie(0) {
+      DU(DWU), IndexTyDie(0), Section(0) {
   DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
 }
 
-CompileUnit::CompileUnit(unsigned UID, DIE *D, DICompileUnit Node,
-                         AsmPrinter *A, DwarfDebug *DW, DwarfUnits *DWU)
-    : Unit(UID, D, Node, A, DW, DWU) {
+DwarfCompileUnit::DwarfCompileUnit(unsigned UID, DIE *D, DICompileUnit Node,
+                                   AsmPrinter *A, DwarfDebug *DW,
+                                   DwarfFile *DWU)
+    : DwarfUnit(UID, D, Node, A, DW, DWU) {
   insertDIE(Node, D);
 }
 
-TypeUnit::TypeUnit(unsigned UID, DIE *D, uint16_t Language, AsmPrinter *A,
-                   DwarfDebug *DW, DwarfUnits *DWU)
-    : Unit(UID, D, DICompileUnit(), A, DW, DWU), Language(Language) {}
+DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DIE *D, uint16_t Language,
+                             AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
+    : DwarfUnit(UID, D, DICompileUnit(), A, DW, DWU), Language(Language) {}
 
 /// ~Unit - Destructor for compile unit.
-Unit::~Unit() {
+DwarfUnit::~DwarfUnit() {
   for (unsigned j = 0, M = DIEBlocks.size(); j < M; ++j)
     DIEBlocks[j]->~DIEBlock();
 }
 
 /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
 /// information entry.
-DIEEntry *Unit::createDIEEntry(DIE *Entry) {
+DIEEntry *DwarfUnit::createDIEEntry(DIE *Entry) {
   DIEEntry *Value = new (DIEValueAllocator) DIEEntry(Entry);
   return Value;
 }
 
 /// getDefaultLowerBound - Return the default lower bound for an array. If the
 /// DWARF version doesn't handle the language, return -1.
-int64_t Unit::getDefaultLowerBound() const {
+int64_t DwarfUnit::getDefaultLowerBound() const {
   switch (getLanguage()) {
   default:
     break;
@@ -123,14 +125,14 @@ static bool isShareableAcrossCUs(DIDescriptor D) {
   // together.
   return (D.isType() ||
           (D.isSubprogram() && !DISubprogram(D).isDefinition())) &&
-         !GenerateTypeUnits;
+         !GenerateDwarfTypeUnits;
 }
 
 /// getDIE - Returns the debug information entry map slot for the
 /// specified debug variable. We delegate the request to DwarfDebug
 /// when the DIE for this MDNode can be shared across CUs. The mappings
 /// will be kept in DwarfDebug for shareable DIEs.
-DIE *Unit::getDIE(DIDescriptor D) const {
+DIE *DwarfUnit::getDIE(DIDescriptor D) const {
   if (isShareableAcrossCUs(D))
     return DD->getDIE(D);
   return MDNodeToDieMap.lookup(D);
@@ -139,7 +141,7 @@ DIE *Unit::getDIE(DIDescriptor D) const {
 /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
 /// when the DIE for this MDNode can be shared across CUs. The mappings
 /// will be kept in DwarfDebug for shareable DIEs.
-void Unit::insertDIE(DIDescriptor Desc, DIE *D) {
+void DwarfUnit::insertDIE(DIDescriptor Desc, DIE *D) {
   if (isShareableAcrossCUs(Desc)) {
     DD->insertDIE(Desc, D);
     return;
@@ -148,7 +150,7 @@ void Unit::insertDIE(DIDescriptor Desc, DIE *D) {
 }
 
 /// addFlag - Add a flag that is true.
-void Unit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
+void DwarfUnit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
   if (DD->getDwarfVersion() >= 4)
     Die->addValue(Attribute, dwarf::DW_FORM_flag_present, DIEIntegerOne);
   else
@@ -157,8 +159,8 @@ void Unit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
 
 /// addUInt - Add an unsigned integer attribute data and value.
 ///
-void Unit::addUInt(DIE *Die, dwarf::Attribute Attribute,
-                   Optional<dwarf::Form> Form, uint64_t Integer) {
+void DwarfUnit::addUInt(DIE *Die, dwarf::Attribute Attribute,
+                        Optional<dwarf::Form> Form, uint64_t Integer) {
   if (!Form)
     Form = DIEInteger::BestForm(false, Integer);
   DIEValue *Value = Integer == 1 ? DIEIntegerOne : new (DIEValueAllocator)
@@ -166,21 +168,22 @@ void Unit::addUInt(DIE *Die, dwarf::Attribute Attribute,
   Die->addValue(Attribute, *Form, Value);
 }
 
-void Unit::addUInt(DIEBlock *Block, dwarf::Form Form, uint64_t Integer) {
+void DwarfUnit::addUInt(DIEBlock *Block, dwarf::Form Form, uint64_t Integer) {
   addUInt(Block, (dwarf::Attribute)0, Form, Integer);
 }
 
 /// addSInt - Add an signed integer attribute data and value.
 ///
-void Unit::addSInt(DIE *Die, dwarf::Attribute Attribute,
-                   Optional<dwarf::Form> Form, int64_t Integer) {
+void DwarfUnit::addSInt(DIE *Die, dwarf::Attribute Attribute,
+                        Optional<dwarf::Form> Form, int64_t Integer) {
   if (!Form)
     Form = DIEInteger::BestForm(true, Integer);
   DIEValue *Value = new (DIEValueAllocator) DIEInteger(Integer);
   Die->addValue(Attribute, *Form, Value);
 }
 
-void Unit::addSInt(DIEBlock *Die, Optional<dwarf::Form> Form, int64_t Integer) {
+void DwarfUnit::addSInt(DIEBlock *Die, Optional<dwarf::Form> Form,
+                        int64_t Integer) {
   addSInt(Die, (dwarf::Attribute)0, Form, Integer);
 }
 
@@ -189,7 +192,8 @@ void Unit::addSInt(DIEBlock *Die, Optional<dwarf::Form> Form, int64_t Integer) {
 /// more predictable sizes. In the case of split dwarf we emit an index
 /// into another table which gets us the static offset into the string
 /// table.
-void Unit::addString(DIE *Die, dwarf::Attribute Attribute, StringRef String) {
+void DwarfUnit::addString(DIE *Die, dwarf::Attribute Attribute,
+                          StringRef String) {
   DIEValue *Value;
   dwarf::Form Form;
   if (!DD->useSplitDwarf()) {
@@ -212,8 +216,8 @@ void Unit::addString(DIE *Die, dwarf::Attribute Attribute, StringRef String) {
 
 /// addLocalString - Add a string attribute data and value. This is guaranteed
 /// to be in the local string pool instead of indirected.
-void Unit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
-                          StringRef String) {
+void DwarfUnit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
+                               StringRef String) {
   MCSymbol *Symb = DU->getStringPoolEntry(String);
   DIEValue *Value;
   if (Asm->needsRelocationsForDwarfStringPool())
@@ -227,27 +231,28 @@ void Unit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
 
 /// addExpr - Add a Dwarf expression attribute data and value.
 ///
-void Unit::addExpr(DIEBlock *Die, dwarf::Form Form, const MCExpr *Expr) {
+void DwarfUnit::addExpr(DIEBlock *Die, dwarf::Form Form, const MCExpr *Expr) {
   DIEValue *Value = new (DIEValueAllocator) DIEExpr(Expr);
   Die->addValue((dwarf::Attribute)0, Form, Value);
 }
 
 /// addLabel - Add a Dwarf label attribute data and value.
 ///
-void Unit::addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
-                    const MCSymbol *Label) {
+void DwarfUnit::addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
+                         const MCSymbol *Label) {
   DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
   Die->addValue(Attribute, Form, Value);
 }
 
-void Unit::addLabel(DIEBlock *Die, dwarf::Form Form, const MCSymbol *Label) {
+void DwarfUnit::addLabel(DIEBlock *Die, dwarf::Form Form,
+                         const MCSymbol *Label) {
   addLabel(Die, (dwarf::Attribute)0, Form, Label);
 }
 
 /// addSectionLabel - Add a Dwarf section label attribute data and value.
 ///
-void Unit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
-                           const MCSymbol *Label) {
+void DwarfUnit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
+                                const MCSymbol *Label) {
   if (DD->getDwarfVersion() >= 4)
     addLabel(Die, Attribute, dwarf::DW_FORM_sec_offset, Label);
   else
@@ -256,8 +261,8 @@ void Unit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
 
 /// addSectionOffset - Add an offset into a section attribute data and value.
 ///
-void Unit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
-                            uint64_t Integer) {
+void DwarfUnit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
+                                 uint64_t Integer) {
   if (DD->getDwarfVersion() >= 4)
     addUInt(Die, Attribute, dwarf::DW_FORM_sec_offset, Integer);
   else
@@ -267,8 +272,8 @@ void Unit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
 /// addLabelAddress - Add a dwarf label attribute data and value using
 /// DW_FORM_addr or DW_FORM_GNU_addr_index.
 ///
-void CompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
-                                  MCSymbol *Label) {
+void DwarfCompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
+                                       MCSymbol *Label) {
   if (Label)
     DD->addArangeLabel(SymbolCU(this, Label));
 
@@ -290,7 +295,7 @@ void CompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
 /// addOpAddress - Add a dwarf op address data and value using the
 /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
 ///
-void Unit::addOpAddress(DIEBlock *Die, const MCSymbol *Sym) {
+void DwarfUnit::addOpAddress(DIEBlock *Die, const MCSymbol *Sym) {
   if (!DD->useSplitDwarf()) {
     addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_addr);
     addLabel(Die, dwarf::DW_FORM_udata, Sym);
@@ -302,8 +307,8 @@ void Unit::addOpAddress(DIEBlock *Die, const MCSymbol *Sym) {
 
 /// addSectionDelta - Add a section label delta attribute data and value.
 ///
-void Unit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
-                           const MCSymbol *Hi, const MCSymbol *Lo) {
+void DwarfUnit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
+                                const MCSymbol *Hi, const MCSymbol *Lo) {
   DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
   if (DD->getDwarfVersion() >= 4)
     Die->addValue(Attribute, dwarf::DW_FORM_sec_offset, Value);
@@ -313,11 +318,17 @@ void Unit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
 
 /// addDIEEntry - Add a DIE attribute data and value.
 ///
-void Unit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
+void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
   addDIEEntry(Die, Attribute, createDIEEntry(Entry));
 }
 
-void Unit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIEEntry *Entry) {
+void DwarfUnit::addDIETypeSignature(DIE *Die, const DwarfTypeUnit &Type) {
+  Die->addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
+                new (DIEValueAllocator) DIETypeSignature(Type));
+}
+
+void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute,
+                            DIEEntry *Entry) {
   const DIE *DieCU = Die->getUnitOrNull();
   const DIE *EntryCU = Entry->getEntry()->getUnitOrNull();
   if (!DieCU)
@@ -332,7 +343,7 @@ void Unit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIEEntry *Entry) {
 
 /// Create a DIE with the given Tag, add the DIE to its parent, and
 /// call insertDIE if MD is not null.
-DIE *Unit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
+DIE *DwarfUnit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
   DIE *Die = new DIE(Tag);
   Parent.addChild(Die);
   if (N)
@@ -342,7 +353,8 @@ DIE *Unit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
 
 /// addBlock - Add block data.
 ///
-void Unit::addBlock(DIE *Die, dwarf::Attribute Attribute, DIEBlock *Block) {
+void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute,
+                         DIEBlock *Block) {
   Block->ComputeSize(Asm);
   DIEBlocks.push_back(Block); // Memoize so we can call the destructor later on.
   Die->addValue(Attribute, Block->BestForm(), Block);
@@ -350,7 +362,7 @@ void Unit::addBlock(DIE *Die, dwarf::Attribute Attribute, DIEBlock *Block) {
 
 /// addSourceLine - Add location information to specified debug information
 /// entry.
-void Unit::addSourceLine(DIE *Die, DIVariable V) {
+void DwarfUnit::addSourceLine(DIE *Die, DIVariable V) {
   // Verify variable.
   if (!V.isVariable())
     return;
@@ -368,7 +380,7 @@ void Unit::addSourceLine(DIE *Die, DIVariable V) {
 
 /// addSourceLine - Add location information to specified debug information
 /// entry.
-void Unit::addSourceLine(DIE *Die, DIGlobalVariable G) {
+void DwarfUnit::addSourceLine(DIE *Die, DIGlobalVariable G) {
   // Verify global variable.
   if (!G.isGlobalVariable())
     return;
@@ -385,7 +397,7 @@ void Unit::addSourceLine(DIE *Die, DIGlobalVariable G) {
 
 /// addSourceLine - Add location information to specified debug information
 /// entry.
-void Unit::addSourceLine(DIE *Die, DISubprogram SP) {
+void DwarfUnit::addSourceLine(DIE *Die, DISubprogram SP) {
   // Verify subprogram.
   if (!SP.isSubprogram())
     return;
@@ -404,7 +416,7 @@ void Unit::addSourceLine(DIE *Die, DISubprogram SP) {
 
 /// addSourceLine - Add location information to specified debug information
 /// entry.
-void Unit::addSourceLine(DIE *Die, DIType Ty) {
+void DwarfUnit::addSourceLine(DIE *Die, DIType Ty) {
   // Verify type.
   if (!Ty.isType())
     return;
@@ -421,7 +433,7 @@ void Unit::addSourceLine(DIE *Die, DIType Ty) {
 
 /// addSourceLine - Add location information to specified debug information
 /// entry.
-void Unit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
+void DwarfUnit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
   // Verify type.
   if (!Ty.isObjCProperty())
     return;
@@ -439,7 +451,7 @@ void Unit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
 
 /// addSourceLine - Add location information to specified debug information
 /// entry.
-void Unit::addSourceLine(DIE *Die, DINameSpace NS) {
+void DwarfUnit::addSourceLine(DIE *Die, DINameSpace NS) {
   // Verify namespace.
   if (!NS.Verify())
     return;
@@ -458,8 +470,8 @@ void Unit::addSourceLine(DIE *Die, DINameSpace NS) {
 
 /// addVariableAddress - Add DW_AT_location attribute for a
 /// DbgVariable based on provided MachineLocation.
-void Unit::addVariableAddress(const DbgVariable &DV, DIE *Die,
-                              MachineLocation Location) {
+void DwarfUnit::addVariableAddress(const DbgVariable &DV, DIE *Die,
+                                   MachineLocation Location) {
   if (DV.variableHasComplexAddress())
     addComplexAddress(DV, Die, dwarf::DW_AT_location, Location);
   else if (DV.isBlockByrefVariable())
@@ -470,7 +482,7 @@ void Unit::addVariableAddress(const DbgVariable &DV, DIE *Die,
 }
 
 /// addRegisterOp - Add register operand.
-void Unit::addRegisterOp(DIEBlock *TheDie, unsigned Reg) {
+void DwarfUnit::addRegisterOp(DIEBlock *TheDie, unsigned Reg) {
   const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
   unsigned DWReg = RI->getDwarfRegNum(Reg, false);
   if (DWReg < 32)
@@ -482,7 +494,8 @@ void Unit::addRegisterOp(DIEBlock *TheDie, unsigned Reg) {
 }
 
 /// addRegisterOffset - Add register offset.
-void Unit::addRegisterOffset(DIEBlock *TheDie, unsigned Reg, int64_t Offset) {
+void DwarfUnit::addRegisterOffset(DIEBlock *TheDie, unsigned Reg,
+                                  int64_t Offset) {
   const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
   unsigned DWReg = RI->getDwarfRegNum(Reg, false);
   const TargetRegisterInfo *TRI = Asm->TM.getRegisterInfo();
@@ -500,8 +513,8 @@ void Unit::addRegisterOffset(DIEBlock *TheDie, unsigned Reg, int64_t Offset) {
 
 /// addAddress - Add an address attribute to a die based on the location
 /// provided.
-void Unit::addAddress(DIE *Die, dwarf::Attribute Attribute,
-                      const MachineLocation &Location, bool Indirect) {
+void DwarfUnit::addAddress(DIE *Die, dwarf::Attribute Attribute,
+                           const MachineLocation &Location, bool Indirect) {
   DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
 
   if (Location.isReg() && !Indirect)
@@ -522,9 +535,9 @@ void Unit::addAddress(DIE *Die, dwarf::Attribute Attribute,
 /// given the extra address information encoded in the DbgVariable, starting
 /// from the starting location.  Add the DWARF information to the die.
 ///
-void Unit::addComplexAddress(const DbgVariable &DV, DIE *Die,
-                             dwarf::Attribute Attribute,
-                             const MachineLocation &Location) {
+void DwarfUnit::addComplexAddress(const DbgVariable &DV, DIE *Die,
+                                  dwarf::Attribute Attribute,
+                                  const MachineLocation &Location) {
   DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
   unsigned N = DV.getNumAddrElements();
   unsigned i = 0;
@@ -615,9 +628,9 @@ void Unit::addComplexAddress(const DbgVariable &DV, DIE *Die,
 /// starting location.  Add the DWARF information to the die.  For
 /// more information, read large comment just above here.
 ///
-void Unit::addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
-                                dwarf::Attribute Attribute,
-                                const MachineLocation &Location) {
+void DwarfUnit::addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
+                                     dwarf::Attribute Attribute,
+                                     const MachineLocation &Location) {
   DIType Ty = DV.getType();
   DIType TmpTy = Ty;
   uint16_t Tag = Ty.getTag();
@@ -750,7 +763,8 @@ static uint64_t getBaseTypeSize(DwarfDebug *DD, DIDerivedType Ty) {
 }
 
 /// addConstantValue - Add constant value entry in variable DIE.
-void Unit::addConstantValue(DIE *Die, const MachineOperand &MO, DIType Ty) {
+void DwarfUnit::addConstantValue(DIE *Die, const MachineOperand &MO,
+                                 DIType Ty) {
   // FIXME: This is a bit conservative/simple - it emits negative values at
   // their maximum bit width which is a bit unfortunate (& doesn't prefer
   // udata/sdata over dataN as suggested by the DWARF spec)
@@ -788,7 +802,7 @@ void Unit::addConstantValue(DIE *Die, const MachineOperand &MO, DIType Ty) {
 }
 
 /// addConstantFPValue - Add constant value entry in variable DIE.
-void Unit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
+void DwarfUnit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
   assert(MO.isFPImm() && "Invalid machine operand!");
   DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
   APFloat FPImm = MO.getFPImm()->getValueAPF();
@@ -811,18 +825,19 @@ void Unit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
 }
 
 /// addConstantFPValue - Add constant value entry in variable DIE.
-void Unit::addConstantFPValue(DIE *Die, const ConstantFP *CFP) {
+void DwarfUnit::addConstantFPValue(DIE *Die, const ConstantFP *CFP) {
   // Pass this down to addConstantValue as an unsigned bag of bits.
   addConstantValue(Die, CFP->getValueAPF().bitcastToAPInt(), true);
 }
 
 /// addConstantValue - Add constant value entry in variable DIE.
-void Unit::addConstantValue(DIE *Die, const ConstantInt *CI, bool Unsigned) {
+void DwarfUnit::addConstantValue(DIE *Die, const ConstantInt *CI,
+                                 bool Unsigned) {
   addConstantValue(Die, CI->getValue(), Unsigned);
 }
 
 // addConstantValue - Add constant value entry in variable DIE.
-void Unit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
+void DwarfUnit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
   unsigned CIBitWidth = Val.getBitWidth();
   if (CIBitWidth <= 64) {
     // If we're a signed constant definitely use sdata.
@@ -878,7 +893,7 @@ void Unit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
 }
 
 /// addTemplateParams - Add template parameters into buffer.
-void Unit::addTemplateParams(DIE &Buffer, DIArray TParams) {
+void DwarfUnit::addTemplateParams(DIE &Buffer, DIArray TParams) {
   // Add template parameters.
   for (unsigned i = 0, e = TParams.getNumElements(); i != e; ++i) {
     DIDescriptor Element = TParams.getElement(i);
@@ -892,7 +907,7 @@ void Unit::addTemplateParams(DIE &Buffer, DIArray TParams) {
 }
 
 /// getOrCreateContextDIE - Get context owner's DIE.
-DIE *Unit::getOrCreateContextDIE(DIScope Context) {
+DIE *DwarfUnit::getOrCreateContextDIE(DIScope Context) {
   if (!Context || Context.isFile())
     return getUnitDie();
   if (Context.isType())
@@ -904,7 +919,7 @@ DIE *Unit::getOrCreateContextDIE(DIScope Context) {
   return getDIE(Context);
 }
 
-DIE *Unit::createTypeDIE(DICompositeType Ty) {
+DIE *DwarfUnit::createTypeDIE(DICompositeType Ty) {
   DIScope Context = resolve(Ty.getContext());
   DIE *ContextDIE = getOrCreateContextDIE(Context);
 
@@ -923,7 +938,7 @@ DIE *Unit::createTypeDIE(DICompositeType Ty) {
 
 /// Return true if the type is appropriately scoped to be contained inside
 /// its own type unit.
-static bool isTypeUnitScoped(DIType Ty, const DwarfDebug *DD) {
+static bool isDwarfTypeUnitScoped(DIType Ty, const DwarfDebug *DD) {
   DIScope Parent = DD->resolve(Ty.getContext());
   while (Parent) {
     // Don't generate a hash for anything scoped inside a function.
@@ -935,8 +950,9 @@ static bool isTypeUnitScoped(DIType Ty, const DwarfDebug *DD) {
 }
 
 /// Return true if the type should be split out into a type unit.
-static bool shouldCreateTypeUnit(DICompositeType CTy, const DwarfDebug *DD) {
-  if (!GenerateTypeUnits)
+static bool shouldCreateDwarfTypeUnit(DICompositeType CTy,
+                                      const DwarfDebug *DD) {
+  if (!GenerateDwarfTypeUnits)
     return false;
 
   uint16_t Tag = CTy.getTag();
@@ -949,7 +965,7 @@ static bool shouldCreateTypeUnit(DICompositeType CTy, const DwarfDebug *DD) {
     // If this is a class, structure, union, or enumeration type
     // that is a definition (not a declaration), and not scoped
     // inside a function then separate this out as a type unit.
-    return !CTy.isForwardDecl() && isTypeUnitScoped(CTy, DD);
+    return !CTy.isForwardDecl() && isDwarfTypeUnitScoped(CTy, DD);
   default:
     return false;
   }
@@ -957,7 +973,7 @@ static bool shouldCreateTypeUnit(DICompositeType CTy, const DwarfDebug *DD) {
 
 /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
 /// given DIType.
-DIE *Unit::getOrCreateTypeDIE(const MDNode *TyNode) {
+DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
   if (!TyNode)
     return NULL;
 
@@ -981,8 +997,8 @@ DIE *Unit::getOrCreateTypeDIE(const MDNode *TyNode) {
     constructTypeDIE(*TyDIE, DIBasicType(Ty));
   else if (Ty.isCompositeType()) {
     DICompositeType CTy(Ty);
-    if (shouldCreateTypeUnit(CTy, DD)) {
-      DD->addTypeUnitType(getLanguage(), TyDIE, CTy);
+    if (shouldCreateDwarfTypeUnit(CTy, DD)) {
+      DD->addDwarfTypeUnitType(getLanguage(), TyDIE, CTy);
       // Skip updating the accellerator tables since this is not the full type
       return TyDIE;
     }
@@ -997,8 +1013,8 @@ DIE *Unit::getOrCreateTypeDIE(const MDNode *TyNode) {
   return TyDIE;
 }
 
-void Unit::updateAcceleratorTables(DIScope Context, DIType Ty,
-                                   const DIE *TyDIE) {
+void DwarfUnit::updateAcceleratorTables(DIScope Context, DIType Ty,
+                                        const DIE *TyDIE) {
   if (!Ty.getName().empty() && !Ty.isForwardDecl()) {
     bool IsImplementation = 0;
     if (Ty.isCompositeType()) {
@@ -1017,7 +1033,7 @@ void Unit::updateAcceleratorTables(DIScope Context, DIType Ty,
 }
 
 /// addType - Add a new type attribute to the specified entity.
-void Unit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
+void DwarfUnit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
   assert(Ty && "Trying to add a type that doesn't exist?");
 
   // Check for pre-existence.
@@ -1041,32 +1057,33 @@ void Unit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
 // DIE to the proper table while ensuring that the name that we're going
 // to reference is in the string table. We do this since the names we
 // add may not only be identical to the names in the DIE.
-void Unit::addAccelName(StringRef Name, const DIE *Die) {
+void DwarfUnit::addAccelName(StringRef Name, const DIE *Die) {
   DU->getStringPoolEntry(Name);
   std::vector<const DIE *> &DIEs = AccelNames[Name];
   DIEs.push_back(Die);
 }
 
-void Unit::addAccelObjC(StringRef Name, const DIE *Die) {
+void DwarfUnit::addAccelObjC(StringRef Name, const DIE *Die) {
   DU->getStringPoolEntry(Name);
   std::vector<const DIE *> &DIEs = AccelObjC[Name];
   DIEs.push_back(Die);
 }
 
-void Unit::addAccelNamespace(StringRef Name, const DIE *Die) {
+void DwarfUnit::addAccelNamespace(StringRef Name, const DIE *Die) {
   DU->getStringPoolEntry(Name);
   std::vector<const DIE *> &DIEs = AccelNamespace[Name];
   DIEs.push_back(Die);
 }
 
-void Unit::addAccelType(StringRef Name, std::pair<const DIE *, unsigned> Die) {
+void DwarfUnit::addAccelType(StringRef Name,
+                             std::pair<const DIE *, unsigned> Die) {
   DU->getStringPoolEntry(Name);
   std::vector<std::pair<const DIE *, unsigned> > &DIEs = AccelTypes[Name];
   DIEs.push_back(Die);
 }
 
 /// addGlobalName - Add a new global name to the compile unit.
-void Unit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
+void DwarfUnit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
   std::string FullName = getParentContextString(Context) + Name.str();
   GlobalNames[FullName] = Die;
 }
@@ -1076,7 +1093,7 @@ void Unit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
 /// it as a string. This is done at the metadata level because DIEs may
 /// not currently have been added to the parent context and walking the
 /// DIEs looking for names is more expensive than walking the metadata.
-std::string Unit::getParentContextString(DIScope Context) const {
+std::string DwarfUnit::getParentContextString(DIScope Context) const {
   if (!Context)
     return "";
 
@@ -1112,7 +1129,7 @@ std::string Unit::getParentContextString(DIScope Context) const {
 }
 
 /// constructTypeDIE - Construct basic type die from DIBasicType.
-void Unit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
+void DwarfUnit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
   // Get core information.
   StringRef Name = BTy.getName();
   // Add name if not anonymous or intermediate type.
@@ -1131,7 +1148,7 @@ void Unit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
 }
 
 /// constructTypeDIE - Construct derived type die from DIDerivedType.
-void Unit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
+void DwarfUnit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
   // Get core information.
   StringRef Name = DTy.getName();
   uint64_t Size = DTy.getSizeInBits() >> 3;
@@ -1159,7 +1176,7 @@ void Unit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
 }
 
 /// constructTypeDIE - Construct type DIE from DICompositeType.
-void Unit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
+void DwarfUnit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
   // Add name if not anonymous or intermediate type.
   StringRef Name = CTy.getName();
 
@@ -1201,6 +1218,12 @@ void Unit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
         (Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
          Language == dwarf::DW_LANG_ObjC))
       addFlag(&Buffer, dwarf::DW_AT_prototyped);
+
+    if (CTy.isLValueReference())
+      addFlag(&Buffer, dwarf::DW_AT_reference);
+
+    if (CTy.isRValueReference())
+      addFlag(&Buffer, dwarf::DW_AT_rvalue_reference);
   } break;
   case dwarf::DW_TAG_structure_type:
   case dwarf::DW_TAG_union_type:
@@ -1330,8 +1353,8 @@ void Unit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
 
 /// constructTemplateTypeParameterDIE - Construct new DIE for the given
 /// DITemplateTypeParameter.
-void Unit::constructTemplateTypeParameterDIE(DIE &Buffer,
-                                             DITemplateTypeParameter TP) {
+void DwarfUnit::constructTemplateTypeParameterDIE(DIE &Buffer,
+                                                  DITemplateTypeParameter TP) {
   DIE *ParamDIE =
       createAndAddDIE(dwarf::DW_TAG_template_type_parameter, Buffer);
   // Add the type if it exists, it could be void and therefore no type.
@@ -1343,7 +1366,8 @@ void Unit::constructTemplateTypeParameterDIE(DIE &Buffer,
 
 /// constructTemplateValueParameterDIE - Construct new DIE for the given
 /// DITemplateValueParameter.
-void Unit::constructTemplateValueParameterDIE(DIE &Buffer,
+void
+DwarfUnit::constructTemplateValueParameterDIE(DIE &Buffer,
                                               DITemplateValueParameter VP) {
   DIE *ParamDIE = createAndAddDIE(VP.getTag(), Buffer);
 
@@ -1379,7 +1403,7 @@ void Unit::constructTemplateValueParameterDIE(DIE &Buffer,
 }
 
 /// getOrCreateNameSpace - Create a DIE for DINameSpace.
-DIE *Unit::getOrCreateNameSpace(DINameSpace NS) {
+DIE *DwarfUnit::getOrCreateNameSpace(DINameSpace NS) {
   // Construct the context before querying for the existence of the DIE in case
   // such construction creates the DIE.
   DIE *ContextDIE = getOrCreateContextDIE(NS.getContext());
@@ -1400,7 +1424,7 @@ DIE *Unit::getOrCreateNameSpace(DINameSpace NS) {
 }
 
 /// getOrCreateSubprogramDIE - Create new DIE using SP.
-DIE *Unit::getOrCreateSubprogramDIE(DISubprogram SP) {
+DIE *DwarfUnit::getOrCreateSubprogramDIE(DISubprogram SP) {
   // Construct the context before querying for the existence of the DIE in case
   // such construction creates the DIE (as is the case for member function
   // declarations).
@@ -1502,6 +1526,12 @@ DIE *Unit::getOrCreateSubprogramDIE(DISubprogram SP) {
     addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
   }
 
+  if (SP.isLValueReference())
+    addFlag(SPDie, dwarf::DW_AT_reference);
+
+  if (SP.isRValueReference())
+    addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
+
   return SPDie;
 }
 
@@ -1533,7 +1563,7 @@ static const ConstantExpr *getMergedGlobalExpr(const Value *V) {
 }
 
 /// createGlobalVariableDIE - create global variable DIE.
-void CompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
+void DwarfCompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
   // Check for pre-existence.
   if (getDIE(GV))
     return;
@@ -1674,7 +1704,7 @@ void CompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
 }
 
 /// constructSubrangeDIE - Construct subrange DIE from DISubrange.
-void Unit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
+void DwarfUnit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
   DIE *DW_Subrange = createAndAddDIE(dwarf::DW_TAG_subrange_type, Buffer);
   addDIEEntry(DW_Subrange, dwarf::DW_AT_type, IndexTy);
 
@@ -1699,7 +1729,7 @@ void Unit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
 }
 
 /// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
-void Unit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
+void DwarfUnit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
   if (CTy.isVector())
     addFlag(&Buffer, dwarf::DW_AT_GNU_vector);
 
@@ -1730,7 +1760,7 @@ void Unit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
 }
 
 /// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
-void Unit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
+void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
   DIArray Elements = CTy.getTypeArray();
 
   // Add enumerators to enumeration type.
@@ -1754,7 +1784,7 @@ void Unit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
 
 /// constructContainingTypeDIEs - Construct DIEs for types that contain
 /// vtables.
-void Unit::constructContainingTypeDIEs() {
+void DwarfUnit::constructContainingTypeDIEs() {
   for (DenseMap<DIE *, const MDNode *>::iterator CI = ContainingTypeMap.begin(),
                                                  CE = ContainingTypeMap.end();
        CI != CE; ++CI) {
@@ -1770,7 +1800,7 @@ void Unit::constructContainingTypeDIEs() {
 }
 
 /// constructVariableDIE - Construct a DIE for the given DbgVariable.
-DIE *Unit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
+DIE *DwarfUnit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
   StringRef Name = DV.getName();
 
   // Define variable debug information entry.
@@ -1843,7 +1873,7 @@ DIE *Unit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
 }
 
 /// constructMemberDIE - Construct member DIE from DIDerivedType.
-void Unit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
+void DwarfUnit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
   DIE *MemberDie = createAndAddDIE(DT.getTag(), Buffer);
   StringRef Name = DT.getName();
   if (!Name.empty())
@@ -1928,7 +1958,7 @@ void Unit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
 }
 
 /// getOrCreateStaticMemberDIE - Create new DIE for C++ static member.
-DIE *Unit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
+DIE *DwarfUnit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
   if (!DT.Verify())
     return NULL;
 
@@ -1972,7 +2002,8 @@ DIE *Unit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
   return StaticMemberDIE;
 }
 
-void Unit::emitHeader(const MCSection *ASection, const MCSymbol *ASectionSym) {
+void DwarfUnit::emitHeader(const MCSection *ASection,
+                           const MCSymbol *ASectionSym) const {
   Asm->OutStreamer.AddComment("DWARF version number");
   Asm->EmitInt16(DD->getDwarfVersion());
   Asm->OutStreamer.AddComment("Offset Into Abbrev. Section");
@@ -1983,3 +2014,30 @@ void Unit::emitHeader(const MCSection *ASection, const MCSymbol *ASectionSym) {
   Asm->OutStreamer.AddComment("Address Size (in bytes)");
   Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
 }
+
+DwarfCompileUnit::~DwarfCompileUnit() {}
+DwarfTypeUnit::~DwarfTypeUnit() {}
+
+void DwarfTypeUnit::emitHeader(const MCSection *ASection,
+                               const MCSymbol *ASectionSym) const {
+  DwarfUnit::emitHeader(ASection, ASectionSym);
+  Asm->OutStreamer.AddComment("Type Signature");
+  Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
+  Asm->OutStreamer.AddComment("Type DIE Offset");
+  Asm->OutStreamer.EmitIntValue(Ty->getOffset(), sizeof(Ty->getOffset()));
+}
+
+void DwarfTypeUnit::initSection(const MCSection *Section) {
+  assert(!this->Section);
+  this->Section = Section;
+  // Since each type unit is contained in its own COMDAT section, the begin
+  // label and the section label are the same. Using the begin label emission in
+  // DwarfDebug to emit the section label as well is slightly subtle/sneaky, but
+  // the only other alternative of lazily constructing start-of-section labels
+  // and storing a mapping in DwarfDebug (or AsmPrinter).
+  this->SectionSym = this->LabelBegin =
+      Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
+  this->LabelEnd =
+      Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
+  this->LabelRange = Asm->GetTempSymbol("gnu_ranges", getUniqueID());
+}