index 709f5bec031b6c32bedd7ea8a4f20c8bdaf8a168..a1db1e0a2ed0ffe78940cdf1666c95c8efa9cbbf 100644 (file)
#include "llvm/IR/DataLayout.h"
#include "llvm/IR/GlobalVariable.h"
#include "llvm/IR/Instructions.h"
+#include "llvm/IR/Mangler.h"
+#include "llvm/MC/MCAsmInfo.h"
#include "llvm/MC/MCSection.h"
#include "llvm/MC/MCStreamer.h"
-#include "llvm/Target/Mangler.h"
+#include "llvm/Support/CommandLine.h"
#include "llvm/Target/TargetFrameLowering.h"
-#include "llvm/Target/TargetMachine.h"
#include "llvm/Target/TargetLoweringObjectFile.h"
+#include "llvm/Target/TargetMachine.h"
#include "llvm/Target/TargetRegisterInfo.h"
-#include "llvm/Support/CommandLine.h"
using namespace llvm;
/// Unit - Unit constructor.
DwarfUnit::DwarfUnit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
DwarfDebug *DW, DwarfFile *DWU)
- : UniqueID(UID), Node(Node), UnitDie(D), DebugInfoOffset(0), Asm(A), DD(DW),
- DU(DWU), IndexTyDie(0), Section(0) {
+ : UniqueID(UID), CUNode(Node), UnitDie(D), DebugInfoOffset(0), Asm(A),
+ DD(DW), DU(DWU), IndexTyDie(0), Section(0), Skeleton(0) {
DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
}
insertDIE(Node, D);
}
-DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DIE *D, uint16_t Language,
+DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DIE *D, DICompileUnit CUNode,
AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
- : DwarfUnit(UID, D, DICompileUnit(), A, DW, DWU), Language(Language) {}
+ : DwarfUnit(UID, D, CUNode, A, DW, DWU) {}
/// ~Unit - Destructor for compile unit.
DwarfUnit::~DwarfUnit() {
/// table.
void DwarfUnit::addString(DIE *Die, dwarf::Attribute Attribute,
StringRef String) {
- DIEValue *Value;
- dwarf::Form Form;
- if (!DD->useSplitDwarf()) {
- MCSymbol *Symb = DU->getStringPoolEntry(String);
- if (Asm->needsRelocationsForDwarfStringPool())
- Value = new (DIEValueAllocator) DIELabel(Symb);
- else {
- MCSymbol *StringPool = DU->getStringPoolSym();
- Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
- }
- Form = dwarf::DW_FORM_strp;
- } else {
- unsigned idx = DU->getStringPoolIndex(String);
- Value = new (DIEValueAllocator) DIEInteger(idx);
- Form = dwarf::DW_FORM_GNU_str_index;
- }
+
+ if (!DD->useSplitDwarf())
+ return addLocalString(Die, Attribute, String);
+
+ unsigned idx = DU->getStringPoolIndex(String);
+ DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
- Die->addValue(Attribute, Form, Str);
+ Die->addValue(Attribute, dwarf::DW_FORM_GNU_str_index, Str);
}
/// addLocalString - Add a string attribute data and value. This is guaranteed
StringRef String) {
MCSymbol *Symb = DU->getStringPoolEntry(String);
DIEValue *Value;
- if (Asm->needsRelocationsForDwarfStringPool())
+ if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
Value = new (DIEValueAllocator) DIELabel(Symb);
else {
MCSymbol *StringPool = DU->getStringPoolSym();
Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
}
- Die->addValue(Attribute, dwarf::DW_FORM_strp, Value);
+ DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
+ Die->addValue(Attribute, dwarf::DW_FORM_strp, Str);
}
/// addExpr - Add a Dwarf expression attribute data and value.
DD->addArangeLabel(SymbolCU(this, Label));
if (!DD->useSplitDwarf()) {
- if (Label != NULL) {
+ if (Label) {
DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
} else {
@@ -322,6 +314,11 @@ void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
addDIEEntry(Die, Attribute, createDIEEntry(Entry));
}
+void DwarfUnit::addDIETypeSignature(DIE *Die, const DwarfTypeUnit &Type) {
+ Die->addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
+ new (DIEValueAllocator) DIETypeSignature(Type));
+}
+
void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute,
DIEEntry *Entry) {
const DIE *DieCU = Die->getUnitOrNull();
return TyDIE;
}
-/// Return true if the type is appropriately scoped to be contained inside
-/// its own type unit.
-static bool isDwarfTypeUnitScoped(DIType Ty, const DwarfDebug *DD) {
- DIScope Parent = DD->resolve(Ty.getContext());
- while (Parent) {
- // Don't generate a hash for anything scoped inside a function.
- if (Parent.isSubprogram())
- return false;
- Parent = DD->resolve(Parent.getContext());
- }
- return true;
-}
-
-/// Return true if the type should be split out into a type unit.
-static bool shouldCreateDwarfTypeUnit(DICompositeType CTy,
- const DwarfDebug *DD) {
- if (!GenerateDwarfTypeUnits)
- return false;
-
- uint16_t Tag = CTy.getTag();
-
- switch (Tag) {
- case dwarf::DW_TAG_structure_type:
- case dwarf::DW_TAG_union_type:
- case dwarf::DW_TAG_enumeration_type:
- case dwarf::DW_TAG_class_type:
- // If this is a class, structure, union, or enumeration type
- // that is a definition (not a declaration), and not scoped
- // inside a function then separate this out as a type unit.
- return !CTy.isForwardDecl() && isDwarfTypeUnitScoped(CTy, DD);
- default:
- return false;
- }
-}
-
/// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
/// given DIType.
DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
constructTypeDIE(*TyDIE, DIBasicType(Ty));
else if (Ty.isCompositeType()) {
DICompositeType CTy(Ty);
- if (shouldCreateDwarfTypeUnit(CTy, DD)) {
- DD->addDwarfTypeUnitType(getLanguage(), TyDIE, CTy);
- // Skip updating the accellerator tables since this is not the full type
- return TyDIE;
- }
+ if (GenerateDwarfTypeUnits && !Ty.isForwardDecl())
+ if (MDString *TypeId = CTy.getIdentifier()) {
+ DD->addDwarfTypeUnitType(getCUNode(), TypeId->getString(), TyDIE, CTy);
+ // Skip updating the accellerator tables since this is not the full type
+ return TyDIE;
+ }
constructTypeDIE(*TyDIE, CTy);
} else {
assert(Ty.isDerivedType() && "Unknown kind of DIType");
@@ -1053,18 +1016,21 @@ void DwarfUnit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
// to reference is in the string table. We do this since the names we
// add may not only be identical to the names in the DIE.
void DwarfUnit::addAccelName(StringRef Name, const DIE *Die) {
+ if (!DD->useDwarfAccelTables()) return;
DU->getStringPoolEntry(Name);
std::vector<const DIE *> &DIEs = AccelNames[Name];
DIEs.push_back(Die);
}
void DwarfUnit::addAccelObjC(StringRef Name, const DIE *Die) {
+ if (!DD->useDwarfAccelTables()) return;
DU->getStringPoolEntry(Name);
std::vector<const DIE *> &DIEs = AccelObjC[Name];
DIEs.push_back(Die);
}
void DwarfUnit::addAccelNamespace(StringRef Name, const DIE *Die) {
+ if (!DD->useDwarfAccelTables()) return;
DU->getStringPoolEntry(Name);
std::vector<const DIE *> &DIEs = AccelNamespace[Name];
DIEs.push_back(Die);
void DwarfUnit::addAccelType(StringRef Name,
std::pair<const DIE *, unsigned> Die) {
+ if (!DD->useDwarfAccelTables()) return;
DU->getStringPoolEntry(Name);
std::vector<std::pair<const DIE *, unsigned> > &DIEs = AccelTypes[Name];
DIEs.push_back(Die);
(Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
Language == dwarf::DW_LANG_ObjC))
addFlag(&Buffer, dwarf::DW_AT_prototyped);
+
+ if (CTy.isLValueReference())
+ addFlag(&Buffer, dwarf::DW_AT_reference);
+
+ if (CTy.isRValueReference())
+ addFlag(&Buffer, dwarf::DW_AT_rvalue_reference);
} break;
case dwarf::DW_TAG_structure_type:
case dwarf::DW_TAG_union_type:
for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
DIDescriptor Element = Elements.getElement(i);
DIE *ElemDie = NULL;
- if (Element.isSubprogram()) {
- DISubprogram SP(Element);
- ElemDie = getOrCreateSubprogramDIE(SP);
- if (SP.isProtected())
- addUInt(ElemDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
- dwarf::DW_ACCESS_protected);
- else if (SP.isPrivate())
- addUInt(ElemDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
- dwarf::DW_ACCESS_private);
- else
- addUInt(ElemDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
- dwarf::DW_ACCESS_public);
- if (SP.isExplicit())
- addFlag(ElemDie, dwarf::DW_AT_explicit);
- } else if (Element.isDerivedType()) {
+ if (Element.isSubprogram())
+ ElemDie = getOrCreateSubprogramDIE(DISubprogram(Element));
+ else if (Element.isDerivedType()) {
DIDerivedType DDTy(Element);
if (DDTy.getTag() == dwarf::DW_TAG_friend) {
ElemDie = createAndAddDIE(dwarf::DW_TAG_friend, Buffer);
ElemDie = createAndAddDIE(Property.getTag(), Buffer);
StringRef PropertyName = Property.getObjCPropertyName();
addString(ElemDie, dwarf::DW_AT_APPLE_property_name, PropertyName);
- addType(ElemDie, Property.getType());
+ if (Property.getType())
+ addType(ElemDie, Property.getType());
addSourceLine(ElemDie, Property);
StringRef GetterName = Property.getObjCPropertyGetterName();
if (!GetterName.empty())
addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
}
+ if (SP.isLValueReference())
+ addFlag(SPDie, dwarf::DW_AT_reference);
+
+ if (SP.isRValueReference())
+ addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
+
+ if (SP.isProtected())
+ addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
+ dwarf::DW_ACCESS_protected);
+ else if (SP.isPrivate())
+ addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
+ dwarf::DW_ACCESS_private);
+ else
+ addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
+ dwarf::DW_ACCESS_public);
+
+ if (SP.isExplicit())
+ addFlag(SPDie, dwarf::DW_AT_explicit);
+
return SPDie;
}
if (getDIE(GV))
return;
- if (!GV.isGlobalVariable())
- return;
+ assert(GV.isGlobalVariable());
DIScope GVContext = GV.getContext();
DIType GTy = GV.getType();
addSourceLine(MemberDie, DT);
- DIEBlock *MemLocationDie = new (DIEValueAllocator) DIEBlock();
- addUInt(MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
-
if (DT.getTag() == dwarf::DW_TAG_inheritance && DT.isVirtual()) {
// For C++, virtual base classes are not at fixed offset. Use following
Offset = FieldSize - (Offset + Size);
addUInt(MemberDie, dwarf::DW_AT_bit_offset, None, Offset);
- // Here WD_AT_data_member_location points to the anonymous
+ // Here DW_AT_data_member_location points to the anonymous
// field that includes this bit field.
OffsetInBytes = FieldOffset >> 3;
} else
// This is not a bitfield.
OffsetInBytes = DT.getOffsetInBits() >> 3;
- addUInt(MemberDie, dwarf::DW_AT_data_member_location, None, OffsetInBytes);
+
+ if (DD->getDwarfVersion() <= 2) {
+ DIEBlock *MemLocationDie = new (DIEValueAllocator) DIEBlock();
+ addUInt(MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
+ addUInt(MemLocationDie, dwarf::DW_FORM_udata, OffsetInBytes);
+ addBlock(MemberDie, dwarf::DW_AT_data_member_location, MemLocationDie);
+ } else
+ addUInt(MemberDie, dwarf::DW_AT_data_member_location, None,
+ OffsetInBytes);
}
if (DT.isProtected())
Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
}
+DwarfCompileUnit::~DwarfCompileUnit() {}
+DwarfTypeUnit::~DwarfTypeUnit() {}
+
void DwarfTypeUnit::emitHeader(const MCSection *ASection,
const MCSymbol *ASectionSym) const {
DwarfUnit::emitHeader(ASection, ASectionSym);
Asm->OutStreamer.AddComment("Type Signature");
Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
Asm->OutStreamer.AddComment("Type DIE Offset");
- Asm->OutStreamer.EmitIntValue(Ty->getOffset(), sizeof(Ty->getOffset()));
+ // In a skeleton type unit there is no type DIE so emit a zero offset.
+ Asm->OutStreamer.EmitIntValue(Ty ? Ty->getOffset() : 0,
+ sizeof(Ty->getOffset()));
}
void DwarfTypeUnit::initSection(const MCSection *Section) {