index 40b7476f4bd248fd15f67a1abad3e61c1e2dce8b..dbdcf9d2e118767281afadac1d509b9afa84c044 100644 (file)
#include "DwarfAccelTable.h"
#include "DwarfDebug.h"
#include "llvm/ADT/APFloat.h"
-#include "llvm/DIBuilder.h"
#include "llvm/IR/Constants.h"
+#include "llvm/IR/DIBuilder.h"
#include "llvm/IR/DataLayout.h"
#include "llvm/IR/GlobalVariable.h"
#include "llvm/IR/Instructions.h"
+#include "llvm/IR/Mangler.h"
+#include "llvm/MC/MCAsmInfo.h"
+#include "llvm/MC/MCContext.h"
#include "llvm/MC/MCSection.h"
#include "llvm/MC/MCStreamer.h"
-#include "llvm/Target/Mangler.h"
+#include "llvm/Support/CommandLine.h"
#include "llvm/Target/TargetFrameLowering.h"
-#include "llvm/Target/TargetMachine.h"
#include "llvm/Target/TargetLoweringObjectFile.h"
+#include "llvm/Target/TargetMachine.h"
#include "llvm/Target/TargetRegisterInfo.h"
-#include "llvm/Support/CommandLine.h"
using namespace llvm;
-static cl::opt<bool> GenerateTypeUnits("generate-type-units", cl::Hidden,
- cl::desc("Generate DWARF4 type units."),
- cl::init(false));
+static cl::opt<bool>
+GenerateDwarfTypeUnits("generate-type-units", cl::Hidden,
+ cl::desc("Generate DWARF4 type units."),
+ cl::init(false));
/// Unit - Unit constructor.
-Unit::Unit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
- DwarfDebug *DW, DwarfFile *DWU)
- : UniqueID(UID), Node(Node), UnitDie(D), DebugInfoOffset(0), Asm(A), DD(DW),
- DU(DWU), IndexTyDie(0), Section(0) {
+DwarfUnit::DwarfUnit(unsigned UID, DIE *D, DICompileUnit Node, AsmPrinter *A,
+ DwarfDebug *DW, DwarfFile *DWU)
+ : UniqueID(UID), CUNode(Node), UnitDie(D), DebugInfoOffset(0), Asm(A),
+ DD(DW), DU(DWU), IndexTyDie(0), Section(0), Skeleton(0) {
DIEIntegerOne = new (DIEValueAllocator) DIEInteger(1);
}
-CompileUnit::CompileUnit(unsigned UID, DIE *D, DICompileUnit Node,
- AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
- : Unit(UID, D, Node, A, DW, DWU) {
+DwarfCompileUnit::DwarfCompileUnit(unsigned UID, DIE *D, DICompileUnit Node,
+ AsmPrinter *A, DwarfDebug *DW,
+ DwarfFile *DWU)
+ : DwarfUnit(UID, D, Node, A, DW, DWU) {
insertDIE(Node, D);
}
-TypeUnit::TypeUnit(unsigned UID, DIE *D, uint16_t Language, AsmPrinter *A,
- DwarfDebug *DW, DwarfFile *DWU)
- : Unit(UID, D, DICompileUnit(), A, DW, DWU), Language(Language) {}
+DwarfTypeUnit::DwarfTypeUnit(unsigned UID, DIE *D, DwarfCompileUnit &CU,
+ AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU)
+ : DwarfUnit(UID, D, CU.getCUNode(), A, DW, DWU), CU(CU) {}
/// ~Unit - Destructor for compile unit.
-Unit::~Unit() {
+DwarfUnit::~DwarfUnit() {
for (unsigned j = 0, M = DIEBlocks.size(); j < M; ++j)
DIEBlocks[j]->~DIEBlock();
+ for (unsigned j = 0, M = DIELocs.size(); j < M; ++j)
+ DIELocs[j]->~DIELoc();
}
/// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug
/// information entry.
-DIEEntry *Unit::createDIEEntry(DIE *Entry) {
+DIEEntry *DwarfUnit::createDIEEntry(DIE *Entry) {
DIEEntry *Value = new (DIEValueAllocator) DIEEntry(Entry);
return Value;
}
/// getDefaultLowerBound - Return the default lower bound for an array. If the
/// DWARF version doesn't handle the language, return -1.
-int64_t Unit::getDefaultLowerBound() const {
+int64_t DwarfUnit::getDefaultLowerBound() const {
switch (getLanguage()) {
default:
break;
// together.
return (D.isType() ||
(D.isSubprogram() && !DISubprogram(D).isDefinition())) &&
- !GenerateTypeUnits;
+ !GenerateDwarfTypeUnits;
}
/// getDIE - Returns the debug information entry map slot for the
/// specified debug variable. We delegate the request to DwarfDebug
/// when the DIE for this MDNode can be shared across CUs. The mappings
/// will be kept in DwarfDebug for shareable DIEs.
-DIE *Unit::getDIE(DIDescriptor D) const {
+DIE *DwarfUnit::getDIE(DIDescriptor D) const {
if (isShareableAcrossCUs(D))
return DD->getDIE(D);
return MDNodeToDieMap.lookup(D);
/// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug
/// when the DIE for this MDNode can be shared across CUs. The mappings
/// will be kept in DwarfDebug for shareable DIEs.
-void Unit::insertDIE(DIDescriptor Desc, DIE *D) {
+void DwarfUnit::insertDIE(DIDescriptor Desc, DIE *D) {
if (isShareableAcrossCUs(Desc)) {
DD->insertDIE(Desc, D);
return;
}
/// addFlag - Add a flag that is true.
-void Unit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
+void DwarfUnit::addFlag(DIE *Die, dwarf::Attribute Attribute) {
if (DD->getDwarfVersion() >= 4)
Die->addValue(Attribute, dwarf::DW_FORM_flag_present, DIEIntegerOne);
else
/// addUInt - Add an unsigned integer attribute data and value.
///
-void Unit::addUInt(DIE *Die, dwarf::Attribute Attribute,
- Optional<dwarf::Form> Form, uint64_t Integer) {
+void DwarfUnit::addUInt(DIE *Die, dwarf::Attribute Attribute,
+ Optional<dwarf::Form> Form, uint64_t Integer) {
if (!Form)
Form = DIEInteger::BestForm(false, Integer);
DIEValue *Value = Integer == 1 ? DIEIntegerOne : new (DIEValueAllocator)
Die->addValue(Attribute, *Form, Value);
}
-void Unit::addUInt(DIEBlock *Block, dwarf::Form Form, uint64_t Integer) {
+void DwarfUnit::addUInt(DIE *Block, dwarf::Form Form, uint64_t Integer) {
addUInt(Block, (dwarf::Attribute)0, Form, Integer);
}
/// addSInt - Add an signed integer attribute data and value.
///
-void Unit::addSInt(DIE *Die, dwarf::Attribute Attribute,
- Optional<dwarf::Form> Form, int64_t Integer) {
+void DwarfUnit::addSInt(DIE *Die, dwarf::Attribute Attribute,
+ Optional<dwarf::Form> Form, int64_t Integer) {
if (!Form)
Form = DIEInteger::BestForm(true, Integer);
DIEValue *Value = new (DIEValueAllocator) DIEInteger(Integer);
Die->addValue(Attribute, *Form, Value);
}
-void Unit::addSInt(DIEBlock *Die, Optional<dwarf::Form> Form, int64_t Integer) {
+void DwarfUnit::addSInt(DIELoc *Die, Optional<dwarf::Form> Form,
+ int64_t Integer) {
addSInt(Die, (dwarf::Attribute)0, Form, Integer);
}
@@ -189,65 +196,67 @@ void Unit::addSInt(DIEBlock *Die, Optional<dwarf::Form> Form, int64_t Integer) {
/// more predictable sizes. In the case of split dwarf we emit an index
/// into another table which gets us the static offset into the string
/// table.
-void Unit::addString(DIE *Die, dwarf::Attribute Attribute, StringRef String) {
- DIEValue *Value;
- dwarf::Form Form;
- if (!DD->useSplitDwarf()) {
- MCSymbol *Symb = DU->getStringPoolEntry(String);
- if (Asm->needsRelocationsForDwarfStringPool())
- Value = new (DIEValueAllocator) DIELabel(Symb);
- else {
- MCSymbol *StringPool = DU->getStringPoolSym();
- Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
- }
- Form = dwarf::DW_FORM_strp;
- } else {
- unsigned idx = DU->getStringPoolIndex(String);
- Value = new (DIEValueAllocator) DIEInteger(idx);
- Form = dwarf::DW_FORM_GNU_str_index;
- }
+void DwarfUnit::addString(DIE *Die, dwarf::Attribute Attribute,
+ StringRef String) {
+
+ if (!DD->useSplitDwarf())
+ return addLocalString(Die, Attribute, String);
+
+ unsigned idx = DU->getStringPoolIndex(String);
+ DIEValue *Value = new (DIEValueAllocator) DIEInteger(idx);
DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
- Die->addValue(Attribute, Form, Str);
+ Die->addValue(Attribute, dwarf::DW_FORM_GNU_str_index, Str);
}
/// addLocalString - Add a string attribute data and value. This is guaranteed
/// to be in the local string pool instead of indirected.
-void Unit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
- StringRef String) {
+void DwarfUnit::addLocalString(DIE *Die, dwarf::Attribute Attribute,
+ StringRef String) {
MCSymbol *Symb = DU->getStringPoolEntry(String);
DIEValue *Value;
- if (Asm->needsRelocationsForDwarfStringPool())
+ if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
Value = new (DIEValueAllocator) DIELabel(Symb);
else {
MCSymbol *StringPool = DU->getStringPoolSym();
Value = new (DIEValueAllocator) DIEDelta(Symb, StringPool);
}
- Die->addValue(Attribute, dwarf::DW_FORM_strp, Value);
+ DIEValue *Str = new (DIEValueAllocator) DIEString(Value, String);
+ Die->addValue(Attribute, dwarf::DW_FORM_strp, Str);
}
/// addExpr - Add a Dwarf expression attribute data and value.
///
-void Unit::addExpr(DIEBlock *Die, dwarf::Form Form, const MCExpr *Expr) {
+void DwarfUnit::addExpr(DIELoc *Die, dwarf::Form Form, const MCExpr *Expr) {
DIEValue *Value = new (DIEValueAllocator) DIEExpr(Expr);
Die->addValue((dwarf::Attribute)0, Form, Value);
}
+/// addLocationList - Add a Dwarf loclistptr attribute data and value.
+///
+void DwarfUnit::addLocationList(DIE *Die, dwarf::Attribute Attribute,
+ unsigned Index) {
+ DIEValue *Value = new (DIEValueAllocator) DIELocList(Index);
+ dwarf::Form Form = DD->getDwarfVersion() >= 4 ? dwarf::DW_FORM_sec_offset
+ : dwarf::DW_FORM_data4;
+ Die->addValue(Attribute, Form, Value);
+}
+
/// addLabel - Add a Dwarf label attribute data and value.
///
-void Unit::addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
- const MCSymbol *Label) {
+void DwarfUnit::addLabel(DIE *Die, dwarf::Attribute Attribute, dwarf::Form Form,
+ const MCSymbol *Label) {
DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
Die->addValue(Attribute, Form, Value);
}
-void Unit::addLabel(DIEBlock *Die, dwarf::Form Form, const MCSymbol *Label) {
+void DwarfUnit::addLabel(DIELoc *Die, dwarf::Form Form, const MCSymbol *Label) {
addLabel(Die, (dwarf::Attribute)0, Form, Label);
}
/// addSectionLabel - Add a Dwarf section label attribute data and value.
///
-void Unit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
- const MCSymbol *Label) {
+void DwarfUnit::addSectionLabel(DIE *Die, dwarf::Attribute Attribute,
+ const MCSymbol *Label) {
if (DD->getDwarfVersion() >= 4)
addLabel(Die, Attribute, dwarf::DW_FORM_sec_offset, Label);
else
/// addSectionOffset - Add an offset into a section attribute data and value.
///
-void Unit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
- uint64_t Integer) {
+void DwarfUnit::addSectionOffset(DIE *Die, dwarf::Attribute Attribute,
+ uint64_t Integer) {
if (DD->getDwarfVersion() >= 4)
addUInt(Die, Attribute, dwarf::DW_FORM_sec_offset, Integer);
else
/// addLabelAddress - Add a dwarf label attribute data and value using
/// DW_FORM_addr or DW_FORM_GNU_addr_index.
///
-void CompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
- MCSymbol *Label) {
+void DwarfCompileUnit::addLabelAddress(DIE *Die, dwarf::Attribute Attribute,
+ MCSymbol *Label) {
if (Label)
DD->addArangeLabel(SymbolCU(this, Label));
if (!DD->useSplitDwarf()) {
- if (Label != NULL) {
+ if (Label) {
DIEValue *Value = new (DIEValueAllocator) DIELabel(Label);
Die->addValue(Attribute, dwarf::DW_FORM_addr, Value);
} else {
/// addOpAddress - Add a dwarf op address data and value using the
/// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index.
///
-void Unit::addOpAddress(DIEBlock *Die, const MCSymbol *Sym) {
+void DwarfUnit::addOpAddress(DIELoc *Die, const MCSymbol *Sym) {
if (!DD->useSplitDwarf()) {
addUInt(Die, dwarf::DW_FORM_data1, dwarf::DW_OP_addr);
addLabel(Die, dwarf::DW_FORM_udata, Sym);
/// addSectionDelta - Add a section label delta attribute data and value.
///
-void Unit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
- const MCSymbol *Hi, const MCSymbol *Lo) {
+void DwarfUnit::addSectionDelta(DIE *Die, dwarf::Attribute Attribute,
+ const MCSymbol *Hi, const MCSymbol *Lo) {
DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
if (DD->getDwarfVersion() >= 4)
Die->addValue(Attribute, dwarf::DW_FORM_sec_offset, Value);
Die->addValue(Attribute, dwarf::DW_FORM_data4, Value);
}
+void DwarfUnit::addLabelDelta(DIE *Die, dwarf::Attribute Attribute,
+ const MCSymbol *Hi, const MCSymbol *Lo) {
+ DIEValue *Value = new (DIEValueAllocator) DIEDelta(Hi, Lo);
+ Die->addValue(Attribute, dwarf::DW_FORM_data4, Value);
+}
+
/// addDIEEntry - Add a DIE attribute data and value.
///
-void Unit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
+void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIE *Entry) {
addDIEEntry(Die, Attribute, createDIEEntry(Entry));
}
-void Unit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute, DIEEntry *Entry) {
+void DwarfUnit::addDIETypeSignature(DIE *Die, const DwarfTypeUnit &Type) {
+ Die->addValue(dwarf::DW_AT_signature, dwarf::DW_FORM_ref_sig8,
+ new (DIEValueAllocator) DIETypeSignature(Type));
+}
+
+void DwarfUnit::addDIEEntry(DIE *Die, dwarf::Attribute Attribute,
+ DIEEntry *Entry) {
const DIE *DieCU = Die->getUnitOrNull();
const DIE *EntryCU = Entry->getEntry()->getUnitOrNull();
if (!DieCU)
/// Create a DIE with the given Tag, add the DIE to its parent, and
/// call insertDIE if MD is not null.
-DIE *Unit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
+DIE *DwarfUnit::createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N) {
DIE *Die = new DIE(Tag);
Parent.addChild(Die);
if (N)
/// addBlock - Add block data.
///
-void Unit::addBlock(DIE *Die, dwarf::Attribute Attribute, DIEBlock *Block) {
+void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute, DIELoc *Loc) {
+ Loc->ComputeSize(Asm);
+ DIELocs.push_back(Loc); // Memoize so we can call the destructor later on.
+ Die->addValue(Attribute, Loc->BestForm(DD->getDwarfVersion()), Loc);
+}
+
+void DwarfUnit::addBlock(DIE *Die, dwarf::Attribute Attribute,
+ DIEBlock *Block) {
Block->ComputeSize(Asm);
DIEBlocks.push_back(Block); // Memoize so we can call the destructor later on.
Die->addValue(Attribute, Block->BestForm(), Block);
/// addSourceLine - Add location information to specified debug information
/// entry.
-void Unit::addSourceLine(DIE *Die, DIVariable V) {
- // Verify variable.
- if (!V.isVariable())
- return;
-
- unsigned Line = V.getLineNumber();
+void DwarfUnit::addSourceLine(DIE *Die, unsigned Line, StringRef File,
+ StringRef Directory) {
if (Line == 0)
return;
+
unsigned FileID =
- DD->getOrCreateSourceID(V.getContext().getFilename(),
- V.getContext().getDirectory(), getUniqueID());
+ DD->getOrCreateSourceID(File, Directory, getCU().getUniqueID());
assert(FileID && "Invalid file id");
addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
/// addSourceLine - Add location information to specified debug information
/// entry.
-void Unit::addSourceLine(DIE *Die, DIGlobalVariable G) {
- // Verify global variable.
- if (!G.isGlobalVariable())
- return;
+void DwarfUnit::addSourceLine(DIE *Die, DIVariable V) {
+ assert(V.isVariable());
- unsigned Line = G.getLineNumber();
- if (Line == 0)
- return;
- unsigned FileID =
- DD->getOrCreateSourceID(G.getFilename(), G.getDirectory(), getUniqueID());
- assert(FileID && "Invalid file id");
- addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
- addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
+ addSourceLine(Die, V.getLineNumber(), V.getContext().getFilename(),
+ V.getContext().getDirectory());
}
/// addSourceLine - Add location information to specified debug information
/// entry.
-void Unit::addSourceLine(DIE *Die, DISubprogram SP) {
- // Verify subprogram.
- if (!SP.isSubprogram())
- return;
+void DwarfUnit::addSourceLine(DIE *Die, DIGlobalVariable G) {
+ assert(G.isGlobalVariable());
- // If the line number is 0, don't add it.
- unsigned Line = SP.getLineNumber();
- if (Line == 0)
- return;
+ addSourceLine(Die, G.getLineNumber(), G.getFilename(), G.getDirectory());
+}
- unsigned FileID = DD->getOrCreateSourceID(SP.getFilename(), SP.getDirectory(),
- getUniqueID());
- assert(FileID && "Invalid file id");
- addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
- addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
+/// addSourceLine - Add location information to specified debug information
+/// entry.
+void DwarfUnit::addSourceLine(DIE *Die, DISubprogram SP) {
+ assert(SP.isSubprogram());
+
+ addSourceLine(Die, SP.getLineNumber(), SP.getFilename(), SP.getDirectory());
}
/// addSourceLine - Add location information to specified debug information
/// entry.
-void Unit::addSourceLine(DIE *Die, DIType Ty) {
- // Verify type.
- if (!Ty.isType())
- return;
+void DwarfUnit::addSourceLine(DIE *Die, DIType Ty) {
+ assert(Ty.isType());
- unsigned Line = Ty.getLineNumber();
- if (Line == 0)
- return;
- unsigned FileID = DD->getOrCreateSourceID(Ty.getFilename(), Ty.getDirectory(),
- getUniqueID());
- assert(FileID && "Invalid file id");
- addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
- addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
+ addSourceLine(Die, Ty.getLineNumber(), Ty.getFilename(), Ty.getDirectory());
}
/// addSourceLine - Add location information to specified debug information
/// entry.
-void Unit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
- // Verify type.
- if (!Ty.isObjCProperty())
- return;
+void DwarfUnit::addSourceLine(DIE *Die, DIObjCProperty Ty) {
+ assert(Ty.isObjCProperty());
- unsigned Line = Ty.getLineNumber();
- if (Line == 0)
- return;
DIFile File = Ty.getFile();
- unsigned FileID = DD->getOrCreateSourceID(File.getFilename(),
- File.getDirectory(), getUniqueID());
- assert(FileID && "Invalid file id");
- addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
- addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
+ addSourceLine(Die, Ty.getLineNumber(), File.getFilename(),
+ File.getDirectory());
}
/// addSourceLine - Add location information to specified debug information
/// entry.
-void Unit::addSourceLine(DIE *Die, DINameSpace NS) {
- // Verify namespace.
- if (!NS.Verify())
- return;
+void DwarfUnit::addSourceLine(DIE *Die, DINameSpace NS) {
+ assert(NS.Verify());
- unsigned Line = NS.getLineNumber();
- if (Line == 0)
- return;
- StringRef FN = NS.getFilename();
-
- unsigned FileID =
- DD->getOrCreateSourceID(FN, NS.getDirectory(), getUniqueID());
- assert(FileID && "Invalid file id");
- addUInt(Die, dwarf::DW_AT_decl_file, None, FileID);
- addUInt(Die, dwarf::DW_AT_decl_line, None, Line);
+ addSourceLine(Die, NS.getLineNumber(), NS.getFilename(), NS.getDirectory());
}
/// addVariableAddress - Add DW_AT_location attribute for a
/// DbgVariable based on provided MachineLocation.
-void Unit::addVariableAddress(const DbgVariable &DV, DIE *Die,
- MachineLocation Location) {
+void DwarfUnit::addVariableAddress(const DbgVariable &DV, DIE *Die,
+ MachineLocation Location) {
if (DV.variableHasComplexAddress())
addComplexAddress(DV, Die, dwarf::DW_AT_location, Location);
else if (DV.isBlockByrefVariable())
}
/// addRegisterOp - Add register operand.
-void Unit::addRegisterOp(DIEBlock *TheDie, unsigned Reg) {
+void DwarfUnit::addRegisterOp(DIELoc *TheDie, unsigned Reg) {
const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
- unsigned DWReg = RI->getDwarfRegNum(Reg, false);
+ int DWReg = RI->getDwarfRegNum(Reg, false);
+ bool isSubRegister = DWReg < 0;
+
+ unsigned Idx = 0;
+
+ // Go up the super-register chain until we hit a valid dwarf register number.
+ for (MCSuperRegIterator SR(Reg, RI); SR.isValid() && DWReg < 0; ++SR) {
+ DWReg = RI->getDwarfRegNum(*SR, false);
+ if (DWReg >= 0)
+ Idx = RI->getSubRegIndex(*SR, Reg);
+ }
+
+ if (DWReg < 0) {
+ DEBUG(dbgs() << "Invalid Dwarf register number.\n");
+ addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_nop);
+ return;
+ }
+
+ // Emit register
if (DWReg < 32)
addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_reg0 + DWReg);
else {
addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_regx);
addUInt(TheDie, dwarf::DW_FORM_udata, DWReg);
}
+
+ // Emit Mask
+ if (isSubRegister) {
+ unsigned Size = RI->getSubRegIdxSize(Idx);
+ unsigned Offset = RI->getSubRegIdxOffset(Idx);
+ if (Offset > 0) {
+ addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_bit_piece);
+ addUInt(TheDie, dwarf::DW_FORM_data1, Size);
+ addUInt(TheDie, dwarf::DW_FORM_data1, Offset);
+ } else {
+ unsigned ByteSize = Size / 8; // Assuming 8 bits per byte.
+ addUInt(TheDie, dwarf::DW_FORM_data1, dwarf::DW_OP_piece);
+ addUInt(TheDie, dwarf::DW_FORM_data1, ByteSize);
+ }
+ }
}
/// addRegisterOffset - Add register offset.
-void Unit::addRegisterOffset(DIEBlock *TheDie, unsigned Reg, int64_t Offset) {
+void DwarfUnit::addRegisterOffset(DIELoc *TheDie, unsigned Reg,
+ int64_t Offset) {
const TargetRegisterInfo *RI = Asm->TM.getRegisterInfo();
unsigned DWReg = RI->getDwarfRegNum(Reg, false);
const TargetRegisterInfo *TRI = Asm->TM.getRegisterInfo();
@@ -500,21 +519,21 @@ void Unit::addRegisterOffset(DIEBlock *TheDie, unsigned Reg, int64_t Offset) {
/// addAddress - Add an address attribute to a die based on the location
/// provided.
-void Unit::addAddress(DIE *Die, dwarf::Attribute Attribute,
- const MachineLocation &Location, bool Indirect) {
- DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
+void DwarfUnit::addAddress(DIE *Die, dwarf::Attribute Attribute,
+ const MachineLocation &Location, bool Indirect) {
+ DIELoc *Loc = new (DIEValueAllocator) DIELoc();
if (Location.isReg() && !Indirect)
- addRegisterOp(Block, Location.getReg());
+ addRegisterOp(Loc, Location.getReg());
else {
- addRegisterOffset(Block, Location.getReg(), Location.getOffset());
+ addRegisterOffset(Loc, Location.getReg(), Location.getOffset());
if (Indirect && !Location.isReg()) {
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
}
}
// Now attach the location information to the DIE.
- addBlock(Die, Attribute, Block);
+ addBlock(Die, Attribute, Loc);
}
/// addComplexAddress - Start with the address based on the location provided,
/// given the extra address information encoded in the DbgVariable, starting
/// from the starting location. Add the DWARF information to the die.
///
-void Unit::addComplexAddress(const DbgVariable &DV, DIE *Die,
- dwarf::Attribute Attribute,
- const MachineLocation &Location) {
- DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
+void DwarfUnit::addComplexAddress(const DbgVariable &DV, DIE *Die,
+ dwarf::Attribute Attribute,
+ const MachineLocation &Location) {
+ DIELoc *Loc = new (DIEValueAllocator) DIELoc();
unsigned N = DV.getNumAddrElements();
unsigned i = 0;
if (Location.isReg()) {
if (N >= 2 && DV.getAddrElement(0) == DIBuilder::OpPlus) {
// If first address element is OpPlus then emit
// DW_OP_breg + Offset instead of DW_OP_reg + Offset.
- addRegisterOffset(Block, Location.getReg(), DV.getAddrElement(1));
+ addRegisterOffset(Loc, Location.getReg(), DV.getAddrElement(1));
i = 2;
} else
- addRegisterOp(Block, Location.getReg());
+ addRegisterOp(Loc, Location.getReg());
} else
- addRegisterOffset(Block, Location.getReg(), Location.getOffset());
+ addRegisterOffset(Loc, Location.getReg(), Location.getOffset());
for (; i < N; ++i) {
uint64_t Element = DV.getAddrElement(i);
if (Element == DIBuilder::OpPlus) {
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
- addUInt(Block, dwarf::DW_FORM_udata, DV.getAddrElement(++i));
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
+ addUInt(Loc, dwarf::DW_FORM_udata, DV.getAddrElement(++i));
} else if (Element == DIBuilder::OpDeref) {
if (!Location.isReg())
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
} else
llvm_unreachable("unknown DIBuilder Opcode");
}
// Now attach the location information to the DIE.
- addBlock(Die, Attribute, Block);
+ addBlock(Die, Attribute, Loc);
}
/* Byref variables, in Blocks, are declared by the programmer as "SomeType
/// starting location. Add the DWARF information to the die. For
/// more information, read large comment just above here.
///
-void Unit::addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
- dwarf::Attribute Attribute,
- const MachineLocation &Location) {
+void DwarfUnit::addBlockByrefAddress(const DbgVariable &DV, DIE *Die,
+ dwarf::Attribute Attribute,
+ const MachineLocation &Location) {
DIType Ty = DV.getType();
DIType TmpTy = Ty;
uint16_t Tag = Ty.getTag();
// Decode the original location, and use that as the start of the byref
// variable's location.
- DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
+ DIELoc *Loc = new (DIEValueAllocator) DIELoc();
if (Location.isReg())
- addRegisterOp(Block, Location.getReg());
+ addRegisterOp(Loc, Location.getReg());
else
- addRegisterOffset(Block, Location.getReg(), Location.getOffset());
+ addRegisterOffset(Loc, Location.getReg(), Location.getOffset());
// If we started with a pointer to the __Block_byref... struct, then
// the first thing we need to do is dereference the pointer (DW_OP_deref).
if (isPointer)
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
// Next add the offset for the '__forwarding' field:
// DW_OP_plus_uconst ForwardingFieldOffset. Note there's no point in
// adding the offset if it's 0.
if (forwardingFieldOffset > 0) {
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
- addUInt(Block, dwarf::DW_FORM_udata, forwardingFieldOffset);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
+ addUInt(Loc, dwarf::DW_FORM_udata, forwardingFieldOffset);
}
// Now dereference the __forwarding field to get to the real __Block_byref
// struct: DW_OP_deref.
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
// Now that we've got the real __Block_byref... struct, add the offset
// for the variable's field to get to the location of the actual variable:
// DW_OP_plus_uconst varFieldOffset. Again, don't add if it's 0.
if (varFieldOffset > 0) {
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
- addUInt(Block, dwarf::DW_FORM_udata, varFieldOffset);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
+ addUInt(Loc, dwarf::DW_FORM_udata, varFieldOffset);
}
// Now attach the location information to the DIE.
- addBlock(Die, Attribute, Block);
+ addBlock(Die, Attribute, Loc);
}
/// isTypeSigned - Return true if the type is signed.
DIType BaseType = DD->resolve(Ty.getTypeDerivedFrom());
- // If this type is not derived from any type then take conservative approach.
- if (!BaseType.isValid())
+ // If this type is not derived from any type or the type is a declaration then
+ // take conservative approach.
+ if (!BaseType.isValid() || BaseType.isForwardDecl())
return Ty.getSizeInBits();
// If this is a derived type, go ahead and get the base type, unless it's a
}
/// addConstantValue - Add constant value entry in variable DIE.
-void Unit::addConstantValue(DIE *Die, const MachineOperand &MO, DIType Ty) {
+void DwarfUnit::addConstantValue(DIE *Die, const MachineOperand &MO,
+ DIType Ty) {
// FIXME: This is a bit conservative/simple - it emits negative values at
// their maximum bit width which is a bit unfortunate (& doesn't prefer
// udata/sdata over dataN as suggested by the DWARF spec)
}
/// addConstantFPValue - Add constant value entry in variable DIE.
-void Unit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
+void DwarfUnit::addConstantFPValue(DIE *Die, const MachineOperand &MO) {
assert(MO.isFPImm() && "Invalid machine operand!");
DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
APFloat FPImm = MO.getFPImm()->getValueAPF();
}
/// addConstantFPValue - Add constant value entry in variable DIE.
-void Unit::addConstantFPValue(DIE *Die, const ConstantFP *CFP) {
+void DwarfUnit::addConstantFPValue(DIE *Die, const ConstantFP *CFP) {
// Pass this down to addConstantValue as an unsigned bag of bits.
addConstantValue(Die, CFP->getValueAPF().bitcastToAPInt(), true);
}
/// addConstantValue - Add constant value entry in variable DIE.
-void Unit::addConstantValue(DIE *Die, const ConstantInt *CI, bool Unsigned) {
+void DwarfUnit::addConstantValue(DIE *Die, const ConstantInt *CI,
+ bool Unsigned) {
addConstantValue(Die, CI->getValue(), Unsigned);
}
// addConstantValue - Add constant value entry in variable DIE.
-void Unit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
+void DwarfUnit::addConstantValue(DIE *Die, const APInt &Val, bool Unsigned) {
unsigned CIBitWidth = Val.getBitWidth();
if (CIBitWidth <= 64) {
// If we're a signed constant definitely use sdata.
}
/// addTemplateParams - Add template parameters into buffer.
-void Unit::addTemplateParams(DIE &Buffer, DIArray TParams) {
+void DwarfUnit::addTemplateParams(DIE &Buffer, DIArray TParams) {
// Add template parameters.
for (unsigned i = 0, e = TParams.getNumElements(); i != e; ++i) {
DIDescriptor Element = TParams.getElement(i);
}
/// getOrCreateContextDIE - Get context owner's DIE.
-DIE *Unit::getOrCreateContextDIE(DIScope Context) {
+DIE *DwarfUnit::getOrCreateContextDIE(DIScope Context) {
if (!Context || Context.isFile())
return getUnitDie();
if (Context.isType())
return getDIE(Context);
}
-DIE *Unit::createTypeDIE(DICompositeType Ty) {
+DIE *DwarfUnit::createTypeDIE(DICompositeType Ty) {
DIScope Context = resolve(Ty.getContext());
DIE *ContextDIE = getOrCreateContextDIE(Context);
return TyDIE;
}
-/// Return true if the type is appropriately scoped to be contained inside
-/// its own type unit.
-static bool isTypeUnitScoped(DIType Ty, const DwarfDebug *DD) {
- DIScope Parent = DD->resolve(Ty.getContext());
- while (Parent) {
- // Don't generate a hash for anything scoped inside a function.
- if (Parent.isSubprogram())
- return false;
- Parent = DD->resolve(Parent.getContext());
- }
- return true;
-}
-
-/// Return true if the type should be split out into a type unit.
-static bool shouldCreateTypeUnit(DICompositeType CTy, const DwarfDebug *DD) {
- if (!GenerateTypeUnits)
- return false;
-
- uint16_t Tag = CTy.getTag();
-
- switch (Tag) {
- case dwarf::DW_TAG_structure_type:
- case dwarf::DW_TAG_union_type:
- case dwarf::DW_TAG_enumeration_type:
- case dwarf::DW_TAG_class_type:
- // If this is a class, structure, union, or enumeration type
- // that is a definition (not a declaration), and not scoped
- // inside a function then separate this out as a type unit.
- return !CTy.isForwardDecl() && isTypeUnitScoped(CTy, DD);
- default:
- return false;
- }
-}
-
/// getOrCreateTypeDIE - Find existing DIE or create new DIE for the
/// given DIType.
-DIE *Unit::getOrCreateTypeDIE(const MDNode *TyNode) {
+DIE *DwarfUnit::getOrCreateTypeDIE(const MDNode *TyNode) {
if (!TyNode)
return NULL;
// Create new type.
TyDIE = createAndAddDIE(Ty.getTag(), *ContextDIE, Ty);
+ updateAcceleratorTables(Context, Ty, TyDIE);
+
if (Ty.isBasicType())
constructTypeDIE(*TyDIE, DIBasicType(Ty));
else if (Ty.isCompositeType()) {
DICompositeType CTy(Ty);
- if (shouldCreateTypeUnit(CTy, DD)) {
- DD->addTypeUnitType(getLanguage(), TyDIE, CTy);
- // Skip updating the accellerator tables since this is not the full type
- return TyDIE;
- }
+ if (GenerateDwarfTypeUnits && !Ty.isForwardDecl())
+ if (MDString *TypeId = CTy.getIdentifier()) {
+ DD->addDwarfTypeUnitType(getCU(), TypeId->getString(), TyDIE, CTy);
+ // Skip updating the accelerator tables since this is not the full type.
+ return TyDIE;
+ }
constructTypeDIE(*TyDIE, CTy);
} else {
assert(Ty.isDerivedType() && "Unknown kind of DIType");
constructTypeDIE(*TyDIE, DIDerivedType(Ty));
}
- updateAcceleratorTables(Context, Ty, TyDIE);
-
return TyDIE;
}
-void Unit::updateAcceleratorTables(DIScope Context, DIType Ty,
- const DIE *TyDIE) {
+void DwarfUnit::updateAcceleratorTables(DIScope Context, DIType Ty,
+ const DIE *TyDIE) {
if (!Ty.getName().empty() && !Ty.isForwardDecl()) {
bool IsImplementation = 0;
if (Ty.isCompositeType()) {
unsigned Flags = IsImplementation ? dwarf::DW_FLAG_type_implementation : 0;
addAccelType(Ty.getName(), std::make_pair(TyDIE, Flags));
- if (!Context || Context.isCompileUnit() || Context.isFile() ||
- Context.isNameSpace())
+ if ((!Context || Context.isCompileUnit() || Context.isFile() ||
+ Context.isNameSpace()) &&
+ getCUNode().getEmissionKind() != DIBuilder::LineTablesOnly)
GlobalTypes[getParentContextString(Context) + Ty.getName().str()] = TyDIE;
}
}
/// addType - Add a new type attribute to the specified entity.
-void Unit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
+void DwarfUnit::addType(DIE *Entity, DIType Ty, dwarf::Attribute Attribute) {
assert(Ty && "Trying to add a type that doesn't exist?");
// Check for pre-existence.
// DIE to the proper table while ensuring that the name that we're going
// to reference is in the string table. We do this since the names we
// add may not only be identical to the names in the DIE.
-void Unit::addAccelName(StringRef Name, const DIE *Die) {
+void DwarfUnit::addAccelName(StringRef Name, const DIE *Die) {
+ if (!DD->useDwarfAccelTables())
+ return;
DU->getStringPoolEntry(Name);
std::vector<const DIE *> &DIEs = AccelNames[Name];
DIEs.push_back(Die);
}
-void Unit::addAccelObjC(StringRef Name, const DIE *Die) {
+void DwarfUnit::addAccelObjC(StringRef Name, const DIE *Die) {
+ if (!DD->useDwarfAccelTables())
+ return;
DU->getStringPoolEntry(Name);
std::vector<const DIE *> &DIEs = AccelObjC[Name];
DIEs.push_back(Die);
}
-void Unit::addAccelNamespace(StringRef Name, const DIE *Die) {
+void DwarfUnit::addAccelNamespace(StringRef Name, const DIE *Die) {
+ if (!DD->useDwarfAccelTables())
+ return;
DU->getStringPoolEntry(Name);
std::vector<const DIE *> &DIEs = AccelNamespace[Name];
DIEs.push_back(Die);
}
-void Unit::addAccelType(StringRef Name, std::pair<const DIE *, unsigned> Die) {
+void DwarfUnit::addAccelType(StringRef Name,
+ std::pair<const DIE *, unsigned> Die) {
+ if (!DD->useDwarfAccelTables())
+ return;
DU->getStringPoolEntry(Name);
std::vector<std::pair<const DIE *, unsigned> > &DIEs = AccelTypes[Name];
DIEs.push_back(Die);
}
/// addGlobalName - Add a new global name to the compile unit.
-void Unit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
+void DwarfUnit::addGlobalName(StringRef Name, DIE *Die, DIScope Context) {
+ if (getCUNode().getEmissionKind() == DIBuilder::LineTablesOnly)
+ return;
std::string FullName = getParentContextString(Context) + Name.str();
GlobalNames[FullName] = Die;
}
/// it as a string. This is done at the metadata level because DIEs may
/// not currently have been added to the parent context and walking the
/// DIEs looking for names is more expensive than walking the metadata.
-std::string Unit::getParentContextString(DIScope Context) const {
+std::string DwarfUnit::getParentContextString(DIScope Context) const {
if (!Context)
return "";
}
/// constructTypeDIE - Construct basic type die from DIBasicType.
-void Unit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
+void DwarfUnit::constructTypeDIE(DIE &Buffer, DIBasicType BTy) {
// Get core information.
StringRef Name = BTy.getName();
// Add name if not anonymous or intermediate type.
}
/// constructTypeDIE - Construct derived type die from DIDerivedType.
-void Unit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
+void DwarfUnit::constructTypeDIE(DIE &Buffer, DIDerivedType DTy) {
// Get core information.
StringRef Name = DTy.getName();
uint64_t Size = DTy.getSizeInBits() >> 3;
addSourceLine(&Buffer, DTy);
}
+/// constructSubprogramArguments - Construct function argument DIEs.
+void DwarfUnit::constructSubprogramArguments(DIE &Buffer, DIArray Args) {
+ for (unsigned i = 1, N = Args.getNumElements(); i < N; ++i) {
+ DIDescriptor Ty = Args.getElement(i);
+ if (Ty.isUnspecifiedParameter()) {
+ assert(i == N-1 && "Unspecified parameter must be the last argument");
+ createAndAddDIE(dwarf::DW_TAG_unspecified_parameters, Buffer);
+ } else {
+ DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, Buffer);
+ addType(Arg, DIType(Ty));
+ if (DIType(Ty).isArtificial())
+ addFlag(Arg, dwarf::DW_AT_artificial);
+ }
+ }
+}
+
/// constructTypeDIE - Construct type DIE from DICompositeType.
-void Unit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
+void DwarfUnit::constructTypeDIE(DIE &Buffer, DICompositeType CTy) {
// Add name if not anonymous or intermediate type.
StringRef Name = CTy.getName();
addType(&Buffer, RTy);
bool isPrototyped = true;
- // Add arguments.
- for (unsigned i = 1, N = Elements.getNumElements(); i < N; ++i) {
- DIDescriptor Ty = Elements.getElement(i);
- if (Ty.isUnspecifiedParameter()) {
- createAndAddDIE(dwarf::DW_TAG_unspecified_parameters, Buffer);
- isPrototyped = false;
- } else {
- DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, Buffer);
- addType(Arg, DIType(Ty));
- if (DIType(Ty).isArtificial())
- addFlag(Arg, dwarf::DW_AT_artificial);
- }
- }
+ if (Elements.getNumElements() == 2 &&
+ Elements.getElement(1).isUnspecifiedParameter())
+ isPrototyped = false;
+
+ constructSubprogramArguments(Buffer, Elements);
+
// Add prototype flag if we're dealing with a C language and the
// function has been prototyped.
uint16_t Language = getLanguage();
(Language == dwarf::DW_LANG_C89 || Language == dwarf::DW_LANG_C99 ||
Language == dwarf::DW_LANG_ObjC))
addFlag(&Buffer, dwarf::DW_AT_prototyped);
+
+ if (CTy.isLValueReference())
+ addFlag(&Buffer, dwarf::DW_AT_reference);
+
+ if (CTy.isRValueReference())
+ addFlag(&Buffer, dwarf::DW_AT_rvalue_reference);
} break;
case dwarf::DW_TAG_structure_type:
case dwarf::DW_TAG_union_type:
for (unsigned i = 0, N = Elements.getNumElements(); i < N; ++i) {
DIDescriptor Element = Elements.getElement(i);
DIE *ElemDie = NULL;
- if (Element.isSubprogram()) {
- DISubprogram SP(Element);
- ElemDie = getOrCreateSubprogramDIE(SP);
- if (SP.isProtected())
- addUInt(ElemDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
- dwarf::DW_ACCESS_protected);
- else if (SP.isPrivate())
- addUInt(ElemDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
- dwarf::DW_ACCESS_private);
- else
- addUInt(ElemDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
- dwarf::DW_ACCESS_public);
- if (SP.isExplicit())
- addFlag(ElemDie, dwarf::DW_AT_explicit);
- } else if (Element.isDerivedType()) {
+ if (Element.isSubprogram())
+ ElemDie = getOrCreateSubprogramDIE(DISubprogram(Element));
+ else if (Element.isDerivedType()) {
DIDerivedType DDTy(Element);
if (DDTy.getTag() == dwarf::DW_TAG_friend) {
ElemDie = createAndAddDIE(dwarf::DW_TAG_friend, Buffer);
ElemDie = createAndAddDIE(Property.getTag(), Buffer);
StringRef PropertyName = Property.getObjCPropertyName();
addString(ElemDie, dwarf::DW_AT_APPLE_property_name, PropertyName);
- addType(ElemDie, Property.getType());
+ if (Property.getType())
+ addType(ElemDie, Property.getType());
addSourceLine(ElemDie, Property);
StringRef GetterName = Property.getObjCPropertyGetterName();
if (!GetterName.empty())
/// constructTemplateTypeParameterDIE - Construct new DIE for the given
/// DITemplateTypeParameter.
-void Unit::constructTemplateTypeParameterDIE(DIE &Buffer,
- DITemplateTypeParameter TP) {
+void DwarfUnit::constructTemplateTypeParameterDIE(DIE &Buffer,
+ DITemplateTypeParameter TP) {
DIE *ParamDIE =
createAndAddDIE(dwarf::DW_TAG_template_type_parameter, Buffer);
// Add the type if it exists, it could be void and therefore no type.
/// constructTemplateValueParameterDIE - Construct new DIE for the given
/// DITemplateValueParameter.
-void Unit::constructTemplateValueParameterDIE(DIE &Buffer,
+void
+DwarfUnit::constructTemplateValueParameterDIE(DIE &Buffer,
DITemplateValueParameter VP) {
DIE *ParamDIE = createAndAddDIE(VP.getTag(), Buffer);
else if (GlobalValue *GV = dyn_cast<GlobalValue>(Val)) {
// For declaration non-type template parameters (such as global values and
// functions)
- DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
- addOpAddress(Block, Asm->getSymbol(GV));
+ DIELoc *Loc = new (DIEValueAllocator) DIELoc();
+ addOpAddress(Loc, Asm->getSymbol(GV));
// Emit DW_OP_stack_value to use the address as the immediate value of the
// parameter, rather than a pointer to it.
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_stack_value);
- addBlock(ParamDIE, dwarf::DW_AT_location, Block);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_stack_value);
+ addBlock(ParamDIE, dwarf::DW_AT_location, Loc);
} else if (VP.getTag() == dwarf::DW_TAG_GNU_template_template_param) {
assert(isa<MDString>(Val));
addString(ParamDIE, dwarf::DW_AT_GNU_template_name,
}
/// getOrCreateNameSpace - Create a DIE for DINameSpace.
-DIE *Unit::getOrCreateNameSpace(DINameSpace NS) {
+DIE *DwarfUnit::getOrCreateNameSpace(DINameSpace NS) {
// Construct the context before querying for the existence of the DIE in case
// such construction creates the DIE.
DIE *ContextDIE = getOrCreateContextDIE(NS.getContext());
}
/// getOrCreateSubprogramDIE - Create new DIE using SP.
-DIE *Unit::getOrCreateSubprogramDIE(DISubprogram SP) {
+DIE *DwarfUnit::getOrCreateSubprogramDIE(DISubprogram SP) {
// Construct the context before querying for the existence of the DIE in case
// such construction creates the DIE (as is the case for member function
// declarations).
unsigned VK = SP.getVirtuality();
if (VK) {
addUInt(SPDie, dwarf::DW_AT_virtuality, dwarf::DW_FORM_data1, VK);
- DIEBlock *Block = getDIEBlock();
+ DIELoc *Block = getDIELoc();
addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
addUInt(Block, dwarf::DW_FORM_udata, SP.getVirtualIndex());
addBlock(SPDie, dwarf::DW_AT_vtable_elem_location, Block);
// Add arguments. Do not add arguments for subprogram definition. They will
// be handled while processing variables.
- for (unsigned i = 1, N = Args.getNumElements(); i < N; ++i) {
- DIE *Arg = createAndAddDIE(dwarf::DW_TAG_formal_parameter, *SPDie);
- DIType ATy(Args.getElement(i));
- addType(Arg, ATy);
- if (ATy.isArtificial())
- addFlag(Arg, dwarf::DW_AT_artificial);
- }
+ constructSubprogramArguments(*SPDie, Args);
}
if (SP.isArtificial())
addUInt(SPDie, dwarf::DW_AT_APPLE_isa, dwarf::DW_FORM_flag, isa);
}
+ if (SP.isLValueReference())
+ addFlag(SPDie, dwarf::DW_AT_reference);
+
+ if (SP.isRValueReference())
+ addFlag(SPDie, dwarf::DW_AT_rvalue_reference);
+
+ if (SP.isProtected())
+ addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
+ dwarf::DW_ACCESS_protected);
+ else if (SP.isPrivate())
+ addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
+ dwarf::DW_ACCESS_private);
+ else
+ addUInt(SPDie, dwarf::DW_AT_accessibility, dwarf::DW_FORM_data1,
+ dwarf::DW_ACCESS_public);
+
+ if (SP.isExplicit())
+ addFlag(SPDie, dwarf::DW_AT_explicit);
+
return SPDie;
}
}
/// createGlobalVariableDIE - create global variable DIE.
-void CompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
+void DwarfCompileUnit::createGlobalVariableDIE(DIGlobalVariable GV) {
// Check for pre-existence.
if (getDIE(GV))
return;
- if (!GV.isGlobalVariable())
- return;
+ assert(GV.isGlobalVariable());
DIScope GVContext = GV.getContext();
DIType GTy = GV.getType();
bool isGlobalVariable = GV.getGlobal() != NULL;
if (isGlobalVariable) {
addToAccelTable = true;
- DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
+ DIELoc *Loc = new (DIEValueAllocator) DIELoc();
const MCSymbol *Sym = Asm->getSymbol(GV.getGlobal());
if (GV.getGlobal()->isThreadLocal()) {
// FIXME: Make this work with -gsplit-dwarf.
unsigned PointerSize = Asm->getDataLayout().getPointerSize();
assert((PointerSize == 4 || PointerSize == 8) &&
"Add support for other sizes if necessary");
- const MCExpr *Expr =
- Asm->getObjFileLowering().getDebugThreadLocalSymbol(Sym);
// Based on GCC's support for TLS:
if (!DD->useSplitDwarf()) {
// 1) Start with a constNu of the appropriate pointer size
- addUInt(Block, dwarf::DW_FORM_data1,
+ addUInt(Loc, dwarf::DW_FORM_data1,
PointerSize == 4 ? dwarf::DW_OP_const4u : dwarf::DW_OP_const8u);
// 2) containing the (relocated) offset of the TLS variable
// within the module's TLS block.
- addExpr(Block, dwarf::DW_FORM_udata, Expr);
+ addExpr(Loc, dwarf::DW_FORM_udata,
+ Asm->getObjFileLowering().getDebugThreadLocalSymbol(Sym));
} else {
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_const_index);
- addUInt(Block, dwarf::DW_FORM_udata, DU->getAddrPoolIndex(Expr));
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_const_index);
+ addUInt(Loc, dwarf::DW_FORM_udata,
+ DU->getAddrPoolIndex(Sym, /* TLS */ true));
}
// 3) followed by a custom OP to make the debugger do a TLS lookup.
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_push_tls_address);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_GNU_push_tls_address);
} else {
DD->addArangeLabel(SymbolCU(this, Sym));
- addOpAddress(Block, Sym);
+ addOpAddress(Loc, Sym);
}
// Do not create specification DIE if context is either compile unit
// or a subprogram.
// Create specification DIE.
VariableSpecDIE = createAndAddDIE(dwarf::DW_TAG_variable, *UnitDie);
addDIEEntry(VariableSpecDIE, dwarf::DW_AT_specification, VariableDIE);
- addBlock(VariableSpecDIE, dwarf::DW_AT_location, Block);
+ addBlock(VariableSpecDIE, dwarf::DW_AT_location, Loc);
// A static member's declaration is already flagged as such.
if (!SDMDecl.Verify())
addFlag(VariableDIE, dwarf::DW_AT_declaration);
} else {
- addBlock(VariableDIE, dwarf::DW_AT_location, Block);
+ addBlock(VariableDIE, dwarf::DW_AT_location, Loc);
}
// Add the linkage name.
StringRef LinkageName = GV.getLinkageName();
// TAG_variable.
addString(IsStaticMember && VariableSpecDIE ? VariableSpecDIE
: VariableDIE,
- dwarf::DW_AT_MIPS_linkage_name,
+ DD->getDwarfVersion() >= 4 ? dwarf::DW_AT_linkage_name
+ : dwarf::DW_AT_MIPS_linkage_name,
GlobalValue::getRealLinkageName(LinkageName));
} else if (const ConstantInt *CI =
dyn_cast_or_null<ConstantInt>(GV.getConstant())) {
} else if (const ConstantExpr *CE = getMergedGlobalExpr(GV->getOperand(11))) {
addToAccelTable = true;
// GV is a merged global.
- DIEBlock *Block = new (DIEValueAllocator) DIEBlock();
+ DIELoc *Loc = new (DIEValueAllocator) DIELoc();
Value *Ptr = CE->getOperand(0);
MCSymbol *Sym = Asm->getSymbol(cast<GlobalValue>(Ptr));
DD->addArangeLabel(SymbolCU(this, Sym));
- addOpAddress(Block, Sym);
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
+ addOpAddress(Loc, Sym);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
SmallVector<Value *, 3> Idx(CE->op_begin() + 1, CE->op_end());
- addUInt(Block, dwarf::DW_FORM_udata,
+ addUInt(Loc, dwarf::DW_FORM_udata,
Asm->getDataLayout().getIndexedOffset(Ptr->getType(), Idx));
- addUInt(Block, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
- addBlock(VariableDIE, dwarf::DW_AT_location, Block);
+ addUInt(Loc, dwarf::DW_FORM_data1, dwarf::DW_OP_plus);
+ addBlock(VariableDIE, dwarf::DW_AT_location, Loc);
}
if (addToAccelTable) {
}
/// constructSubrangeDIE - Construct subrange DIE from DISubrange.
-void Unit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
+void DwarfUnit::constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy) {
DIE *DW_Subrange = createAndAddDIE(dwarf::DW_TAG_subrange_type, Buffer);
addDIEEntry(DW_Subrange, dwarf::DW_AT_type, IndexTy);
}
/// constructArrayTypeDIE - Construct array type DIE from DICompositeType.
-void Unit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
+void DwarfUnit::constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy) {
if (CTy.isVector())
addFlag(&Buffer, dwarf::DW_AT_GNU_vector);
}
/// constructEnumTypeDIE - Construct an enum type DIE from DICompositeType.
-void Unit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
+void DwarfUnit::constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy) {
DIArray Elements = CTy.getTypeArray();
// Add enumerators to enumeration type.
/// constructContainingTypeDIEs - Construct DIEs for types that contain
/// vtables.
-void Unit::constructContainingTypeDIEs() {
+void DwarfUnit::constructContainingTypeDIEs() {
for (DenseMap<DIE *, const MDNode *>::iterator CI = ContainingTypeMap.begin(),
CE = ContainingTypeMap.end();
CI != CE; ++CI) {
}
/// constructVariableDIE - Construct a DIE for the given DbgVariable.
-DIE *Unit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
+DIE *DwarfUnit::constructVariableDIE(DbgVariable &DV, bool isScopeAbstract) {
StringRef Name = DV.getName();
// Define variable debug information entry.
unsigned Offset = DV.getDotDebugLocOffset();
if (Offset != ~0U) {
- addSectionLabel(VariableDie, dwarf::DW_AT_location,
- Asm->GetTempSymbol("debug_loc", Offset));
+ addLocationList(VariableDie, dwarf::DW_AT_location, Offset);
DV.setDIE(VariableDie);
return VariableDie;
}
}
/// constructMemberDIE - Construct member DIE from DIDerivedType.
-void Unit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
+void DwarfUnit::constructMemberDIE(DIE &Buffer, DIDerivedType DT) {
DIE *MemberDie = createAndAddDIE(DT.getTag(), Buffer);
StringRef Name = DT.getName();
if (!Name.empty())
addSourceLine(MemberDie, DT);
- DIEBlock *MemLocationDie = new (DIEValueAllocator) DIEBlock();
- addUInt(MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
-
if (DT.getTag() == dwarf::DW_TAG_inheritance && DT.isVirtual()) {
// For C++, virtual base classes are not at fixed offset. Use following
// expression to extract appropriate offset from vtable.
// BaseAddr = ObAddr + *((*ObAddr) - Offset)
- DIEBlock *VBaseLocationDie = new (DIEValueAllocator) DIEBlock();
+ DIELoc *VBaseLocationDie = new (DIEValueAllocator) DIELoc();
addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_dup);
addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_deref);
addUInt(VBaseLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_constu);
uint64_t OffsetInBytes;
if (Size != FieldSize) {
- // Handle bitfield.
- addUInt(MemberDie, dwarf::DW_AT_byte_size, None,
- getBaseTypeSize(DD, DT) >> 3);
- addUInt(MemberDie, dwarf::DW_AT_bit_size, None, DT.getSizeInBits());
+ // Handle bitfield, assume bytes are 8 bits.
+ addUInt(MemberDie, dwarf::DW_AT_byte_size, None, FieldSize/8);
+ addUInt(MemberDie, dwarf::DW_AT_bit_size, None, Size);
uint64_t Offset = DT.getOffsetInBits();
uint64_t AlignMask = ~(DT.getAlignInBits() - 1);
Offset = FieldSize - (Offset + Size);
addUInt(MemberDie, dwarf::DW_AT_bit_offset, None, Offset);
- // Here WD_AT_data_member_location points to the anonymous
+ // Here DW_AT_data_member_location points to the anonymous
// field that includes this bit field.
OffsetInBytes = FieldOffset >> 3;
} else
// This is not a bitfield.
OffsetInBytes = DT.getOffsetInBits() >> 3;
- addUInt(MemberDie, dwarf::DW_AT_data_member_location, None, OffsetInBytes);
+
+ if (DD->getDwarfVersion() <= 2) {
+ DIELoc *MemLocationDie = new (DIEValueAllocator) DIELoc();
+ addUInt(MemLocationDie, dwarf::DW_FORM_data1, dwarf::DW_OP_plus_uconst);
+ addUInt(MemLocationDie, dwarf::DW_FORM_udata, OffsetInBytes);
+ addBlock(MemberDie, dwarf::DW_AT_data_member_location, MemLocationDie);
+ } else
+ addUInt(MemberDie, dwarf::DW_AT_data_member_location, None,
+ OffsetInBytes);
}
if (DT.isProtected())
}
/// getOrCreateStaticMemberDIE - Create new DIE for C++ static member.
-DIE *Unit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
+DIE *DwarfUnit::getOrCreateStaticMemberDIE(DIDerivedType DT) {
if (!DT.Verify())
return NULL;
return StaticMemberDIE;
}
-void Unit::emitHeader(const MCSection *ASection, const MCSymbol *ASectionSym) {
+void DwarfUnit::emitHeader(const MCSection *ASection,
+ const MCSymbol *ASectionSym) const {
Asm->OutStreamer.AddComment("DWARF version number");
Asm->EmitInt16(DD->getDwarfVersion());
Asm->OutStreamer.AddComment("Offset Into Abbrev. Section");
@@ -1983,3 +2006,63 @@ void Unit::emitHeader(const MCSection *ASection, const MCSymbol *ASectionSym) {
Asm->OutStreamer.AddComment("Address Size (in bytes)");
Asm->EmitInt8(Asm->getDataLayout().getPointerSize());
}
+
+void DwarfCompileUnit::initStmtList(MCSymbol *DwarfLineSectionSym) {
+ // Define start line table label for each Compile Unit.
+ MCSymbol *LineTableStartSym =
+ Asm->GetTempSymbol("line_table_start", getUniqueID());
+ Asm->OutStreamer.getContext().setMCLineTableSymbol(LineTableStartSym,
+ getUniqueID());
+
+ // Use a single line table if we are generating assembly.
+ bool UseTheFirstCU =
+ Asm->OutStreamer.hasRawTextSupport() || (getUniqueID() == 0);
+
+ stmtListIndex = UnitDie->getValues().size();
+
+ // DW_AT_stmt_list is a offset of line number information for this
+ // compile unit in debug_line section. For split dwarf this is
+ // left in the skeleton CU and so not included.
+ // The line table entries are not always emitted in assembly, so it
+ // is not okay to use line_table_start here.
+ if (Asm->MAI->doesDwarfUseRelocationsAcrossSections())
+ addSectionLabel(UnitDie.get(), dwarf::DW_AT_stmt_list,
+ UseTheFirstCU ? DwarfLineSectionSym : LineTableStartSym);
+ else if (UseTheFirstCU)
+ addSectionOffset(UnitDie.get(), dwarf::DW_AT_stmt_list, 0);
+ else
+ addSectionDelta(UnitDie.get(), dwarf::DW_AT_stmt_list, LineTableStartSym,
+ DwarfLineSectionSym);
+}
+
+void DwarfCompileUnit::applyStmtList(DIE &D) {
+ D.addValue(dwarf::DW_AT_stmt_list,
+ UnitDie->getAbbrev().getData()[stmtListIndex].getForm(),
+ UnitDie->getValues()[stmtListIndex]);
+}
+
+void DwarfTypeUnit::emitHeader(const MCSection *ASection,
+ const MCSymbol *ASectionSym) const {
+ DwarfUnit::emitHeader(ASection, ASectionSym);
+ Asm->OutStreamer.AddComment("Type Signature");
+ Asm->OutStreamer.EmitIntValue(TypeSignature, sizeof(TypeSignature));
+ Asm->OutStreamer.AddComment("Type DIE Offset");
+ // In a skeleton type unit there is no type DIE so emit a zero offset.
+ Asm->OutStreamer.EmitIntValue(Ty ? Ty->getOffset() : 0,
+ sizeof(Ty->getOffset()));
+}
+
+void DwarfTypeUnit::initSection(const MCSection *Section) {
+ assert(!this->Section);
+ this->Section = Section;
+ // Since each type unit is contained in its own COMDAT section, the begin
+ // label and the section label are the same. Using the begin label emission in
+ // DwarfDebug to emit the section label as well is slightly subtle/sneaky, but
+ // the only other alternative of lazily constructing start-of-section labels
+ // and storing a mapping in DwarfDebug (or AsmPrinter).
+ this->SectionSym = this->LabelBegin =
+ Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID());
+ this->LabelEnd =
+ Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID());
+ this->LabelRange = Asm->GetTempSymbol("gnu_ranges", getUniqueID());
+}