index d54a0133fed6205025463787859ff40cb4cd38e8..0b117ac6566bbcc24e4a1fe3983d0a9e9154a7ab 100644 (file)
class UserValue {
const MDNode *variable; ///< The debug info variable we are part of.
unsigned offset; ///< Byte offset into variable.
- bool Indirect; ///< true if this is a register-indirect+offset value.
DebugLoc dl; ///< The debug location for the variable. This is
///< used by dwarf writer to find lexical scope.
UserValue *leader; ///< Equivalence class leader.
public:
/// UserValue - Create a new UserValue.
- UserValue(const MDNode *var, unsigned o, bool i, DebugLoc L,
+ UserValue(const MDNode *var, unsigned o, DebugLoc L,
LocMap::Allocator &alloc)
- : variable(var), offset(o), Indirect(i), dl(L), leader(this),
- next(0), locInts(alloc)
+ : variable(var), offset(o), dl(L), leader(this), next(0), locInts(alloc)
{}
/// getLeader - Get the leader of this value's equivalence class.
UVMap userVarMap;
/// getUserValue - Find or create a UserValue.
- UserValue *getUserValue(const MDNode *Var, unsigned Offset,
- bool Indirect, DebugLoc DL);
+ UserValue *getUserValue(const MDNode *Var, unsigned Offset, DebugLoc DL);
/// lookupVirtReg - Find the EC leader for VirtReg or null.
UserValue *lookupVirtReg(unsigned VirtReg);
}
UserValue *LDVImpl::getUserValue(const MDNode *Var, unsigned Offset,
- bool Indirect, DebugLoc DL) {
+ DebugLoc DL) {
UserValue *&Leader = userVarMap[Var];
if (Leader) {
UserValue *UV = Leader->getLeader();
return UV;
}
- UserValue *UV = new UserValue(Var, Offset, Indirect, DL, allocator);
+ UserValue *UV = new UserValue(Var, Offset, DL, allocator);
userValues.push_back(UV);
Leader = UserValue::merge(Leader, UV);
return UV;
bool LDVImpl::handleDebugValue(MachineInstr *MI, SlotIndex Idx) {
// DBG_VALUE loc, offset, variable
if (MI->getNumOperands() != 3 ||
- !(MI->getOperand(1).isReg() || MI->getOperand(1).isImm()) ||
- !MI->getOperand(2).isMetadata()) {
+ !MI->getOperand(1).isImm() || !MI->getOperand(2).isMetadata()) {
DEBUG(dbgs() << "Can't handle " << *MI);
return false;
}
// Get or create the UserValue for (variable,offset).
- bool Indirect = MI->getOperand(1).isImm();
- unsigned Offset = Indirect ? MI->getOperand(1).getImm() : 0;
+ unsigned Offset = MI->getOperand(1).getImm();
const MDNode *Var = MI->getOperand(2).getMetadata();
- UserValue *UV = getUserValue(Var, Offset, Indirect, MI->getDebugLoc());
+ UserValue *UV = getUserValue(Var, Offset, MI->getDebugLoc());
UV->addDef(Idx, MI->getOperand(0));
return true;
}
// Frame index locations may require a target callback.
if (Loc.isFI()) {
MachineInstr *MI = TII.emitFrameIndexDebugValue(*MBB->getParent(),
- Loc.getIndex(),
- offset, variable,
+ Loc.getIndex(), offset, variable,
findDebugLoc());
if (MI) {
MBB->insert(I, MI);
}
}
// This is not a frame index, or the target is happy with a standard FI.
-
- if (Loc.isReg())
- BuildMI(*MBB, I, findDebugLoc(), TII.get(TargetOpcode::DBG_VALUE),
- Indirect, Loc.getReg(), offset, variable);
- else
- BuildMI(*MBB, I, findDebugLoc(), TII.get(TargetOpcode::DBG_VALUE))
- .addOperand(Loc).addImm(offset).addMetadata(variable);
+ BuildMI(*MBB, I, findDebugLoc(), TII.get(TargetOpcode::DBG_VALUE))
+ .addOperand(Loc).addImm(offset).addMetadata(variable);
}
void UserValue::emitDebugValues(VirtRegMap *VRM, LiveIntervals &LIS,