index dd0f5488675d07b819713d87906a66104da671bd..ec40656e4f0e8ecd6e415f922e39668d3e7b9e46 100644 (file)
//
//===----------------------------------------------------------------------===//
-#define DEBUG_TYPE "regalloc"
#include "RegisterCoalescer.h"
-#include "LiveDebugVariables.h"
-#include "VirtRegMap.h"
-
-#include "llvm/Pass.h"
-#include "llvm/Value.h"
-#include "llvm/ADT/OwningPtr.h"
#include "llvm/ADT/STLExtras.h"
#include "llvm/ADT/SmallSet.h"
#include "llvm/ADT/Statistic.h"
#include "llvm/Analysis/AliasAnalysis.h"
#include "llvm/CodeGen/LiveIntervalAnalysis.h"
-#include "llvm/CodeGen/LiveIntervalAnalysis.h"
#include "llvm/CodeGen/LiveRangeEdit.h"
#include "llvm/CodeGen/MachineFrameInfo.h"
#include "llvm/CodeGen/MachineInstr.h"
-#include "llvm/CodeGen/MachineInstr.h"
#include "llvm/CodeGen/MachineLoopInfo.h"
#include "llvm/CodeGen/MachineRegisterInfo.h"
-#include "llvm/CodeGen/MachineRegisterInfo.h"
#include "llvm/CodeGen/Passes.h"
#include "llvm/CodeGen/RegisterClassInfo.h"
+#include "llvm/CodeGen/VirtRegMap.h"
+#include "llvm/IR/Value.h"
+#include "llvm/Pass.h"
#include "llvm/Support/CommandLine.h"
#include "llvm/Support/Debug.h"
#include "llvm/Support/ErrorHandling.h"
#include "llvm/Support/raw_ostream.h"
#include "llvm/Target/TargetInstrInfo.h"
-#include "llvm/Target/TargetInstrInfo.h"
#include "llvm/Target/TargetMachine.h"
-#include "llvm/Target/TargetOptions.h"
#include "llvm/Target/TargetRegisterInfo.h"
+#include "llvm/Target/TargetSubtargetInfo.h"
#include <algorithm>
#include <cmath>
using namespace llvm;
+#define DEBUG_TYPE "regalloc"
+
STATISTIC(numJoins , "Number of interval joins performed");
STATISTIC(numCrossRCs , "Number of cross class joins performed");
STATISTIC(numCommutes , "Number of instruction commuting performed");
cl::desc("Coalesce copies (default=true)"),
cl::init(true));
+// Temporary flag to test critical edge unsplitting.
+static cl::opt<bool>
+EnableJoinSplits("join-splitedges",
+ cl::desc("Coalesce copies on split edges (default=subtarget)"), cl::Hidden);
+
+// Temporary flag to test global copy optimization.
+static cl::opt<cl::boolOrDefault>
+EnableGlobalCopies("join-globalcopies",
+ cl::desc("Coalesce copies that span blocks (default=subtarget)"),
+ cl::init(cl::BOU_UNSET), cl::Hidden);
+
static cl::opt<bool>
VerifyCoalescing("verify-coalescing",
cl::desc("Verify machine instrs before and after register coalescing"),
cl::Hidden);
-// Temporary option for testing new coalescer algo.
-static cl::opt<bool>
-NewCoalescer("new-coalescer", cl::Hidden,
- cl::desc("Use new coalescer algorithm"));
-
namespace {
class RegisterCoalescer : public MachineFunctionPass,
private LiveRangeEdit::Delegate {
const TargetRegisterInfo* TRI;
const TargetInstrInfo* TII;
LiveIntervals *LIS;
- LiveDebugVariables *LDV;
const MachineLoopInfo* Loops;
AliasAnalysis *AA;
RegisterClassInfo RegClassInfo;
- /// WorkList - Copy instructions yet to be coalesced.
+ /// \brief True if the coalescer should aggressively coalesce global copies
+ /// in favor of keeping local copies.
+ bool JoinGlobalCopies;
+
+ /// \brief True if the coalescer should aggressively coalesce fall-thru
+ /// blocks exclusively containing copies.
+ bool JoinSplitEdges;
+
+ /// Copy instructions yet to be coalesced.
SmallVector<MachineInstr*, 8> WorkList;
+ SmallVector<MachineInstr*, 8> LocalWorkList;
- /// ErasedInstrs - Set of instruction pointers that have been erased, and
+ /// Set of instruction pointers that have been erased, and
/// that may be present in WorkList.
SmallPtrSet<MachineInstr*, 8> ErasedInstrs;
void eliminateDeadDefs();
/// LiveRangeEdit callback.
- void LRE_WillEraseInstruction(MachineInstr *MI);
+ void LRE_WillEraseInstruction(MachineInstr *MI) override;
- /// joinAllIntervals - join compatible live intervals
+ /// Coalesce the LocalWorkList.
+ void coalesceLocals();
+
+ /// Join compatible live intervals
void joinAllIntervals();
- /// copyCoalesceInMBB - Coalesce copies in the specified MBB, putting
+ /// Coalesce copies in the specified MBB, putting
/// copies that cannot yet be coalesced into WorkList.
void copyCoalesceInMBB(MachineBasicBlock *MBB);
- /// copyCoalesceWorkList - Try to coalesce all copies in WorkList after
- /// position From. Return true if any progress was made.
- bool copyCoalesceWorkList(unsigned From = 0);
+ /// Try to coalesce all copies in CurrList. Return
+ /// true if any progress was made.
+ bool copyCoalesceWorkList(MutableArrayRef<MachineInstr*> CurrList);
- /// joinCopy - Attempt to join intervals corresponding to SrcReg/DstReg,
+ /// Attempt to join intervals corresponding to SrcReg/DstReg,
/// which are the src/dst of the copy instruction CopyMI. This returns
/// true if the copy was successfully coalesced away. If it is not
/// currently possible to coalesce this interval, but it may be possible if
/// 'Again'.
bool joinCopy(MachineInstr *TheCopy, bool &Again);
- /// joinIntervals - Attempt to join these two intervals. On failure, this
+ /// Attempt to join these two intervals. On failure, this
/// returns false. The output "SrcInt" will not have been modified, so we
/// can use this information below to update aliases.
bool joinIntervals(CoalescerPair &CP);
/// Attempt joining with a reserved physreg.
bool joinReservedPhysReg(CoalescerPair &CP);
- /// adjustCopiesBackFrom - We found a non-trivially-coalescable copy. If
+ /// We found a non-trivially-coalescable copy. If
/// the source value number is defined by a copy from the destination reg
/// see if we can merge these two destination reg valno# into a single
/// value number, eliminating a copy.
bool adjustCopiesBackFrom(const CoalescerPair &CP, MachineInstr *CopyMI);
- /// hasOtherReachingDefs - Return true if there are definitions of IntB
+ /// Return true if there are definitions of IntB
/// other than BValNo val# that can reach uses of AValno val# of IntA.
bool hasOtherReachingDefs(LiveInterval &IntA, LiveInterval &IntB,
VNInfo *AValNo, VNInfo *BValNo);
- /// removeCopyByCommutingDef - We found a non-trivially-coalescable copy.
+ /// We found a non-trivially-coalescable copy.
/// If the source value number is defined by a commutable instruction and
/// its other operand is coalesced to the copy dest register, see if we
/// can transform the copy into a noop by commuting the definition.
bool removeCopyByCommutingDef(const CoalescerPair &CP,MachineInstr *CopyMI);
- /// reMaterializeTrivialDef - If the source of a copy is defined by a
+ /// If the source of a copy is defined by a
/// trivial computation, replace the copy by rematerialize the definition.
- bool reMaterializeTrivialDef(LiveInterval &SrcInt, unsigned DstReg,
- MachineInstr *CopyMI);
+ bool reMaterializeTrivialDef(CoalescerPair &CP, MachineInstr *CopyMI,
+ bool &IsDefCopy);
- /// canJoinPhys - Return true if a physreg copy should be joined.
- bool canJoinPhys(CoalescerPair &CP);
+ /// Return true if a physreg copy should be joined.
+ bool canJoinPhys(const CoalescerPair &CP);
- /// updateRegDefsUses - Replace all defs and uses of SrcReg to DstReg and
+ /// Replace all defs and uses of SrcReg to DstReg and
/// update the subregister number if it is not zero. If DstReg is a
/// physical register and the existing subregister number of the def / use
/// being updated is not zero, make sure to set it to the correct physical
/// subregister.
void updateRegDefsUses(unsigned SrcReg, unsigned DstReg, unsigned SubIdx);
- /// eliminateUndefCopy - Handle copies of undef values.
+ /// Handle copies of undef values.
bool eliminateUndefCopy(MachineInstr *CopyMI, const CoalescerPair &CP);
public:
initializeRegisterCoalescerPass(*PassRegistry::getPassRegistry());
}
- virtual void getAnalysisUsage(AnalysisUsage &AU) const;
+ void getAnalysisUsage(AnalysisUsage &AU) const override;
- virtual void releaseMemory();
+ void releaseMemory() override;
- /// runOnMachineFunction - pass entry point
- virtual bool runOnMachineFunction(MachineFunction&);
+ /// This is the pass entry point.
+ bool runOnMachineFunction(MachineFunction&) override;
- /// print - Implement the dump method.
- virtual void print(raw_ostream &O, const Module* = 0) const;
+ /// Implement the dump method.
+ void print(raw_ostream &O, const Module* = nullptr) const override;
};
} /// end anonymous namespace
INITIALIZE_PASS_BEGIN(RegisterCoalescer, "simple-register-coalescing",
"Simple Register Coalescing", false, false)
INITIALIZE_PASS_DEPENDENCY(LiveIntervals)
-INITIALIZE_PASS_DEPENDENCY(LiveDebugVariables)
INITIALIZE_PASS_DEPENDENCY(SlotIndexes)
INITIALIZE_PASS_DEPENDENCY(MachineLoopInfo)
INITIALIZE_AG_DEPENDENCY(AliasAnalysis)
char RegisterCoalescer::ID = 0;
-static unsigned compose(const TargetRegisterInfo &tri, unsigned a, unsigned b) {
- if (!a) return b;
- if (!b) return a;
- return tri.composeSubRegIndices(a, b);
-}
-
static bool isMoveInstr(const TargetRegisterInfo &tri, const MachineInstr *MI,
unsigned &Src, unsigned &Dst,
unsigned &SrcSub, unsigned &DstSub) {
SrcSub = MI->getOperand(1).getSubReg();
} else if (MI->isSubregToReg()) {
Dst = MI->getOperand(0).getReg();
- DstSub = compose(tri, MI->getOperand(0).getSubReg(),
- MI->getOperand(3).getImm());
+ DstSub = tri.composeSubRegIndices(MI->getOperand(0).getSubReg(),
+ MI->getOperand(3).getImm());
Src = MI->getOperand(2).getReg();
SrcSub = MI->getOperand(2).getSubReg();
} else
@@ -228,10 +232,26 @@ static bool isMoveInstr(const TargetRegisterInfo &tri, const MachineInstr *MI,
return true;
}
+// Return true if this block should be vacated by the coalescer to eliminate
+// branches. The important cases to handle in the coalescer are critical edges
+// split during phi elimination which contain only copies. Simple blocks that
+// contain non-branches should also be vacated, but this can be handled by an
+// earlier pass similar to early if-conversion.
+static bool isSplitEdge(const MachineBasicBlock *MBB) {
+ if (MBB->pred_size() != 1 || MBB->succ_size() != 1)
+ return false;
+
+ for (const auto &MI : *MBB) {
+ if (!MI.isCopyLike() && !MI.isUnconditionalBranch())
+ return false;
+ }
+ return true;
+}
+
bool CoalescerPair::setRegisters(const MachineInstr *MI) {
SrcReg = DstReg = 0;
SrcIdx = DstIdx = 0;
- NewRC = 0;
+ NewRC = nullptr;
Flipped = CrossClass = false;
unsigned Src, Dst, SrcSub, DstSub;
if (SrcSub) {
Dst = TRI.getMatchingSuperReg(Dst, SrcSub, MRI.getRegClass(Src));
if (!Dst) return false;
- SrcSub = 0;
} else if (!MRI.getRegClass(Src)->contains(Dst)) {
return false;
}
if (DstReg != Dst)
return false;
// Registers match, do the subregisters line up?
- return compose(TRI, SrcIdx, SrcSub) == compose(TRI, DstIdx, DstSub);
+ return TRI.composeSubRegIndices(SrcIdx, SrcSub) ==
+ TRI.composeSubRegIndices(DstIdx, DstSub);
}
}
AU.addRequired<AliasAnalysis>();
AU.addRequired<LiveIntervals>();
AU.addPreserved<LiveIntervals>();
- AU.addRequired<LiveDebugVariables>();
- AU.addPreserved<LiveDebugVariables>();
AU.addPreserved<SlotIndexes>();
AU.addRequired<MachineLoopInfo>();
AU.addPreserved<MachineLoopInfo>();
}
void RegisterCoalescer::eliminateDeadDefs() {
- SmallVector<LiveInterval*, 8> NewRegs;
- LiveRangeEdit(0, NewRegs, *MF, *LIS, 0, this).eliminateDeadDefs(DeadDefs);
+ SmallVector<unsigned, 8> NewRegs;
+ LiveRangeEdit(nullptr, NewRegs, *MF, *LIS,
+ nullptr, this).eliminateDeadDefs(DeadDefs);
}
// Callback from eliminateDeadDefs().
ErasedInstrs.insert(MI);
}
-/// adjustCopiesBackFrom - We found a non-trivially-coalescable copy with IntA
+/// We found a non-trivially-coalescable copy with IntA
/// being the source and IntB being the dest, thus this defines a value number
/// in IntB. If the source value number (in IntA) is defined by a copy from B,
/// see if we can merge these two pieces of B into a single value number,
LIS->getInterval(CP.isFlipped() ? CP.getSrcReg() : CP.getDstReg());
SlotIndex CopyIdx = LIS->getInstructionIndex(CopyMI).getRegSlot();
- // BValNo is a value number in B that is defined by a copy from A. 'B3' in
+ // BValNo is a value number in B that is defined by a copy from A. 'B1' in
// the example above.
- LiveInterval::iterator BLR = IntB.FindLiveRangeContaining(CopyIdx);
- if (BLR == IntB.end()) return false;
- VNInfo *BValNo = BLR->valno;
+ LiveInterval::iterator BS = IntB.FindSegmentContaining(CopyIdx);
+ if (BS == IntB.end()) return false;
+ VNInfo *BValNo = BS->valno;
// Get the location that B is defined at. Two options: either this value has
// an unknown definition point or it is defined at CopyIdx. If unknown, we
// AValNo is the value number in A that defines the copy, A3 in the example.
SlotIndex CopyUseIdx = CopyIdx.getRegSlot(true);
- LiveInterval::iterator ALR = IntA.FindLiveRangeContaining(CopyUseIdx);
- // The live range might not exist after fun with physreg coalescing.
- if (ALR == IntA.end()) return false;
- VNInfo *AValNo = ALR->valno;
+ LiveInterval::iterator AS = IntA.FindSegmentContaining(CopyUseIdx);
+ // The live segment might not exist after fun with physreg coalescing.
+ if (AS == IntA.end()) return false;
+ VNInfo *AValNo = AS->valno;
// If AValNo is defined as a copy from IntB, we can potentially process this.
// Get the instruction that defines this value number.
MachineInstr *ACopyMI = LIS->getInstructionFromIndex(AValNo->def);
- if (!CP.isCoalescable(ACopyMI))
+ // Don't allow any partial copies, even if isCoalescable() allows them.
+ if (!CP.isCoalescable(ACopyMI) || !ACopyMI->isFullCopy())
return false;
- // Get the LiveRange in IntB that this value number starts with.
- LiveInterval::iterator ValLR =
- IntB.FindLiveRangeContaining(AValNo->def.getPrevSlot());
- if (ValLR == IntB.end())
+ // Get the Segment in IntB that this value number starts with.
+ LiveInterval::iterator ValS =
+ IntB.FindSegmentContaining(AValNo->def.getPrevSlot());
+ if (ValS == IntB.end())
return false;
- // Make sure that the end of the live range is inside the same block as
+ // Make sure that the end of the live segment is inside the same block as
// CopyMI.
- MachineInstr *ValLREndInst =
- LIS->getInstructionFromIndex(ValLR->end.getPrevSlot());
- if (!ValLREndInst || ValLREndInst->getParent() != CopyMI->getParent())
+ MachineInstr *ValSEndInst =
+ LIS->getInstructionFromIndex(ValS->end.getPrevSlot());
+ if (!ValSEndInst || ValSEndInst->getParent() != CopyMI->getParent())
return false;
- // Okay, we now know that ValLR ends in the same block that the CopyMI
- // live-range starts. If there are no intervening live ranges between them in
- // IntB, we can merge them.
- if (ValLR+1 != BLR) return false;
+ // Okay, we now know that ValS ends in the same block that the CopyMI
+ // live-range starts. If there are no intervening live segments between them
+ // in IntB, we can merge them.
+ if (ValS+1 != BS) return false;
DEBUG(dbgs() << "Extending: " << PrintReg(IntB.reg, TRI));
- SlotIndex FillerStart = ValLR->end, FillerEnd = BLR->start;
+ SlotIndex FillerStart = ValS->end, FillerEnd = BS->start;
// We are about to delete CopyMI, so need to remove it as the 'instruction
// that defines this value #'. Update the valnum with the new defining
// instruction #.
BValNo->def = FillerStart;
// Okay, we can merge them. We need to insert a new liverange:
- // [ValLR.end, BLR.begin) of either value number, then we merge the
+ // [ValS.end, BS.begin) of either value number, then we merge the
// two value numbers.
- IntB.addRange(LiveRange(FillerStart, FillerEnd, BValNo));
+ IntB.addSegment(LiveInterval::Segment(FillerStart, FillerEnd, BValNo));
// Okay, merge "B1" into the same value number as "B0".
- if (BValNo != ValLR->valno)
- IntB.MergeValueNumberInto(BValNo, ValLR->valno);
+ if (BValNo != ValS->valno)
+ IntB.MergeValueNumberInto(BValNo, ValS->valno);
DEBUG(dbgs() << " result = " << IntB << '\n');
// If the source instruction was killing the source register before the
// merge, unset the isKill marker given the live range has been extended.
- int UIdx = ValLREndInst->findRegisterUseOperandIdx(IntB.reg, true);
+ int UIdx = ValSEndInst->findRegisterUseOperandIdx(IntB.reg, true);
if (UIdx != -1) {
- ValLREndInst->getOperand(UIdx).setIsKill(false);
+ ValSEndInst->getOperand(UIdx).setIsKill(false);
}
// Rewrite the copy. If the copy instruction was killing the destination
// register before the merge, find the last use and trim the live range. That
// will also add the isKill marker.
CopyMI->substituteRegister(IntA.reg, IntB.reg, 0, *TRI);
- if (ALR->end == CopyIdx)
+ if (AS->end == CopyIdx)
LIS->shrinkToUses(&IntA);
++numExtends;
return true;
}
-/// hasOtherReachingDefs - Return true if there are definitions of IntB
+/// Return true if there are definitions of IntB
/// other than BValNo val# that can reach uses of AValno val# of IntA.
bool RegisterCoalescer::hasOtherReachingDefs(LiveInterval &IntA,
LiveInterval &IntB,
for (LiveInterval::iterator AI = IntA.begin(), AE = IntA.end();
AI != AE; ++AI) {
if (AI->valno != AValNo) continue;
- LiveInterval::Ranges::iterator BI =
- std::upper_bound(IntB.ranges.begin(), IntB.ranges.end(), AI->start);
- if (BI != IntB.ranges.begin())
+ LiveInterval::iterator BI =
+ std::upper_bound(IntB.begin(), IntB.end(), AI->start);
+ if (BI != IntB.begin())
--BI;
- for (; BI != IntB.ranges.end() && AI->end >= BI->start; ++BI) {
+ for (; BI != IntB.end() && AI->end >= BI->start; ++BI) {
if (BI->valno == BValNo)
continue;
if (BI->start <= AI->start && BI->end > AI->start)
return false;
}
-/// removeCopyByCommutingDef - We found a non-trivially-coalescable copy with
+/// We found a non-trivially-coalescable copy with
/// IntA being the source and IntB being the dest, thus this defines a value
/// number in IntB. If the source value number (in IntA) is defined by a
/// commutable instruction and its other operand is coalesced to the copy dest
LiveInterval &IntB =
LIS->getInterval(CP.isFlipped() ? CP.getSrcReg() : CP.getDstReg());
- // BValNo is a value number in B that is defined by a copy from A. 'B3' in
+ // BValNo is a value number in B that is defined by a copy from A. 'B1' in
// the example above.
VNInfo *BValNo = IntB.getVNInfoAt(CopyIdx);
if (!BValNo || BValNo->def != CopyIdx)
return false;
- assert(BValNo->def == CopyIdx && "Copy doesn't define the value?");
-
// AValNo is the value number in A that defines the copy, A3 in the example.
VNInfo *AValNo = IntA.getVNInfoAt(CopyIdx.getRegSlot(true));
assert(AValNo && "COPY source not live");
MachineOperand &NewDstMO = DefMI->getOperand(NewDstIdx);
unsigned NewReg = NewDstMO.getReg();
- if (NewReg != IntB.reg || !LiveRangeQuery(IntB, AValNo->def).isKill())
+ if (NewReg != IntB.reg || !IntB.Query(AValNo->def).isKill())
return false;
// Make sure there are no other definitions of IntB that would reach the
// If some of the uses of IntA.reg is already coalesced away, return false.
// It's not possible to determine whether it's safe to perform the coalescing.
- for (MachineRegisterInfo::use_nodbg_iterator UI =
- MRI->use_nodbg_begin(IntA.reg),
- UE = MRI->use_nodbg_end(); UI != UE; ++UI) {
- MachineInstr *UseMI = &*UI;
+ for (MachineOperand &MO : MRI->use_nodbg_operands(IntA.reg)) {
+ MachineInstr *UseMI = MO.getParent();
+ unsigned OpNo = &MO - &UseMI->getOperand(0);
SlotIndex UseIdx = LIS->getInstructionIndex(UseMI);
- LiveInterval::iterator ULR = IntA.FindLiveRangeContaining(UseIdx);
- if (ULR == IntA.end() || ULR->valno != AValNo)
+ LiveInterval::iterator US = IntA.FindSegmentContaining(UseIdx);
+ if (US == IntA.end() || US->valno != AValNo)
continue;
// If this use is tied to a def, we can't rewrite the register.
- if (UseMI->isRegTiedToDefOperand(UI.getOperandNo()))
+ if (UseMI->isRegTiedToDefOperand(OpNo))
return false;
}
// Update uses of IntA of the specific Val# with IntB.
for (MachineRegisterInfo::use_iterator UI = MRI->use_begin(IntA.reg),
UE = MRI->use_end(); UI != UE;) {
- MachineOperand &UseMO = UI.getOperand();
- MachineInstr *UseMI = &*UI;
+ MachineOperand &UseMO = *UI;
+ MachineInstr *UseMI = UseMO.getParent();
++UI;
if (UseMI->isDebugValue()) {
// FIXME These don't have an instruction index. Not clear we have enough
continue;
}
SlotIndex UseIdx = LIS->getInstructionIndex(UseMI).getRegSlot(true);
- LiveInterval::iterator ULR = IntA.FindLiveRangeContaining(UseIdx);
- if (ULR == IntA.end() || ULR->valno != AValNo)
+ LiveInterval::iterator US = IntA.FindSegmentContaining(UseIdx);
+ if (US == IntA.end() || US->valno != AValNo)
continue;
// Kill flags are no longer accurate. They are recomputed after RA.
UseMO.setIsKill(false);
UseMI->eraseFromParent();
}
- // Extend BValNo by merging in IntA live ranges of AValNo. Val# definition
+ // Extend BValNo by merging in IntA live segments of AValNo. Val# definition
// is updated.
VNInfo *ValNo = BValNo;
ValNo->def = AValNo->def;
for (LiveInterval::iterator AI = IntA.begin(), AE = IntA.end();
AI != AE; ++AI) {
if (AI->valno != AValNo) continue;
- IntB.addRange(LiveRange(AI->start, AI->end, ValNo));
+ IntB.addSegment(LiveInterval::Segment(AI->start, AI->end, ValNo));
}
DEBUG(dbgs() << "\t\textended: " << IntB << '\n');
return true;
}
-/// reMaterializeTrivialDef - If the source of a copy is defined by a trivial
+/// If the source of a copy is defined by a trivial
/// computation, replace the copy by rematerialize the definition.
-bool RegisterCoalescer::reMaterializeTrivialDef(LiveInterval &SrcInt,
- unsigned DstReg,
- MachineInstr *CopyMI) {
- SlotIndex CopyIdx = LIS->getInstructionIndex(CopyMI).getRegSlot(true);
- LiveInterval::iterator SrcLR = SrcInt.FindLiveRangeContaining(CopyIdx);
- assert(SrcLR != SrcInt.end() && "Live range not found!");
- VNInfo *ValNo = SrcLR->valno;
+bool RegisterCoalescer::reMaterializeTrivialDef(CoalescerPair &CP,
+ MachineInstr *CopyMI,
+ bool &IsDefCopy) {
+ IsDefCopy = false;
+ unsigned SrcReg = CP.isFlipped() ? CP.getDstReg() : CP.getSrcReg();
+ unsigned SrcIdx = CP.isFlipped() ? CP.getDstIdx() : CP.getSrcIdx();
+ unsigned DstReg = CP.isFlipped() ? CP.getSrcReg() : CP.getDstReg();
+ unsigned DstIdx = CP.isFlipped() ? CP.getSrcIdx() : CP.getDstIdx();
+ if (TargetRegisterInfo::isPhysicalRegister(SrcReg))
+ return false;
+
+ LiveInterval &SrcInt = LIS->getInterval(SrcReg);
+ SlotIndex CopyIdx = LIS->getInstructionIndex(CopyMI);
+ VNInfo *ValNo = SrcInt.Query(CopyIdx).valueIn();
+ assert(ValNo && "CopyMI input register not live");
if (ValNo->isPHIDef() || ValNo->isUnused())
return false;
MachineInstr *DefMI = LIS->getInstructionFromIndex(ValNo->def);
if (!DefMI)
return false;
- assert(DefMI && "Defining instruction disappeared");
- if (!DefMI->isAsCheapAsAMove())
+ if (DefMI->isCopyLike()) {
+ IsDefCopy = true;
+ return false;
+ }
+ if (!TII->isAsCheapAsAMove(DefMI))
return false;
if (!TII->isTriviallyReMaterializable(DefMI, AA))
return false;
const MCInstrDesc &MCID = DefMI->getDesc();
if (MCID.getNumDefs() != 1)
return false;
+ // Only support subregister destinations when the def is read-undef.
+ MachineOperand &DstOperand = CopyMI->getOperand(0);
+ unsigned CopyDstReg = DstOperand.getReg();
+ if (DstOperand.getSubReg() && !DstOperand.isUndef())
+ return false;
+
+ // If both SrcIdx and DstIdx are set, correct rematerialization would widen
+ // the register substantially (beyond both source and dest size). This is bad
+ // for performance since it can cascade through a function, introducing many
+ // extra spills and fills (e.g. ARM can easily end up copying QQQQPR registers
+ // around after a few subreg copies).
+ if (SrcIdx && DstIdx)
+ return false;
+
+ const TargetRegisterClass *DefRC = TII->getRegClass(MCID, 0, TRI, *MF);
if (!DefMI->isImplicitDef()) {
- // Make sure the copy destination register class fits the instruction
- // definition register class. The mismatch can happen as a result of earlier
- // extract_subreg, insert_subreg, subreg_to_reg coalescing.
- const TargetRegisterClass *RC = TII->getRegClass(MCID, 0, TRI, *MF);
- if (TargetRegisterInfo::isVirtualRegister(DstReg)) {
- if (MRI->getRegClass(DstReg) != RC)
+ if (TargetRegisterInfo::isPhysicalRegister(DstReg)) {
+ unsigned NewDstReg = DstReg;
+
+ unsigned NewDstIdx = TRI->composeSubRegIndices(CP.getSrcIdx(),
+ DefMI->getOperand(0).getSubReg());
+ if (NewDstIdx)
+ NewDstReg = TRI->getSubReg(DstReg, NewDstIdx);
+
+ // Finally, make sure that the physical subregister that will be
+ // constructed later is permitted for the instruction.
+ if (!DefRC->contains(NewDstReg))
return false;
- } else if (!RC->contains(DstReg))
- return false;
+ } else {
+ // Theoretically, some stack frame reference could exist. Just make sure
+ // it hasn't actually happened.
+ assert(TargetRegisterInfo::isVirtualRegister(DstReg) &&
+ "Only expect to deal with virtual or physical registers");
+ }
}
MachineBasicBlock *MBB = CopyMI->getParent();
MachineBasicBlock::iterator MII =
- llvm::next(MachineBasicBlock::iterator(CopyMI));
- TII->reMaterialize(*MBB, MII, DstReg, 0, DefMI, *TRI);
- MachineInstr *NewMI = prior(MII);
+ std::next(MachineBasicBlock::iterator(CopyMI));
+ TII->reMaterialize(*MBB, MII, DstReg, SrcIdx, DefMI, *TRI);
+ MachineInstr *NewMI = std::prev(MII);
+
+ LIS->ReplaceMachineInstrInMaps(CopyMI, NewMI);
+ CopyMI->eraseFromParent();
+ ErasedInstrs.insert(CopyMI);
// NewMI may have dead implicit defs (E.g. EFLAGS for MOV<bits>r0 on X86).
// We need to remember these so we can add intervals once we insert
}
}
+ if (TargetRegisterInfo::isVirtualRegister(DstReg)) {
+ const TargetRegisterClass *NewRC = CP.getNewRC();
+ unsigned NewIdx = NewMI->getOperand(0).getSubReg();
+
+ if (NewIdx)
+ NewRC = TRI->getMatchingSuperRegClass(NewRC, DefRC, NewIdx);
+ else
+ NewRC = TRI->getCommonSubClass(NewRC, DefRC);
+
+ assert(NewRC && "subreg chosen for remat incompatible with instruction");
+ MRI->setRegClass(DstReg, NewRC);
+
+ updateRegDefsUses(DstReg, DstReg, DstIdx);
+ NewMI->getOperand(0).setSubReg(NewIdx);
+ } else if (NewMI->getOperand(0).getReg() != CopyDstReg) {
+ // The New instruction may be defining a sub-register of what's actually
+ // been asked for. If so it must implicitly define the whole thing.
+ assert(TargetRegisterInfo::isPhysicalRegister(DstReg) &&
+ "Only expect virtual or physical registers in remat");
+ NewMI->getOperand(0).setIsDead(true);
+ NewMI->addOperand(MachineOperand::CreateReg(CopyDstReg,
+ true /*IsDef*/,
+ true /*IsImp*/,
+ false /*IsKill*/));
+ // Record small dead def live-ranges for all the subregisters
+ // of the destination register.
+ // Otherwise, variables that live through may miss some
+ // interferences, thus creating invalid allocation.
+ // E.g., i386 code:
+ // vreg1 = somedef ; vreg1 GR8
+ // vreg2 = remat ; vreg2 GR32
+ // CL = COPY vreg2.sub_8bit
+ // = somedef vreg1 ; vreg1 GR8
+ // =>
+ // vreg1 = somedef ; vreg1 GR8
+ // ECX<def, dead> = remat ; CL<imp-def>
+ // = somedef vreg1 ; vreg1 GR8
+ // vreg1 will see the inteferences with CL but not with CH since
+ // no live-ranges would have been created for ECX.
+ // Fix that!
+ SlotIndex NewMIIdx = LIS->getInstructionIndex(NewMI);
+ for (MCRegUnitIterator Units(NewMI->getOperand(0).getReg(), TRI);
+ Units.isValid(); ++Units)
+ if (LiveRange *LR = LIS->getCachedRegUnit(*Units))
+ LR->createDeadDef(NewMIIdx.getRegSlot(), LIS->getVNInfoAllocator());
+ }
+
+ if (NewMI->getOperand(0).getSubReg())
+ NewMI->getOperand(0).setIsUndef();
+
// CopyMI may have implicit operands, transfer them over to the newly
// rematerialized instruction. And update implicit def interval valnos.
for (unsigned i = CopyMI->getDesc().getNumOperands(),
}
}
- LIS->ReplaceMachineInstrInMaps(CopyMI, NewMI);
-
SlotIndex NewMIIdx = LIS->getInstructionIndex(NewMI);
for (unsigned i = 0, e = NewMIImplDefs.size(); i != e; ++i) {
unsigned Reg = NewMIImplDefs[i];
for (MCRegUnitIterator Units(Reg, TRI); Units.isValid(); ++Units)
- if (LiveInterval *LI = LIS->getCachedRegUnit(*Units))
- LI->createDeadDef(NewMIIdx.getRegSlot(), LIS->getVNInfoAllocator());
+ if (LiveRange *LR = LIS->getCachedRegUnit(*Units))
+ LR->createDeadDef(NewMIIdx.getRegSlot(), LIS->getVNInfoAllocator());
}
- CopyMI->eraseFromParent();
- ErasedInstrs.insert(CopyMI);
DEBUG(dbgs() << "Remat: " << *NewMI);
++NumReMats;
// The source interval can become smaller because we removed a use.
LIS->shrinkToUses(&SrcInt, &DeadDefs);
- if (!DeadDefs.empty())
+ if (!DeadDefs.empty()) {
+ // If the virtual SrcReg is completely eliminated, update all DBG_VALUEs
+ // to describe DstReg instead.
+ for (MachineOperand &UseMO : MRI->use_operands(SrcReg)) {
+ MachineInstr *UseMI = UseMO.getParent();
+ if (UseMI->isDebugValue()) {
+ UseMO.setReg(DstReg);
+ DEBUG(dbgs() << "\t\tupdated: " << *UseMI);
+ }
+ }
eliminateDeadDefs();
+ }
return true;
}
-/// eliminateUndefCopy - ProcessImpicitDefs may leave some copies of <undef>
+/// ProcessImpicitDefs may leave some copies of <undef>
/// values, it only removes local variables. When we have a copy like:
///
/// %vreg1 = COPY %vreg2<undef>
// No intervals are live-in to CopyMI - it is undef.
if (CP.isFlipped())
DstInt = SrcInt;
- SrcInt = 0;
+ SrcInt = nullptr;
VNInfo *DeadVNI = DstInt->getVNInfoAt(Idx.getRegSlot());
assert(DeadVNI && "No value defined in DstInt");
DstInt->removeValNo(DeadVNI);
// Find new undef uses.
- for (MachineRegisterInfo::reg_nodbg_iterator
- I = MRI->reg_nodbg_begin(DstInt->reg), E = MRI->reg_nodbg_end();
- I != E; ++I) {
- MachineOperand &MO = I.getOperand();
+ for (MachineOperand &MO : MRI->reg_nodbg_operands(DstInt->reg)) {
if (MO.isDef() || MO.isUndef())
continue;
MachineInstr *MI = MO.getParent();
return true;
}
-/// updateRegDefsUses - Replace all defs and uses of SrcReg to DstReg and
-/// update the subregister number if it is not zero. If DstReg is a
-/// physical register and the existing subregister number of the def / use
-/// being updated is not zero, make sure to set it to the correct physical
-/// subregister.
+/// Replace all defs and uses of SrcReg to DstReg and update the subregister
+/// number if it is not zero. If DstReg is a physical register and the existing
+/// subregister number of the def / use being updated is not zero, make sure to
+/// set it to the correct physical subregister.
void RegisterCoalescer::updateRegDefsUses(unsigned SrcReg,
unsigned DstReg,
unsigned SubIdx) {
bool DstIsPhys = TargetRegisterInfo::isPhysicalRegister(DstReg);
- LiveInterval *DstInt = DstIsPhys ? 0 : &LIS->getInterval(DstReg);
-
- // Update LiveDebugVariables.
- LDV->renameRegister(SrcReg, DstReg, SubIdx);
+ LiveInterval *DstInt = DstIsPhys ? nullptr : &LIS->getInterval(DstReg);
+
+ SmallPtrSet<MachineInstr*, 8> Visited;
+ for (MachineRegisterInfo::reg_instr_iterator
+ I = MRI->reg_instr_begin(SrcReg), E = MRI->reg_instr_end();
+ I != E; ) {
+ MachineInstr *UseMI = &*(I++);
+
+ // Each instruction can only be rewritten once because sub-register
+ // composition is not always idempotent. When SrcReg != DstReg, rewriting
+ // the UseMI operands removes them from the SrcReg use-def chain, but when
+ // SrcReg is DstReg we could encounter UseMI twice if it has multiple
+ // operands mentioning the virtual register.
+ if (SrcReg == DstReg && !Visited.insert(UseMI).second)
+ continue;
- for (MachineRegisterInfo::reg_iterator I = MRI->reg_begin(SrcReg);
- MachineInstr *UseMI = I.skipInstruction();) {
SmallVector<unsigned,8> Ops;
bool Reads, Writes;
- tie(Reads, Writes) = UseMI->readsWritesVirtualRegister(SrcReg, &Ops);
+ std::tie(Reads, Writes) = UseMI->readsWritesVirtualRegister(SrcReg, &Ops);
// If SrcReg wasn't read, it may still be the case that DstReg is live-in
// because SrcReg is a sub-register.
}
}
-/// canJoinPhys - Return true if a copy involving a physreg should be joined.
-bool RegisterCoalescer::canJoinPhys(CoalescerPair &CP) {
+/// Return true if a copy involving a physreg should be joined.
+bool RegisterCoalescer::canJoinPhys(const CoalescerPair &CP) {
/// Always join simple intervals that are defined by a single copy from a
/// reserved register. This doesn't increase register pressure, so it is
/// always beneficial.
- if (!RegClassInfo.isReserved(CP.getDstReg())) {
+ if (!MRI->isReserved(CP.getDstReg())) {
DEBUG(dbgs() << "\tCan only merge into reserved registers.\n");
return false;
}
return false;
}
-/// joinCopy - Attempt to join intervals corresponding to SrcReg/DstReg,
+/// Attempt to join intervals corresponding to SrcReg/DstReg,
/// which are the src/dst of the copy instruction CopyMI. This returns true
/// if the copy was successfully coalesced away. If it is not currently
/// possible to coalesce this interval, but it may be possible if other
return false;
}
+ if (CP.getNewRC()) {
+ auto SrcRC = MRI->getRegClass(CP.getSrcReg());
+ auto DstRC = MRI->getRegClass(CP.getDstReg());
+ unsigned SrcIdx = CP.getSrcIdx();
+ unsigned DstIdx = CP.getDstIdx();
+ if (CP.isFlipped()) {
+ std::swap(SrcIdx, DstIdx);
+ std::swap(SrcRC, DstRC);
+ }
+ if (!TRI->shouldCoalesce(CopyMI, SrcRC, SrcIdx, DstRC, DstIdx,
+ CP.getNewRC())) {
+ DEBUG(dbgs() << "\tSubtarget bailed on coalescing.\n");
+ return false;
+ }
+ }
+
// Dead code elimination. This really should be handled by MachineDCE, but
// sometimes dead copies slip through, and we can't generate invalid live
// ranges.
if (CP.getSrcReg() == CP.getDstReg()) {
LiveInterval &LI = LIS->getInterval(CP.getSrcReg());
DEBUG(dbgs() << "\tCopy already coalesced: " << LI << '\n');
- LiveRangeQuery LRQ(LI, LIS->getInstructionIndex(CopyMI));
+ LiveQueryResult LRQ = LI.Query(LIS->getInstructionIndex(CopyMI));
if (VNInfo *DefVNI = LRQ.valueDefined()) {
VNInfo *ReadVNI = LRQ.valueIn();
assert(ReadVNI && "No value before copy and no <undef> flag.");
if (!canJoinPhys(CP)) {
// Before giving up coalescing, if definition of source is defined by
// trivial computation, try rematerializing it.
- if (!CP.isFlipped() &&
- reMaterializeTrivialDef(LIS->getInterval(CP.getSrcReg()),
- CP.getDstReg(), CopyMI))
+ bool IsDefCopy;
+ if (reMaterializeTrivialDef(CP, CopyMI, IsDefCopy))
return true;
+ if (IsDefCopy)
+ Again = true; // May be possible to coalesce later.
return false;
}
} else {
+ // When possible, let DstReg be the larger interval.
+ if (!CP.isPartial() && LIS->getInterval(CP.getSrcReg()).size() >
+ LIS->getInterval(CP.getDstReg()).size())
+ CP.flip();
+
DEBUG({
- dbgs() << "\tConsidering merging to " << CP.getNewRC()->getName()
- << " with ";
+ dbgs() << "\tConsidering merging to "
+ << TRI->getRegClassName(CP.getNewRC()) << " with ";
if (CP.getDstIdx() && CP.getSrcIdx())
dbgs() << PrintReg(CP.getDstReg()) << " in "
<< TRI->getSubRegIndexName(CP.getDstIdx()) << " and "
dbgs() << PrintReg(CP.getSrcReg(), TRI) << " in "
<< PrintReg(CP.getDstReg(), TRI, CP.getSrcIdx()) << '\n';
});
-
- // When possible, let DstReg be the larger interval.
- if (!CP.isPartial() && LIS->getInterval(CP.getSrcReg()).ranges.size() >
- LIS->getInterval(CP.getDstReg()).ranges.size())
- CP.flip();
}
// Okay, attempt to join these two intervals. On failure, this returns false.
// If definition of source is defined by trivial computation, try
// rematerializing it.
- if (!CP.isFlipped() &&
- reMaterializeTrivialDef(LIS->getInterval(CP.getSrcReg()),
- CP.getDstReg(), CopyMI))
+ bool IsDefCopy;
+ if (reMaterializeTrivialDef(CP, CopyMI, IsDefCopy))
return true;
- // If we can eliminate the copy without merging the live ranges, do so now.
+ // If we can eliminate the copy without merging the live segments, do so
+ // now.
if (!CP.isPartial() && !CP.isPhys()) {
if (adjustCopiesBackFrom(CP, CopyMI) ||
removeCopyByCommutingDef(CP, CopyMI)) {
TRI->UpdateRegAllocHint(CP.getSrcReg(), CP.getDstReg(), *MF);
DEBUG({
- dbgs() << "\tJoined. Result = " << PrintReg(CP.getDstReg(), TRI);
- if (!CP.isPhys())
+ dbgs() << "\tSuccess: " << PrintReg(CP.getSrcReg(), TRI, CP.getSrcIdx())
+ << " -> " << PrintReg(CP.getDstReg(), TRI, CP.getDstIdx()) << '\n';
+ dbgs() << "\tResult = ";
+ if (CP.isPhys())
+ dbgs() << PrintReg(CP.getDstReg(), TRI);
+ else
dbgs() << LIS->getInterval(CP.getDstReg());
- dbgs() << '\n';
+ dbgs() << '\n';
});
++numJoins;
/// Attempt joining with a reserved physreg.
bool RegisterCoalescer::joinReservedPhysReg(CoalescerPair &CP) {
assert(CP.isPhys() && "Must be a physreg copy");
- assert(RegClassInfo.isReserved(CP.getDstReg()) && "Not a reserved register");
+ assert(MRI->isReserved(CP.getDstReg()) && "Not a reserved register");
LiveInterval &RHS = LIS->getInterval(CP.getSrcReg());
- DEBUG(dbgs() << "\t\tRHS = " << PrintReg(CP.getSrcReg()) << ' ' << RHS
- << '\n');
+ DEBUG(dbgs() << "\t\tRHS = " << RHS << '\n');
assert(CP.isFlipped() && RHS.containsOneValue() &&
"Invalid join with reserved register");
// Value in the other live range that overlaps this def, if any.
VNInfo *OtherVNI;
+ // Is this value an IMPLICIT_DEF that can be erased?
+ //
+ // IMPLICIT_DEF values should only exist at the end of a basic block that
+ // is a predecessor to a phi-value. These IMPLICIT_DEF instructions can be
+ // safely erased if they are overlapping a live value in the other live
+ // interval.
+ //
+ // Weird control flow graphs and incomplete PHI handling in
+ // ProcessImplicitDefs can very rarely create IMPLICIT_DEF values with
+ // longer live ranges. Such IMPLICIT_DEF values should be treated like
+ // normal values.
+ bool ErasableImplicitDef;
+
// True when the live range of this value will be pruned because of an
// overlapping CR_Replace value in the other live range.
bool Pruned;
bool PrunedComputed;
Val() : Resolution(CR_Keep), WriteLanes(0), ValidLanes(0),
- RedefVNI(0), OtherVNI(0), Pruned(false), PrunedComputed(false) {}
+ RedefVNI(nullptr), OtherVNI(nullptr), ErasableImplicitDef(false),
+ Pruned(false), PrunedComputed(false) {}
bool isAnalyzed() const { return WriteLanes != 0; }
};
/// Add erased instructions to ErasedInstrs.
/// Add foreign virtual registers to ShrinkRegs if their live range ended at
/// the erased instrs.
- void eraseInstrs(SmallPtrSet<MachineInstr*, 8> &ErasedInstrs,
+ void eraseInstrs(SmallPtrSetImpl<MachineInstr*> &ErasedInstrs,
SmallVectorImpl<unsigned> &ShrinkRegs);
/// Get the value assignments suitable for passing to LiveInterval::join.
- const int *getAssignments() const { return &Assignments[0]; }
+ const int *getAssignments() const { return Assignments.data(); }
};
} // end anonymous namespace
@@ -1315,7 +1466,8 @@ unsigned JoinVals::computeWriteLanes(const MachineInstr *DefMI, bool &Redef) {
for (ConstMIOperands MO(DefMI); MO.isValid(); ++MO) {
if (!MO->isReg() || MO->getReg() != LI.reg || !MO->isDef())
continue;
- L |= TRI->getSubRegIndexLaneMask(compose(*TRI, SubIdx, MO->getSubReg()));
+ L |= TRI->getSubRegIndexLaneMask(
+ TRI->composeSubRegIndices(SubIdx, MO->getSubReg()));
if (MO->readsReg())
Redef = true;
}
unsigned Reg = MI->getOperand(1).getReg();
if (!TargetRegisterInfo::isVirtualRegister(Reg))
break;
- LiveRangeQuery LRQ(LIS->getInterval(Reg), VNI->def);
+ LiveQueryResult LRQ = LIS->getInterval(Reg).Query(VNI->def);
if (!LRQ.valueIn())
break;
VNI = LRQ.valueIn();
}
// Get the instruction defining this value, compute the lanes written.
- const MachineInstr *DefMI = 0;
+ const MachineInstr *DefMI = nullptr;
if (VNI->isPHIDef()) {
// Conservatively assume that all lanes in a PHI are valid.
V.ValidLanes = V.WriteLanes = TRI->getSubRegIndexLaneMask(SubIdx);
// The <read-undef> flag on the def operand means that old lane values are
// not important.
if (Redef) {
- V.RedefVNI = LiveRangeQuery(LI, VNI->def).valueIn();
+ V.RedefVNI = LI.Query(VNI->def).valueIn();
assert(V.RedefVNI && "Instruction is reading nonexistent value");
computeAssignment(V.RedefVNI->id, Other);
V.ValidLanes |= Vals[V.RedefVNI->id].ValidLanes;
}
// An IMPLICIT_DEF writes undef values.
- if (DefMI->isImplicitDef())
+ if (DefMI->isImplicitDef()) {
+ // We normally expect IMPLICIT_DEF values to be live only until the end
+ // of their block. If the value is really live longer and gets pruned in
+ // another block, this flag is cleared again.
+ V.ErasableImplicitDef = true;
V.ValidLanes &= ~V.WriteLanes;
+ }
}
// Find the value in Other that overlaps VNI->def, if any.
- LiveRangeQuery OtherLRQ(Other.LI, VNI->def);
+ LiveQueryResult OtherLRQ = Other.LI.Query(VNI->def);
// It is possible that both values are defined by the same instruction, or
// the values are PHIs defined in the same block. When that happens, the two
// We have overlapping values, or possibly a kill of Other.
// Recursively compute assignments up the dominator tree.
Other.computeAssignment(V.OtherVNI->id, *this);
- const Val &OtherV = Other.Vals[V.OtherVNI->id];
+ Val &OtherV = Other.Vals[V.OtherVNI->id];
+
+ // Check if OtherV is an IMPLICIT_DEF that extends beyond its basic block.
+ // This shouldn't normally happen, but ProcessImplicitDefs can leave such
+ // IMPLICIT_DEF instructions behind, and there is nothing wrong with it
+ // technically.
+ //
+ // WHen it happens, treat that IMPLICIT_DEF as a normal value, and don't try
+ // to erase the IMPLICIT_DEF instruction.
+ if (OtherV.ErasableImplicitDef && DefMI &&
+ DefMI->getParent() != Indexes->getMBBFromIndex(V.OtherVNI->def)) {
+ DEBUG(dbgs() << "IMPLICIT_DEF defined at " << V.OtherVNI->def
+ << " extends into BB#" << DefMI->getParent()->getNumber()
+ << ", keeping it.\n");
+ OtherV.ErasableImplicitDef = false;
+ }
// Allow overlapping PHI values. Any real interference would show up in a
// predecessor, the PHI itself can't introduce any conflicts.
if ((V.WriteLanes & OtherV.ValidLanes) == 0)
return CR_Replace;
+ // If the other live range is killed by DefMI and the live ranges are still
+ // overlapping, it must be because we're looking at an early clobber def:
+ //
+ // %dst<def,early-clobber> = ASM %src<kill>
+ //
+ // In this case, it is illegal to merge the two live ranges since the early
+ // clobber def would clobber %src before it was read.
+ if (OtherLRQ.isKill()) {
+ // This case where the def doesn't overlap the kill is handled above.
+ assert(VNI->def.isEarlyClobber() &&
+ "Only early clobber defs can overlap a kill");
+ return CR_Impossible;
+ }
+
// VNI is clobbering live lanes in OtherVNI, but there is still the
// possibility that no instructions actually read the clobbered lanes.
// If we're clobbering all the lanes in OtherVNI, at least one must be read.
continue;
if (!MO->readsReg())
continue;
- if (Lanes &
- TRI->getSubRegIndexLaneMask(compose(*TRI, SubIdx, MO->getSubReg())))
+ if (Lanes & TRI->getSubRegIndexLaneMask(
+ TRI->composeSubRegIndices(SubIdx, MO->getSubReg())))
return true;
}
return false;
switch (Vals[i].Resolution) {
case CR_Keep:
break;
- case CR_Replace:
+ case CR_Replace: {
// This value takes precedence over the value in Other.LI.
LIS->pruneValue(&Other.LI, Def, &EndPoints);
+ // Check if we're replacing an IMPLICIT_DEF value. The IMPLICIT_DEF
+ // instructions are only inserted to provide a live-out value for PHI
+ // predecessors, so the instruction should simply go away once its value
+ // has been replaced.
+ Val &OtherV = Other.Vals[Vals[i].OtherVNI->id];
+ bool EraseImpDef = OtherV.ErasableImplicitDef &&
+ OtherV.Resolution == CR_Keep;
+ if (!Def.isBlock()) {
+ // Remove <def,read-undef> flags. This def is now a partial redef.
+ // Also remove <def,dead> flags since the joined live range will
+ // continue past this instruction.
+ for (MIOperands MO(Indexes->getInstructionFromIndex(Def));
+ MO.isValid(); ++MO)
+ if (MO->isReg() && MO->isDef() && MO->getReg() == LI.reg) {
+ MO->setIsUndef(EraseImpDef);
+ MO->setIsDead(false);
+ }
+ // This value will reach instructions below, but we need to make sure
+ // the live range also reaches the instruction at Def.
+ if (!EraseImpDef)
+ EndPoints.push_back(Def);
+ }
DEBUG(dbgs() << "\t\tpruned " << PrintReg(Other.LI.reg) << " at " << Def
<< ": " << Other.LI << '\n');
break;
+ }
case CR_Erase:
case CR_Merge:
if (isPrunedValue(i, Other)) {
}
}
-void JoinVals::eraseInstrs(SmallPtrSet<MachineInstr*, 8> &ErasedInstrs,
+void JoinVals::eraseInstrs(SmallPtrSetImpl<MachineInstr*> &ErasedInstrs,
SmallVectorImpl<unsigned> &ShrinkRegs) {
for (unsigned i = 0, e = LI.getNumValNums(); i != e; ++i) {
- if (Vals[i].Resolution != CR_Erase)
- continue;
+ // Get the def location before markUnused() below invalidates it.
SlotIndex Def = LI.getValNumInfo(i)->def;
- MachineInstr *MI = Indexes->getInstructionFromIndex(Def);
- assert(MI && "No instruction to erase");
- if (MI->isCopy()) {
- unsigned Reg = MI->getOperand(1).getReg();
- if (TargetRegisterInfo::isVirtualRegister(Reg) &&
- Reg != CP.getSrcReg() && Reg != CP.getDstReg())
- ShrinkRegs.push_back(Reg);
+ switch (Vals[i].Resolution) {
+ case CR_Keep:
+ // If an IMPLICIT_DEF value is pruned, it doesn't serve a purpose any
+ // longer. The IMPLICIT_DEF instructions are only inserted by
+ // PHIElimination to guarantee that all PHI predecessors have a value.
+ if (!Vals[i].ErasableImplicitDef || !Vals[i].Pruned)
+ break;
+ // Remove value number i from LI. Note that this VNInfo is still present
+ // in NewVNInfo, so it will appear as an unused value number in the final
+ // joined interval.
+ LI.getValNumInfo(i)->markUnused();
+ LI.removeValNo(LI.getValNumInfo(i));
+ DEBUG(dbgs() << "\t\tremoved " << i << '@' << Def << ": " << LI << '\n');
+ // FALL THROUGH.
+
+ case CR_Erase: {
+ MachineInstr *MI = Indexes->getInstructionFromIndex(Def);
+ assert(MI && "No instruction to erase");
+ if (MI->isCopy()) {
+ unsigned Reg = MI->getOperand(1).getReg();
+ if (TargetRegisterInfo::isVirtualRegister(Reg) &&
+ Reg != CP.getSrcReg() && Reg != CP.getDstReg())
+ ShrinkRegs.push_back(Reg);
+ }
+ ErasedInstrs.insert(MI);
+ DEBUG(dbgs() << "\t\terased:\t" << Def << '\t' << *MI);
+ LIS->RemoveMachineInstrFromMaps(MI);
+ MI->eraseFromParent();
+ break;
+ }
+ default:
+ break;
}
- ErasedInstrs.insert(MI);
- DEBUG(dbgs() << "\t\terased:\t" << Def << '\t' << *MI);
- LIS->RemoveMachineInstrFromMaps(MI);
- MI->eraseFromParent();
}
}
JoinVals RHSVals(RHS, CP.getSrcIdx(), NewVNInfo, CP, LIS, TRI);
JoinVals LHSVals(LHS, CP.getDstIdx(), NewVNInfo, CP, LIS, TRI);
- DEBUG(dbgs() << "\t\tRHS = " << PrintReg(CP.getSrcReg()) << ' ' << RHS
- << "\n\t\tLHS = " << PrintReg(CP.getDstReg()) << ' ' << LHS
+ DEBUG(dbgs() << "\t\tRHS = " << RHS
+ << "\n\t\tLHS = " << LHS
<< '\n');
// First compute NewVNInfo and the simple value mappings.
LIS->shrinkToUses(&LIS->getInterval(ShrinkRegs.pop_back_val()));
// Join RHS into LHS.
- LHS.join(RHS, LHSVals.getAssignments(), RHSVals.getAssignments(), NewVNInfo,
- MRI);
+ LHS.join(RHS, LHSVals.getAssignments(), RHSVals.getAssignments(), NewVNInfo);
// Kill flags are going to be wrong if the live ranges were overlapping.
// Eventually, we should simply clear all kill flags when computing live
// CR_Replace conflicts.
DEBUG(dbgs() << "\t\trestoring liveness to " << EndPoints.size()
<< " points: " << LHS << '\n');
- LIS->extendToIndices(&LHS, EndPoints);
+ LIS->extendToIndices(LHS, EndPoints);
return true;
}
-/// ComputeUltimateVN - Assuming we are going to join two live intervals,
-/// compute what the resultant value numbers for each value in the input two
-/// ranges will be. This is complicated by copies between the two which can
-/// and will commonly cause multiple value numbers to be merged into one.
-///
-/// VN is the value number that we're trying to resolve. InstDefiningValue
-/// keeps track of the new InstDefiningValue assignment for the result
-/// LiveInterval. ThisFromOther/OtherFromThis are sets that keep track of
-/// whether a value in this or other is a copy from the opposite set.
-/// ThisValNoAssignments/OtherValNoAssignments keep track of value #'s that have
-/// already been assigned.
-///
-/// ThisFromOther[x] - If x is defined as a copy from the other interval, this
-/// contains the value number the copy is from.
-///
-static unsigned ComputeUltimateVN(VNInfo *VNI,
- SmallVector<VNInfo*, 16> &NewVNInfo,
- DenseMap<VNInfo*, VNInfo*> &ThisFromOther,
- DenseMap<VNInfo*, VNInfo*> &OtherFromThis,
- SmallVector<int, 16> &ThisValNoAssignments,
- SmallVector<int, 16> &OtherValNoAssignments) {
- unsigned VN = VNI->id;
-
- // If the VN has already been computed, just return it.
- if (ThisValNoAssignments[VN] >= 0)
- return ThisValNoAssignments[VN];
- assert(ThisValNoAssignments[VN] != -2 && "Cyclic value numbers");
-
- // If this val is not a copy from the other val, then it must be a new value
- // number in the destination.
- DenseMap<VNInfo*, VNInfo*>::iterator I = ThisFromOther.find(VNI);
- if (I == ThisFromOther.end()) {
- NewVNInfo.push_back(VNI);
- return ThisValNoAssignments[VN] = NewVNInfo.size()-1;
- }
- VNInfo *OtherValNo = I->second;
-
- // Otherwise, this *is* a copy from the RHS. If the other side has already
- // been computed, return it.
- if (OtherValNoAssignments[OtherValNo->id] >= 0)
- return ThisValNoAssignments[VN] = OtherValNoAssignments[OtherValNo->id];
-
- // Mark this value number as currently being computed, then ask what the
- // ultimate value # of the other value is.
- ThisValNoAssignments[VN] = -2;
- unsigned UltimateVN =
- ComputeUltimateVN(OtherValNo, NewVNInfo, OtherFromThis, ThisFromOther,
- OtherValNoAssignments, ThisValNoAssignments);
- return ThisValNoAssignments[VN] = UltimateVN;
+/// Attempt to join these two intervals. On failure, this returns false.
+bool RegisterCoalescer::joinIntervals(CoalescerPair &CP) {
+ return CP.isPhys() ? joinReservedPhysReg(CP) : joinVirtRegs(CP);
}
+namespace {
+// Information concerning MBB coalescing priority.
+struct MBBPriorityInfo {
+ MachineBasicBlock *MBB;
+ unsigned Depth;
+ bool IsSplit;
+
+ MBBPriorityInfo(MachineBasicBlock *mbb, unsigned depth, bool issplit)
+ : MBB(mbb), Depth(depth), IsSplit(issplit) {}
+};
+}
-// Find out if we have something like
-// A = X
-// B = X
-// if so, we can pretend this is actually
-// A = X
-// B = A
-// which allows us to coalesce A and B.
-// VNI is the definition of B. LR is the life range of A that includes
-// the slot just before B. If we return true, we add "B = X" to DupCopies.
-// This implies that A dominates B.
-static bool RegistersDefinedFromSameValue(LiveIntervals &li,
- const TargetRegisterInfo &tri,
- CoalescerPair &CP,
- VNInfo *VNI,
- VNInfo *OtherVNI,
- SmallVector<MachineInstr*, 8> &DupCopies) {
- // FIXME: This is very conservative. For example, we don't handle
- // physical registers.
-
- MachineInstr *MI = li.getInstructionFromIndex(VNI->def);
-
- if (!MI || CP.isPartial() || CP.isPhys())
- return false;
+// C-style comparator that sorts first based on the loop depth of the basic
+// block (the unsigned), and then on the MBB number.
+//
+// EnableGlobalCopies assumes that the primary sort key is loop depth.
+static int compareMBBPriority(const MBBPriorityInfo *LHS,
+ const MBBPriorityInfo *RHS) {
+ // Deeper loops first
+ if (LHS->Depth != RHS->Depth)
+ return LHS->Depth > RHS->Depth ? -1 : 1;
+
+ // Try to unsplit critical edges next.
+ if (LHS->IsSplit != RHS->IsSplit)
+ return LHS->IsSplit ? -1 : 1;
+
+ // Prefer blocks that are more connected in the CFG. This takes care of
+ // the most difficult copies first while intervals are short.
+ unsigned cl = LHS->MBB->pred_size() + LHS->MBB->succ_size();
+ unsigned cr = RHS->MBB->pred_size() + RHS->MBB->succ_size();
+ if (cl != cr)
+ return cl > cr ? -1 : 1;
+
+ // As a last resort, sort by block number.
+ return LHS->MBB->getNumber() < RHS->MBB->getNumber() ? -1 : 1;
+}
- unsigned A = CP.getDstReg();
- if (!TargetRegisterInfo::isVirtualRegister(A))
+/// \returns true if the given copy uses or defines a local live range.
+static bool isLocalCopy(MachineInstr *Copy, const LiveIntervals *LIS) {
+ if (!Copy->isCopy())
return false;
- unsigned B = CP.getSrcReg();
- if (!TargetRegisterInfo::isVirtualRegister(B))
+ if (Copy->getOperand(1).isUndef())
return false;
- MachineInstr *OtherMI = li.getInstructionFromIndex(OtherVNI->def);
- if (!OtherMI)
+ unsigned SrcReg = Copy->getOperand(1).getReg();
+ unsigned DstReg = Copy->getOperand(0).getReg();
+ if (TargetRegisterInfo::isPhysicalRegister(SrcReg)
+ || TargetRegisterInfo::isPhysicalRegister(DstReg))
return false;
- if (MI->isImplicitDef()) {
- DupCopies.push_back(MI);
- return true;
- } else {
- if (!MI->isFullCopy())
- return false;
- unsigned Src = MI->getOperand(1).getReg();
- if (!TargetRegisterInfo::isVirtualRegister(Src))
- return false;
- if (!OtherMI->isFullCopy())
- return false;
- unsigned OtherSrc = OtherMI->getOperand(1).getReg();
- if (!TargetRegisterInfo::isVirtualRegister(OtherSrc))
- return false;
-
- if (Src != OtherSrc)
- return false;
-
- // If the copies use two different value numbers of X, we cannot merge
- // A and B.
- LiveInterval &SrcInt = li.getInterval(Src);
- // getVNInfoBefore returns NULL for undef copies. In this case, the
- // optimization is still safe.
- if (SrcInt.getVNInfoBefore(OtherVNI->def) !=
- SrcInt.getVNInfoBefore(VNI->def))
- return false;
-
- DupCopies.push_back(MI);
- return true;
- }
-}
-
-/// joinIntervals - Attempt to join these two intervals. On failure, this
-/// returns false.
-bool RegisterCoalescer::joinIntervals(CoalescerPair &CP) {
- // Handle physreg joins separately.
- if (CP.isPhys())
- return joinReservedPhysReg(CP);
-
- if (NewCoalescer)
- return joinVirtRegs(CP);
-
- LiveInterval &RHS = LIS->getInterval(CP.getSrcReg());
- DEBUG(dbgs() << "\t\tRHS = " << PrintReg(CP.getSrcReg()) << ' ' << RHS
- << '\n');
-
- // Compute the final value assignment, assuming that the live ranges can be
- // coalesced.
- SmallVector<int, 16> LHSValNoAssignments;
- SmallVector<int, 16> RHSValNoAssignments;
- DenseMap<VNInfo*, VNInfo*> LHSValsDefinedFromRHS;
- DenseMap<VNInfo*, VNInfo*> RHSValsDefinedFromLHS;
- SmallVector<VNInfo*, 16> NewVNInfo;
-
- SmallVector<MachineInstr*, 8> DupCopies;
- SmallVector<MachineInstr*, 8> DeadCopies;
-
- LiveInterval &LHS = LIS->getOrCreateInterval(CP.getDstReg());
- DEBUG(dbgs() << "\t\tLHS = " << PrintReg(CP.getDstReg(), TRI) << ' ' << LHS
- << '\n');
-
- // Loop over the value numbers of the LHS, seeing if any are defined from
- // the RHS.
- for (LiveInterval::vni_iterator i = LHS.vni_begin(), e = LHS.vni_end();
- i != e; ++i) {
- VNInfo *VNI = *i;
- if (VNI->isUnused() || VNI->isPHIDef())
- continue;
- MachineInstr *MI = LIS->getInstructionFromIndex(VNI->def);
- assert(MI && "Missing def");
- if (!MI->isCopyLike() && !MI->isImplicitDef()) // Src not defined by a copy?
- continue;
-
- // Figure out the value # from the RHS.
- VNInfo *OtherVNI = RHS.getVNInfoBefore(VNI->def);
- // The copy could be to an aliased physreg.
- if (!OtherVNI)
- continue;
-
- // DstReg is known to be a register in the LHS interval. If the src is
- // from the RHS interval, we can use its value #.
- if (CP.isCoalescable(MI))
- DeadCopies.push_back(MI);
- else if (!RegistersDefinedFromSameValue(*LIS, *TRI, CP, VNI, OtherVNI,
- DupCopies))
- continue;
-
- LHSValsDefinedFromRHS[VNI] = OtherVNI;
- }
-
- // Loop over the value numbers of the RHS, seeing if any are defined from
- // the LHS.
- for (LiveInterval::vni_iterator i = RHS.vni_begin(), e = RHS.vni_end();
- i != e; ++i) {
- VNInfo *VNI = *i;
- if (VNI->isUnused() || VNI->isPHIDef())
- continue;
- MachineInstr *MI = LIS->getInstructionFromIndex(VNI->def);
- assert(MI && "Missing def");
- if (!MI->isCopyLike() && !MI->isImplicitDef()) // Src not defined by a copy?
- continue;
-
- // Figure out the value # from the LHS.
- VNInfo *OtherVNI = LHS.getVNInfoBefore(VNI->def);
- // The copy could be to an aliased physreg.
- if (!OtherVNI)
- continue;
-
- // DstReg is known to be a register in the RHS interval. If the src is
- // from the LHS interval, we can use its value #.
- if (CP.isCoalescable(MI))
- DeadCopies.push_back(MI);
- else if (!RegistersDefinedFromSameValue(*LIS, *TRI, CP, VNI, OtherVNI,
- DupCopies))
- continue;
-
- RHSValsDefinedFromLHS[VNI] = OtherVNI;
- }
-
- LHSValNoAssignments.resize(LHS.getNumValNums(), -1);
- RHSValNoAssignments.resize(RHS.getNumValNums(), -1);
- NewVNInfo.reserve(LHS.getNumValNums() + RHS.getNumValNums());
-
- for (LiveInterval::vni_iterator i = LHS.vni_begin(), e = LHS.vni_end();
- i != e; ++i) {
- VNInfo *VNI = *i;
- unsigned VN = VNI->id;
- if (LHSValNoAssignments[VN] >= 0 || VNI->isUnused())
- continue;
- ComputeUltimateVN(VNI, NewVNInfo,
- LHSValsDefinedFromRHS, RHSValsDefinedFromLHS,
- LHSValNoAssignments, RHSValNoAssignments);
- }
- for (LiveInterval::vni_iterator i = RHS.vni_begin(), e = RHS.vni_end();
- i != e; ++i) {
- VNInfo *VNI = *i;
- unsigned VN = VNI->id;
- if (RHSValNoAssignments[VN] >= 0 || VNI->isUnused())
- continue;
- // If this value number isn't a copy from the LHS, it's a new number.
- if (RHSValsDefinedFromLHS.find(VNI) == RHSValsDefinedFromLHS.end()) {
- NewVNInfo.push_back(VNI);
- RHSValNoAssignments[VN] = NewVNInfo.size()-1;
- continue;
- }
-
- ComputeUltimateVN(VNI, NewVNInfo,
- RHSValsDefinedFromLHS, LHSValsDefinedFromRHS,
- RHSValNoAssignments, LHSValNoAssignments);
- }
-
- // Armed with the mappings of LHS/RHS values to ultimate values, walk the
- // interval lists to see if these intervals are coalescable.
- LiveInterval::const_iterator I = LHS.begin();
- LiveInterval::const_iterator IE = LHS.end();
- LiveInterval::const_iterator J = RHS.begin();
- LiveInterval::const_iterator JE = RHS.end();
-
- // Collect interval end points that will no longer be kills.
- SmallVector<MachineInstr*, 8> LHSOldKills;
- SmallVector<MachineInstr*, 8> RHSOldKills;
-
- // Skip ahead until the first place of potential sharing.
- if (I != IE && J != JE) {
- if (I->start < J->start) {
- I = std::upper_bound(I, IE, J->start);
- if (I != LHS.begin()) --I;
- } else if (J->start < I->start) {
- J = std::upper_bound(J, JE, I->start);
- if (J != RHS.begin()) --J;
- }
- }
-
- while (I != IE && J != JE) {
- // Determine if these two live ranges overlap.
- // If so, check value # info to determine if they are really different.
- if (I->end > J->start && J->end > I->start) {
- // If the live range overlap will map to the same value number in the
- // result liverange, we can still coalesce them. If not, we can't.
- if (LHSValNoAssignments[I->valno->id] !=
- RHSValNoAssignments[J->valno->id])
- return false;
-
- // Extended live ranges should no longer be killed.
- if (!I->end.isBlock() && I->end < J->end)
- if (MachineInstr *MI = LIS->getInstructionFromIndex(I->end))
- LHSOldKills.push_back(MI);
- if (!J->end.isBlock() && J->end < I->end)
- if (MachineInstr *MI = LIS->getInstructionFromIndex(J->end))
- RHSOldKills.push_back(MI);
- }
-
- if (I->end < J->end)
- ++I;
- else
- ++J;
- }
-
- // Clear kill flags where live ranges are extended.
- while (!LHSOldKills.empty())
- LHSOldKills.pop_back_val()->clearRegisterKills(LHS.reg, TRI);
- while (!RHSOldKills.empty())
- RHSOldKills.pop_back_val()->clearRegisterKills(RHS.reg, TRI);
-
- if (LHSValNoAssignments.empty())
- LHSValNoAssignments.push_back(-1);
- if (RHSValNoAssignments.empty())
- RHSValNoAssignments.push_back(-1);
-
- // Now erase all the redundant copies.
- for (unsigned i = 0, e = DeadCopies.size(); i != e; ++i) {
- MachineInstr *MI = DeadCopies[i];
- if (!ErasedInstrs.insert(MI))
- continue;
- DEBUG(dbgs() << "\t\terased:\t" << LIS->getInstructionIndex(MI)
- << '\t' << *MI);
- LIS->RemoveMachineInstrFromMaps(MI);
- MI->eraseFromParent();
- }
-
- SmallVector<unsigned, 8> SourceRegisters;
- for (SmallVector<MachineInstr*, 8>::iterator I = DupCopies.begin(),
- E = DupCopies.end(); I != E; ++I) {
- MachineInstr *MI = *I;
- if (!ErasedInstrs.insert(MI))
- continue;
-
- // If MI is a copy, then we have pretended that the assignment to B in
- // A = X
- // B = X
- // was actually a copy from A. Now that we decided to coalesce A and B,
- // transform the code into
- // A = X
- // In the case of the implicit_def, we just have to remove it.
- if (!MI->isImplicitDef()) {
- unsigned Src = MI->getOperand(1).getReg();
- SourceRegisters.push_back(Src);
- }
- LIS->RemoveMachineInstrFromMaps(MI);
- MI->eraseFromParent();
- }
-
- // If B = X was the last use of X in a liverange, we have to shrink it now
- // that B = X is gone.
- for (SmallVector<unsigned, 8>::iterator I = SourceRegisters.begin(),
- E = SourceRegisters.end(); I != E; ++I) {
- LIS->shrinkToUses(&LIS->getInterval(*I));
- }
-
- // If we get here, we know that we can coalesce the live ranges. Ask the
- // intervals to coalesce themselves now.
- LHS.join(RHS, &LHSValNoAssignments[0], &RHSValNoAssignments[0], NewVNInfo,
- MRI);
- return true;
-}
-
-namespace {
- // DepthMBBCompare - Comparison predicate that sort first based on the loop
- // depth of the basic block (the unsigned), and then on the MBB number.
- struct DepthMBBCompare {
- typedef std::pair<unsigned, MachineBasicBlock*> DepthMBBPair;
- bool operator()(const DepthMBBPair &LHS, const DepthMBBPair &RHS) const {
- // Deeper loops first
- if (LHS.first != RHS.first)
- return LHS.first > RHS.first;
-
- // Prefer blocks that are more connected in the CFG. This takes care of
- // the most difficult copies first while intervals are short.
- unsigned cl = LHS.second->pred_size() + LHS.second->succ_size();
- unsigned cr = RHS.second->pred_size() + RHS.second->succ_size();
- if (cl != cr)
- return cl > cr;
-
- // As a last resort, sort by block number.
- return LHS.second->getNumber() < RHS.second->getNumber();
- }
- };
+ return LIS->intervalIsInOneMBB(LIS->getInterval(SrcReg))
+ || LIS->intervalIsInOneMBB(LIS->getInterval(DstReg));
}
// Try joining WorkList copies starting from index From.
// Null out any successful joins.
-bool RegisterCoalescer::copyCoalesceWorkList(unsigned From) {
- assert(From <= WorkList.size() && "Out of range");
+bool RegisterCoalescer::
+copyCoalesceWorkList(MutableArrayRef<MachineInstr*> CurrList) {
bool Progress = false;
- for (unsigned i = From, e = WorkList.size(); i != e; ++i) {
- if (!WorkList[i])
+ for (unsigned i = 0, e = CurrList.size(); i != e; ++i) {
+ if (!CurrList[i])
continue;
// Skip instruction pointers that have already been erased, for example by
// dead code elimination.
- if (ErasedInstrs.erase(WorkList[i])) {
- WorkList[i] = 0;
+ if (ErasedInstrs.erase(CurrList[i])) {
+ CurrList[i] = nullptr;
continue;
}
bool Again = false;
- bool Success = joinCopy(WorkList[i], Again);
+ bool Success = joinCopy(CurrList[i], Again);
Progress |= Success;
if (Success || !Again)
- WorkList[i] = 0;
+ CurrList[i] = nullptr;
}
return Progress;
}
// Collect all copy-like instructions in MBB. Don't start coalescing anything
// yet, it might invalidate the iterator.
const unsigned PrevSize = WorkList.size();
- for (MachineBasicBlock::iterator MII = MBB->begin(), E = MBB->end();
- MII != E; ++MII)
- if (MII->isCopyLike())
- WorkList.push_back(MII);
-
+ if (JoinGlobalCopies) {
+ // Coalesce copies bottom-up to coalesce local defs before local uses. They
+ // are not inherently easier to resolve, but slightly preferable until we
+ // have local live range splitting. In particular this is required by
+ // cmp+jmp macro fusion.
+ for (MachineBasicBlock::iterator MII = MBB->begin(), E = MBB->end();
+ MII != E; ++MII) {
+ if (!MII->isCopyLike())
+ continue;
+ if (isLocalCopy(&(*MII), LIS))
+ LocalWorkList.push_back(&(*MII));
+ else
+ WorkList.push_back(&(*MII));
+ }
+ }
+ else {
+ for (MachineBasicBlock::iterator MII = MBB->begin(), E = MBB->end();
+ MII != E; ++MII)
+ if (MII->isCopyLike())
+ WorkList.push_back(MII);
+ }
// Try coalescing the collected copies immediately, and remove the nulls.
// This prevents the WorkList from getting too large since most copies are
// joinable on the first attempt.
- if (copyCoalesceWorkList(PrevSize))
+ MutableArrayRef<MachineInstr*>
+ CurrList(WorkList.begin() + PrevSize, WorkList.end());
+ if (copyCoalesceWorkList(CurrList))
WorkList.erase(std::remove(WorkList.begin() + PrevSize, WorkList.end(),
- (MachineInstr*)0), WorkList.end());
+ (MachineInstr*)nullptr), WorkList.end());
+}
+
+void RegisterCoalescer::coalesceLocals() {
+ copyCoalesceWorkList(LocalWorkList);
+ for (unsigned j = 0, je = LocalWorkList.size(); j != je; ++j) {
+ if (LocalWorkList[j])
+ WorkList.push_back(LocalWorkList[j]);
+ }
+ LocalWorkList.clear();
}
void RegisterCoalescer::joinAllIntervals() {
DEBUG(dbgs() << "********** JOINING INTERVALS ***********\n");
- assert(WorkList.empty() && "Old data still around.");
-
- if (Loops->empty()) {
- // If there are no loops in the function, join intervals in function order.
- for (MachineFunction::iterator I = MF->begin(), E = MF->end();
- I != E; ++I)
- copyCoalesceInMBB(I);
- } else {
- // Otherwise, join intervals in inner loops before other intervals.
- // Unfortunately we can't just iterate over loop hierarchy here because
- // there may be more MBB's than BB's. Collect MBB's for sorting.
-
- // Join intervals in the function prolog first. We want to join physical
- // registers with virtual registers before the intervals got too long.
- std::vector<std::pair<unsigned, MachineBasicBlock*> > MBBs;
- for (MachineFunction::iterator I = MF->begin(), E = MF->end();I != E;++I){
- MachineBasicBlock *MBB = I;
- MBBs.push_back(std::make_pair(Loops->getLoopDepth(MBB), I));
+ assert(WorkList.empty() && LocalWorkList.empty() && "Old data still around.");
+
+ std::vector<MBBPriorityInfo> MBBs;
+ MBBs.reserve(MF->size());
+ for (MachineFunction::iterator I = MF->begin(), E = MF->end();I != E;++I){
+ MachineBasicBlock *MBB = I;
+ MBBs.push_back(MBBPriorityInfo(MBB, Loops->getLoopDepth(MBB),
+ JoinSplitEdges && isSplitEdge(MBB)));
+ }
+ array_pod_sort(MBBs.begin(), MBBs.end(), compareMBBPriority);
+
+ // Coalesce intervals in MBB priority order.
+ unsigned CurrDepth = UINT_MAX;
+ for (unsigned i = 0, e = MBBs.size(); i != e; ++i) {
+ // Try coalescing the collected local copies for deeper loops.
+ if (JoinGlobalCopies && MBBs[i].Depth < CurrDepth) {
+ coalesceLocals();
+ CurrDepth = MBBs[i].Depth;
}
-
- // Sort by loop depth.
- std::sort(MBBs.begin(), MBBs.end(), DepthMBBCompare());
-
- // Finally, join intervals in loop nest order.
- for (unsigned i = 0, e = MBBs.size(); i != e; ++i)
- copyCoalesceInMBB(MBBs[i].second);
+ copyCoalesceInMBB(MBBs[i].MBB);
}
+ coalesceLocals();
// Joining intervals can allow other intervals to be joined. Iteratively join
// until we make no progress.
- while (copyCoalesceWorkList())
+ while (copyCoalesceWorkList(WorkList))
/* empty */ ;
}
MF = &fn;
MRI = &fn.getRegInfo();
TM = &fn.getTarget();
- TRI = TM->getRegisterInfo();
- TII = TM->getInstrInfo();
+ TRI = TM->getSubtargetImpl()->getRegisterInfo();
+ TII = TM->getSubtargetImpl()->getInstrInfo();
LIS = &getAnalysis<LiveIntervals>();
- LDV = &getAnalysis<LiveDebugVariables>();
AA = &getAnalysis<AliasAnalysis>();
Loops = &getAnalysis<MachineLoopInfo>();
+ const TargetSubtargetInfo &ST = TM->getSubtarget<TargetSubtargetInfo>();
+ if (EnableGlobalCopies == cl::BOU_UNSET)
+ JoinGlobalCopies = ST.useMachineScheduler();
+ else
+ JoinGlobalCopies = (EnableGlobalCopies == cl::BOU_TRUE);
+
+ // The MachineScheduler does not currently require JoinSplitEdges. This will
+ // either be enabled unconditionally or replaced by a more general live range
+ // splitting optimization.
+ JoinSplitEdges = EnableJoinSplits;
+
DEBUG(dbgs() << "********** SIMPLE REGISTER COALESCING **********\n"
<< "********** Function: " << MF->getName() << '\n');
continue;
if (MRI->recomputeRegClass(Reg, *TM)) {
DEBUG(dbgs() << PrintReg(Reg) << " inflated to "
- << MRI->getRegClass(Reg)->getName() << '\n');
+ << TRI->getRegClassName(MRI->getRegClass(Reg)) << '\n');
++NumInflated;
}
}
DEBUG(dump());
- DEBUG(LDV->dump());
if (VerifyCoalescing)
MF->verify(this, "After register coalescing");
return true;
}
-/// print - Implement the dump method.
+/// Implement the dump method.
void RegisterCoalescer::print(raw_ostream &O, const Module* m) const {
LIS->print(O, m);
}