index d547c962c2dc68574f04f8ccdf93637c3eeb6e04..c134454e0d03812cccd4627030d05850f577ba83 100644 (file)
//
//===----------------------------------------------------------------------===//
-#define DEBUG_TYPE "instr-emitter"
#include "InstrEmitter.h"
#include "SDNodeDbgValue.h"
+#include "llvm/ADT/Statistic.h"
#include "llvm/CodeGen/MachineConstantPool.h"
#include "llvm/CodeGen/MachineFunction.h"
#include "llvm/CodeGen/MachineInstrBuilder.h"
#include "llvm/CodeGen/MachineRegisterInfo.h"
-#include "llvm/Target/TargetData.h"
-#include "llvm/Target/TargetMachine.h"
-#include "llvm/Target/TargetInstrInfo.h"
-#include "llvm/Target/TargetLowering.h"
-#include "llvm/ADT/Statistic.h"
+#include "llvm/CodeGen/StackMaps.h"
+#include "llvm/IR/DataLayout.h"
#include "llvm/Support/Debug.h"
#include "llvm/Support/ErrorHandling.h"
#include "llvm/Support/MathExtras.h"
+#include "llvm/Target/TargetInstrInfo.h"
+#include "llvm/Target/TargetLowering.h"
+#include "llvm/Target/TargetMachine.h"
using namespace llvm;
+#define DEBUG_TYPE "instr-emitter"
+
+/// MinRCSize - Smallest register class we allow when constraining virtual
+/// registers. If satisfying all register class constraints would require
+/// using a smaller register class, emit a COPY to a new virtual register
+/// instead.
+const unsigned MinRCSize = 4;
+
/// CountResults - The results of target nodes have register or immediate
/// operands first, then an optional chain, and optional glue operands (which do
/// not go into the resulting MachineInstr).
return N;
}
-/// CountOperands - The inputs to target nodes have any actual inputs first,
+/// countOperands - The inputs to target nodes have any actual inputs first,
/// followed by an optional chain operand, then an optional glue operand.
/// Compute the number of actual operands that will go into the resulting
/// MachineInstr.
-unsigned InstrEmitter::CountOperands(SDNode *Node) {
+///
+/// Also count physreg RegisterSDNode and RegisterMaskSDNode operands preceding
+/// the chain and glue. These operands may be implicit on the machine instr.
+static unsigned countOperands(SDNode *Node, unsigned NumExpUses,
+ unsigned &NumImpUses) {
unsigned N = Node->getNumOperands();
while (N && Node->getOperand(N - 1).getValueType() == MVT::Glue)
--N;
if (N && Node->getOperand(N - 1).getValueType() == MVT::Other)
--N; // Ignore chain if it exists.
+
+ // Count RegisterSDNode and RegisterMaskSDNode operands for NumImpUses.
+ NumImpUses = N - NumExpUses;
+ for (unsigned I = N; I > NumExpUses; --I) {
+ if (isa<RegisterMaskSDNode>(Node->getOperand(I - 1)))
+ continue;
+ if (RegisterSDNode *RN = dyn_cast<RegisterSDNode>(Node->getOperand(I - 1)))
+ if (TargetRegisterInfo::isPhysicalRegister(RN->getReg()))
+ continue;
+ NumImpUses = N - I;
+ break;
+ }
+
return N;
}
// If the node is only used by a CopyToReg and the dest reg is a vreg, use
// the CopyToReg'd destination register instead of creating a new vreg.
bool MatchReg = true;
- const TargetRegisterClass *UseRC = NULL;
- EVT VT = Node->getValueType(ResNo);
+ const TargetRegisterClass *UseRC = nullptr;
+ MVT VT = Node->getSimpleValueType(ResNo);
// Stick to the preferred register classes for legal types.
if (TLI->isTypeLegal(VT))
UseRC = TLI->getRegClassFor(VT);
if (!IsClone && !IsCloned)
- for (SDNode::use_iterator UI = Node->use_begin(), E = Node->use_end();
- UI != E; ++UI) {
- SDNode *User = *UI;
+ for (SDNode *User : Node->uses()) {
bool Match = true;
if (User->getOpcode() == ISD::CopyToReg &&
User->getOperand(2).getNode() == Node &&
SDValue Op = User->getOperand(i);
if (Op.getNode() != Node || Op.getResNo() != ResNo)
continue;
- EVT VT = Node->getValueType(Op.getResNo());
+ MVT VT = Node->getSimpleValueType(Op.getResNo());
if (VT == MVT::Other || VT == MVT::Glue)
continue;
Match = false;
if (User->isMachineOpcode()) {
const MCInstrDesc &II = TII->get(User->getMachineOpcode());
- const TargetRegisterClass *RC = 0;
- if (i+II.getNumDefs() < II.getNumOperands())
- RC = TII->getRegClass(II, i+II.getNumDefs(), TRI);
+ const TargetRegisterClass *RC = nullptr;
+ if (i+II.getNumDefs() < II.getNumOperands()) {
+ RC = TRI->getAllocatableClass(
+ TII->getRegClass(II, i+II.getNumDefs(), TRI, *MF));
+ }
if (!UseRC)
UseRC = RC;
else if (RC) {
break;
}
- const TargetRegisterClass *SrcRC = 0, *DstRC = 0;
+ const TargetRegisterClass *SrcRC = nullptr, *DstRC = nullptr;
SrcRC = TRI->getMinimalPhysRegClass(SrcReg, VT);
// Figure out the register class to create for the destreg.
return 0;
}
-void InstrEmitter::CreateVirtualRegisters(SDNode *Node, MachineInstr *MI,
+void InstrEmitter::CreateVirtualRegisters(SDNode *Node,
+ MachineInstrBuilder &MIB,
const MCInstrDesc &II,
bool IsClone, bool IsCloned,
DenseMap<SDValue, unsigned> &VRBaseMap) {
assert(Node->getMachineOpcode() != TargetOpcode::IMPLICIT_DEF &&
"IMPLICIT_DEF should have been handled as a special case elsewhere!");
+ unsigned NumResults = CountResults(Node);
for (unsigned i = 0; i < II.getNumDefs(); ++i) {
// If the specific node value is only used by a CopyToReg and the dest reg
// is a vreg in the same register class, use the CopyToReg'd destination
// register instead of creating a new vreg.
unsigned VRBase = 0;
- const TargetRegisterClass *RC = TII->getRegClass(II, i, TRI);
+ const TargetRegisterClass *RC =
+ TRI->getAllocatableClass(TII->getRegClass(II, i, TRI, *MF));
+ // Always let the value type influence the used register class. The
+ // constraints on the instruction may be too lax to represent the value
+ // type correctly. For example, a 64-bit float (X86::FR64) can't live in
+ // the 32-bit float super-class (X86::FR32).
+ if (i < NumResults && TLI->isTypeLegal(Node->getSimpleValueType(i))) {
+ const TargetRegisterClass *VTRC =
+ TLI->getRegClassFor(Node->getSimpleValueType(i));
+ if (RC)
+ VTRC = TRI->getCommonSubClass(RC, VTRC);
+ if (VTRC)
+ RC = VTRC;
+ }
+
if (II.OpInfo[i].isOptionalDef()) {
// Optional def must be a physical register.
unsigned NumResults = CountResults(Node);
VRBase = cast<RegisterSDNode>(Node->getOperand(i-NumResults))->getReg();
assert(TargetRegisterInfo::isPhysicalRegister(VRBase));
- MI->addOperand(MachineOperand::CreateReg(VRBase, true));
+ MIB.addReg(VRBase, RegState::Define);
}
if (!VRBase && !IsClone && !IsCloned)
- for (SDNode::use_iterator UI = Node->use_begin(), E = Node->use_end();
- UI != E; ++UI) {
- SDNode *User = *UI;
+ for (SDNode *User : Node->uses()) {
if (User->getOpcode() == ISD::CopyToReg &&
User->getOperand(2).getNode() == Node &&
User->getOperand(2).getResNo() == i) {
const TargetRegisterClass *RegRC = MRI->getRegClass(Reg);
if (RegRC == RC) {
VRBase = Reg;
- MI->addOperand(MachineOperand::CreateReg(Reg, true));
+ MIB.addReg(VRBase, RegState::Define);
break;
}
}
if (VRBase == 0) {
assert(RC && "Isn't a register operand!");
VRBase = MRI->createVirtualRegister(RC);
- MI->addOperand(MachineOperand::CreateReg(VRBase, true));
+ MIB.addReg(VRBase, RegState::Define);
}
SDValue Op(Node, i);
// IMPLICIT_DEF can produce any type of result so its MCInstrDesc
// does not include operand register class info.
if (!VReg) {
- const TargetRegisterClass *RC = TLI->getRegClassFor(Op.getValueType());
+ const TargetRegisterClass *RC =
+ TLI->getRegClassFor(Op.getSimpleValueType());
VReg = MRI->createVirtualRegister(RC);
}
BuildMI(*MBB, InsertPos, Op.getDebugLoc(),
/// specified machine instr. Insert register copies if the register is
/// not in the required register class.
void
-InstrEmitter::AddRegisterOperand(MachineInstr *MI, SDValue Op,
+InstrEmitter::AddRegisterOperand(MachineInstrBuilder &MIB,
+ SDValue Op,
unsigned IIOpNum,
const MCInstrDesc *II,
DenseMap<SDValue, unsigned> &VRBaseMap,
unsigned VReg = getVR(Op, VRBaseMap);
assert(TargetRegisterInfo::isVirtualRegister(VReg) && "Not a vreg?");
- const MCInstrDesc &MCID = MI->getDesc();
+ const MCInstrDesc &MCID = MIB->getDesc();
bool isOptDef = IIOpNum < MCID.getNumOperands() &&
MCID.OpInfo[IIOpNum].isOptionalDef();
// a new virtual register and copy the value into it, but first attempt to
// shrink VReg's register class within reason. For example, if VReg == GR32
// and II requires a GR32_NOSP, just constrain VReg to GR32_NOSP.
- const unsigned MinRCSize = 4;
if (II) {
- const TargetRegisterClass *DstRC = 0;
+ const TargetRegisterClass *DstRC = nullptr;
if (IIOpNum < II->getNumOperands())
- DstRC = TII->getRegClass(*II, IIOpNum, TRI);
- assert((DstRC || (MCID.isVariadic() && IIOpNum >= MCID.getNumOperands())) &&
- "Don't have operand info for this instruction!");
+ DstRC = TRI->getAllocatableClass(TII->getRegClass(*II,IIOpNum,TRI,*MF));
if (DstRC && !MRI->constrainRegClass(VReg, DstRC, MinRCSize)) {
unsigned NewVReg = MRI->createVirtualRegister(DstRC);
BuildMI(*MBB, InsertPos, Op.getNode()->getDebugLoc(),
!IsDebug &&
!(IsClone || IsCloned);
if (isKill) {
- unsigned Idx = MI->getNumOperands();
+ unsigned Idx = MIB->getNumOperands();
while (Idx > 0 &&
- MI->getOperand(Idx-1).isReg() && MI->getOperand(Idx-1).isImplicit())
+ MIB->getOperand(Idx-1).isReg() &&
+ MIB->getOperand(Idx-1).isImplicit())
--Idx;
- bool isTied = MI->getDesc().getOperandConstraint(Idx, MCOI::TIED_TO) != -1;
+ bool isTied = MCID.getOperandConstraint(Idx, MCOI::TIED_TO) != -1;
if (isTied)
isKill = false;
}
- MI->addOperand(MachineOperand::CreateReg(VReg, isOptDef,
- false/*isImp*/, isKill,
- false/*isDead*/, false/*isUndef*/,
- false/*isEarlyClobber*/,
- 0/*SubReg*/, IsDebug));
+ MIB.addReg(VReg, getDefRegState(isOptDef) | getKillRegState(isKill) |
+ getDebugRegState(IsDebug));
}
/// AddOperand - Add the specified operand to the specified machine instr. II
/// specifies the instruction information for the node, and IIOpNum is the
-/// operand number (in the II) that we are adding. IIOpNum and II are used for
-/// assertions only.
-void InstrEmitter::AddOperand(MachineInstr *MI, SDValue Op,
+/// operand number (in the II) that we are adding.
+void InstrEmitter::AddOperand(MachineInstrBuilder &MIB,
+ SDValue Op,
unsigned IIOpNum,
const MCInstrDesc *II,
DenseMap<SDValue, unsigned> &VRBaseMap,
bool IsDebug, bool IsClone, bool IsCloned) {
if (Op.isMachineOpcode()) {
- AddRegisterOperand(MI, Op, IIOpNum, II, VRBaseMap,
+ AddRegisterOperand(MIB, Op, IIOpNum, II, VRBaseMap,
IsDebug, IsClone, IsCloned);
} else if (ConstantSDNode *C = dyn_cast<ConstantSDNode>(Op)) {
- MI->addOperand(MachineOperand::CreateImm(C->getSExtValue()));
+ MIB.addImm(C->getSExtValue());
} else if (ConstantFPSDNode *F = dyn_cast<ConstantFPSDNode>(Op)) {
- const ConstantFP *CFP = F->getConstantFPValue();
- MI->addOperand(MachineOperand::CreateFPImm(CFP));
+ MIB.addFPImm(F->getConstantFPValue());
} else if (RegisterSDNode *R = dyn_cast<RegisterSDNode>(Op)) {
- MI->addOperand(MachineOperand::CreateReg(R->getReg(), false));
+ // Turn additional physreg operands into implicit uses on non-variadic
+ // instructions. This is used by call and return instructions passing
+ // arguments in registers.
+ bool Imp = II && (IIOpNum >= II->getNumOperands() && !II->isVariadic());
+ MIB.addReg(R->getReg(), getImplRegState(Imp));
+ } else if (RegisterMaskSDNode *RM = dyn_cast<RegisterMaskSDNode>(Op)) {
+ MIB.addRegMask(RM->getRegMask());
} else if (GlobalAddressSDNode *TGA = dyn_cast<GlobalAddressSDNode>(Op)) {
- MI->addOperand(MachineOperand::CreateGA(TGA->getGlobal(), TGA->getOffset(),
- TGA->getTargetFlags()));
+ MIB.addGlobalAddress(TGA->getGlobal(), TGA->getOffset(),
+ TGA->getTargetFlags());
} else if (BasicBlockSDNode *BBNode = dyn_cast<BasicBlockSDNode>(Op)) {
- MI->addOperand(MachineOperand::CreateMBB(BBNode->getBasicBlock()));
+ MIB.addMBB(BBNode->getBasicBlock());
} else if (FrameIndexSDNode *FI = dyn_cast<FrameIndexSDNode>(Op)) {
- MI->addOperand(MachineOperand::CreateFI(FI->getIndex()));
+ MIB.addFrameIndex(FI->getIndex());
} else if (JumpTableSDNode *JT = dyn_cast<JumpTableSDNode>(Op)) {
- MI->addOperand(MachineOperand::CreateJTI(JT->getIndex(),
- JT->getTargetFlags()));
+ MIB.addJumpTableIndex(JT->getIndex(), JT->getTargetFlags());
} else if (ConstantPoolSDNode *CP = dyn_cast<ConstantPoolSDNode>(Op)) {
int Offset = CP->getOffset();
unsigned Align = CP->getAlignment();
Type *Type = CP->getType();
// MachineConstantPool wants an explicit alignment.
if (Align == 0) {
- Align = TM->getTargetData()->getPrefTypeAlignment(Type);
+ Align = TM->getDataLayout()->getPrefTypeAlignment(Type);
if (Align == 0) {
// Alignment of vector types. FIXME!
- Align = TM->getTargetData()->getTypeAllocSize(Type);
+ Align = TM->getDataLayout()->getTypeAllocSize(Type);
}
}
Idx = MCP->getConstantPoolIndex(CP->getMachineCPVal(), Align);
else
Idx = MCP->getConstantPoolIndex(CP->getConstVal(), Align);
- MI->addOperand(MachineOperand::CreateCPI(Idx, Offset,
- CP->getTargetFlags()));
+ MIB.addConstantPoolIndex(Idx, Offset, CP->getTargetFlags());
} else if (ExternalSymbolSDNode *ES = dyn_cast<ExternalSymbolSDNode>(Op)) {
- MI->addOperand(MachineOperand::CreateES(ES->getSymbol(),
- ES->getTargetFlags()));
+ MIB.addExternalSymbol(ES->getSymbol(), ES->getTargetFlags());
} else if (BlockAddressSDNode *BA = dyn_cast<BlockAddressSDNode>(Op)) {
- MI->addOperand(MachineOperand::CreateBA(BA->getBlockAddress(),
- BA->getTargetFlags()));
+ MIB.addBlockAddress(BA->getBlockAddress(),
+ BA->getOffset(),
+ BA->getTargetFlags());
+ } else if (TargetIndexSDNode *TI = dyn_cast<TargetIndexSDNode>(Op)) {
+ MIB.addTargetIndex(TI->getIndex(), TI->getOffset(), TI->getTargetFlags());
} else {
assert(Op.getValueType() != MVT::Other &&
Op.getValueType() != MVT::Glue &&
"Chain and glue operands should occur at end of operand list!");
- AddRegisterOperand(MI, Op, IIOpNum, II, VRBaseMap,
+ AddRegisterOperand(MIB, Op, IIOpNum, II, VRBaseMap,
IsDebug, IsClone, IsCloned);
}
}
-/// getSuperRegisterRegClass - Returns the register class of a superreg A whose
-/// "SubIdx"'th sub-register class is the specified register class and whose
-/// type matches the specified type.
-static const TargetRegisterClass*
-getSuperRegisterRegClass(const TargetRegisterClass *TRC,
- unsigned SubIdx, EVT VT) {
- // Pick the register class of the superegister for this type
- for (TargetRegisterInfo::regclass_iterator I = TRC->superregclasses_begin(),
- E = TRC->superregclasses_end(); I != E; ++I)
- if ((*I)->hasType(VT) && (*I)->getSubRegisterRegClass(SubIdx) == TRC)
- return *I;
- assert(false && "Couldn't find the register class");
- return 0;
+unsigned InstrEmitter::ConstrainForSubReg(unsigned VReg, unsigned SubIdx,
+ MVT VT, DebugLoc DL) {
+ const TargetRegisterClass *VRC = MRI->getRegClass(VReg);
+ const TargetRegisterClass *RC = TRI->getSubClassWithSubReg(VRC, SubIdx);
+
+ // RC is a sub-class of VRC that supports SubIdx. Try to constrain VReg
+ // within reason.
+ if (RC && RC != VRC)
+ RC = MRI->constrainRegClass(VReg, RC, MinRCSize);
+
+ // VReg has been adjusted. It can be used with SubIdx operands now.
+ if (RC)
+ return VReg;
+
+ // VReg couldn't be reasonably constrained. Emit a COPY to a new virtual
+ // register instead.
+ RC = TRI->getSubClassWithSubReg(TLI->getRegClassFor(VT), SubIdx);
+ assert(RC && "No legal register class for VT supports that SubIdx");
+ unsigned NewReg = MRI->createVirtualRegister(RC);
+ BuildMI(*MBB, InsertPos, DL, TII->get(TargetOpcode::COPY), NewReg)
+ .addReg(VReg);
+ return NewReg;
}
/// EmitSubregNode - Generate machine code for subreg nodes.
// If the node is only used by a CopyToReg and the dest reg is a vreg, use
// the CopyToReg'd destination register instead of creating a new vreg.
- for (SDNode::use_iterator UI = Node->use_begin(), E = Node->use_end();
- UI != E; ++UI) {
- SDNode *User = *UI;
+ for (SDNode *User : Node->uses()) {
if (User->getOpcode() == ISD::CopyToReg &&
User->getOperand(2).getNode() == Node) {
unsigned DestReg = cast<RegisterSDNode>(User->getOperand(1))->getReg();
}
if (Opc == TargetOpcode::EXTRACT_SUBREG) {
- // EXTRACT_SUBREG is lowered as %dst = COPY %src:sub
+ // EXTRACT_SUBREG is lowered as %dst = COPY %src:sub. There are no
+ // constraints on the %dst register, COPY can target all legal register
+ // classes.
unsigned SubIdx = cast<ConstantSDNode>(Node->getOperand(1))->getZExtValue();
+ const TargetRegisterClass *TRC =
+ TLI->getRegClassFor(Node->getSimpleValueType(0));
- // Figure out the register class to create for the destreg.
unsigned VReg = getVR(Node->getOperand(0), VRBaseMap);
MachineInstr *DefMI = MRI->getVRegDef(VReg);
unsigned SrcReg, DstReg, DefSubIdx;
if (DefMI &&
TII->isCoalescableExtInstr(*DefMI, SrcReg, DstReg, DefSubIdx) &&
- SubIdx == DefSubIdx) {
+ SubIdx == DefSubIdx &&
+ TRC == MRI->getRegClass(SrcReg)) {
// Optimize these:
// r1025 = s/zext r1024, 4
// r1026 = extract_subreg r1025, 4
// to a copy
// r1026 = copy r1024
- const TargetRegisterClass *TRC = MRI->getRegClass(SrcReg);
VRBase = MRI->createVirtualRegister(TRC);
BuildMI(*MBB, InsertPos, Node->getDebugLoc(),
TII->get(TargetOpcode::COPY), VRBase).addReg(SrcReg);
+ MRI->clearKillFlags(SrcReg);
} else {
- const TargetRegisterClass *TRC = MRI->getRegClass(VReg);
- const TargetRegisterClass *SRC = TRC->getSubRegisterRegClass(SubIdx);
- assert(SRC && "Invalid subregister index in EXTRACT_SUBREG");
-
- // Figure out the register class to create for the destreg.
- // Note that if we're going to directly use an existing register,
- // it must be precisely the required class, and not a subclass
- // thereof.
- if (VRBase == 0 || SRC != MRI->getRegClass(VRBase)) {
- // Create the reg
- assert(SRC && "Couldn't find source register class");
- VRBase = MRI->createVirtualRegister(SRC);
- }
+ // VReg may not support a SubIdx sub-register, and we may need to
+ // constrain its register class or issue a COPY to a compatible register
+ // class.
+ VReg = ConstrainForSubReg(VReg, SubIdx,
+ Node->getOperand(0).getSimpleValueType(),
+ Node->getDebugLoc());
- // Create the extract_subreg machine instruction.
- MachineInstr *MI = BuildMI(*MF, Node->getDebugLoc(),
- TII->get(TargetOpcode::COPY), VRBase);
+ // Create the destreg if it is missing.
+ if (VRBase == 0)
+ VRBase = MRI->createVirtualRegister(TRC);
- // Add source, and subreg index
- AddOperand(MI, Node->getOperand(0), 0, 0, VRBaseMap, /*IsDebug=*/false,
- IsClone, IsCloned);
- assert(TargetRegisterInfo::isVirtualRegister(MI->getOperand(1).getReg())&&
- "Cannot yet extract from physregs");
- MI->getOperand(1).setSubReg(SubIdx);
- MBB->insert(InsertPos, MI);
+ // Create the extract_subreg machine instruction.
+ BuildMI(*MBB, InsertPos, Node->getDebugLoc(),
+ TII->get(TargetOpcode::COPY), VRBase).addReg(VReg, 0, SubIdx);
}
} else if (Opc == TargetOpcode::INSERT_SUBREG ||
Opc == TargetOpcode::SUBREG_TO_REG) {
SDValue N0 = Node->getOperand(0);
SDValue N1 = Node->getOperand(1);
SDValue N2 = Node->getOperand(2);
- unsigned SubReg = getVR(N1, VRBaseMap);
unsigned SubIdx = cast<ConstantSDNode>(N2)->getZExtValue();
- const TargetRegisterClass *TRC = MRI->getRegClass(SubReg);
- const TargetRegisterClass *SRC =
- getSuperRegisterRegClass(TRC, SubIdx, Node->getValueType(0));
-
- // Figure out the register class to create for the destreg.
- // Note that if we're going to directly use an existing register,
- // it must be precisely the required class, and not a subclass
- // thereof.
- if (VRBase == 0 || SRC != MRI->getRegClass(VRBase)) {
- // Create the reg
- assert(SRC && "Couldn't find source register class");
+
+ // Figure out the register class to create for the destreg. It should be
+ // the largest legal register class supporting SubIdx sub-registers.
+ // RegisterCoalescer will constrain it further if it decides to eliminate
+ // the INSERT_SUBREG instruction.
+ //
+ // %dst = INSERT_SUBREG %src, %sub, SubIdx
+ //
+ // is lowered by TwoAddressInstructionPass to:
+ //
+ // %dst = COPY %src
+ // %dst:SubIdx = COPY %sub
+ //
+ // There is no constraint on the %src register class.
+ //
+ const TargetRegisterClass *SRC = TLI->getRegClassFor(Node->getSimpleValueType(0));
+ SRC = TRI->getSubClassWithSubReg(SRC, SubIdx);
+ assert(SRC && "No register class supports VT and SubIdx for INSERT_SUBREG");
+
+ if (VRBase == 0 || !SRC->hasSubClassEq(MRI->getRegClass(VRBase)))
VRBase = MRI->createVirtualRegister(SRC);
- }
// Create the insert_subreg or subreg_to_reg machine instruction.
- MachineInstr *MI = BuildMI(*MF, Node->getDebugLoc(), TII->get(Opc));
- MI->addOperand(MachineOperand::CreateReg(VRBase, true));
+ MachineInstrBuilder MIB =
+ BuildMI(*MF, Node->getDebugLoc(), TII->get(Opc), VRBase);
// If creating a subreg_to_reg, then the first input operand
// is an implicit value immediate, otherwise it's a register
if (Opc == TargetOpcode::SUBREG_TO_REG) {
const ConstantSDNode *SD = cast<ConstantSDNode>(N0);
- MI->addOperand(MachineOperand::CreateImm(SD->getZExtValue()));
+ MIB.addImm(SD->getZExtValue());
} else
- AddOperand(MI, N0, 0, 0, VRBaseMap, /*IsDebug=*/false,
+ AddOperand(MIB, N0, 0, nullptr, VRBaseMap, /*IsDebug=*/false,
IsClone, IsCloned);
// Add the subregster being inserted
- AddOperand(MI, N1, 0, 0, VRBaseMap, /*IsDebug=*/false,
+ AddOperand(MIB, N1, 0, nullptr, VRBaseMap, /*IsDebug=*/false,
IsClone, IsCloned);
- MI->addOperand(MachineOperand::CreateImm(SubIdx));
- MBB->insert(InsertPos, MI);
+ MIB.addImm(SubIdx);
+ MBB->insert(InsertPos, MIB);
} else
llvm_unreachable("Node is not insert_subreg, extract_subreg, or subreg_to_reg");
// Create the new VReg in the destination class and emit a copy.
unsigned DstRCIdx = cast<ConstantSDNode>(Node->getOperand(1))->getZExtValue();
- const TargetRegisterClass *DstRC = TRI->getRegClass(DstRCIdx);
+ const TargetRegisterClass *DstRC =
+ TRI->getAllocatableClass(TRI->getRegClass(DstRCIdx));
unsigned NewVReg = MRI->createVirtualRegister(DstRC);
BuildMI(*MBB, InsertPos, Node->getDebugLoc(), TII->get(TargetOpcode::COPY),
NewVReg).addReg(VReg);
bool IsClone, bool IsCloned) {
unsigned DstRCIdx = cast<ConstantSDNode>(Node->getOperand(0))->getZExtValue();
const TargetRegisterClass *RC = TRI->getRegClass(DstRCIdx);
- unsigned NewVReg = MRI->createVirtualRegister(RC);
- MachineInstr *MI = BuildMI(*MF, Node->getDebugLoc(),
- TII->get(TargetOpcode::REG_SEQUENCE), NewVReg);
+ unsigned NewVReg = MRI->createVirtualRegister(TRI->getAllocatableClass(RC));
+ const MCInstrDesc &II = TII->get(TargetOpcode::REG_SEQUENCE);
+ MachineInstrBuilder MIB = BuildMI(*MF, Node->getDebugLoc(), II, NewVReg);
unsigned NumOps = Node->getNumOperands();
assert((NumOps & 1) == 1 &&
"REG_SEQUENCE must have an odd number of operands!");
- const MCInstrDesc &II = TII->get(TargetOpcode::REG_SEQUENCE);
for (unsigned i = 1; i != NumOps; ++i) {
SDValue Op = Node->getOperand(i);
if ((i & 1) == 0) {
- unsigned SubIdx = cast<ConstantSDNode>(Op)->getZExtValue();
- unsigned SubReg = getVR(Node->getOperand(i-1), VRBaseMap);
- const TargetRegisterClass *TRC = MRI->getRegClass(SubReg);
- const TargetRegisterClass *SRC =
+ RegisterSDNode *R = dyn_cast<RegisterSDNode>(Node->getOperand(i-1));
+ // Skip physical registers as they don't have a vreg to get and we'll
+ // insert copies for them in TwoAddressInstructionPass anyway.
+ if (!R || !TargetRegisterInfo::isPhysicalRegister(R->getReg())) {
+ unsigned SubIdx = cast<ConstantSDNode>(Op)->getZExtValue();
+ unsigned SubReg = getVR(Node->getOperand(i-1), VRBaseMap);
+ const TargetRegisterClass *TRC = MRI->getRegClass(SubReg);
+ const TargetRegisterClass *SRC =
TRI->getMatchingSuperRegClass(RC, TRC, SubIdx);
- if (SRC && SRC != RC) {
- MRI->setRegClass(NewVReg, SRC);
- RC = SRC;
+ if (SRC && SRC != RC) {
+ MRI->setRegClass(NewVReg, SRC);
+ RC = SRC;
+ }
}
}
- AddOperand(MI, Op, i+1, &II, VRBaseMap, /*IsDebug=*/false,
+ AddOperand(MIB, Op, i+1, &II, VRBaseMap, /*IsDebug=*/false,
IsClone, IsCloned);
}
- MBB->insert(InsertPos, MI);
+ MBB->insert(InsertPos, MIB);
SDValue Op(Node, 0);
bool isNew = VRBaseMap.insert(std::make_pair(Op, NewVReg)).second;
(void)isNew; // Silence compiler warning.
if (SD->getKind() == SDDbgValue::FRAMEIX) {
// Stack address; this needs to be lowered in target-dependent fashion.
// EmitTargetCodeForFrameDebugValue is responsible for allocation.
- unsigned FrameIx = SD->getFrameIx();
- return TII->emitFrameIndexDebugValue(*MF, FrameIx, Offset, MDPtr, DL);
+ return BuildMI(*MF, DL, TII->get(TargetOpcode::DBG_VALUE))
+ .addFrameIndex(SD->getFrameIx()).addImm(Offset).addMetadata(MDPtr);
}
// Otherwise, we're going to create an instruction here.
const MCInstrDesc &II = TII->get(TargetOpcode::DBG_VALUE);
if (I==VRBaseMap.end())
MIB.addReg(0U); // undef
else
- AddOperand(&*MIB, Op, (*MIB).getNumOperands(), &II, VRBaseMap,
+ AddOperand(MIB, Op, (*MIB).getNumOperands(), &II, VRBaseMap,
/*IsDebug=*/true, /*IsClone=*/false, /*IsCloned=*/false);
} else if (SD->getKind() == SDDbgValue::CONST) {
const Value *V = SD->getConst();
MIB.addReg(0U);
}
- MIB.addImm(Offset).addMetadata(MDPtr);
+ if (Offset != 0) // Indirect addressing.
+ MIB.addImm(Offset);
+ else
+ MIB.addReg(0U, RegState::Debug);
+
+ MIB.addMetadata(MDPtr);
+
return &*MIB;
}
const MCInstrDesc &II = TII->get(Opc);
unsigned NumResults = CountResults(Node);
- unsigned NodeOperands = CountOperands(Node);
- bool HasPhysRegOuts = NumResults > II.getNumDefs() && II.getImplicitDefs()!=0;
+ unsigned NumDefs = II.getNumDefs();
+ const MCPhysReg *ScratchRegs = nullptr;
+
+ // Handle STACKMAP and PATCHPOINT specially and then use the generic code.
+ if (Opc == TargetOpcode::STACKMAP || Opc == TargetOpcode::PATCHPOINT) {
+ // Stackmaps do not have arguments and do not preserve their calling
+ // convention. However, to simplify runtime support, they clobber the same
+ // scratch registers as AnyRegCC.
+ unsigned CC = CallingConv::AnyReg;
+ if (Opc == TargetOpcode::PATCHPOINT) {
+ CC = Node->getConstantOperandVal(PatchPointOpers::CCPos);
+ NumDefs = NumResults;
+ }
+ ScratchRegs = TLI->getScratchRegisters((CallingConv::ID) CC);
+ }
+
+ unsigned NumImpUses = 0;
+ unsigned NodeOperands =
+ countOperands(Node, II.getNumOperands() - NumDefs, NumImpUses);
+ bool HasPhysRegOuts = NumResults > NumDefs && II.getImplicitDefs()!=nullptr;
#ifndef NDEBUG
unsigned NumMIOperands = NodeOperands + NumResults;
if (II.isVariadic())
"Too few operands for a variadic node!");
else
assert(NumMIOperands >= II.getNumOperands() &&
- NumMIOperands <= II.getNumOperands()+II.getNumImplicitDefs() &&
+ NumMIOperands <= II.getNumOperands() + II.getNumImplicitDefs() +
+ NumImpUses &&
"#operands for dag node doesn't match .td file!");
#endif
// Create the new machine instruction.
- MachineInstr *MI = BuildMI(*MF, Node->getDebugLoc(), II);
-
- // The MachineInstr constructor adds implicit-def operands. Scan through
- // these to determine which are dead.
- if (MI->getNumOperands() != 0 &&
- Node->getValueType(Node->getNumValues()-1) == MVT::Glue) {
- // First, collect all used registers.
- SmallVector<unsigned, 8> UsedRegs;
- for (SDNode *F = Node->getGluedUser(); F; F = F->getGluedUser())
- if (F->getOpcode() == ISD::CopyFromReg)
- UsedRegs.push_back(cast<RegisterSDNode>(F->getOperand(1))->getReg());
- else {
- // Collect declared implicit uses.
- const MCInstrDesc &MCID = TII->get(F->getMachineOpcode());
- UsedRegs.append(MCID.getImplicitUses(),
- MCID.getImplicitUses() + MCID.getNumImplicitUses());
- // In addition to declared implicit uses, we must also check for
- // direct RegisterSDNode operands.
- for (unsigned i = 0, e = F->getNumOperands(); i != e; ++i)
- if (RegisterSDNode *R = dyn_cast<RegisterSDNode>(F->getOperand(i))) {
- unsigned Reg = R->getReg();
- if (TargetRegisterInfo::isPhysicalRegister(Reg))
- UsedRegs.push_back(Reg);
- }
- }
- // Then mark unused registers as dead.
- MI->setPhysRegsDeadExcept(UsedRegs, *TRI);
- }
+ MachineInstrBuilder MIB = BuildMI(*MF, Node->getDebugLoc(), II);
// Add result register values for things that are defined by this
// instruction.
if (NumResults)
- CreateVirtualRegisters(Node, MI, II, IsClone, IsCloned, VRBaseMap);
+ CreateVirtualRegisters(Node, MIB, II, IsClone, IsCloned, VRBaseMap);
// Emit all of the actual operands of this instruction, adding them to the
// instruction as appropriate.
- bool HasOptPRefs = II.getNumDefs() > NumResults;
+ bool HasOptPRefs = NumDefs > NumResults;
assert((!HasOptPRefs || !HasPhysRegOuts) &&
"Unable to cope with optional defs and phys regs defs!");
- unsigned NumSkip = HasOptPRefs ? II.getNumDefs() - NumResults : 0;
+ unsigned NumSkip = HasOptPRefs ? NumDefs - NumResults : 0;
for (unsigned i = NumSkip; i != NodeOperands; ++i)
- AddOperand(MI, Node->getOperand(i), i-NumSkip+II.getNumDefs(), &II,
+ AddOperand(MIB, Node->getOperand(i), i-NumSkip+NumDefs, &II,
VRBaseMap, /*IsDebug=*/false, IsClone, IsCloned);
+ // Add scratch registers as implicit def and early clobber
+ if (ScratchRegs)
+ for (unsigned i = 0; ScratchRegs[i]; ++i)
+ MIB.addReg(ScratchRegs[i], RegState::ImplicitDefine |
+ RegState::EarlyClobber);
+
// Transfer all of the memory reference descriptions of this instruction.
- MI->setMemRefs(cast<MachineSDNode>(Node)->memoperands_begin(),
+ MIB.setMemRefs(cast<MachineSDNode>(Node)->memoperands_begin(),
cast<MachineSDNode>(Node)->memoperands_end());
// Insert the instruction into position in the block. This needs to
// happen before any custom inserter hook is called so that the
// hook knows where in the block to insert the replacement code.
- MBB->insert(InsertPos, MI);
+ MBB->insert(InsertPos, MIB);
+
+ // The MachineInstr may also define physregs instead of virtregs. These
+ // physreg values can reach other instructions in different ways:
+ //
+ // 1. When there is a use of a Node value beyond the explicitly defined
+ // virtual registers, we emit a CopyFromReg for one of the implicitly
+ // defined physregs. This only happens when HasPhysRegOuts is true.
+ //
+ // 2. A CopyFromReg reading a physreg may be glued to this instruction.
+ //
+ // 3. A glued instruction may implicitly use a physreg.
+ //
+ // 4. A glued instruction may use a RegisterSDNode operand.
+ //
+ // Collect all the used physreg defs, and make sure that any unused physreg
+ // defs are marked as dead.
+ SmallVector<unsigned, 8> UsedRegs;
// Additional results must be physical register defs.
if (HasPhysRegOuts) {
- for (unsigned i = II.getNumDefs(); i < NumResults; ++i) {
- unsigned Reg = II.getImplicitDefs()[i - II.getNumDefs()];
- if (Node->hasAnyUseOfValue(i))
- EmitCopyFromReg(Node, i, IsClone, IsCloned, Reg, VRBaseMap);
- // If there are no uses, mark the register as dead now, so that
- // MachineLICM/Sink can see that it's dead. Don't do this if the
- // node has a Glue value, for the benefit of targets still using
- // Glue for values in physregs.
- else if (Node->getValueType(Node->getNumValues()-1) != MVT::Glue)
- MI->addRegisterDead(Reg, TRI);
+ for (unsigned i = NumDefs; i < NumResults; ++i) {
+ unsigned Reg = II.getImplicitDefs()[i - NumDefs];
+ if (!Node->hasAnyUseOfValue(i))
+ continue;
+ // This implicitly defined physreg has a use.
+ UsedRegs.push_back(Reg);
+ EmitCopyFromReg(Node, i, IsClone, IsCloned, Reg, VRBaseMap);
}
}
- // If the instruction has implicit defs and the node doesn't, mark the
- // implicit def as dead. If the node has any glue outputs, we don't do this
- // because we don't know what implicit defs are being used by glued nodes.
- if (Node->getValueType(Node->getNumValues()-1) != MVT::Glue)
- if (const unsigned *IDList = II.getImplicitDefs()) {
- for (unsigned i = NumResults, e = II.getNumDefs()+II.getNumImplicitDefs();
- i != e; ++i)
- MI->addRegisterDead(IDList[i-II.getNumDefs()], TRI);
+ // Scan the glue chain for any used physregs.
+ if (Node->getValueType(Node->getNumValues()-1) == MVT::Glue) {
+ for (SDNode *F = Node->getGluedUser(); F; F = F->getGluedUser()) {
+ if (F->getOpcode() == ISD::CopyFromReg) {
+ UsedRegs.push_back(cast<RegisterSDNode>(F->getOperand(1))->getReg());
+ continue;
+ } else if (F->getOpcode() == ISD::CopyToReg) {
+ // Skip CopyToReg nodes that are internal to the glue chain.
+ continue;
+ }
+ // Collect declared implicit uses.
+ const MCInstrDesc &MCID = TII->get(F->getMachineOpcode());
+ UsedRegs.append(MCID.getImplicitUses(),
+ MCID.getImplicitUses() + MCID.getNumImplicitUses());
+ // In addition to declared implicit uses, we must also check for
+ // direct RegisterSDNode operands.
+ for (unsigned i = 0, e = F->getNumOperands(); i != e; ++i)
+ if (RegisterSDNode *R = dyn_cast<RegisterSDNode>(F->getOperand(i))) {
+ unsigned Reg = R->getReg();
+ if (TargetRegisterInfo::isPhysicalRegister(Reg))
+ UsedRegs.push_back(Reg);
+ }
}
+ }
+
+ // Finally mark unused registers as dead.
+ if (!UsedRegs.empty() || II.getImplicitDefs())
+ MIB->setPhysRegsDeadExcept(UsedRegs, *TRI);
// Run post-isel target hook to adjust this instruction if needed.
#ifdef NDEBUG
if (II.hasPostISelHook())
#endif
- TLI->AdjustInstrPostInstrSelection(MI, Node);
+ TLI->AdjustInstrPostInstrSelection(MIB, Node);
}
/// EmitSpecialNode - Generate machine code for a target-independent node and
Node->dump();
#endif
llvm_unreachable("This target-independent node should have been selected!");
- break;
case ISD::EntryToken:
llvm_unreachable("EntryToken should have been excluded from the schedule!");
- break;
case ISD::MERGE_VALUES:
case ISD::TokenFactor: // fall thru
break;
break;
}
+ case ISD::LIFETIME_START:
+ case ISD::LIFETIME_END: {
+ unsigned TarOp = (Node->getOpcode() == ISD::LIFETIME_START) ?
+ TargetOpcode::LIFETIME_START : TargetOpcode::LIFETIME_END;
+
+ FrameIndexSDNode *FI = dyn_cast<FrameIndexSDNode>(Node->getOperand(1));
+ BuildMI(*MBB, InsertPos, Node->getDebugLoc(), TII->get(TarOp))
+ .addFrameIndex(FI->getIndex());
+ break;
+ }
+
case ISD::INLINEASM: {
unsigned NumOps = Node->getNumOperands();
if (Node->getOperand(NumOps-1).getValueType() == MVT::Glue)
--NumOps; // Ignore the glue operand.
// Create the inline asm machine instruction.
- MachineInstr *MI = BuildMI(*MF, Node->getDebugLoc(),
- TII->get(TargetOpcode::INLINEASM));
+ MachineInstrBuilder MIB = BuildMI(*MF, Node->getDebugLoc(),
+ TII->get(TargetOpcode::INLINEASM));
// Add the asm string as an external symbol operand.
SDValue AsmStrV = Node->getOperand(InlineAsm::Op_AsmString);
const char *AsmStr = cast<ExternalSymbolSDNode>(AsmStrV)->getSymbol();
- MI->addOperand(MachineOperand::CreateES(AsmStr));
+ MIB.addExternalSymbol(AsmStr);
- // Add the HasSideEffect and isAlignStack bits.
+ // Add the HasSideEffect, isAlignStack, AsmDialect, MayLoad and MayStore
+ // bits.
int64_t ExtraInfo =
cast<ConstantSDNode>(Node->getOperand(InlineAsm::Op_ExtraInfo))->
getZExtValue();
- MI->addOperand(MachineOperand::CreateImm(ExtraInfo));
+ MIB.addImm(ExtraInfo);
+
+ // Remember to operand index of the group flags.
+ SmallVector<unsigned, 8> GroupIdx;
// Add all of the operand registers to the instruction.
for (unsigned i = InlineAsm::Op_FirstOperand; i != NumOps;) {
unsigned Flags =
cast<ConstantSDNode>(Node->getOperand(i))->getZExtValue();
- unsigned NumVals = InlineAsm::getNumOperandRegisters(Flags);
+ const unsigned NumVals = InlineAsm::getNumOperandRegisters(Flags);
- MI->addOperand(MachineOperand::CreateImm(Flags));
+ GroupIdx.push_back(MIB->getNumOperands());
+ MIB.addImm(Flags);
++i; // Skip the ID value.
switch (InlineAsm::getKind(Flags)) {
default: llvm_unreachable("Bad flags!");
case InlineAsm::Kind_RegDef:
- for (; NumVals; --NumVals, ++i) {
+ for (unsigned j = 0; j != NumVals; ++j, ++i) {
unsigned Reg = cast<RegisterSDNode>(Node->getOperand(i))->getReg();
// FIXME: Add dead flags for physical and virtual registers defined.
// For now, mark physical register defs as implicit to help fast
// regalloc. This makes inline asm look a lot like calls.
- MI->addOperand(MachineOperand::CreateReg(Reg, true,
- /*isImp=*/ TargetRegisterInfo::isPhysicalRegister(Reg)));
+ MIB.addReg(Reg, RegState::Define |
+ getImplRegState(TargetRegisterInfo::isPhysicalRegister(Reg)));
}
break;
case InlineAsm::Kind_RegDefEarlyClobber:
case InlineAsm::Kind_Clobber:
- for (; NumVals; --NumVals, ++i) {
+ for (unsigned j = 0; j != NumVals; ++j, ++i) {
unsigned Reg = cast<RegisterSDNode>(Node->getOperand(i))->getReg();
- MI->addOperand(MachineOperand::CreateReg(Reg, /*isDef=*/ true,
- /*isImp=*/ TargetRegisterInfo::isPhysicalRegister(Reg),
- /*isKill=*/ false,
- /*isDead=*/ false,
- /*isUndef=*/false,
- /*isEarlyClobber=*/ true));
+ MIB.addReg(Reg, RegState::Define | RegState::EarlyClobber |
+ getImplRegState(TargetRegisterInfo::isPhysicalRegister(Reg)));
}
break;
case InlineAsm::Kind_RegUse: // Use of register.
case InlineAsm::Kind_Mem: // Addressing mode.
// The addressing mode has been selected, just add all of the
// operands to the machine instruction.
- for (; NumVals; --NumVals, ++i)
- AddOperand(MI, Node->getOperand(i), 0, 0, VRBaseMap,
+ for (unsigned j = 0; j != NumVals; ++j, ++i)
+ AddOperand(MIB, Node->getOperand(i), 0, nullptr, VRBaseMap,
/*IsDebug=*/false, IsClone, IsCloned);
+
+ // Manually set isTied bits.
+ if (InlineAsm::getKind(Flags) == InlineAsm::Kind_RegUse) {
+ unsigned DefGroup = 0;
+ if (InlineAsm::isUseOperandTiedToDef(Flags, DefGroup)) {
+ unsigned DefIdx = GroupIdx[DefGroup] + 1;
+ unsigned UseIdx = GroupIdx.back() + 1;
+ for (unsigned j = 0; j != NumVals; ++j)
+ MIB->tieOperands(DefIdx + j, UseIdx + j);
+ }
+ }
break;
}
}
SDValue MDV = Node->getOperand(InlineAsm::Op_MDNode);
const MDNode *MD = cast<MDNodeSDNode>(MDV)->getMD();
if (MD)
- MI->addOperand(MachineOperand::CreateMetadata(MD));
+ MIB.addMetadata(MD);
- MBB->insert(InsertPos, MI);
+ MBB->insert(InsertPos, MIB);
break;
}
}