index e107276359b681595045f4ac93cf3ab03d8f6d58..c134454e0d03812cccd4627030d05850f577ba83 100644 (file)
//
//===----------------------------------------------------------------------===//
-#define DEBUG_TYPE "instr-emitter"
#include "InstrEmitter.h"
#include "SDNodeDbgValue.h"
#include "llvm/ADT/Statistic.h"
#include "llvm/CodeGen/MachineFunction.h"
#include "llvm/CodeGen/MachineInstrBuilder.h"
#include "llvm/CodeGen/MachineRegisterInfo.h"
+#include "llvm/CodeGen/StackMaps.h"
#include "llvm/IR/DataLayout.h"
#include "llvm/Support/Debug.h"
#include "llvm/Support/ErrorHandling.h"
#include "llvm/Target/TargetMachine.h"
using namespace llvm;
+#define DEBUG_TYPE "instr-emitter"
+
/// MinRCSize - Smallest register class we allow when constraining virtual
/// registers. If satisfying all register class constraints would require
/// using a smaller register class, emit a COPY to a new virtual register
// If the node is only used by a CopyToReg and the dest reg is a vreg, use
// the CopyToReg'd destination register instead of creating a new vreg.
bool MatchReg = true;
- const TargetRegisterClass *UseRC = NULL;
+ const TargetRegisterClass *UseRC = nullptr;
MVT VT = Node->getSimpleValueType(ResNo);
// Stick to the preferred register classes for legal types.
UseRC = TLI->getRegClassFor(VT);
if (!IsClone && !IsCloned)
- for (SDNode::use_iterator UI = Node->use_begin(), E = Node->use_end();
- UI != E; ++UI) {
- SDNode *User = *UI;
+ for (SDNode *User : Node->uses()) {
bool Match = true;
if (User->getOpcode() == ISD::CopyToReg &&
User->getOperand(2).getNode() == Node &&
Match = false;
if (User->isMachineOpcode()) {
const MCInstrDesc &II = TII->get(User->getMachineOpcode());
- const TargetRegisterClass *RC = 0;
+ const TargetRegisterClass *RC = nullptr;
if (i+II.getNumDefs() < II.getNumOperands()) {
RC = TRI->getAllocatableClass(
TII->getRegClass(II, i+II.getNumDefs(), TRI, *MF));
break;
}
- const TargetRegisterClass *SrcRC = 0, *DstRC = 0;
+ const TargetRegisterClass *SrcRC = nullptr, *DstRC = nullptr;
SrcRC = TRI->getMinimalPhysRegClass(SrcReg, VT);
// Figure out the register class to create for the destreg.
assert(Node->getMachineOpcode() != TargetOpcode::IMPLICIT_DEF &&
"IMPLICIT_DEF should have been handled as a special case elsewhere!");
+ unsigned NumResults = CountResults(Node);
for (unsigned i = 0; i < II.getNumDefs(); ++i) {
// If the specific node value is only used by a CopyToReg and the dest reg
// is a vreg in the same register class, use the CopyToReg'd destination
unsigned VRBase = 0;
const TargetRegisterClass *RC =
TRI->getAllocatableClass(TII->getRegClass(II, i, TRI, *MF));
+ // Always let the value type influence the used register class. The
+ // constraints on the instruction may be too lax to represent the value
+ // type correctly. For example, a 64-bit float (X86::FR64) can't live in
+ // the 32-bit float super-class (X86::FR32).
+ if (i < NumResults && TLI->isTypeLegal(Node->getSimpleValueType(i))) {
+ const TargetRegisterClass *VTRC =
+ TLI->getRegClassFor(Node->getSimpleValueType(i));
+ if (RC)
+ VTRC = TRI->getCommonSubClass(RC, VTRC);
+ if (VTRC)
+ RC = VTRC;
+ }
+
if (II.OpInfo[i].isOptionalDef()) {
// Optional def must be a physical register.
unsigned NumResults = CountResults(Node);
}
if (!VRBase && !IsClone && !IsCloned)
- for (SDNode::use_iterator UI = Node->use_begin(), E = Node->use_end();
- UI != E; ++UI) {
- SDNode *User = *UI;
+ for (SDNode *User : Node->uses()) {
if (User->getOpcode() == ISD::CopyToReg &&
User->getOperand(2).getNode() == Node &&
User->getOperand(2).getResNo() == i) {
// shrink VReg's register class within reason. For example, if VReg == GR32
// and II requires a GR32_NOSP, just constrain VReg to GR32_NOSP.
if (II) {
- const TargetRegisterClass *DstRC = 0;
+ const TargetRegisterClass *DstRC = nullptr;
if (IIOpNum < II->getNumOperands())
DstRC = TRI->getAllocatableClass(TII->getRegClass(*II,IIOpNum,TRI,*MF));
if (DstRC && !MRI->constrainRegClass(VReg, DstRC, MinRCSize)) {
// If the node is only used by a CopyToReg and the dest reg is a vreg, use
// the CopyToReg'd destination register instead of creating a new vreg.
- for (SDNode::use_iterator UI = Node->use_begin(), E = Node->use_end();
- UI != E; ++UI) {
- SDNode *User = *UI;
+ for (SDNode *User : Node->uses()) {
if (User->getOpcode() == ISD::CopyToReg &&
User->getOperand(2).getNode() == Node) {
unsigned DestReg = cast<RegisterSDNode>(User->getOperand(1))->getReg();
const ConstantSDNode *SD = cast<ConstantSDNode>(N0);
MIB.addImm(SD->getZExtValue());
} else
- AddOperand(MIB, N0, 0, 0, VRBaseMap, /*IsDebug=*/false,
+ AddOperand(MIB, N0, 0, nullptr, VRBaseMap, /*IsDebug=*/false,
IsClone, IsCloned);
// Add the subregster being inserted
- AddOperand(MIB, N1, 0, 0, VRBaseMap, /*IsDebug=*/false,
+ AddOperand(MIB, N1, 0, nullptr, VRBaseMap, /*IsDebug=*/false,
IsClone, IsCloned);
MIB.addImm(SubIdx);
MBB->insert(InsertPos, MIB);
const MCInstrDesc &II = TII->get(Opc);
unsigned NumResults = CountResults(Node);
+ unsigned NumDefs = II.getNumDefs();
+ const MCPhysReg *ScratchRegs = nullptr;
+
+ // Handle STACKMAP and PATCHPOINT specially and then use the generic code.
+ if (Opc == TargetOpcode::STACKMAP || Opc == TargetOpcode::PATCHPOINT) {
+ // Stackmaps do not have arguments and do not preserve their calling
+ // convention. However, to simplify runtime support, they clobber the same
+ // scratch registers as AnyRegCC.
+ unsigned CC = CallingConv::AnyReg;
+ if (Opc == TargetOpcode::PATCHPOINT) {
+ CC = Node->getConstantOperandVal(PatchPointOpers::CCPos);
+ NumDefs = NumResults;
+ }
+ ScratchRegs = TLI->getScratchRegisters((CallingConv::ID) CC);
+ }
+
unsigned NumImpUses = 0;
unsigned NodeOperands =
- countOperands(Node, II.getNumOperands() - II.getNumDefs(), NumImpUses);
- bool HasPhysRegOuts = NumResults > II.getNumDefs() && II.getImplicitDefs()!=0;
+ countOperands(Node, II.getNumOperands() - NumDefs, NumImpUses);
+ bool HasPhysRegOuts = NumResults > NumDefs && II.getImplicitDefs()!=nullptr;
#ifndef NDEBUG
unsigned NumMIOperands = NodeOperands + NumResults;
if (II.isVariadic())
// Emit all of the actual operands of this instruction, adding them to the
// instruction as appropriate.
- bool HasOptPRefs = II.getNumDefs() > NumResults;
+ bool HasOptPRefs = NumDefs > NumResults;
assert((!HasOptPRefs || !HasPhysRegOuts) &&
"Unable to cope with optional defs and phys regs defs!");
- unsigned NumSkip = HasOptPRefs ? II.getNumDefs() - NumResults : 0;
+ unsigned NumSkip = HasOptPRefs ? NumDefs - NumResults : 0;
for (unsigned i = NumSkip; i != NodeOperands; ++i)
- AddOperand(MIB, Node->getOperand(i), i-NumSkip+II.getNumDefs(), &II,
+ AddOperand(MIB, Node->getOperand(i), i-NumSkip+NumDefs, &II,
VRBaseMap, /*IsDebug=*/false, IsClone, IsCloned);
+ // Add scratch registers as implicit def and early clobber
+ if (ScratchRegs)
+ for (unsigned i = 0; ScratchRegs[i]; ++i)
+ MIB.addReg(ScratchRegs[i], RegState::ImplicitDefine |
+ RegState::EarlyClobber);
+
// Transfer all of the memory reference descriptions of this instruction.
MIB.setMemRefs(cast<MachineSDNode>(Node)->memoperands_begin(),
cast<MachineSDNode>(Node)->memoperands_end());
// Additional results must be physical register defs.
if (HasPhysRegOuts) {
- for (unsigned i = II.getNumDefs(); i < NumResults; ++i) {
- unsigned Reg = II.getImplicitDefs()[i - II.getNumDefs()];
+ for (unsigned i = NumDefs; i < NumResults; ++i) {
+ unsigned Reg = II.getImplicitDefs()[i - NumDefs];
if (!Node->hasAnyUseOfValue(i))
continue;
// This implicitly defined physreg has a use.
// The addressing mode has been selected, just add all of the
// operands to the machine instruction.
for (unsigned j = 0; j != NumVals; ++j, ++i)
- AddOperand(MIB, Node->getOperand(i), 0, 0, VRBaseMap,
+ AddOperand(MIB, Node->getOperand(i), 0, nullptr, VRBaseMap,
/*IsDebug=*/false, IsClone, IsCloned);
// Manually set isTied bits.