diff --git a/lib/CodeGen/SelectionDAG/SelectionDAGBuilder.h b/lib/CodeGen/SelectionDAG/SelectionDAGBuilder.h
index 66835bf55752f1d7bb49e442f4892171a920c66c..a04108d56adf691e23865242a5235c530dd09e47 100644 (file)
DebugLoc dl;
unsigned SDNodeOrder;
public:
- DanglingDebugInfo() : DI(0), dl(DebugLoc()), SDNodeOrder(0) { }
+ DanglingDebugInfo() : DI(nullptr), dl(DebugLoc()), SDNodeOrder(0) { }
DanglingDebugInfo(const DbgValueInst *di, DebugLoc DL, unsigned SDNO) :
DI(di), dl(DL), SDNodeOrder(SDNO) { }
const DbgValueInst* getDI() { return DI; }
MachineBasicBlock* BB;
uint32_t ExtraWeight;
- Case() : Low(0), High(0), BB(0), ExtraWeight(0) { }
+ Case() : Low(nullptr), High(nullptr), BB(nullptr), ExtraWeight(0) { }
Case(const Constant *low, const Constant *high, MachineBasicBlock *bb,
uint32_t extraweight) : Low(low), High(high), BB(bb),
ExtraWeight(extraweight) { }
/// the same function, use the same failure basic block).
class StackProtectorDescriptor {
public:
- StackProtectorDescriptor() : ParentMBB(0), SuccessMBB(0), FailureMBB(0),
- Guard(0) { }
+ StackProtectorDescriptor() : ParentMBB(nullptr), SuccessMBB(nullptr),
+ FailureMBB(nullptr), Guard(nullptr) { }
~StackProtectorDescriptor() { }
/// Returns true if all fields of the stack protector descriptor are
/// parent mbb after we create the stack protector check (SuccessMBB). This
/// BB is visited only on stack protector check success.
void resetPerBBState() {
- ParentMBB = 0;
- SuccessMBB = 0;
+ ParentMBB = nullptr;
+ SuccessMBB = nullptr;
}
/// Reset state that only changes when we switch functions.
/// 2.The guard variable since the guard variable we are checking against is
/// always the same.
void resetPerFunctionState() {
- FailureMBB = 0;
- Guard = 0;
+ FailureMBB = nullptr;
+ Guard = nullptr;
}
MachineBasicBlock *getParentMBB() { return ParentMBB; }
/// block will be created.
MachineBasicBlock *AddSuccessorMBB(const BasicBlock *BB,
MachineBasicBlock *ParentMBB,
- MachineBasicBlock *SuccMBB = 0);
+ MachineBasicBlock *SuccMBB = nullptr);
};
private:
SelectionDAGBuilder(SelectionDAG &dag, FunctionLoweringInfo &funcinfo,
CodeGenOpt::Level ol)
- : CurInst(NULL), SDNodeOrder(LowestSDNodeOrder), TM(dag.getTarget()),
+ : CurInst(nullptr), SDNodeOrder(LowestSDNodeOrder), TM(dag.getTarget()),
DAG(dag), FuncInfo(funcinfo), OptLevel(ol),
HasTailCall(false) {
}
void setValue(const Value *V, SDValue NewN) {
SDValue &N = NodeMap[V];
- assert(N.getNode() == 0 && "Already set a value for this node!");
+ assert(!N.getNode() && "Already set a value for this node!");
N = NewN;
}
void setUnusedArgValue(const Value *V, SDValue NewN) {
SDValue &N = UnusedArgNodeMap[V];
- assert(N.getNode() == 0 && "Already set a value for this node!");
+ assert(!N.getNode() && "Already set a value for this node!");
N = NewN;
}
void CopyToExportRegsIfNeeded(const Value *V);
void ExportFromCurrentBlock(const Value *V);
void LowerCallTo(ImmutableCallSite CS, SDValue Callee, bool IsTailCall,
- MachineBasicBlock *LandingPad = NULL);
+ MachineBasicBlock *LandingPad = nullptr);
std::pair<SDValue, SDValue> LowerCallOperands(const CallInst &CI,
unsigned ArgIdx,
void visitBr(const BranchInst &I);
void visitSwitch(const SwitchInst &I);
void visitIndirectBr(const IndirectBrInst &I);
- void visitUnreachable(const UnreachableInst &I) { /* noop */ }
+ void visitUnreachable(const UnreachableInst &I);
// Helpers for visitSwitch
bool handleSmallSwitchRange(CaseRec& CR,